]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AsmPrinter/DwarfAccelTable.h
Remove unnecessary test for Darwin and update testcase to be a little less
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfAccelTable.h
1 //==-- llvm/CodeGen/DwarfAccelTable.h - Dwarf Accelerator Tables -*- C++ -*-==//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf accelerator tables.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFACCELTABLE_H__
15 #define CODEGEN_ASMPRINTER_DWARFACCELTABLE_H__
17 #include "DIE.h"
18 #include "llvm/ADT/ArrayRef.h"
19 #include "llvm/ADT/StringMap.h"
20 #include "llvm/MC/MCSymbol.h"
21 #include "llvm/Support/DataTypes.h"
22 #include "llvm/Support/Debug.h"
23 #include "llvm/Support/Dwarf.h"
24 #include "llvm/Support/ErrorHandling.h"
25 #include "llvm/Support/Format.h"
26 #include "llvm/Support/FormattedStream.h"
27 #include <map>
28 #include <vector>
30 // The dwarf accelerator tables are an indirect hash table optimized
31 // for null lookup rather than access to known data. They are output into
32 // an on-disk format that looks like this:
33 //
34 // .-------------.
35 // |  HEADER     |
36 // |-------------|
37 // |  BUCKETS    |
38 // |-------------|
39 // |  HASHES     |
40 // |-------------|
41 // |  OFFSETS    |
42 // |-------------|
43 // |  DATA       |
44 // `-------------'
45 //
46 // where the header contains a magic number, version, type of hash function,
47 // the number of buckets, total number of hashes, and room for a special
48 // struct of data and the length of that struct.
49 //
50 // The buckets contain an index (e.g. 6) into the hashes array. The hashes
51 // section contains all of the 32-bit hash values in contiguous memory, and
52 // the offsets contain the offset into the data area for the particular
53 // hash.
54 //
55 // For a lookup example, we could hash a function name and take it modulo the
56 // number of buckets giving us our bucket. From there we take the bucket value
57 // as an index into the hashes table and look at each successive hash as long
58 // as the hash value is still the same modulo result (bucket value) as earlier.
59 // If we have a match we look at that same entry in the offsets table and
60 // grab the offset in the data for our final match.
62 namespace llvm {
64 class AsmPrinter;
65 class DIE;
66 class DwarfFile;
68 class DwarfAccelTable {
70   static uint32_t HashDJB(StringRef Str) {
71     uint32_t h = 5381;
72     for (unsigned i = 0, e = Str.size(); i != e; ++i)
73       h = ((h << 5) + h) + Str[i];
74     return h;
75   }
77   // Helper function to compute the number of buckets needed based on
78   // the number of unique hashes.
79   void ComputeBucketCount(void);
81   struct TableHeader {
82     uint32_t magic;           // 'HASH' magic value to allow endian detection
83     uint16_t version;         // Version number.
84     uint16_t hash_function;   // The hash function enumeration that was used.
85     uint32_t bucket_count;    // The number of buckets in this hash table.
86     uint32_t hashes_count;    // The total number of unique hash values
87                               // and hash data offsets in this table.
88     uint32_t header_data_len; // The bytes to skip to get to the hash
89                               // indexes (buckets) for correct alignment.
90     // Also written to disk is the implementation specific header data.
92     static const uint32_t MagicHash = 0x48415348;
94     TableHeader(uint32_t data_len)
95         : magic(MagicHash), version(1),
96           hash_function(dwarf::DW_hash_function_djb), bucket_count(0),
97           hashes_count(0), header_data_len(data_len) {}
99 #ifndef NDEBUG
100     void print(raw_ostream &O) {
101       O << "Magic: " << format("0x%x", magic) << "\n"
102         << "Version: " << version << "\n"
103         << "Hash Function: " << hash_function << "\n"
104         << "Bucket Count: " << bucket_count << "\n"
105         << "Header Data Length: " << header_data_len << "\n";
106     }
107     void dump() { print(dbgs()); }
108 #endif
109   };
111 public:
112   // The HeaderData describes the form of each set of data. In general this
113   // is as a list of atoms (atom_count) where each atom contains a type
114   // (AtomType type) of data, and an encoding form (form). In the case of
115   // data that is referenced via DW_FORM_ref_* the die_offset_base is
116   // used to describe the offset for all forms in the list of atoms.
117   // This also serves as a public interface of sorts.
118   // When written to disk this will have the form:
119   //
120   // uint32_t die_offset_base
121   // uint32_t atom_count
122   // atom_count Atoms
124   // Make these public so that they can be used as a general interface to
125   // the class.
126   struct Atom {
127     uint16_t type; // enum AtomType
128     uint16_t form; // DWARF DW_FORM_ defines
130     Atom(uint16_t type, uint16_t form) : type(type), form(form) {}
131 #ifndef NDEBUG
132     void print(raw_ostream &O) {
133       O << "Type: " << dwarf::AtomTypeString(type) << "\n"
134         << "Form: " << dwarf::FormEncodingString(form) << "\n";
135     }
136     void dump() { print(dbgs()); }
137 #endif
138   };
140 private:
141   struct TableHeaderData {
142     uint32_t die_offset_base;
143     SmallVector<Atom, 1> Atoms;
145     TableHeaderData(ArrayRef<Atom> AtomList, uint32_t offset = 0)
146         : die_offset_base(offset), Atoms(AtomList.begin(), AtomList.end()) {}
148 #ifndef NDEBUG
149     void print(raw_ostream &O) {
150       O << "die_offset_base: " << die_offset_base << "\n";
151       for (size_t i = 0; i < Atoms.size(); i++)
152         Atoms[i].print(O);
153     }
154     void dump() { print(dbgs()); }
155 #endif
156   };
158   // The data itself consists of a str_offset, a count of the DIEs in the
159   // hash and the offsets to the DIEs themselves.
160   // On disk each data section is ended with a 0 KeyType as the end of the
161   // hash chain.
162   // On output this looks like:
163   // uint32_t str_offset
164   // uint32_t hash_data_count
165   // HashData[hash_data_count]
166 public:
167   struct HashDataContents {
168     const DIE *Die;   // Offsets
169     char Flags; // Specific flags to output
171     HashDataContents(const DIE *D, char Flags) : Die(D), Flags(Flags) {}
172 #ifndef NDEBUG
173     void print(raw_ostream &O) const {
174       O << "  Offset: " << Die->getOffset() << "\n";
175       O << "  Tag: " << dwarf::TagString(Die->getTag()) << "\n";
176       O << "  Flags: " << Flags << "\n";
177     }
178 #endif
179   };
181 private:
182   struct HashData {
183     StringRef Str;
184     uint32_t HashValue;
185     MCSymbol *Sym;
186     ArrayRef<HashDataContents *> Data; // offsets
187     HashData(StringRef S, ArrayRef<HashDataContents *> Data)
188         : Str(S), Data(Data) {
189       HashValue = DwarfAccelTable::HashDJB(S);
190     }
191 #ifndef NDEBUG
192     void print(raw_ostream &O) {
193       O << "Name: " << Str << "\n";
194       O << "  Hash Value: " << format("0x%x", HashValue) << "\n";
195       O << "  Symbol: ";
196       if (Sym)
197         Sym->print(O);
198       else
199         O << "<none>";
200       O << "\n";
201       for (size_t i = 0; i < Data.size(); i++) {
202         O << "  Offset: " << Data[i]->Die->getOffset() << "\n";
203         O << "  Tag: " << dwarf::TagString(Data[i]->Die->getTag()) << "\n";
204         O << "  Flags: " << Data[i]->Flags << "\n";
205       }
206     }
207     void dump() { print(dbgs()); }
208 #endif
209   };
211   DwarfAccelTable(const DwarfAccelTable &) LLVM_DELETED_FUNCTION;
212   void operator=(const DwarfAccelTable &) LLVM_DELETED_FUNCTION;
214   // Internal Functions
215   void EmitHeader(AsmPrinter *);
216   void EmitBuckets(AsmPrinter *);
217   void EmitHashes(AsmPrinter *);
218   void EmitOffsets(AsmPrinter *, MCSymbol *);
219   void EmitData(AsmPrinter *, DwarfFile *D);
221   // Allocator for HashData and HashDataContents.
222   BumpPtrAllocator Allocator;
224   // Output Variables
225   TableHeader Header;
226   TableHeaderData HeaderData;
227   std::vector<HashData *> Data;
229   // String Data
230   typedef std::vector<HashDataContents *> DataArray;
231   typedef StringMap<DataArray, BumpPtrAllocator &> StringEntries;
232   StringEntries Entries;
234   // Buckets/Hashes/Offsets
235   typedef std::vector<HashData *> HashList;
236   typedef std::vector<HashList> BucketList;
237   BucketList Buckets;
238   HashList Hashes;
240   // Public Implementation
241 public:
242   DwarfAccelTable(ArrayRef<DwarfAccelTable::Atom>);
243   ~DwarfAccelTable();
244   void AddName(StringRef, const DIE *, char = 0);
245   void FinalizeTable(AsmPrinter *, StringRef);
246   void Emit(AsmPrinter *, MCSymbol *, DwarfFile *);
247 #ifndef NDEBUG
248   void print(raw_ostream &O);
249   void dump() { print(dbgs()); }
250 #endif
251 };
253 #endif