1 //==-- llvm/CodeGen/DwarfAccelTable.h - Dwarf Accelerator Tables -*- C++ -*-==//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf accelerator tables.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFACCELTABLE_H__
15 #define CODEGEN_ASMPRINTER_DWARFACCELTABLE_H__
17 #include "DIE.h"
18 #include "llvm/ADT/ArrayRef.h"
19 #include "llvm/ADT/StringMap.h"
20 #include "llvm/MC/MCSymbol.h"
21 #include "llvm/Support/Compiler.h"
22 #include "llvm/Support/DataTypes.h"
23 #include "llvm/Support/Debug.h"
24 #include "llvm/Support/Dwarf.h"
25 #include "llvm/Support/ErrorHandling.h"
26 #include "llvm/Support/Format.h"
27 #include "llvm/Support/FormattedStream.h"
28 #include <vector>
30 // The dwarf accelerator tables are an indirect hash table optimized
31 // for null lookup rather than access to known data. They are output into
32 // an on-disk format that looks like this:
33 //
34 // .-------------.
35 // | HEADER |
36 // |-------------|
37 // | BUCKETS |
38 // |-------------|
39 // | HASHES |
40 // |-------------|
41 // | OFFSETS |
42 // |-------------|
43 // | DATA |
44 // `-------------'
45 //
46 // where the header contains a magic number, version, type of hash function,
47 // the number of buckets, total number of hashes, and room for a special
48 // struct of data and the length of that struct.
49 //
50 // The buckets contain an index (e.g. 6) into the hashes array. The hashes
51 // section contains all of the 32-bit hash values in contiguous memory, and
52 // the offsets contain the offset into the data area for the particular
53 // hash.
54 //
55 // For a lookup example, we could hash a function name and take it modulo the
56 // number of buckets giving us our bucket. From there we take the bucket value
57 // as an index into the hashes table and look at each successive hash as long
58 // as the hash value is still the same modulo result (bucket value) as earlier.
59 // If we have a match we look at that same entry in the offsets table and
60 // grab the offset in the data for our final match.
62 namespace llvm {
64 class AsmPrinter;
65 class DwarfFile;
67 class DwarfAccelTable {
69 static uint32_t HashDJB(StringRef Str) {
70 uint32_t h = 5381;
71 for (unsigned i = 0, e = Str.size(); i != e; ++i)
72 h = ((h << 5) + h) + Str[i];
73 return h;
74 }
76 // Helper function to compute the number of buckets needed based on
77 // the number of unique hashes.
78 void ComputeBucketCount(void);
80 struct TableHeader {
81 uint32_t magic; // 'HASH' magic value to allow endian detection
82 uint16_t version; // Version number.
83 uint16_t hash_function; // The hash function enumeration that was used.
84 uint32_t bucket_count; // The number of buckets in this hash table.
85 uint32_t hashes_count; // The total number of unique hash values
86 // and hash data offsets in this table.
87 uint32_t header_data_len; // The bytes to skip to get to the hash
88 // indexes (buckets) for correct alignment.
89 // Also written to disk is the implementation specific header data.
91 static const uint32_t MagicHash = 0x48415348;
93 TableHeader(uint32_t data_len)
94 : magic(MagicHash), version(1),
95 hash_function(dwarf::DW_hash_function_djb), bucket_count(0),
96 hashes_count(0), header_data_len(data_len) {}
98 #ifndef NDEBUG
99 void print(raw_ostream &O) {
100 O << "Magic: " << format("0x%x", magic) << "\n"
101 << "Version: " << version << "\n"
102 << "Hash Function: " << hash_function << "\n"
103 << "Bucket Count: " << bucket_count << "\n"
104 << "Header Data Length: " << header_data_len << "\n";
105 }
106 void dump() { print(dbgs()); }
107 #endif
108 };
110 public:
111 // The HeaderData describes the form of each set of data. In general this
112 // is as a list of atoms (atom_count) where each atom contains a type
113 // (AtomType type) of data, and an encoding form (form). In the case of
114 // data that is referenced via DW_FORM_ref_* the die_offset_base is
115 // used to describe the offset for all forms in the list of atoms.
116 // This also serves as a public interface of sorts.
117 // When written to disk this will have the form:
118 //
119 // uint32_t die_offset_base
120 // uint32_t atom_count
121 // atom_count Atoms
123 // Make these public so that they can be used as a general interface to
124 // the class.
125 struct Atom {
126 uint16_t type; // enum AtomType
127 uint16_t form; // DWARF DW_FORM_ defines
129 LLVM_CONSTEXPR Atom(uint16_t type, uint16_t form)
130 : type(type), form(form) {}
131 #ifndef NDEBUG
132 void print(raw_ostream &O) {
133 O << "Type: " << dwarf::AtomTypeString(type) << "\n"
134 << "Form: " << dwarf::FormEncodingString(form) << "\n";
135 }
136 void dump() { print(dbgs()); }
137 #endif
138 };
140 private:
141 struct TableHeaderData {
142 uint32_t die_offset_base;
143 SmallVector<Atom, 1> Atoms;
145 TableHeaderData(ArrayRef<Atom> AtomList, uint32_t offset = 0)
146 : die_offset_base(offset), Atoms(AtomList.begin(), AtomList.end()) {}
148 #ifndef NDEBUG
149 void print(raw_ostream &O) {
150 O << "die_offset_base: " << die_offset_base << "\n";
151 for (size_t i = 0; i < Atoms.size(); i++)
152 Atoms[i].print(O);
153 }
154 void dump() { print(dbgs()); }
155 #endif
156 };
158 // The data itself consists of a str_offset, a count of the DIEs in the
159 // hash and the offsets to the DIEs themselves.
160 // On disk each data section is ended with a 0 KeyType as the end of the
161 // hash chain.
162 // On output this looks like:
163 // uint32_t str_offset
164 // uint32_t hash_data_count
165 // HashData[hash_data_count]
166 public:
167 struct HashDataContents {
168 const DIE *Die; // Offsets
169 char Flags; // Specific flags to output
171 HashDataContents(const DIE *D, char Flags) : Die(D), Flags(Flags) {}
172 #ifndef NDEBUG
173 void print(raw_ostream &O) const {
174 O << " Offset: " << Die->getOffset() << "\n";
175 O << " Tag: " << dwarf::TagString(Die->getTag()) << "\n";
176 O << " Flags: " << Flags << "\n";
177 }
178 #endif
179 };
181 private:
182 // String Data
183 struct DataArray {
184 MCSymbol *StrSym;
185 std::vector<HashDataContents *> Values;
186 DataArray() : StrSym(nullptr) {}
187 };
188 friend struct HashData;
189 struct HashData {
190 StringRef Str;
191 uint32_t HashValue;
192 MCSymbol *Sym;
193 DwarfAccelTable::DataArray &Data; // offsets
194 HashData(StringRef S, DwarfAccelTable::DataArray &Data)
195 : Str(S), Data(Data) {
196 HashValue = DwarfAccelTable::HashDJB(S);
197 }
198 #ifndef NDEBUG
199 void print(raw_ostream &O) {
200 O << "Name: " << Str << "\n";
201 O << " Hash Value: " << format("0x%x", HashValue) << "\n";
202 O << " Symbol: ";
203 if (Sym)
204 Sym->print(O);
205 else
206 O << "<none>";
207 O << "\n";
208 for (HashDataContents *C : Data.Values) {
209 O << " Offset: " << C->Die->getOffset() << "\n";
210 O << " Tag: " << dwarf::TagString(C->Die->getTag()) << "\n";
211 O << " Flags: " << C->Flags << "\n";
212 }
213 }
214 void dump() { print(dbgs()); }
215 #endif
216 };
218 DwarfAccelTable(const DwarfAccelTable &) LLVM_DELETED_FUNCTION;
219 void operator=(const DwarfAccelTable &) LLVM_DELETED_FUNCTION;
221 // Internal Functions
222 void EmitHeader(AsmPrinter *);
223 void EmitBuckets(AsmPrinter *);
224 void EmitHashes(AsmPrinter *);
225 void EmitOffsets(AsmPrinter *, MCSymbol *);
226 void EmitData(AsmPrinter *, DwarfFile *D);
228 // Allocator for HashData and HashDataContents.
229 BumpPtrAllocator Allocator;
231 // Output Variables
232 TableHeader Header;
233 TableHeaderData HeaderData;
234 std::vector<HashData *> Data;
236 typedef StringMap<DataArray, BumpPtrAllocator &> StringEntries;
237 StringEntries Entries;
239 // Buckets/Hashes/Offsets
240 typedef std::vector<HashData *> HashList;
241 typedef std::vector<HashList> BucketList;
242 BucketList Buckets;
243 HashList Hashes;
245 // Public Implementation
246 public:
247 DwarfAccelTable(ArrayRef<DwarfAccelTable::Atom>);
248 void AddName(StringRef Name, MCSymbol *StrSym, const DIE *Die,
249 char Flags = 0);
250 void FinalizeTable(AsmPrinter *, StringRef);
251 void Emit(AsmPrinter *, MCSymbol *, DwarfFile *);
252 #ifndef NDEBUG
253 void print(raw_ostream &O);
254 void dump() { print(dbgs()); }
255 #endif
256 };
257 }
258 #endif