]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AsmPrinter/DwarfCompileUnit.h
remove extra semicolon
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfCompileUnit.h
1 //===-- llvm/CodeGen/DwarfCompileUnit.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
15 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
17 #include "DwarfUnit.h"
18 #include "llvm/Support/Dwarf.h"
19 #include "llvm/ADT/StringRef.h"
20 #include "llvm/IR/DebugInfo.h"
22 namespace llvm {
24 class AsmPrinter;
25 class DIE;
26 class DwarfDebug;
27 class DwarfFile;
28 class MCSymbol;
29 class LexicalScope;
31 class DwarfCompileUnit : public DwarfUnit {
32   /// The attribute index of DW_AT_stmt_list in the compile unit DIE, avoiding
33   /// the need to search for it in applyStmtList.
34   unsigned stmtListIndex;
36   /// Skeleton unit associated with this unit.
37   DwarfCompileUnit *Skeleton;
39   /// A label at the start of the non-dwo section related to this unit.
40   MCSymbol *SectionSym;
42   /// The start of the unit within its section.
43   MCSymbol *LabelBegin;
45   /// GlobalNames - A map of globally visible named entities for this unit.
46   StringMap<const DIE *> GlobalNames;
48   /// GlobalTypes - A map of globally visible types for this unit.
49   StringMap<const DIE *> GlobalTypes;
51   // List of range lists for a given compile unit, separate from the ranges for
52   // the CU itself.
53   SmallVector<RangeSpanList, 1> CURangeLists;
55   // List of ranges for a given compile unit.
56   SmallVector<RangeSpan, 2> CURanges;
58   // The base address of this unit, if any. Used for relative references in
59   // ranges/locs.
60   const MCSymbol *BaseAddress;
62   /// \brief Construct a DIE for the given DbgVariable without initializing the
63   /// DbgVariable's DIE reference.
64   std::unique_ptr<DIE> constructVariableDIEImpl(const DbgVariable &DV,
65                                                 bool Abstract);
67   bool isDwoUnit() const override;
69   bool includeMinimalInlineScopes() const;
71 public:
72   DwarfCompileUnit(unsigned UID, DICompileUnit Node, AsmPrinter *A,
73                    DwarfDebug *DW, DwarfFile *DWU);
75   DwarfCompileUnit *getSkeleton() const {
76     return Skeleton;
77   }
79   void initStmtList(MCSymbol *DwarfLineSectionSym);
81   /// Apply the DW_AT_stmt_list from this compile unit to the specified DIE.
82   void applyStmtList(DIE &D);
84   /// getOrCreateGlobalVariableDIE - get or create global variable DIE.
85   DIE *getOrCreateGlobalVariableDIE(DIGlobalVariable GV);
87   /// addLabelAddress - Add a dwarf label attribute data and value using
88   /// either DW_FORM_addr or DW_FORM_GNU_addr_index.
89   void addLabelAddress(DIE &Die, dwarf::Attribute Attribute,
90                        const MCSymbol *Label);
92   /// addLocalLabelAddress - Add a dwarf label attribute data and value using
93   /// DW_FORM_addr only.
94   void addLocalLabelAddress(DIE &Die, dwarf::Attribute Attribute,
95                             const MCSymbol *Label);
97   /// addSectionDelta - Add a label delta attribute data and value.
98   void addSectionDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
99                        const MCSymbol *Lo);
101   DwarfCompileUnit &getCU() override { return *this; }
103   unsigned getOrCreateSourceID(StringRef FileName, StringRef DirName) override;
105   /// addRange - Add an address range to the list of ranges for this unit.
106   void addRange(RangeSpan Range);
108   void attachLowHighPC(DIE &D, const MCSymbol *Begin, const MCSymbol *End);
110   /// addSectionLabel - Add a Dwarf section label attribute data and value.
111   ///
112   void addSectionLabel(DIE &Die, dwarf::Attribute Attribute,
113                        const MCSymbol *Label, const MCSymbol *Sec);
115   /// \brief Find DIE for the given subprogram and attach appropriate
116   /// DW_AT_low_pc and DW_AT_high_pc attributes. If there are global
117   /// variables in this scope then create and insert DIEs for these
118   /// variables.
119   DIE &updateSubprogramScopeDIE(DISubprogram SP);
121   void constructScopeDIE(LexicalScope *Scope,
122                          SmallVectorImpl<std::unique_ptr<DIE>> &FinalChildren);
124   /// \brief A helper function to construct a RangeSpanList for a given
125   /// lexical scope.
126   void addScopeRangeList(DIE &ScopeDIE, SmallVector<RangeSpan, 2> Range);
128   void attachRangesOrLowHighPC(DIE &D, SmallVector<RangeSpan, 2> Ranges);
130   void attachRangesOrLowHighPC(DIE &D,
131                                const SmallVectorImpl<InsnRange> &Ranges);
132   /// \brief This scope represents inlined body of a function. Construct
133   /// DIE to represent this concrete inlined copy of the function.
134   std::unique_ptr<DIE> constructInlinedScopeDIE(LexicalScope *Scope);
136   /// \brief Construct new DW_TAG_lexical_block for this scope and
137   /// attach DW_AT_low_pc/DW_AT_high_pc labels.
138   std::unique_ptr<DIE> constructLexicalScopeDIE(LexicalScope *Scope);
140   /// constructVariableDIE - Construct a DIE for the given DbgVariable.
141   std::unique_ptr<DIE> constructVariableDIE(DbgVariable &DV,
142                                             bool Abstract = false);
144   std::unique_ptr<DIE> constructVariableDIE(DbgVariable &DV,
145                                             const LexicalScope &Scope,
146                                             DIE *&ObjectPointer);
148   /// A helper function to create children of a Scope DIE.
149   DIE *createScopeChildrenDIE(LexicalScope *Scope,
150                               SmallVectorImpl<std::unique_ptr<DIE>> &Children,
151                               unsigned *ChildScopeCount = nullptr);
153   /// \brief Construct a DIE for this subprogram scope.
154   void constructSubprogramScopeDIE(LexicalScope *Scope);
156   DIE *createAndAddScopeChildren(LexicalScope *Scope, DIE &ScopeDIE);
158   void constructAbstractSubprogramScopeDIE(LexicalScope *Scope);
160   /// \brief Construct import_module DIE.
161   std::unique_ptr<DIE>
162   constructImportedEntityDIE(const DIImportedEntity &Module);
164   void finishSubprogramDefinition(DISubprogram SP);
166   void collectDeadVariables(DISubprogram SP);
168   /// Set the skeleton unit associated with this unit.
169   void setSkeleton(DwarfCompileUnit &Skel) { Skeleton = &Skel; }
171   MCSymbol *getSectionSym() const {
172     assert(Section);
173     return SectionSym;
174   }
176   /// Pass in the SectionSym even though we could recreate it in every compile
177   /// unit (type units will have actually distinct symbols once they're in
178   /// comdat sections).
179   void initSection(const MCSection *Section, MCSymbol *SectionSym) {
180     DwarfUnit::initSection(Section);
181     this->SectionSym = SectionSym;
183     // Don't bother labeling the .dwo unit, as its offset isn't used.
184     if (!Skeleton)
185       LabelBegin =
186           Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
187   }
189   unsigned getLength() {
190     return sizeof(uint32_t) + // Length field
191         getHeaderSize() + UnitDie.getSize();
192   }
194   void emitHeader(const MCSymbol *ASectionSym) const override;
196   MCSymbol *getLabelBegin() const {
197     assert(Section);
198     return LabelBegin;
199   }
201   /// Add a new global name to the compile unit.
202   void addGlobalName(StringRef Name, DIE &Die, DIScope Context) override;
204   /// Add a new global type to the compile unit.
205   void addGlobalType(DIType Ty, const DIE &Die, DIScope Context) override;
207   const StringMap<const DIE *> &getGlobalNames() const { return GlobalNames; }
208   const StringMap<const DIE *> &getGlobalTypes() const { return GlobalTypes; }
210   /// Add DW_AT_location attribute for a DbgVariable based on provided
211   /// MachineLocation.
212   void addVariableAddress(const DbgVariable &DV, DIE &Die,
213                           MachineLocation Location);
214   /// Add an address attribute to a die based on the location provided.
215   void addAddress(DIE &Die, dwarf::Attribute Attribute,
216                   const MachineLocation &Location, bool Indirect = false);
218   /// Start with the address based on the location provided, and generate the
219   /// DWARF information necessary to find the actual variable (navigating the
220   /// extra location information encoded in the type) based on the starting
221   /// location.  Add the DWARF information to the die.
222   void addComplexAddress(const DbgVariable &DV, DIE &Die,
223                          dwarf::Attribute Attribute,
224                          const MachineLocation &Location);
226   /// Add a Dwarf loclistptr attribute data and value.
227   void addLocationList(DIE &Die, dwarf::Attribute Attribute, unsigned Index);
228   void applyVariableAttributes(const DbgVariable &Var, DIE &VariableDie);
230   /// Add a Dwarf expression attribute data and value.
231   void addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr);
233   void applySubprogramAttributesToDefinition(DISubprogram SP, DIE &SPDie);
235   /// getRangeLists - Get the vector of range lists.
236   const SmallVectorImpl<RangeSpanList> &getRangeLists() const {
237     return (Skeleton ? Skeleton : this)->CURangeLists;
238   }
240   /// getRanges - Get the list of ranges for this unit.
241   const SmallVectorImpl<RangeSpan> &getRanges() const { return CURanges; }
242   SmallVector<RangeSpan, 2> takeRanges() { return std::move(CURanges); }
244   void setBaseAddress(const MCSymbol *Base) { BaseAddress = Base; }
245   const MCSymbol *getBaseAddress() const { return BaseAddress; }
246 };
248 } // end llvm namespace
250 #endif