2f6c2546ed4ae38af8b66b0a4dda6b2f579e269d
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.h
1 //===-- llvm/CodeGen/DwarfDebug.h - Dwarf Debug Framework ------*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf debug info into asm files.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFDEBUG_H__
15 #define CODEGEN_ASMPRINTER_DWARFDEBUG_H__
17 #include "AsmPrinterHandler.h"
18 #include "DIE.h"
19 #include "llvm/ADT/DenseMap.h"
20 #include "llvm/ADT/FoldingSet.h"
21 #include "llvm/ADT/MapVector.h"
22 #include "llvm/ADT/SetVector.h"
23 #include "llvm/ADT/SmallPtrSet.h"
24 #include "llvm/ADT/StringMap.h"
25 #include "llvm/CodeGen/LexicalScopes.h"
26 #include "llvm/IR/DebugInfo.h"
27 #include "llvm/IR/DebugLoc.h"
28 #include "llvm/MC/MachineLocation.h"
29 #include "llvm/MC/MCDwarf.h"
30 #include "llvm/Support/Allocator.h"
32 namespace llvm {
34 class AsmPrinter;
35 class ByteStreamer;
36 class DwarfDebug;
37 class DwarfUnit;
38 class DwarfCompileUnit;
39 class ConstantInt;
40 class ConstantFP;
41 class DbgVariable;
42 class MachineFrameInfo;
43 class MachineModuleInfo;
44 class MachineOperand;
45 class MCAsmInfo;
46 class MCObjectFileInfo;
47 class DIEAbbrev;
48 class DIE;
49 class DIELoc;
50 class DIEEntry;
52 //===----------------------------------------------------------------------===//
53 /// \brief This class is used to record source line correspondence.
54 class SrcLineInfo {
55   unsigned Line;     // Source line number.
56   unsigned Column;   // Source column.
57   unsigned SourceID; // Source ID number.
58   MCSymbol *Label;   // Label in code ID number.
59 public:
60   SrcLineInfo(unsigned L, unsigned C, unsigned S, MCSymbol *label)
61       : Line(L), Column(C), SourceID(S), Label(label) {}
63   // Accessors
64   unsigned getLine() const { return Line; }
65   unsigned getColumn() const { return Column; }
66   unsigned getSourceID() const { return SourceID; }
67   MCSymbol *getLabel() const { return Label; }
68 };
70 /// \brief This struct describes location entries emitted in the .debug_loc
71 /// section.
72 class DebugLocEntry {
73   // Begin and end symbols for the address range that this location is valid.
74   const MCSymbol *Begin;
75   const MCSymbol *End;
77   // Type of entry that this represents.
78   enum EntryType { E_Location, E_Integer, E_ConstantFP, E_ConstantInt };
79   enum EntryType EntryKind;
81   union {
82     int64_t Int;
83     const ConstantFP *CFP;
84     const ConstantInt *CIP;
85   } Constants;
87   // The location in the machine frame.
88   MachineLocation Loc;
90   // The variable to which this location entry corresponds.
91   const MDNode *Variable;
93   // Whether this location has been merged.
94   bool Merged;
96 public:
97   DebugLocEntry() : Begin(0), End(0), Variable(0), Merged(false) {
98     Constants.Int = 0;
99   }
100   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
101                 const MDNode *V)
102       : Begin(B), End(E), Loc(L), Variable(V), Merged(false) {
103     Constants.Int = 0;
104     EntryKind = E_Location;
105   }
106   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i)
107       : Begin(B), End(E), Variable(0), Merged(false) {
108     Constants.Int = i;
109     EntryKind = E_Integer;
110   }
111   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr)
112       : Begin(B), End(E), Variable(0), Merged(false) {
113     Constants.CFP = FPtr;
114     EntryKind = E_ConstantFP;
115   }
116   DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantInt *IPtr)
117       : Begin(B), End(E), Variable(0), Merged(false) {
118     Constants.CIP = IPtr;
119     EntryKind = E_ConstantInt;
120   }
122   /// \brief Empty entries are also used as a trigger to emit temp label. Such
123   /// labels are referenced is used to find debug_loc offset for a given DIE.
124   bool isEmpty() const { return Begin == 0 && End == 0; }
125   bool isMerged() const { return Merged; }
126   void Merge(DebugLocEntry *Next) {
127     if (!(Begin && Loc == Next->Loc && End == Next->Begin))
128       return;
129     Next->Begin = Begin;
130     Merged = true;
131   }
132   bool isLocation() const { return EntryKind == E_Location; }
133   bool isInt() const { return EntryKind == E_Integer; }
134   bool isConstantFP() const { return EntryKind == E_ConstantFP; }
135   bool isConstantInt() const { return EntryKind == E_ConstantInt; }
136   int64_t getInt() const { return Constants.Int; }
137   const ConstantFP *getConstantFP() const { return Constants.CFP; }
138   const ConstantInt *getConstantInt() const { return Constants.CIP; }
139   const MDNode *getVariable() const { return Variable; }
140   const MCSymbol *getBeginSym() const { return Begin; }
141   const MCSymbol *getEndSym() const { return End; }
142   MachineLocation getLoc() const { return Loc; }
143 };
145 //===----------------------------------------------------------------------===//
146 /// \brief This class is used to track local variable information.
147 class DbgVariable {
148   DIVariable Var;             // Variable Descriptor.
149   DIE *TheDIE;                // Variable DIE.
150   unsigned DotDebugLocOffset; // Offset in DotDebugLocEntries.
151   DbgVariable *AbsVar;        // Corresponding Abstract variable, if any.
152   const MachineInstr *MInsn;  // DBG_VALUE instruction of the variable.
153   int FrameIndex;
154   DwarfDebug *DD;
156 public:
157   // AbsVar may be NULL.
158   DbgVariable(DIVariable V, DbgVariable *AV, DwarfDebug *DD)
159       : Var(V), TheDIE(0), DotDebugLocOffset(~0U), AbsVar(AV), MInsn(0),
160         FrameIndex(~0), DD(DD) {}
162   // Accessors.
163   DIVariable getVariable() const { return Var; }
164   void setDIE(DIE *D) { TheDIE = D; }
165   DIE *getDIE() const { return TheDIE; }
166   void setDotDebugLocOffset(unsigned O) { DotDebugLocOffset = O; }
167   unsigned getDotDebugLocOffset() const { return DotDebugLocOffset; }
168   StringRef getName() const { return Var.getName(); }
169   DbgVariable *getAbstractVariable() const { return AbsVar; }
170   const MachineInstr *getMInsn() const { return MInsn; }
171   void setMInsn(const MachineInstr *M) { MInsn = M; }
172   int getFrameIndex() const { return FrameIndex; }
173   void setFrameIndex(int FI) { FrameIndex = FI; }
174   // Translate tag to proper Dwarf tag.
175   uint16_t getTag() const {
176     if (Var.getTag() == dwarf::DW_TAG_arg_variable)
177       return dwarf::DW_TAG_formal_parameter;
179     return dwarf::DW_TAG_variable;
180   }
181   /// \brief Return true if DbgVariable is artificial.
182   bool isArtificial() const {
183     if (Var.isArtificial())
184       return true;
185     if (getType().isArtificial())
186       return true;
187     return false;
188   }
190   bool isObjectPointer() const {
191     if (Var.isObjectPointer())
192       return true;
193     if (getType().isObjectPointer())
194       return true;
195     return false;
196   }
198   bool variableHasComplexAddress() const {
199     assert(Var.isVariable() && "Invalid complex DbgVariable!");
200     return Var.hasComplexAddress();
201   }
202   bool isBlockByrefVariable() const;
203   unsigned getNumAddrElements() const {
204     assert(Var.isVariable() && "Invalid complex DbgVariable!");
205     return Var.getNumAddrElements();
206   }
207   uint64_t getAddrElement(unsigned i) const { return Var.getAddrElement(i); }
208   DIType getType() const;
210 private:
211   /// resolve - Look in the DwarfDebug map for the MDNode that
212   /// corresponds to the reference.
213   template <typename T> T resolve(DIRef<T> Ref) const;
214 };
216 /// \brief Collects and handles information specific to a particular
217 /// collection of units. This collection represents all of the units
218 /// that will be ultimately output into a single object file.
219 class DwarfFile {
220   // Target of Dwarf emission, used for sizing of abbreviations.
221   AsmPrinter *Asm;
223   // Used to uniquely define abbreviations.
224   FoldingSet<DIEAbbrev> AbbreviationsSet;
226   // A list of all the unique abbreviations in use.
227   std::vector<DIEAbbrev *> Abbreviations;
229   // A pointer to all units in the section.
230   SmallVector<DwarfUnit *, 1> CUs;
232   // Collection of strings for this unit and assorted symbols.
233   // A String->Symbol mapping of strings used by indirect
234   // references.
235   typedef StringMap<std::pair<MCSymbol *, unsigned>, BumpPtrAllocator &>
236   StrPool;
237   StrPool StringPool;
238   unsigned NextStringPoolNumber;
239   std::string StringPref;
241   struct AddressPoolEntry {
242     unsigned Number;
243     bool TLS;
244     AddressPoolEntry(unsigned Number, bool TLS) : Number(Number), TLS(TLS) {}
245   };
246   // Collection of addresses for this unit and assorted labels.
247   // A Symbol->unsigned mapping of addresses used by indirect
248   // references.
249   typedef DenseMap<const MCSymbol *, AddressPoolEntry> AddrPool;
250   AddrPool AddressPool;
251   unsigned NextAddrPoolNumber;
253 public:
254   DwarfFile(AsmPrinter *AP, const char *Pref, BumpPtrAllocator &DA)
255       : Asm(AP), StringPool(DA), NextStringPoolNumber(0), StringPref(Pref),
256         AddressPool(), NextAddrPoolNumber(0) {}
258   ~DwarfFile();
260   const SmallVectorImpl<DwarfUnit *> &getUnits() { return CUs; }
262   /// \brief Compute the size and offset of a DIE given an incoming Offset.
263   unsigned computeSizeAndOffset(DIE *Die, unsigned Offset);
265   /// \brief Compute the size and offset of all the DIEs.
266   void computeSizeAndOffsets();
268   /// \brief Define a unique number for the abbreviation.
269   void assignAbbrevNumber(DIEAbbrev &Abbrev);
271   /// \brief Add a unit to the list of CUs.
272   void addUnit(DwarfUnit *CU) { CUs.push_back(CU); }
274   /// \brief Emit all of the units to the section listed with the given
275   /// abbreviation section.
276   void emitUnits(DwarfDebug *DD, const MCSection *ASection,
277                  const MCSymbol *ASectionSym);
279   /// \brief Emit a set of abbreviations to the specific section.
280   void emitAbbrevs(const MCSection *);
282   /// \brief Emit all of the strings to the section given.
283   void emitStrings(const MCSection *StrSection, const MCSection *OffsetSection,
284                    const MCSymbol *StrSecSym);
286   /// \brief Emit all of the addresses to the section given.
287   void emitAddresses(const MCSection *AddrSection);
289   /// \brief Returns the entry into the start of the pool.
290   MCSymbol *getStringPoolSym();
292   /// \brief Returns an entry into the string pool with the given
293   /// string text.
294   MCSymbol *getStringPoolEntry(StringRef Str);
296   /// \brief Returns the index into the string pool with the given
297   /// string text.
298   unsigned getStringPoolIndex(StringRef Str);
300   /// \brief Returns the string pool.
301   StrPool *getStringPool() { return &StringPool; }
303   /// \brief Returns the index into the address pool with the given
304   /// label/symbol.
305   unsigned getAddrPoolIndex(const MCSymbol *Sym, bool TLS = false);
307   /// \brief Returns the address pool.
308   AddrPool *getAddrPool() { return &AddressPool; }
309 };
311 /// \brief Helper used to pair up a symbol and its DWARF compile unit.
312 struct SymbolCU {
313   SymbolCU(DwarfCompileUnit *CU, const MCSymbol *Sym) : Sym(Sym), CU(CU) {}
314   const MCSymbol *Sym;
315   DwarfCompileUnit *CU;
316 };
318 /// \brief Collects and handles dwarf debug information.
319 class DwarfDebug : public AsmPrinterHandler {
320   // Target of Dwarf emission.
321   AsmPrinter *Asm;
323   // Collected machine module information.
324   MachineModuleInfo *MMI;
326   // All DIEValues are allocated through this allocator.
327   BumpPtrAllocator DIEValueAllocator;
329   // Handle to the compile unit used for the inline extension handling,
330   // this is just so that the DIEValue allocator has a place to store
331   // the particular elements.
332   // FIXME: Store these off of DwarfDebug instead?
333   DwarfCompileUnit *FirstCU;
335   // Maps MDNode with its corresponding DwarfCompileUnit.
336   MapVector<const MDNode *, DwarfCompileUnit *> CUMap;
338   // Maps subprogram MDNode with its corresponding DwarfCompileUnit.
339   DenseMap<const MDNode *, DwarfCompileUnit *> SPMap;
341   // Maps a CU DIE with its corresponding DwarfCompileUnit.
342   DenseMap<const DIE *, DwarfCompileUnit *> CUDieMap;
344   /// Maps MDNodes for type sysstem with the corresponding DIEs. These DIEs can
345   /// be shared across CUs, that is why we keep the map here instead
346   /// of in DwarfCompileUnit.
347   DenseMap<const MDNode *, DIE *> MDTypeNodeToDieMap;
349   // Used to unique C++ member function declarations.
350   StringMap<const MDNode *> OdrMemberMap;
352   // List of all labels used in aranges generation.
353   std::vector<SymbolCU> ArangeLabels;
355   // Size of each symbol emitted (for those symbols that have a specific size).
356   DenseMap<const MCSymbol *, uint64_t> SymSize;
358   // Provides a unique id per text section.
359   typedef DenseMap<const MCSection *, SmallVector<SymbolCU, 8> > SectionMapType;
360   SectionMapType SectionMap;
362   // List of arguments for current function.
363   SmallVector<DbgVariable *, 8> CurrentFnArguments;
365   LexicalScopes LScopes;
367   // Collection of abstract subprogram DIEs.
368   DenseMap<const MDNode *, DIE *> AbstractSPDies;
370   // Collection of dbg variables of a scope.
371   typedef DenseMap<LexicalScope *, SmallVector<DbgVariable *, 8> >
372   ScopeVariablesMap;
373   ScopeVariablesMap ScopeVariables;
375   // Collection of abstract variables.
376   DenseMap<const MDNode *, DbgVariable *> AbstractVariables;
378   // Collection of DebugLocEntry.
379   SmallVector<DebugLocEntry, 4> DotDebugLocEntries;
381   // Collection of subprogram DIEs that are marked (at the end of the module)
382   // as DW_AT_inline.
383   SmallPtrSet<DIE *, 4> InlinedSubprogramDIEs;
385   // This is a collection of subprogram MDNodes that are processed to
386   // create DIEs.
387   SmallPtrSet<const MDNode *, 16> ProcessedSPNodes;
389   // Maps instruction with label emitted before instruction.
390   DenseMap<const MachineInstr *, MCSymbol *> LabelsBeforeInsn;
392   // Maps instruction with label emitted after instruction.
393   DenseMap<const MachineInstr *, MCSymbol *> LabelsAfterInsn;
395   // Every user variable mentioned by a DBG_VALUE instruction in order of
396   // appearance.
397   SmallVector<const MDNode *, 8> UserVariables;
399   // For each user variable, keep a list of DBG_VALUE instructions in order.
400   // The list can also contain normal instructions that clobber the previous
401   // DBG_VALUE.
402   typedef DenseMap<const MDNode *, SmallVector<const MachineInstr *, 4> >
403   DbgValueHistoryMap;
404   DbgValueHistoryMap DbgValues;
406   // Previous instruction's location information. This is used to determine
407   // label location to indicate scope boundries in dwarf debug info.
408   DebugLoc PrevInstLoc;
409   MCSymbol *PrevLabel;
411   // This location indicates end of function prologue and beginning of function
412   // body.
413   DebugLoc PrologEndLoc;
415   // If nonnull, stores the current machine function we're processing.
416   const MachineFunction *CurFn;
418   // If nonnull, stores the current machine instruction we're processing.
419   const MachineInstr *CurMI;
421   // Section Symbols: these are assembler temporary labels that are emitted at
422   // the beginning of each supported dwarf section.  These are used to form
423   // section offsets and are created by EmitSectionLabels.
424   MCSymbol *DwarfInfoSectionSym, *DwarfAbbrevSectionSym;
425   MCSymbol *DwarfStrSectionSym, *TextSectionSym, *DwarfDebugRangeSectionSym;
426   MCSymbol *DwarfDebugLocSectionSym, *DwarfLineSectionSym, *DwarfAddrSectionSym;
427   MCSymbol *FunctionBeginSym, *FunctionEndSym;
428   MCSymbol *DwarfInfoDWOSectionSym, *DwarfAbbrevDWOSectionSym;
429   MCSymbol *DwarfStrDWOSectionSym;
430   MCSymbol *DwarfGnuPubNamesSectionSym, *DwarfGnuPubTypesSectionSym;
432   // As an optimization, there is no need to emit an entry in the directory
433   // table for the same directory as DW_AT_comp_dir.
434   StringRef CompilationDir;
436   // Counter for assigning globally unique IDs for ranges.
437   unsigned GlobalRangeCount;
439   // Holder for the file specific debug information.
440   DwarfFile InfoHolder;
442   // Holders for the various debug information flags that we might need to
443   // have exposed. See accessor functions below for description.
445   // Holder for imported entities.
446   typedef SmallVector<std::pair<const MDNode *, const MDNode *>, 32>
447   ImportedEntityMap;
448   ImportedEntityMap ScopesWithImportedEntities;
450   // Map from MDNodes for user-defined types to the type units that describe
451   // them.
452   DenseMap<const MDNode *, const DwarfTypeUnit *> DwarfTypeUnits;
454   // Whether to emit the pubnames/pubtypes sections.
455   bool HasDwarfPubSections;
457   // Whether or not to use AT_ranges for compilation units.
458   bool HasCURanges;
460   // Whether we emitted a function into a section other than the default
461   // text.
462   bool UsedNonDefaultText;
464   // Version of dwarf we're emitting.
465   unsigned DwarfVersion;
467   // Maps from a type identifier to the actual MDNode.
468   DITypeIdentifierMap TypeIdentifierMap;
470   // DWARF5 Experimental Options
471   bool HasDwarfAccelTables;
472   bool HasSplitDwarf;
474   // Separated Dwarf Variables
475   // In general these will all be for bits that are left in the
476   // original object file, rather than things that are meant
477   // to be in the .dwo sections.
479   // Holder for the skeleton information.
480   DwarfFile SkeletonHolder;
482   // Store file names for type units under fission in a line table header that
483   // will be emitted into debug_line.dwo.
484   MCDwarfDwoLineTable SplitTypeUnitFileTable;
486   void addScopeVariable(LexicalScope *LS, DbgVariable *Var);
488   const SmallVectorImpl<DwarfUnit *> &getUnits() {
489     return InfoHolder.getUnits();
490   }
492   /// \brief Find abstract variable associated with Var.
493   DbgVariable *findAbstractVariable(DIVariable &Var, DebugLoc Loc);
495   /// \brief Find DIE for the given subprogram and attach appropriate
496   /// DW_AT_low_pc and DW_AT_high_pc attributes. If there are global
497   /// variables in this scope then create and insert DIEs for these
498   /// variables.
499   DIE *updateSubprogramScopeDIE(DwarfCompileUnit *SPCU, DISubprogram SP);
501   /// \brief A helper function to check whether the DIE for a given Scope is
502   /// going to be null.
503   bool isLexicalScopeDIENull(LexicalScope *Scope);
505   /// \brief A helper function to construct a RangeSpanList for a given
506   /// lexical scope.
507   void addScopeRangeList(DwarfCompileUnit *TheCU, DIE *ScopeDIE,
508                          const SmallVectorImpl<InsnRange> &Range);
510   /// \brief Construct new DW_TAG_lexical_block for this scope and
511   /// attach DW_AT_low_pc/DW_AT_high_pc labels.
512   DIE *constructLexicalScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
514   /// \brief This scope represents inlined body of a function. Construct
515   /// DIE to represent this concrete inlined copy of the function.
516   DIE *constructInlinedScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
518   /// \brief Construct a DIE for this scope.
519   DIE *constructScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
520   /// A helper function to create children of a Scope DIE.
521   DIE *createScopeChildrenDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope,
522                               SmallVectorImpl<DIE *> &Children);
524   /// \brief Emit initial Dwarf sections with a label at the start of each one.
525   void emitSectionLabels();
527   /// \brief Compute the size and offset of a DIE given an incoming Offset.
528   unsigned computeSizeAndOffset(DIE *Die, unsigned Offset);
530   /// \brief Compute the size and offset of all the DIEs.
531   void computeSizeAndOffsets();
533   /// \brief Attach DW_AT_inline attribute with inlined subprogram DIEs.
534   void computeInlinedDIEs();
536   /// \brief Collect info for variables that were optimized out.
537   void collectDeadVariables();
539   /// \brief Finish off debug information after all functions have been
540   /// processed.
541   void finalizeModuleInfo();
543   /// \brief Emit labels to close any remaining sections that have been left
544   /// open.
545   void endSections();
547   /// \brief Emit the debug info section.
548   void emitDebugInfo();
550   /// \brief Emit the abbreviation section.
551   void emitAbbreviations();
553   /// \brief Emit the last address of the section and the end of
554   /// the line matrix.
555   void emitEndOfLineMatrix(unsigned SectionEnd);
557   /// \brief Emit visible names into a hashed accelerator table section.
558   void emitAccelNames();
560   /// \brief Emit objective C classes and categories into a hashed
561   /// accelerator table section.
562   void emitAccelObjC();
564   /// \brief Emit namespace dies into a hashed accelerator table.
565   void emitAccelNamespaces();
567   /// \brief Emit type dies into a hashed accelerator table.
568   void emitAccelTypes();
570   /// \brief Emit visible names into a debug pubnames section.
571   /// \param GnuStyle determines whether or not we want to emit
572   /// additional information into the table ala newer gcc for gdb
573   /// index.
574   void emitDebugPubNames(bool GnuStyle = false);
576   /// \brief Emit visible types into a debug pubtypes section.
577   /// \param GnuStyle determines whether or not we want to emit
578   /// additional information into the table ala newer gcc for gdb
579   /// index.
580   void emitDebugPubTypes(bool GnuStyle = false);
582   void
583   emitDebugPubSection(bool GnuStyle, const MCSection *PSec, StringRef Name,
584                       const StringMap<const DIE *> &(DwarfUnit::*Accessor)()
585                       const);
587   /// \brief Emit visible names into a debug str section.
588   void emitDebugStr();
590   /// \brief Emit visible names into a debug loc section.
591   void emitDebugLoc();
593   /// \brief Emit visible names into a debug aranges section.
594   void emitDebugARanges();
596   /// \brief Emit visible names into a debug ranges section.
597   void emitDebugRanges();
599   /// \brief Emit inline info using custom format.
600   void emitDebugInlineInfo();
602   /// DWARF 5 Experimental Split Dwarf Emitters
604   /// \brief Initialize common features of skeleton units.
605   void initSkeletonUnit(const DwarfUnit *U, DIE *Die, DwarfUnit *NewU);
607   /// \brief Construct the split debug info compile unit for the debug info
608   /// section.
609   DwarfCompileUnit *constructSkeletonCU(const DwarfCompileUnit *CU);
611   /// \brief Construct the split debug info compile unit for the debug info
612   /// section.
613   DwarfTypeUnit *constructSkeletonTU(DwarfTypeUnit *TU);
615   /// \brief Emit the debug info dwo section.
616   void emitDebugInfoDWO();
618   /// \brief Emit the debug abbrev dwo section.
619   void emitDebugAbbrevDWO();
621   /// \brief Emit the debug line dwo section.
622   void emitDebugLineDWO();
624   /// \brief Emit the debug str dwo section.
625   void emitDebugStrDWO();
627   /// Flags to let the linker know we have emitted new style pubnames. Only
628   /// emit it here if we don't have a skeleton CU for split dwarf.
629   void addGnuPubAttributes(DwarfUnit *U, DIE *D) const;
631   /// \brief Create new DwarfCompileUnit for the given metadata node with tag
632   /// DW_TAG_compile_unit.
633   DwarfCompileUnit *constructDwarfCompileUnit(DICompileUnit DIUnit,
634                                               bool Singular);
636   /// \brief Construct subprogram DIE.
637   void constructSubprogramDIE(DwarfCompileUnit *TheCU, const MDNode *N);
639   /// \brief Construct imported_module or imported_declaration DIE.
640   void constructImportedEntityDIE(DwarfCompileUnit *TheCU, const MDNode *N);
642   /// \brief Construct import_module DIE.
643   void constructImportedEntityDIE(DwarfCompileUnit *TheCU, const MDNode *N,
644                                   DIE *Context);
646   /// \brief Construct import_module DIE.
647   void constructImportedEntityDIE(DwarfCompileUnit *TheCU,
648                                   const DIImportedEntity &Module, DIE *Context);
650   /// \brief Register a source line with debug info. Returns the unique
651   /// label that was emitted and which provides correspondence to the
652   /// source line list.
653   void recordSourceLine(unsigned Line, unsigned Col, const MDNode *Scope,
654                         unsigned Flags);
656   /// \brief Indentify instructions that are marking the beginning of or
657   /// ending of a scope.
658   void identifyScopeMarkers();
660   /// \brief If Var is an current function argument that add it in
661   /// CurrentFnArguments list.
662   bool addCurrentFnArgument(DbgVariable *Var, LexicalScope *Scope);
664   /// \brief Populate LexicalScope entries with variables' info.
665   void collectVariableInfo(SmallPtrSet<const MDNode *, 16> &ProcessedVars);
667   /// \brief Collect variable information from the side table maintained
668   /// by MMI.
669   void collectVariableInfoFromMMITable(SmallPtrSet<const MDNode *, 16> &P);
671   /// \brief Ensure that a label will be emitted before MI.
672   void requestLabelBeforeInsn(const MachineInstr *MI) {
673     LabelsBeforeInsn.insert(std::make_pair(MI, (MCSymbol *)0));
674   }
676   /// \brief Return Label preceding the instruction.
677   MCSymbol *getLabelBeforeInsn(const MachineInstr *MI);
679   /// \brief Ensure that a label will be emitted after MI.
680   void requestLabelAfterInsn(const MachineInstr *MI) {
681     LabelsAfterInsn.insert(std::make_pair(MI, (MCSymbol *)0));
682   }
684   /// \brief Return Label immediately following the instruction.
685   MCSymbol *getLabelAfterInsn(const MachineInstr *MI);
687   void attachLowHighPC(DwarfCompileUnit *Unit, DIE *D, MCSymbol *Begin,
688                        MCSymbol *End);
690 public:
691   //===--------------------------------------------------------------------===//
692   // Main entry points.
693   //
694   DwarfDebug(AsmPrinter *A, Module *M);
696   void insertDIE(const MDNode *TypeMD, DIE *Die) {
697     MDTypeNodeToDieMap.insert(std::make_pair(TypeMD, Die));
698   }
699   DIE *getDIE(const MDNode *TypeMD) {
700     return MDTypeNodeToDieMap.lookup(TypeMD);
701   }
703   /// \brief Look up or create an entry in the OdrMemberMap.
704   const MDNode *&getOrCreateOdrMember(StringRef Key) {
705     return OdrMemberMap.GetOrCreateValue(Key).getValue();
706   }
708   /// \brief Emit all Dwarf sections that should come prior to the
709   /// content.
710   void beginModule();
712   /// \brief Emit all Dwarf sections that should come after the content.
713   void endModule() override;
715   /// \brief Gather pre-function debug information.
716   void beginFunction(const MachineFunction *MF) override;
718   /// \brief Gather and emit post-function debug information.
719   void endFunction(const MachineFunction *MF) override;
721   /// \brief Process beginning of an instruction.
722   void beginInstruction(const MachineInstr *MI) override;
724   /// \brief Process end of an instruction.
725   void endInstruction() override;
727   /// \brief Add a DIE to the set of types that we're going to pull into
728   /// type units.
729   void addDwarfTypeUnitType(DwarfCompileUnit &CU, StringRef Identifier,
730                             DIE *Die, DICompositeType CTy);
732   /// \brief Add a label so that arange data can be generated for it.
733   void addArangeLabel(SymbolCU SCU) { ArangeLabels.push_back(SCU); }
735   /// \brief For symbols that have a size designated (e.g. common symbols),
736   /// this tracks that size.
737   void setSymbolSize(const MCSymbol *Sym, uint64_t Size) override {
738     SymSize[Sym] = Size;
739   }
741   /// \brief Recursively Emits a debug information entry.
742   void emitDIE(DIE *Die);
744   // Experimental DWARF5 features.
746   /// \brief Returns whether or not to emit tables that dwarf consumers can
747   /// use to accelerate lookup.
748   bool useDwarfAccelTables() const { return HasDwarfAccelTables; }
750   /// \brief Returns whether or not to change the current debug info for the
751   /// split dwarf proposal support.
752   bool useSplitDwarf() const { return HasSplitDwarf; }
754   /// \brief Returns whether or not to use AT_ranges for compilation units.
755   bool useCURanges() const { return HasCURanges; }
757   /// Returns the Dwarf Version.
758   unsigned getDwarfVersion() const { return DwarfVersion; }
760   /// Returns the section symbol for the .debug_loc section.
761   MCSymbol *getDebugLocSym() const { return DwarfDebugLocSectionSym; }
763   /// Returns the entries for the .debug_loc section.
764   const SmallVectorImpl<DebugLocEntry> &getDebugLocEntries() const {
765     return DotDebugLocEntries;
766   }
768   /// \brief Emit an entry for the debug loc section. This can be used to
769   /// handle an entry that's going to be emitted into the debug loc section.
770   void emitDebugLocEntry(ByteStreamer &Streamer, const DebugLocEntry &Entry);
772   /// Find the MDNode for the given reference.
773   template <typename T> T resolve(DIRef<T> Ref) const {
774     return Ref.resolve(TypeIdentifierMap);
775   }
777   /// \brief Return the TypeIdentifierMap.
778   const DITypeIdentifierMap& getTypeIdentifierMap() const {
779     return TypeIdentifierMap;
780   }
782   /// Find the DwarfCompileUnit for the given CU Die.
783   DwarfCompileUnit *lookupUnit(const DIE *CU) const {
784     return CUDieMap.lookup(CU);
785   }
786   /// isSubprogramContext - Return true if Context is either a subprogram
787   /// or another context nested inside a subprogram.
788   bool isSubprogramContext(const MDNode *Context);
789 };
790 } // End of namespace llvm
792 #endif