]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AsmPrinter/DwarfExpression.cpp
remove extra semicolon
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.cpp
1 //===-- llvm/CodeGen/DwarfExpression.cpp - Dwarf Debug Framework ----------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf debug info into asm files.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "DwarfExpression.h"
15 #include "llvm/ADT/SmallBitVector.h"
16 #include "llvm/Support/Dwarf.h"
17 #include "llvm/Target/TargetMachine.h"
18 #include "llvm/Target/TargetRegisterInfo.h"
19 #include "llvm/Target/TargetSubtargetInfo.h"
22 using namespace llvm;
24 void DwarfExpression::AddReg(int DwarfReg, const char* Comment) {
25   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
26   if (DwarfReg < 32) {
27     EmitOp(dwarf::DW_OP_reg0 + DwarfReg, Comment);
28   } else {
29     EmitOp(dwarf::DW_OP_regx, Comment);
30     EmitUnsigned(DwarfReg);
31   }
32 }
34 void DwarfExpression::AddRegIndirect(int DwarfReg, int Offset, bool Deref) {
35   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
36   if (DwarfReg < 32) {
37     EmitOp(dwarf::DW_OP_breg0 + DwarfReg);
38   } else {
39     EmitOp(dwarf::DW_OP_bregx);
40     EmitUnsigned(DwarfReg);
41   }
42   EmitSigned(Offset);
43   if (Deref)
44     EmitOp(dwarf::DW_OP_deref);
45 }
47 void DwarfExpression::AddOpPiece(unsigned SizeInBits,
48                                  unsigned OffsetInBits) {
49   assert(SizeInBits > 0 && "piece has size zero");
50   const unsigned SizeOfByte = 8;
51   if (OffsetInBits > 0 || SizeInBits % SizeOfByte) {
52     EmitOp(dwarf::DW_OP_bit_piece);
53     EmitUnsigned(SizeInBits);
54     EmitUnsigned(OffsetInBits);
55   } else {
56     EmitOp(dwarf::DW_OP_piece);
57     unsigned ByteSize = SizeInBits / SizeOfByte;
58     EmitUnsigned(ByteSize);
59   }
60 }
62 void DwarfExpression::AddShr(unsigned ShiftBy) {
63   EmitOp(dwarf::DW_OP_constu);
64   EmitUnsigned(ShiftBy);
65   EmitOp(dwarf::DW_OP_shr);
66 }
68 bool DwarfExpression::AddMachineRegIndirect(unsigned MachineReg, int Offset) {
69   const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
70   int DwarfReg = TRI->getDwarfRegNum(MachineReg, false);
71   if (DwarfReg < 0)
72     return false;
74   if (MachineReg == getFrameRegister()) {
75     // If variable offset is based in frame register then use fbreg.
76     EmitOp(dwarf::DW_OP_fbreg);
77     EmitSigned(Offset);
78   } else {
79     AddRegIndirect(DwarfReg, Offset);
80   }
81   return true;
82 }
84 void DwarfExpression::AddMachineRegPiece(unsigned MachineReg,
85                                          unsigned PieceSizeInBits,
86                                          unsigned PieceOffsetInBits) {
87   const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
88   int Reg = TRI->getDwarfRegNum(MachineReg, false);
90   // If this is a valid register number, emit it.
91   if (Reg >= 0) {
92     AddReg(Reg);
93     if (PieceSizeInBits)
94       AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
95     return;
96   }
98   // Walk up the super-register chain until we find a valid number.
99   // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0.
100   for (MCSuperRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
101     Reg = TRI->getDwarfRegNum(*SR, false);
102     if (Reg >= 0) {
103       unsigned Idx = TRI->getSubRegIndex(*SR, MachineReg);
104       unsigned Size = TRI->getSubRegIdxSize(Idx);
105       unsigned RegOffset = TRI->getSubRegIdxOffset(Idx);
106       AddReg(Reg, "super-register");
107       if (PieceOffsetInBits == RegOffset) {
108         AddOpPiece(Size, RegOffset);
109       } else {
110         // If this is part of a variable in a sub-register at a
111         // non-zero offset, we need to manually shift the value into
112         // place, since the DW_OP_piece describes the part of the
113         // variable, not the position of the subregister.
114         if (RegOffset)
115           AddShr(RegOffset);
116         AddOpPiece(Size, PieceOffsetInBits);
117       }
118       return;
119     }
120   }
122   // Otherwise, attempt to find a covering set of sub-register numbers.
123   // For example, Q0 on ARM is a composition of D0+D1.
124   //
125   // Keep track of the current position so we can emit the more
126   // efficient DW_OP_piece.
127   unsigned CurPos = PieceOffsetInBits;
128   // The size of the register in bits, assuming 8 bits per byte.
129   unsigned RegSize = TRI->getMinimalPhysRegClass(MachineReg)->getSize() * 8;
130   // Keep track of the bits in the register we already emitted, so we
131   // can avoid emitting redundant aliasing subregs.
132   SmallBitVector Coverage(RegSize, false);
133   for (MCSubRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
134     unsigned Idx = TRI->getSubRegIndex(MachineReg, *SR);
135     unsigned Size = TRI->getSubRegIdxSize(Idx);
136     unsigned Offset = TRI->getSubRegIdxOffset(Idx);
137     Reg = TRI->getDwarfRegNum(*SR, false);
139     // Intersection between the bits we already emitted and the bits
140     // covered by this subregister.
141     SmallBitVector Intersection(RegSize, false);
142     Intersection.set(Offset, Offset + Size);
143     Intersection ^= Coverage;
145     // If this sub-register has a DWARF number and we haven't covered
146     // its range, emit a DWARF piece for it.
147     if (Reg >= 0 && Intersection.any()) {
148       AddReg(Reg, "sub-register");
149       AddOpPiece(Size, Offset == CurPos ? 0 : Offset);
150       CurPos = Offset + Size;
152       // Mark it as emitted.
153       Coverage.set(Offset, Offset + Size);
154     }
155   }
157   if (CurPos == PieceOffsetInBits)
158     // FIXME: We have no reasonable way of handling errors in here.
159     EmitOp(dwarf::DW_OP_nop, "nop (could not find a dwarf register number)");