[cleanup] Re-sort all the #include lines in LLVM using
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.cpp
1 //===-- llvm/CodeGen/DwarfExpression.cpp - Dwarf Debug Framework ----------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf debug info into asm files.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "DwarfExpression.h"
15 #include "DwarfDebug.h"
16 #include "llvm/ADT/SmallBitVector.h"
17 #include "llvm/CodeGen/AsmPrinter.h"
18 #include "llvm/Support/Dwarf.h"
19 #include "llvm/Target/TargetMachine.h"
20 #include "llvm/Target/TargetRegisterInfo.h"
21 #include "llvm/Target/TargetSubtargetInfo.h"
23 using namespace llvm;
25 const TargetRegisterInfo *DwarfExpression::getTRI() const {
26   return AP.TM.getSubtargetImpl()->getRegisterInfo();
27 }
29 unsigned DwarfExpression::getDwarfVersion() const {
30   return AP.getDwarfDebug()->getDwarfVersion();
31 }
33 void DwarfExpression::AddReg(int DwarfReg, const char *Comment) {
34   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
35   if (DwarfReg < 32) {
36     EmitOp(dwarf::DW_OP_reg0 + DwarfReg, Comment);
37   } else {
38     EmitOp(dwarf::DW_OP_regx, Comment);
39     EmitUnsigned(DwarfReg);
40   }
41 }
43 void DwarfExpression::AddRegIndirect(int DwarfReg, int Offset, bool Deref) {
44   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
45   if (DwarfReg < 32) {
46     EmitOp(dwarf::DW_OP_breg0 + DwarfReg);
47   } else {
48     EmitOp(dwarf::DW_OP_bregx);
49     EmitUnsigned(DwarfReg);
50   }
51   EmitSigned(Offset);
52   if (Deref)
53     EmitOp(dwarf::DW_OP_deref);
54 }
56 void DwarfExpression::AddOpPiece(unsigned SizeInBits, unsigned OffsetInBits) {
57   assert(SizeInBits > 0 && "piece has size zero");
58   const unsigned SizeOfByte = 8;
59   if (OffsetInBits > 0 || SizeInBits % SizeOfByte) {
60     EmitOp(dwarf::DW_OP_bit_piece);
61     EmitUnsigned(SizeInBits);
62     EmitUnsigned(OffsetInBits);
63   } else {
64     EmitOp(dwarf::DW_OP_piece);
65     unsigned ByteSize = SizeInBits / SizeOfByte;
66     EmitUnsigned(ByteSize);
67   }
68 }
70 void DwarfExpression::AddShr(unsigned ShiftBy) {
71   EmitOp(dwarf::DW_OP_constu);
72   EmitUnsigned(ShiftBy);
73   EmitOp(dwarf::DW_OP_shr);
74 }
76 bool DwarfExpression::AddMachineRegIndirect(unsigned MachineReg, int Offset) {
77   int DwarfReg = getTRI()->getDwarfRegNum(MachineReg, false);
78   if (DwarfReg < 0)
79     return false;
81   if (isFrameRegister(MachineReg)) {
82     // If variable offset is based in frame register then use fbreg.
83     EmitOp(dwarf::DW_OP_fbreg);
84     EmitSigned(Offset);
85   } else {
86     AddRegIndirect(DwarfReg, Offset);
87   }
88   return true;
89 }
91 bool DwarfExpression::AddMachineRegPiece(unsigned MachineReg,
92                                          unsigned PieceSizeInBits,
93                                          unsigned PieceOffsetInBits) {
94   const TargetRegisterInfo *TRI = getTRI();
95   int Reg = TRI->getDwarfRegNum(MachineReg, false);
97   // If this is a valid register number, emit it.
98   if (Reg >= 0) {
99     AddReg(Reg);
100     if (PieceSizeInBits)
101       AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
102     return true;
103   }
105   // Walk up the super-register chain until we find a valid number.
106   // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0.
107   for (MCSuperRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
108     Reg = TRI->getDwarfRegNum(*SR, false);
109     if (Reg >= 0) {
110       unsigned Idx = TRI->getSubRegIndex(*SR, MachineReg);
111       unsigned Size = TRI->getSubRegIdxSize(Idx);
112       unsigned RegOffset = TRI->getSubRegIdxOffset(Idx);
113       AddReg(Reg, "super-register");
114       if (PieceOffsetInBits == RegOffset) {
115         AddOpPiece(Size, RegOffset);
116       } else {
117         // If this is part of a variable in a sub-register at a
118         // non-zero offset, we need to manually shift the value into
119         // place, since the DW_OP_piece describes the part of the
120         // variable, not the position of the subregister.
121         if (RegOffset)
122           AddShr(RegOffset);
123         AddOpPiece(Size, PieceOffsetInBits);
124       }
125       return true;
126     }
127   }
129   // Otherwise, attempt to find a covering set of sub-register numbers.
130   // For example, Q0 on ARM is a composition of D0+D1.
131   //
132   // Keep track of the current position so we can emit the more
133   // efficient DW_OP_piece.
134   unsigned CurPos = PieceOffsetInBits;
135   // The size of the register in bits, assuming 8 bits per byte.
136   unsigned RegSize = TRI->getMinimalPhysRegClass(MachineReg)->getSize() * 8;
137   // Keep track of the bits in the register we already emitted, so we
138   // can avoid emitting redundant aliasing subregs.
139   SmallBitVector Coverage(RegSize, false);
140   for (MCSubRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
141     unsigned Idx = TRI->getSubRegIndex(MachineReg, *SR);
142     unsigned Size = TRI->getSubRegIdxSize(Idx);
143     unsigned Offset = TRI->getSubRegIdxOffset(Idx);
144     Reg = TRI->getDwarfRegNum(*SR, false);
146     // Intersection between the bits we already emitted and the bits
147     // covered by this subregister.
148     SmallBitVector Intersection(RegSize, false);
149     Intersection.set(Offset, Offset + Size);
150     Intersection ^= Coverage;
152     // If this sub-register has a DWARF number and we haven't covered
153     // its range, emit a DWARF piece for it.
154     if (Reg >= 0 && Intersection.any()) {
155       AddReg(Reg, "sub-register");
156       AddOpPiece(Size, Offset == CurPos ? 0 : Offset);
157       CurPos = Offset + Size;
159       // Mark it as emitted.
160       Coverage.set(Offset, Offset + Size);
161     }
162   }
164   return CurPos > PieceOffsetInBits;
167 void DwarfExpression::AddSignedConstant(int Value) {
168   EmitOp(dwarf::DW_OP_consts);
169   EmitSigned(Value);
170   // The proper way to describe a constant value is
171   // DW_OP_constu <const>, DW_OP_stack_value.
172   // Unfortunately, DW_OP_stack_value was not available until DWARF-4,
173   // so we will continue to generate DW_OP_constu <const> for DWARF-2
174   // and DWARF-3. Technically, this is incorrect since DW_OP_const <const>
175   // actually describes a value at a constant addess, not a constant value.
176   // However, in the past there was no better way  to describe a constant
177   // value, so the producers and consumers started to rely on heuristics
178   // to disambiguate the value vs. location status of the expression.
179   // See PR21176 for more details.
180   if (getDwarfVersion() >= 4)
181     EmitOp(dwarf::DW_OP_stack_value);
184 void DwarfExpression::AddUnsignedConstant(unsigned Value) {
185   EmitOp(dwarf::DW_OP_constu);
186   EmitUnsigned(Value);
187   // cf. comment in DwarfExpression::AddSignedConstant().
188   if (getDwarfVersion() >= 4)
189     EmitOp(dwarf::DW_OP_stack_value);
192 static unsigned getOffsetOrZero(unsigned OffsetInBits,
193                                 unsigned PieceOffsetInBits) {
194   if (OffsetInBits == PieceOffsetInBits)
195     return 0;
196   assert(OffsetInBits >= PieceOffsetInBits && "overlapping pieces");
197   return OffsetInBits;
200 bool DwarfExpression::AddMachineRegExpression(DIExpression Expr,
201                                               unsigned MachineReg,
202                                               unsigned PieceOffsetInBits) {
203   unsigned N = Expr.getNumElements();
204   unsigned I = 0;
205   bool ValidReg = false;
206   // Pattern-match combinations for which more efficient representations exist
207   // first.
208   if (N >= 3 && Expr.getElement(0) == dwarf::DW_OP_piece) {
209     unsigned SizeOfByte = 8;
210     unsigned OffsetInBits = Expr.getElement(1) * SizeOfByte;
211     unsigned SizeInBits = Expr.getElement(2) * SizeOfByte;
212     ValidReg =
213         AddMachineRegPiece(MachineReg, SizeInBits,
214                            getOffsetOrZero(OffsetInBits, PieceOffsetInBits));
215     I = 3;
216   } else if (N >= 3 && Expr.getElement(0) == dwarf::DW_OP_plus &&
217              Expr.getElement(2) == dwarf::DW_OP_deref) {
218     // [DW_OP_reg,Offset,DW_OP_plus,DW_OP_deref] --> [DW_OP_breg,Offset].
219     unsigned Offset = Expr.getElement(1);
220     ValidReg = AddMachineRegIndirect(MachineReg, Offset);
221     I = 3;
222   } else if (N >= 1 && Expr.getElement(0) == dwarf::DW_OP_deref) {
223     // [DW_OP_reg,DW_OP_deref] --> [DW_OP_breg].
224     ValidReg = AddMachineRegIndirect(MachineReg);
225     I = 1;
226   } else
227     ValidReg = AddMachineRegPiece(MachineReg);
229   if (!ValidReg)
230     return false;
232   // Emit remaining elements of the expression.
233   AddExpression(Expr, I);
234   return true;
237 void DwarfExpression::AddExpression(DIExpression Expr, unsigned I,
238                                     unsigned PieceOffsetInBits) {
239   unsigned N = Expr.getNumElements();
240   for (; I < N; ++I) {
241     switch (Expr.getElement(I)) {
242     case dwarf::DW_OP_piece: {
243       unsigned SizeOfByte = 8;
244       unsigned OffsetInBits = Expr.getElement(++I) * SizeOfByte;
245       unsigned SizeInBits = Expr.getElement(++I) * SizeOfByte;
246       AddOpPiece(SizeInBits, getOffsetOrZero(OffsetInBits, PieceOffsetInBits));
247       break;
248     }
249     case dwarf::DW_OP_plus:
250       EmitOp(dwarf::DW_OP_plus_uconst);
251       EmitUnsigned(Expr.getElement(++I));
252       break;
253     case dwarf::DW_OP_deref:
254       EmitOp(dwarf::DW_OP_deref);
255       break;
256     default:
257       llvm_unreachable("unhandled opcode found in DIExpression");
258     }
259   }