Make DwarfExpression store the AsmPrinter instead of the TargetMachine.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.cpp
1 //===-- llvm/CodeGen/DwarfExpression.cpp - Dwarf Debug Framework ----------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf debug info into asm files.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "DwarfExpression.h"
16 #include "DwarfDebug.h"
17 #include "llvm/ADT/SmallBitVector.h"
18 #include "llvm/CodeGen/AsmPrinter.h"
19 #include "llvm/Support/Dwarf.h"
20 #include "llvm/Target/TargetMachine.h"
21 #include "llvm/Target/TargetRegisterInfo.h"
22 #include "llvm/Target/TargetSubtargetInfo.h"
25 using namespace llvm;
27 const TargetRegisterInfo *DwarfExpression::getTRI() const {
28   return AP.TM.getSubtargetImpl()->getRegisterInfo();
29 }
31 void DwarfExpression::AddReg(int DwarfReg, const char* Comment) {
32   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
33   if (DwarfReg < 32) {
34     EmitOp(dwarf::DW_OP_reg0 + DwarfReg, Comment);
35   } else {
36     EmitOp(dwarf::DW_OP_regx, Comment);
37     EmitUnsigned(DwarfReg);
38   }
39 }
41 void DwarfExpression::AddRegIndirect(int DwarfReg, int Offset, bool Deref) {
42   assert(DwarfReg >= 0 && "invalid negative dwarf register number");
43   if (DwarfReg < 32) {
44     EmitOp(dwarf::DW_OP_breg0 + DwarfReg);
45   } else {
46     EmitOp(dwarf::DW_OP_bregx);
47     EmitUnsigned(DwarfReg);
48   }
49   EmitSigned(Offset);
50   if (Deref)
51     EmitOp(dwarf::DW_OP_deref);
52 }
54 void DwarfExpression::AddOpPiece(unsigned SizeInBits,
55                                  unsigned OffsetInBits) {
56   assert(SizeInBits > 0 && "piece has size zero");
57   const unsigned SizeOfByte = 8;
58   if (OffsetInBits > 0 || SizeInBits % SizeOfByte) {
59     EmitOp(dwarf::DW_OP_bit_piece);
60     EmitUnsigned(SizeInBits);
61     EmitUnsigned(OffsetInBits);
62   } else {
63     EmitOp(dwarf::DW_OP_piece);
64     unsigned ByteSize = SizeInBits / SizeOfByte;
65     EmitUnsigned(ByteSize);
66   }
67 }
69 void DwarfExpression::AddShr(unsigned ShiftBy) {
70   EmitOp(dwarf::DW_OP_constu);
71   EmitUnsigned(ShiftBy);
72   EmitOp(dwarf::DW_OP_shr);
73 }
75 bool DwarfExpression::AddMachineRegIndirect(unsigned MachineReg, int Offset) {
76   int DwarfReg = getTRI()->getDwarfRegNum(MachineReg, false);
77   if (DwarfReg < 0)
78     return false;
80   if (MachineReg == getFrameRegister()) {
81     // If variable offset is based in frame register then use fbreg.
82     EmitOp(dwarf::DW_OP_fbreg);
83     EmitSigned(Offset);
84   } else {
85     AddRegIndirect(DwarfReg, Offset);
86   }
87   return true;
88 }
90 void DwarfExpression::AddMachineRegPiece(unsigned MachineReg,
91                                          unsigned PieceSizeInBits,
92                                          unsigned PieceOffsetInBits) {
93   const TargetRegisterInfo *TRI = getTRI();
94   int Reg = TRI->getDwarfRegNum(MachineReg, false);
96   // If this is a valid register number, emit it.
97   if (Reg >= 0) {
98     AddReg(Reg);
99     if (PieceSizeInBits)
100       AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
101     return;
102   }
104   // Walk up the super-register chain until we find a valid number.
105   // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0.
106   for (MCSuperRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
107     Reg = TRI->getDwarfRegNum(*SR, false);
108     if (Reg >= 0) {
109       unsigned Idx = TRI->getSubRegIndex(*SR, MachineReg);
110       unsigned Size = TRI->getSubRegIdxSize(Idx);
111       unsigned RegOffset = TRI->getSubRegIdxOffset(Idx);
112       AddReg(Reg, "super-register");
113       if (PieceOffsetInBits == RegOffset) {
114         AddOpPiece(Size, RegOffset);
115       } else {
116         // If this is part of a variable in a sub-register at a
117         // non-zero offset, we need to manually shift the value into
118         // place, since the DW_OP_piece describes the part of the
119         // variable, not the position of the subregister.
120         if (RegOffset)
121           AddShr(RegOffset);
122         AddOpPiece(Size, PieceOffsetInBits);
123       }
124       return;
125     }
126   }
128   // Otherwise, attempt to find a covering set of sub-register numbers.
129   // For example, Q0 on ARM is a composition of D0+D1.
130   //
131   // Keep track of the current position so we can emit the more
132   // efficient DW_OP_piece.
133   unsigned CurPos = PieceOffsetInBits;
134   // The size of the register in bits, assuming 8 bits per byte.
135   unsigned RegSize = TRI->getMinimalPhysRegClass(MachineReg)->getSize() * 8;
136   // Keep track of the bits in the register we already emitted, so we
137   // can avoid emitting redundant aliasing subregs.
138   SmallBitVector Coverage(RegSize, false);
139   for (MCSubRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) {
140     unsigned Idx = TRI->getSubRegIndex(MachineReg, *SR);
141     unsigned Size = TRI->getSubRegIdxSize(Idx);
142     unsigned Offset = TRI->getSubRegIdxOffset(Idx);
143     Reg = TRI->getDwarfRegNum(*SR, false);
145     // Intersection between the bits we already emitted and the bits
146     // covered by this subregister.
147     SmallBitVector Intersection(RegSize, false);
148     Intersection.set(Offset, Offset + Size);
149     Intersection ^= Coverage;
151     // If this sub-register has a DWARF number and we haven't covered
152     // its range, emit a DWARF piece for it.
153     if (Reg >= 0 && Intersection.any()) {
154       AddReg(Reg, "sub-register");
155       AddOpPiece(Size, Offset == CurPos ? 0 : Offset);
156       CurPos = Offset + Size;
158       // Mark it as emitted.
159       Coverage.set(Offset, Offset + Size);
160     }
161   }
163   if (CurPos == PieceOffsetInBits)
164     // FIXME: We have no reasonable way of handling errors in here.
165     EmitOp(dwarf::DW_OP_nop, "nop (could not find a dwarf register number)");