[cleanup] Re-sort all the #include lines in LLVM using
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.h
1 //===-- llvm/CodeGen/DwarfExpression.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
15 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
17 #include "llvm/IR/DebugInfo.h"
18 #include "llvm/Support/DataTypes.h"
20 namespace llvm {
22 class AsmPrinter;
23 class ByteStreamer;
24 class TargetRegisterInfo;
25 class DwarfUnit;
26 class DIELoc;
28 /// Base class containing the logic for constructing DWARF expressions
29 /// independently of whether they are emitted into a DIE or into a .debug_loc
30 /// entry.
31 class DwarfExpression {
32 protected:
33   const AsmPrinter ≈
34   // Various convenience accessors that extract things out of AsmPrinter.
35   const TargetRegisterInfo *getTRI() const;
36   unsigned getDwarfVersion() const;
38 public:
39   DwarfExpression(const AsmPrinter &AP) : AP(AP) {}
40   virtual ~DwarfExpression() {}
42   /// Output a dwarf operand and an optional assembler comment.
43   virtual void EmitOp(uint8_t Op, const char *Comment = nullptr) = 0;
44   /// Emit a raw signed value.
45   virtual void EmitSigned(int Value) = 0;
46   /// Emit a raw unsigned value.
47   virtual void EmitUnsigned(unsigned Value) = 0;
48   /// Return whether the given machine register is the frame register in the
49   /// current function.
50   virtual bool isFrameRegister(unsigned MachineReg) = 0;
52   /// Emit a dwarf register operation.
53   void AddReg(int DwarfReg, const char *Comment = nullptr);
54   /// Emit an (double-)indirect dwarf register operation.
55   void AddRegIndirect(int DwarfReg, int Offset, bool Deref = false);
57   /// Emit a dwarf register operation for describing
58   /// - a small value occupying only part of a register or
59   /// - a register representing only part of a value.
60   void AddOpPiece(unsigned SizeInBits, unsigned OffsetInBits = 0);
61   /// Emit a shift-right dwarf expression.
62   void AddShr(unsigned ShiftBy);
64   /// Emit an indirect dwarf register operation for the given machine register.
65   /// \return false if no DWARF register exists for MachineReg.
66   bool AddMachineRegIndirect(unsigned MachineReg, int Offset = 0);
68   /// \brief Emit a partial DWARF register operation.
69   /// \param MachineReg        the register
70   /// \param PieceSizeInBits   size and
71   /// \param PieceOffsetInBits offset of the piece in bits, if this is one
72   ///                          piece of an aggregate value.
73   ///
74   /// If size and offset is zero an operation for the entire
75   /// register is emitted: Some targets do not provide a DWARF
76   /// register number for every register.  If this is the case, this
77   /// function will attempt to emit a DWARF register by emitting a
78   /// piece of a super-register or by piecing together multiple
79   /// subregisters that alias the register.
80   ///
81   /// \return false if no DWARF register exists for MachineReg.
82   bool AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0,
83                           unsigned PieceOffsetInBits = 0);
85   /// Emit a signed constant.
86   void AddSignedConstant(int Value);
87   /// Emit an unsigned constant.
88   void AddUnsignedConstant(unsigned Value);
90   /// Emit an entire DIExpression on top of a machine register location.
91   /// \param PieceOffsetInBits If this is one piece out of a fragmented
92   /// location, this is the offset of the piece inside the entire variable.
93   /// \return false if no DWARF register exists for MachineReg.
94   bool AddMachineRegExpression(DIExpression Expr, unsigned MachineReg,
95                                unsigned PieceOffsetInBits = 0);
96   /// Emit a the operations in a DIExpression, starting from element I.
97   /// \param PieceOffsetInBits If this is one piece out of a fragmented
98   /// location, this is the offset of the piece inside the entire variable.
99   void AddExpression(DIExpression Expr, unsigned PieceOffsetInBits = 0,
100                      unsigned I = 0);
101 };
103 /// DwarfExpression implementation for .debug_loc entries.
104 class DebugLocDwarfExpression : public DwarfExpression {
105   ByteStreamer &BS;
107 public:
108   DebugLocDwarfExpression(const AsmPrinter &AP, ByteStreamer &BS)
109       : DwarfExpression(AP), BS(BS) {}
111   void EmitOp(uint8_t Op, const char *Comment = nullptr) override;
112   void EmitSigned(int Value) override;
113   void EmitUnsigned(unsigned Value) override;
114   bool isFrameRegister(unsigned MachineReg) override;
115 };
117 /// DwarfExpression implementation for singular DW_AT_location.
118 class DIEDwarfExpression : public DwarfExpression {
119   DwarfUnit &DU;
120   DIELoc ¨
122 public:
123   DIEDwarfExpression(const AsmPrinter &AP, DwarfUnit &DU, DIELoc &DIE)
124       : DwarfExpression(AP), DU(DU), DIE(DIE) {}
126   void EmitOp(uint8_t Op, const char *Comment = nullptr) override;
127   void EmitSigned(int Value) override;
128   void EmitUnsigned(unsigned Value) override;
129   bool isFrameRegister(unsigned MachineReg) override;
130 };
133 #endif