]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AsmPrinter/DwarfStringPool.cpp
Debug Info: Remove unused code. The MInsn of an _abstract_ variable is
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfStringPool.cpp
1 //===-- llvm/CodeGen/DwarfStringPool.cpp - Dwarf Debug Framework ----------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #include "DwarfStringPool.h"
11 #include "llvm/MC/MCStreamer.h"
13 using namespace llvm;
15 MCSymbol *DwarfStringPool::getSectionSymbol() { return SectionSymbol; }
17 static std::pair<MCSymbol *, unsigned> &
18 getEntry(AsmPrinter &Asm,
19          StringMap<std::pair<MCSymbol *, unsigned>, BumpPtrAllocator &> &Pool,
20          StringRef Prefix, StringRef Str) {
21   std::pair<MCSymbol *, unsigned> &Entry =
22       Pool.GetOrCreateValue(Str).getValue();
23   if (!Entry.first) {
24     Entry.second = Pool.size() - 1;
25     Entry.first = Asm.GetTempSymbol(Prefix, Entry.second);
26   }
27   return Entry;
28 }
30 MCSymbol *DwarfStringPool::getSymbol(AsmPrinter &Asm, StringRef Str) {
31   return getEntry(Asm, Pool, Prefix, Str).first;
32 }
34 unsigned DwarfStringPool::getIndex(AsmPrinter &Asm, StringRef Str) {
35   return getEntry(Asm, Pool, Prefix, Str).second;
36 }
38 void DwarfStringPool::emit(AsmPrinter &Asm, const MCSection *StrSection,
39                            const MCSection *OffsetSection,
40                            const MCSymbol *StrSecSym) {
41   if (Pool.empty())
42     return;
44   // Start the dwarf str section.
45   Asm.OutStreamer.SwitchSection(StrSection);
47   // Get all of the string pool entries and put them in an array by their ID so
48   // we can sort them.
49   SmallVector<const StringMapEntry<std::pair<MCSymbol *, unsigned>> *, 64>
50   Entries(Pool.size());
52   for (const auto &E : Pool)
53     Entries[E.getValue().second] = &E;
55   for (const auto &Entry : Entries) {
56     // Emit a label for reference from debug information entries.
57     Asm.OutStreamer.EmitLabel(Entry->getValue().first);
59     // Emit the string itself with a terminating null byte.
60     Asm.OutStreamer.EmitBytes(
61         StringRef(Entry->getKeyData(), Entry->getKeyLength() + 1));
62   }
64   // If we've got an offset section go ahead and emit that now as well.
65   if (OffsetSection) {
66     Asm.OutStreamer.SwitchSection(OffsetSection);
67     unsigned offset = 0;
68     unsigned size = 4; // FIXME: DWARF64 is 8.
69     for (const auto &Entry : Entries) {
70       Asm.OutStreamer.EmitIntValue(offset, size);
71       offset += Entry->getKeyLength() + 1;
72     }
73   }
74 }