1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DwarfUnit.h"
17 #include "DwarfAccelTable.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/DIBuilder.h"
21 #include "llvm/IR/Constants.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCSection.h"
28 #include "llvm/MC/MCStreamer.h"
29 #include "llvm/Support/CommandLine.h"
30 #include "llvm/Target/TargetFrameLowering.h"
31 #include "llvm/Target/TargetLoweringObjectFile.h"
32 #include "llvm/Target/TargetMachine.h"
33 #include "llvm/Target/TargetRegisterInfo.h"
35 using namespace llvm;
37 static cl::opt<bool>
38 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
39 cl::desc("Generate DWARF4 type units."),
40 cl::init(false));
42 /// Unit - Unit constructor.
43 DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
44 DwarfDebug *DW, DwarfFile *DWU)
45 : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
46 DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
47 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
48 }
50 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
51 AsmPrinter *A, DwarfDebug *DW,
52 DwarfFile *DWU)
53 : DwarfUnit(UID, D, Node, A, DW, DWU) {
54 insertDIE(Node, D);
55 }
57 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DICompileUnit CUNode,
58 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
59 : DwarfUnit(UID, D, CUNode, A, DW, DWU) {}
61 /// ~Unit - Destructor for compile unit.
62 DwarfUnit::~DwarfUnit() {
63 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
64 DIEBlocks[j]->~DIEBlock();
65 }
67 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
68 /// information entry.
69 DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
70 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
71 return Value;
72 }
74 /// getDefaultLowerBound - Return the default lower bound for an array. If the
75 /// DWARF version doesn't handle the language, return -1.
76 int64_t DwarfUnit::getDefaultLowerBound() const {
77 switch (getLanguage()) {
78 default:
79 break;
81 case dwarf::DW_LANG_C89:
82 case dwarf::DW_LANG_C99:
83 case dwarf::DW_LANG_C:
84 case dwarf::DW_LANG_C_plus_plus:
85 case dwarf::DW_LANG_ObjC:
86 case dwarf::DW_LANG_ObjC_plus_plus:
87 return 0;
89 case dwarf::DW_LANG_Fortran77:
90 case dwarf::DW_LANG_Fortran90:
91 case dwarf::DW_LANG_Fortran95:
92 return 1;
94 // The languages below have valid values only if the DWARF version >= 4.
95 case dwarf::DW_LANG_Java:
96 case dwarf::DW_LANG_Python:
97 case dwarf::DW_LANG_UPC:
98 case dwarf::DW_LANG_D:
99 if (dwarf::DWARF_VERSION >= 4)
100 return 0;
101 break;
103 case dwarf::DW_LANG_Ada83:
104 case dwarf::DW_LANG_Ada95:
105 case dwarf::DW_LANG_Cobol74:
106 case dwarf::DW_LANG_Cobol85:
107 case dwarf::DW_LANG_Modula2:
108 case dwarf::DW_LANG_Pascal83:
109 case dwarf::DW_LANG_PLI:
110 if (dwarf::DWARF_VERSION >= 4)
111 return 1;
112 break;
113 }
115 return -1;
116 }
118 /// Check whether the DIE for this MDNode can be shared across CUs.
119 static bool isShareableAcrossCUs(DIDescriptor D) {
120 // When the MDNode can be part of the type system, the DIE can be shared
121 // across CUs.
122 // Combining type units and cross-CU DIE sharing is lower value (since
123 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
124 // level already) but may be implementable for some value in projects
125 // building multiple independent libraries with LTO and then linking those
126 // together.
127 return (D.isType() ||
128 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
129 !GenerateDwarfTypeUnits;
130 }
132 /// getDIE - Returns the debug information entry map slot for the
133 /// specified debug variable. We delegate the request to DwarfDebug
134 /// when the DIE for this MDNode can be shared across CUs. The mappings
135 /// will be kept in DwarfDebug for shareable DIEs.
136 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
137 if (isShareableAcrossCUs(D))
138 return DD->getDIE(D);
139 return MDNodeToDieMap.lookup(D);
140 }
142 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
143 /// when the DIE for this MDNode can be shared across CUs. The mappings
144 /// will be kept in DwarfDebug for shareable DIEs.
145 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
146 if (isShareableAcrossCUs(Desc)) {
147 DD->insertDIE(Desc, D);
148 return;
149 }
150 MDNodeToDieMap.insert(std::make_pair(Desc, D));
151 }
153 /// addFlag - Add a flag that is true.
154 void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
155 if (DD->getDwarfVersion() >= 4)
156 Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
157 else
158 Die->addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
159 }
161 /// addUInt - Add an unsigned integer attribute data and value.
162 ///
163 void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
164 Optional<dwarf::Form> Form, uint64_t Integer) {
165 if (!Form)
166 Form = DIEInteger::BestForm(false, Integer);
167 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
168 DIEInteger(Integer);
169 Die->addValue(Attribute, *Form, Value);
170 }
172 void DwarfUnit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
173 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
174 }
176 /// addSInt - Add an signed integer attribute data and value.
177 ///
178 void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
179 Optional<dwarf::Form> Form, int64_t Integer) {
180 if (!Form)
181 Form = DIEInteger::BestForm(true, Integer);
182 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
183 Die->addValue(Attribute, *Form, Value);
184 }
186 void DwarfUnit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form,
187 int64_t Integer) {
188 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
189 }
191 /// addString - Add a string attribute data and value. We always emit a
192 /// reference to the string pool instead of immediate strings so that DIEs have
193 /// more predictable sizes. In the case of split dwarf we emit an index
194 /// into another table which gets us the static offset into the string
195 /// table.
196 void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
197 StringRef String) {
199 if (!DD->useSplitDwarf())
200 return addLocalString(Die, Attribute, String);
202 unsigned idx = DU->getStringPoolIndex(String);
203 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
204 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
205 Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
206 }
208 /// addLocalString - Add a string attribute data and value. This is guaranteed
209 /// to be in the local string pool instead of indirected.
210 void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
211 StringRef String) {
212 MCSymbol *Symb = DU->getStringPoolEntry(String);
213 DIEValue *Value;
214 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
215 Value = new (DIEValueAllocator) DIELabel(Symb);
216 else {
217 MCSymbol *StringPool = DU->getStringPoolSym();
218 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
219 }
220 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
221 Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
222 }
224 /// addExpr - Add a Dwarf expression attribute data and value.
225 ///
226 void DwarfUnit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
227 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
228 Die->addValue((dwarf::Attribute)0, Form, Value);
229 }
231 /// addLabel - Add a Dwarf label attribute data and value.
232 ///
233 void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
234 const MCSymbol *Label) {
235 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
236 Die->addValue(Attribute, Form, Value);
237 }
239 void DwarfUnit::addLabel(DIEBlock *Die, dwarf::Form Form,
240 const MCSymbol *Label) {
241 addLabel(Die, (dwarf::Attribute)0, Form, Label);
242 }
244 /// addSectionLabel - Add a Dwarf section label attribute data and value.
245 ///
246 void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
247 const MCSymbol *Label) {
248 if (DD->getDwarfVersion() >= 4)
249 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
250 else
251 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
252 }
254 /// addSectionOffset - Add an offset into a section attribute data and value.
255 ///
256 void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
257 uint64_t Integer) {
258 if (DD->getDwarfVersion() >= 4)
259 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
260 else
261 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
262 }
264 /// addLabelAddress - Add a dwarf label attribute data and value using
265 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
266 ///
267 void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
268 MCSymbol *Label) {
269 if (Label)
270 DD->addArangeLabel(SymbolCU(this, Label));
272 if (!DD->useSplitDwarf()) {
273 if (Label) {
274 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
275 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
276 } else {
277 DIEValue *Value = new (DIEValueAllocator) DIEInteger(0);
278 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
279 }
280 } else {
281 unsigned idx = DU->getAddrPoolIndex(Label);
282 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
283 Die->addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
284 }
285 }
287 /// addOpAddress - Add a dwarf op address data and value using the
288 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
289 ///
290 void DwarfUnit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
291 if (!DD->useSplitDwarf()) {
292 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
293 addLabel(Die, dwarf::DW_FORM_udata, Sym);
294 } else {
295 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
296 addUInt(Die, dwarf::DW_FORM_GNU_addr_index, DU->getAddrPoolIndex(Sym));
297 }
298 }
300 /// addSectionDelta - Add a section label delta attribute data and value.
301 ///
302 void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
303 const MCSymbol *Hi, const MCSymbol *Lo) {
304 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
305 if (DD->getDwarfVersion() >= 4)
306 Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
307 else
308 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
309 }
311 /// addDIEEntry - Add a DIE attribute data and value.
312 ///
313 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
314 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
315 }
317 void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
318 Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
319 new (DIEValueAllocator) DIETypeSignature(Type));
320 }
322 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
323 DIEEntry *Entry) {
324 const DIE *DieCU = Die->getUnitOrNull();
325 const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
326 if (!DieCU)
327 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
328 DieCU = getUnitDie();
329 if (!EntryCU)
330 EntryCU = getUnitDie();
331 Die->addValue(Attribute, EntryCU == DieCU ? dwarf::DW_FORM_ref4
332 : dwarf::DW_FORM_ref_addr,
333 Entry);
334 }
336 /// Create a DIE with the given Tag, add the DIE to its parent, and
337 /// call insertDIE if MD is not null.
338 DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
339 DIE *Die = new DIE(Tag);
340 Parent.addChild(Die);
341 if (N)
342 insertDIE(N, Die);
343 return Die;
344 }
346 /// addBlock - Add block data.
347 ///
348 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
349 DIEBlock *Block) {
350 Block->ComputeSize(Asm);
351 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
352 Die->addValue(Attribute, Block->BestForm(), Block);
353 }
355 /// addSourceLine - Add location information to specified debug information
356 /// entry.
357 void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
358 // Verify variable.
359 if (!V.isVariable())
360 return;
362 unsigned Line = V.getLineNumber();
363 if (Line == 0)
364 return;
365 unsigned FileID =
366 DD->getOrCreateSourceID(V.getContext().getFilename(),
367 V.getContext().getDirectory(), getUniqueID());
368 assert(FileID && "Invalid file id");
369 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
370 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
371 }
373 /// addSourceLine - Add location information to specified debug information
374 /// entry.
375 void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
376 // Verify global variable.
377 if (!G.isGlobalVariable())
378 return;
380 unsigned Line = G.getLineNumber();
381 if (Line == 0)
382 return;
383 unsigned FileID =
384 DD->getOrCreateSourceID(G.getFilename(), G.getDirectory(), getUniqueID());
385 assert(FileID && "Invalid file id");
386 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
387 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
388 }
390 /// addSourceLine - Add location information to specified debug information
391 /// entry.
392 void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
393 // Verify subprogram.
394 if (!SP.isSubprogram())
395 return;
397 // If the line number is 0, don't add it.
398 unsigned Line = SP.getLineNumber();
399 if (Line == 0)
400 return;
402 unsigned FileID = DD->getOrCreateSourceID(SP.getFilename(), SP.getDirectory(),
403 getUniqueID());
404 assert(FileID && "Invalid file id");
405 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
406 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
407 }
409 /// addSourceLine - Add location information to specified debug information
410 /// entry.
411 void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
412 // Verify type.
413 if (!Ty.isType())
414 return;
416 unsigned Line = Ty.getLineNumber();
417 if (Line == 0)
418 return;
419 unsigned FileID = DD->getOrCreateSourceID(Ty.getFilename(), Ty.getDirectory(),
420 getUniqueID());
421 assert(FileID && "Invalid file id");
422 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
423 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
424 }
426 /// addSourceLine - Add location information to specified debug information
427 /// entry.
428 void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
429 // Verify type.
430 if (!Ty.isObjCProperty())
431 return;
433 unsigned Line = Ty.getLineNumber();
434 if (Line == 0)
435 return;
436 DIFile File = Ty.getFile();
437 unsigned FileID = DD->getOrCreateSourceID(File.getFilename(),
438 File.getDirectory(), getUniqueID());
439 assert(FileID && "Invalid file id");
440 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
441 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
442 }
444 /// addSourceLine - Add location information to specified debug information
445 /// entry.
446 void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
447 // Verify namespace.
448 if (!NS.Verify())
449 return;
451 unsigned Line = NS.getLineNumber();
452 if (Line == 0)
453 return;
454 StringRef FN = NS.getFilename();
456 unsigned FileID =
457 DD->getOrCreateSourceID(FN, NS.getDirectory(), getUniqueID());
458 assert(FileID && "Invalid file id");
459 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
460 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
461 }
463 /// addVariableAddress - Add DW_AT_location attribute for a
464 /// DbgVariable based on provided MachineLocation.
465 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
466 MachineLocation Location) {
467 if (DV.variableHasComplexAddress())
468 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
469 else if (DV.isBlockByrefVariable())
470 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
471 else
472 addAddress(Die, dwarf::DW_AT_location, Location,
473 DV.getVariable().isIndirect());
474 }
476 /// addRegisterOp - Add register operand.
477 void DwarfUnit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
478 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
479 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
480 if (DWReg < 32)
481 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
482 else {
483 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
484 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
485 }
486 }
488 /// addRegisterOffset - Add register offset.
489 void DwarfUnit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg,
490 int64_t Offset) {
491 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
492 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
493 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
494 if (Reg == TRI->getFrameRegister(*Asm->MF))
495 // If variable offset is based in frame register then use fbreg.
496 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
497 else if (DWReg < 32)
498 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
499 else {
500 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
501 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
502 }
503 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
504 }
506 /// addAddress - Add an address attribute to a die based on the location
507 /// provided.
508 void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
509 const MachineLocation &Location, bool Indirect) {
510 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
512 if (Location.isReg() && !Indirect)
513 addRegisterOp(Block, Location.getReg());
514 else {
515 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
516 if (Indirect && !Location.isReg()) {
517 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
518 }
519 }
521 // Now attach the location information to the DIE.
522 addBlock(Die, Attribute, Block);
523 }
525 /// addComplexAddress - Start with the address based on the location provided,
526 /// and generate the DWARF information necessary to find the actual variable
527 /// given the extra address information encoded in the DbgVariable, starting
528 /// from the starting location. Add the DWARF information to the die.
529 ///
530 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
531 dwarf::Attribute Attribute,
532 const MachineLocation &Location) {
533 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
534 unsigned N = DV.getNumAddrElements();
535 unsigned i = 0;
536 if (Location.isReg()) {
537 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
538 // If first address element is OpPlus then emit
539 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
540 addRegisterOffset(Block, Location.getReg(), DV.getAddrElement(1));
541 i = 2;
542 } else
543 addRegisterOp(Block, Location.getReg());
544 } else
545 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
547 for (; i < N; ++i) {
548 uint64_t Element = DV.getAddrElement(i);
549 if (Element == DIBuilder::OpPlus) {
550 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
551 addUInt(Block, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
552 } else if (Element == DIBuilder::OpDeref) {
553 if (!Location.isReg())
554 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
555 } else
556 llvm_unreachable("unknown DIBuilder Opcode");
557 }
559 // Now attach the location information to the DIE.
560 addBlock(Die, Attribute, Block);
561 }
563 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
564 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
565 gives the variable VarName either the struct, or a pointer to the struct, as
566 its type. This is necessary for various behind-the-scenes things the
567 compiler needs to do with by-reference variables in Blocks.
569 However, as far as the original *programmer* is concerned, the variable
570 should still have type 'SomeType', as originally declared.
572 The function getBlockByrefType dives into the __Block_byref_x_VarName
573 struct to find the original type of the variable, which is then assigned to
574 the variable's Debug Information Entry as its real type. So far, so good.
575 However now the debugger will expect the variable VarName to have the type
576 SomeType. So we need the location attribute for the variable to be an
577 expression that explains to the debugger how to navigate through the
578 pointers and struct to find the actual variable of type SomeType.
580 The following function does just that. We start by getting
581 the "normal" location for the variable. This will be the location
582 of either the struct __Block_byref_x_VarName or the pointer to the
583 struct __Block_byref_x_VarName.
585 The struct will look something like:
587 struct __Block_byref_x_VarName {
588 ... <various fields>
589 struct __Block_byref_x_VarName *forwarding;
590 ... <various other fields>
591 SomeType VarName;
592 ... <maybe more fields>
593 };
595 If we are given the struct directly (as our starting point) we
596 need to tell the debugger to:
598 1). Add the offset of the forwarding field.
600 2). Follow that pointer to get the real __Block_byref_x_VarName
601 struct to use (the real one may have been copied onto the heap).
603 3). Add the offset for the field VarName, to find the actual variable.
605 If we started with a pointer to the struct, then we need to
606 dereference that pointer first, before the other steps.
607 Translating this into DWARF ops, we will need to append the following
608 to the current location description for the variable:
610 DW_OP_deref -- optional, if we start with a pointer
611 DW_OP_plus_uconst <forward_fld_offset>
612 DW_OP_deref
613 DW_OP_plus_uconst <varName_fld_offset>
615 That is what this function does. */
617 /// addBlockByrefAddress - Start with the address based on the location
618 /// provided, and generate the DWARF information necessary to find the
619 /// actual Block variable (navigating the Block struct) based on the
620 /// starting location. Add the DWARF information to the die. For
621 /// more information, read large comment just above here.
622 ///
623 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
624 dwarf::Attribute Attribute,
625 const MachineLocation &Location) {
626 DIType Ty = DV.getType();
627 DIType TmpTy = Ty;
628 uint16_t Tag = Ty.getTag();
629 bool isPointer = false;
631 StringRef varName = DV.getName();
633 if (Tag == dwarf::DW_TAG_pointer_type) {
634 DIDerivedType DTy(Ty);
635 TmpTy = resolve(DTy.getTypeDerivedFrom());
636 isPointer = true;
637 }
639 DICompositeType blockStruct(TmpTy);
641 // Find the __forwarding field and the variable field in the __Block_byref
642 // struct.
643 DIArray Fields = blockStruct.getTypeArray();
644 DIDerivedType varField;
645 DIDerivedType forwardingField;
647 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
648 DIDerivedType DT(Fields.getElement(i));
649 StringRef fieldName = DT.getName();
650 if (fieldName == "__forwarding")
651 forwardingField = DT;
652 else if (fieldName == varName)
653 varField = DT;
654 }
656 // Get the offsets for the forwarding field and the variable field.
657 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
658 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
660 // Decode the original location, and use that as the start of the byref
661 // variable's location.
662 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
664 if (Location.isReg())
665 addRegisterOp(Block, Location.getReg());
666 else
667 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
669 // If we started with a pointer to the __Block_byref... struct, then
670 // the first thing we need to do is dereference the pointer (DW_OP_deref).
671 if (isPointer)
672 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
674 // Next add the offset for the '__forwarding' field:
675 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
676 // adding the offset if it's 0.
677 if (forwardingFieldOffset > 0) {
678 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
679 addUInt(Block, dwarf::DW_FORM_udata, forwardingFieldOffset);
680 }
682 // Now dereference the __forwarding field to get to the real __Block_byref
683 // struct: DW_OP_deref.
684 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
686 // Now that we've got the real __Block_byref... struct, add the offset
687 // for the variable's field to get to the location of the actual variable:
688 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
689 if (varFieldOffset > 0) {
690 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
691 addUInt(Block, dwarf::DW_FORM_udata, varFieldOffset);
692 }
694 // Now attach the location information to the DIE.
695 addBlock(Die, Attribute, Block);
696 }
698 /// isTypeSigned - Return true if the type is signed.
699 static bool isTypeSigned(DwarfDebug *DD, DIType Ty, int *SizeInBits) {
700 if (Ty.isDerivedType())
701 return isTypeSigned(DD, DD->resolve(DIDerivedType(Ty).getTypeDerivedFrom()),
702 SizeInBits);
703 if (Ty.isBasicType())
704 if (DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed ||
705 DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed_char) {
706 *SizeInBits = Ty.getSizeInBits();
707 return true;
708 }
709 return false;
710 }
712 /// Return true if type encoding is unsigned.
713 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
714 DIDerivedType DTy(Ty);
715 if (DTy.isDerivedType())
716 return isUnsignedDIType(DD, DD->resolve(DTy.getTypeDerivedFrom()));
718 DIBasicType BTy(Ty);
719 if (BTy.isBasicType()) {
720 unsigned Encoding = BTy.getEncoding();
721 if (Encoding == dwarf::DW_ATE_unsigned ||
722 Encoding == dwarf::DW_ATE_unsigned_char ||
723 Encoding == dwarf::DW_ATE_boolean)
724 return true;
725 }
726 return false;
727 }
729 /// If this type is derived from a base type then return base type size.
730 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
731 unsigned Tag = Ty.getTag();
733 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
734 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
735 Tag != dwarf::DW_TAG_restrict_type)
736 return Ty.getSizeInBits();
738 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
740 // If this type is not derived from any type then take conservative approach.
741 if (!BaseType.isValid())
742 return Ty.getSizeInBits();
744 // If this is a derived type, go ahead and get the base type, unless it's a
745 // reference then it's just the size of the field. Pointer types have no need
746 // of this since they're a different type of qualification on the type.
747 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
748 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
749 return Ty.getSizeInBits();
751 if (BaseType.isDerivedType())
752 return getBaseTypeSize(DD, DIDerivedType(BaseType));
754 return BaseType.getSizeInBits();
755 }
757 /// addConstantValue - Add constant value entry in variable DIE.
758 void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
759 DIType Ty) {
760 // FIXME: This is a bit conservative/simple - it emits negative values at
761 // their maximum bit width which is a bit unfortunate (& doesn't prefer
762 // udata/sdata over dataN as suggested by the DWARF spec)
763 assert(MO.isImm() && "Invalid machine operand!");
764 int SizeInBits = -1;
765 bool SignedConstant = isTypeSigned(DD, Ty, &SizeInBits);
766 dwarf::Form Form;
768 // If we're a signed constant definitely use sdata.
769 if (SignedConstant) {
770 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata, MO.getImm());
771 return;
772 }
774 // Else use data for now unless it's larger than we can deal with.
775 switch (SizeInBits) {
776 case 8:
777 Form = dwarf::DW_FORM_data1;
778 break;
779 case 16:
780 Form = dwarf::DW_FORM_data2;
781 break;
782 case 32:
783 Form = dwarf::DW_FORM_data4;
784 break;
785 case 64:
786 Form = dwarf::DW_FORM_data8;
787 break;
788 default:
789 Form = dwarf::DW_FORM_udata;
790 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
791 return;
792 }
793 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
794 }
796 /// addConstantFPValue - Add constant value entry in variable DIE.
797 void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
798 assert(MO.isFPImm() && "Invalid machine operand!");
799 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
800 APFloat FPImm = MO.getFPImm()->getValueAPF();
802 // Get the raw data form of the floating point.
803 const APInt FltVal = FPImm.bitcastToAPInt();
804 const char *FltPtr = (const char *)FltVal.getRawData();
806 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
807 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
808 int Incr = (LittleEndian ? 1 : -1);
809 int Start = (LittleEndian ? 0 : NumBytes - 1);
810 int Stop = (LittleEndian ? NumBytes : -1);
812 // Output the constant to DWARF one byte at a time.
813 for (; Start != Stop; Start += Incr)
814 addUInt(Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
816 addBlock(Die, dwarf::DW_AT_const_value, Block);
817 }
819 /// addConstantFPValue - Add constant value entry in variable DIE.
820 void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
821 // Pass this down to addConstantValue as an unsigned bag of bits.
822 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
823 }
825 /// addConstantValue - Add constant value entry in variable DIE.
826 void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
827 bool Unsigned) {
828 addConstantValue(Die, CI->getValue(), Unsigned);
829 }
831 // addConstantValue - Add constant value entry in variable DIE.
832 void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
833 unsigned CIBitWidth = Val.getBitWidth();
834 if (CIBitWidth <= 64) {
835 // If we're a signed constant definitely use sdata.
836 if (!Unsigned) {
837 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
838 Val.getSExtValue());
839 return;
840 }
842 // Else use data for now unless it's larger than we can deal with.
843 dwarf::Form Form;
844 switch (CIBitWidth) {
845 case 8:
846 Form = dwarf::DW_FORM_data1;
847 break;
848 case 16:
849 Form = dwarf::DW_FORM_data2;
850 break;
851 case 32:
852 Form = dwarf::DW_FORM_data4;
853 break;
854 case 64:
855 Form = dwarf::DW_FORM_data8;
856 break;
857 default:
858 addUInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_udata,
859 Val.getZExtValue());
860 return;
861 }
862 addUInt(Die, dwarf::DW_AT_const_value, Form, Val.getZExtValue());
863 return;
864 }
866 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
868 // Get the raw data form of the large APInt.
869 const uint64_t *Ptr64 = Val.getRawData();
871 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
872 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
874 // Output the constant to DWARF one byte at a time.
875 for (int i = 0; i < NumBytes; i++) {
876 uint8_t c;
877 if (LittleEndian)
878 c = Ptr64[i / 8] >> (8 * (i & 7));
879 else
880 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
881 addUInt(Block, dwarf::DW_FORM_data1, c);
882 }
884 addBlock(Die, dwarf::DW_AT_const_value, Block);
885 }
887 /// addTemplateParams - Add template parameters into buffer.
888 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
889 // Add template parameters.
890 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
891 DIDescriptor Element = TParams.getElement(i);
892 if (Element.isTemplateTypeParameter())
893 constructTemplateTypeParameterDIE(Buffer,
894 DITemplateTypeParameter(Element));
895 else if (Element.isTemplateValueParameter())
896 constructTemplateValueParameterDIE(Buffer,
897 DITemplateValueParameter(Element));
898 }
899 }
901 /// getOrCreateContextDIE - Get context owner's DIE.
902 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
903 if (!Context || Context.isFile())
904 return getUnitDie();
905 if (Context.isType())
906 return getOrCreateTypeDIE(DIType(Context));
907 if (Context.isNameSpace())
908 return getOrCreateNameSpace(DINameSpace(Context));
909 if (Context.isSubprogram())
910 return getOrCreateSubprogramDIE(DISubprogram(Context));
911 return getDIE(Context);
912 }
914 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
915 DIScope Context = resolve(Ty.getContext());
916 DIE *ContextDIE = getOrCreateContextDIE(Context);
918 DIE *TyDIE = getDIE(Ty);
919 if (TyDIE)
920 return TyDIE;
922 // Create new type.
923 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
925 constructTypeDIE(*TyDIE, Ty);
927 updateAcceleratorTables(Context, Ty, TyDIE);
928 return TyDIE;
929 }
931 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
932 /// given DIType.
933 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
934 if (!TyNode)
935 return NULL;
937 DIType Ty(TyNode);
938 assert(Ty.isType());
940 // Construct the context before querying for the existence of the DIE in case
941 // such construction creates the DIE.
942 DIScope Context = resolve(Ty.getContext());
943 DIE *ContextDIE = getOrCreateContextDIE(Context);
944 assert(ContextDIE);
946 DIE *TyDIE = getDIE(Ty);
947 if (TyDIE)
948 return TyDIE;
950 // Create new type.
951 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
953 if (Ty.isBasicType())
954 constructTypeDIE(*TyDIE, DIBasicType(Ty));
955 else if (Ty.isCompositeType()) {
956 DICompositeType CTy(Ty);
957 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
958 if (MDString *TypeId = CTy.getIdentifier()) {
959 DD->addDwarfTypeUnitType(getCUNode(), TypeId->getString(), TyDIE, CTy);
960 // Skip updating the accellerator tables since this is not the full type
961 return TyDIE;
962 }
963 constructTypeDIE(*TyDIE, CTy);
964 } else {
965 assert(Ty.isDerivedType() && "Unknown kind of DIType");
966 constructTypeDIE(*TyDIE, DIDerivedType(Ty));
967 }
969 updateAcceleratorTables(Context, Ty, TyDIE);
971 return TyDIE;
972 }
974 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
975 const DIE *TyDIE) {
976 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
977 bool IsImplementation = 0;
978 if (Ty.isCompositeType()) {
979 DICompositeType CT(Ty);
980 // A runtime language of 0 actually means C/C++ and that any
981 // non-negative value is some version of Objective-C/C++.
982 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
983 }
984 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
985 addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
987 if (!Context || Context.isCompileUnit() || Context.isFile() ||
988 Context.isNameSpace())
989 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
990 }
991 }
993 /// addType - Add a new type attribute to the specified entity.
994 void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
995 assert(Ty && "Trying to add a type that doesn't exist?");
997 // Check for pre-existence.
998 DIEEntry *Entry = getDIEEntry(Ty);
999 // If it exists then use the existing value.
1000 if (Entry) {
1001 addDIEEntry(Entity, Attribute, Entry);
1002 return;
1003 }
1005 // Construct type.
1006 DIE *Buffer = getOrCreateTypeDIE(Ty);
1008 // Set up proxy.
1009 Entry = createDIEEntry(Buffer);
1010 insertDIEEntry(Ty, Entry);
1011 addDIEEntry(Entity, Attribute, Entry);
1012 }
1014 // Accelerator table mutators - add each name along with its companion
1015 // DIE to the proper table while ensuring that the name that we're going
1016 // to reference is in the string table. We do this since the names we
1017 // add may not only be identical to the names in the DIE.
1018 void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
1019 DU->getStringPoolEntry(Name);
1020 std::vector<const DIE *> &DIEs = AccelNames[Name];
1021 DIEs.push_back(Die);
1022 }
1024 void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
1025 DU->getStringPoolEntry(Name);
1026 std::vector<const DIE *> &DIEs = AccelObjC[Name];
1027 DIEs.push_back(Die);
1028 }
1030 void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
1031 DU->getStringPoolEntry(Name);
1032 std::vector<const DIE *> &DIEs = AccelNamespace[Name];
1033 DIEs.push_back(Die);
1034 }
1036 void DwarfUnit::addAccelType(StringRef Name,
1037 std::pair<const DIE *, unsigned> Die) {
1038 DU->getStringPoolEntry(Name);
1039 std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
1040 DIEs.push_back(Die);
1041 }
1043 /// addGlobalName - Add a new global name to the compile unit.
1044 void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
1045 std::string FullName = getParentContextString(Context) + Name.str();
1046 GlobalNames[FullName] = Die;
1047 }
1049 /// getParentContextString - Walks the metadata parent chain in a language
1050 /// specific manner (using the compile unit language) and returns
1051 /// it as a string. This is done at the metadata level because DIEs may
1052 /// not currently have been added to the parent context and walking the
1053 /// DIEs looking for names is more expensive than walking the metadata.
1054 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1055 if (!Context)
1056 return "";
1058 // FIXME: Decide whether to implement this for non-C++ languages.
1059 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1060 return "";
1062 std::string CS;
1063 SmallVector<DIScope, 1> Parents;
1064 while (!Context.isCompileUnit()) {
1065 Parents.push_back(Context);
1066 if (Context.getContext())
1067 Context = resolve(Context.getContext());
1068 else
1069 // Structure, etc types will have a NULL context if they're at the top
1070 // level.
1071 break;
1072 }
1074 // Reverse iterate over our list to go from the outermost construct to the
1075 // innermost.
1076 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1077 E = Parents.rend();
1078 I != E; ++I) {
1079 DIScope Ctx = *I;
1080 StringRef Name = Ctx.getName();
1081 if (!Name.empty()) {
1082 CS += Name;
1083 CS += "::";
1084 }
1085 }
1086 return CS;
1087 }
1089 /// constructTypeDIE - Construct basic type die from DIBasicType.
1090 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1091 // Get core information.
1092 StringRef Name = BTy.getName();
1093 // Add name if not anonymous or intermediate type.
1094 if (!Name.empty())
1095 addString(&Buffer, dwarf::DW_AT_name, Name);
1097 // An unspecified type only has a name attribute.
1098 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1099 return;
1101 addUInt(&Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1102 BTy.getEncoding());
1104 uint64_t Size = BTy.getSizeInBits() >> 3;
1105 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1106 }
1108 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1109 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1110 // Get core information.
1111 StringRef Name = DTy.getName();
1112 uint64_t Size = DTy.getSizeInBits() >> 3;
1113 uint16_t Tag = Buffer.getTag();
1115 // Map to main type, void will not have a type.
1116 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1117 if (FromTy)
1118 addType(&Buffer, FromTy);
1120 // Add name if not anonymous or intermediate type.
1121 if (!Name.empty())
1122 addString(&Buffer, dwarf::DW_AT_name, Name);
1124 // Add size if non-zero (derived types might be zero-sized.)
1125 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1126 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1128 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1129 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1130 getOrCreateTypeDIE(resolve(DTy.getClassType())));
1131 // Add source line info if available and TyDesc is not a forward declaration.
1132 if (!DTy.isForwardDecl())
1133 addSourceLine(&Buffer, DTy);
1134 }
1136 /// constructTypeDIE - Construct type DIE from DICompositeType.
1137 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1138 // Add name if not anonymous or intermediate type.
1139 StringRef Name = CTy.getName();
1141 uint64_t Size = CTy.getSizeInBits() >> 3;
1142 uint16_t Tag = Buffer.getTag();
1144 switch (Tag) {
1145 case dwarf::DW_TAG_array_type:
1146 constructArrayTypeDIE(Buffer, CTy);
1147 break;
1148 case dwarf::DW_TAG_enumeration_type:
1149 constructEnumTypeDIE(Buffer, CTy);
1150 break;
1151 case dwarf::DW_TAG_subroutine_type: {
1152 // Add return type. A void return won't have a type.
1153 DIArray Elements = CTy.getTypeArray();
1154 DIType RTy(Elements.getElement(0));
1155 if (RTy)
1156 addType(&Buffer, RTy);
1158 bool isPrototyped = true;
1159 // Add arguments.
1160 for (unsigned i = 1, N = Elements.getNumElements(); i < N; ++i) {
1161 DIDescriptor Ty = Elements.getElement(i);
1162 if (Ty.isUnspecifiedParameter()) {
1163 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1164 isPrototyped = false;
1165 } else {
1166 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1167 addType(Arg, DIType(Ty));
1168 if (DIType(Ty).isArtificial())
1169 addFlag(Arg, dwarf::DW_AT_artificial);
1170 }
1171 }
1172 // Add prototype flag if we're dealing with a C language and the
1173 // function has been prototyped.
1174 uint16_t Language = getLanguage();
1175 if (isPrototyped &&
1176 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1177 Language == dwarf::DW_LANG_ObjC))
1178 addFlag(&Buffer, dwarf::DW_AT_prototyped);
1180 if (CTy.isLValueReference())
1181 addFlag(&Buffer, dwarf::DW_AT_reference);
1183 if (CTy.isRValueReference())
1184 addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
1185 } break;
1186 case dwarf::DW_TAG_structure_type:
1187 case dwarf::DW_TAG_union_type:
1188 case dwarf::DW_TAG_class_type: {
1189 // Add elements to structure type.
1190 DIArray Elements = CTy.getTypeArray();
1191 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1192 DIDescriptor Element = Elements.getElement(i);
1193 DIE *ElemDie = NULL;
1194 if (Element.isSubprogram())
1195 ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
1196 else if (Element.isDerivedType()) {
1197 DIDerivedType DDTy(Element);
1198 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1199 ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1200 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1201 dwarf::DW_AT_friend);
1202 } else if (DDTy.isStaticMember()) {
1203 getOrCreateStaticMemberDIE(DDTy);
1204 } else {
1205 constructMemberDIE(Buffer, DDTy);
1206 }
1207 } else if (Element.isObjCProperty()) {
1208 DIObjCProperty Property(Element);
1209 ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1210 StringRef PropertyName = Property.getObjCPropertyName();
1211 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1212 if (Property.getType())
1213 addType(ElemDie, Property.getType());
1214 addSourceLine(ElemDie, Property);
1215 StringRef GetterName = Property.getObjCPropertyGetterName();
1216 if (!GetterName.empty())
1217 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1218 StringRef SetterName = Property.getObjCPropertySetterName();
1219 if (!SetterName.empty())
1220 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1221 unsigned PropertyAttributes = 0;
1222 if (Property.isReadOnlyObjCProperty())
1223 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1224 if (Property.isReadWriteObjCProperty())
1225 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1226 if (Property.isAssignObjCProperty())
1227 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1228 if (Property.isRetainObjCProperty())
1229 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1230 if (Property.isCopyObjCProperty())
1231 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1232 if (Property.isNonAtomicObjCProperty())
1233 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1234 if (PropertyAttributes)
1235 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1236 PropertyAttributes);
1238 DIEEntry *Entry = getDIEEntry(Element);
1239 if (!Entry) {
1240 Entry = createDIEEntry(ElemDie);
1241 insertDIEEntry(Element, Entry);
1242 }
1243 } else
1244 continue;
1245 }
1247 if (CTy.isAppleBlockExtension())
1248 addFlag(&Buffer, dwarf::DW_AT_APPLE_block);
1250 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1251 if (ContainingType)
1252 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1253 getOrCreateTypeDIE(ContainingType));
1255 if (CTy.isObjcClassComplete())
1256 addFlag(&Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1258 // Add template parameters to a class, structure or union types.
1259 // FIXME: The support isn't in the metadata for this yet.
1260 if (Tag == dwarf::DW_TAG_class_type ||
1261 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1262 addTemplateParams(Buffer, CTy.getTemplateParams());
1264 break;
1265 }
1266 default:
1267 break;
1268 }
1270 // Add name if not anonymous or intermediate type.
1271 if (!Name.empty())
1272 addString(&Buffer, dwarf::DW_AT_name, Name);
1274 if (Tag == dwarf::DW_TAG_enumeration_type ||
1275 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1276 Tag == dwarf::DW_TAG_union_type) {
1277 // Add size if non-zero (derived types might be zero-sized.)
1278 // TODO: Do we care about size for enum forward declarations?
1279 if (Size)
1280 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1281 else if (!CTy.isForwardDecl())
1282 // Add zero size if it is not a forward declaration.
1283 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, 0);
1285 // If we're a forward decl, say so.
1286 if (CTy.isForwardDecl())
1287 addFlag(&Buffer, dwarf::DW_AT_declaration);
1289 // Add source line info if available.
1290 if (!CTy.isForwardDecl())
1291 addSourceLine(&Buffer, CTy);
1293 // No harm in adding the runtime language to the declaration.
1294 unsigned RLang = CTy.getRunTimeLang();
1295 if (RLang)
1296 addUInt(&Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1297 RLang);
1298 }
1299 }
1301 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1302 /// DITemplateTypeParameter.
1303 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1304 DITemplateTypeParameter TP) {
1305 DIE *ParamDIE =
1306 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1307 // Add the type if it exists, it could be void and therefore no type.
1308 if (TP.getType())
1309 addType(ParamDIE, resolve(TP.getType()));
1310 if (!TP.getName().empty())
1311 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1312 }
1314 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1315 /// DITemplateValueParameter.
1316 void
1317 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1318 DITemplateValueParameter VP) {
1319 DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1321 // Add the type if there is one, template template and template parameter
1322 // packs will not have a type.
1323 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1324 addType(ParamDIE, resolve(VP.getType()));
1325 if (!VP.getName().empty())
1326 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1327 if (Value *Val = VP.getValue()) {
1328 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1329 addConstantValue(ParamDIE, CI,
1330 isUnsignedDIType(DD, resolve(VP.getType())));
1331 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1332 // For declaration non-type template parameters (such as global values and
1333 // functions)
1334 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1335 addOpAddress(Block, Asm->getSymbol(GV));
1336 // Emit DW_OP_stack_value to use the address as the immediate value of the
1337 // parameter, rather than a pointer to it.
1338 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1339 addBlock(ParamDIE, dwarf::DW_AT_location, Block);
1340 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1341 assert(isa<MDString>(Val));
1342 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1343 cast<MDString>(Val)->getString());
1344 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1345 assert(isa<MDNode>(Val));
1346 DIArray A(cast<MDNode>(Val));
1347 addTemplateParams(*ParamDIE, A);
1348 }
1349 }
1350 }
1352 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1353 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1354 // Construct the context before querying for the existence of the DIE in case
1355 // such construction creates the DIE.
1356 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1358 DIE *NDie = getDIE(NS);
1359 if (NDie)
1360 return NDie;
1361 NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1363 if (!NS.getName().empty()) {
1364 addString(NDie, dwarf::DW_AT_name, NS.getName());
1365 addAccelNamespace(NS.getName(), NDie);
1366 addGlobalName(NS.getName(), NDie, NS.getContext());
1367 } else
1368 addAccelNamespace("(anonymous namespace)", NDie);
1369 addSourceLine(NDie, NS);
1370 return NDie;
1371 }
1373 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1374 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1375 // Construct the context before querying for the existence of the DIE in case
1376 // such construction creates the DIE (as is the case for member function
1377 // declarations).
1378 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1380 DIE *SPDie = getDIE(SP);
1381 if (SPDie)
1382 return SPDie;
1384 DISubprogram SPDecl = SP.getFunctionDeclaration();
1385 if (SPDecl.isSubprogram())
1386 // Add subprogram definitions to the CU die directly.
1387 ContextDIE = UnitDie.get();
1389 // DW_TAG_inlined_subroutine may refer to this DIE.
1390 SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1392 DIE *DeclDie = NULL;
1393 if (SPDecl.isSubprogram())
1394 DeclDie = getOrCreateSubprogramDIE(SPDecl);
1396 // Add function template parameters.
1397 addTemplateParams(*SPDie, SP.getTemplateParams());
1399 // If this DIE is going to refer declaration info using AT_specification
1400 // then there is no need to add other attributes.
1401 if (DeclDie) {
1402 // Refer function declaration directly.
1403 addDIEEntry(SPDie, dwarf::DW_AT_specification, DeclDie);
1405 return SPDie;
1406 }
1408 // Add the linkage name if we have one.
1409 StringRef LinkageName = SP.getLinkageName();
1410 if (!LinkageName.empty())
1411 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1412 GlobalValue::getRealLinkageName(LinkageName));
1414 // Constructors and operators for anonymous aggregates do not have names.
1415 if (!SP.getName().empty())
1416 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1418 addSourceLine(SPDie, SP);
1420 // Add the prototype if we have a prototype and we have a C like
1421 // language.
1422 uint16_t Language = getLanguage();
1423 if (SP.isPrototyped() &&
1424 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1425 Language == dwarf::DW_LANG_ObjC))
1426 addFlag(SPDie, dwarf::DW_AT_prototyped);
1428 DICompositeType SPTy = SP.getType();
1429 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1430 "the type of a subprogram should be a subroutine");
1432 DIArray Args = SPTy.getTypeArray();
1433 // Add a return type. If this is a type like a C/C++ void type we don't add a
1434 // return type.
1435 if (Args.getElement(0))
1436 addType(SPDie, DIType(Args.getElement(0)));
1438 unsigned VK = SP.getVirtuality();
1439 if (VK) {
1440 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1441 DIEBlock *Block = getDIEBlock();
1442 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1443 addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1444 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1445 ContainingTypeMap.insert(
1446 std::make_pair(SPDie, resolve(SP.getContainingType())));
1447 }
1449 if (!SP.isDefinition()) {
1450 addFlag(SPDie, dwarf::DW_AT_declaration);
1452 // Add arguments. Do not add arguments for subprogram definition. They will
1453 // be handled while processing variables.
1454 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1455 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, *SPDie);
1456 DIType ATy(Args.getElement(i));
1457 addType(Arg, ATy);
1458 if (ATy.isArtificial())
1459 addFlag(Arg, dwarf::DW_AT_artificial);
1460 }
1461 }
1463 if (SP.isArtificial())
1464 addFlag(SPDie, dwarf::DW_AT_artificial);
1466 if (!SP.isLocalToUnit())
1467 addFlag(SPDie, dwarf::DW_AT_external);
1469 if (SP.isOptimized())
1470 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1472 if (unsigned isa = Asm->getISAEncoding()) {
1473 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1474 }
1476 if (SP.isLValueReference())
1477 addFlag(SPDie, dwarf::DW_AT_reference);
1479 if (SP.isRValueReference())
1480 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1482 if (SP.isProtected())
1483 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1484 dwarf::DW_ACCESS_protected);
1485 else if (SP.isPrivate())
1486 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1487 dwarf::DW_ACCESS_private);
1488 else
1489 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1490 dwarf::DW_ACCESS_public);
1492 if (SP.isExplicit())
1493 addFlag(SPDie, dwarf::DW_AT_explicit);
1495 return SPDie;
1496 }
1498 // Return const expression if value is a GEP to access merged global
1499 // constant. e.g.
1500 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1501 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1502 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1503 if (!CE || CE->getNumOperands() != 3 ||
1504 CE->getOpcode() != Instruction::GetElementPtr)
1505 return NULL;
1507 // First operand points to a global struct.
1508 Value *Ptr = CE->getOperand(0);
1509 if (!isa<GlobalValue>(Ptr) ||
1510 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1511 return NULL;
1513 // Second operand is zero.
1514 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1515 if (!CI || !CI->isZero())
1516 return NULL;
1518 // Third operand is offset.
1519 if (!isa<ConstantInt>(CE->getOperand(2)))
1520 return NULL;
1522 return CE;
1523 }
1525 /// createGlobalVariableDIE - create global variable DIE.
1526 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1527 // Check for pre-existence.
1528 if (getDIE(GV))
1529 return;
1531 if (!GV.isGlobalVariable())
1532 return;
1534 DIScope GVContext = GV.getContext();
1535 DIType GTy = GV.getType();
1537 // If this is a static data member definition, some attributes belong
1538 // to the declaration DIE.
1539 DIE *VariableDIE = NULL;
1540 bool IsStaticMember = false;
1541 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1542 if (SDMDecl.Verify()) {
1543 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1544 // We need the declaration DIE that is in the static member's class.
1545 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1546 IsStaticMember = true;
1547 }
1549 // If this is not a static data member definition, create the variable
1550 // DIE and add the initial set of attributes to it.
1551 if (!VariableDIE) {
1552 // Construct the context before querying for the existence of the DIE in
1553 // case such construction creates the DIE.
1554 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1556 // Add to map.
1557 VariableDIE = createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1559 // Add name and type.
1560 addString(VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1561 addType(VariableDIE, GTy);
1563 // Add scoping info.
1564 if (!GV.isLocalToUnit())
1565 addFlag(VariableDIE, dwarf::DW_AT_external);
1567 // Add line number info.
1568 addSourceLine(VariableDIE, GV);
1569 }
1571 // Add location.
1572 bool addToAccelTable = false;
1573 DIE *VariableSpecDIE = NULL;
1574 bool isGlobalVariable = GV.getGlobal() != NULL;
1575 if (isGlobalVariable) {
1576 addToAccelTable = true;
1577 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1578 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1579 if (GV.getGlobal()->isThreadLocal()) {
1580 // FIXME: Make this work with -gsplit-dwarf.
1581 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1582 assert((PointerSize == 4 || PointerSize == 8) &&
1583 "Add support for other sizes if necessary");
1584 const MCExpr *Expr =
1585 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym);
1586 // Based on GCC's support for TLS:
1587 if (!DD->useSplitDwarf()) {
1588 // 1) Start with a constNu of the appropriate pointer size
1589 addUInt(Block, dwarf::DW_FORM_data1,
1590 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1591 // 2) containing the (relocated) offset of the TLS variable
1592 // within the module's TLS block.
1593 addExpr(Block, dwarf::DW_FORM_udata, Expr);
1594 } else {
1595 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1596 addUInt(Block, dwarf::DW_FORM_udata, DU->getAddrPoolIndex(Expr));
1597 }
1598 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1599 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1600 } else {
1601 DD->addArangeLabel(SymbolCU(this, Sym));
1602 addOpAddress(Block, Sym);
1603 }
1604 // Do not create specification DIE if context is either compile unit
1605 // or a subprogram.
1606 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1607 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1608 // Create specification DIE.
1609 VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
1610 addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
1611 addBlock(VariableSpecDIE, dwarf::DW_AT_location, Block);
1612 // A static member's declaration is already flagged as such.
1613 if (!SDMDecl.Verify())
1614 addFlag(VariableDIE, dwarf::DW_AT_declaration);
1615 } else {
1616 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1617 }
1618 // Add the linkage name.
1619 StringRef LinkageName = GV.getLinkageName();
1620 if (!LinkageName.empty())
1621 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1622 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1623 // TAG_variable.
1624 addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
1625 : VariableDIE,
1626 dwarf::DW_AT_MIPS_linkage_name,
1627 GlobalValue::getRealLinkageName(LinkageName));
1628 } else if (const ConstantInt *CI =
1629 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1630 // AT_const_value was added when the static member was created. To avoid
1631 // emitting AT_const_value multiple times, we only add AT_const_value when
1632 // it is not a static member.
1633 if (!IsStaticMember)
1634 addConstantValue(VariableDIE, CI, isUnsignedDIType(DD, GTy));
1635 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1636 addToAccelTable = true;
1637 // GV is a merged global.
1638 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1639 Value *Ptr = CE->getOperand(0);
1640 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1641 DD->addArangeLabel(SymbolCU(this, Sym));
1642 addOpAddress(Block, Sym);
1643 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1644 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1645 addUInt(Block, dwarf::DW_FORM_udata,
1646 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1647 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1648 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1649 }
1651 if (addToAccelTable) {
1652 DIE *AddrDIE = VariableSpecDIE ? VariableSpecDIE : VariableDIE;
1653 addAccelName(GV.getName(), AddrDIE);
1655 // If the linkage name is different than the name, go ahead and output
1656 // that as well into the name table.
1657 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1658 addAccelName(GV.getLinkageName(), AddrDIE);
1659 }
1661 if (!GV.isLocalToUnit())
1662 addGlobalName(GV.getName(), VariableSpecDIE ? VariableSpecDIE : VariableDIE,
1663 GV.getContext());
1664 }
1666 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1667 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1668 DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1669 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
1671 // The LowerBound value defines the lower bounds which is typically zero for
1672 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1673 // Count == -1 then the array is unbounded and we do not emit
1674 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1675 // Count == 0, then the array has zero elements in which case we do not emit
1676 // an upper bound.
1677 int64_t LowerBound = SR.getLo();
1678 int64_t DefaultLowerBound = getDefaultLowerBound();
1679 int64_t Count = SR.getCount();
1681 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1682 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1684 if (Count != -1 && Count != 0)
1685 // FIXME: An unbounded array should reference the expression that defines
1686 // the array.
1687 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1688 LowerBound + Count - 1);
1689 }
1691 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1692 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1693 if (CTy.isVector())
1694 addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
1696 // Emit the element type.
1697 addType(&Buffer, resolve(CTy.getTypeDerivedFrom()));
1699 // Get an anonymous type for index type.
1700 // FIXME: This type should be passed down from the front end
1701 // as different languages may have different sizes for indexes.
1702 DIE *IdxTy = getIndexTyDie();
1703 if (!IdxTy) {
1704 // Construct an anonymous type for index type.
1705 IdxTy = createAndAddDIE(dwarf::DW_TAG_base_type, *UnitDie);
1706 addString(IdxTy, dwarf::DW_AT_name, "int");
1707 addUInt(IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int32_t));
1708 addUInt(IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1709 dwarf::DW_ATE_signed);
1710 setIndexTyDie(IdxTy);
1711 }
1713 // Add subranges to array type.
1714 DIArray Elements = CTy.getTypeArray();
1715 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1716 DIDescriptor Element = Elements.getElement(i);
1717 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1718 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1719 }
1720 }
1722 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1723 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1724 DIArray Elements = CTy.getTypeArray();
1726 // Add enumerators to enumeration type.
1727 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1728 DIEnumerator Enum(Elements.getElement(i));
1729 if (Enum.isEnumerator()) {
1730 DIE *Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1731 StringRef Name = Enum.getName();
1732 addString(Enumerator, dwarf::DW_AT_name, Name);
1733 int64_t Value = Enum.getEnumValue();
1734 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1735 Value);
1736 }
1737 }
1738 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1739 if (DTy) {
1740 addType(&Buffer, DTy);
1741 addFlag(&Buffer, dwarf::DW_AT_enum_class);
1742 }
1743 }
1745 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1746 /// vtables.
1747 void DwarfUnit::constructContainingTypeDIEs() {
1748 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1749 CE = ContainingTypeMap.end();
1750 CI != CE; ++CI) {
1751 DIE *SPDie = CI->first;
1752 DIDescriptor D(CI->second);
1753 if (!D)
1754 continue;
1755 DIE *NDie = getDIE(D);
1756 if (!NDie)
1757 continue;
1758 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, NDie);
1759 }
1760 }
1762 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1763 DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
1764 StringRef Name = DV.getName();
1766 // Define variable debug information entry.
1767 DIE *VariableDie = new DIE(DV.getTag());
1768 DbgVariable *AbsVar = DV.getAbstractVariable();
1769 DIE *AbsDIE = AbsVar ? AbsVar->getDIE() : NULL;
1770 if (AbsDIE)
1771 addDIEEntry(VariableDie, dwarf::DW_AT_abstract_origin, AbsDIE);
1772 else {
1773 if (!Name.empty())
1774 addString(VariableDie, dwarf::DW_AT_name, Name);
1775 addSourceLine(VariableDie, DV.getVariable());
1776 addType(VariableDie, DV.getType());
1777 }
1779 if (DV.isArtificial())
1780 addFlag(VariableDie, dwarf::DW_AT_artificial);
1782 if (isScopeAbstract) {
1783 DV.setDIE(VariableDie);
1784 return VariableDie;
1785 }
1787 // Add variable address.
1789 unsigned Offset = DV.getDotDebugLocOffset();
1790 if (Offset != ~0U) {
1791 addSectionLabel(VariableDie, dwarf::DW_AT_location,
1792 Asm->GetTempSymbol("debug_loc", Offset));
1793 DV.setDIE(VariableDie);
1794 return VariableDie;
1795 }
1797 // Check if variable is described by a DBG_VALUE instruction.
1798 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1799 assert(DVInsn->getNumOperands() == 3);
1800 if (DVInsn->getOperand(0).isReg()) {
1801 const MachineOperand RegOp = DVInsn->getOperand(0);
1802 // If the second operand is an immediate, this is an indirect value.
1803 if (DVInsn->getOperand(1).isImm()) {
1804 MachineLocation Location(RegOp.getReg(),
1805 DVInsn->getOperand(1).getImm());
1806 addVariableAddress(DV, VariableDie, Location);
1807 } else if (RegOp.getReg())
1808 addVariableAddress(DV, VariableDie, MachineLocation(RegOp.getReg()));
1809 } else if (DVInsn->getOperand(0).isImm())
1810 addConstantValue(VariableDie, DVInsn->getOperand(0), DV.getType());
1811 else if (DVInsn->getOperand(0).isFPImm())
1812 addConstantFPValue(VariableDie, DVInsn->getOperand(0));
1813 else if (DVInsn->getOperand(0).isCImm())
1814 addConstantValue(VariableDie, DVInsn->getOperand(0).getCImm(),
1815 isUnsignedDIType(DD, DV.getType()));
1817 DV.setDIE(VariableDie);
1818 return VariableDie;
1819 } else {
1820 // .. else use frame index.
1821 int FI = DV.getFrameIndex();
1822 if (FI != ~0) {
1823 unsigned FrameReg = 0;
1824 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1825 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1826 MachineLocation Location(FrameReg, Offset);
1827 addVariableAddress(DV, VariableDie, Location);
1828 }
1829 }
1831 DV.setDIE(VariableDie);
1832 return VariableDie;
1833 }
1835 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1836 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1837 DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1838 StringRef Name = DT.getName();
1839 if (!Name.empty())
1840 addString(MemberDie, dwarf::DW_AT_name, Name);
1842 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1844 addSourceLine(MemberDie, DT);
1846 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1848 // For C++, virtual base classes are not at fixed offset. Use following
1849 // expression to extract appropriate offset from vtable.
1850 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1852 DIEBlock *VBaseLocationDie = new (DIEValueAllocator) DIEBlock();
1853 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1854 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1855 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1856 addUInt(VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1857 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1858 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1859 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1861 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1862 } else {
1863 uint64_t Size = DT.getSizeInBits();
1864 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1865 uint64_t OffsetInBytes;
1867 if (Size != FieldSize) {
1868 // Handle bitfield.
1869 addUInt(MemberDie, dwarf::DW_AT_byte_size, None,
1870 getBaseTypeSize(DD, DT) >> 3);
1871 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, DT.getSizeInBits());
1873 uint64_t Offset = DT.getOffsetInBits();
1874 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1875 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1876 uint64_t FieldOffset = (HiMark - FieldSize);
1877 Offset -= FieldOffset;
1879 // Maybe we need to work from the other end.
1880 if (Asm->getDataLayout().isLittleEndian())
1881 Offset = FieldSize - (Offset + Size);
1882 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1884 // Here WD_AT_data_member_location points to the anonymous
1885 // field that includes this bit field.
1886 OffsetInBytes = FieldOffset >> 3;
1887 } else
1888 // This is not a bitfield.
1889 OffsetInBytes = DT.getOffsetInBits() >> 3;
1891 if (DD->getDwarfVersion() <= 2) {
1892 DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
1893 addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1894 addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1895 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1896 } else
1897 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1898 OffsetInBytes);
1899 }
1901 if (DT.isProtected())
1902 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1903 dwarf::DW_ACCESS_protected);
1904 else if (DT.isPrivate())
1905 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1906 dwarf::DW_ACCESS_private);
1907 // Otherwise C++ member and base classes are considered public.
1908 else
1909 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1910 dwarf::DW_ACCESS_public);
1911 if (DT.isVirtual())
1912 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1913 dwarf::DW_VIRTUALITY_virtual);
1915 // Objective-C properties.
1916 if (MDNode *PNode = DT.getObjCProperty())
1917 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1918 MemberDie->addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1919 PropertyDie);
1921 if (DT.isArtificial())
1922 addFlag(MemberDie, dwarf::DW_AT_artificial);
1923 }
1925 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1926 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1927 if (!DT.Verify())
1928 return NULL;
1930 // Construct the context before querying for the existence of the DIE in case
1931 // such construction creates the DIE.
1932 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1933 assert(dwarf::isType(ContextDIE->getTag()) &&
1934 "Static member should belong to a type.");
1936 DIE *StaticMemberDIE = getDIE(DT);
1937 if (StaticMemberDIE)
1938 return StaticMemberDIE;
1940 StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1942 DIType Ty = resolve(DT.getTypeDerivedFrom());
1944 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1945 addType(StaticMemberDIE, Ty);
1946 addSourceLine(StaticMemberDIE, DT);
1947 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1948 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1950 // FIXME: We could omit private if the parent is a class_type, and
1951 // public if the parent is something else.
1952 if (DT.isProtected())
1953 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1954 dwarf::DW_ACCESS_protected);
1955 else if (DT.isPrivate())
1956 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1957 dwarf::DW_ACCESS_private);
1958 else
1959 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1960 dwarf::DW_ACCESS_public);
1962 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1963 addConstantValue(StaticMemberDIE, CI, isUnsignedDIType(DD, Ty));
1964 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1965 addConstantFPValue(StaticMemberDIE, CFP);
1967 return StaticMemberDIE;
1968 }
1970 void DwarfUnit::emitHeader(const MCSection *ASection,
1971 const MCSymbol *ASectionSym) const {
1972 Asm->OutStreamer.AddComment("DWARF version number");
1973 Asm->EmitInt16(DD->getDwarfVersion());
1974 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1975 // We share one abbreviations table across all units so it's always at the
1976 // start of the section. Use a relocatable offset where needed to ensure
1977 // linking doesn't invalidate that offset.
1978 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1979 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1980 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1981 }
1983 DwarfCompileUnit::~DwarfCompileUnit() {}
1984 DwarfTypeUnit::~DwarfTypeUnit() {}
1986 void DwarfTypeUnit::emitHeader(const MCSection *ASection,
1987 const MCSymbol *ASectionSym) const {
1988 DwarfUnit::emitHeader(ASection, ASectionSym);
1989 Asm->OutStreamer.AddComment("Type Signature");
1990 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
1991 Asm->OutStreamer.AddComment("Type DIE Offset");
1992 // In a skeleton type unit there is no type DIE so emit a zero offset.
1993 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
1994 sizeof(Ty->getOffset()));
1995 }
1997 void DwarfTypeUnit::initSection(const MCSection *Section) {
1998 assert(!this->Section);
1999 this->Section = Section;
2000 // Since each type unit is contained in its own COMDAT section, the begin
2001 // label and the section label are the same. Using the begin label emission in
2002 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2003 // the only other alternative of lazily constructing start-of-section labels
2004 // and storing a mapping in DwarfDebug (or AsmPrinter).
2005 this->SectionSym = this->LabelBegin =
2006 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2007 this->LabelEnd =
2008 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2009 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
2010 }