1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DwarfUnit.h"
17 #include "DwarfAccelTable.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/IR/Constants.h"
21 #include "llvm/IR/DIBuilder.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCContext.h"
28 #include "llvm/MC/MCSection.h"
29 #include "llvm/MC/MCStreamer.h"
30 #include "llvm/Support/CommandLine.h"
31 #include "llvm/Target/TargetFrameLowering.h"
32 #include "llvm/Target/TargetLoweringObjectFile.h"
33 #include "llvm/Target/TargetMachine.h"
34 #include "llvm/Target/TargetRegisterInfo.h"
36 using namespace llvm;
38 static cl::opt<bool>
39 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
40 cl::desc("Generate DWARF4 type units."),
41 cl::init(false));
43 /// Unit - Unit constructor.
44 DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
45 DwarfDebug *DW, DwarfFile *DWU)
46 : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
47 DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
48 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
49 }
51 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
52 AsmPrinter *A, DwarfDebug *DW,
53 DwarfFile *DWU)
54 : DwarfUnit(UID, D, Node, A, DW, DWU) {
55 insertDIE(Node, D);
56 }
58 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DwarfCompileUnit &CU,
59 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
60 : DwarfUnit(UID, D, CU.getCUNode(), A, DW, DWU), CU(CU) {}
62 /// ~Unit - Destructor for compile unit.
63 DwarfUnit::~DwarfUnit() {
64 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
65 DIEBlocks[j]->~DIEBlock();
66 for (unsigned j = 0, M = DIELocs.size(); j < M; ++j)
67 DIELocs[j]->~DIELoc();
68 }
70 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
71 /// information entry.
72 DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
73 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
74 return Value;
75 }
77 /// getDefaultLowerBound - Return the default lower bound for an array. If the
78 /// DWARF version doesn't handle the language, return -1.
79 int64_t DwarfUnit::getDefaultLowerBound() const {
80 switch (getLanguage()) {
81 default:
82 break;
84 case dwarf::DW_LANG_C89:
85 case dwarf::DW_LANG_C99:
86 case dwarf::DW_LANG_C:
87 case dwarf::DW_LANG_C_plus_plus:
88 case dwarf::DW_LANG_ObjC:
89 case dwarf::DW_LANG_ObjC_plus_plus:
90 return 0;
92 case dwarf::DW_LANG_Fortran77:
93 case dwarf::DW_LANG_Fortran90:
94 case dwarf::DW_LANG_Fortran95:
95 return 1;
97 // The languages below have valid values only if the DWARF version >= 4.
98 case dwarf::DW_LANG_Java:
99 case dwarf::DW_LANG_Python:
100 case dwarf::DW_LANG_UPC:
101 case dwarf::DW_LANG_D:
102 if (dwarf::DWARF_VERSION >= 4)
103 return 0;
104 break;
106 case dwarf::DW_LANG_Ada83:
107 case dwarf::DW_LANG_Ada95:
108 case dwarf::DW_LANG_Cobol74:
109 case dwarf::DW_LANG_Cobol85:
110 case dwarf::DW_LANG_Modula2:
111 case dwarf::DW_LANG_Pascal83:
112 case dwarf::DW_LANG_PLI:
113 if (dwarf::DWARF_VERSION >= 4)
114 return 1;
115 break;
116 }
118 return -1;
119 }
121 /// Check whether the DIE for this MDNode can be shared across CUs.
122 static bool isShareableAcrossCUs(DIDescriptor D) {
123 // When the MDNode can be part of the type system, the DIE can be shared
124 // across CUs.
125 // Combining type units and cross-CU DIE sharing is lower value (since
126 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
127 // level already) but may be implementable for some value in projects
128 // building multiple independent libraries with LTO and then linking those
129 // together.
130 return (D.isType() ||
131 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
132 !GenerateDwarfTypeUnits;
133 }
135 /// getDIE - Returns the debug information entry map slot for the
136 /// specified debug variable. We delegate the request to DwarfDebug
137 /// when the DIE for this MDNode can be shared across CUs. The mappings
138 /// will be kept in DwarfDebug for shareable DIEs.
139 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
140 if (isShareableAcrossCUs(D))
141 return DD->getDIE(D);
142 return MDNodeToDieMap.lookup(D);
143 }
145 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
146 /// when the DIE for this MDNode can be shared across CUs. The mappings
147 /// will be kept in DwarfDebug for shareable DIEs.
148 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
149 if (isShareableAcrossCUs(Desc)) {
150 DD->insertDIE(Desc, D);
151 return;
152 }
153 MDNodeToDieMap.insert(std::make_pair(Desc, D));
154 }
156 /// addFlag - Add a flag that is true.
157 void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
158 if (DD->getDwarfVersion() >= 4)
159 Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
160 else
161 Die->addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
162 }
164 /// addUInt - Add an unsigned integer attribute data and value.
165 ///
166 void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
167 Optional<dwarf::Form> Form, uint64_t Integer) {
168 if (!Form)
169 Form = DIEInteger::BestForm(false, Integer);
170 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
171 DIEInteger(Integer);
172 Die->addValue(Attribute, *Form, Value);
173 }
175 void DwarfUnit::addUInt(DIE *Block, dwarf::Form Form, uint64_t Integer) {
176 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
177 }
179 /// addSInt - Add an signed integer attribute data and value.
180 ///
181 void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
182 Optional<dwarf::Form> Form, int64_t Integer) {
183 if (!Form)
184 Form = DIEInteger::BestForm(true, Integer);
185 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
186 Die->addValue(Attribute, *Form, Value);
187 }
189 void DwarfUnit::addSInt(DIELoc *Die, Optional<dwarf::Form> Form,
190 int64_t Integer) {
191 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
192 }
194 /// addString - Add a string attribute data and value. We always emit a
195 /// reference to the string pool instead of immediate strings so that DIEs have
196 /// more predictable sizes. In the case of split dwarf we emit an index
197 /// into another table which gets us the static offset into the string
198 /// table.
199 void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
200 StringRef String) {
202 if (!DD->useSplitDwarf())
203 return addLocalString(Die, Attribute, String);
205 unsigned idx = DU->getStringPoolIndex(String);
206 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
207 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
208 Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
209 }
211 /// addLocalString - Add a string attribute data and value. This is guaranteed
212 /// to be in the local string pool instead of indirected.
213 void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
214 StringRef String) {
215 MCSymbol *Symb = DU->getStringPoolEntry(String);
216 DIEValue *Value;
217 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
218 Value = new (DIEValueAllocator) DIELabel(Symb);
219 else {
220 MCSymbol *StringPool = DU->getStringPoolSym();
221 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
222 }
223 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
224 Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
225 }
227 /// addExpr - Add a Dwarf expression attribute data and value.
228 ///
229 void DwarfUnit::addExpr(DIELoc *Die, dwarf::Form Form, const MCExpr *Expr) {
230 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
231 Die->addValue((dwarf::Attribute)0, Form, Value);
232 }
234 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
235 ///
236 void DwarfUnit::addLocationList(DIE *Die, dwarf::Attribute Attribute,
237 unsigned Index) {
238 DIEValue *Value = new (DIEValueAllocator) DIELocList(Index);
239 dwarf::Form Form = DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
240 : dwarf::DW_FORM_data4;
241 Die->addValue(Attribute, Form, Value);
242 }
244 /// addLabel - Add a Dwarf label attribute data and value.
245 ///
246 void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
247 const MCSymbol *Label) {
248 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
249 Die->addValue(Attribute, Form, Value);
250 }
252 void DwarfUnit::addLabel(DIELoc *Die, dwarf::Form Form, const MCSymbol *Label) {
253 addLabel(Die, (dwarf::Attribute)0, Form, Label);
254 }
256 /// addSectionLabel - Add a Dwarf section label attribute data and value.
257 ///
258 void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
259 const MCSymbol *Label) {
260 if (DD->getDwarfVersion() >= 4)
261 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
262 else
263 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
264 }
266 /// addSectionOffset - Add an offset into a section attribute data and value.
267 ///
268 void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
269 uint64_t Integer) {
270 if (DD->getDwarfVersion() >= 4)
271 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
272 else
273 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
274 }
276 /// addLabelAddress - Add a dwarf label attribute data and value using
277 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
278 ///
279 void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
280 MCSymbol *Label) {
281 if (Label)
282 DD->addArangeLabel(SymbolCU(this, Label));
284 if (!DD->useSplitDwarf()) {
285 if (Label) {
286 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
287 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
288 } else {
289 DIEValue *Value = new (DIEValueAllocator) DIEInteger(0);
290 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
291 }
292 } else {
293 unsigned idx = DU->getAddrPoolIndex(Label);
294 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
295 Die->addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
296 }
297 }
299 /// addOpAddress - Add a dwarf op address data and value using the
300 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
301 ///
302 void DwarfUnit::addOpAddress(DIELoc *Die, const MCSymbol *Sym) {
303 if (!DD->useSplitDwarf()) {
304 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
305 addLabel(Die, dwarf::DW_FORM_udata, Sym);
306 } else {
307 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
308 addUInt(Die, dwarf::DW_FORM_GNU_addr_index, DU->getAddrPoolIndex(Sym));
309 }
310 }
312 /// addSectionDelta - Add a section label delta attribute data and value.
313 ///
314 void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
315 const MCSymbol *Hi, const MCSymbol *Lo) {
316 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
317 if (DD->getDwarfVersion() >= 4)
318 Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
319 else
320 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
321 }
323 void DwarfUnit::addLabelDelta(DIE *Die, dwarf::Attribute Attribute,
324 const MCSymbol *Hi, const MCSymbol *Lo) {
325 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
326 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
327 }
329 /// addDIEEntry - Add a DIE attribute data and value.
330 ///
331 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
332 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
333 }
335 void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
336 Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
337 new (DIEValueAllocator) DIETypeSignature(Type));
338 }
340 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
341 DIEEntry *Entry) {
342 const DIE *DieCU = Die->getUnitOrNull();
343 const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
344 if (!DieCU)
345 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
346 DieCU = getUnitDie();
347 if (!EntryCU)
348 EntryCU = getUnitDie();
349 Die->addValue(Attribute, EntryCU == DieCU ? dwarf::DW_FORM_ref4
350 : dwarf::DW_FORM_ref_addr,
351 Entry);
352 }
354 /// Create a DIE with the given Tag, add the DIE to its parent, and
355 /// call insertDIE if MD is not null.
356 DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
357 DIE *Die = new DIE(Tag);
358 Parent.addChild(Die);
359 if (N)
360 insertDIE(N, Die);
361 return Die;
362 }
364 /// addBlock - Add block data.
365 ///
366 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIELoc *Loc) {
367 Loc->ComputeSize(Asm);
368 DIELocs.push_back(Loc); // Memoize so we can call the destructor later on.
369 Die->addValue(Attribute, Loc->BestForm(DD->getDwarfVersion()), Loc);
370 }
372 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
373 DIEBlock *Block) {
374 Block->ComputeSize(Asm);
375 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
376 Die->addValue(Attribute, Block->BestForm(), Block);
377 }
379 /// addSourceLine - Add location information to specified debug information
380 /// entry.
381 void DwarfUnit::addSourceLine(DIE *Die, unsigned Line, StringRef File,
382 StringRef Directory) {
383 if (Line == 0)
384 return;
386 unsigned FileID =
387 DD->getOrCreateSourceID(File, Directory, getCU().getUniqueID());
388 assert(FileID && "Invalid file id");
389 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
390 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
391 }
393 /// addSourceLine - Add location information to specified debug information
394 /// entry.
395 void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
396 assert(V.isVariable());
398 addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
399 V.getContext().getDirectory());
400 }
402 /// addSourceLine - Add location information to specified debug information
403 /// entry.
404 void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
405 assert(G.isGlobalVariable());
407 addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
408 }
410 /// addSourceLine - Add location information to specified debug information
411 /// entry.
412 void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
413 assert(SP.isSubprogram());
415 addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
416 }
418 /// addSourceLine - Add location information to specified debug information
419 /// entry.
420 void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
421 assert(Ty.isType());
423 addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
424 }
426 /// addSourceLine - Add location information to specified debug information
427 /// entry.
428 void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
429 assert(Ty.isObjCProperty());
431 DIFile File = Ty.getFile();
432 addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
433 File.getDirectory());
434 }
436 /// addSourceLine - Add location information to specified debug information
437 /// entry.
438 void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
439 assert(NS.Verify());
441 addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
442 }
444 /// addVariableAddress - Add DW_AT_location attribute for a
445 /// DbgVariable based on provided MachineLocation.
446 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
447 MachineLocation Location) {
448 if (DV.variableHasComplexAddress())
449 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
450 else if (DV.isBlockByrefVariable())
451 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
452 else
453 addAddress(Die, dwarf::DW_AT_location, Location,
454 DV.getVariable().isIndirect());
455 }
457 /// addRegisterOp - Add register operand.
458 void DwarfUnit::addRegisterOp(DIELoc *TheDie, unsigned Reg) {
459 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
460 int DWReg = RI->getDwarfRegNum(Reg, false);
461 bool isSubRegister = DWReg < 0;
463 unsigned Idx = 0;
465 // Go up the super-register chain until we hit a valid dwarf register number.
466 for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
467 DWReg = RI->getDwarfRegNum(*SR, false);
468 if (DWReg >= 0)
469 Idx = RI->getSubRegIndex(*SR, Reg);
470 }
472 if (DWReg < 0) {
473 DEBUG(dbgs() << "Invalid Dwarf register number.\n");
474 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
475 return;
476 }
478 // Emit register
479 if (DWReg < 32)
480 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
481 else {
482 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
483 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
484 }
486 // Emit Mask
487 if (isSubRegister) {
488 unsigned Size = RI->getSubRegIdxSize(Idx);
489 unsigned Offset = RI->getSubRegIdxOffset(Idx);
490 if (Offset > 0) {
491 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
492 addUInt(TheDie, dwarf::DW_FORM_data1, Size);
493 addUInt(TheDie, dwarf::DW_FORM_data1, Offset);
494 } else {
495 unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
496 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
497 addUInt(TheDie, dwarf::DW_FORM_data1, ByteSize);
498 }
499 }
500 }
502 /// addRegisterOffset - Add register offset.
503 void DwarfUnit::addRegisterOffset(DIELoc *TheDie, unsigned Reg,
504 int64_t Offset) {
505 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
506 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
507 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
508 if (Reg == TRI->getFrameRegister(*Asm->MF))
509 // If variable offset is based in frame register then use fbreg.
510 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
511 else if (DWReg < 32)
512 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
513 else {
514 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
515 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
516 }
517 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
518 }
520 /// addAddress - Add an address attribute to a die based on the location
521 /// provided.
522 void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
523 const MachineLocation &Location, bool Indirect) {
524 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
526 if (Location.isReg() && !Indirect)
527 addRegisterOp(Loc, Location.getReg());
528 else {
529 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
530 if (Indirect && !Location.isReg()) {
531 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
532 }
533 }
535 // Now attach the location information to the DIE.
536 addBlock(Die, Attribute, Loc);
537 }
539 /// addComplexAddress - Start with the address based on the location provided,
540 /// and generate the DWARF information necessary to find the actual variable
541 /// given the extra address information encoded in the DbgVariable, starting
542 /// from the starting location. Add the DWARF information to the die.
543 ///
544 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
545 dwarf::Attribute Attribute,
546 const MachineLocation &Location) {
547 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
548 unsigned N = DV.getNumAddrElements();
549 unsigned i = 0;
550 if (Location.isReg()) {
551 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
552 // If first address element is OpPlus then emit
553 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
554 addRegisterOffset(Loc, Location.getReg(), DV.getAddrElement(1));
555 i = 2;
556 } else
557 addRegisterOp(Loc, Location.getReg());
558 } else
559 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
561 for (; i < N; ++i) {
562 uint64_t Element = DV.getAddrElement(i);
563 if (Element == DIBuilder::OpPlus) {
564 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
565 addUInt(Loc, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
566 } else if (Element == DIBuilder::OpDeref) {
567 if (!Location.isReg())
568 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
569 } else
570 llvm_unreachable("unknown DIBuilder Opcode");
571 }
573 // Now attach the location information to the DIE.
574 addBlock(Die, Attribute, Loc);
575 }
577 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
578 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
579 gives the variable VarName either the struct, or a pointer to the struct, as
580 its type. This is necessary for various behind-the-scenes things the
581 compiler needs to do with by-reference variables in Blocks.
583 However, as far as the original *programmer* is concerned, the variable
584 should still have type 'SomeType', as originally declared.
586 The function getBlockByrefType dives into the __Block_byref_x_VarName
587 struct to find the original type of the variable, which is then assigned to
588 the variable's Debug Information Entry as its real type. So far, so good.
589 However now the debugger will expect the variable VarName to have the type
590 SomeType. So we need the location attribute for the variable to be an
591 expression that explains to the debugger how to navigate through the
592 pointers and struct to find the actual variable of type SomeType.
594 The following function does just that. We start by getting
595 the "normal" location for the variable. This will be the location
596 of either the struct __Block_byref_x_VarName or the pointer to the
597 struct __Block_byref_x_VarName.
599 The struct will look something like:
601 struct __Block_byref_x_VarName {
602 ... <various fields>
603 struct __Block_byref_x_VarName *forwarding;
604 ... <various other fields>
605 SomeType VarName;
606 ... <maybe more fields>
607 };
609 If we are given the struct directly (as our starting point) we
610 need to tell the debugger to:
612 1). Add the offset of the forwarding field.
614 2). Follow that pointer to get the real __Block_byref_x_VarName
615 struct to use (the real one may have been copied onto the heap).
617 3). Add the offset for the field VarName, to find the actual variable.
619 If we started with a pointer to the struct, then we need to
620 dereference that pointer first, before the other steps.
621 Translating this into DWARF ops, we will need to append the following
622 to the current location description for the variable:
624 DW_OP_deref -- optional, if we start with a pointer
625 DW_OP_plus_uconst <forward_fld_offset>
626 DW_OP_deref
627 DW_OP_plus_uconst <varName_fld_offset>
629 That is what this function does. */
631 /// addBlockByrefAddress - Start with the address based on the location
632 /// provided, and generate the DWARF information necessary to find the
633 /// actual Block variable (navigating the Block struct) based on the
634 /// starting location. Add the DWARF information to the die. For
635 /// more information, read large comment just above here.
636 ///
637 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
638 dwarf::Attribute Attribute,
639 const MachineLocation &Location) {
640 DIType Ty = DV.getType();
641 DIType TmpTy = Ty;
642 uint16_t Tag = Ty.getTag();
643 bool isPointer = false;
645 StringRef varName = DV.getName();
647 if (Tag == dwarf::DW_TAG_pointer_type) {
648 DIDerivedType DTy(Ty);
649 TmpTy = resolve(DTy.getTypeDerivedFrom());
650 isPointer = true;
651 }
653 DICompositeType blockStruct(TmpTy);
655 // Find the __forwarding field and the variable field in the __Block_byref
656 // struct.
657 DIArray Fields = blockStruct.getTypeArray();
658 DIDerivedType varField;
659 DIDerivedType forwardingField;
661 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
662 DIDerivedType DT(Fields.getElement(i));
663 StringRef fieldName = DT.getName();
664 if (fieldName == "__forwarding")
665 forwardingField = DT;
666 else if (fieldName == varName)
667 varField = DT;
668 }
670 // Get the offsets for the forwarding field and the variable field.
671 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
672 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
674 // Decode the original location, and use that as the start of the byref
675 // variable's location.
676 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
678 if (Location.isReg())
679 addRegisterOp(Loc, Location.getReg());
680 else
681 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
683 // If we started with a pointer to the __Block_byref... struct, then
684 // the first thing we need to do is dereference the pointer (DW_OP_deref).
685 if (isPointer)
686 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
688 // Next add the offset for the '__forwarding' field:
689 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
690 // adding the offset if it's 0.
691 if (forwardingFieldOffset > 0) {
692 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
693 addUInt(Loc, dwarf::DW_FORM_udata, forwardingFieldOffset);
694 }
696 // Now dereference the __forwarding field to get to the real __Block_byref
697 // struct: DW_OP_deref.
698 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
700 // Now that we've got the real __Block_byref... struct, add the offset
701 // for the variable's field to get to the location of the actual variable:
702 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
703 if (varFieldOffset > 0) {
704 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
705 addUInt(Loc, dwarf::DW_FORM_udata, varFieldOffset);
706 }
708 // Now attach the location information to the DIE.
709 addBlock(Die, Attribute, Loc);
710 }
712 /// isTypeSigned - Return true if the type is signed.
713 static bool isTypeSigned(DwarfDebug *DD, DIType Ty, int *SizeInBits) {
714 if (Ty.isDerivedType())
715 return isTypeSigned(DD, DD->resolve(DIDerivedType(Ty).getTypeDerivedFrom()),
716 SizeInBits);
717 if (Ty.isBasicType())
718 if (DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed ||
719 DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed_char) {
720 *SizeInBits = Ty.getSizeInBits();
721 return true;
722 }
723 return false;
724 }
726 /// Return true if type encoding is unsigned.
727 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
728 DIDerivedType DTy(Ty);
729 if (DTy.isDerivedType())
730 return isUnsignedDIType(DD, DD->resolve(DTy.getTypeDerivedFrom()));
732 DIBasicType BTy(Ty);
733 if (BTy.isBasicType()) {
734 unsigned Encoding = BTy.getEncoding();
735 if (Encoding == dwarf::DW_ATE_unsigned ||
736 Encoding == dwarf::DW_ATE_unsigned_char ||
737 Encoding == dwarf::DW_ATE_boolean)
738 return true;
739 }
740 return false;
741 }
743 /// If this type is derived from a base type then return base type size.
744 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
745 unsigned Tag = Ty.getTag();
747 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
748 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
749 Tag != dwarf::DW_TAG_restrict_type)
750 return Ty.getSizeInBits();
752 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
754 // If this type is not derived from any type or the type is a declaration then
755 // take conservative approach.
756 if (!BaseType.isValid() || BaseType.isForwardDecl())
757 return Ty.getSizeInBits();
759 // If this is a derived type, go ahead and get the base type, unless it's a
760 // reference then it's just the size of the field. Pointer types have no need
761 // of this since they're a different type of qualification on the type.
762 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
763 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
764 return Ty.getSizeInBits();
766 if (BaseType.isDerivedType())
767 return getBaseTypeSize(DD, DIDerivedType(BaseType));
769 return BaseType.getSizeInBits();
770 }
772 /// addConstantValue - Add constant value entry in variable DIE.
773 void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
774 DIType Ty) {
775 // FIXME: This is a bit conservative/simple - it emits negative values at
776 // their maximum bit width which is a bit unfortunate (& doesn't prefer
777 // udata/sdata over dataN as suggested by the DWARF spec)
778 assert(MO.isImm() && "Invalid machine operand!");
779 int SizeInBits = -1;
780 bool SignedConstant = isTypeSigned(DD, Ty, &SizeInBits);
781 dwarf::Form Form;
783 // If we're a signed constant definitely use sdata.
784 if (SignedConstant) {
785 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata, MO.getImm());
786 return;
787 }
789 // Else use data for now unless it's larger than we can deal with.
790 switch (SizeInBits) {
791 case 8:
792 Form = dwarf::DW_FORM_data1;
793 break;
794 case 16:
795 Form = dwarf::DW_FORM_data2;
796 break;
797 case 32:
798 Form = dwarf::DW_FORM_data4;
799 break;
800 case 64:
801 Form = dwarf::DW_FORM_data8;
802 break;
803 default:
804 Form = dwarf::DW_FORM_udata;
805 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
806 return;
807 }
808 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
809 }
811 /// addConstantFPValue - Add constant value entry in variable DIE.
812 void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
813 assert(MO.isFPImm() && "Invalid machine operand!");
814 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
815 APFloat FPImm = MO.getFPImm()->getValueAPF();
817 // Get the raw data form of the floating point.
818 const APInt FltVal = FPImm.bitcastToAPInt();
819 const char *FltPtr = (const char *)FltVal.getRawData();
821 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
822 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
823 int Incr = (LittleEndian ? 1 : -1);
824 int Start = (LittleEndian ? 0 : NumBytes - 1);
825 int Stop = (LittleEndian ? NumBytes : -1);
827 // Output the constant to DWARF one byte at a time.
828 for (; Start != Stop; Start += Incr)
829 addUInt(Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
831 addBlock(Die, dwarf::DW_AT_const_value, Block);
832 }
834 /// addConstantFPValue - Add constant value entry in variable DIE.
835 void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
836 // Pass this down to addConstantValue as an unsigned bag of bits.
837 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
838 }
840 /// addConstantValue - Add constant value entry in variable DIE.
841 void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
842 bool Unsigned) {
843 addConstantValue(Die, CI->getValue(), Unsigned);
844 }
846 // addConstantValue - Add constant value entry in variable DIE.
847 void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
848 unsigned CIBitWidth = Val.getBitWidth();
849 if (CIBitWidth <= 64) {
850 // If we're a signed constant definitely use sdata.
851 if (!Unsigned) {
852 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
853 Val.getSExtValue());
854 return;
855 }
857 // Else use data for now unless it's larger than we can deal with.
858 dwarf::Form Form;
859 switch (CIBitWidth) {
860 case 8:
861 Form = dwarf::DW_FORM_data1;
862 break;
863 case 16:
864 Form = dwarf::DW_FORM_data2;
865 break;
866 case 32:
867 Form = dwarf::DW_FORM_data4;
868 break;
869 case 64:
870 Form = dwarf::DW_FORM_data8;
871 break;
872 default:
873 addUInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_udata,
874 Val.getZExtValue());
875 return;
876 }
877 addUInt(Die, dwarf::DW_AT_const_value, Form, Val.getZExtValue());
878 return;
879 }
881 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
883 // Get the raw data form of the large APInt.
884 const uint64_t *Ptr64 = Val.getRawData();
886 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
887 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
889 // Output the constant to DWARF one byte at a time.
890 for (int i = 0; i < NumBytes; i++) {
891 uint8_t c;
892 if (LittleEndian)
893 c = Ptr64[i / 8] >> (8 * (i & 7));
894 else
895 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
896 addUInt(Block, dwarf::DW_FORM_data1, c);
897 }
899 addBlock(Die, dwarf::DW_AT_const_value, Block);
900 }
902 /// addTemplateParams - Add template parameters into buffer.
903 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
904 // Add template parameters.
905 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
906 DIDescriptor Element = TParams.getElement(i);
907 if (Element.isTemplateTypeParameter())
908 constructTemplateTypeParameterDIE(Buffer,
909 DITemplateTypeParameter(Element));
910 else if (Element.isTemplateValueParameter())
911 constructTemplateValueParameterDIE(Buffer,
912 DITemplateValueParameter(Element));
913 }
914 }
916 /// getOrCreateContextDIE - Get context owner's DIE.
917 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
918 if (!Context || Context.isFile())
919 return getUnitDie();
920 if (Context.isType())
921 return getOrCreateTypeDIE(DIType(Context));
922 if (Context.isNameSpace())
923 return getOrCreateNameSpace(DINameSpace(Context));
924 if (Context.isSubprogram())
925 return getOrCreateSubprogramDIE(DISubprogram(Context));
926 return getDIE(Context);
927 }
929 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
930 DIScope Context = resolve(Ty.getContext());
931 DIE *ContextDIE = getOrCreateContextDIE(Context);
933 DIE *TyDIE = getDIE(Ty);
934 if (TyDIE)
935 return TyDIE;
937 // Create new type.
938 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
940 constructTypeDIE(*TyDIE, Ty);
942 updateAcceleratorTables(Context, Ty, TyDIE);
943 return TyDIE;
944 }
946 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
947 /// given DIType.
948 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
949 if (!TyNode)
950 return NULL;
952 DIType Ty(TyNode);
953 assert(Ty.isType());
955 // Construct the context before querying for the existence of the DIE in case
956 // such construction creates the DIE.
957 DIScope Context = resolve(Ty.getContext());
958 DIE *ContextDIE = getOrCreateContextDIE(Context);
959 assert(ContextDIE);
961 DIE *TyDIE = getDIE(Ty);
962 if (TyDIE)
963 return TyDIE;
965 // Create new type.
966 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
968 updateAcceleratorTables(Context, Ty, TyDIE);
970 if (Ty.isBasicType())
971 constructTypeDIE(*TyDIE, DIBasicType(Ty));
972 else if (Ty.isCompositeType()) {
973 DICompositeType CTy(Ty);
974 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
975 if (MDString *TypeId = CTy.getIdentifier()) {
976 DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
977 // Skip updating the accelerator tables since this is not the full type.
978 return TyDIE;
979 }
980 constructTypeDIE(*TyDIE, CTy);
981 } else {
982 assert(Ty.isDerivedType() && "Unknown kind of DIType");
983 constructTypeDIE(*TyDIE, DIDerivedType(Ty));
984 }
986 return TyDIE;
987 }
989 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
990 const DIE *TyDIE) {
991 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
992 bool IsImplementation = 0;
993 if (Ty.isCompositeType()) {
994 DICompositeType CT(Ty);
995 // A runtime language of 0 actually means C/C++ and that any
996 // non-negative value is some version of Objective-C/C++.
997 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
998 }
999 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
1000 addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
1002 if ((!Context || Context.isCompileUnit() || Context.isFile() ||
1003 Context.isNameSpace()) &&
1004 getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
1005 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
1006 }
1007 }
1009 /// addType - Add a new type attribute to the specified entity.
1010 void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
1011 assert(Ty && "Trying to add a type that doesn't exist?");
1013 // Check for pre-existence.
1014 DIEEntry *Entry = getDIEEntry(Ty);
1015 // If it exists then use the existing value.
1016 if (Entry) {
1017 addDIEEntry(Entity, Attribute, Entry);
1018 return;
1019 }
1021 // Construct type.
1022 DIE *Buffer = getOrCreateTypeDIE(Ty);
1024 // Set up proxy.
1025 Entry = createDIEEntry(Buffer);
1026 insertDIEEntry(Ty, Entry);
1027 addDIEEntry(Entity, Attribute, Entry);
1028 }
1030 // Accelerator table mutators - add each name along with its companion
1031 // DIE to the proper table while ensuring that the name that we're going
1032 // to reference is in the string table. We do this since the names we
1033 // add may not only be identical to the names in the DIE.
1034 void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
1035 if (!DD->useDwarfAccelTables())
1036 return;
1037 DU->getStringPoolEntry(Name);
1038 std::vector<const DIE *> &DIEs = AccelNames[Name];
1039 DIEs.push_back(Die);
1040 }
1042 void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
1043 if (!DD->useDwarfAccelTables())
1044 return;
1045 DU->getStringPoolEntry(Name);
1046 std::vector<const DIE *> &DIEs = AccelObjC[Name];
1047 DIEs.push_back(Die);
1048 }
1050 void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
1051 if (!DD->useDwarfAccelTables())
1052 return;
1053 DU->getStringPoolEntry(Name);
1054 std::vector<const DIE *> &DIEs = AccelNamespace[Name];
1055 DIEs.push_back(Die);
1056 }
1058 void DwarfUnit::addAccelType(StringRef Name,
1059 std::pair<const DIE *, unsigned> Die) {
1060 if (!DD->useDwarfAccelTables())
1061 return;
1062 DU->getStringPoolEntry(Name);
1063 std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
1064 DIEs.push_back(Die);
1065 }
1067 /// addGlobalName - Add a new global name to the compile unit.
1068 void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
1069 if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
1070 return;
1071 std::string FullName = getParentContextString(Context) + Name.str();
1072 GlobalNames[FullName] = Die;
1073 }
1075 /// getParentContextString - Walks the metadata parent chain in a language
1076 /// specific manner (using the compile unit language) and returns
1077 /// it as a string. This is done at the metadata level because DIEs may
1078 /// not currently have been added to the parent context and walking the
1079 /// DIEs looking for names is more expensive than walking the metadata.
1080 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1081 if (!Context)
1082 return "";
1084 // FIXME: Decide whether to implement this for non-C++ languages.
1085 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1086 return "";
1088 std::string CS;
1089 SmallVector<DIScope, 1> Parents;
1090 while (!Context.isCompileUnit()) {
1091 Parents.push_back(Context);
1092 if (Context.getContext())
1093 Context = resolve(Context.getContext());
1094 else
1095 // Structure, etc types will have a NULL context if they're at the top
1096 // level.
1097 break;
1098 }
1100 // Reverse iterate over our list to go from the outermost construct to the
1101 // innermost.
1102 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1103 E = Parents.rend();
1104 I != E; ++I) {
1105 DIScope Ctx = *I;
1106 StringRef Name = Ctx.getName();
1107 if (!Name.empty()) {
1108 CS += Name;
1109 CS += "::";
1110 }
1111 }
1112 return CS;
1113 }
1115 /// constructTypeDIE - Construct basic type die from DIBasicType.
1116 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1117 // Get core information.
1118 StringRef Name = BTy.getName();
1119 // Add name if not anonymous or intermediate type.
1120 if (!Name.empty())
1121 addString(&Buffer, dwarf::DW_AT_name, Name);
1123 // An unspecified type only has a name attribute.
1124 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1125 return;
1127 addUInt(&Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1128 BTy.getEncoding());
1130 uint64_t Size = BTy.getSizeInBits() >> 3;
1131 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1132 }
1134 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1135 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1136 // Get core information.
1137 StringRef Name = DTy.getName();
1138 uint64_t Size = DTy.getSizeInBits() >> 3;
1139 uint16_t Tag = Buffer.getTag();
1141 // Map to main type, void will not have a type.
1142 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1143 if (FromTy)
1144 addType(&Buffer, FromTy);
1146 // Add name if not anonymous or intermediate type.
1147 if (!Name.empty())
1148 addString(&Buffer, dwarf::DW_AT_name, Name);
1150 // Add size if non-zero (derived types might be zero-sized.)
1151 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1152 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1154 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1155 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1156 getOrCreateTypeDIE(resolve(DTy.getClassType())));
1157 // Add source line info if available and TyDesc is not a forward declaration.
1158 if (!DTy.isForwardDecl())
1159 addSourceLine(&Buffer, DTy);
1160 }
1162 /// constructSubprogramArguments - Construct function argument DIEs.
1163 void DwarfUnit::constructSubprogramArguments(DIE &Buffer, DIArray Args) {
1164 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1165 DIDescriptor Ty = Args.getElement(i);
1166 if (Ty.isUnspecifiedParameter()) {
1167 assert(i == N-1 && "Unspecified parameter must be the last argument");
1168 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1169 } else {
1170 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1171 addType(Arg, DIType(Ty));
1172 if (DIType(Ty).isArtificial())
1173 addFlag(Arg, dwarf::DW_AT_artificial);
1174 }
1175 }
1176 }
1178 /// constructTypeDIE - Construct type DIE from DICompositeType.
1179 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1180 // Add name if not anonymous or intermediate type.
1181 StringRef Name = CTy.getName();
1183 uint64_t Size = CTy.getSizeInBits() >> 3;
1184 uint16_t Tag = Buffer.getTag();
1186 switch (Tag) {
1187 case dwarf::DW_TAG_array_type:
1188 constructArrayTypeDIE(Buffer, CTy);
1189 break;
1190 case dwarf::DW_TAG_enumeration_type:
1191 constructEnumTypeDIE(Buffer, CTy);
1192 break;
1193 case dwarf::DW_TAG_subroutine_type: {
1194 // Add return type. A void return won't have a type.
1195 DIArray Elements = CTy.getTypeArray();
1196 DIType RTy(Elements.getElement(0));
1197 if (RTy)
1198 addType(&Buffer, RTy);
1200 bool isPrototyped = true;
1201 if (Elements.getNumElements() == 2 &&
1202 Elements.getElement(1).isUnspecifiedParameter())
1203 isPrototyped = false;
1205 constructSubprogramArguments(Buffer, Elements);
1207 // Add prototype flag if we're dealing with a C language and the
1208 // function has been prototyped.
1209 uint16_t Language = getLanguage();
1210 if (isPrototyped &&
1211 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1212 Language == dwarf::DW_LANG_ObjC))
1213 addFlag(&Buffer, dwarf::DW_AT_prototyped);
1215 if (CTy.isLValueReference())
1216 addFlag(&Buffer, dwarf::DW_AT_reference);
1218 if (CTy.isRValueReference())
1219 addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
1220 } break;
1221 case dwarf::DW_TAG_structure_type:
1222 case dwarf::DW_TAG_union_type:
1223 case dwarf::DW_TAG_class_type: {
1224 // Add elements to structure type.
1225 DIArray Elements = CTy.getTypeArray();
1226 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1227 DIDescriptor Element = Elements.getElement(i);
1228 DIE *ElemDie = NULL;
1229 if (Element.isSubprogram())
1230 ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
1231 else if (Element.isDerivedType()) {
1232 DIDerivedType DDTy(Element);
1233 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1234 ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1235 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1236 dwarf::DW_AT_friend);
1237 } else if (DDTy.isStaticMember()) {
1238 getOrCreateStaticMemberDIE(DDTy);
1239 } else {
1240 constructMemberDIE(Buffer, DDTy);
1241 }
1242 } else if (Element.isObjCProperty()) {
1243 DIObjCProperty Property(Element);
1244 ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1245 StringRef PropertyName = Property.getObjCPropertyName();
1246 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1247 if (Property.getType())
1248 addType(ElemDie, Property.getType());
1249 addSourceLine(ElemDie, Property);
1250 StringRef GetterName = Property.getObjCPropertyGetterName();
1251 if (!GetterName.empty())
1252 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1253 StringRef SetterName = Property.getObjCPropertySetterName();
1254 if (!SetterName.empty())
1255 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1256 unsigned PropertyAttributes = 0;
1257 if (Property.isReadOnlyObjCProperty())
1258 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1259 if (Property.isReadWriteObjCProperty())
1260 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1261 if (Property.isAssignObjCProperty())
1262 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1263 if (Property.isRetainObjCProperty())
1264 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1265 if (Property.isCopyObjCProperty())
1266 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1267 if (Property.isNonAtomicObjCProperty())
1268 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1269 if (PropertyAttributes)
1270 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1271 PropertyAttributes);
1273 DIEEntry *Entry = getDIEEntry(Element);
1274 if (!Entry) {
1275 Entry = createDIEEntry(ElemDie);
1276 insertDIEEntry(Element, Entry);
1277 }
1278 } else
1279 continue;
1280 }
1282 if (CTy.isAppleBlockExtension())
1283 addFlag(&Buffer, dwarf::DW_AT_APPLE_block);
1285 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1286 if (ContainingType)
1287 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1288 getOrCreateTypeDIE(ContainingType));
1290 if (CTy.isObjcClassComplete())
1291 addFlag(&Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1293 // Add template parameters to a class, structure or union types.
1294 // FIXME: The support isn't in the metadata for this yet.
1295 if (Tag == dwarf::DW_TAG_class_type ||
1296 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1297 addTemplateParams(Buffer, CTy.getTemplateParams());
1299 break;
1300 }
1301 default:
1302 break;
1303 }
1305 // Add name if not anonymous or intermediate type.
1306 if (!Name.empty())
1307 addString(&Buffer, dwarf::DW_AT_name, Name);
1309 if (Tag == dwarf::DW_TAG_enumeration_type ||
1310 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1311 Tag == dwarf::DW_TAG_union_type) {
1312 // Add size if non-zero (derived types might be zero-sized.)
1313 // TODO: Do we care about size for enum forward declarations?
1314 if (Size)
1315 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1316 else if (!CTy.isForwardDecl())
1317 // Add zero size if it is not a forward declaration.
1318 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, 0);
1320 // If we're a forward decl, say so.
1321 if (CTy.isForwardDecl())
1322 addFlag(&Buffer, dwarf::DW_AT_declaration);
1324 // Add source line info if available.
1325 if (!CTy.isForwardDecl())
1326 addSourceLine(&Buffer, CTy);
1328 // No harm in adding the runtime language to the declaration.
1329 unsigned RLang = CTy.getRunTimeLang();
1330 if (RLang)
1331 addUInt(&Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1332 RLang);
1333 }
1334 }
1336 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1337 /// DITemplateTypeParameter.
1338 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1339 DITemplateTypeParameter TP) {
1340 DIE *ParamDIE =
1341 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1342 // Add the type if it exists, it could be void and therefore no type.
1343 if (TP.getType())
1344 addType(ParamDIE, resolve(TP.getType()));
1345 if (!TP.getName().empty())
1346 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1347 }
1349 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1350 /// DITemplateValueParameter.
1351 void
1352 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1353 DITemplateValueParameter VP) {
1354 DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1356 // Add the type if there is one, template template and template parameter
1357 // packs will not have a type.
1358 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1359 addType(ParamDIE, resolve(VP.getType()));
1360 if (!VP.getName().empty())
1361 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1362 if (Value *Val = VP.getValue()) {
1363 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1364 addConstantValue(ParamDIE, CI,
1365 isUnsignedDIType(DD, resolve(VP.getType())));
1366 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1367 // For declaration non-type template parameters (such as global values and
1368 // functions)
1369 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1370 addOpAddress(Loc, Asm->getSymbol(GV));
1371 // Emit DW_OP_stack_value to use the address as the immediate value of the
1372 // parameter, rather than a pointer to it.
1373 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1374 addBlock(ParamDIE, dwarf::DW_AT_location, Loc);
1375 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1376 assert(isa<MDString>(Val));
1377 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1378 cast<MDString>(Val)->getString());
1379 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1380 assert(isa<MDNode>(Val));
1381 DIArray A(cast<MDNode>(Val));
1382 addTemplateParams(*ParamDIE, A);
1383 }
1384 }
1385 }
1387 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1388 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1389 // Construct the context before querying for the existence of the DIE in case
1390 // such construction creates the DIE.
1391 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1393 DIE *NDie = getDIE(NS);
1394 if (NDie)
1395 return NDie;
1396 NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1398 if (!NS.getName().empty()) {
1399 addString(NDie, dwarf::DW_AT_name, NS.getName());
1400 addAccelNamespace(NS.getName(), NDie);
1401 addGlobalName(NS.getName(), NDie, NS.getContext());
1402 } else
1403 addAccelNamespace("(anonymous namespace)", NDie);
1404 addSourceLine(NDie, NS);
1405 return NDie;
1406 }
1408 /// Unique C++ member function declarations based on their
1409 /// context and mangled name.
1410 DISubprogram
1411 DwarfUnit::getOdrUniqueSubprogram(DIScope Context, DISubprogram SP) const {
1412 if (!hasODR() ||
1413 !Context.isCompositeType() ||
1414 SP.getLinkageName().empty() ||
1415 SP.isDefinition())
1416 return SP;
1417 // Create a key with the UID of the parent class and this SP's name.
1418 Twine Key = SP.getContext().getName() + SP.getLinkageName();
1419 const MDNode *&Entry = DD->getOrCreateOdrMember(Key.str());
1420 if (!Entry)
1421 Entry = &*SP;
1423 return DISubprogram(Entry);
1424 }
1426 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1427 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1428 // Construct the context before querying for the existence of the DIE in case
1429 // such construction creates the DIE (as is the case for member function
1430 // declarations).
1431 DIScope Context = resolve(SP.getContext());
1432 DIE *ContextDIE = getOrCreateContextDIE(Context);
1433 // Unique declarations based on the ODR, where applicable.
1434 SP = getOdrUniqueSubprogram(Context, SP);
1436 DIE *SPDie = getDIE(SP);
1437 if (SPDie)
1438 return SPDie;
1440 DISubprogram SPDecl = SP.getFunctionDeclaration();
1441 if (SPDecl.isSubprogram())
1442 // Add subprogram definitions to the CU die directly.
1443 ContextDIE = UnitDie.get();
1445 // DW_TAG_inlined_subroutine may refer to this DIE.
1446 SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1448 DIE *DeclDie = NULL;
1449 if (SPDecl.isSubprogram())
1450 DeclDie = getOrCreateSubprogramDIE(SPDecl);
1452 // Add function template parameters.
1453 addTemplateParams(*SPDie, SP.getTemplateParams());
1455 // If this DIE is going to refer declaration info using AT_specification
1456 // then there is no need to add other attributes.
1457 if (DeclDie) {
1458 // Refer function declaration directly.
1459 addDIEEntry(SPDie, dwarf::DW_AT_specification, DeclDie);
1461 return SPDie;
1462 }
1464 // Add the linkage name if we have one.
1465 StringRef LinkageName = SP.getLinkageName();
1466 if (!LinkageName.empty())
1467 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1468 GlobalValue::getRealLinkageName(LinkageName));
1470 // Constructors and operators for anonymous aggregates do not have names.
1471 if (!SP.getName().empty())
1472 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1474 addSourceLine(SPDie, SP);
1476 // Add the prototype if we have a prototype and we have a C like
1477 // language.
1478 uint16_t Language = getLanguage();
1479 if (SP.isPrototyped() &&
1480 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1481 Language == dwarf::DW_LANG_ObjC))
1482 addFlag(SPDie, dwarf::DW_AT_prototyped);
1484 DICompositeType SPTy = SP.getType();
1485 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1486 "the type of a subprogram should be a subroutine");
1488 DIArray Args = SPTy.getTypeArray();
1489 // Add a return type. If this is a type like a C/C++ void type we don't add a
1490 // return type.
1491 if (Args.getElement(0))
1492 addType(SPDie, DIType(Args.getElement(0)));
1494 unsigned VK = SP.getVirtuality();
1495 if (VK) {
1496 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1497 DIELoc *Block = getDIELoc();
1498 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1499 addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1500 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1501 ContainingTypeMap.insert(
1502 std::make_pair(SPDie, resolve(SP.getContainingType())));
1503 }
1505 if (!SP.isDefinition()) {
1506 addFlag(SPDie, dwarf::DW_AT_declaration);
1508 // Add arguments. Do not add arguments for subprogram definition. They will
1509 // be handled while processing variables.
1510 constructSubprogramArguments(*SPDie, Args);
1511 }
1513 if (SP.isArtificial())
1514 addFlag(SPDie, dwarf::DW_AT_artificial);
1516 if (!SP.isLocalToUnit())
1517 addFlag(SPDie, dwarf::DW_AT_external);
1519 if (SP.isOptimized())
1520 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1522 if (unsigned isa = Asm->getISAEncoding()) {
1523 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1524 }
1526 if (SP.isLValueReference())
1527 addFlag(SPDie, dwarf::DW_AT_reference);
1529 if (SP.isRValueReference())
1530 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1532 if (SP.isProtected())
1533 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1534 dwarf::DW_ACCESS_protected);
1535 else if (SP.isPrivate())
1536 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1537 dwarf::DW_ACCESS_private);
1538 else
1539 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1540 dwarf::DW_ACCESS_public);
1542 if (SP.isExplicit())
1543 addFlag(SPDie, dwarf::DW_AT_explicit);
1545 return SPDie;
1546 }
1548 // Return const expression if value is a GEP to access merged global
1549 // constant. e.g.
1550 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1551 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1552 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1553 if (!CE || CE->getNumOperands() != 3 ||
1554 CE->getOpcode() != Instruction::GetElementPtr)
1555 return NULL;
1557 // First operand points to a global struct.
1558 Value *Ptr = CE->getOperand(0);
1559 if (!isa<GlobalValue>(Ptr) ||
1560 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1561 return NULL;
1563 // Second operand is zero.
1564 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1565 if (!CI || !CI->isZero())
1566 return NULL;
1568 // Third operand is offset.
1569 if (!isa<ConstantInt>(CE->getOperand(2)))
1570 return NULL;
1572 return CE;
1573 }
1575 /// createGlobalVariableDIE - create global variable DIE.
1576 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1577 // Check for pre-existence.
1578 if (getDIE(GV))
1579 return;
1581 assert(GV.isGlobalVariable());
1583 DIScope GVContext = GV.getContext();
1584 DIType GTy = GV.getType();
1586 // If this is a static data member definition, some attributes belong
1587 // to the declaration DIE.
1588 DIE *VariableDIE = NULL;
1589 bool IsStaticMember = false;
1590 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1591 if (SDMDecl.Verify()) {
1592 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1593 // We need the declaration DIE that is in the static member's class.
1594 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1595 IsStaticMember = true;
1596 }
1598 // If this is not a static data member definition, create the variable
1599 // DIE and add the initial set of attributes to it.
1600 if (!VariableDIE) {
1601 // Construct the context before querying for the existence of the DIE in
1602 // case such construction creates the DIE.
1603 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1605 // Add to map.
1606 VariableDIE = createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1608 // Add name and type.
1609 addString(VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1610 addType(VariableDIE, GTy);
1612 // Add scoping info.
1613 if (!GV.isLocalToUnit())
1614 addFlag(VariableDIE, dwarf::DW_AT_external);
1616 // Add line number info.
1617 addSourceLine(VariableDIE, GV);
1618 }
1620 // Add location.
1621 bool addToAccelTable = false;
1622 DIE *VariableSpecDIE = NULL;
1623 bool isGlobalVariable = GV.getGlobal() != NULL;
1624 if (isGlobalVariable) {
1625 addToAccelTable = true;
1626 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1627 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1628 if (GV.getGlobal()->isThreadLocal()) {
1629 // FIXME: Make this work with -gsplit-dwarf.
1630 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1631 assert((PointerSize == 4 || PointerSize == 8) &&
1632 "Add support for other sizes if necessary");
1633 // Based on GCC's support for TLS:
1634 if (!DD->useSplitDwarf()) {
1635 // 1) Start with a constNu of the appropriate pointer size
1636 addUInt(Loc, dwarf::DW_FORM_data1,
1637 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1638 // 2) containing the (relocated) offset of the TLS variable
1639 // within the module's TLS block.
1640 addExpr(Loc, dwarf::DW_FORM_udata,
1641 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym));
1642 } else {
1643 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1644 addUInt(Loc, dwarf::DW_FORM_udata,
1645 DU->getAddrPoolIndex(Sym, /* TLS */ true));
1646 }
1647 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1648 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1649 } else {
1650 DD->addArangeLabel(SymbolCU(this, Sym));
1651 addOpAddress(Loc, Sym);
1652 }
1653 // Do not create specification DIE if context is either compile unit
1654 // or a subprogram.
1655 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1656 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1657 // Create specification DIE.
1658 VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
1659 addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
1660 addBlock(VariableSpecDIE, dwarf::DW_AT_location, Loc);
1661 // A static member's declaration is already flagged as such.
1662 if (!SDMDecl.Verify())
1663 addFlag(VariableDIE, dwarf::DW_AT_declaration);
1664 } else {
1665 addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
1666 }
1667 // Add the linkage name.
1668 StringRef LinkageName = GV.getLinkageName();
1669 if (!LinkageName.empty())
1670 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1671 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1672 // TAG_variable.
1673 addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
1674 : VariableDIE,
1675 DD->getDwarfVersion() >= 4 ? dwarf::DW_AT_linkage_name
1676 : dwarf::DW_AT_MIPS_linkage_name,
1677 GlobalValue::getRealLinkageName(LinkageName));
1678 } else if (const ConstantInt *CI =
1679 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1680 // AT_const_value was added when the static member was created. To avoid
1681 // emitting AT_const_value multiple times, we only add AT_const_value when
1682 // it is not a static member.
1683 if (!IsStaticMember)
1684 addConstantValue(VariableDIE, CI, isUnsignedDIType(DD, GTy));
1685 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1686 addToAccelTable = true;
1687 // GV is a merged global.
1688 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1689 Value *Ptr = CE->getOperand(0);
1690 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1691 DD->addArangeLabel(SymbolCU(this, Sym));
1692 addOpAddress(Loc, Sym);
1693 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1694 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1695 addUInt(Loc, dwarf::DW_FORM_udata,
1696 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1697 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1698 addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
1699 }
1701 if (addToAccelTable) {
1702 DIE *AddrDIE = VariableSpecDIE ? VariableSpecDIE : VariableDIE;
1703 addAccelName(GV.getName(), AddrDIE);
1705 // If the linkage name is different than the name, go ahead and output
1706 // that as well into the name table.
1707 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1708 addAccelName(GV.getLinkageName(), AddrDIE);
1709 }
1711 if (!GV.isLocalToUnit())
1712 addGlobalName(GV.getName(), VariableSpecDIE ? VariableSpecDIE : VariableDIE,
1713 GV.getContext());
1714 }
1716 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1717 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1718 DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1719 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
1721 // The LowerBound value defines the lower bounds which is typically zero for
1722 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1723 // Count == -1 then the array is unbounded and we do not emit
1724 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1725 // Count == 0, then the array has zero elements in which case we do not emit
1726 // an upper bound.
1727 int64_t LowerBound = SR.getLo();
1728 int64_t DefaultLowerBound = getDefaultLowerBound();
1729 int64_t Count = SR.getCount();
1731 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1732 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1734 if (Count != -1 && Count != 0)
1735 // FIXME: An unbounded array should reference the expression that defines
1736 // the array.
1737 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1738 LowerBound + Count - 1);
1739 }
1741 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1742 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1743 if (CTy.isVector())
1744 addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
1746 // Emit the element type.
1747 addType(&Buffer, resolve(CTy.getTypeDerivedFrom()));
1749 // Get an anonymous type for index type.
1750 // FIXME: This type should be passed down from the front end
1751 // as different languages may have different sizes for indexes.
1752 DIE *IdxTy = getIndexTyDie();
1753 if (!IdxTy) {
1754 // Construct an anonymous type for index type.
1755 IdxTy = createAndAddDIE(dwarf::DW_TAG_base_type, *UnitDie);
1756 addString(IdxTy, dwarf::DW_AT_name, "int");
1757 addUInt(IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int32_t));
1758 addUInt(IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1759 dwarf::DW_ATE_signed);
1760 setIndexTyDie(IdxTy);
1761 }
1763 // Add subranges to array type.
1764 DIArray Elements = CTy.getTypeArray();
1765 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1766 DIDescriptor Element = Elements.getElement(i);
1767 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1768 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1769 }
1770 }
1772 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1773 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1774 DIArray Elements = CTy.getTypeArray();
1776 // Add enumerators to enumeration type.
1777 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1778 DIEnumerator Enum(Elements.getElement(i));
1779 if (Enum.isEnumerator()) {
1780 DIE *Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1781 StringRef Name = Enum.getName();
1782 addString(Enumerator, dwarf::DW_AT_name, Name);
1783 int64_t Value = Enum.getEnumValue();
1784 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1785 Value);
1786 }
1787 }
1788 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1789 if (DTy) {
1790 addType(&Buffer, DTy);
1791 addFlag(&Buffer, dwarf::DW_AT_enum_class);
1792 }
1793 }
1795 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1796 /// vtables.
1797 void DwarfUnit::constructContainingTypeDIEs() {
1798 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1799 CE = ContainingTypeMap.end();
1800 CI != CE; ++CI) {
1801 DIE *SPDie = CI->first;
1802 DIDescriptor D(CI->second);
1803 if (!D)
1804 continue;
1805 DIE *NDie = getDIE(D);
1806 if (!NDie)
1807 continue;
1808 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, NDie);
1809 }
1810 }
1812 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1813 DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
1814 StringRef Name = DV.getName();
1816 // Define variable debug information entry.
1817 DIE *VariableDie = new DIE(DV.getTag());
1818 DbgVariable *AbsVar = DV.getAbstractVariable();
1819 DIE *AbsDIE = AbsVar ? AbsVar->getDIE() : NULL;
1820 if (AbsDIE)
1821 addDIEEntry(VariableDie, dwarf::DW_AT_abstract_origin, AbsDIE);
1822 else {
1823 if (!Name.empty())
1824 addString(VariableDie, dwarf::DW_AT_name, Name);
1825 addSourceLine(VariableDie, DV.getVariable());
1826 addType(VariableDie, DV.getType());
1827 }
1829 if (DV.isArtificial())
1830 addFlag(VariableDie, dwarf::DW_AT_artificial);
1832 if (isScopeAbstract) {
1833 DV.setDIE(VariableDie);
1834 return VariableDie;
1835 }
1837 // Add variable address.
1839 unsigned Offset = DV.getDotDebugLocOffset();
1840 if (Offset != ~0U) {
1841 addLocationList(VariableDie, dwarf::DW_AT_location, Offset);
1842 DV.setDIE(VariableDie);
1843 return VariableDie;
1844 }
1846 // Check if variable is described by a DBG_VALUE instruction.
1847 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1848 assert(DVInsn->getNumOperands() == 3);
1849 if (DVInsn->getOperand(0).isReg()) {
1850 const MachineOperand RegOp = DVInsn->getOperand(0);
1851 // If the second operand is an immediate, this is an indirect value.
1852 if (DVInsn->getOperand(1).isImm()) {
1853 MachineLocation Location(RegOp.getReg(),
1854 DVInsn->getOperand(1).getImm());
1855 addVariableAddress(DV, VariableDie, Location);
1856 } else if (RegOp.getReg())
1857 addVariableAddress(DV, VariableDie, MachineLocation(RegOp.getReg()));
1858 } else if (DVInsn->getOperand(0).isImm())
1859 addConstantValue(VariableDie, DVInsn->getOperand(0), DV.getType());
1860 else if (DVInsn->getOperand(0).isFPImm())
1861 addConstantFPValue(VariableDie, DVInsn->getOperand(0));
1862 else if (DVInsn->getOperand(0).isCImm())
1863 addConstantValue(VariableDie, DVInsn->getOperand(0).getCImm(),
1864 isUnsignedDIType(DD, DV.getType()));
1866 DV.setDIE(VariableDie);
1867 return VariableDie;
1868 } else {
1869 // .. else use frame index.
1870 int FI = DV.getFrameIndex();
1871 if (FI != ~0) {
1872 unsigned FrameReg = 0;
1873 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1874 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1875 MachineLocation Location(FrameReg, Offset);
1876 addVariableAddress(DV, VariableDie, Location);
1877 }
1878 }
1880 DV.setDIE(VariableDie);
1881 return VariableDie;
1882 }
1884 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1885 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1886 DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1887 StringRef Name = DT.getName();
1888 if (!Name.empty())
1889 addString(MemberDie, dwarf::DW_AT_name, Name);
1891 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1893 addSourceLine(MemberDie, DT);
1895 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1897 // For C++, virtual base classes are not at fixed offset. Use following
1898 // expression to extract appropriate offset from vtable.
1899 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1901 DIELoc *VBaseLocationDie = new (DIEValueAllocator) DIELoc();
1902 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1903 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1904 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1905 addUInt(VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1906 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1907 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1908 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1910 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1911 } else {
1912 uint64_t Size = DT.getSizeInBits();
1913 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1914 uint64_t OffsetInBytes;
1916 if (Size != FieldSize) {
1917 // Handle bitfield, assume bytes are 8 bits.
1918 addUInt(MemberDie, dwarf::DW_AT_byte_size, None, FieldSize/8);
1919 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, Size);
1921 uint64_t Offset = DT.getOffsetInBits();
1922 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1923 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1924 uint64_t FieldOffset = (HiMark - FieldSize);
1925 Offset -= FieldOffset;
1927 // Maybe we need to work from the other end.
1928 if (Asm->getDataLayout().isLittleEndian())
1929 Offset = FieldSize - (Offset + Size);
1930 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1932 // Here DW_AT_data_member_location points to the anonymous
1933 // field that includes this bit field.
1934 OffsetInBytes = FieldOffset >> 3;
1935 } else
1936 // This is not a bitfield.
1937 OffsetInBytes = DT.getOffsetInBits() >> 3;
1939 if (DD->getDwarfVersion() <= 2) {
1940 DIELoc *MemLocationDie = new (DIEValueAllocator) DIELoc();
1941 addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1942 addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1943 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1944 } else
1945 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1946 OffsetInBytes);
1947 }
1949 if (DT.isProtected())
1950 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1951 dwarf::DW_ACCESS_protected);
1952 else if (DT.isPrivate())
1953 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1954 dwarf::DW_ACCESS_private);
1955 // Otherwise C++ member and base classes are considered public.
1956 else
1957 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1958 dwarf::DW_ACCESS_public);
1959 if (DT.isVirtual())
1960 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1961 dwarf::DW_VIRTUALITY_virtual);
1963 // Objective-C properties.
1964 if (MDNode *PNode = DT.getObjCProperty())
1965 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1966 MemberDie->addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1967 PropertyDie);
1969 if (DT.isArtificial())
1970 addFlag(MemberDie, dwarf::DW_AT_artificial);
1971 }
1973 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1974 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1975 if (!DT.Verify())
1976 return NULL;
1978 // Construct the context before querying for the existence of the DIE in case
1979 // such construction creates the DIE.
1980 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1981 assert(dwarf::isType(ContextDIE->getTag()) &&
1982 "Static member should belong to a type.");
1984 DIE *StaticMemberDIE = getDIE(DT);
1985 if (StaticMemberDIE)
1986 return StaticMemberDIE;
1988 StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1990 DIType Ty = resolve(DT.getTypeDerivedFrom());
1992 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1993 addType(StaticMemberDIE, Ty);
1994 addSourceLine(StaticMemberDIE, DT);
1995 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1996 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1998 // FIXME: We could omit private if the parent is a class_type, and
1999 // public if the parent is something else.
2000 if (DT.isProtected())
2001 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
2002 dwarf::DW_ACCESS_protected);
2003 else if (DT.isPrivate())
2004 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
2005 dwarf::DW_ACCESS_private);
2006 else
2007 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
2008 dwarf::DW_ACCESS_public);
2010 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
2011 addConstantValue(StaticMemberDIE, CI, isUnsignedDIType(DD, Ty));
2012 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
2013 addConstantFPValue(StaticMemberDIE, CFP);
2015 return StaticMemberDIE;
2016 }
2018 void DwarfUnit::emitHeader(const MCSection *ASection,
2019 const MCSymbol *ASectionSym) const {
2020 Asm->OutStreamer.AddComment("DWARF version number");
2021 Asm->EmitInt16(DD->getDwarfVersion());
2022 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
2023 // We share one abbreviations table across all units so it's always at the
2024 // start of the section. Use a relocatable offset where needed to ensure
2025 // linking doesn't invalidate that offset.
2026 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
2027 Asm->OutStreamer.AddComment("Address Size (in bytes)");
2028 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
2029 }
2031 void DwarfCompileUnit::initStmtList(MCSymbol *DwarfLineSectionSym) {
2032 // Define start line table label for each Compile Unit.
2033 MCSymbol *LineTableStartSym =
2034 Asm->GetTempSymbol("line_table_start", getUniqueID());
2035 Asm->OutStreamer.getContext().setMCLineTableSymbol(LineTableStartSym,
2036 getUniqueID());
2038 // Use a single line table if we are generating assembly.
2039 bool UseTheFirstCU =
2040 Asm->OutStreamer.hasRawTextSupport() || (getUniqueID() == 0);
2042 stmtListIndex = UnitDie->getValues().size();
2044 // DW_AT_stmt_list is a offset of line number information for this
2045 // compile unit in debug_line section. For split dwarf this is
2046 // left in the skeleton CU and so not included.
2047 // The line table entries are not always emitted in assembly, so it
2048 // is not okay to use line_table_start here.
2049 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
2050 addSectionLabel(UnitDie.get(), dwarf::DW_AT_stmt_list,
2051 UseTheFirstCU ? DwarfLineSectionSym : LineTableStartSym);
2052 else if (UseTheFirstCU)
2053 addSectionOffset(UnitDie.get(), dwarf::DW_AT_stmt_list, 0);
2054 else
2055 addSectionDelta(UnitDie.get(), dwarf::DW_AT_stmt_list, LineTableStartSym,
2056 DwarfLineSectionSym);
2057 }
2059 void DwarfCompileUnit::applyStmtList(DIE &D) {
2060 D.addValue(dwarf::DW_AT_stmt_list,
2061 UnitDie->getAbbrev().getData()[stmtListIndex].getForm(),
2062 UnitDie->getValues()[stmtListIndex]);
2063 }
2065 void DwarfTypeUnit::emitHeader(const MCSection *ASection,
2066 const MCSymbol *ASectionSym) const {
2067 DwarfUnit::emitHeader(ASection, ASectionSym);
2068 Asm->OutStreamer.AddComment("Type Signature");
2069 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
2070 Asm->OutStreamer.AddComment("Type DIE Offset");
2071 // In a skeleton type unit there is no type DIE so emit a zero offset.
2072 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
2073 sizeof(Ty->getOffset()));
2074 }
2076 void DwarfTypeUnit::initSection(const MCSection *Section) {
2077 assert(!this->Section);
2078 this->Section = Section;
2079 // Since each type unit is contained in its own COMDAT section, the begin
2080 // label and the section label are the same. Using the begin label emission in
2081 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2082 // the only other alternative of lazily constructing start-of-section labels
2083 // and storing a mapping in DwarfDebug (or AsmPrinter).
2084 this->SectionSym = this->LabelBegin =
2085 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2086 this->LabelEnd =
2087 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2088 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
2089 }