1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DwarfUnit.h"
17 #include "DwarfAccelTable.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/DIBuilder.h"
21 #include "llvm/IR/Constants.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCSection.h"
28 #include "llvm/MC/MCStreamer.h"
29 #include "llvm/Support/CommandLine.h"
30 #include "llvm/Target/TargetFrameLowering.h"
31 #include "llvm/Target/TargetLoweringObjectFile.h"
32 #include "llvm/Target/TargetMachine.h"
33 #include "llvm/Target/TargetRegisterInfo.h"
35 using namespace llvm;
37 static cl::opt<bool>
38 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
39 cl::desc("Generate DWARF4 type units."),
40 cl::init(false));
42 /// Unit - Unit constructor.
43 DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
44 DwarfDebug *DW, DwarfFile *DWU)
45 : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
46 DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
47 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
48 }
50 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
51 AsmPrinter *A, DwarfDebug *DW,
52 DwarfFile *DWU)
53 : DwarfUnit(UID, D, Node, A, DW, DWU) {
54 insertDIE(Node, D);
55 }
57 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DICompileUnit CUNode,
58 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
59 : DwarfUnit(UID, D, CUNode, A, DW, DWU) {}
61 /// ~Unit - Destructor for compile unit.
62 DwarfUnit::~DwarfUnit() {
63 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
64 DIEBlocks[j]->~DIEBlock();
65 }
67 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
68 /// information entry.
69 DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
70 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
71 return Value;
72 }
74 /// getDefaultLowerBound - Return the default lower bound for an array. If the
75 /// DWARF version doesn't handle the language, return -1.
76 int64_t DwarfUnit::getDefaultLowerBound() const {
77 switch (getLanguage()) {
78 default:
79 break;
81 case dwarf::DW_LANG_C89:
82 case dwarf::DW_LANG_C99:
83 case dwarf::DW_LANG_C:
84 case dwarf::DW_LANG_C_plus_plus:
85 case dwarf::DW_LANG_ObjC:
86 case dwarf::DW_LANG_ObjC_plus_plus:
87 return 0;
89 case dwarf::DW_LANG_Fortran77:
90 case dwarf::DW_LANG_Fortran90:
91 case dwarf::DW_LANG_Fortran95:
92 return 1;
94 // The languages below have valid values only if the DWARF version >= 4.
95 case dwarf::DW_LANG_Java:
96 case dwarf::DW_LANG_Python:
97 case dwarf::DW_LANG_UPC:
98 case dwarf::DW_LANG_D:
99 if (dwarf::DWARF_VERSION >= 4)
100 return 0;
101 break;
103 case dwarf::DW_LANG_Ada83:
104 case dwarf::DW_LANG_Ada95:
105 case dwarf::DW_LANG_Cobol74:
106 case dwarf::DW_LANG_Cobol85:
107 case dwarf::DW_LANG_Modula2:
108 case dwarf::DW_LANG_Pascal83:
109 case dwarf::DW_LANG_PLI:
110 if (dwarf::DWARF_VERSION >= 4)
111 return 1;
112 break;
113 }
115 return -1;
116 }
118 /// Check whether the DIE for this MDNode can be shared across CUs.
119 static bool isShareableAcrossCUs(DIDescriptor D) {
120 // When the MDNode can be part of the type system, the DIE can be shared
121 // across CUs.
122 // Combining type units and cross-CU DIE sharing is lower value (since
123 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
124 // level already) but may be implementable for some value in projects
125 // building multiple independent libraries with LTO and then linking those
126 // together.
127 return (D.isType() ||
128 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
129 !GenerateDwarfTypeUnits;
130 }
132 /// getDIE - Returns the debug information entry map slot for the
133 /// specified debug variable. We delegate the request to DwarfDebug
134 /// when the DIE for this MDNode can be shared across CUs. The mappings
135 /// will be kept in DwarfDebug for shareable DIEs.
136 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
137 if (isShareableAcrossCUs(D))
138 return DD->getDIE(D);
139 return MDNodeToDieMap.lookup(D);
140 }
142 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
143 /// when the DIE for this MDNode can be shared across CUs. The mappings
144 /// will be kept in DwarfDebug for shareable DIEs.
145 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
146 if (isShareableAcrossCUs(Desc)) {
147 DD->insertDIE(Desc, D);
148 return;
149 }
150 MDNodeToDieMap.insert(std::make_pair(Desc, D));
151 }
153 /// addFlag - Add a flag that is true.
154 void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
155 if (DD->getDwarfVersion() >= 4)
156 Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
157 else
158 Die->addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
159 }
161 /// addUInt - Add an unsigned integer attribute data and value.
162 ///
163 void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
164 Optional<dwarf::Form> Form, uint64_t Integer) {
165 if (!Form)
166 Form = DIEInteger::BestForm(false, Integer);
167 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
168 DIEInteger(Integer);
169 Die->addValue(Attribute, *Form, Value);
170 }
172 void DwarfUnit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
173 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
174 }
176 /// addSInt - Add an signed integer attribute data and value.
177 ///
178 void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
179 Optional<dwarf::Form> Form, int64_t Integer) {
180 if (!Form)
181 Form = DIEInteger::BestForm(true, Integer);
182 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
183 Die->addValue(Attribute, *Form, Value);
184 }
186 void DwarfUnit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form,
187 int64_t Integer) {
188 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
189 }
191 /// addString - Add a string attribute data and value. We always emit a
192 /// reference to the string pool instead of immediate strings so that DIEs have
193 /// more predictable sizes. In the case of split dwarf we emit an index
194 /// into another table which gets us the static offset into the string
195 /// table.
196 void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
197 StringRef String) {
199 if (!DD->useSplitDwarf())
200 return addLocalString(Die, Attribute, String);
202 unsigned idx = DU->getStringPoolIndex(String);
203 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
204 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
205 Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
206 }
208 /// addLocalString - Add a string attribute data and value. This is guaranteed
209 /// to be in the local string pool instead of indirected.
210 void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
211 StringRef String) {
212 MCSymbol *Symb = DU->getStringPoolEntry(String);
213 DIEValue *Value;
214 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
215 Value = new (DIEValueAllocator) DIELabel(Symb);
216 else {
217 MCSymbol *StringPool = DU->getStringPoolSym();
218 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
219 }
220 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
221 Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
222 }
224 /// addExpr - Add a Dwarf expression attribute data and value.
225 ///
226 void DwarfUnit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
227 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
228 Die->addValue((dwarf::Attribute)0, Form, Value);
229 }
231 /// addLabel - Add a Dwarf label attribute data and value.
232 ///
233 void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
234 const MCSymbol *Label) {
235 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
236 Die->addValue(Attribute, Form, Value);
237 }
239 void DwarfUnit::addLabel(DIEBlock *Die, dwarf::Form Form,
240 const MCSymbol *Label) {
241 addLabel(Die, (dwarf::Attribute)0, Form, Label);
242 }
244 /// addSectionLabel - Add a Dwarf section label attribute data and value.
245 ///
246 void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
247 const MCSymbol *Label) {
248 if (DD->getDwarfVersion() >= 4)
249 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
250 else
251 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
252 }
254 /// addSectionOffset - Add an offset into a section attribute data and value.
255 ///
256 void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
257 uint64_t Integer) {
258 if (DD->getDwarfVersion() >= 4)
259 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
260 else
261 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
262 }
264 /// addLabelAddress - Add a dwarf label attribute data and value using
265 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
266 ///
267 void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
268 MCSymbol *Label) {
269 if (Label)
270 DD->addArangeLabel(SymbolCU(this, Label));
272 if (!DD->useSplitDwarf()) {
273 if (Label) {
274 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
275 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
276 } else {
277 DIEValue *Value = new (DIEValueAllocator) DIEInteger(0);
278 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
279 }
280 } else {
281 unsigned idx = DU->getAddrPoolIndex(Label);
282 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
283 Die->addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
284 }
285 }
287 /// addOpAddress - Add a dwarf op address data and value using the
288 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
289 ///
290 void DwarfUnit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
291 if (!DD->useSplitDwarf()) {
292 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
293 addLabel(Die, dwarf::DW_FORM_udata, Sym);
294 } else {
295 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
296 addUInt(Die, dwarf::DW_FORM_GNU_addr_index, DU->getAddrPoolIndex(Sym));
297 }
298 }
300 /// addSectionDelta - Add a section label delta attribute data and value.
301 ///
302 void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
303 const MCSymbol *Hi, const MCSymbol *Lo) {
304 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
305 if (DD->getDwarfVersion() >= 4)
306 Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
307 else
308 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
309 }
311 /// addDIEEntry - Add a DIE attribute data and value.
312 ///
313 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
314 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
315 }
317 void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
318 Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
319 new (DIEValueAllocator) DIETypeSignature(Type));
320 }
322 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
323 DIEEntry *Entry) {
324 const DIE *DieCU = Die->getUnitOrNull();
325 const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
326 if (!DieCU)
327 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
328 DieCU = getUnitDie();
329 if (!EntryCU)
330 EntryCU = getUnitDie();
331 Die->addValue(Attribute, EntryCU == DieCU ? dwarf::DW_FORM_ref4
332 : dwarf::DW_FORM_ref_addr,
333 Entry);
334 }
336 /// Create a DIE with the given Tag, add the DIE to its parent, and
337 /// call insertDIE if MD is not null.
338 DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
339 DIE *Die = new DIE(Tag);
340 Parent.addChild(Die);
341 if (N)
342 insertDIE(N, Die);
343 return Die;
344 }
346 /// addBlock - Add block data.
347 ///
348 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
349 DIEBlock *Block) {
350 Block->ComputeSize(Asm);
351 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
352 Die->addValue(Attribute, Block->BestForm(), Block);
353 }
355 /// addSourceLine - Add location information to specified debug information
356 /// entry.
357 void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
358 // Verify variable.
359 if (!V.isVariable())
360 return;
362 unsigned Line = V.getLineNumber();
363 if (Line == 0)
364 return;
365 unsigned FileID =
366 DD->getOrCreateSourceID(V.getContext().getFilename(),
367 V.getContext().getDirectory(), getUniqueID());
368 assert(FileID && "Invalid file id");
369 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
370 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
371 }
373 /// addSourceLine - Add location information to specified debug information
374 /// entry.
375 void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
376 // Verify global variable.
377 if (!G.isGlobalVariable())
378 return;
380 unsigned Line = G.getLineNumber();
381 if (Line == 0)
382 return;
383 unsigned FileID =
384 DD->getOrCreateSourceID(G.getFilename(), G.getDirectory(), getUniqueID());
385 assert(FileID && "Invalid file id");
386 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
387 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
388 }
390 /// addSourceLine - Add location information to specified debug information
391 /// entry.
392 void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
393 // Verify subprogram.
394 if (!SP.isSubprogram())
395 return;
397 // If the line number is 0, don't add it.
398 unsigned Line = SP.getLineNumber();
399 if (Line == 0)
400 return;
402 unsigned FileID = DD->getOrCreateSourceID(SP.getFilename(), SP.getDirectory(),
403 getUniqueID());
404 assert(FileID && "Invalid file id");
405 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
406 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
407 }
409 /// addSourceLine - Add location information to specified debug information
410 /// entry.
411 void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
412 // Verify type.
413 if (!Ty.isType())
414 return;
416 unsigned Line = Ty.getLineNumber();
417 if (Line == 0)
418 return;
419 unsigned FileID = DD->getOrCreateSourceID(Ty.getFilename(), Ty.getDirectory(),
420 getUniqueID());
421 assert(FileID && "Invalid file id");
422 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
423 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
424 }
426 /// addSourceLine - Add location information to specified debug information
427 /// entry.
428 void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
429 // Verify type.
430 if (!Ty.isObjCProperty())
431 return;
433 unsigned Line = Ty.getLineNumber();
434 if (Line == 0)
435 return;
436 DIFile File = Ty.getFile();
437 unsigned FileID = DD->getOrCreateSourceID(File.getFilename(),
438 File.getDirectory(), getUniqueID());
439 assert(FileID && "Invalid file id");
440 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
441 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
442 }
444 /// addSourceLine - Add location information to specified debug information
445 /// entry.
446 void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
447 // Verify namespace.
448 if (!NS.Verify())
449 return;
451 unsigned Line = NS.getLineNumber();
452 if (Line == 0)
453 return;
454 StringRef FN = NS.getFilename();
456 unsigned FileID =
457 DD->getOrCreateSourceID(FN, NS.getDirectory(), getUniqueID());
458 assert(FileID && "Invalid file id");
459 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
460 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
461 }
463 /// addVariableAddress - Add DW_AT_location attribute for a
464 /// DbgVariable based on provided MachineLocation.
465 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
466 MachineLocation Location) {
467 if (DV.variableHasComplexAddress())
468 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
469 else if (DV.isBlockByrefVariable())
470 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
471 else
472 addAddress(Die, dwarf::DW_AT_location, Location,
473 DV.getVariable().isIndirect());
474 }
476 /// addRegisterOp - Add register operand.
477 void DwarfUnit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
478 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
479 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
480 if (DWReg < 32)
481 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
482 else {
483 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
484 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
485 }
486 }
488 /// addRegisterOffset - Add register offset.
489 void DwarfUnit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg,
490 int64_t Offset) {
491 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
492 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
493 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
494 if (Reg == TRI->getFrameRegister(*Asm->MF))
495 // If variable offset is based in frame register then use fbreg.
496 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
497 else if (DWReg < 32)
498 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
499 else {
500 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
501 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
502 }
503 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
504 }
506 /// addAddress - Add an address attribute to a die based on the location
507 /// provided.
508 void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
509 const MachineLocation &Location, bool Indirect) {
510 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
512 if (Location.isReg() && !Indirect)
513 addRegisterOp(Block, Location.getReg());
514 else {
515 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
516 if (Indirect && !Location.isReg()) {
517 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
518 }
519 }
521 // Now attach the location information to the DIE.
522 addBlock(Die, Attribute, Block);
523 }
525 /// addComplexAddress - Start with the address based on the location provided,
526 /// and generate the DWARF information necessary to find the actual variable
527 /// given the extra address information encoded in the DbgVariable, starting
528 /// from the starting location. Add the DWARF information to the die.
529 ///
530 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
531 dwarf::Attribute Attribute,
532 const MachineLocation &Location) {
533 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
534 unsigned N = DV.getNumAddrElements();
535 unsigned i = 0;
536 if (Location.isReg()) {
537 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
538 // If first address element is OpPlus then emit
539 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
540 addRegisterOffset(Block, Location.getReg(), DV.getAddrElement(1));
541 i = 2;
542 } else
543 addRegisterOp(Block, Location.getReg());
544 } else
545 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
547 for (; i < N; ++i) {
548 uint64_t Element = DV.getAddrElement(i);
549 if (Element == DIBuilder::OpPlus) {
550 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
551 addUInt(Block, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
552 } else if (Element == DIBuilder::OpDeref) {
553 if (!Location.isReg())
554 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
555 } else
556 llvm_unreachable("unknown DIBuilder Opcode");
557 }
559 // Now attach the location information to the DIE.
560 addBlock(Die, Attribute, Block);
561 }
563 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
564 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
565 gives the variable VarName either the struct, or a pointer to the struct, as
566 its type. This is necessary for various behind-the-scenes things the
567 compiler needs to do with by-reference variables in Blocks.
569 However, as far as the original *programmer* is concerned, the variable
570 should still have type 'SomeType', as originally declared.
572 The function getBlockByrefType dives into the __Block_byref_x_VarName
573 struct to find the original type of the variable, which is then assigned to
574 the variable's Debug Information Entry as its real type. So far, so good.
575 However now the debugger will expect the variable VarName to have the type
576 SomeType. So we need the location attribute for the variable to be an
577 expression that explains to the debugger how to navigate through the
578 pointers and struct to find the actual variable of type SomeType.
580 The following function does just that. We start by getting
581 the "normal" location for the variable. This will be the location
582 of either the struct __Block_byref_x_VarName or the pointer to the
583 struct __Block_byref_x_VarName.
585 The struct will look something like:
587 struct __Block_byref_x_VarName {
588 ... <various fields>
589 struct __Block_byref_x_VarName *forwarding;
590 ... <various other fields>
591 SomeType VarName;
592 ... <maybe more fields>
593 };
595 If we are given the struct directly (as our starting point) we
596 need to tell the debugger to:
598 1). Add the offset of the forwarding field.
600 2). Follow that pointer to get the real __Block_byref_x_VarName
601 struct to use (the real one may have been copied onto the heap).
603 3). Add the offset for the field VarName, to find the actual variable.
605 If we started with a pointer to the struct, then we need to
606 dereference that pointer first, before the other steps.
607 Translating this into DWARF ops, we will need to append the following
608 to the current location description for the variable:
610 DW_OP_deref -- optional, if we start with a pointer
611 DW_OP_plus_uconst <forward_fld_offset>
612 DW_OP_deref
613 DW_OP_plus_uconst <varName_fld_offset>
615 That is what this function does. */
617 /// addBlockByrefAddress - Start with the address based on the location
618 /// provided, and generate the DWARF information necessary to find the
619 /// actual Block variable (navigating the Block struct) based on the
620 /// starting location. Add the DWARF information to the die. For
621 /// more information, read large comment just above here.
622 ///
623 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
624 dwarf::Attribute Attribute,
625 const MachineLocation &Location) {
626 DIType Ty = DV.getType();
627 DIType TmpTy = Ty;
628 uint16_t Tag = Ty.getTag();
629 bool isPointer = false;
631 StringRef varName = DV.getName();
633 if (Tag == dwarf::DW_TAG_pointer_type) {
634 DIDerivedType DTy(Ty);
635 TmpTy = resolve(DTy.getTypeDerivedFrom());
636 isPointer = true;
637 }
639 DICompositeType blockStruct(TmpTy);
641 // Find the __forwarding field and the variable field in the __Block_byref
642 // struct.
643 DIArray Fields = blockStruct.getTypeArray();
644 DIDerivedType varField;
645 DIDerivedType forwardingField;
647 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
648 DIDerivedType DT(Fields.getElement(i));
649 StringRef fieldName = DT.getName();
650 if (fieldName == "__forwarding")
651 forwardingField = DT;
652 else if (fieldName == varName)
653 varField = DT;
654 }
656 // Get the offsets for the forwarding field and the variable field.
657 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
658 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
660 // Decode the original location, and use that as the start of the byref
661 // variable's location.
662 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
664 if (Location.isReg())
665 addRegisterOp(Block, Location.getReg());
666 else
667 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
669 // If we started with a pointer to the __Block_byref... struct, then
670 // the first thing we need to do is dereference the pointer (DW_OP_deref).
671 if (isPointer)
672 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
674 // Next add the offset for the '__forwarding' field:
675 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
676 // adding the offset if it's 0.
677 if (forwardingFieldOffset > 0) {
678 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
679 addUInt(Block, dwarf::DW_FORM_udata, forwardingFieldOffset);
680 }
682 // Now dereference the __forwarding field to get to the real __Block_byref
683 // struct: DW_OP_deref.
684 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
686 // Now that we've got the real __Block_byref... struct, add the offset
687 // for the variable's field to get to the location of the actual variable:
688 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
689 if (varFieldOffset > 0) {
690 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
691 addUInt(Block, dwarf::DW_FORM_udata, varFieldOffset);
692 }
694 // Now attach the location information to the DIE.
695 addBlock(Die, Attribute, Block);
696 }
698 /// isTypeSigned - Return true if the type is signed.
699 static bool isTypeSigned(DwarfDebug *DD, DIType Ty, int *SizeInBits) {
700 if (Ty.isDerivedType())
701 return isTypeSigned(DD, DD->resolve(DIDerivedType(Ty).getTypeDerivedFrom()),
702 SizeInBits);
703 if (Ty.isBasicType())
704 if (DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed ||
705 DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed_char) {
706 *SizeInBits = Ty.getSizeInBits();
707 return true;
708 }
709 return false;
710 }
712 /// Return true if type encoding is unsigned.
713 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
714 DIDerivedType DTy(Ty);
715 if (DTy.isDerivedType())
716 return isUnsignedDIType(DD, DD->resolve(DTy.getTypeDerivedFrom()));
718 DIBasicType BTy(Ty);
719 if (BTy.isBasicType()) {
720 unsigned Encoding = BTy.getEncoding();
721 if (Encoding == dwarf::DW_ATE_unsigned ||
722 Encoding == dwarf::DW_ATE_unsigned_char ||
723 Encoding == dwarf::DW_ATE_boolean)
724 return true;
725 }
726 return false;
727 }
729 /// If this type is derived from a base type then return base type size.
730 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
731 unsigned Tag = Ty.getTag();
733 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
734 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
735 Tag != dwarf::DW_TAG_restrict_type)
736 return Ty.getSizeInBits();
738 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
740 // If this type is not derived from any type then take conservative approach.
741 if (!BaseType.isValid())
742 return Ty.getSizeInBits();
744 // If this is a derived type, go ahead and get the base type, unless it's a
745 // reference then it's just the size of the field. Pointer types have no need
746 // of this since they're a different type of qualification on the type.
747 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
748 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
749 return Ty.getSizeInBits();
751 if (BaseType.isDerivedType())
752 return getBaseTypeSize(DD, DIDerivedType(BaseType));
754 return BaseType.getSizeInBits();
755 }
757 /// addConstantValue - Add constant value entry in variable DIE.
758 void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
759 DIType Ty) {
760 // FIXME: This is a bit conservative/simple - it emits negative values at
761 // their maximum bit width which is a bit unfortunate (& doesn't prefer
762 // udata/sdata over dataN as suggested by the DWARF spec)
763 assert(MO.isImm() && "Invalid machine operand!");
764 int SizeInBits = -1;
765 bool SignedConstant = isTypeSigned(DD, Ty, &SizeInBits);
766 dwarf::Form Form;
768 // If we're a signed constant definitely use sdata.
769 if (SignedConstant) {
770 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata, MO.getImm());
771 return;
772 }
774 // Else use data for now unless it's larger than we can deal with.
775 switch (SizeInBits) {
776 case 8:
777 Form = dwarf::DW_FORM_data1;
778 break;
779 case 16:
780 Form = dwarf::DW_FORM_data2;
781 break;
782 case 32:
783 Form = dwarf::DW_FORM_data4;
784 break;
785 case 64:
786 Form = dwarf::DW_FORM_data8;
787 break;
788 default:
789 Form = dwarf::DW_FORM_udata;
790 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
791 return;
792 }
793 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
794 }
796 /// addConstantFPValue - Add constant value entry in variable DIE.
797 void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
798 assert(MO.isFPImm() && "Invalid machine operand!");
799 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
800 APFloat FPImm = MO.getFPImm()->getValueAPF();
802 // Get the raw data form of the floating point.
803 const APInt FltVal = FPImm.bitcastToAPInt();
804 const char *FltPtr = (const char *)FltVal.getRawData();
806 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
807 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
808 int Incr = (LittleEndian ? 1 : -1);
809 int Start = (LittleEndian ? 0 : NumBytes - 1);
810 int Stop = (LittleEndian ? NumBytes : -1);
812 // Output the constant to DWARF one byte at a time.
813 for (; Start != Stop; Start += Incr)
814 addUInt(Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
816 addBlock(Die, dwarf::DW_AT_const_value, Block);
817 }
819 /// addConstantFPValue - Add constant value entry in variable DIE.
820 void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
821 // Pass this down to addConstantValue as an unsigned bag of bits.
822 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
823 }
825 /// addConstantValue - Add constant value entry in variable DIE.
826 void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
827 bool Unsigned) {
828 addConstantValue(Die, CI->getValue(), Unsigned);
829 }
831 // addConstantValue - Add constant value entry in variable DIE.
832 void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
833 unsigned CIBitWidth = Val.getBitWidth();
834 if (CIBitWidth <= 64) {
835 // If we're a signed constant definitely use sdata.
836 if (!Unsigned) {
837 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
838 Val.getSExtValue());
839 return;
840 }
842 // Else use data for now unless it's larger than we can deal with.
843 dwarf::Form Form;
844 switch (CIBitWidth) {
845 case 8:
846 Form = dwarf::DW_FORM_data1;
847 break;
848 case 16:
849 Form = dwarf::DW_FORM_data2;
850 break;
851 case 32:
852 Form = dwarf::DW_FORM_data4;
853 break;
854 case 64:
855 Form = dwarf::DW_FORM_data8;
856 break;
857 default:
858 addUInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_udata,
859 Val.getZExtValue());
860 return;
861 }
862 addUInt(Die, dwarf::DW_AT_const_value, Form, Val.getZExtValue());
863 return;
864 }
866 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
868 // Get the raw data form of the large APInt.
869 const uint64_t *Ptr64 = Val.getRawData();
871 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
872 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
874 // Output the constant to DWARF one byte at a time.
875 for (int i = 0; i < NumBytes; i++) {
876 uint8_t c;
877 if (LittleEndian)
878 c = Ptr64[i / 8] >> (8 * (i & 7));
879 else
880 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
881 addUInt(Block, dwarf::DW_FORM_data1, c);
882 }
884 addBlock(Die, dwarf::DW_AT_const_value, Block);
885 }
887 /// addTemplateParams - Add template parameters into buffer.
888 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
889 // Add template parameters.
890 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
891 DIDescriptor Element = TParams.getElement(i);
892 if (Element.isTemplateTypeParameter())
893 constructTemplateTypeParameterDIE(Buffer,
894 DITemplateTypeParameter(Element));
895 else if (Element.isTemplateValueParameter())
896 constructTemplateValueParameterDIE(Buffer,
897 DITemplateValueParameter(Element));
898 }
899 }
901 /// getOrCreateContextDIE - Get context owner's DIE.
902 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
903 if (!Context || Context.isFile())
904 return getUnitDie();
905 if (Context.isType())
906 return getOrCreateTypeDIE(DIType(Context));
907 if (Context.isNameSpace())
908 return getOrCreateNameSpace(DINameSpace(Context));
909 if (Context.isSubprogram())
910 return getOrCreateSubprogramDIE(DISubprogram(Context));
911 return getDIE(Context);
912 }
914 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
915 DIScope Context = resolve(Ty.getContext());
916 DIE *ContextDIE = getOrCreateContextDIE(Context);
918 DIE *TyDIE = getDIE(Ty);
919 if (TyDIE)
920 return TyDIE;
922 // Create new type.
923 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
925 constructTypeDIE(*TyDIE, Ty);
927 updateAcceleratorTables(Context, Ty, TyDIE);
928 return TyDIE;
929 }
931 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
932 /// given DIType.
933 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
934 if (!TyNode)
935 return NULL;
937 DIType Ty(TyNode);
938 assert(Ty.isType());
940 // Construct the context before querying for the existence of the DIE in case
941 // such construction creates the DIE.
942 DIScope Context = resolve(Ty.getContext());
943 DIE *ContextDIE = getOrCreateContextDIE(Context);
944 assert(ContextDIE);
946 DIE *TyDIE = getDIE(Ty);
947 if (TyDIE)
948 return TyDIE;
950 // Create new type.
951 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
953 if (Ty.isBasicType())
954 constructTypeDIE(*TyDIE, DIBasicType(Ty));
955 else if (Ty.isCompositeType()) {
956 DICompositeType CTy(Ty);
957 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
958 if (MDString *TypeId = CTy.getIdentifier()) {
959 DD->addDwarfTypeUnitType(getCUNode(), TypeId->getString(), TyDIE, CTy);
960 // Skip updating the accellerator tables since this is not the full type
961 return TyDIE;
962 }
963 constructTypeDIE(*TyDIE, CTy);
964 } else {
965 assert(Ty.isDerivedType() && "Unknown kind of DIType");
966 constructTypeDIE(*TyDIE, DIDerivedType(Ty));
967 }
969 updateAcceleratorTables(Context, Ty, TyDIE);
971 return TyDIE;
972 }
974 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
975 const DIE *TyDIE) {
976 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
977 bool IsImplementation = 0;
978 if (Ty.isCompositeType()) {
979 DICompositeType CT(Ty);
980 // A runtime language of 0 actually means C/C++ and that any
981 // non-negative value is some version of Objective-C/C++.
982 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
983 }
984 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
985 addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
987 if (!Context || Context.isCompileUnit() || Context.isFile() ||
988 Context.isNameSpace())
989 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
990 }
991 }
993 /// addType - Add a new type attribute to the specified entity.
994 void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
995 assert(Ty && "Trying to add a type that doesn't exist?");
997 // Check for pre-existence.
998 DIEEntry *Entry = getDIEEntry(Ty);
999 // If it exists then use the existing value.
1000 if (Entry) {
1001 addDIEEntry(Entity, Attribute, Entry);
1002 return;
1003 }
1005 // Construct type.
1006 DIE *Buffer = getOrCreateTypeDIE(Ty);
1008 // Set up proxy.
1009 Entry = createDIEEntry(Buffer);
1010 insertDIEEntry(Ty, Entry);
1011 addDIEEntry(Entity, Attribute, Entry);
1012 }
1014 // Accelerator table mutators - add each name along with its companion
1015 // DIE to the proper table while ensuring that the name that we're going
1016 // to reference is in the string table. We do this since the names we
1017 // add may not only be identical to the names in the DIE.
1018 void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
1019 if (!DD->useDwarfAccelTables()) return;
1020 DU->getStringPoolEntry(Name);
1021 std::vector<const DIE *> &DIEs = AccelNames[Name];
1022 DIEs.push_back(Die);
1023 }
1025 void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
1026 if (!DD->useDwarfAccelTables()) return;
1027 DU->getStringPoolEntry(Name);
1028 std::vector<const DIE *> &DIEs = AccelObjC[Name];
1029 DIEs.push_back(Die);
1030 }
1032 void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
1033 if (!DD->useDwarfAccelTables()) return;
1034 DU->getStringPoolEntry(Name);
1035 std::vector<const DIE *> &DIEs = AccelNamespace[Name];
1036 DIEs.push_back(Die);
1037 }
1039 void DwarfUnit::addAccelType(StringRef Name,
1040 std::pair<const DIE *, unsigned> Die) {
1041 if (!DD->useDwarfAccelTables()) return;
1042 DU->getStringPoolEntry(Name);
1043 std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
1044 DIEs.push_back(Die);
1045 }
1047 /// addGlobalName - Add a new global name to the compile unit.
1048 void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
1049 std::string FullName = getParentContextString(Context) + Name.str();
1050 GlobalNames[FullName] = Die;
1051 }
1053 /// getParentContextString - Walks the metadata parent chain in a language
1054 /// specific manner (using the compile unit language) and returns
1055 /// it as a string. This is done at the metadata level because DIEs may
1056 /// not currently have been added to the parent context and walking the
1057 /// DIEs looking for names is more expensive than walking the metadata.
1058 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1059 if (!Context)
1060 return "";
1062 // FIXME: Decide whether to implement this for non-C++ languages.
1063 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1064 return "";
1066 std::string CS;
1067 SmallVector<DIScope, 1> Parents;
1068 while (!Context.isCompileUnit()) {
1069 Parents.push_back(Context);
1070 if (Context.getContext())
1071 Context = resolve(Context.getContext());
1072 else
1073 // Structure, etc types will have a NULL context if they're at the top
1074 // level.
1075 break;
1076 }
1078 // Reverse iterate over our list to go from the outermost construct to the
1079 // innermost.
1080 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1081 E = Parents.rend();
1082 I != E; ++I) {
1083 DIScope Ctx = *I;
1084 StringRef Name = Ctx.getName();
1085 if (!Name.empty()) {
1086 CS += Name;
1087 CS += "::";
1088 }
1089 }
1090 return CS;
1091 }
1093 /// constructTypeDIE - Construct basic type die from DIBasicType.
1094 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1095 // Get core information.
1096 StringRef Name = BTy.getName();
1097 // Add name if not anonymous or intermediate type.
1098 if (!Name.empty())
1099 addString(&Buffer, dwarf::DW_AT_name, Name);
1101 // An unspecified type only has a name attribute.
1102 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1103 return;
1105 addUInt(&Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1106 BTy.getEncoding());
1108 uint64_t Size = BTy.getSizeInBits() >> 3;
1109 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1110 }
1112 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1113 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1114 // Get core information.
1115 StringRef Name = DTy.getName();
1116 uint64_t Size = DTy.getSizeInBits() >> 3;
1117 uint16_t Tag = Buffer.getTag();
1119 // Map to main type, void will not have a type.
1120 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1121 if (FromTy)
1122 addType(&Buffer, FromTy);
1124 // Add name if not anonymous or intermediate type.
1125 if (!Name.empty())
1126 addString(&Buffer, dwarf::DW_AT_name, Name);
1128 // Add size if non-zero (derived types might be zero-sized.)
1129 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1130 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1132 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1133 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1134 getOrCreateTypeDIE(resolve(DTy.getClassType())));
1135 // Add source line info if available and TyDesc is not a forward declaration.
1136 if (!DTy.isForwardDecl())
1137 addSourceLine(&Buffer, DTy);
1138 }
1140 /// constructTypeDIE - Construct type DIE from DICompositeType.
1141 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1142 // Add name if not anonymous or intermediate type.
1143 StringRef Name = CTy.getName();
1145 uint64_t Size = CTy.getSizeInBits() >> 3;
1146 uint16_t Tag = Buffer.getTag();
1148 switch (Tag) {
1149 case dwarf::DW_TAG_array_type:
1150 constructArrayTypeDIE(Buffer, CTy);
1151 break;
1152 case dwarf::DW_TAG_enumeration_type:
1153 constructEnumTypeDIE(Buffer, CTy);
1154 break;
1155 case dwarf::DW_TAG_subroutine_type: {
1156 // Add return type. A void return won't have a type.
1157 DIArray Elements = CTy.getTypeArray();
1158 DIType RTy(Elements.getElement(0));
1159 if (RTy)
1160 addType(&Buffer, RTy);
1162 bool isPrototyped = true;
1163 // Add arguments.
1164 for (unsigned i = 1, N = Elements.getNumElements(); i < N; ++i) {
1165 DIDescriptor Ty = Elements.getElement(i);
1166 if (Ty.isUnspecifiedParameter()) {
1167 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1168 isPrototyped = false;
1169 } else {
1170 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1171 addType(Arg, DIType(Ty));
1172 if (DIType(Ty).isArtificial())
1173 addFlag(Arg, dwarf::DW_AT_artificial);
1174 }
1175 }
1176 // Add prototype flag if we're dealing with a C language and the
1177 // function has been prototyped.
1178 uint16_t Language = getLanguage();
1179 if (isPrototyped &&
1180 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1181 Language == dwarf::DW_LANG_ObjC))
1182 addFlag(&Buffer, dwarf::DW_AT_prototyped);
1184 if (CTy.isLValueReference())
1185 addFlag(&Buffer, dwarf::DW_AT_reference);
1187 if (CTy.isRValueReference())
1188 addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
1189 } break;
1190 case dwarf::DW_TAG_structure_type:
1191 case dwarf::DW_TAG_union_type:
1192 case dwarf::DW_TAG_class_type: {
1193 // Add elements to structure type.
1194 DIArray Elements = CTy.getTypeArray();
1195 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1196 DIDescriptor Element = Elements.getElement(i);
1197 DIE *ElemDie = NULL;
1198 if (Element.isSubprogram())
1199 ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
1200 else if (Element.isDerivedType()) {
1201 DIDerivedType DDTy(Element);
1202 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1203 ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1204 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1205 dwarf::DW_AT_friend);
1206 } else if (DDTy.isStaticMember()) {
1207 getOrCreateStaticMemberDIE(DDTy);
1208 } else {
1209 constructMemberDIE(Buffer, DDTy);
1210 }
1211 } else if (Element.isObjCProperty()) {
1212 DIObjCProperty Property(Element);
1213 ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1214 StringRef PropertyName = Property.getObjCPropertyName();
1215 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1216 if (Property.getType())
1217 addType(ElemDie, Property.getType());
1218 addSourceLine(ElemDie, Property);
1219 StringRef GetterName = Property.getObjCPropertyGetterName();
1220 if (!GetterName.empty())
1221 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1222 StringRef SetterName = Property.getObjCPropertySetterName();
1223 if (!SetterName.empty())
1224 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1225 unsigned PropertyAttributes = 0;
1226 if (Property.isReadOnlyObjCProperty())
1227 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1228 if (Property.isReadWriteObjCProperty())
1229 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1230 if (Property.isAssignObjCProperty())
1231 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1232 if (Property.isRetainObjCProperty())
1233 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1234 if (Property.isCopyObjCProperty())
1235 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1236 if (Property.isNonAtomicObjCProperty())
1237 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1238 if (PropertyAttributes)
1239 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1240 PropertyAttributes);
1242 DIEEntry *Entry = getDIEEntry(Element);
1243 if (!Entry) {
1244 Entry = createDIEEntry(ElemDie);
1245 insertDIEEntry(Element, Entry);
1246 }
1247 } else
1248 continue;
1249 }
1251 if (CTy.isAppleBlockExtension())
1252 addFlag(&Buffer, dwarf::DW_AT_APPLE_block);
1254 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1255 if (ContainingType)
1256 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1257 getOrCreateTypeDIE(ContainingType));
1259 if (CTy.isObjcClassComplete())
1260 addFlag(&Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1262 // Add template parameters to a class, structure or union types.
1263 // FIXME: The support isn't in the metadata for this yet.
1264 if (Tag == dwarf::DW_TAG_class_type ||
1265 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1266 addTemplateParams(Buffer, CTy.getTemplateParams());
1268 break;
1269 }
1270 default:
1271 break;
1272 }
1274 // Add name if not anonymous or intermediate type.
1275 if (!Name.empty())
1276 addString(&Buffer, dwarf::DW_AT_name, Name);
1278 if (Tag == dwarf::DW_TAG_enumeration_type ||
1279 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1280 Tag == dwarf::DW_TAG_union_type) {
1281 // Add size if non-zero (derived types might be zero-sized.)
1282 // TODO: Do we care about size for enum forward declarations?
1283 if (Size)
1284 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1285 else if (!CTy.isForwardDecl())
1286 // Add zero size if it is not a forward declaration.
1287 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, 0);
1289 // If we're a forward decl, say so.
1290 if (CTy.isForwardDecl())
1291 addFlag(&Buffer, dwarf::DW_AT_declaration);
1293 // Add source line info if available.
1294 if (!CTy.isForwardDecl())
1295 addSourceLine(&Buffer, CTy);
1297 // No harm in adding the runtime language to the declaration.
1298 unsigned RLang = CTy.getRunTimeLang();
1299 if (RLang)
1300 addUInt(&Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1301 RLang);
1302 }
1303 }
1305 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1306 /// DITemplateTypeParameter.
1307 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1308 DITemplateTypeParameter TP) {
1309 DIE *ParamDIE =
1310 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1311 // Add the type if it exists, it could be void and therefore no type.
1312 if (TP.getType())
1313 addType(ParamDIE, resolve(TP.getType()));
1314 if (!TP.getName().empty())
1315 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1316 }
1318 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1319 /// DITemplateValueParameter.
1320 void
1321 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1322 DITemplateValueParameter VP) {
1323 DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1325 // Add the type if there is one, template template and template parameter
1326 // packs will not have a type.
1327 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1328 addType(ParamDIE, resolve(VP.getType()));
1329 if (!VP.getName().empty())
1330 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1331 if (Value *Val = VP.getValue()) {
1332 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1333 addConstantValue(ParamDIE, CI,
1334 isUnsignedDIType(DD, resolve(VP.getType())));
1335 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1336 // For declaration non-type template parameters (such as global values and
1337 // functions)
1338 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1339 addOpAddress(Block, Asm->getSymbol(GV));
1340 // Emit DW_OP_stack_value to use the address as the immediate value of the
1341 // parameter, rather than a pointer to it.
1342 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1343 addBlock(ParamDIE, dwarf::DW_AT_location, Block);
1344 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1345 assert(isa<MDString>(Val));
1346 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1347 cast<MDString>(Val)->getString());
1348 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1349 assert(isa<MDNode>(Val));
1350 DIArray A(cast<MDNode>(Val));
1351 addTemplateParams(*ParamDIE, A);
1352 }
1353 }
1354 }
1356 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1357 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1358 // Construct the context before querying for the existence of the DIE in case
1359 // such construction creates the DIE.
1360 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1362 DIE *NDie = getDIE(NS);
1363 if (NDie)
1364 return NDie;
1365 NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1367 if (!NS.getName().empty()) {
1368 addString(NDie, dwarf::DW_AT_name, NS.getName());
1369 addAccelNamespace(NS.getName(), NDie);
1370 addGlobalName(NS.getName(), NDie, NS.getContext());
1371 } else
1372 addAccelNamespace("(anonymous namespace)", NDie);
1373 addSourceLine(NDie, NS);
1374 return NDie;
1375 }
1377 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1378 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1379 // Construct the context before querying for the existence of the DIE in case
1380 // such construction creates the DIE (as is the case for member function
1381 // declarations).
1382 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1384 DIE *SPDie = getDIE(SP);
1385 if (SPDie)
1386 return SPDie;
1388 DISubprogram SPDecl = SP.getFunctionDeclaration();
1389 if (SPDecl.isSubprogram())
1390 // Add subprogram definitions to the CU die directly.
1391 ContextDIE = UnitDie.get();
1393 // DW_TAG_inlined_subroutine may refer to this DIE.
1394 SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1396 DIE *DeclDie = NULL;
1397 if (SPDecl.isSubprogram())
1398 DeclDie = getOrCreateSubprogramDIE(SPDecl);
1400 // Add function template parameters.
1401 addTemplateParams(*SPDie, SP.getTemplateParams());
1403 // If this DIE is going to refer declaration info using AT_specification
1404 // then there is no need to add other attributes.
1405 if (DeclDie) {
1406 // Refer function declaration directly.
1407 addDIEEntry(SPDie, dwarf::DW_AT_specification, DeclDie);
1409 return SPDie;
1410 }
1412 // Add the linkage name if we have one.
1413 StringRef LinkageName = SP.getLinkageName();
1414 if (!LinkageName.empty())
1415 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1416 GlobalValue::getRealLinkageName(LinkageName));
1418 // Constructors and operators for anonymous aggregates do not have names.
1419 if (!SP.getName().empty())
1420 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1422 addSourceLine(SPDie, SP);
1424 // Add the prototype if we have a prototype and we have a C like
1425 // language.
1426 uint16_t Language = getLanguage();
1427 if (SP.isPrototyped() &&
1428 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1429 Language == dwarf::DW_LANG_ObjC))
1430 addFlag(SPDie, dwarf::DW_AT_prototyped);
1432 DICompositeType SPTy = SP.getType();
1433 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1434 "the type of a subprogram should be a subroutine");
1436 DIArray Args = SPTy.getTypeArray();
1437 // Add a return type. If this is a type like a C/C++ void type we don't add a
1438 // return type.
1439 if (Args.getElement(0))
1440 addType(SPDie, DIType(Args.getElement(0)));
1442 unsigned VK = SP.getVirtuality();
1443 if (VK) {
1444 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1445 DIEBlock *Block = getDIEBlock();
1446 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1447 addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1448 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1449 ContainingTypeMap.insert(
1450 std::make_pair(SPDie, resolve(SP.getContainingType())));
1451 }
1453 if (!SP.isDefinition()) {
1454 addFlag(SPDie, dwarf::DW_AT_declaration);
1456 // Add arguments. Do not add arguments for subprogram definition. They will
1457 // be handled while processing variables.
1458 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1459 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, *SPDie);
1460 DIType ATy(Args.getElement(i));
1461 addType(Arg, ATy);
1462 if (ATy.isArtificial())
1463 addFlag(Arg, dwarf::DW_AT_artificial);
1464 }
1465 }
1467 if (SP.isArtificial())
1468 addFlag(SPDie, dwarf::DW_AT_artificial);
1470 if (!SP.isLocalToUnit())
1471 addFlag(SPDie, dwarf::DW_AT_external);
1473 if (SP.isOptimized())
1474 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1476 if (unsigned isa = Asm->getISAEncoding()) {
1477 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1478 }
1480 if (SP.isLValueReference())
1481 addFlag(SPDie, dwarf::DW_AT_reference);
1483 if (SP.isRValueReference())
1484 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1486 if (SP.isProtected())
1487 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1488 dwarf::DW_ACCESS_protected);
1489 else if (SP.isPrivate())
1490 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1491 dwarf::DW_ACCESS_private);
1492 else
1493 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1494 dwarf::DW_ACCESS_public);
1496 if (SP.isExplicit())
1497 addFlag(SPDie, dwarf::DW_AT_explicit);
1499 return SPDie;
1500 }
1502 // Return const expression if value is a GEP to access merged global
1503 // constant. e.g.
1504 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1505 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1506 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1507 if (!CE || CE->getNumOperands() != 3 ||
1508 CE->getOpcode() != Instruction::GetElementPtr)
1509 return NULL;
1511 // First operand points to a global struct.
1512 Value *Ptr = CE->getOperand(0);
1513 if (!isa<GlobalValue>(Ptr) ||
1514 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1515 return NULL;
1517 // Second operand is zero.
1518 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1519 if (!CI || !CI->isZero())
1520 return NULL;
1522 // Third operand is offset.
1523 if (!isa<ConstantInt>(CE->getOperand(2)))
1524 return NULL;
1526 return CE;
1527 }
1529 /// createGlobalVariableDIE - create global variable DIE.
1530 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1531 // Check for pre-existence.
1532 if (getDIE(GV))
1533 return;
1535 assert(GV.isGlobalVariable());
1537 DIScope GVContext = GV.getContext();
1538 DIType GTy = GV.getType();
1540 // If this is a static data member definition, some attributes belong
1541 // to the declaration DIE.
1542 DIE *VariableDIE = NULL;
1543 bool IsStaticMember = false;
1544 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1545 if (SDMDecl.Verify()) {
1546 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1547 // We need the declaration DIE that is in the static member's class.
1548 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1549 IsStaticMember = true;
1550 }
1552 // If this is not a static data member definition, create the variable
1553 // DIE and add the initial set of attributes to it.
1554 if (!VariableDIE) {
1555 // Construct the context before querying for the existence of the DIE in
1556 // case such construction creates the DIE.
1557 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1559 // Add to map.
1560 VariableDIE = createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1562 // Add name and type.
1563 addString(VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1564 addType(VariableDIE, GTy);
1566 // Add scoping info.
1567 if (!GV.isLocalToUnit())
1568 addFlag(VariableDIE, dwarf::DW_AT_external);
1570 // Add line number info.
1571 addSourceLine(VariableDIE, GV);
1572 }
1574 // Add location.
1575 bool addToAccelTable = false;
1576 DIE *VariableSpecDIE = NULL;
1577 bool isGlobalVariable = GV.getGlobal() != NULL;
1578 if (isGlobalVariable) {
1579 addToAccelTable = true;
1580 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1581 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1582 if (GV.getGlobal()->isThreadLocal()) {
1583 // FIXME: Make this work with -gsplit-dwarf.
1584 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1585 assert((PointerSize == 4 || PointerSize == 8) &&
1586 "Add support for other sizes if necessary");
1587 const MCExpr *Expr =
1588 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym);
1589 // Based on GCC's support for TLS:
1590 if (!DD->useSplitDwarf()) {
1591 // 1) Start with a constNu of the appropriate pointer size
1592 addUInt(Block, dwarf::DW_FORM_data1,
1593 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1594 // 2) containing the (relocated) offset of the TLS variable
1595 // within the module's TLS block.
1596 addExpr(Block, dwarf::DW_FORM_udata, Expr);
1597 } else {
1598 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1599 addUInt(Block, dwarf::DW_FORM_udata, DU->getAddrPoolIndex(Expr));
1600 }
1601 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1602 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1603 } else {
1604 DD->addArangeLabel(SymbolCU(this, Sym));
1605 addOpAddress(Block, Sym);
1606 }
1607 // Do not create specification DIE if context is either compile unit
1608 // or a subprogram.
1609 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1610 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1611 // Create specification DIE.
1612 VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
1613 addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
1614 addBlock(VariableSpecDIE, dwarf::DW_AT_location, Block);
1615 // A static member's declaration is already flagged as such.
1616 if (!SDMDecl.Verify())
1617 addFlag(VariableDIE, dwarf::DW_AT_declaration);
1618 } else {
1619 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1620 }
1621 // Add the linkage name.
1622 StringRef LinkageName = GV.getLinkageName();
1623 if (!LinkageName.empty())
1624 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1625 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1626 // TAG_variable.
1627 addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
1628 : VariableDIE,
1629 dwarf::DW_AT_MIPS_linkage_name,
1630 GlobalValue::getRealLinkageName(LinkageName));
1631 } else if (const ConstantInt *CI =
1632 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1633 // AT_const_value was added when the static member was created. To avoid
1634 // emitting AT_const_value multiple times, we only add AT_const_value when
1635 // it is not a static member.
1636 if (!IsStaticMember)
1637 addConstantValue(VariableDIE, CI, isUnsignedDIType(DD, GTy));
1638 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1639 addToAccelTable = true;
1640 // GV is a merged global.
1641 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1642 Value *Ptr = CE->getOperand(0);
1643 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1644 DD->addArangeLabel(SymbolCU(this, Sym));
1645 addOpAddress(Block, Sym);
1646 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1647 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1648 addUInt(Block, dwarf::DW_FORM_udata,
1649 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1650 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1651 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1652 }
1654 if (addToAccelTable) {
1655 DIE *AddrDIE = VariableSpecDIE ? VariableSpecDIE : VariableDIE;
1656 addAccelName(GV.getName(), AddrDIE);
1658 // If the linkage name is different than the name, go ahead and output
1659 // that as well into the name table.
1660 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1661 addAccelName(GV.getLinkageName(), AddrDIE);
1662 }
1664 if (!GV.isLocalToUnit())
1665 addGlobalName(GV.getName(), VariableSpecDIE ? VariableSpecDIE : VariableDIE,
1666 GV.getContext());
1667 }
1669 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1670 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1671 DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1672 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
1674 // The LowerBound value defines the lower bounds which is typically zero for
1675 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1676 // Count == -1 then the array is unbounded and we do not emit
1677 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1678 // Count == 0, then the array has zero elements in which case we do not emit
1679 // an upper bound.
1680 int64_t LowerBound = SR.getLo();
1681 int64_t DefaultLowerBound = getDefaultLowerBound();
1682 int64_t Count = SR.getCount();
1684 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1685 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1687 if (Count != -1 && Count != 0)
1688 // FIXME: An unbounded array should reference the expression that defines
1689 // the array.
1690 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1691 LowerBound + Count - 1);
1692 }
1694 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1695 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1696 if (CTy.isVector())
1697 addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
1699 // Emit the element type.
1700 addType(&Buffer, resolve(CTy.getTypeDerivedFrom()));
1702 // Get an anonymous type for index type.
1703 // FIXME: This type should be passed down from the front end
1704 // as different languages may have different sizes for indexes.
1705 DIE *IdxTy = getIndexTyDie();
1706 if (!IdxTy) {
1707 // Construct an anonymous type for index type.
1708 IdxTy = createAndAddDIE(dwarf::DW_TAG_base_type, *UnitDie);
1709 addString(IdxTy, dwarf::DW_AT_name, "int");
1710 addUInt(IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int32_t));
1711 addUInt(IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1712 dwarf::DW_ATE_signed);
1713 setIndexTyDie(IdxTy);
1714 }
1716 // Add subranges to array type.
1717 DIArray Elements = CTy.getTypeArray();
1718 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1719 DIDescriptor Element = Elements.getElement(i);
1720 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1721 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1722 }
1723 }
1725 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1726 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1727 DIArray Elements = CTy.getTypeArray();
1729 // Add enumerators to enumeration type.
1730 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1731 DIEnumerator Enum(Elements.getElement(i));
1732 if (Enum.isEnumerator()) {
1733 DIE *Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1734 StringRef Name = Enum.getName();
1735 addString(Enumerator, dwarf::DW_AT_name, Name);
1736 int64_t Value = Enum.getEnumValue();
1737 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1738 Value);
1739 }
1740 }
1741 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1742 if (DTy) {
1743 addType(&Buffer, DTy);
1744 addFlag(&Buffer, dwarf::DW_AT_enum_class);
1745 }
1746 }
1748 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1749 /// vtables.
1750 void DwarfUnit::constructContainingTypeDIEs() {
1751 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1752 CE = ContainingTypeMap.end();
1753 CI != CE; ++CI) {
1754 DIE *SPDie = CI->first;
1755 DIDescriptor D(CI->second);
1756 if (!D)
1757 continue;
1758 DIE *NDie = getDIE(D);
1759 if (!NDie)
1760 continue;
1761 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, NDie);
1762 }
1763 }
1765 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1766 DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
1767 StringRef Name = DV.getName();
1769 // Define variable debug information entry.
1770 DIE *VariableDie = new DIE(DV.getTag());
1771 DbgVariable *AbsVar = DV.getAbstractVariable();
1772 DIE *AbsDIE = AbsVar ? AbsVar->getDIE() : NULL;
1773 if (AbsDIE)
1774 addDIEEntry(VariableDie, dwarf::DW_AT_abstract_origin, AbsDIE);
1775 else {
1776 if (!Name.empty())
1777 addString(VariableDie, dwarf::DW_AT_name, Name);
1778 addSourceLine(VariableDie, DV.getVariable());
1779 addType(VariableDie, DV.getType());
1780 }
1782 if (DV.isArtificial())
1783 addFlag(VariableDie, dwarf::DW_AT_artificial);
1785 if (isScopeAbstract) {
1786 DV.setDIE(VariableDie);
1787 return VariableDie;
1788 }
1790 // Add variable address.
1792 unsigned Offset = DV.getDotDebugLocOffset();
1793 if (Offset != ~0U) {
1794 addSectionLabel(VariableDie, dwarf::DW_AT_location,
1795 Asm->GetTempSymbol("debug_loc", Offset));
1796 DV.setDIE(VariableDie);
1797 return VariableDie;
1798 }
1800 // Check if variable is described by a DBG_VALUE instruction.
1801 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1802 assert(DVInsn->getNumOperands() == 3);
1803 if (DVInsn->getOperand(0).isReg()) {
1804 const MachineOperand RegOp = DVInsn->getOperand(0);
1805 // If the second operand is an immediate, this is an indirect value.
1806 if (DVInsn->getOperand(1).isImm()) {
1807 MachineLocation Location(RegOp.getReg(),
1808 DVInsn->getOperand(1).getImm());
1809 addVariableAddress(DV, VariableDie, Location);
1810 } else if (RegOp.getReg())
1811 addVariableAddress(DV, VariableDie, MachineLocation(RegOp.getReg()));
1812 } else if (DVInsn->getOperand(0).isImm())
1813 addConstantValue(VariableDie, DVInsn->getOperand(0), DV.getType());
1814 else if (DVInsn->getOperand(0).isFPImm())
1815 addConstantFPValue(VariableDie, DVInsn->getOperand(0));
1816 else if (DVInsn->getOperand(0).isCImm())
1817 addConstantValue(VariableDie, DVInsn->getOperand(0).getCImm(),
1818 isUnsignedDIType(DD, DV.getType()));
1820 DV.setDIE(VariableDie);
1821 return VariableDie;
1822 } else {
1823 // .. else use frame index.
1824 int FI = DV.getFrameIndex();
1825 if (FI != ~0) {
1826 unsigned FrameReg = 0;
1827 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1828 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1829 MachineLocation Location(FrameReg, Offset);
1830 addVariableAddress(DV, VariableDie, Location);
1831 }
1832 }
1834 DV.setDIE(VariableDie);
1835 return VariableDie;
1836 }
1838 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1839 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1840 DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1841 StringRef Name = DT.getName();
1842 if (!Name.empty())
1843 addString(MemberDie, dwarf::DW_AT_name, Name);
1845 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1847 addSourceLine(MemberDie, DT);
1849 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1851 // For C++, virtual base classes are not at fixed offset. Use following
1852 // expression to extract appropriate offset from vtable.
1853 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1855 DIEBlock *VBaseLocationDie = new (DIEValueAllocator) DIEBlock();
1856 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1857 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1858 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1859 addUInt(VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1860 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1861 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1862 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1864 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1865 } else {
1866 uint64_t Size = DT.getSizeInBits();
1867 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1868 uint64_t OffsetInBytes;
1870 if (Size != FieldSize) {
1871 // Handle bitfield.
1872 addUInt(MemberDie, dwarf::DW_AT_byte_size, None,
1873 getBaseTypeSize(DD, DT) >> 3);
1874 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, DT.getSizeInBits());
1876 uint64_t Offset = DT.getOffsetInBits();
1877 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1878 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1879 uint64_t FieldOffset = (HiMark - FieldSize);
1880 Offset -= FieldOffset;
1882 // Maybe we need to work from the other end.
1883 if (Asm->getDataLayout().isLittleEndian())
1884 Offset = FieldSize - (Offset + Size);
1885 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1887 // Here DW_AT_data_member_location points to the anonymous
1888 // field that includes this bit field.
1889 OffsetInBytes = FieldOffset >> 3;
1890 } else
1891 // This is not a bitfield.
1892 OffsetInBytes = DT.getOffsetInBits() >> 3;
1894 if (DD->getDwarfVersion() <= 2) {
1895 DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
1896 addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1897 addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1898 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1899 } else
1900 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1901 OffsetInBytes);
1902 }
1904 if (DT.isProtected())
1905 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1906 dwarf::DW_ACCESS_protected);
1907 else if (DT.isPrivate())
1908 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1909 dwarf::DW_ACCESS_private);
1910 // Otherwise C++ member and base classes are considered public.
1911 else
1912 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1913 dwarf::DW_ACCESS_public);
1914 if (DT.isVirtual())
1915 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1916 dwarf::DW_VIRTUALITY_virtual);
1918 // Objective-C properties.
1919 if (MDNode *PNode = DT.getObjCProperty())
1920 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1921 MemberDie->addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1922 PropertyDie);
1924 if (DT.isArtificial())
1925 addFlag(MemberDie, dwarf::DW_AT_artificial);
1926 }
1928 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1929 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1930 if (!DT.Verify())
1931 return NULL;
1933 // Construct the context before querying for the existence of the DIE in case
1934 // such construction creates the DIE.
1935 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1936 assert(dwarf::isType(ContextDIE->getTag()) &&
1937 "Static member should belong to a type.");
1939 DIE *StaticMemberDIE = getDIE(DT);
1940 if (StaticMemberDIE)
1941 return StaticMemberDIE;
1943 StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1945 DIType Ty = resolve(DT.getTypeDerivedFrom());
1947 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1948 addType(StaticMemberDIE, Ty);
1949 addSourceLine(StaticMemberDIE, DT);
1950 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1951 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1953 // FIXME: We could omit private if the parent is a class_type, and
1954 // public if the parent is something else.
1955 if (DT.isProtected())
1956 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1957 dwarf::DW_ACCESS_protected);
1958 else if (DT.isPrivate())
1959 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1960 dwarf::DW_ACCESS_private);
1961 else
1962 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1963 dwarf::DW_ACCESS_public);
1965 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1966 addConstantValue(StaticMemberDIE, CI, isUnsignedDIType(DD, Ty));
1967 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1968 addConstantFPValue(StaticMemberDIE, CFP);
1970 return StaticMemberDIE;
1971 }
1973 void DwarfUnit::emitHeader(const MCSection *ASection,
1974 const MCSymbol *ASectionSym) const {
1975 Asm->OutStreamer.AddComment("DWARF version number");
1976 Asm->EmitInt16(DD->getDwarfVersion());
1977 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1978 // We share one abbreviations table across all units so it's always at the
1979 // start of the section. Use a relocatable offset where needed to ensure
1980 // linking doesn't invalidate that offset.
1981 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1982 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1983 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1984 }
1986 DwarfCompileUnit::~DwarfCompileUnit() {}
1987 DwarfTypeUnit::~DwarfTypeUnit() {}
1989 void DwarfTypeUnit::emitHeader(const MCSection *ASection,
1990 const MCSymbol *ASectionSym) const {
1991 DwarfUnit::emitHeader(ASection, ASectionSym);
1992 Asm->OutStreamer.AddComment("Type Signature");
1993 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
1994 Asm->OutStreamer.AddComment("Type DIE Offset");
1995 // In a skeleton type unit there is no type DIE so emit a zero offset.
1996 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
1997 sizeof(Ty->getOffset()));
1998 }
2000 void DwarfTypeUnit::initSection(const MCSection *Section) {
2001 assert(!this->Section);
2002 this->Section = Section;
2003 // Since each type unit is contained in its own COMDAT section, the begin
2004 // label and the section label are the same. Using the begin label emission in
2005 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2006 // the only other alternative of lazily constructing start-of-section labels
2007 // and storing a mapping in DwarfDebug (or AsmPrinter).
2008 this->SectionSym = this->LabelBegin =
2009 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2010 this->LabelEnd =
2011 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2012 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
2013 }