ddc1c2f4bc0d0b68531bcc43a69834517d58be83
1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DwarfUnit.h"
17 #include "DwarfAccelTable.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/IR/Constants.h"
21 #include "llvm/IR/DIBuilder.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCContext.h"
28 #include "llvm/MC/MCSection.h"
29 #include "llvm/MC/MCStreamer.h"
30 #include "llvm/Support/CommandLine.h"
31 #include "llvm/Target/TargetFrameLowering.h"
32 #include "llvm/Target/TargetLoweringObjectFile.h"
33 #include "llvm/Target/TargetMachine.h"
34 #include "llvm/Target/TargetRegisterInfo.h"
36 using namespace llvm;
38 static cl::opt<bool>
39 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
40 cl::desc("Generate DWARF4 type units."),
41 cl::init(false));
43 /// Unit - Unit constructor.
44 DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
45 DwarfDebug *DW, DwarfFile *DWU)
46 : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
47 DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
48 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
49 }
51 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
52 AsmPrinter *A, DwarfDebug *DW,
53 DwarfFile *DWU)
54 : DwarfUnit(UID, D, Node, A, DW, DWU) {
55 insertDIE(Node, D);
56 }
58 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DwarfCompileUnit &CU,
59 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
60 : DwarfUnit(UID, D, CU.getCUNode(), A, DW, DWU), CU(CU) {}
62 /// ~Unit - Destructor for compile unit.
63 DwarfUnit::~DwarfUnit() {
64 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
65 DIEBlocks[j]->~DIEBlock();
66 for (unsigned j = 0, M = DIELocs.size(); j < M; ++j)
67 DIELocs[j]->~DIELoc();
68 }
70 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
71 /// information entry.
72 DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
73 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
74 return Value;
75 }
77 /// getDefaultLowerBound - Return the default lower bound for an array. If the
78 /// DWARF version doesn't handle the language, return -1.
79 int64_t DwarfUnit::getDefaultLowerBound() const {
80 switch (getLanguage()) {
81 default:
82 break;
84 case dwarf::DW_LANG_C89:
85 case dwarf::DW_LANG_C99:
86 case dwarf::DW_LANG_C:
87 case dwarf::DW_LANG_C_plus_plus:
88 case dwarf::DW_LANG_ObjC:
89 case dwarf::DW_LANG_ObjC_plus_plus:
90 return 0;
92 case dwarf::DW_LANG_Fortran77:
93 case dwarf::DW_LANG_Fortran90:
94 case dwarf::DW_LANG_Fortran95:
95 return 1;
97 // The languages below have valid values only if the DWARF version >= 4.
98 case dwarf::DW_LANG_Java:
99 case dwarf::DW_LANG_Python:
100 case dwarf::DW_LANG_UPC:
101 case dwarf::DW_LANG_D:
102 if (dwarf::DWARF_VERSION >= 4)
103 return 0;
104 break;
106 case dwarf::DW_LANG_Ada83:
107 case dwarf::DW_LANG_Ada95:
108 case dwarf::DW_LANG_Cobol74:
109 case dwarf::DW_LANG_Cobol85:
110 case dwarf::DW_LANG_Modula2:
111 case dwarf::DW_LANG_Pascal83:
112 case dwarf::DW_LANG_PLI:
113 if (dwarf::DWARF_VERSION >= 4)
114 return 1;
115 break;
116 }
118 return -1;
119 }
121 /// Check whether the DIE for this MDNode can be shared across CUs.
122 static bool isShareableAcrossCUs(DIDescriptor D) {
123 // When the MDNode can be part of the type system, the DIE can be shared
124 // across CUs.
125 // Combining type units and cross-CU DIE sharing is lower value (since
126 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
127 // level already) but may be implementable for some value in projects
128 // building multiple independent libraries with LTO and then linking those
129 // together.
130 return (D.isType() ||
131 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
132 !GenerateDwarfTypeUnits;
133 }
135 /// getDIE - Returns the debug information entry map slot for the
136 /// specified debug variable. We delegate the request to DwarfDebug
137 /// when the DIE for this MDNode can be shared across CUs. The mappings
138 /// will be kept in DwarfDebug for shareable DIEs.
139 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
140 if (isShareableAcrossCUs(D))
141 return DD->getDIE(D);
142 return MDNodeToDieMap.lookup(D);
143 }
145 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
146 /// when the DIE for this MDNode can be shared across CUs. The mappings
147 /// will be kept in DwarfDebug for shareable DIEs.
148 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
149 if (isShareableAcrossCUs(Desc)) {
150 DD->insertDIE(Desc, D);
151 return;
152 }
153 MDNodeToDieMap.insert(std::make_pair(Desc, D));
154 }
156 /// addFlag - Add a flag that is true.
157 void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
158 if (DD->getDwarfVersion() >= 4)
159 Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
160 else
161 Die->addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
162 }
164 /// addUInt - Add an unsigned integer attribute data and value.
165 ///
166 void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
167 Optional<dwarf::Form> Form, uint64_t Integer) {
168 if (!Form)
169 Form = DIEInteger::BestForm(false, Integer);
170 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
171 DIEInteger(Integer);
172 Die->addValue(Attribute, *Form, Value);
173 }
175 void DwarfUnit::addUInt(DIE *Block, dwarf::Form Form, uint64_t Integer) {
176 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
177 }
179 /// addSInt - Add an signed integer attribute data and value.
180 ///
181 void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
182 Optional<dwarf::Form> Form, int64_t Integer) {
183 if (!Form)
184 Form = DIEInteger::BestForm(true, Integer);
185 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
186 Die->addValue(Attribute, *Form, Value);
187 }
189 void DwarfUnit::addSInt(DIELoc *Die, Optional<dwarf::Form> Form,
190 int64_t Integer) {
191 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
192 }
194 /// addString - Add a string attribute data and value. We always emit a
195 /// reference to the string pool instead of immediate strings so that DIEs have
196 /// more predictable sizes. In the case of split dwarf we emit an index
197 /// into another table which gets us the static offset into the string
198 /// table.
199 void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
200 StringRef String) {
202 if (!DD->useSplitDwarf())
203 return addLocalString(Die, Attribute, String);
205 unsigned idx = DU->getStringPoolIndex(String);
206 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
207 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
208 Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
209 }
211 /// addLocalString - Add a string attribute data and value. This is guaranteed
212 /// to be in the local string pool instead of indirected.
213 void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
214 StringRef String) {
215 MCSymbol *Symb = DU->getStringPoolEntry(String);
216 DIEValue *Value;
217 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
218 Value = new (DIEValueAllocator) DIELabel(Symb);
219 else {
220 MCSymbol *StringPool = DU->getStringPoolSym();
221 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
222 }
223 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
224 Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
225 }
227 /// addExpr - Add a Dwarf expression attribute data and value.
228 ///
229 void DwarfUnit::addExpr(DIELoc *Die, dwarf::Form Form, const MCExpr *Expr) {
230 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
231 Die->addValue((dwarf::Attribute)0, Form, Value);
232 }
234 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
235 ///
236 void DwarfUnit::addLocationList(DIE *Die, dwarf::Attribute Attribute,
237 unsigned Index) {
238 DIEValue *Value = new (DIEValueAllocator) DIELocList(Index);
239 dwarf::Form Form = DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
240 : dwarf::DW_FORM_data4;
241 Die->addValue(Attribute, Form, Value);
242 }
244 /// addLabel - Add a Dwarf label attribute data and value.
245 ///
246 void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
247 const MCSymbol *Label) {
248 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
249 Die->addValue(Attribute, Form, Value);
250 }
252 void DwarfUnit::addLabel(DIELoc *Die, dwarf::Form Form, const MCSymbol *Label) {
253 addLabel(Die, (dwarf::Attribute)0, Form, Label);
254 }
256 /// addSectionLabel - Add a Dwarf section label attribute data and value.
257 ///
258 void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
259 const MCSymbol *Label) {
260 if (DD->getDwarfVersion() >= 4)
261 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
262 else
263 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
264 }
266 /// addSectionOffset - Add an offset into a section attribute data and value.
267 ///
268 void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
269 uint64_t Integer) {
270 if (DD->getDwarfVersion() >= 4)
271 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
272 else
273 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
274 }
276 /// addLabelAddress - Add a dwarf label attribute data and value using
277 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
278 ///
279 void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
280 MCSymbol *Label) {
281 if (Label)
282 DD->addArangeLabel(SymbolCU(this, Label));
284 if (!DD->useSplitDwarf()) {
285 if (Label) {
286 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
287 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
288 } else {
289 DIEValue *Value = new (DIEValueAllocator) DIEInteger(0);
290 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
291 }
292 } else {
293 unsigned idx = DU->getAddrPoolIndex(Label);
294 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
295 Die->addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
296 }
297 }
299 /// addOpAddress - Add a dwarf op address data and value using the
300 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
301 ///
302 void DwarfUnit::addOpAddress(DIELoc *Die, const MCSymbol *Sym) {
303 if (!DD->useSplitDwarf()) {
304 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
305 addLabel(Die, dwarf::DW_FORM_udata, Sym);
306 } else {
307 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
308 addUInt(Die, dwarf::DW_FORM_GNU_addr_index, DU->getAddrPoolIndex(Sym));
309 }
310 }
312 /// addSectionDelta - Add a section label delta attribute data and value.
313 ///
314 void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
315 const MCSymbol *Hi, const MCSymbol *Lo) {
316 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
317 if (DD->getDwarfVersion() >= 4)
318 Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
319 else
320 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
321 }
323 /// addDIEEntry - Add a DIE attribute data and value.
324 ///
325 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
326 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
327 }
329 void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
330 Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
331 new (DIEValueAllocator) DIETypeSignature(Type));
332 }
334 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
335 DIEEntry *Entry) {
336 const DIE *DieCU = Die->getUnitOrNull();
337 const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
338 if (!DieCU)
339 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
340 DieCU = getUnitDie();
341 if (!EntryCU)
342 EntryCU = getUnitDie();
343 Die->addValue(Attribute, EntryCU == DieCU ? dwarf::DW_FORM_ref4
344 : dwarf::DW_FORM_ref_addr,
345 Entry);
346 }
348 /// Create a DIE with the given Tag, add the DIE to its parent, and
349 /// call insertDIE if MD is not null.
350 DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
351 DIE *Die = new DIE(Tag);
352 Parent.addChild(Die);
353 if (N)
354 insertDIE(N, Die);
355 return Die;
356 }
358 /// addBlock - Add block data.
359 ///
360 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIELoc *Loc) {
361 Loc->ComputeSize(Asm);
362 DIELocs.push_back(Loc); // Memoize so we can call the destructor later on.
363 Die->addValue(Attribute, Loc->BestForm(DD->getDwarfVersion()), Loc);
364 }
366 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
367 DIEBlock *Block) {
368 Block->ComputeSize(Asm);
369 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
370 Die->addValue(Attribute, Block->BestForm(), Block);
371 }
373 /// addSourceLine - Add location information to specified debug information
374 /// entry.
375 void DwarfUnit::addSourceLine(DIE *Die, unsigned Line, StringRef File,
376 StringRef Directory) {
377 if (Line == 0)
378 return;
380 unsigned FileID =
381 DD->getOrCreateSourceID(File, Directory, getCU().getUniqueID());
382 assert(FileID && "Invalid file id");
383 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
384 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
385 }
387 /// addSourceLine - Add location information to specified debug information
388 /// entry.
389 void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
390 assert(V.isVariable());
392 addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
393 V.getContext().getDirectory());
394 }
396 /// addSourceLine - Add location information to specified debug information
397 /// entry.
398 void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
399 assert(G.isGlobalVariable());
401 addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
402 }
404 /// addSourceLine - Add location information to specified debug information
405 /// entry.
406 void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
407 assert(SP.isSubprogram());
409 addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
410 }
412 /// addSourceLine - Add location information to specified debug information
413 /// entry.
414 void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
415 assert(Ty.isType());
417 addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
418 }
420 /// addSourceLine - Add location information to specified debug information
421 /// entry.
422 void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
423 assert(Ty.isObjCProperty());
425 DIFile File = Ty.getFile();
426 addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
427 File.getDirectory());
428 }
430 /// addSourceLine - Add location information to specified debug information
431 /// entry.
432 void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
433 assert(NS.Verify());
435 addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
436 }
438 /// addVariableAddress - Add DW_AT_location attribute for a
439 /// DbgVariable based on provided MachineLocation.
440 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
441 MachineLocation Location) {
442 if (DV.variableHasComplexAddress())
443 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
444 else if (DV.isBlockByrefVariable())
445 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
446 else
447 addAddress(Die, dwarf::DW_AT_location, Location,
448 DV.getVariable().isIndirect());
449 }
451 /// addRegisterOp - Add register operand.
452 void DwarfUnit::addRegisterOp(DIELoc *TheDie, unsigned Reg) {
453 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
454 int DWReg = RI->getDwarfRegNum(Reg, false);
455 bool isSubRegister = DWReg < 0;
457 unsigned Idx = 0;
459 // Go up the super-register chain until we hit a valid dwarf register number.
460 for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
461 DWReg = RI->getDwarfRegNum(*SR, false);
462 if (DWReg >= 0)
463 Idx = RI->getSubRegIndex(*SR, Reg);
464 }
466 if (DWReg < 0) {
467 DEBUG(dbgs() << "Invalid Dwarf register number.\n");
468 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
469 return;
470 }
472 // Emit register
473 if (DWReg < 32)
474 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
475 else {
476 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
477 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
478 }
480 // Emit Mask
481 if (isSubRegister) {
482 unsigned Size = RI->getSubRegIdxSize(Idx);
483 unsigned Offset = RI->getSubRegIdxOffset(Idx);
484 if (Offset > 0) {
485 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
486 addUInt(TheDie, dwarf::DW_FORM_data1, Size);
487 addUInt(TheDie, dwarf::DW_FORM_data1, Offset);
488 } else {
489 unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
490 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
491 addUInt(TheDie, dwarf::DW_FORM_data1, ByteSize);
492 }
493 }
494 }
496 /// addRegisterOffset - Add register offset.
497 void DwarfUnit::addRegisterOffset(DIELoc *TheDie, unsigned Reg,
498 int64_t Offset) {
499 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
500 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
501 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
502 if (Reg == TRI->getFrameRegister(*Asm->MF))
503 // If variable offset is based in frame register then use fbreg.
504 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
505 else if (DWReg < 32)
506 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
507 else {
508 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
509 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
510 }
511 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
512 }
514 /// addAddress - Add an address attribute to a die based on the location
515 /// provided.
516 void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
517 const MachineLocation &Location, bool Indirect) {
518 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
520 if (Location.isReg() && !Indirect)
521 addRegisterOp(Loc, Location.getReg());
522 else {
523 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
524 if (Indirect && !Location.isReg()) {
525 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
526 }
527 }
529 // Now attach the location information to the DIE.
530 addBlock(Die, Attribute, Loc);
531 }
533 /// addComplexAddress - Start with the address based on the location provided,
534 /// and generate the DWARF information necessary to find the actual variable
535 /// given the extra address information encoded in the DbgVariable, starting
536 /// from the starting location. Add the DWARF information to the die.
537 ///
538 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
539 dwarf::Attribute Attribute,
540 const MachineLocation &Location) {
541 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
542 unsigned N = DV.getNumAddrElements();
543 unsigned i = 0;
544 if (Location.isReg()) {
545 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
546 // If first address element is OpPlus then emit
547 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
548 addRegisterOffset(Loc, Location.getReg(), DV.getAddrElement(1));
549 i = 2;
550 } else
551 addRegisterOp(Loc, Location.getReg());
552 } else
553 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
555 for (; i < N; ++i) {
556 uint64_t Element = DV.getAddrElement(i);
557 if (Element == DIBuilder::OpPlus) {
558 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
559 addUInt(Loc, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
560 } else if (Element == DIBuilder::OpDeref) {
561 if (!Location.isReg())
562 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
563 } else
564 llvm_unreachable("unknown DIBuilder Opcode");
565 }
567 // Now attach the location information to the DIE.
568 addBlock(Die, Attribute, Loc);
569 }
571 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
572 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
573 gives the variable VarName either the struct, or a pointer to the struct, as
574 its type. This is necessary for various behind-the-scenes things the
575 compiler needs to do with by-reference variables in Blocks.
577 However, as far as the original *programmer* is concerned, the variable
578 should still have type 'SomeType', as originally declared.
580 The function getBlockByrefType dives into the __Block_byref_x_VarName
581 struct to find the original type of the variable, which is then assigned to
582 the variable's Debug Information Entry as its real type. So far, so good.
583 However now the debugger will expect the variable VarName to have the type
584 SomeType. So we need the location attribute for the variable to be an
585 expression that explains to the debugger how to navigate through the
586 pointers and struct to find the actual variable of type SomeType.
588 The following function does just that. We start by getting
589 the "normal" location for the variable. This will be the location
590 of either the struct __Block_byref_x_VarName or the pointer to the
591 struct __Block_byref_x_VarName.
593 The struct will look something like:
595 struct __Block_byref_x_VarName {
596 ... <various fields>
597 struct __Block_byref_x_VarName *forwarding;
598 ... <various other fields>
599 SomeType VarName;
600 ... <maybe more fields>
601 };
603 If we are given the struct directly (as our starting point) we
604 need to tell the debugger to:
606 1). Add the offset of the forwarding field.
608 2). Follow that pointer to get the real __Block_byref_x_VarName
609 struct to use (the real one may have been copied onto the heap).
611 3). Add the offset for the field VarName, to find the actual variable.
613 If we started with a pointer to the struct, then we need to
614 dereference that pointer first, before the other steps.
615 Translating this into DWARF ops, we will need to append the following
616 to the current location description for the variable:
618 DW_OP_deref -- optional, if we start with a pointer
619 DW_OP_plus_uconst <forward_fld_offset>
620 DW_OP_deref
621 DW_OP_plus_uconst <varName_fld_offset>
623 That is what this function does. */
625 /// addBlockByrefAddress - Start with the address based on the location
626 /// provided, and generate the DWARF information necessary to find the
627 /// actual Block variable (navigating the Block struct) based on the
628 /// starting location. Add the DWARF information to the die. For
629 /// more information, read large comment just above here.
630 ///
631 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
632 dwarf::Attribute Attribute,
633 const MachineLocation &Location) {
634 DIType Ty = DV.getType();
635 DIType TmpTy = Ty;
636 uint16_t Tag = Ty.getTag();
637 bool isPointer = false;
639 StringRef varName = DV.getName();
641 if (Tag == dwarf::DW_TAG_pointer_type) {
642 DIDerivedType DTy(Ty);
643 TmpTy = resolve(DTy.getTypeDerivedFrom());
644 isPointer = true;
645 }
647 DICompositeType blockStruct(TmpTy);
649 // Find the __forwarding field and the variable field in the __Block_byref
650 // struct.
651 DIArray Fields = blockStruct.getTypeArray();
652 DIDerivedType varField;
653 DIDerivedType forwardingField;
655 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
656 DIDerivedType DT(Fields.getElement(i));
657 StringRef fieldName = DT.getName();
658 if (fieldName == "__forwarding")
659 forwardingField = DT;
660 else if (fieldName == varName)
661 varField = DT;
662 }
664 // Get the offsets for the forwarding field and the variable field.
665 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
666 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
668 // Decode the original location, and use that as the start of the byref
669 // variable's location.
670 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
672 if (Location.isReg())
673 addRegisterOp(Loc, Location.getReg());
674 else
675 addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
677 // If we started with a pointer to the __Block_byref... struct, then
678 // the first thing we need to do is dereference the pointer (DW_OP_deref).
679 if (isPointer)
680 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
682 // Next add the offset for the '__forwarding' field:
683 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
684 // adding the offset if it's 0.
685 if (forwardingFieldOffset > 0) {
686 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
687 addUInt(Loc, dwarf::DW_FORM_udata, forwardingFieldOffset);
688 }
690 // Now dereference the __forwarding field to get to the real __Block_byref
691 // struct: DW_OP_deref.
692 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
694 // Now that we've got the real __Block_byref... struct, add the offset
695 // for the variable's field to get to the location of the actual variable:
696 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
697 if (varFieldOffset > 0) {
698 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
699 addUInt(Loc, dwarf::DW_FORM_udata, varFieldOffset);
700 }
702 // Now attach the location information to the DIE.
703 addBlock(Die, Attribute, Loc);
704 }
706 /// isTypeSigned - Return true if the type is signed.
707 static bool isTypeSigned(DwarfDebug *DD, DIType Ty, int *SizeInBits) {
708 if (Ty.isDerivedType())
709 return isTypeSigned(DD, DD->resolve(DIDerivedType(Ty).getTypeDerivedFrom()),
710 SizeInBits);
711 if (Ty.isBasicType())
712 if (DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed ||
713 DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed_char) {
714 *SizeInBits = Ty.getSizeInBits();
715 return true;
716 }
717 return false;
718 }
720 /// Return true if type encoding is unsigned.
721 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
722 DIDerivedType DTy(Ty);
723 if (DTy.isDerivedType())
724 return isUnsignedDIType(DD, DD->resolve(DTy.getTypeDerivedFrom()));
726 DIBasicType BTy(Ty);
727 if (BTy.isBasicType()) {
728 unsigned Encoding = BTy.getEncoding();
729 if (Encoding == dwarf::DW_ATE_unsigned ||
730 Encoding == dwarf::DW_ATE_unsigned_char ||
731 Encoding == dwarf::DW_ATE_boolean)
732 return true;
733 }
734 return false;
735 }
737 /// If this type is derived from a base type then return base type size.
738 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
739 unsigned Tag = Ty.getTag();
741 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
742 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
743 Tag != dwarf::DW_TAG_restrict_type)
744 return Ty.getSizeInBits();
746 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
748 // If this type is not derived from any type then take conservative approach.
749 if (!BaseType.isValid())
750 return Ty.getSizeInBits();
752 // If this is a derived type, go ahead and get the base type, unless it's a
753 // reference then it's just the size of the field. Pointer types have no need
754 // of this since they're a different type of qualification on the type.
755 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
756 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
757 return Ty.getSizeInBits();
759 if (BaseType.isDerivedType())
760 return getBaseTypeSize(DD, DIDerivedType(BaseType));
762 return BaseType.getSizeInBits();
763 }
765 /// addConstantValue - Add constant value entry in variable DIE.
766 void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
767 DIType Ty) {
768 // FIXME: This is a bit conservative/simple - it emits negative values at
769 // their maximum bit width which is a bit unfortunate (& doesn't prefer
770 // udata/sdata over dataN as suggested by the DWARF spec)
771 assert(MO.isImm() && "Invalid machine operand!");
772 int SizeInBits = -1;
773 bool SignedConstant = isTypeSigned(DD, Ty, &SizeInBits);
774 dwarf::Form Form;
776 // If we're a signed constant definitely use sdata.
777 if (SignedConstant) {
778 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata, MO.getImm());
779 return;
780 }
782 // Else use data for now unless it's larger than we can deal with.
783 switch (SizeInBits) {
784 case 8:
785 Form = dwarf::DW_FORM_data1;
786 break;
787 case 16:
788 Form = dwarf::DW_FORM_data2;
789 break;
790 case 32:
791 Form = dwarf::DW_FORM_data4;
792 break;
793 case 64:
794 Form = dwarf::DW_FORM_data8;
795 break;
796 default:
797 Form = dwarf::DW_FORM_udata;
798 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
799 return;
800 }
801 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
802 }
804 /// addConstantFPValue - Add constant value entry in variable DIE.
805 void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
806 assert(MO.isFPImm() && "Invalid machine operand!");
807 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
808 APFloat FPImm = MO.getFPImm()->getValueAPF();
810 // Get the raw data form of the floating point.
811 const APInt FltVal = FPImm.bitcastToAPInt();
812 const char *FltPtr = (const char *)FltVal.getRawData();
814 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
815 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
816 int Incr = (LittleEndian ? 1 : -1);
817 int Start = (LittleEndian ? 0 : NumBytes - 1);
818 int Stop = (LittleEndian ? NumBytes : -1);
820 // Output the constant to DWARF one byte at a time.
821 for (; Start != Stop; Start += Incr)
822 addUInt(Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
824 addBlock(Die, dwarf::DW_AT_const_value, Block);
825 }
827 /// addConstantFPValue - Add constant value entry in variable DIE.
828 void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
829 // Pass this down to addConstantValue as an unsigned bag of bits.
830 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
831 }
833 /// addConstantValue - Add constant value entry in variable DIE.
834 void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
835 bool Unsigned) {
836 addConstantValue(Die, CI->getValue(), Unsigned);
837 }
839 // addConstantValue - Add constant value entry in variable DIE.
840 void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
841 unsigned CIBitWidth = Val.getBitWidth();
842 if (CIBitWidth <= 64) {
843 // If we're a signed constant definitely use sdata.
844 if (!Unsigned) {
845 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
846 Val.getSExtValue());
847 return;
848 }
850 // Else use data for now unless it's larger than we can deal with.
851 dwarf::Form Form;
852 switch (CIBitWidth) {
853 case 8:
854 Form = dwarf::DW_FORM_data1;
855 break;
856 case 16:
857 Form = dwarf::DW_FORM_data2;
858 break;
859 case 32:
860 Form = dwarf::DW_FORM_data4;
861 break;
862 case 64:
863 Form = dwarf::DW_FORM_data8;
864 break;
865 default:
866 addUInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_udata,
867 Val.getZExtValue());
868 return;
869 }
870 addUInt(Die, dwarf::DW_AT_const_value, Form, Val.getZExtValue());
871 return;
872 }
874 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
876 // Get the raw data form of the large APInt.
877 const uint64_t *Ptr64 = Val.getRawData();
879 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
880 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
882 // Output the constant to DWARF one byte at a time.
883 for (int i = 0; i < NumBytes; i++) {
884 uint8_t c;
885 if (LittleEndian)
886 c = Ptr64[i / 8] >> (8 * (i & 7));
887 else
888 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
889 addUInt(Block, dwarf::DW_FORM_data1, c);
890 }
892 addBlock(Die, dwarf::DW_AT_const_value, Block);
893 }
895 /// addTemplateParams - Add template parameters into buffer.
896 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
897 // Add template parameters.
898 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
899 DIDescriptor Element = TParams.getElement(i);
900 if (Element.isTemplateTypeParameter())
901 constructTemplateTypeParameterDIE(Buffer,
902 DITemplateTypeParameter(Element));
903 else if (Element.isTemplateValueParameter())
904 constructTemplateValueParameterDIE(Buffer,
905 DITemplateValueParameter(Element));
906 }
907 }
909 /// getOrCreateContextDIE - Get context owner's DIE.
910 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
911 if (!Context || Context.isFile())
912 return getUnitDie();
913 if (Context.isType())
914 return getOrCreateTypeDIE(DIType(Context));
915 if (Context.isNameSpace())
916 return getOrCreateNameSpace(DINameSpace(Context));
917 if (Context.isSubprogram())
918 return getOrCreateSubprogramDIE(DISubprogram(Context));
919 return getDIE(Context);
920 }
922 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
923 DIScope Context = resolve(Ty.getContext());
924 DIE *ContextDIE = getOrCreateContextDIE(Context);
926 DIE *TyDIE = getDIE(Ty);
927 if (TyDIE)
928 return TyDIE;
930 // Create new type.
931 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
933 constructTypeDIE(*TyDIE, Ty);
935 updateAcceleratorTables(Context, Ty, TyDIE);
936 return TyDIE;
937 }
939 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
940 /// given DIType.
941 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
942 if (!TyNode)
943 return NULL;
945 DIType Ty(TyNode);
946 assert(Ty.isType());
948 // Construct the context before querying for the existence of the DIE in case
949 // such construction creates the DIE.
950 DIScope Context = resolve(Ty.getContext());
951 DIE *ContextDIE = getOrCreateContextDIE(Context);
952 assert(ContextDIE);
954 DIE *TyDIE = getDIE(Ty);
955 if (TyDIE)
956 return TyDIE;
958 // Create new type.
959 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
961 updateAcceleratorTables(Context, Ty, TyDIE);
963 if (Ty.isBasicType())
964 constructTypeDIE(*TyDIE, DIBasicType(Ty));
965 else if (Ty.isCompositeType()) {
966 DICompositeType CTy(Ty);
967 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
968 if (MDString *TypeId = CTy.getIdentifier()) {
969 DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
970 // Skip updating the accellerator tables since this is not the full type
971 return TyDIE;
972 }
973 constructTypeDIE(*TyDIE, CTy);
974 } else {
975 assert(Ty.isDerivedType() && "Unknown kind of DIType");
976 constructTypeDIE(*TyDIE, DIDerivedType(Ty));
977 }
979 return TyDIE;
980 }
982 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
983 const DIE *TyDIE) {
984 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
985 bool IsImplementation = 0;
986 if (Ty.isCompositeType()) {
987 DICompositeType CT(Ty);
988 // A runtime language of 0 actually means C/C++ and that any
989 // non-negative value is some version of Objective-C/C++.
990 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
991 }
992 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
993 addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
995 if (!Context || Context.isCompileUnit() || Context.isFile() ||
996 Context.isNameSpace())
997 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
998 }
999 }
1001 /// addType - Add a new type attribute to the specified entity.
1002 void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
1003 assert(Ty && "Trying to add a type that doesn't exist?");
1005 // Check for pre-existence.
1006 DIEEntry *Entry = getDIEEntry(Ty);
1007 // If it exists then use the existing value.
1008 if (Entry) {
1009 addDIEEntry(Entity, Attribute, Entry);
1010 return;
1011 }
1013 // Construct type.
1014 DIE *Buffer = getOrCreateTypeDIE(Ty);
1016 // Set up proxy.
1017 Entry = createDIEEntry(Buffer);
1018 insertDIEEntry(Ty, Entry);
1019 addDIEEntry(Entity, Attribute, Entry);
1020 }
1022 // Accelerator table mutators - add each name along with its companion
1023 // DIE to the proper table while ensuring that the name that we're going
1024 // to reference is in the string table. We do this since the names we
1025 // add may not only be identical to the names in the DIE.
1026 void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
1027 if (!DD->useDwarfAccelTables())
1028 return;
1029 DU->getStringPoolEntry(Name);
1030 std::vector<const DIE *> &DIEs = AccelNames[Name];
1031 DIEs.push_back(Die);
1032 }
1034 void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
1035 if (!DD->useDwarfAccelTables())
1036 return;
1037 DU->getStringPoolEntry(Name);
1038 std::vector<const DIE *> &DIEs = AccelObjC[Name];
1039 DIEs.push_back(Die);
1040 }
1042 void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
1043 if (!DD->useDwarfAccelTables())
1044 return;
1045 DU->getStringPoolEntry(Name);
1046 std::vector<const DIE *> &DIEs = AccelNamespace[Name];
1047 DIEs.push_back(Die);
1048 }
1050 void DwarfUnit::addAccelType(StringRef Name,
1051 std::pair<const DIE *, unsigned> Die) {
1052 if (!DD->useDwarfAccelTables())
1053 return;
1054 DU->getStringPoolEntry(Name);
1055 std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
1056 DIEs.push_back(Die);
1057 }
1059 /// addGlobalName - Add a new global name to the compile unit.
1060 void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
1061 std::string FullName = getParentContextString(Context) + Name.str();
1062 GlobalNames[FullName] = Die;
1063 }
1065 /// getParentContextString - Walks the metadata parent chain in a language
1066 /// specific manner (using the compile unit language) and returns
1067 /// it as a string. This is done at the metadata level because DIEs may
1068 /// not currently have been added to the parent context and walking the
1069 /// DIEs looking for names is more expensive than walking the metadata.
1070 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1071 if (!Context)
1072 return "";
1074 // FIXME: Decide whether to implement this for non-C++ languages.
1075 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1076 return "";
1078 std::string CS;
1079 SmallVector<DIScope, 1> Parents;
1080 while (!Context.isCompileUnit()) {
1081 Parents.push_back(Context);
1082 if (Context.getContext())
1083 Context = resolve(Context.getContext());
1084 else
1085 // Structure, etc types will have a NULL context if they're at the top
1086 // level.
1087 break;
1088 }
1090 // Reverse iterate over our list to go from the outermost construct to the
1091 // innermost.
1092 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1093 E = Parents.rend();
1094 I != E; ++I) {
1095 DIScope Ctx = *I;
1096 StringRef Name = Ctx.getName();
1097 if (!Name.empty()) {
1098 CS += Name;
1099 CS += "::";
1100 }
1101 }
1102 return CS;
1103 }
1105 /// constructTypeDIE - Construct basic type die from DIBasicType.
1106 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1107 // Get core information.
1108 StringRef Name = BTy.getName();
1109 // Add name if not anonymous or intermediate type.
1110 if (!Name.empty())
1111 addString(&Buffer, dwarf::DW_AT_name, Name);
1113 // An unspecified type only has a name attribute.
1114 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1115 return;
1117 addUInt(&Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1118 BTy.getEncoding());
1120 uint64_t Size = BTy.getSizeInBits() >> 3;
1121 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1122 }
1124 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1125 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1126 // Get core information.
1127 StringRef Name = DTy.getName();
1128 uint64_t Size = DTy.getSizeInBits() >> 3;
1129 uint16_t Tag = Buffer.getTag();
1131 // Map to main type, void will not have a type.
1132 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1133 if (FromTy)
1134 addType(&Buffer, FromTy);
1136 // Add name if not anonymous or intermediate type.
1137 if (!Name.empty())
1138 addString(&Buffer, dwarf::DW_AT_name, Name);
1140 // Add size if non-zero (derived types might be zero-sized.)
1141 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1142 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1144 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1145 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1146 getOrCreateTypeDIE(resolve(DTy.getClassType())));
1147 // Add source line info if available and TyDesc is not a forward declaration.
1148 if (!DTy.isForwardDecl())
1149 addSourceLine(&Buffer, DTy);
1150 }
1152 /// constructSubprogramArguments - Construct function argument DIEs.
1153 void DwarfUnit::constructSubprogramArguments(DIE &Buffer, DIArray Args) {
1154 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1155 DIDescriptor Ty = Args.getElement(i);
1156 if (Ty.isUnspecifiedParameter()) {
1157 assert(i == N-1 && "Unspecified parameter must be the last argument");
1158 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1159 } else {
1160 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1161 addType(Arg, DIType(Ty));
1162 if (DIType(Ty).isArtificial())
1163 addFlag(Arg, dwarf::DW_AT_artificial);
1164 }
1165 }
1166 }
1168 /// constructTypeDIE - Construct type DIE from DICompositeType.
1169 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1170 // Add name if not anonymous or intermediate type.
1171 StringRef Name = CTy.getName();
1173 uint64_t Size = CTy.getSizeInBits() >> 3;
1174 uint16_t Tag = Buffer.getTag();
1176 switch (Tag) {
1177 case dwarf::DW_TAG_array_type:
1178 constructArrayTypeDIE(Buffer, CTy);
1179 break;
1180 case dwarf::DW_TAG_enumeration_type:
1181 constructEnumTypeDIE(Buffer, CTy);
1182 break;
1183 case dwarf::DW_TAG_subroutine_type: {
1184 // Add return type. A void return won't have a type.
1185 DIArray Elements = CTy.getTypeArray();
1186 DIType RTy(Elements.getElement(0));
1187 if (RTy)
1188 addType(&Buffer, RTy);
1190 bool isPrototyped = true;
1191 if (Elements.getNumElements() == 2 &&
1192 Elements.getElement(1).isUnspecifiedParameter())
1193 isPrototyped = false;
1195 constructSubprogramArguments(Buffer, Elements);
1197 // Add prototype flag if we're dealing with a C language and the
1198 // function has been prototyped.
1199 uint16_t Language = getLanguage();
1200 if (isPrototyped &&
1201 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1202 Language == dwarf::DW_LANG_ObjC))
1203 addFlag(&Buffer, dwarf::DW_AT_prototyped);
1205 if (CTy.isLValueReference())
1206 addFlag(&Buffer, dwarf::DW_AT_reference);
1208 if (CTy.isRValueReference())
1209 addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
1210 } break;
1211 case dwarf::DW_TAG_structure_type:
1212 case dwarf::DW_TAG_union_type:
1213 case dwarf::DW_TAG_class_type: {
1214 // Add elements to structure type.
1215 DIArray Elements = CTy.getTypeArray();
1216 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1217 DIDescriptor Element = Elements.getElement(i);
1218 DIE *ElemDie = NULL;
1219 if (Element.isSubprogram())
1220 ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
1221 else if (Element.isDerivedType()) {
1222 DIDerivedType DDTy(Element);
1223 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1224 ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1225 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1226 dwarf::DW_AT_friend);
1227 } else if (DDTy.isStaticMember()) {
1228 getOrCreateStaticMemberDIE(DDTy);
1229 } else {
1230 constructMemberDIE(Buffer, DDTy);
1231 }
1232 } else if (Element.isObjCProperty()) {
1233 DIObjCProperty Property(Element);
1234 ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1235 StringRef PropertyName = Property.getObjCPropertyName();
1236 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1237 if (Property.getType())
1238 addType(ElemDie, Property.getType());
1239 addSourceLine(ElemDie, Property);
1240 StringRef GetterName = Property.getObjCPropertyGetterName();
1241 if (!GetterName.empty())
1242 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1243 StringRef SetterName = Property.getObjCPropertySetterName();
1244 if (!SetterName.empty())
1245 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1246 unsigned PropertyAttributes = 0;
1247 if (Property.isReadOnlyObjCProperty())
1248 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1249 if (Property.isReadWriteObjCProperty())
1250 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1251 if (Property.isAssignObjCProperty())
1252 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1253 if (Property.isRetainObjCProperty())
1254 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1255 if (Property.isCopyObjCProperty())
1256 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1257 if (Property.isNonAtomicObjCProperty())
1258 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1259 if (PropertyAttributes)
1260 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1261 PropertyAttributes);
1263 DIEEntry *Entry = getDIEEntry(Element);
1264 if (!Entry) {
1265 Entry = createDIEEntry(ElemDie);
1266 insertDIEEntry(Element, Entry);
1267 }
1268 } else
1269 continue;
1270 }
1272 if (CTy.isAppleBlockExtension())
1273 addFlag(&Buffer, dwarf::DW_AT_APPLE_block);
1275 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1276 if (ContainingType)
1277 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1278 getOrCreateTypeDIE(ContainingType));
1280 if (CTy.isObjcClassComplete())
1281 addFlag(&Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1283 // Add template parameters to a class, structure or union types.
1284 // FIXME: The support isn't in the metadata for this yet.
1285 if (Tag == dwarf::DW_TAG_class_type ||
1286 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1287 addTemplateParams(Buffer, CTy.getTemplateParams());
1289 break;
1290 }
1291 default:
1292 break;
1293 }
1295 // Add name if not anonymous or intermediate type.
1296 if (!Name.empty())
1297 addString(&Buffer, dwarf::DW_AT_name, Name);
1299 if (Tag == dwarf::DW_TAG_enumeration_type ||
1300 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1301 Tag == dwarf::DW_TAG_union_type) {
1302 // Add size if non-zero (derived types might be zero-sized.)
1303 // TODO: Do we care about size for enum forward declarations?
1304 if (Size)
1305 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1306 else if (!CTy.isForwardDecl())
1307 // Add zero size if it is not a forward declaration.
1308 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, 0);
1310 // If we're a forward decl, say so.
1311 if (CTy.isForwardDecl())
1312 addFlag(&Buffer, dwarf::DW_AT_declaration);
1314 // Add source line info if available.
1315 if (!CTy.isForwardDecl())
1316 addSourceLine(&Buffer, CTy);
1318 // No harm in adding the runtime language to the declaration.
1319 unsigned RLang = CTy.getRunTimeLang();
1320 if (RLang)
1321 addUInt(&Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1322 RLang);
1323 }
1324 }
1326 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1327 /// DITemplateTypeParameter.
1328 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1329 DITemplateTypeParameter TP) {
1330 DIE *ParamDIE =
1331 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1332 // Add the type if it exists, it could be void and therefore no type.
1333 if (TP.getType())
1334 addType(ParamDIE, resolve(TP.getType()));
1335 if (!TP.getName().empty())
1336 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1337 }
1339 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1340 /// DITemplateValueParameter.
1341 void
1342 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1343 DITemplateValueParameter VP) {
1344 DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1346 // Add the type if there is one, template template and template parameter
1347 // packs will not have a type.
1348 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1349 addType(ParamDIE, resolve(VP.getType()));
1350 if (!VP.getName().empty())
1351 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1352 if (Value *Val = VP.getValue()) {
1353 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1354 addConstantValue(ParamDIE, CI,
1355 isUnsignedDIType(DD, resolve(VP.getType())));
1356 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1357 // For declaration non-type template parameters (such as global values and
1358 // functions)
1359 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1360 addOpAddress(Loc, Asm->getSymbol(GV));
1361 // Emit DW_OP_stack_value to use the address as the immediate value of the
1362 // parameter, rather than a pointer to it.
1363 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1364 addBlock(ParamDIE, dwarf::DW_AT_location, Loc);
1365 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1366 assert(isa<MDString>(Val));
1367 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1368 cast<MDString>(Val)->getString());
1369 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1370 assert(isa<MDNode>(Val));
1371 DIArray A(cast<MDNode>(Val));
1372 addTemplateParams(*ParamDIE, A);
1373 }
1374 }
1375 }
1377 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1378 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1379 // Construct the context before querying for the existence of the DIE in case
1380 // such construction creates the DIE.
1381 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1383 DIE *NDie = getDIE(NS);
1384 if (NDie)
1385 return NDie;
1386 NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1388 if (!NS.getName().empty()) {
1389 addString(NDie, dwarf::DW_AT_name, NS.getName());
1390 addAccelNamespace(NS.getName(), NDie);
1391 addGlobalName(NS.getName(), NDie, NS.getContext());
1392 } else
1393 addAccelNamespace("(anonymous namespace)", NDie);
1394 addSourceLine(NDie, NS);
1395 return NDie;
1396 }
1398 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1399 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1400 // Construct the context before querying for the existence of the DIE in case
1401 // such construction creates the DIE (as is the case for member function
1402 // declarations).
1403 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1405 DIE *SPDie = getDIE(SP);
1406 if (SPDie)
1407 return SPDie;
1409 DISubprogram SPDecl = SP.getFunctionDeclaration();
1410 if (SPDecl.isSubprogram())
1411 // Add subprogram definitions to the CU die directly.
1412 ContextDIE = UnitDie.get();
1414 // DW_TAG_inlined_subroutine may refer to this DIE.
1415 SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1417 DIE *DeclDie = NULL;
1418 if (SPDecl.isSubprogram())
1419 DeclDie = getOrCreateSubprogramDIE(SPDecl);
1421 // Add function template parameters.
1422 addTemplateParams(*SPDie, SP.getTemplateParams());
1424 // If this DIE is going to refer declaration info using AT_specification
1425 // then there is no need to add other attributes.
1426 if (DeclDie) {
1427 // Refer function declaration directly.
1428 addDIEEntry(SPDie, dwarf::DW_AT_specification, DeclDie);
1430 return SPDie;
1431 }
1433 // Add the linkage name if we have one.
1434 StringRef LinkageName = SP.getLinkageName();
1435 if (!LinkageName.empty())
1436 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1437 GlobalValue::getRealLinkageName(LinkageName));
1439 // Constructors and operators for anonymous aggregates do not have names.
1440 if (!SP.getName().empty())
1441 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1443 addSourceLine(SPDie, SP);
1445 // Add the prototype if we have a prototype and we have a C like
1446 // language.
1447 uint16_t Language = getLanguage();
1448 if (SP.isPrototyped() &&
1449 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1450 Language == dwarf::DW_LANG_ObjC))
1451 addFlag(SPDie, dwarf::DW_AT_prototyped);
1453 DICompositeType SPTy = SP.getType();
1454 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1455 "the type of a subprogram should be a subroutine");
1457 DIArray Args = SPTy.getTypeArray();
1458 // Add a return type. If this is a type like a C/C++ void type we don't add a
1459 // return type.
1460 if (Args.getElement(0))
1461 addType(SPDie, DIType(Args.getElement(0)));
1463 unsigned VK = SP.getVirtuality();
1464 if (VK) {
1465 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1466 DIELoc *Block = getDIELoc();
1467 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1468 addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1469 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1470 ContainingTypeMap.insert(
1471 std::make_pair(SPDie, resolve(SP.getContainingType())));
1472 }
1474 if (!SP.isDefinition()) {
1475 addFlag(SPDie, dwarf::DW_AT_declaration);
1477 // Add arguments. Do not add arguments for subprogram definition. They will
1478 // be handled while processing variables.
1479 constructSubprogramArguments(*SPDie, Args);
1480 }
1482 if (SP.isArtificial())
1483 addFlag(SPDie, dwarf::DW_AT_artificial);
1485 if (!SP.isLocalToUnit())
1486 addFlag(SPDie, dwarf::DW_AT_external);
1488 if (SP.isOptimized())
1489 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1491 if (unsigned isa = Asm->getISAEncoding()) {
1492 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1493 }
1495 if (SP.isLValueReference())
1496 addFlag(SPDie, dwarf::DW_AT_reference);
1498 if (SP.isRValueReference())
1499 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1501 if (SP.isProtected())
1502 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1503 dwarf::DW_ACCESS_protected);
1504 else if (SP.isPrivate())
1505 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1506 dwarf::DW_ACCESS_private);
1507 else
1508 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1509 dwarf::DW_ACCESS_public);
1511 if (SP.isExplicit())
1512 addFlag(SPDie, dwarf::DW_AT_explicit);
1514 return SPDie;
1515 }
1517 // Return const expression if value is a GEP to access merged global
1518 // constant. e.g.
1519 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1520 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1521 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1522 if (!CE || CE->getNumOperands() != 3 ||
1523 CE->getOpcode() != Instruction::GetElementPtr)
1524 return NULL;
1526 // First operand points to a global struct.
1527 Value *Ptr = CE->getOperand(0);
1528 if (!isa<GlobalValue>(Ptr) ||
1529 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1530 return NULL;
1532 // Second operand is zero.
1533 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1534 if (!CI || !CI->isZero())
1535 return NULL;
1537 // Third operand is offset.
1538 if (!isa<ConstantInt>(CE->getOperand(2)))
1539 return NULL;
1541 return CE;
1542 }
1544 /// createGlobalVariableDIE - create global variable DIE.
1545 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1546 // Check for pre-existence.
1547 if (getDIE(GV))
1548 return;
1550 assert(GV.isGlobalVariable());
1552 DIScope GVContext = GV.getContext();
1553 DIType GTy = GV.getType();
1555 // If this is a static data member definition, some attributes belong
1556 // to the declaration DIE.
1557 DIE *VariableDIE = NULL;
1558 bool IsStaticMember = false;
1559 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1560 if (SDMDecl.Verify()) {
1561 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1562 // We need the declaration DIE that is in the static member's class.
1563 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1564 IsStaticMember = true;
1565 }
1567 // If this is not a static data member definition, create the variable
1568 // DIE and add the initial set of attributes to it.
1569 if (!VariableDIE) {
1570 // Construct the context before querying for the existence of the DIE in
1571 // case such construction creates the DIE.
1572 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1574 // Add to map.
1575 VariableDIE = createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1577 // Add name and type.
1578 addString(VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1579 addType(VariableDIE, GTy);
1581 // Add scoping info.
1582 if (!GV.isLocalToUnit())
1583 addFlag(VariableDIE, dwarf::DW_AT_external);
1585 // Add line number info.
1586 addSourceLine(VariableDIE, GV);
1587 }
1589 // Add location.
1590 bool addToAccelTable = false;
1591 DIE *VariableSpecDIE = NULL;
1592 bool isGlobalVariable = GV.getGlobal() != NULL;
1593 if (isGlobalVariable) {
1594 addToAccelTable = true;
1595 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1596 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1597 if (GV.getGlobal()->isThreadLocal()) {
1598 // FIXME: Make this work with -gsplit-dwarf.
1599 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1600 assert((PointerSize == 4 || PointerSize == 8) &&
1601 "Add support for other sizes if necessary");
1602 // Based on GCC's support for TLS:
1603 if (!DD->useSplitDwarf()) {
1604 // 1) Start with a constNu of the appropriate pointer size
1605 addUInt(Loc, dwarf::DW_FORM_data1,
1606 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1607 // 2) containing the (relocated) offset of the TLS variable
1608 // within the module's TLS block.
1609 addExpr(Loc, dwarf::DW_FORM_udata,
1610 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym));
1611 } else {
1612 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1613 addUInt(Loc, dwarf::DW_FORM_udata,
1614 DU->getAddrPoolIndex(Sym, /* TLS */ true));
1615 }
1616 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1617 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1618 } else {
1619 DD->addArangeLabel(SymbolCU(this, Sym));
1620 addOpAddress(Loc, Sym);
1621 }
1622 // Do not create specification DIE if context is either compile unit
1623 // or a subprogram.
1624 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1625 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1626 // Create specification DIE.
1627 VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
1628 addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
1629 addBlock(VariableSpecDIE, dwarf::DW_AT_location, Loc);
1630 // A static member's declaration is already flagged as such.
1631 if (!SDMDecl.Verify())
1632 addFlag(VariableDIE, dwarf::DW_AT_declaration);
1633 } else {
1634 addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
1635 }
1636 // Add the linkage name.
1637 StringRef LinkageName = GV.getLinkageName();
1638 if (!LinkageName.empty())
1639 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1640 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1641 // TAG_variable.
1642 addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
1643 : VariableDIE,
1644 dwarf::DW_AT_MIPS_linkage_name,
1645 GlobalValue::getRealLinkageName(LinkageName));
1646 } else if (const ConstantInt *CI =
1647 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1648 // AT_const_value was added when the static member was created. To avoid
1649 // emitting AT_const_value multiple times, we only add AT_const_value when
1650 // it is not a static member.
1651 if (!IsStaticMember)
1652 addConstantValue(VariableDIE, CI, isUnsignedDIType(DD, GTy));
1653 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1654 addToAccelTable = true;
1655 // GV is a merged global.
1656 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1657 Value *Ptr = CE->getOperand(0);
1658 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1659 DD->addArangeLabel(SymbolCU(this, Sym));
1660 addOpAddress(Loc, Sym);
1661 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1662 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1663 addUInt(Loc, dwarf::DW_FORM_udata,
1664 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1665 addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1666 addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
1667 }
1669 if (addToAccelTable) {
1670 DIE *AddrDIE = VariableSpecDIE ? VariableSpecDIE : VariableDIE;
1671 addAccelName(GV.getName(), AddrDIE);
1673 // If the linkage name is different than the name, go ahead and output
1674 // that as well into the name table.
1675 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1676 addAccelName(GV.getLinkageName(), AddrDIE);
1677 }
1679 if (!GV.isLocalToUnit())
1680 addGlobalName(GV.getName(), VariableSpecDIE ? VariableSpecDIE : VariableDIE,
1681 GV.getContext());
1682 }
1684 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1685 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1686 DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1687 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
1689 // The LowerBound value defines the lower bounds which is typically zero for
1690 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1691 // Count == -1 then the array is unbounded and we do not emit
1692 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1693 // Count == 0, then the array has zero elements in which case we do not emit
1694 // an upper bound.
1695 int64_t LowerBound = SR.getLo();
1696 int64_t DefaultLowerBound = getDefaultLowerBound();
1697 int64_t Count = SR.getCount();
1699 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1700 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1702 if (Count != -1 && Count != 0)
1703 // FIXME: An unbounded array should reference the expression that defines
1704 // the array.
1705 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1706 LowerBound + Count - 1);
1707 }
1709 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1710 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1711 if (CTy.isVector())
1712 addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
1714 // Emit the element type.
1715 addType(&Buffer, resolve(CTy.getTypeDerivedFrom()));
1717 // Get an anonymous type for index type.
1718 // FIXME: This type should be passed down from the front end
1719 // as different languages may have different sizes for indexes.
1720 DIE *IdxTy = getIndexTyDie();
1721 if (!IdxTy) {
1722 // Construct an anonymous type for index type.
1723 IdxTy = createAndAddDIE(dwarf::DW_TAG_base_type, *UnitDie);
1724 addString(IdxTy, dwarf::DW_AT_name, "int");
1725 addUInt(IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int32_t));
1726 addUInt(IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1727 dwarf::DW_ATE_signed);
1728 setIndexTyDie(IdxTy);
1729 }
1731 // Add subranges to array type.
1732 DIArray Elements = CTy.getTypeArray();
1733 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1734 DIDescriptor Element = Elements.getElement(i);
1735 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1736 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1737 }
1738 }
1740 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1741 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1742 DIArray Elements = CTy.getTypeArray();
1744 // Add enumerators to enumeration type.
1745 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1746 DIEnumerator Enum(Elements.getElement(i));
1747 if (Enum.isEnumerator()) {
1748 DIE *Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1749 StringRef Name = Enum.getName();
1750 addString(Enumerator, dwarf::DW_AT_name, Name);
1751 int64_t Value = Enum.getEnumValue();
1752 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1753 Value);
1754 }
1755 }
1756 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1757 if (DTy) {
1758 addType(&Buffer, DTy);
1759 addFlag(&Buffer, dwarf::DW_AT_enum_class);
1760 }
1761 }
1763 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1764 /// vtables.
1765 void DwarfUnit::constructContainingTypeDIEs() {
1766 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1767 CE = ContainingTypeMap.end();
1768 CI != CE; ++CI) {
1769 DIE *SPDie = CI->first;
1770 DIDescriptor D(CI->second);
1771 if (!D)
1772 continue;
1773 DIE *NDie = getDIE(D);
1774 if (!NDie)
1775 continue;
1776 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, NDie);
1777 }
1778 }
1780 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1781 DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
1782 StringRef Name = DV.getName();
1784 // Define variable debug information entry.
1785 DIE *VariableDie = new DIE(DV.getTag());
1786 DbgVariable *AbsVar = DV.getAbstractVariable();
1787 DIE *AbsDIE = AbsVar ? AbsVar->getDIE() : NULL;
1788 if (AbsDIE)
1789 addDIEEntry(VariableDie, dwarf::DW_AT_abstract_origin, AbsDIE);
1790 else {
1791 if (!Name.empty())
1792 addString(VariableDie, dwarf::DW_AT_name, Name);
1793 addSourceLine(VariableDie, DV.getVariable());
1794 addType(VariableDie, DV.getType());
1795 }
1797 if (DV.isArtificial())
1798 addFlag(VariableDie, dwarf::DW_AT_artificial);
1800 if (isScopeAbstract) {
1801 DV.setDIE(VariableDie);
1802 return VariableDie;
1803 }
1805 // Add variable address.
1807 unsigned Offset = DV.getDotDebugLocOffset();
1808 if (Offset != ~0U) {
1809 addLocationList(VariableDie, dwarf::DW_AT_location, Offset);
1810 DV.setDIE(VariableDie);
1811 return VariableDie;
1812 }
1814 // Check if variable is described by a DBG_VALUE instruction.
1815 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1816 assert(DVInsn->getNumOperands() == 3);
1817 if (DVInsn->getOperand(0).isReg()) {
1818 const MachineOperand RegOp = DVInsn->getOperand(0);
1819 // If the second operand is an immediate, this is an indirect value.
1820 if (DVInsn->getOperand(1).isImm()) {
1821 MachineLocation Location(RegOp.getReg(),
1822 DVInsn->getOperand(1).getImm());
1823 addVariableAddress(DV, VariableDie, Location);
1824 } else if (RegOp.getReg())
1825 addVariableAddress(DV, VariableDie, MachineLocation(RegOp.getReg()));
1826 } else if (DVInsn->getOperand(0).isImm())
1827 addConstantValue(VariableDie, DVInsn->getOperand(0), DV.getType());
1828 else if (DVInsn->getOperand(0).isFPImm())
1829 addConstantFPValue(VariableDie, DVInsn->getOperand(0));
1830 else if (DVInsn->getOperand(0).isCImm())
1831 addConstantValue(VariableDie, DVInsn->getOperand(0).getCImm(),
1832 isUnsignedDIType(DD, DV.getType()));
1834 DV.setDIE(VariableDie);
1835 return VariableDie;
1836 } else {
1837 // .. else use frame index.
1838 int FI = DV.getFrameIndex();
1839 if (FI != ~0) {
1840 unsigned FrameReg = 0;
1841 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1842 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1843 MachineLocation Location(FrameReg, Offset);
1844 addVariableAddress(DV, VariableDie, Location);
1845 }
1846 }
1848 DV.setDIE(VariableDie);
1849 return VariableDie;
1850 }
1852 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1853 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1854 DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1855 StringRef Name = DT.getName();
1856 if (!Name.empty())
1857 addString(MemberDie, dwarf::DW_AT_name, Name);
1859 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1861 addSourceLine(MemberDie, DT);
1863 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1865 // For C++, virtual base classes are not at fixed offset. Use following
1866 // expression to extract appropriate offset from vtable.
1867 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1869 DIELoc *VBaseLocationDie = new (DIEValueAllocator) DIELoc();
1870 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1871 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1872 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1873 addUInt(VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1874 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1875 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1876 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1878 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1879 } else {
1880 uint64_t Size = DT.getSizeInBits();
1881 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1882 uint64_t OffsetInBytes;
1884 if (Size != FieldSize) {
1885 // Handle bitfield.
1886 addUInt(MemberDie, dwarf::DW_AT_byte_size, None,
1887 getBaseTypeSize(DD, DT) >> 3);
1888 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, DT.getSizeInBits());
1890 uint64_t Offset = DT.getOffsetInBits();
1891 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1892 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1893 uint64_t FieldOffset = (HiMark - FieldSize);
1894 Offset -= FieldOffset;
1896 // Maybe we need to work from the other end.
1897 if (Asm->getDataLayout().isLittleEndian())
1898 Offset = FieldSize - (Offset + Size);
1899 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1901 // Here DW_AT_data_member_location points to the anonymous
1902 // field that includes this bit field.
1903 OffsetInBytes = FieldOffset >> 3;
1904 } else
1905 // This is not a bitfield.
1906 OffsetInBytes = DT.getOffsetInBits() >> 3;
1908 if (DD->getDwarfVersion() <= 2) {
1909 DIELoc *MemLocationDie = new (DIEValueAllocator) DIELoc();
1910 addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1911 addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1912 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1913 } else
1914 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1915 OffsetInBytes);
1916 }
1918 if (DT.isProtected())
1919 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1920 dwarf::DW_ACCESS_protected);
1921 else if (DT.isPrivate())
1922 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1923 dwarf::DW_ACCESS_private);
1924 // Otherwise C++ member and base classes are considered public.
1925 else
1926 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1927 dwarf::DW_ACCESS_public);
1928 if (DT.isVirtual())
1929 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1930 dwarf::DW_VIRTUALITY_virtual);
1932 // Objective-C properties.
1933 if (MDNode *PNode = DT.getObjCProperty())
1934 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1935 MemberDie->addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1936 PropertyDie);
1938 if (DT.isArtificial())
1939 addFlag(MemberDie, dwarf::DW_AT_artificial);
1940 }
1942 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1943 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1944 if (!DT.Verify())
1945 return NULL;
1947 // Construct the context before querying for the existence of the DIE in case
1948 // such construction creates the DIE.
1949 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1950 assert(dwarf::isType(ContextDIE->getTag()) &&
1951 "Static member should belong to a type.");
1953 DIE *StaticMemberDIE = getDIE(DT);
1954 if (StaticMemberDIE)
1955 return StaticMemberDIE;
1957 StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1959 DIType Ty = resolve(DT.getTypeDerivedFrom());
1961 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1962 addType(StaticMemberDIE, Ty);
1963 addSourceLine(StaticMemberDIE, DT);
1964 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1965 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1967 // FIXME: We could omit private if the parent is a class_type, and
1968 // public if the parent is something else.
1969 if (DT.isProtected())
1970 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1971 dwarf::DW_ACCESS_protected);
1972 else if (DT.isPrivate())
1973 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1974 dwarf::DW_ACCESS_private);
1975 else
1976 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1977 dwarf::DW_ACCESS_public);
1979 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1980 addConstantValue(StaticMemberDIE, CI, isUnsignedDIType(DD, Ty));
1981 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1982 addConstantFPValue(StaticMemberDIE, CFP);
1984 return StaticMemberDIE;
1985 }
1987 void DwarfUnit::emitHeader(const MCSection *ASection,
1988 const MCSymbol *ASectionSym) const {
1989 Asm->OutStreamer.AddComment("DWARF version number");
1990 Asm->EmitInt16(DD->getDwarfVersion());
1991 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1992 // We share one abbreviations table across all units so it's always at the
1993 // start of the section. Use a relocatable offset where needed to ensure
1994 // linking doesn't invalidate that offset.
1995 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1996 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1997 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1998 }
2000 void DwarfCompileUnit::initStmtList(MCSymbol *DwarfLineSectionSym) {
2001 // Define start line table label for each Compile Unit.
2002 MCSymbol *LineTableStartSym =
2003 Asm->GetTempSymbol("line_table_start", getUniqueID());
2004 Asm->OutStreamer.getContext().setMCLineTableSymbol(LineTableStartSym,
2005 getUniqueID());
2007 // Use a single line table if we are generating assembly.
2008 bool UseTheFirstCU =
2009 Asm->OutStreamer.hasRawTextSupport() || (getUniqueID() == 0);
2011 stmtListIndex = UnitDie->getValues().size();
2013 // DW_AT_stmt_list is a offset of line number information for this
2014 // compile unit in debug_line section. For split dwarf this is
2015 // left in the skeleton CU and so not included.
2016 // The line table entries are not always emitted in assembly, so it
2017 // is not okay to use line_table_start here.
2018 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
2019 addSectionLabel(UnitDie.get(), dwarf::DW_AT_stmt_list,
2020 UseTheFirstCU ? DwarfLineSectionSym : LineTableStartSym);
2021 else if (UseTheFirstCU)
2022 addSectionOffset(UnitDie.get(), dwarf::DW_AT_stmt_list, 0);
2023 else
2024 addSectionDelta(UnitDie.get(), dwarf::DW_AT_stmt_list, LineTableStartSym,
2025 DwarfLineSectionSym);
2026 }
2028 void DwarfCompileUnit::applyStmtList(DIE &D) {
2029 D.addValue(dwarf::DW_AT_stmt_list,
2030 UnitDie->getAbbrev().getData()[stmtListIndex].getForm(),
2031 UnitDie->getValues()[stmtListIndex]);
2032 }
2034 void DwarfTypeUnit::emitHeader(const MCSection *ASection,
2035 const MCSymbol *ASectionSym) const {
2036 DwarfUnit::emitHeader(ASection, ASectionSym);
2037 Asm->OutStreamer.AddComment("Type Signature");
2038 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
2039 Asm->OutStreamer.AddComment("Type DIE Offset");
2040 // In a skeleton type unit there is no type DIE so emit a zero offset.
2041 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
2042 sizeof(Ty->getOffset()));
2043 }
2045 void DwarfTypeUnit::initSection(const MCSection *Section) {
2046 assert(!this->Section);
2047 this->Section = Section;
2048 // Since each type unit is contained in its own COMDAT section, the begin
2049 // label and the section label are the same. Using the begin label emission in
2050 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2051 // the only other alternative of lazily constructing start-of-section labels
2052 // and storing a mapping in DwarfDebug (or AsmPrinter).
2053 this->SectionSym = this->LabelBegin =
2054 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2055 this->LabelEnd =
2056 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2057 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
2058 }