1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "DwarfUnit.h"
15 #include "DwarfAccelTable.h"
16 #include "DwarfDebug.h"
17 #include "llvm/ADT/APFloat.h"
18 #include "llvm/IR/Constants.h"
19 #include "llvm/IR/DIBuilder.h"
20 #include "llvm/IR/DataLayout.h"
21 #include "llvm/IR/GlobalVariable.h"
22 #include "llvm/IR/Instructions.h"
23 #include "llvm/IR/Mangler.h"
24 #include "llvm/MC/MCAsmInfo.h"
25 #include "llvm/MC/MCContext.h"
26 #include "llvm/MC/MCSection.h"
27 #include "llvm/MC/MCStreamer.h"
28 #include "llvm/Support/CommandLine.h"
29 #include "llvm/Target/TargetFrameLowering.h"
30 #include "llvm/Target/TargetLoweringObjectFile.h"
31 #include "llvm/Target/TargetMachine.h"
32 #include "llvm/Target/TargetRegisterInfo.h"
34 using namespace llvm;
36 #define DEBUG_TYPE "dwarfdebug"
38 static cl::opt<bool>
39 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
40 cl::desc("Generate DWARF4 type units."),
41 cl::init(false));
43 /// Unit - Unit constructor.
44 DwarfUnit::DwarfUnit(unsigned UID, dwarf::Tag UnitTag, DICompileUnit Node,
45 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
46 : UniqueID(UID), CUNode(Node), UnitDie(UnitTag), DebugInfoOffset(0), Asm(A),
47 DD(DW), DU(DWU), IndexTyDie(nullptr), Section(nullptr),
48 Skeleton(nullptr) {
49 assert(UnitTag == dwarf::DW_TAG_compile_unit ||
50 UnitTag == dwarf::DW_TAG_type_unit);
51 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
52 }
54 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DICompileUnit Node,
55 AsmPrinter *A, DwarfDebug *DW,
56 DwarfFile *DWU)
57 : DwarfUnit(UID, dwarf::DW_TAG_compile_unit, Node, A, DW, DWU) {
58 insertDIE(Node, &getUnitDie());
59 }
61 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A,
62 DwarfDebug *DW, DwarfFile *DWU,
63 MCDwarfDwoLineTable *SplitLineTable)
64 : DwarfUnit(UID, dwarf::DW_TAG_type_unit, CU.getCUNode(), A, DW, DWU),
65 CU(CU), SplitLineTable(SplitLineTable) {
66 if (SplitLineTable)
67 addSectionOffset(UnitDie, dwarf::DW_AT_stmt_list, 0);
68 }
70 /// ~Unit - Destructor for compile unit.
71 DwarfUnit::~DwarfUnit() {
72 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
73 DIEBlocks[j]->~DIEBlock();
74 for (unsigned j = 0, M = DIELocs.size(); j < M; ++j)
75 DIELocs[j]->~DIELoc();
76 }
78 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
79 /// information entry.
80 DIEEntry *DwarfUnit::createDIEEntry(DIE &Entry) {
81 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
82 return Value;
83 }
85 /// getDefaultLowerBound - Return the default lower bound for an array. If the
86 /// DWARF version doesn't handle the language, return -1.
87 int64_t DwarfUnit::getDefaultLowerBound() const {
88 switch (getLanguage()) {
89 default:
90 break;
92 case dwarf::DW_LANG_C89:
93 case dwarf::DW_LANG_C99:
94 case dwarf::DW_LANG_C:
95 case dwarf::DW_LANG_C_plus_plus:
96 case dwarf::DW_LANG_ObjC:
97 case dwarf::DW_LANG_ObjC_plus_plus:
98 return 0;
100 case dwarf::DW_LANG_Fortran77:
101 case dwarf::DW_LANG_Fortran90:
102 case dwarf::DW_LANG_Fortran95:
103 return 1;
105 // The languages below have valid values only if the DWARF version >= 4.
106 case dwarf::DW_LANG_Java:
107 case dwarf::DW_LANG_Python:
108 case dwarf::DW_LANG_UPC:
109 case dwarf::DW_LANG_D:
110 if (dwarf::DWARF_VERSION >= 4)
111 return 0;
112 break;
114 case dwarf::DW_LANG_Ada83:
115 case dwarf::DW_LANG_Ada95:
116 case dwarf::DW_LANG_Cobol74:
117 case dwarf::DW_LANG_Cobol85:
118 case dwarf::DW_LANG_Modula2:
119 case dwarf::DW_LANG_Pascal83:
120 case dwarf::DW_LANG_PLI:
121 if (dwarf::DWARF_VERSION >= 4)
122 return 1;
123 break;
124 }
126 return -1;
127 }
129 /// Check whether the DIE for this MDNode can be shared across CUs.
130 static bool isShareableAcrossCUs(DIDescriptor D) {
131 // When the MDNode can be part of the type system, the DIE can be shared
132 // across CUs.
133 // Combining type units and cross-CU DIE sharing is lower value (since
134 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
135 // level already) but may be implementable for some value in projects
136 // building multiple independent libraries with LTO and then linking those
137 // together.
138 return (D.isType() ||
139 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
140 !GenerateDwarfTypeUnits;
141 }
143 /// getDIE - Returns the debug information entry map slot for the
144 /// specified debug variable. We delegate the request to DwarfDebug
145 /// when the DIE for this MDNode can be shared across CUs. The mappings
146 /// will be kept in DwarfDebug for shareable DIEs.
147 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
148 if (isShareableAcrossCUs(D))
149 return DD->getDIE(D);
150 return MDNodeToDieMap.lookup(D);
151 }
153 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
154 /// when the DIE for this MDNode can be shared across CUs. The mappings
155 /// will be kept in DwarfDebug for shareable DIEs.
156 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
157 if (isShareableAcrossCUs(Desc)) {
158 DD->insertDIE(Desc, D);
159 return;
160 }
161 MDNodeToDieMap.insert(std::make_pair(Desc, D));
162 }
164 /// addFlag - Add a flag that is true.
165 void DwarfUnit::addFlag(DIE &Die, dwarf::Attribute Attribute) {
166 if (DD->getDwarfVersion() >= 4)
167 Die.addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
168 else
169 Die.addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
170 }
172 /// addUInt - Add an unsigned integer attribute data and value.
173 ///
174 void DwarfUnit::addUInt(DIE &Die, dwarf::Attribute Attribute,
175 Optional<dwarf::Form> Form, uint64_t Integer) {
176 if (!Form)
177 Form = DIEInteger::BestForm(false, Integer);
178 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
179 DIEInteger(Integer);
180 Die.addValue(Attribute, *Form, Value);
181 }
183 void DwarfUnit::addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer) {
184 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
185 }
187 /// addSInt - Add an signed integer attribute data and value.
188 ///
189 void DwarfUnit::addSInt(DIE &Die, dwarf::Attribute Attribute,
190 Optional<dwarf::Form> Form, int64_t Integer) {
191 if (!Form)
192 Form = DIEInteger::BestForm(true, Integer);
193 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
194 Die.addValue(Attribute, *Form, Value);
195 }
197 void DwarfUnit::addSInt(DIELoc &Die, Optional<dwarf::Form> Form,
198 int64_t Integer) {
199 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
200 }
202 /// addString - Add a string attribute data and value. We always emit a
203 /// reference to the string pool instead of immediate strings so that DIEs have
204 /// more predictable sizes. In the case of split dwarf we emit an index
205 /// into another table which gets us the static offset into the string
206 /// table.
207 void DwarfUnit::addString(DIE &Die, dwarf::Attribute Attribute,
208 StringRef String) {
210 if (!DD->useSplitDwarf())
211 return addLocalString(Die, Attribute, String);
213 unsigned idx = DU->getStringPool().getIndex(*Asm, String);
214 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
215 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
216 Die.addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
217 }
219 /// addLocalString - Add a string attribute data and value. This is guaranteed
220 /// to be in the local string pool instead of indirected.
221 void DwarfUnit::addLocalString(DIE &Die, dwarf::Attribute Attribute,
222 StringRef String) {
223 MCSymbol *Symb = DU->getStringPool().getSymbol(*Asm, String);
224 DIEValue *Value;
225 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
226 Value = new (DIEValueAllocator) DIELabel(Symb);
227 else {
228 MCSymbol *StringPool = DU->getStringPool().getSectionSymbol();
229 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
230 }
231 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
232 Die.addValue(Attribute, dwarf::DW_FORM_strp, Str);
233 }
235 /// addExpr - Add a Dwarf expression attribute data and value.
236 ///
237 void DwarfUnit::addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr) {
238 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
239 Die.addValue((dwarf::Attribute)0, Form, Value);
240 }
242 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
243 ///
244 void DwarfUnit::addLocationList(DIE &Die, dwarf::Attribute Attribute,
245 unsigned Index) {
246 DIEValue *Value = new (DIEValueAllocator) DIELocList(Index);
247 dwarf::Form Form = DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
248 : dwarf::DW_FORM_data4;
249 Die.addValue(Attribute, Form, Value);
250 }
252 /// addLabel - Add a Dwarf label attribute data and value.
253 ///
254 void DwarfUnit::addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form,
255 const MCSymbol *Label) {
256 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
257 Die.addValue(Attribute, Form, Value);
258 }
260 void DwarfUnit::addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label) {
261 addLabel(Die, (dwarf::Attribute)0, Form, Label);
262 }
264 /// addSectionLabel - Add a Dwarf section label attribute data and value.
265 ///
266 void DwarfUnit::addSectionLabel(DIE &Die, dwarf::Attribute Attribute,
267 const MCSymbol *Label) {
268 if (DD->getDwarfVersion() >= 4)
269 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
270 else
271 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
272 }
274 /// addSectionOffset - Add an offset into a section attribute data and value.
275 ///
276 void DwarfUnit::addSectionOffset(DIE &Die, dwarf::Attribute Attribute,
277 uint64_t Integer) {
278 if (DD->getDwarfVersion() >= 4)
279 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
280 else
281 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
282 }
284 /// addLabelAddress - Add a dwarf label attribute data and value using
285 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
286 ///
287 void DwarfCompileUnit::addLabelAddress(DIE &Die, dwarf::Attribute Attribute,
288 const MCSymbol *Label) {
290 if (!DD->useSplitDwarf())
291 return addLocalLabelAddress(Die, Attribute, Label);
293 if (Label)
294 DD->addArangeLabel(SymbolCU(this, Label));
296 unsigned idx = DD->getAddressPool().getIndex(Label);
297 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
298 Die.addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
299 }
301 void DwarfCompileUnit::addLocalLabelAddress(DIE &Die,
302 dwarf::Attribute Attribute,
303 const MCSymbol *Label) {
304 if (Label)
305 DD->addArangeLabel(SymbolCU(this, Label));
307 Die.addValue(Attribute, dwarf::DW_FORM_addr,
308 Label ? (DIEValue *)new (DIEValueAllocator) DIELabel(Label)
309 : new (DIEValueAllocator) DIEInteger(0));
310 }
312 unsigned DwarfCompileUnit::getOrCreateSourceID(StringRef FileName, StringRef DirName) {
313 // If we print assembly, we can't separate .file entries according to
314 // compile units. Thus all files will belong to the default compile unit.
316 // FIXME: add a better feature test than hasRawTextSupport. Even better,
317 // extend .file to support this.
318 return Asm->OutStreamer.EmitDwarfFileDirective(
319 0, DirName, FileName,
320 Asm->OutStreamer.hasRawTextSupport() ? 0 : getUniqueID());
321 }
323 unsigned DwarfTypeUnit::getOrCreateSourceID(StringRef FileName, StringRef DirName) {
324 return SplitLineTable ? SplitLineTable->getFile(DirName, FileName)
325 : getCU().getOrCreateSourceID(FileName, DirName);
326 }
328 /// addOpAddress - Add a dwarf op address data and value using the
329 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
330 ///
331 void DwarfUnit::addOpAddress(DIELoc &Die, const MCSymbol *Sym) {
332 if (!DD->useSplitDwarf()) {
333 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
334 addLabel(Die, dwarf::DW_FORM_udata, Sym);
335 } else {
336 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
337 addUInt(Die, dwarf::DW_FORM_GNU_addr_index,
338 DD->getAddressPool().getIndex(Sym));
339 }
340 }
342 /// addSectionDelta - Add a section label delta attribute data and value.
343 ///
344 void DwarfUnit::addSectionDelta(DIE &Die, dwarf::Attribute Attribute,
345 const MCSymbol *Hi, const MCSymbol *Lo) {
346 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
347 Die.addValue(Attribute, DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
348 : dwarf::DW_FORM_data4,
349 Value);
350 }
352 void DwarfUnit::addLabelDelta(DIE &Die, dwarf::Attribute Attribute,
353 const MCSymbol *Hi, const MCSymbol *Lo) {
354 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
355 Die.addValue(Attribute, dwarf::DW_FORM_data4, Value);
356 }
358 /// addDIEEntry - Add a DIE attribute data and value.
359 ///
360 void DwarfUnit::addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry) {
361 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
362 }
364 void DwarfUnit::addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type) {
365 // Flag the type unit reference as a declaration so that if it contains
366 // members (implicit special members, static data member definitions, member
367 // declarations for definitions in this CU, etc) consumers don't get confused
368 // and think this is a full definition.
369 addFlag(Die, dwarf::DW_AT_declaration);
371 Die.addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
372 new (DIEValueAllocator) DIETypeSignature(Type));
373 }
375 void DwarfUnit::addDIEEntry(DIE &Die, dwarf::Attribute Attribute,
376 DIEEntry *Entry) {
377 const DIE *DieCU = Die.getUnitOrNull();
378 const DIE *EntryCU = Entry->getEntry().getUnitOrNull();
379 if (!DieCU)
380 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
381 DieCU = &getUnitDie();
382 if (!EntryCU)
383 EntryCU = &getUnitDie();
384 Die.addValue(Attribute,
385 EntryCU == DieCU ? dwarf::DW_FORM_ref4 : dwarf::DW_FORM_ref_addr,
386 Entry);
387 }
389 /// Create a DIE with the given Tag, add the DIE to its parent, and
390 /// call insertDIE if MD is not null.
391 DIE &DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
392 assert(Tag != dwarf::DW_TAG_auto_variable &&
393 Tag != dwarf::DW_TAG_arg_variable);
394 Parent.addChild(make_unique<DIE>((dwarf::Tag)Tag));
395 DIE &Die = *Parent.getChildren().back();
396 if (N)
397 insertDIE(N, &Die);
398 return Die;
399 }
401 /// addBlock - Add block data.
402 ///
403 void DwarfUnit::addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Loc) {
404 Loc->ComputeSize(Asm);
405 DIELocs.push_back(Loc); // Memoize so we can call the destructor later on.
406 Die.addValue(Attribute, Loc->BestForm(DD->getDwarfVersion()), Loc);
407 }
409 void DwarfUnit::addBlock(DIE &Die, dwarf::Attribute Attribute,
410 DIEBlock *Block) {
411 Block->ComputeSize(Asm);
412 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
413 Die.addValue(Attribute, Block->BestForm(), Block);
414 }
416 /// addSourceLine - Add location information to specified debug information
417 /// entry.
418 void DwarfUnit::addSourceLine(DIE &Die, unsigned Line, StringRef File,
419 StringRef Directory) {
420 if (Line == 0)
421 return;
423 unsigned FileID = getOrCreateSourceID(File, Directory);
424 assert(FileID && "Invalid file id");
425 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
426 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
427 }
429 /// addSourceLine - Add location information to specified debug information
430 /// entry.
431 void DwarfUnit::addSourceLine(DIE &Die, DIVariable V) {
432 assert(V.isVariable());
434 addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
435 V.getContext().getDirectory());
436 }
438 /// addSourceLine - Add location information to specified debug information
439 /// entry.
440 void DwarfUnit::addSourceLine(DIE &Die, DIGlobalVariable G) {
441 assert(G.isGlobalVariable());
443 addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
444 }
446 /// addSourceLine - Add location information to specified debug information
447 /// entry.
448 void DwarfUnit::addSourceLine(DIE &Die, DISubprogram SP) {
449 assert(SP.isSubprogram());
451 addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
452 }
454 /// addSourceLine - Add location information to specified debug information
455 /// entry.
456 void DwarfUnit::addSourceLine(DIE &Die, DIType Ty) {
457 assert(Ty.isType());
459 addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
460 }
462 /// addSourceLine - Add location information to specified debug information
463 /// entry.
464 void DwarfUnit::addSourceLine(DIE &Die, DIObjCProperty Ty) {
465 assert(Ty.isObjCProperty());
467 DIFile File = Ty.getFile();
468 addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
469 File.getDirectory());
470 }
472 /// addSourceLine - Add location information to specified debug information
473 /// entry.
474 void DwarfUnit::addSourceLine(DIE &Die, DINameSpace NS) {
475 assert(NS.Verify());
477 addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
478 }
480 /// addVariableAddress - Add DW_AT_location attribute for a
481 /// DbgVariable based on provided MachineLocation.
482 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE &Die,
483 MachineLocation Location) {
484 if (DV.variableHasComplexAddress())
485 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
486 else if (DV.isBlockByrefVariable())
487 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
488 else
489 addAddress(Die, dwarf::DW_AT_location, Location,
490 DV.getVariable().isIndirect());
491 }
493 /// addRegisterOp - Add register operand.
494 void DwarfUnit::addRegisterOp(DIELoc &TheDie, unsigned Reg) {
495 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
496 int DWReg = RI->getDwarfRegNum(Reg, false);
497 bool isSubRegister = DWReg < 0;
499 unsigned Idx = 0;
501 // Go up the super-register chain until we hit a valid dwarf register number.
502 for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
503 DWReg = RI->getDwarfRegNum(*SR, false);
504 if (DWReg >= 0)
505 Idx = RI->getSubRegIndex(*SR, Reg);
506 }
508 if (DWReg < 0) {
509 DEBUG(dbgs() << "Invalid Dwarf register number.\n");
510 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
511 return;
512 }
514 // Emit register
515 if (DWReg < 32)
516 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
517 else {
518 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
519 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
520 }
522 // Emit Mask
523 if (isSubRegister) {
524 unsigned Size = RI->getSubRegIdxSize(Idx);
525 unsigned Offset = RI->getSubRegIdxOffset(Idx);
526 if (Offset > 0) {
527 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
528 addUInt(TheDie, dwarf::DW_FORM_data1, Size);
529 addUInt(TheDie, dwarf::DW_FORM_data1, Offset);
530 } else {
531 unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
532 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
533 addUInt(TheDie, dwarf::DW_FORM_data1, ByteSize);
534 }
535 }
536 }
538 /// addRegisterOffset - Add register offset.
539 void DwarfUnit::addRegisterOffset(DIELoc &TheDie, unsigned Reg,
540 int64_t Offset) {
541 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
542 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
543 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
544 if (Reg == TRI->getFrameRegister(*Asm->MF))
545 // If variable offset is based in frame register then use fbreg.
546 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
547 else if (DWReg < 32)
548 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
549 else {
550 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
551 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
552 }
553 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
554 }
556 /// addAddress - Add an address attribute to a die based on the location
557 /// provided.
558 void DwarfUnit::addAddress(DIE &Die, dwarf::Attribute Attribute,
559 const MachineLocation &Location, bool Indirect) {
560 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
562 if (Location.isReg() && !Indirect)
563 addRegisterOp(*Loc, Location.getReg());
564 else {
565 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
566 if (Indirect && !Location.isReg()) {
567 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
568 }
569 }
571 // Now attach the location information to the DIE.
572 addBlock(Die, Attribute, Loc);
573 }
575 /// addComplexAddress - Start with the address based on the location provided,
576 /// and generate the DWARF information necessary to find the actual variable
577 /// given the extra address information encoded in the DbgVariable, starting
578 /// from the starting location. Add the DWARF information to the die.
579 ///
580 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE &Die,
581 dwarf::Attribute Attribute,
582 const MachineLocation &Location) {
583 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
584 unsigned N = DV.getNumAddrElements();
585 unsigned i = 0;
586 if (Location.isReg()) {
587 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
588 // If first address element is OpPlus then emit
589 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
590 addRegisterOffset(*Loc, Location.getReg(), DV.getAddrElement(1));
591 i = 2;
592 } else
593 addRegisterOp(*Loc, Location.getReg());
594 } else
595 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
597 for (; i < N; ++i) {
598 uint64_t Element = DV.getAddrElement(i);
599 if (Element == DIBuilder::OpPlus) {
600 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
601 addUInt(*Loc, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
602 } else if (Element == DIBuilder::OpDeref) {
603 if (!Location.isReg())
604 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
605 } else
606 llvm_unreachable("unknown DIBuilder Opcode");
607 }
609 // Now attach the location information to the DIE.
610 addBlock(Die, Attribute, Loc);
611 }
613 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
614 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
615 gives the variable VarName either the struct, or a pointer to the struct, as
616 its type. This is necessary for various behind-the-scenes things the
617 compiler needs to do with by-reference variables in Blocks.
619 However, as far as the original *programmer* is concerned, the variable
620 should still have type 'SomeType', as originally declared.
622 The function getBlockByrefType dives into the __Block_byref_x_VarName
623 struct to find the original type of the variable, which is then assigned to
624 the variable's Debug Information Entry as its real type. So far, so good.
625 However now the debugger will expect the variable VarName to have the type
626 SomeType. So we need the location attribute for the variable to be an
627 expression that explains to the debugger how to navigate through the
628 pointers and struct to find the actual variable of type SomeType.
630 The following function does just that. We start by getting
631 the "normal" location for the variable. This will be the location
632 of either the struct __Block_byref_x_VarName or the pointer to the
633 struct __Block_byref_x_VarName.
635 The struct will look something like:
637 struct __Block_byref_x_VarName {
638 ... <various fields>
639 struct __Block_byref_x_VarName *forwarding;
640 ... <various other fields>
641 SomeType VarName;
642 ... <maybe more fields>
643 };
645 If we are given the struct directly (as our starting point) we
646 need to tell the debugger to:
648 1). Add the offset of the forwarding field.
650 2). Follow that pointer to get the real __Block_byref_x_VarName
651 struct to use (the real one may have been copied onto the heap).
653 3). Add the offset for the field VarName, to find the actual variable.
655 If we started with a pointer to the struct, then we need to
656 dereference that pointer first, before the other steps.
657 Translating this into DWARF ops, we will need to append the following
658 to the current location description for the variable:
660 DW_OP_deref -- optional, if we start with a pointer
661 DW_OP_plus_uconst <forward_fld_offset>
662 DW_OP_deref
663 DW_OP_plus_uconst <varName_fld_offset>
665 That is what this function does. */
667 /// addBlockByrefAddress - Start with the address based on the location
668 /// provided, and generate the DWARF information necessary to find the
669 /// actual Block variable (navigating the Block struct) based on the
670 /// starting location. Add the DWARF information to the die. For
671 /// more information, read large comment just above here.
672 ///
673 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE &Die,
674 dwarf::Attribute Attribute,
675 const MachineLocation &Location) {
676 DIType Ty = DV.getType();
677 DIType TmpTy = Ty;
678 uint16_t Tag = Ty.getTag();
679 bool isPointer = false;
681 StringRef varName = DV.getName();
683 if (Tag == dwarf::DW_TAG_pointer_type) {
684 DIDerivedType DTy(Ty);
685 TmpTy = resolve(DTy.getTypeDerivedFrom());
686 isPointer = true;
687 }
689 DICompositeType blockStruct(TmpTy);
691 // Find the __forwarding field and the variable field in the __Block_byref
692 // struct.
693 DIArray Fields = blockStruct.getTypeArray();
694 DIDerivedType varField;
695 DIDerivedType forwardingField;
697 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
698 DIDerivedType DT(Fields.getElement(i));
699 StringRef fieldName = DT.getName();
700 if (fieldName == "__forwarding")
701 forwardingField = DT;
702 else if (fieldName == varName)
703 varField = DT;
704 }
706 // Get the offsets for the forwarding field and the variable field.
707 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
708 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
710 // Decode the original location, and use that as the start of the byref
711 // variable's location.
712 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
714 if (Location.isReg())
715 addRegisterOp(*Loc, Location.getReg());
716 else
717 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
719 // If we started with a pointer to the __Block_byref... struct, then
720 // the first thing we need to do is dereference the pointer (DW_OP_deref).
721 if (isPointer)
722 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
724 // Next add the offset for the '__forwarding' field:
725 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
726 // adding the offset if it's 0.
727 if (forwardingFieldOffset > 0) {
728 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
729 addUInt(*Loc, dwarf::DW_FORM_udata, forwardingFieldOffset);
730 }
732 // Now dereference the __forwarding field to get to the real __Block_byref
733 // struct: DW_OP_deref.
734 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
736 // Now that we've got the real __Block_byref... struct, add the offset
737 // for the variable's field to get to the location of the actual variable:
738 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
739 if (varFieldOffset > 0) {
740 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
741 addUInt(*Loc, dwarf::DW_FORM_udata, varFieldOffset);
742 }
744 // Now attach the location information to the DIE.
745 addBlock(Die, Attribute, Loc);
746 }
748 /// Return true if type encoding is unsigned.
749 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
750 DIDerivedType DTy(Ty);
751 if (DTy.isDerivedType()) {
752 dwarf::Tag T = (dwarf::Tag)Ty.getTag();
753 // Encode pointer constants as unsigned bytes. This is used at least for
754 // null pointer constant emission.
755 // FIXME: reference and rvalue_reference /probably/ shouldn't be allowed
756 // here, but accept them for now due to a bug in SROA producing bogus
757 // dbg.values.
758 if (T == dwarf::DW_TAG_pointer_type ||
759 T == dwarf::DW_TAG_ptr_to_member_type ||
760 T == dwarf::DW_TAG_reference_type ||
761 T == dwarf::DW_TAG_rvalue_reference_type)
762 return true;
763 assert(T == dwarf::DW_TAG_typedef || T == dwarf::DW_TAG_const_type ||
764 T == dwarf::DW_TAG_volatile_type ||
765 T == dwarf::DW_TAG_restrict_type ||
766 T == dwarf::DW_TAG_enumeration_type);
767 if (DITypeRef Deriv = DTy.getTypeDerivedFrom())
768 return isUnsignedDIType(DD, DD->resolve(Deriv));
769 // FIXME: Enums without a fixed underlying type have unknown signedness
770 // here, leading to incorrectly emitted constants.
771 assert(DTy.getTag() == dwarf::DW_TAG_enumeration_type);
772 return false;
773 }
775 DIBasicType BTy(Ty);
776 assert(BTy.isBasicType());
777 unsigned Encoding = BTy.getEncoding();
778 assert((Encoding == dwarf::DW_ATE_unsigned ||
779 Encoding == dwarf::DW_ATE_unsigned_char ||
780 Encoding == dwarf::DW_ATE_signed ||
781 Encoding == dwarf::DW_ATE_signed_char ||
782 Encoding == dwarf::DW_ATE_UTF || Encoding == dwarf::DW_ATE_boolean) &&
783 "Unsupported encoding");
784 return (Encoding == dwarf::DW_ATE_unsigned ||
785 Encoding == dwarf::DW_ATE_unsigned_char ||
786 Encoding == dwarf::DW_ATE_UTF || Encoding == dwarf::DW_ATE_boolean);
787 }
789 /// If this type is derived from a base type then return base type size.
790 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
791 unsigned Tag = Ty.getTag();
793 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
794 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
795 Tag != dwarf::DW_TAG_restrict_type)
796 return Ty.getSizeInBits();
798 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
800 // If this type is not derived from any type or the type is a declaration then
801 // take conservative approach.
802 if (!BaseType.isValid() || BaseType.isForwardDecl())
803 return Ty.getSizeInBits();
805 // If this is a derived type, go ahead and get the base type, unless it's a
806 // reference then it's just the size of the field. Pointer types have no need
807 // of this since they're a different type of qualification on the type.
808 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
809 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
810 return Ty.getSizeInBits();
812 if (BaseType.isDerivedType())
813 return getBaseTypeSize(DD, DIDerivedType(BaseType));
815 return BaseType.getSizeInBits();
816 }
818 /// addConstantFPValue - Add constant value entry in variable DIE.
819 void DwarfUnit::addConstantFPValue(DIE &Die, const MachineOperand &MO) {
820 assert(MO.isFPImm() && "Invalid machine operand!");
821 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
822 APFloat FPImm = MO.getFPImm()->getValueAPF();
824 // Get the raw data form of the floating point.
825 const APInt FltVal = FPImm.bitcastToAPInt();
826 const char *FltPtr = (const char *)FltVal.getRawData();
828 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
829 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
830 int Incr = (LittleEndian ? 1 : -1);
831 int Start = (LittleEndian ? 0 : NumBytes - 1);
832 int Stop = (LittleEndian ? NumBytes : -1);
834 // Output the constant to DWARF one byte at a time.
835 for (; Start != Stop; Start += Incr)
836 addUInt(*Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
838 addBlock(Die, dwarf::DW_AT_const_value, Block);
839 }
841 /// addConstantFPValue - Add constant value entry in variable DIE.
842 void DwarfUnit::addConstantFPValue(DIE &Die, const ConstantFP *CFP) {
843 // Pass this down to addConstantValue as an unsigned bag of bits.
844 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
845 }
847 /// addConstantValue - Add constant value entry in variable DIE.
848 void DwarfUnit::addConstantValue(DIE &Die, const ConstantInt *CI, DIType Ty) {
849 addConstantValue(Die, CI->getValue(), Ty);
850 }
852 /// addConstantValue - Add constant value entry in variable DIE.
853 void DwarfUnit::addConstantValue(DIE &Die, const MachineOperand &MO,
854 DIType Ty) {
855 assert(MO.isImm() && "Invalid machine operand!");
857 addConstantValue(Die, isUnsignedDIType(DD, Ty), MO.getImm());
858 }
860 void DwarfUnit::addConstantValue(DIE &Die, bool Unsigned, uint64_t Val) {
861 // FIXME: This is a bit conservative/simple - it emits negative values always
862 // sign extended to 64 bits rather than minimizing the number of bytes.
863 addUInt(Die, dwarf::DW_AT_const_value,
864 Unsigned ? dwarf::DW_FORM_udata : dwarf::DW_FORM_sdata, Val);
865 }
867 void DwarfUnit::addConstantValue(DIE &Die, const APInt &Val, DIType Ty) {
868 addConstantValue(Die, Val, isUnsignedDIType(DD, Ty));
869 }
871 // addConstantValue - Add constant value entry in variable DIE.
872 void DwarfUnit::addConstantValue(DIE &Die, const APInt &Val, bool Unsigned) {
873 unsigned CIBitWidth = Val.getBitWidth();
874 if (CIBitWidth <= 64) {
875 addConstantValue(Die, Unsigned,
876 Unsigned ? Val.getZExtValue() : Val.getSExtValue());
877 return;
878 }
880 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
882 // Get the raw data form of the large APInt.
883 const uint64_t *Ptr64 = Val.getRawData();
885 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
886 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
888 // Output the constant to DWARF one byte at a time.
889 for (int i = 0; i < NumBytes; i++) {
890 uint8_t c;
891 if (LittleEndian)
892 c = Ptr64[i / 8] >> (8 * (i & 7));
893 else
894 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
895 addUInt(*Block, dwarf::DW_FORM_data1, c);
896 }
898 addBlock(Die, dwarf::DW_AT_const_value, Block);
899 }
901 /// addTemplateParams - Add template parameters into buffer.
902 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
903 // Add template parameters.
904 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
905 DIDescriptor Element = TParams.getElement(i);
906 if (Element.isTemplateTypeParameter())
907 constructTemplateTypeParameterDIE(Buffer,
908 DITemplateTypeParameter(Element));
909 else if (Element.isTemplateValueParameter())
910 constructTemplateValueParameterDIE(Buffer,
911 DITemplateValueParameter(Element));
912 }
913 }
915 /// getOrCreateContextDIE - Get context owner's DIE.
916 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
917 if (!Context || Context.isFile())
918 return &getUnitDie();
919 if (Context.isType())
920 return getOrCreateTypeDIE(DIType(Context));
921 if (Context.isNameSpace())
922 return getOrCreateNameSpace(DINameSpace(Context));
923 if (Context.isSubprogram())
924 return getOrCreateSubprogramDIE(DISubprogram(Context));
925 return getDIE(Context);
926 }
928 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
929 DIScope Context = resolve(Ty.getContext());
930 DIE *ContextDIE = getOrCreateContextDIE(Context);
932 if (DIE *TyDIE = getDIE(Ty))
933 return TyDIE;
935 // Create new type.
936 DIE &TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
938 constructTypeDIE(TyDIE, Ty);
940 updateAcceleratorTables(Context, Ty, TyDIE);
941 return &TyDIE;
942 }
944 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
945 /// given DIType.
946 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
947 if (!TyNode)
948 return nullptr;
950 DIType Ty(TyNode);
951 assert(Ty.isType());
952 assert(Ty == resolve(Ty.getRef()) &&
953 "type was not uniqued, possible ODR violation.");
955 // DW_TAG_restrict_type is not supported in DWARF2
956 if (Ty.getTag() == dwarf::DW_TAG_restrict_type && DD->getDwarfVersion() <= 2)
957 return getOrCreateTypeDIE(resolve(DIDerivedType(Ty).getTypeDerivedFrom()));
959 // Construct the context before querying for the existence of the DIE in case
960 // such construction creates the DIE.
961 DIScope Context = resolve(Ty.getContext());
962 DIE *ContextDIE = getOrCreateContextDIE(Context);
963 assert(ContextDIE);
965 if (DIE *TyDIE = getDIE(Ty))
966 return TyDIE;
968 // Create new type.
969 DIE &TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
971 updateAcceleratorTables(Context, Ty, TyDIE);
973 if (Ty.isBasicType())
974 constructTypeDIE(TyDIE, DIBasicType(Ty));
975 else if (Ty.isCompositeType()) {
976 DICompositeType CTy(Ty);
977 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
978 if (MDString *TypeId = CTy.getIdentifier()) {
979 DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
980 // Skip updating the accelerator tables since this is not the full type.
981 return &TyDIE;
982 }
983 constructTypeDIE(TyDIE, CTy);
984 } else {
985 assert(Ty.isDerivedType() && "Unknown kind of DIType");
986 constructTypeDIE(TyDIE, DIDerivedType(Ty));
987 }
989 return &TyDIE;
990 }
992 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
993 const DIE &TyDIE) {
994 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
995 bool IsImplementation = 0;
996 if (Ty.isCompositeType()) {
997 DICompositeType CT(Ty);
998 // A runtime language of 0 actually means C/C++ and that any
999 // non-negative value is some version of Objective-C/C++.
1000 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
1001 }
1002 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
1003 DD->addAccelType(Ty.getName(), TyDIE, Flags);
1005 if ((!Context || Context.isCompileUnit() || Context.isFile() ||
1006 Context.isNameSpace()) &&
1007 getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
1008 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] =
1009 &TyDIE;
1010 }
1011 }
1013 /// addType - Add a new type attribute to the specified entity.
1014 void DwarfUnit::addType(DIE &Entity, DIType Ty, dwarf::Attribute Attribute) {
1015 assert(Ty && "Trying to add a type that doesn't exist?");
1017 // Check for pre-existence.
1018 DIEEntry *Entry = getDIEEntry(Ty);
1019 // If it exists then use the existing value.
1020 if (Entry) {
1021 addDIEEntry(Entity, Attribute, Entry);
1022 return;
1023 }
1025 // Construct type.
1026 DIE *Buffer = getOrCreateTypeDIE(Ty);
1028 // Set up proxy.
1029 Entry = createDIEEntry(*Buffer);
1030 insertDIEEntry(Ty, Entry);
1031 addDIEEntry(Entity, Attribute, Entry);
1032 }
1034 /// addGlobalName - Add a new global name to the compile unit.
1035 void DwarfUnit::addGlobalName(StringRef Name, DIE &Die, DIScope Context) {
1036 if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
1037 return;
1038 std::string FullName = getParentContextString(Context) + Name.str();
1039 GlobalNames[FullName] = &Die;
1040 }
1042 /// getParentContextString - Walks the metadata parent chain in a language
1043 /// specific manner (using the compile unit language) and returns
1044 /// it as a string. This is done at the metadata level because DIEs may
1045 /// not currently have been added to the parent context and walking the
1046 /// DIEs looking for names is more expensive than walking the metadata.
1047 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1048 if (!Context)
1049 return "";
1051 // FIXME: Decide whether to implement this for non-C++ languages.
1052 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1053 return "";
1055 std::string CS;
1056 SmallVector<DIScope, 1> Parents;
1057 while (!Context.isCompileUnit()) {
1058 Parents.push_back(Context);
1059 if (Context.getContext())
1060 Context = resolve(Context.getContext());
1061 else
1062 // Structure, etc types will have a NULL context if they're at the top
1063 // level.
1064 break;
1065 }
1067 // Reverse iterate over our list to go from the outermost construct to the
1068 // innermost.
1069 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1070 E = Parents.rend();
1071 I != E; ++I) {
1072 DIScope Ctx = *I;
1073 StringRef Name = Ctx.getName();
1074 if (!Name.empty()) {
1075 CS += Name;
1076 CS += "::";
1077 }
1078 }
1079 return CS;
1080 }
1082 /// constructTypeDIE - Construct basic type die from DIBasicType.
1083 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1084 // Get core information.
1085 StringRef Name = BTy.getName();
1086 // Add name if not anonymous or intermediate type.
1087 if (!Name.empty())
1088 addString(Buffer, dwarf::DW_AT_name, Name);
1090 // An unspecified type only has a name attribute.
1091 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1092 return;
1094 addUInt(Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1095 BTy.getEncoding());
1097 uint64_t Size = BTy.getSizeInBits() >> 3;
1098 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1099 }
1101 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1102 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1103 // Get core information.
1104 StringRef Name = DTy.getName();
1105 uint64_t Size = DTy.getSizeInBits() >> 3;
1106 uint16_t Tag = Buffer.getTag();
1108 // Map to main type, void will not have a type.
1109 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1110 if (FromTy)
1111 addType(Buffer, FromTy);
1113 // Add name if not anonymous or intermediate type.
1114 if (!Name.empty())
1115 addString(Buffer, dwarf::DW_AT_name, Name);
1117 // Add size if non-zero (derived types might be zero-sized.)
1118 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1119 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1121 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1122 addDIEEntry(Buffer, dwarf::DW_AT_containing_type,
1123 *getOrCreateTypeDIE(resolve(DTy.getClassType())));
1124 // Add source line info if available and TyDesc is not a forward declaration.
1125 if (!DTy.isForwardDecl())
1126 addSourceLine(Buffer, DTy);
1127 }
1129 /// constructSubprogramArguments - Construct function argument DIEs.
1130 void DwarfUnit::constructSubprogramArguments(DIE &Buffer, DIArray Args) {
1131 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1132 DIDescriptor Ty = Args.getElement(i);
1133 if (Ty.isUnspecifiedParameter()) {
1134 assert(i == N-1 && "Unspecified parameter must be the last argument");
1135 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1136 } else {
1137 DIE &Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1138 addType(Arg, DIType(Ty));
1139 if (DIType(Ty).isArtificial())
1140 addFlag(Arg, dwarf::DW_AT_artificial);
1141 }
1142 }
1143 }
1145 /// constructTypeDIE - Construct type DIE from DICompositeType.
1146 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1147 // Add name if not anonymous or intermediate type.
1148 StringRef Name = CTy.getName();
1150 uint64_t Size = CTy.getSizeInBits() >> 3;
1151 uint16_t Tag = Buffer.getTag();
1153 switch (Tag) {
1154 case dwarf::DW_TAG_array_type:
1155 constructArrayTypeDIE(Buffer, CTy);
1156 break;
1157 case dwarf::DW_TAG_enumeration_type:
1158 constructEnumTypeDIE(Buffer, CTy);
1159 break;
1160 case dwarf::DW_TAG_subroutine_type: {
1161 // Add return type. A void return won't have a type.
1162 DIArray Elements = CTy.getTypeArray();
1163 DIType RTy(Elements.getElement(0));
1164 if (RTy)
1165 addType(Buffer, RTy);
1167 bool isPrototyped = true;
1168 if (Elements.getNumElements() == 2 &&
1169 Elements.getElement(1).isUnspecifiedParameter())
1170 isPrototyped = false;
1172 constructSubprogramArguments(Buffer, Elements);
1174 // Add prototype flag if we're dealing with a C language and the
1175 // function has been prototyped.
1176 uint16_t Language = getLanguage();
1177 if (isPrototyped &&
1178 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1179 Language == dwarf::DW_LANG_ObjC))
1180 addFlag(Buffer, dwarf::DW_AT_prototyped);
1182 if (CTy.isLValueReference())
1183 addFlag(Buffer, dwarf::DW_AT_reference);
1185 if (CTy.isRValueReference())
1186 addFlag(Buffer, dwarf::DW_AT_rvalue_reference);
1187 } break;
1188 case dwarf::DW_TAG_structure_type:
1189 case dwarf::DW_TAG_union_type:
1190 case dwarf::DW_TAG_class_type: {
1191 // Add elements to structure type.
1192 DIArray Elements = CTy.getTypeArray();
1193 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1194 DIDescriptor Element = Elements.getElement(i);
1195 if (Element.isSubprogram())
1196 getOrCreateSubprogramDIE(DISubprogram(Element));
1197 else if (Element.isDerivedType()) {
1198 DIDerivedType DDTy(Element);
1199 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1200 DIE &ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1201 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1202 dwarf::DW_AT_friend);
1203 } else if (DDTy.isStaticMember()) {
1204 getOrCreateStaticMemberDIE(DDTy);
1205 } else {
1206 constructMemberDIE(Buffer, DDTy);
1207 }
1208 } else if (Element.isObjCProperty()) {
1209 DIObjCProperty Property(Element);
1210 DIE &ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1211 StringRef PropertyName = Property.getObjCPropertyName();
1212 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1213 if (Property.getType())
1214 addType(ElemDie, Property.getType());
1215 addSourceLine(ElemDie, Property);
1216 StringRef GetterName = Property.getObjCPropertyGetterName();
1217 if (!GetterName.empty())
1218 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1219 StringRef SetterName = Property.getObjCPropertySetterName();
1220 if (!SetterName.empty())
1221 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1222 unsigned PropertyAttributes = 0;
1223 if (Property.isReadOnlyObjCProperty())
1224 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1225 if (Property.isReadWriteObjCProperty())
1226 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1227 if (Property.isAssignObjCProperty())
1228 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1229 if (Property.isRetainObjCProperty())
1230 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1231 if (Property.isCopyObjCProperty())
1232 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1233 if (Property.isNonAtomicObjCProperty())
1234 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1235 if (PropertyAttributes)
1236 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1237 PropertyAttributes);
1239 DIEEntry *Entry = getDIEEntry(Element);
1240 if (!Entry) {
1241 Entry = createDIEEntry(ElemDie);
1242 insertDIEEntry(Element, Entry);
1243 }
1244 } else
1245 continue;
1246 }
1248 if (CTy.isAppleBlockExtension())
1249 addFlag(Buffer, dwarf::DW_AT_APPLE_block);
1251 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1252 if (ContainingType)
1253 addDIEEntry(Buffer, dwarf::DW_AT_containing_type,
1254 *getOrCreateTypeDIE(ContainingType));
1256 if (CTy.isObjcClassComplete())
1257 addFlag(Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1259 // Add template parameters to a class, structure or union types.
1260 // FIXME: The support isn't in the metadata for this yet.
1261 if (Tag == dwarf::DW_TAG_class_type ||
1262 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1263 addTemplateParams(Buffer, CTy.getTemplateParams());
1265 break;
1266 }
1267 default:
1268 break;
1269 }
1271 // Add name if not anonymous or intermediate type.
1272 if (!Name.empty())
1273 addString(Buffer, dwarf::DW_AT_name, Name);
1275 if (Tag == dwarf::DW_TAG_enumeration_type ||
1276 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1277 Tag == dwarf::DW_TAG_union_type) {
1278 // Add size if non-zero (derived types might be zero-sized.)
1279 // TODO: Do we care about size for enum forward declarations?
1280 if (Size)
1281 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1282 else if (!CTy.isForwardDecl())
1283 // Add zero size if it is not a forward declaration.
1284 addUInt(Buffer, dwarf::DW_AT_byte_size, None, 0);
1286 // If we're a forward decl, say so.
1287 if (CTy.isForwardDecl())
1288 addFlag(Buffer, dwarf::DW_AT_declaration);
1290 // Add source line info if available.
1291 if (!CTy.isForwardDecl())
1292 addSourceLine(Buffer, CTy);
1294 // No harm in adding the runtime language to the declaration.
1295 unsigned RLang = CTy.getRunTimeLang();
1296 if (RLang)
1297 addUInt(Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1298 RLang);
1299 }
1300 }
1302 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1303 /// DITemplateTypeParameter.
1304 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1305 DITemplateTypeParameter TP) {
1306 DIE &ParamDIE =
1307 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1308 // Add the type if it exists, it could be void and therefore no type.
1309 if (TP.getType())
1310 addType(ParamDIE, resolve(TP.getType()));
1311 if (!TP.getName().empty())
1312 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1313 }
1315 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1316 /// DITemplateValueParameter.
1317 void
1318 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1319 DITemplateValueParameter VP) {
1320 DIE &ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1322 // Add the type if there is one, template template and template parameter
1323 // packs will not have a type.
1324 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1325 addType(ParamDIE, resolve(VP.getType()));
1326 if (!VP.getName().empty())
1327 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1328 if (Value *Val = VP.getValue()) {
1329 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1330 addConstantValue(ParamDIE, CI, resolve(VP.getType()));
1331 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1332 // For declaration non-type template parameters (such as global values and
1333 // functions)
1334 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1335 addOpAddress(*Loc, Asm->getSymbol(GV));
1336 // Emit DW_OP_stack_value to use the address as the immediate value of the
1337 // parameter, rather than a pointer to it.
1338 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1339 addBlock(ParamDIE, dwarf::DW_AT_location, Loc);
1340 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1341 assert(isa<MDString>(Val));
1342 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1343 cast<MDString>(Val)->getString());
1344 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1345 assert(isa<MDNode>(Val));
1346 DIArray A(cast<MDNode>(Val));
1347 addTemplateParams(ParamDIE, A);
1348 }
1349 }
1350 }
1352 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1353 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1354 // Construct the context before querying for the existence of the DIE in case
1355 // such construction creates the DIE.
1356 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1358 if (DIE *NDie = getDIE(NS))
1359 return NDie;
1360 DIE &NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1362 if (!NS.getName().empty()) {
1363 addString(NDie, dwarf::DW_AT_name, NS.getName());
1364 DD->addAccelNamespace(NS.getName(), NDie);
1365 addGlobalName(NS.getName(), NDie, NS.getContext());
1366 } else
1367 DD->addAccelNamespace("(anonymous namespace)", NDie);
1368 addSourceLine(NDie, NS);
1369 return &NDie;
1370 }
1372 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1373 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1374 // Construct the context before querying for the existence of the DIE in case
1375 // such construction creates the DIE (as is the case for member function
1376 // declarations).
1377 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1379 if (DIE *SPDie = getDIE(SP))
1380 return SPDie;
1382 if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
1383 // Add subprogram definitions to the CU die directly.
1384 ContextDIE = &getUnitDie();
1385 // Build the decl now to ensure it precedes the definition.
1386 getOrCreateSubprogramDIE(SPDecl);
1387 }
1389 // DW_TAG_inlined_subroutine may refer to this DIE.
1390 DIE &SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1392 // Abort here and fill this in later, depending on whether or not this
1393 // subprogram turns out to have inlined instances or not.
1394 if (SP.isDefinition())
1395 return &SPDie;
1397 applySubprogramAttributes(SP, SPDie);
1398 return &SPDie;
1399 }
1401 void DwarfUnit::applySubprogramAttributes(DISubprogram SP, DIE &SPDie) {
1402 DIE *DeclDie = nullptr;
1403 StringRef DeclLinkageName;
1404 if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
1405 DeclDie = getDIE(SPDecl);
1406 assert(DeclDie);
1407 DeclLinkageName = SPDecl.getLinkageName();
1408 }
1410 // Add function template parameters.
1411 addTemplateParams(SPDie, SP.getTemplateParams());
1413 // Add the linkage name if we have one and it isn't in the Decl.
1414 StringRef LinkageName = SP.getLinkageName();
1415 assert(((LinkageName.empty() || DeclLinkageName.empty()) ||
1416 LinkageName == DeclLinkageName) &&
1417 "decl has a linkage name and it is different");
1418 if (!LinkageName.empty() && DeclLinkageName.empty())
1419 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1420 GlobalValue::getRealLinkageName(LinkageName));
1422 if (DeclDie) {
1423 // Refer to the function declaration where all the other attributes will be
1424 // found.
1425 addDIEEntry(SPDie, dwarf::DW_AT_specification, *DeclDie);
1426 return;
1427 }
1429 // Constructors and operators for anonymous aggregates do not have names.
1430 if (!SP.getName().empty())
1431 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1433 addSourceLine(SPDie, SP);
1435 // Add the prototype if we have a prototype and we have a C like
1436 // language.
1437 uint16_t Language = getLanguage();
1438 if (SP.isPrototyped() &&
1439 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1440 Language == dwarf::DW_LANG_ObjC))
1441 addFlag(SPDie, dwarf::DW_AT_prototyped);
1443 DICompositeType SPTy = SP.getType();
1444 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1445 "the type of a subprogram should be a subroutine");
1447 DIArray Args = SPTy.getTypeArray();
1448 // Add a return type. If this is a type like a C/C++ void type we don't add a
1449 // return type.
1450 if (Args.getElement(0))
1451 addType(SPDie, DIType(Args.getElement(0)));
1453 unsigned VK = SP.getVirtuality();
1454 if (VK) {
1455 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1456 DIELoc *Block = getDIELoc();
1457 addUInt(*Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1458 addUInt(*Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1459 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1460 ContainingTypeMap.insert(
1461 std::make_pair(&SPDie, resolve(SP.getContainingType())));
1462 }
1464 if (!SP.isDefinition()) {
1465 addFlag(SPDie, dwarf::DW_AT_declaration);
1467 // Add arguments. Do not add arguments for subprogram definition. They will
1468 // be handled while processing variables.
1469 constructSubprogramArguments(SPDie, Args);
1470 }
1472 if (SP.isArtificial())
1473 addFlag(SPDie, dwarf::DW_AT_artificial);
1475 if (!SP.isLocalToUnit())
1476 addFlag(SPDie, dwarf::DW_AT_external);
1478 if (SP.isOptimized())
1479 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1481 if (unsigned isa = Asm->getISAEncoding()) {
1482 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1483 }
1485 if (SP.isLValueReference())
1486 addFlag(SPDie, dwarf::DW_AT_reference);
1488 if (SP.isRValueReference())
1489 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1491 if (SP.isProtected())
1492 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1493 dwarf::DW_ACCESS_protected);
1494 else if (SP.isPrivate())
1495 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1496 dwarf::DW_ACCESS_private);
1497 else
1498 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1499 dwarf::DW_ACCESS_public);
1501 if (SP.isExplicit())
1502 addFlag(SPDie, dwarf::DW_AT_explicit);
1503 }
1505 // Return const expression if value is a GEP to access merged global
1506 // constant. e.g.
1507 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1508 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1509 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1510 if (!CE || CE->getNumOperands() != 3 ||
1511 CE->getOpcode() != Instruction::GetElementPtr)
1512 return nullptr;
1514 // First operand points to a global struct.
1515 Value *Ptr = CE->getOperand(0);
1516 if (!isa<GlobalValue>(Ptr) ||
1517 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1518 return nullptr;
1520 // Second operand is zero.
1521 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1522 if (!CI || !CI->isZero())
1523 return nullptr;
1525 // Third operand is offset.
1526 if (!isa<ConstantInt>(CE->getOperand(2)))
1527 return nullptr;
1529 return CE;
1530 }
1532 /// createGlobalVariableDIE - create global variable DIE.
1533 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1534 // Check for pre-existence.
1535 if (getDIE(GV))
1536 return;
1538 assert(GV.isGlobalVariable());
1540 DIScope GVContext = GV.getContext();
1541 DIType GTy = DD->resolve(GV.getType());
1543 // If this is a static data member definition, some attributes belong
1544 // to the declaration DIE.
1545 DIE *VariableDIE = nullptr;
1546 bool IsStaticMember = false;
1547 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1548 if (SDMDecl.Verify()) {
1549 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1550 // We need the declaration DIE that is in the static member's class.
1551 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1552 IsStaticMember = true;
1553 }
1555 // If this is not a static data member definition, create the variable
1556 // DIE and add the initial set of attributes to it.
1557 if (!VariableDIE) {
1558 // Construct the context before querying for the existence of the DIE in
1559 // case such construction creates the DIE.
1560 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1562 // Add to map.
1563 VariableDIE = &createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1565 // Add name and type.
1566 addString(*VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1567 addType(*VariableDIE, GTy);
1569 // Add scoping info.
1570 if (!GV.isLocalToUnit())
1571 addFlag(*VariableDIE, dwarf::DW_AT_external);
1573 // Add line number info.
1574 addSourceLine(*VariableDIE, GV);
1575 }
1577 // Add location.
1578 bool addToAccelTable = false;
1579 DIE *VariableSpecDIE = nullptr;
1580 bool isGlobalVariable = GV.getGlobal() != nullptr;
1581 if (isGlobalVariable) {
1582 addToAccelTable = true;
1583 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1584 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1585 if (GV.getGlobal()->isThreadLocal()) {
1586 // FIXME: Make this work with -gsplit-dwarf.
1587 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1588 assert((PointerSize == 4 || PointerSize == 8) &&
1589 "Add support for other sizes if necessary");
1590 // Based on GCC's support for TLS:
1591 if (!DD->useSplitDwarf()) {
1592 // 1) Start with a constNu of the appropriate pointer size
1593 addUInt(*Loc, dwarf::DW_FORM_data1,
1594 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1595 // 2) containing the (relocated) offset of the TLS variable
1596 // within the module's TLS block.
1597 addExpr(*Loc, dwarf::DW_FORM_udata,
1598 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym));
1599 } else {
1600 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1601 addUInt(*Loc, dwarf::DW_FORM_udata,
1602 DD->getAddressPool().getIndex(Sym, /* TLS */ true));
1603 }
1604 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1605 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1606 } else {
1607 DD->addArangeLabel(SymbolCU(this, Sym));
1608 addOpAddress(*Loc, Sym);
1609 }
1610 // Do not create specification DIE if context is either compile unit
1611 // or a subprogram.
1612 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1613 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1614 // Create specification DIE.
1615 VariableSpecDIE = &createAndAddDIE(dwarf::DW_TAG_variable, UnitDie);
1616 addDIEEntry(*VariableSpecDIE, dwarf::DW_AT_specification, *VariableDIE);
1617 addBlock(*VariableSpecDIE, dwarf::DW_AT_location, Loc);
1618 // A static member's declaration is already flagged as such.
1619 if (!SDMDecl.Verify())
1620 addFlag(*VariableDIE, dwarf::DW_AT_declaration);
1621 } else {
1622 addBlock(*VariableDIE, dwarf::DW_AT_location, Loc);
1623 }
1624 // Add the linkage name.
1625 StringRef LinkageName = GV.getLinkageName();
1626 if (!LinkageName.empty())
1627 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1628 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1629 // TAG_variable.
1630 addString(IsStaticMember && VariableSpecDIE ? *VariableSpecDIE
1631 : *VariableDIE,
1632 DD->getDwarfVersion() >= 4 ? dwarf::DW_AT_linkage_name
1633 : dwarf::DW_AT_MIPS_linkage_name,
1634 GlobalValue::getRealLinkageName(LinkageName));
1635 } else if (const ConstantInt *CI =
1636 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1637 // AT_const_value was added when the static member was created. To avoid
1638 // emitting AT_const_value multiple times, we only add AT_const_value when
1639 // it is not a static member.
1640 if (!IsStaticMember)
1641 addConstantValue(*VariableDIE, CI, GTy);
1642 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1643 addToAccelTable = true;
1644 // GV is a merged global.
1645 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1646 Value *Ptr = CE->getOperand(0);
1647 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1648 DD->addArangeLabel(SymbolCU(this, Sym));
1649 addOpAddress(*Loc, Sym);
1650 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1651 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1652 addUInt(*Loc, dwarf::DW_FORM_udata,
1653 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1654 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1655 addBlock(*VariableDIE, dwarf::DW_AT_location, Loc);
1656 }
1658 if (addToAccelTable) {
1659 DIE &AddrDIE = VariableSpecDIE ? *VariableSpecDIE : *VariableDIE;
1660 DD->addAccelName(GV.getName(), AddrDIE);
1662 // If the linkage name is different than the name, go ahead and output
1663 // that as well into the name table.
1664 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1665 DD->addAccelName(GV.getLinkageName(), AddrDIE);
1666 }
1668 if (!GV.isLocalToUnit())
1669 addGlobalName(GV.getName(),
1670 VariableSpecDIE ? *VariableSpecDIE : *VariableDIE,
1671 GV.getContext());
1672 }
1674 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1675 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1676 DIE &DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1677 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, *IndexTy);
1679 // The LowerBound value defines the lower bounds which is typically zero for
1680 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1681 // Count == -1 then the array is unbounded and we do not emit
1682 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1683 // Count == 0, then the array has zero elements in which case we do not emit
1684 // an upper bound.
1685 int64_t LowerBound = SR.getLo();
1686 int64_t DefaultLowerBound = getDefaultLowerBound();
1687 int64_t Count = SR.getCount();
1689 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1690 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1692 if (Count != -1 && Count != 0)
1693 // FIXME: An unbounded array should reference the expression that defines
1694 // the array.
1695 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1696 LowerBound + Count - 1);
1697 }
1699 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1700 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1701 if (CTy.isVector())
1702 addFlag(Buffer, dwarf::DW_AT_GNU_vector);
1704 // Emit the element type.
1705 addType(Buffer, resolve(CTy.getTypeDerivedFrom()));
1707 // Get an anonymous type for index type.
1708 // FIXME: This type should be passed down from the front end
1709 // as different languages may have different sizes for indexes.
1710 DIE *IdxTy = getIndexTyDie();
1711 if (!IdxTy) {
1712 // Construct an integer type to use for indexes.
1713 IdxTy = &createAndAddDIE(dwarf::DW_TAG_base_type, UnitDie);
1714 addString(*IdxTy, dwarf::DW_AT_name, "sizetype");
1715 addUInt(*IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int64_t));
1716 addUInt(*IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1717 dwarf::DW_ATE_unsigned);
1718 setIndexTyDie(IdxTy);
1719 }
1721 // Add subranges to array type.
1722 DIArray Elements = CTy.getTypeArray();
1723 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1724 DIDescriptor Element = Elements.getElement(i);
1725 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1726 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1727 }
1728 }
1730 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1731 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1732 DIArray Elements = CTy.getTypeArray();
1734 // Add enumerators to enumeration type.
1735 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1736 DIEnumerator Enum(Elements.getElement(i));
1737 if (Enum.isEnumerator()) {
1738 DIE &Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1739 StringRef Name = Enum.getName();
1740 addString(Enumerator, dwarf::DW_AT_name, Name);
1741 int64_t Value = Enum.getEnumValue();
1742 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1743 Value);
1744 }
1745 }
1746 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1747 if (DTy) {
1748 addType(Buffer, DTy);
1749 addFlag(Buffer, dwarf::DW_AT_enum_class);
1750 }
1751 }
1753 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1754 /// vtables.
1755 void DwarfUnit::constructContainingTypeDIEs() {
1756 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1757 CE = ContainingTypeMap.end();
1758 CI != CE; ++CI) {
1759 DIE &SPDie = *CI->first;
1760 DIDescriptor D(CI->second);
1761 if (!D)
1762 continue;
1763 DIE *NDie = getDIE(D);
1764 if (!NDie)
1765 continue;
1766 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, *NDie);
1767 }
1768 }
1770 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1771 std::unique_ptr<DIE> DwarfUnit::constructVariableDIE(DbgVariable &DV,
1772 bool Abstract) {
1773 auto D = constructVariableDIEImpl(DV, Abstract);
1774 DV.setDIE(*D);
1775 return D;
1776 }
1778 std::unique_ptr<DIE> DwarfUnit::constructVariableDIEImpl(const DbgVariable &DV,
1779 bool Abstract) {
1780 StringRef Name = DV.getName();
1782 // Define variable debug information entry.
1783 auto VariableDie = make_unique<DIE>(DV.getTag());
1784 if (DbgVariable *AbsVar = DV.getAbstractVariable())
1785 addDIEEntry(*VariableDie, dwarf::DW_AT_abstract_origin, *AbsVar->getDIE());
1786 else {
1787 if (!Name.empty())
1788 addString(*VariableDie, dwarf::DW_AT_name, Name);
1789 addSourceLine(*VariableDie, DV.getVariable());
1790 addType(*VariableDie, DV.getType());
1791 if (DV.isArtificial())
1792 addFlag(*VariableDie, dwarf::DW_AT_artificial);
1793 }
1795 if (Abstract)
1796 return VariableDie;
1798 // Add variable address.
1800 unsigned Offset = DV.getDotDebugLocOffset();
1801 if (Offset != ~0U) {
1802 addLocationList(*VariableDie, dwarf::DW_AT_location, Offset);
1803 return VariableDie;
1804 }
1806 // Check if variable is described by a DBG_VALUE instruction.
1807 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1808 assert(DVInsn->getNumOperands() == 3);
1809 if (DVInsn->getOperand(0).isReg()) {
1810 const MachineOperand RegOp = DVInsn->getOperand(0);
1811 // If the second operand is an immediate, this is an indirect value.
1812 if (DVInsn->getOperand(1).isImm()) {
1813 MachineLocation Location(RegOp.getReg(),
1814 DVInsn->getOperand(1).getImm());
1815 addVariableAddress(DV, *VariableDie, Location);
1816 } else if (RegOp.getReg())
1817 addVariableAddress(DV, *VariableDie, MachineLocation(RegOp.getReg()));
1818 } else if (DVInsn->getOperand(0).isImm())
1819 addConstantValue(*VariableDie, DVInsn->getOperand(0), DV.getType());
1820 else if (DVInsn->getOperand(0).isFPImm())
1821 addConstantFPValue(*VariableDie, DVInsn->getOperand(0));
1822 else if (DVInsn->getOperand(0).isCImm())
1823 addConstantValue(*VariableDie, DVInsn->getOperand(0).getCImm(),
1824 DV.getType());
1826 return VariableDie;
1827 }
1829 // .. else use frame index.
1830 int FI = DV.getFrameIndex();
1831 if (FI != ~0) {
1832 unsigned FrameReg = 0;
1833 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1834 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1835 MachineLocation Location(FrameReg, Offset);
1836 addVariableAddress(DV, *VariableDie, Location);
1837 }
1839 return VariableDie;
1840 }
1842 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1843 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1844 DIE &MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1845 StringRef Name = DT.getName();
1846 if (!Name.empty())
1847 addString(MemberDie, dwarf::DW_AT_name, Name);
1849 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1851 addSourceLine(MemberDie, DT);
1853 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1855 // For C++, virtual base classes are not at fixed offset. Use following
1856 // expression to extract appropriate offset from vtable.
1857 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1859 DIELoc *VBaseLocationDie = new (DIEValueAllocator) DIELoc();
1860 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1861 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1862 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1863 addUInt(*VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1864 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1865 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1866 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1868 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1869 } else {
1870 uint64_t Size = DT.getSizeInBits();
1871 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1872 uint64_t OffsetInBytes;
1874 if (Size != FieldSize) {
1875 // Handle bitfield, assume bytes are 8 bits.
1876 addUInt(MemberDie, dwarf::DW_AT_byte_size, None, FieldSize/8);
1877 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, Size);
1879 uint64_t Offset = DT.getOffsetInBits();
1880 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1881 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1882 uint64_t FieldOffset = (HiMark - FieldSize);
1883 Offset -= FieldOffset;
1885 // Maybe we need to work from the other end.
1886 if (Asm->getDataLayout().isLittleEndian())
1887 Offset = FieldSize - (Offset + Size);
1888 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1890 // Here DW_AT_data_member_location points to the anonymous
1891 // field that includes this bit field.
1892 OffsetInBytes = FieldOffset >> 3;
1893 } else
1894 // This is not a bitfield.
1895 OffsetInBytes = DT.getOffsetInBits() >> 3;
1897 if (DD->getDwarfVersion() <= 2) {
1898 DIELoc *MemLocationDie = new (DIEValueAllocator) DIELoc();
1899 addUInt(*MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1900 addUInt(*MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1901 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1902 } else
1903 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1904 OffsetInBytes);
1905 }
1907 if (DT.isProtected())
1908 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1909 dwarf::DW_ACCESS_protected);
1910 else if (DT.isPrivate())
1911 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1912 dwarf::DW_ACCESS_private);
1913 // Otherwise C++ member and base classes are considered public.
1914 else
1915 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1916 dwarf::DW_ACCESS_public);
1917 if (DT.isVirtual())
1918 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1919 dwarf::DW_VIRTUALITY_virtual);
1921 // Objective-C properties.
1922 if (MDNode *PNode = DT.getObjCProperty())
1923 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1924 MemberDie.addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1925 PropertyDie);
1927 if (DT.isArtificial())
1928 addFlag(MemberDie, dwarf::DW_AT_artificial);
1929 }
1931 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1932 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1933 if (!DT.Verify())
1934 return nullptr;
1936 // Construct the context before querying for the existence of the DIE in case
1937 // such construction creates the DIE.
1938 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1939 assert(dwarf::isType(ContextDIE->getTag()) &&
1940 "Static member should belong to a type.");
1942 if (DIE *StaticMemberDIE = getDIE(DT))
1943 return StaticMemberDIE;
1945 DIE &StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1947 DIType Ty = resolve(DT.getTypeDerivedFrom());
1949 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1950 addType(StaticMemberDIE, Ty);
1951 addSourceLine(StaticMemberDIE, DT);
1952 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1953 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1955 // FIXME: We could omit private if the parent is a class_type, and
1956 // public if the parent is something else.
1957 if (DT.isProtected())
1958 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1959 dwarf::DW_ACCESS_protected);
1960 else if (DT.isPrivate())
1961 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1962 dwarf::DW_ACCESS_private);
1963 else
1964 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1965 dwarf::DW_ACCESS_public);
1967 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1968 addConstantValue(StaticMemberDIE, CI, Ty);
1969 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1970 addConstantFPValue(StaticMemberDIE, CFP);
1972 return &StaticMemberDIE;
1973 }
1975 void DwarfUnit::emitHeader(const MCSymbol *ASectionSym) const {
1976 Asm->OutStreamer.AddComment("DWARF version number");
1977 Asm->EmitInt16(DD->getDwarfVersion());
1978 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1979 // We share one abbreviations table across all units so it's always at the
1980 // start of the section. Use a relocatable offset where needed to ensure
1981 // linking doesn't invalidate that offset.
1982 if (ASectionSym)
1983 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1984 else
1985 // Use a constant value when no symbol is provided.
1986 Asm->EmitInt32(0);
1987 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1988 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1989 }
1991 void DwarfUnit::addRange(RangeSpan Range) {
1992 // Only add a range for this unit if we're emitting full debug.
1993 if (getCUNode().getEmissionKind() == DIBuilder::FullDebug) {
1994 // If we have no current ranges just add the range and return, otherwise,
1995 // check the current section and CU against the previous section and CU we
1996 // emitted into and the subprogram was contained within. If these are the
1997 // same then extend our current range, otherwise add this as a new range.
1998 if (CURanges.size() == 0 ||
1999 this != DD->getPrevCU() ||
2000 Asm->getCurrentSection() != DD->getPrevSection()) {
2001 CURanges.push_back(Range);
2002 return;
2003 }
2005 assert(&(CURanges.back().getEnd()->getSection()) ==
2006 &(Range.getEnd()->getSection()) &&
2007 "We can only append to a range in the same section!");
2008 CURanges.back().setEnd(Range.getEnd());
2009 }
2010 }
2012 void DwarfCompileUnit::initStmtList(MCSymbol *DwarfLineSectionSym) {
2013 // Define start line table label for each Compile Unit.
2014 MCSymbol *LineTableStartSym =
2015 Asm->OutStreamer.getDwarfLineTableSymbol(getUniqueID());
2017 stmtListIndex = UnitDie.getValues().size();
2019 // DW_AT_stmt_list is a offset of line number information for this
2020 // compile unit in debug_line section. For split dwarf this is
2021 // left in the skeleton CU and so not included.
2022 // The line table entries are not always emitted in assembly, so it
2023 // is not okay to use line_table_start here.
2024 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
2025 addSectionLabel(UnitDie, dwarf::DW_AT_stmt_list, LineTableStartSym);
2026 else
2027 addSectionDelta(UnitDie, dwarf::DW_AT_stmt_list, LineTableStartSym,
2028 DwarfLineSectionSym);
2029 }
2031 void DwarfCompileUnit::applyStmtList(DIE &D) {
2032 D.addValue(dwarf::DW_AT_stmt_list,
2033 UnitDie.getAbbrev().getData()[stmtListIndex].getForm(),
2034 UnitDie.getValues()[stmtListIndex]);
2035 }
2037 void DwarfTypeUnit::emitHeader(const MCSymbol *ASectionSym) const {
2038 DwarfUnit::emitHeader(ASectionSym);
2039 Asm->OutStreamer.AddComment("Type Signature");
2040 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
2041 Asm->OutStreamer.AddComment("Type DIE Offset");
2042 // In a skeleton type unit there is no type DIE so emit a zero offset.
2043 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
2044 sizeof(Ty->getOffset()));
2045 }
2047 void DwarfTypeUnit::initSection(const MCSection *Section) {
2048 assert(!this->Section);
2049 this->Section = Section;
2050 // Since each type unit is contained in its own COMDAT section, the begin
2051 // label and the section label are the same. Using the begin label emission in
2052 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2053 // the only other alternative of lazily constructing start-of-section labels
2054 // and storing a mapping in DwarfDebug (or AsmPrinter).
2055 this->SectionSym = this->LabelBegin =
2056 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2057 this->LabelEnd =
2058 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2059 }