1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #define DEBUG_TYPE "dwarfdebug"
16 #include "DwarfUnit.h"
17 #include "DwarfAccelTable.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/DIBuilder.h"
21 #include "llvm/IR/Constants.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCContext.h"
28 #include "llvm/MC/MCSection.h"
29 #include "llvm/MC/MCStreamer.h"
30 #include "llvm/Support/CommandLine.h"
31 #include "llvm/Target/TargetFrameLowering.h"
32 #include "llvm/Target/TargetLoweringObjectFile.h"
33 #include "llvm/Target/TargetMachine.h"
34 #include "llvm/Target/TargetRegisterInfo.h"
36 using namespace llvm;
38 static cl::opt<bool>
39 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
40 cl::desc("Generate DWARF4 type units."),
41 cl::init(false));
43 /// Unit - Unit constructor.
44 DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
45 DwarfDebug *DW, DwarfFile *DWU)
46 : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
47 DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
48 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
49 }
51 DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
52 AsmPrinter *A, DwarfDebug *DW,
53 DwarfFile *DWU)
54 : DwarfUnit(UID, D, Node, A, DW, DWU) {
55 insertDIE(Node, D);
56 }
58 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DwarfCompileUnit &CU,
59 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
60 : DwarfUnit(UID, D, CU.getCUNode(), A, DW, DWU), CU(CU) {
61 }
63 /// ~Unit - Destructor for compile unit.
64 DwarfUnit::~DwarfUnit() {
65 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
66 DIEBlocks[j]->~DIEBlock();
67 }
69 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
70 /// information entry.
71 DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
72 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
73 return Value;
74 }
76 /// getDefaultLowerBound - Return the default lower bound for an array. If the
77 /// DWARF version doesn't handle the language, return -1.
78 int64_t DwarfUnit::getDefaultLowerBound() const {
79 switch (getLanguage()) {
80 default:
81 break;
83 case dwarf::DW_LANG_C89:
84 case dwarf::DW_LANG_C99:
85 case dwarf::DW_LANG_C:
86 case dwarf::DW_LANG_C_plus_plus:
87 case dwarf::DW_LANG_ObjC:
88 case dwarf::DW_LANG_ObjC_plus_plus:
89 return 0;
91 case dwarf::DW_LANG_Fortran77:
92 case dwarf::DW_LANG_Fortran90:
93 case dwarf::DW_LANG_Fortran95:
94 return 1;
96 // The languages below have valid values only if the DWARF version >= 4.
97 case dwarf::DW_LANG_Java:
98 case dwarf::DW_LANG_Python:
99 case dwarf::DW_LANG_UPC:
100 case dwarf::DW_LANG_D:
101 if (dwarf::DWARF_VERSION >= 4)
102 return 0;
103 break;
105 case dwarf::DW_LANG_Ada83:
106 case dwarf::DW_LANG_Ada95:
107 case dwarf::DW_LANG_Cobol74:
108 case dwarf::DW_LANG_Cobol85:
109 case dwarf::DW_LANG_Modula2:
110 case dwarf::DW_LANG_Pascal83:
111 case dwarf::DW_LANG_PLI:
112 if (dwarf::DWARF_VERSION >= 4)
113 return 1;
114 break;
115 }
117 return -1;
118 }
120 /// Check whether the DIE for this MDNode can be shared across CUs.
121 static bool isShareableAcrossCUs(DIDescriptor D) {
122 // When the MDNode can be part of the type system, the DIE can be shared
123 // across CUs.
124 // Combining type units and cross-CU DIE sharing is lower value (since
125 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
126 // level already) but may be implementable for some value in projects
127 // building multiple independent libraries with LTO and then linking those
128 // together.
129 return (D.isType() ||
130 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
131 !GenerateDwarfTypeUnits;
132 }
134 /// getDIE - Returns the debug information entry map slot for the
135 /// specified debug variable. We delegate the request to DwarfDebug
136 /// when the DIE for this MDNode can be shared across CUs. The mappings
137 /// will be kept in DwarfDebug for shareable DIEs.
138 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
139 if (isShareableAcrossCUs(D))
140 return DD->getDIE(D);
141 return MDNodeToDieMap.lookup(D);
142 }
144 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
145 /// when the DIE for this MDNode can be shared across CUs. The mappings
146 /// will be kept in DwarfDebug for shareable DIEs.
147 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
148 if (isShareableAcrossCUs(Desc)) {
149 DD->insertDIE(Desc, D);
150 return;
151 }
152 MDNodeToDieMap.insert(std::make_pair(Desc, D));
153 }
155 /// addFlag - Add a flag that is true.
156 void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
157 if (DD->getDwarfVersion() >= 4)
158 Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
159 else
160 Die->addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
161 }
163 /// addUInt - Add an unsigned integer attribute data and value.
164 ///
165 void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
166 Optional<dwarf::Form> Form, uint64_t Integer) {
167 if (!Form)
168 Form = DIEInteger::BestForm(false, Integer);
169 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
170 DIEInteger(Integer);
171 Die->addValue(Attribute, *Form, Value);
172 }
174 void DwarfUnit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
175 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
176 }
178 /// addSInt - Add an signed integer attribute data and value.
179 ///
180 void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
181 Optional<dwarf::Form> Form, int64_t Integer) {
182 if (!Form)
183 Form = DIEInteger::BestForm(true, Integer);
184 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
185 Die->addValue(Attribute, *Form, Value);
186 }
188 void DwarfUnit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form,
189 int64_t Integer) {
190 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
191 }
193 /// addString - Add a string attribute data and value. We always emit a
194 /// reference to the string pool instead of immediate strings so that DIEs have
195 /// more predictable sizes. In the case of split dwarf we emit an index
196 /// into another table which gets us the static offset into the string
197 /// table.
198 void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
199 StringRef String) {
201 if (!DD->useSplitDwarf())
202 return addLocalString(Die, Attribute, String);
204 unsigned idx = DU->getStringPoolIndex(String);
205 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
206 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
207 Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
208 }
210 /// addLocalString - Add a string attribute data and value. This is guaranteed
211 /// to be in the local string pool instead of indirected.
212 void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
213 StringRef String) {
214 MCSymbol *Symb = DU->getStringPoolEntry(String);
215 DIEValue *Value;
216 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
217 Value = new (DIEValueAllocator) DIELabel(Symb);
218 else {
219 MCSymbol *StringPool = DU->getStringPoolSym();
220 Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
221 }
222 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
223 Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
224 }
226 /// addExpr - Add a Dwarf expression attribute data and value.
227 ///
228 void DwarfUnit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
229 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
230 Die->addValue((dwarf::Attribute)0, Form, Value);
231 }
233 /// addLabel - Add a Dwarf label attribute data and value.
234 ///
235 void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
236 const MCSymbol *Label) {
237 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
238 Die->addValue(Attribute, Form, Value);
239 }
241 void DwarfUnit::addLabel(DIEBlock *Die, dwarf::Form Form,
242 const MCSymbol *Label) {
243 addLabel(Die, (dwarf::Attribute)0, Form, Label);
244 }
246 /// addSectionLabel - Add a Dwarf section label attribute data and value.
247 ///
248 void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
249 const MCSymbol *Label) {
250 if (DD->getDwarfVersion() >= 4)
251 addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
252 else
253 addLabel(Die, Attribute, dwarf::DW_FORM_data4, Label);
254 }
256 /// addSectionOffset - Add an offset into a section attribute data and value.
257 ///
258 void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
259 uint64_t Integer) {
260 if (DD->getDwarfVersion() >= 4)
261 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
262 else
263 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
264 }
266 /// addLabelAddress - Add a dwarf label attribute data and value using
267 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
268 ///
269 void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
270 MCSymbol *Label) {
271 if (Label)
272 DD->addArangeLabel(SymbolCU(this, Label));
274 if (!DD->useSplitDwarf()) {
275 if (Label) {
276 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
277 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
278 } else {
279 DIEValue *Value = new (DIEValueAllocator) DIEInteger(0);
280 Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
281 }
282 } else {
283 unsigned idx = DU->getAddrPoolIndex(Label);
284 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
285 Die->addValue(Attribute, dwarf::DW_FORM_GNU_addr_index, Value);
286 }
287 }
289 /// addOpAddress - Add a dwarf op address data and value using the
290 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
291 ///
292 void DwarfUnit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
293 if (!DD->useSplitDwarf()) {
294 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
295 addLabel(Die, dwarf::DW_FORM_udata, Sym);
296 } else {
297 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
298 addUInt(Die, dwarf::DW_FORM_GNU_addr_index, DU->getAddrPoolIndex(Sym));
299 }
300 }
302 /// addSectionDelta - Add a section label delta attribute data and value.
303 ///
304 void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
305 const MCSymbol *Hi, const MCSymbol *Lo) {
306 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
307 if (DD->getDwarfVersion() >= 4)
308 Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
309 else
310 Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
311 }
313 /// addDIEEntry - Add a DIE attribute data and value.
314 ///
315 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
316 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
317 }
319 void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
320 Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
321 new (DIEValueAllocator) DIETypeSignature(Type));
322 }
324 void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
325 DIEEntry *Entry) {
326 const DIE *DieCU = Die->getUnitOrNull();
327 const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
328 if (!DieCU)
329 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
330 DieCU = getUnitDie();
331 if (!EntryCU)
332 EntryCU = getUnitDie();
333 Die->addValue(Attribute, EntryCU == DieCU ? dwarf::DW_FORM_ref4
334 : dwarf::DW_FORM_ref_addr,
335 Entry);
336 }
338 /// Create a DIE with the given Tag, add the DIE to its parent, and
339 /// call insertDIE if MD is not null.
340 DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
341 DIE *Die = new DIE(Tag);
342 Parent.addChild(Die);
343 if (N)
344 insertDIE(N, Die);
345 return Die;
346 }
348 /// addBlock - Add block data.
349 ///
350 void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
351 DIEBlock *Block) {
352 Block->ComputeSize(Asm);
353 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
354 Die->addValue(Attribute, Block->BestForm(), Block);
355 }
357 /// addSourceLine - Add location information to specified debug information
358 /// entry.
359 void DwarfUnit::addSourceLine(DIE *Die, unsigned Line, StringRef File,
360 StringRef Directory) {
361 if (Line == 0)
362 return;
364 unsigned FileID =
365 DD->getOrCreateSourceID(File, Directory, getCU().getUniqueID());
366 assert(FileID && "Invalid file id");
367 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
368 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
369 }
371 /// addSourceLine - Add location information to specified debug information
372 /// entry.
373 void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
374 assert(V.isVariable());
376 addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
377 V.getContext().getDirectory());
378 }
380 /// addSourceLine - Add location information to specified debug information
381 /// entry.
382 void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
383 assert(G.isGlobalVariable());
385 addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
386 }
388 /// addSourceLine - Add location information to specified debug information
389 /// entry.
390 void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
391 assert(SP.isSubprogram());
393 addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
394 }
396 /// addSourceLine - Add location information to specified debug information
397 /// entry.
398 void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
399 assert(Ty.isType());
401 addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
402 }
404 /// addSourceLine - Add location information to specified debug information
405 /// entry.
406 void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
407 assert(Ty.isObjCProperty());
409 DIFile File = Ty.getFile();
410 addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
411 File.getDirectory());
412 }
414 /// addSourceLine - Add location information to specified debug information
415 /// entry.
416 void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
417 assert(NS.Verify());
419 addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
420 }
422 /// addVariableAddress - Add DW_AT_location attribute for a
423 /// DbgVariable based on provided MachineLocation.
424 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
425 MachineLocation Location) {
426 if (DV.variableHasComplexAddress())
427 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
428 else if (DV.isBlockByrefVariable())
429 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
430 else
431 addAddress(Die, dwarf::DW_AT_location, Location,
432 DV.getVariable().isIndirect());
433 }
435 /// addRegisterOp - Add register operand.
436 void DwarfUnit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
437 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
438 int DWReg = RI->getDwarfRegNum(Reg, false);
439 bool isSubRegister = DWReg < 0;
441 unsigned Idx = 0;
443 // Go up the super-register chain until we hit a valid dwarf register number.
444 for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
445 DWReg = RI->getDwarfRegNum(*SR, false);
446 if (DWReg >= 0)
447 Idx = RI->getSubRegIndex(*SR, Reg);
448 }
450 if (DWReg < 0) {
451 DEBUG(llvm::dbgs() << "Invalid Dwarf register number.\n");
452 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
453 return;
454 }
456 // Emit register
457 if (DWReg < 32)
458 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
459 else {
460 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
461 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
462 }
464 // Emit Mask
465 if (isSubRegister) {
466 unsigned Size = RI->getSubRegIdxSize(Idx);
467 unsigned Offset = RI->getSubRegIdxOffset(Idx);
468 if (Offset > 0) {
469 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
470 addUInt(TheDie, dwarf::DW_FORM_data1, Size);
471 addUInt(TheDie, dwarf::DW_FORM_data1, Offset);
472 } else {
473 unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
474 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
475 addUInt(TheDie, dwarf::DW_FORM_data1, ByteSize);
476 }
477 }
478 }
480 /// addRegisterOffset - Add register offset.
481 void DwarfUnit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg,
482 int64_t Offset) {
483 const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
484 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
485 const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
486 if (Reg == TRI->getFrameRegister(*Asm->MF))
487 // If variable offset is based in frame register then use fbreg.
488 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
489 else if (DWReg < 32)
490 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
491 else {
492 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
493 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
494 }
495 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
496 }
498 /// addAddress - Add an address attribute to a die based on the location
499 /// provided.
500 void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
501 const MachineLocation &Location, bool Indirect) {
502 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
504 if (Location.isReg() && !Indirect)
505 addRegisterOp(Block, Location.getReg());
506 else {
507 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
508 if (Indirect && !Location.isReg()) {
509 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
510 }
511 }
513 // Now attach the location information to the DIE.
514 addBlock(Die, Attribute, Block);
515 }
517 /// addComplexAddress - Start with the address based on the location provided,
518 /// and generate the DWARF information necessary to find the actual variable
519 /// given the extra address information encoded in the DbgVariable, starting
520 /// from the starting location. Add the DWARF information to the die.
521 ///
522 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
523 dwarf::Attribute Attribute,
524 const MachineLocation &Location) {
525 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
526 unsigned N = DV.getNumAddrElements();
527 unsigned i = 0;
528 if (Location.isReg()) {
529 if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
530 // If first address element is OpPlus then emit
531 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
532 addRegisterOffset(Block, Location.getReg(), DV.getAddrElement(1));
533 i = 2;
534 } else
535 addRegisterOp(Block, Location.getReg());
536 } else
537 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
539 for (; i < N; ++i) {
540 uint64_t Element = DV.getAddrElement(i);
541 if (Element == DIBuilder::OpPlus) {
542 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
543 addUInt(Block, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
544 } else if (Element == DIBuilder::OpDeref) {
545 if (!Location.isReg())
546 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
547 } else
548 llvm_unreachable("unknown DIBuilder Opcode");
549 }
551 // Now attach the location information to the DIE.
552 addBlock(Die, Attribute, Block);
553 }
555 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
556 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
557 gives the variable VarName either the struct, or a pointer to the struct, as
558 its type. This is necessary for various behind-the-scenes things the
559 compiler needs to do with by-reference variables in Blocks.
561 However, as far as the original *programmer* is concerned, the variable
562 should still have type 'SomeType', as originally declared.
564 The function getBlockByrefType dives into the __Block_byref_x_VarName
565 struct to find the original type of the variable, which is then assigned to
566 the variable's Debug Information Entry as its real type. So far, so good.
567 However now the debugger will expect the variable VarName to have the type
568 SomeType. So we need the location attribute for the variable to be an
569 expression that explains to the debugger how to navigate through the
570 pointers and struct to find the actual variable of type SomeType.
572 The following function does just that. We start by getting
573 the "normal" location for the variable. This will be the location
574 of either the struct __Block_byref_x_VarName or the pointer to the
575 struct __Block_byref_x_VarName.
577 The struct will look something like:
579 struct __Block_byref_x_VarName {
580 ... <various fields>
581 struct __Block_byref_x_VarName *forwarding;
582 ... <various other fields>
583 SomeType VarName;
584 ... <maybe more fields>
585 };
587 If we are given the struct directly (as our starting point) we
588 need to tell the debugger to:
590 1). Add the offset of the forwarding field.
592 2). Follow that pointer to get the real __Block_byref_x_VarName
593 struct to use (the real one may have been copied onto the heap).
595 3). Add the offset for the field VarName, to find the actual variable.
597 If we started with a pointer to the struct, then we need to
598 dereference that pointer first, before the other steps.
599 Translating this into DWARF ops, we will need to append the following
600 to the current location description for the variable:
602 DW_OP_deref -- optional, if we start with a pointer
603 DW_OP_plus_uconst <forward_fld_offset>
604 DW_OP_deref
605 DW_OP_plus_uconst <varName_fld_offset>
607 That is what this function does. */
609 /// addBlockByrefAddress - Start with the address based on the location
610 /// provided, and generate the DWARF information necessary to find the
611 /// actual Block variable (navigating the Block struct) based on the
612 /// starting location. Add the DWARF information to the die. For
613 /// more information, read large comment just above here.
614 ///
615 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
616 dwarf::Attribute Attribute,
617 const MachineLocation &Location) {
618 DIType Ty = DV.getType();
619 DIType TmpTy = Ty;
620 uint16_t Tag = Ty.getTag();
621 bool isPointer = false;
623 StringRef varName = DV.getName();
625 if (Tag == dwarf::DW_TAG_pointer_type) {
626 DIDerivedType DTy(Ty);
627 TmpTy = resolve(DTy.getTypeDerivedFrom());
628 isPointer = true;
629 }
631 DICompositeType blockStruct(TmpTy);
633 // Find the __forwarding field and the variable field in the __Block_byref
634 // struct.
635 DIArray Fields = blockStruct.getTypeArray();
636 DIDerivedType varField;
637 DIDerivedType forwardingField;
639 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
640 DIDerivedType DT(Fields.getElement(i));
641 StringRef fieldName = DT.getName();
642 if (fieldName == "__forwarding")
643 forwardingField = DT;
644 else if (fieldName == varName)
645 varField = DT;
646 }
648 // Get the offsets for the forwarding field and the variable field.
649 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
650 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
652 // Decode the original location, and use that as the start of the byref
653 // variable's location.
654 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
656 if (Location.isReg())
657 addRegisterOp(Block, Location.getReg());
658 else
659 addRegisterOffset(Block, Location.getReg(), Location.getOffset());
661 // If we started with a pointer to the __Block_byref... struct, then
662 // the first thing we need to do is dereference the pointer (DW_OP_deref).
663 if (isPointer)
664 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
666 // Next add the offset for the '__forwarding' field:
667 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
668 // adding the offset if it's 0.
669 if (forwardingFieldOffset > 0) {
670 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
671 addUInt(Block, dwarf::DW_FORM_udata, forwardingFieldOffset);
672 }
674 // Now dereference the __forwarding field to get to the real __Block_byref
675 // struct: DW_OP_deref.
676 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
678 // Now that we've got the real __Block_byref... struct, add the offset
679 // for the variable's field to get to the location of the actual variable:
680 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
681 if (varFieldOffset > 0) {
682 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
683 addUInt(Block, dwarf::DW_FORM_udata, varFieldOffset);
684 }
686 // Now attach the location information to the DIE.
687 addBlock(Die, Attribute, Block);
688 }
690 /// isTypeSigned - Return true if the type is signed.
691 static bool isTypeSigned(DwarfDebug *DD, DIType Ty, int *SizeInBits) {
692 if (Ty.isDerivedType())
693 return isTypeSigned(DD, DD->resolve(DIDerivedType(Ty).getTypeDerivedFrom()),
694 SizeInBits);
695 if (Ty.isBasicType())
696 if (DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed ||
697 DIBasicType(Ty).getEncoding() == dwarf::DW_ATE_signed_char) {
698 *SizeInBits = Ty.getSizeInBits();
699 return true;
700 }
701 return false;
702 }
704 /// Return true if type encoding is unsigned.
705 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
706 DIDerivedType DTy(Ty);
707 if (DTy.isDerivedType())
708 return isUnsignedDIType(DD, DD->resolve(DTy.getTypeDerivedFrom()));
710 DIBasicType BTy(Ty);
711 if (BTy.isBasicType()) {
712 unsigned Encoding = BTy.getEncoding();
713 if (Encoding == dwarf::DW_ATE_unsigned ||
714 Encoding == dwarf::DW_ATE_unsigned_char ||
715 Encoding == dwarf::DW_ATE_boolean)
716 return true;
717 }
718 return false;
719 }
721 /// If this type is derived from a base type then return base type size.
722 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
723 unsigned Tag = Ty.getTag();
725 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
726 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
727 Tag != dwarf::DW_TAG_restrict_type)
728 return Ty.getSizeInBits();
730 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
732 // If this type is not derived from any type then take conservative approach.
733 if (!BaseType.isValid())
734 return Ty.getSizeInBits();
736 // If this is a derived type, go ahead and get the base type, unless it's a
737 // reference then it's just the size of the field. Pointer types have no need
738 // of this since they're a different type of qualification on the type.
739 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
740 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
741 return Ty.getSizeInBits();
743 if (BaseType.isDerivedType())
744 return getBaseTypeSize(DD, DIDerivedType(BaseType));
746 return BaseType.getSizeInBits();
747 }
749 /// addConstantValue - Add constant value entry in variable DIE.
750 void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
751 DIType Ty) {
752 // FIXME: This is a bit conservative/simple - it emits negative values at
753 // their maximum bit width which is a bit unfortunate (& doesn't prefer
754 // udata/sdata over dataN as suggested by the DWARF spec)
755 assert(MO.isImm() && "Invalid machine operand!");
756 int SizeInBits = -1;
757 bool SignedConstant = isTypeSigned(DD, Ty, &SizeInBits);
758 dwarf::Form Form;
760 // If we're a signed constant definitely use sdata.
761 if (SignedConstant) {
762 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata, MO.getImm());
763 return;
764 }
766 // Else use data for now unless it's larger than we can deal with.
767 switch (SizeInBits) {
768 case 8:
769 Form = dwarf::DW_FORM_data1;
770 break;
771 case 16:
772 Form = dwarf::DW_FORM_data2;
773 break;
774 case 32:
775 Form = dwarf::DW_FORM_data4;
776 break;
777 case 64:
778 Form = dwarf::DW_FORM_data8;
779 break;
780 default:
781 Form = dwarf::DW_FORM_udata;
782 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
783 return;
784 }
785 addUInt(Die, dwarf::DW_AT_const_value, Form, MO.getImm());
786 }
788 /// addConstantFPValue - Add constant value entry in variable DIE.
789 void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
790 assert(MO.isFPImm() && "Invalid machine operand!");
791 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
792 APFloat FPImm = MO.getFPImm()->getValueAPF();
794 // Get the raw data form of the floating point.
795 const APInt FltVal = FPImm.bitcastToAPInt();
796 const char *FltPtr = (const char *)FltVal.getRawData();
798 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
799 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
800 int Incr = (LittleEndian ? 1 : -1);
801 int Start = (LittleEndian ? 0 : NumBytes - 1);
802 int Stop = (LittleEndian ? NumBytes : -1);
804 // Output the constant to DWARF one byte at a time.
805 for (; Start != Stop; Start += Incr)
806 addUInt(Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
808 addBlock(Die, dwarf::DW_AT_const_value, Block);
809 }
811 /// addConstantFPValue - Add constant value entry in variable DIE.
812 void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
813 // Pass this down to addConstantValue as an unsigned bag of bits.
814 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
815 }
817 /// addConstantValue - Add constant value entry in variable DIE.
818 void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
819 bool Unsigned) {
820 addConstantValue(Die, CI->getValue(), Unsigned);
821 }
823 // addConstantValue - Add constant value entry in variable DIE.
824 void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
825 unsigned CIBitWidth = Val.getBitWidth();
826 if (CIBitWidth <= 64) {
827 // If we're a signed constant definitely use sdata.
828 if (!Unsigned) {
829 addSInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
830 Val.getSExtValue());
831 return;
832 }
834 // Else use data for now unless it's larger than we can deal with.
835 dwarf::Form Form;
836 switch (CIBitWidth) {
837 case 8:
838 Form = dwarf::DW_FORM_data1;
839 break;
840 case 16:
841 Form = dwarf::DW_FORM_data2;
842 break;
843 case 32:
844 Form = dwarf::DW_FORM_data4;
845 break;
846 case 64:
847 Form = dwarf::DW_FORM_data8;
848 break;
849 default:
850 addUInt(Die, dwarf::DW_AT_const_value, dwarf::DW_FORM_udata,
851 Val.getZExtValue());
852 return;
853 }
854 addUInt(Die, dwarf::DW_AT_const_value, Form, Val.getZExtValue());
855 return;
856 }
858 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
860 // Get the raw data form of the large APInt.
861 const uint64_t *Ptr64 = Val.getRawData();
863 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
864 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
866 // Output the constant to DWARF one byte at a time.
867 for (int i = 0; i < NumBytes; i++) {
868 uint8_t c;
869 if (LittleEndian)
870 c = Ptr64[i / 8] >> (8 * (i & 7));
871 else
872 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
873 addUInt(Block, dwarf::DW_FORM_data1, c);
874 }
876 addBlock(Die, dwarf::DW_AT_const_value, Block);
877 }
879 /// addTemplateParams - Add template parameters into buffer.
880 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
881 // Add template parameters.
882 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
883 DIDescriptor Element = TParams.getElement(i);
884 if (Element.isTemplateTypeParameter())
885 constructTemplateTypeParameterDIE(Buffer,
886 DITemplateTypeParameter(Element));
887 else if (Element.isTemplateValueParameter())
888 constructTemplateValueParameterDIE(Buffer,
889 DITemplateValueParameter(Element));
890 }
891 }
893 /// getOrCreateContextDIE - Get context owner's DIE.
894 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
895 if (!Context || Context.isFile())
896 return getUnitDie();
897 if (Context.isType())
898 return getOrCreateTypeDIE(DIType(Context));
899 if (Context.isNameSpace())
900 return getOrCreateNameSpace(DINameSpace(Context));
901 if (Context.isSubprogram())
902 return getOrCreateSubprogramDIE(DISubprogram(Context));
903 return getDIE(Context);
904 }
906 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
907 DIScope Context = resolve(Ty.getContext());
908 DIE *ContextDIE = getOrCreateContextDIE(Context);
910 DIE *TyDIE = getDIE(Ty);
911 if (TyDIE)
912 return TyDIE;
914 // Create new type.
915 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
917 constructTypeDIE(*TyDIE, Ty);
919 updateAcceleratorTables(Context, Ty, TyDIE);
920 return TyDIE;
921 }
923 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
924 /// given DIType.
925 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
926 if (!TyNode)
927 return NULL;
929 DIType Ty(TyNode);
930 assert(Ty.isType());
932 // Construct the context before querying for the existence of the DIE in case
933 // such construction creates the DIE.
934 DIScope Context = resolve(Ty.getContext());
935 DIE *ContextDIE = getOrCreateContextDIE(Context);
936 assert(ContextDIE);
938 DIE *TyDIE = getDIE(Ty);
939 if (TyDIE)
940 return TyDIE;
942 // Create new type.
943 TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
945 if (Ty.isBasicType())
946 constructTypeDIE(*TyDIE, DIBasicType(Ty));
947 else if (Ty.isCompositeType()) {
948 DICompositeType CTy(Ty);
949 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
950 if (MDString *TypeId = CTy.getIdentifier()) {
951 DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
952 // Skip updating the accellerator tables since this is not the full type
953 return TyDIE;
954 }
955 constructTypeDIE(*TyDIE, CTy);
956 } else {
957 assert(Ty.isDerivedType() && "Unknown kind of DIType");
958 constructTypeDIE(*TyDIE, DIDerivedType(Ty));
959 }
961 updateAcceleratorTables(Context, Ty, TyDIE);
963 return TyDIE;
964 }
966 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
967 const DIE *TyDIE) {
968 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
969 bool IsImplementation = 0;
970 if (Ty.isCompositeType()) {
971 DICompositeType CT(Ty);
972 // A runtime language of 0 actually means C/C++ and that any
973 // non-negative value is some version of Objective-C/C++.
974 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
975 }
976 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
977 addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
979 if (!Context || Context.isCompileUnit() || Context.isFile() ||
980 Context.isNameSpace())
981 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
982 }
983 }
985 /// addType - Add a new type attribute to the specified entity.
986 void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
987 assert(Ty && "Trying to add a type that doesn't exist?");
989 // Check for pre-existence.
990 DIEEntry *Entry = getDIEEntry(Ty);
991 // If it exists then use the existing value.
992 if (Entry) {
993 addDIEEntry(Entity, Attribute, Entry);
994 return;
995 }
997 // Construct type.
998 DIE *Buffer = getOrCreateTypeDIE(Ty);
1000 // Set up proxy.
1001 Entry = createDIEEntry(Buffer);
1002 insertDIEEntry(Ty, Entry);
1003 addDIEEntry(Entity, Attribute, Entry);
1004 }
1006 // Accelerator table mutators - add each name along with its companion
1007 // DIE to the proper table while ensuring that the name that we're going
1008 // to reference is in the string table. We do this since the names we
1009 // add may not only be identical to the names in the DIE.
1010 void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
1011 if (!DD->useDwarfAccelTables())
1012 return;
1013 DU->getStringPoolEntry(Name);
1014 std::vector<const DIE *> &DIEs = AccelNames[Name];
1015 DIEs.push_back(Die);
1016 }
1018 void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
1019 if (!DD->useDwarfAccelTables())
1020 return;
1021 DU->getStringPoolEntry(Name);
1022 std::vector<const DIE *> &DIEs = AccelObjC[Name];
1023 DIEs.push_back(Die);
1024 }
1026 void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
1027 if (!DD->useDwarfAccelTables())
1028 return;
1029 DU->getStringPoolEntry(Name);
1030 std::vector<const DIE *> &DIEs = AccelNamespace[Name];
1031 DIEs.push_back(Die);
1032 }
1034 void DwarfUnit::addAccelType(StringRef Name,
1035 std::pair<const DIE *, unsigned> Die) {
1036 if (!DD->useDwarfAccelTables())
1037 return;
1038 DU->getStringPoolEntry(Name);
1039 std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
1040 DIEs.push_back(Die);
1041 }
1043 /// addGlobalName - Add a new global name to the compile unit.
1044 void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
1045 std::string FullName = getParentContextString(Context) + Name.str();
1046 GlobalNames[FullName] = Die;
1047 }
1049 /// getParentContextString - Walks the metadata parent chain in a language
1050 /// specific manner (using the compile unit language) and returns
1051 /// it as a string. This is done at the metadata level because DIEs may
1052 /// not currently have been added to the parent context and walking the
1053 /// DIEs looking for names is more expensive than walking the metadata.
1054 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1055 if (!Context)
1056 return "";
1058 // FIXME: Decide whether to implement this for non-C++ languages.
1059 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1060 return "";
1062 std::string CS;
1063 SmallVector<DIScope, 1> Parents;
1064 while (!Context.isCompileUnit()) {
1065 Parents.push_back(Context);
1066 if (Context.getContext())
1067 Context = resolve(Context.getContext());
1068 else
1069 // Structure, etc types will have a NULL context if they're at the top
1070 // level.
1071 break;
1072 }
1074 // Reverse iterate over our list to go from the outermost construct to the
1075 // innermost.
1076 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1077 E = Parents.rend();
1078 I != E; ++I) {
1079 DIScope Ctx = *I;
1080 StringRef Name = Ctx.getName();
1081 if (!Name.empty()) {
1082 CS += Name;
1083 CS += "::";
1084 }
1085 }
1086 return CS;
1087 }
1089 /// constructTypeDIE - Construct basic type die from DIBasicType.
1090 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1091 // Get core information.
1092 StringRef Name = BTy.getName();
1093 // Add name if not anonymous or intermediate type.
1094 if (!Name.empty())
1095 addString(&Buffer, dwarf::DW_AT_name, Name);
1097 // An unspecified type only has a name attribute.
1098 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1099 return;
1101 addUInt(&Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1102 BTy.getEncoding());
1104 uint64_t Size = BTy.getSizeInBits() >> 3;
1105 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1106 }
1108 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1109 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1110 // Get core information.
1111 StringRef Name = DTy.getName();
1112 uint64_t Size = DTy.getSizeInBits() >> 3;
1113 uint16_t Tag = Buffer.getTag();
1115 // Map to main type, void will not have a type.
1116 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1117 if (FromTy)
1118 addType(&Buffer, FromTy);
1120 // Add name if not anonymous or intermediate type.
1121 if (!Name.empty())
1122 addString(&Buffer, dwarf::DW_AT_name, Name);
1124 // Add size if non-zero (derived types might be zero-sized.)
1125 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1126 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1128 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1129 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1130 getOrCreateTypeDIE(resolve(DTy.getClassType())));
1131 // Add source line info if available and TyDesc is not a forward declaration.
1132 if (!DTy.isForwardDecl())
1133 addSourceLine(&Buffer, DTy);
1134 }
1136 /// constructTypeDIE - Construct type DIE from DICompositeType.
1137 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1138 // Add name if not anonymous or intermediate type.
1139 StringRef Name = CTy.getName();
1141 uint64_t Size = CTy.getSizeInBits() >> 3;
1142 uint16_t Tag = Buffer.getTag();
1144 switch (Tag) {
1145 case dwarf::DW_TAG_array_type:
1146 constructArrayTypeDIE(Buffer, CTy);
1147 break;
1148 case dwarf::DW_TAG_enumeration_type:
1149 constructEnumTypeDIE(Buffer, CTy);
1150 break;
1151 case dwarf::DW_TAG_subroutine_type: {
1152 // Add return type. A void return won't have a type.
1153 DIArray Elements = CTy.getTypeArray();
1154 DIType RTy(Elements.getElement(0));
1155 if (RTy)
1156 addType(&Buffer, RTy);
1158 bool isPrototyped = true;
1159 // Add arguments.
1160 for (unsigned i = 1, N = Elements.getNumElements(); i < N; ++i) {
1161 DIDescriptor Ty = Elements.getElement(i);
1162 if (Ty.isUnspecifiedParameter()) {
1163 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1164 isPrototyped = false;
1165 } else {
1166 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1167 addType(Arg, DIType(Ty));
1168 if (DIType(Ty).isArtificial())
1169 addFlag(Arg, dwarf::DW_AT_artificial);
1170 }
1171 }
1172 // Add prototype flag if we're dealing with a C language and the
1173 // function has been prototyped.
1174 uint16_t Language = getLanguage();
1175 if (isPrototyped &&
1176 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1177 Language == dwarf::DW_LANG_ObjC))
1178 addFlag(&Buffer, dwarf::DW_AT_prototyped);
1180 if (CTy.isLValueReference())
1181 addFlag(&Buffer, dwarf::DW_AT_reference);
1183 if (CTy.isRValueReference())
1184 addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
1185 } break;
1186 case dwarf::DW_TAG_structure_type:
1187 case dwarf::DW_TAG_union_type:
1188 case dwarf::DW_TAG_class_type: {
1189 // Add elements to structure type.
1190 DIArray Elements = CTy.getTypeArray();
1191 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1192 DIDescriptor Element = Elements.getElement(i);
1193 DIE *ElemDie = NULL;
1194 if (Element.isSubprogram())
1195 ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
1196 else if (Element.isDerivedType()) {
1197 DIDerivedType DDTy(Element);
1198 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1199 ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1200 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1201 dwarf::DW_AT_friend);
1202 } else if (DDTy.isStaticMember()) {
1203 getOrCreateStaticMemberDIE(DDTy);
1204 } else {
1205 constructMemberDIE(Buffer, DDTy);
1206 }
1207 } else if (Element.isObjCProperty()) {
1208 DIObjCProperty Property(Element);
1209 ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1210 StringRef PropertyName = Property.getObjCPropertyName();
1211 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1212 if (Property.getType())
1213 addType(ElemDie, Property.getType());
1214 addSourceLine(ElemDie, Property);
1215 StringRef GetterName = Property.getObjCPropertyGetterName();
1216 if (!GetterName.empty())
1217 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1218 StringRef SetterName = Property.getObjCPropertySetterName();
1219 if (!SetterName.empty())
1220 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1221 unsigned PropertyAttributes = 0;
1222 if (Property.isReadOnlyObjCProperty())
1223 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1224 if (Property.isReadWriteObjCProperty())
1225 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1226 if (Property.isAssignObjCProperty())
1227 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1228 if (Property.isRetainObjCProperty())
1229 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1230 if (Property.isCopyObjCProperty())
1231 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1232 if (Property.isNonAtomicObjCProperty())
1233 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1234 if (PropertyAttributes)
1235 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1236 PropertyAttributes);
1238 DIEEntry *Entry = getDIEEntry(Element);
1239 if (!Entry) {
1240 Entry = createDIEEntry(ElemDie);
1241 insertDIEEntry(Element, Entry);
1242 }
1243 } else
1244 continue;
1245 }
1247 if (CTy.isAppleBlockExtension())
1248 addFlag(&Buffer, dwarf::DW_AT_APPLE_block);
1250 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1251 if (ContainingType)
1252 addDIEEntry(&Buffer, dwarf::DW_AT_containing_type,
1253 getOrCreateTypeDIE(ContainingType));
1255 if (CTy.isObjcClassComplete())
1256 addFlag(&Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1258 // Add template parameters to a class, structure or union types.
1259 // FIXME: The support isn't in the metadata for this yet.
1260 if (Tag == dwarf::DW_TAG_class_type ||
1261 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1262 addTemplateParams(Buffer, CTy.getTemplateParams());
1264 break;
1265 }
1266 default:
1267 break;
1268 }
1270 // Add name if not anonymous or intermediate type.
1271 if (!Name.empty())
1272 addString(&Buffer, dwarf::DW_AT_name, Name);
1274 if (Tag == dwarf::DW_TAG_enumeration_type ||
1275 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1276 Tag == dwarf::DW_TAG_union_type) {
1277 // Add size if non-zero (derived types might be zero-sized.)
1278 // TODO: Do we care about size for enum forward declarations?
1279 if (Size)
1280 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, Size);
1281 else if (!CTy.isForwardDecl())
1282 // Add zero size if it is not a forward declaration.
1283 addUInt(&Buffer, dwarf::DW_AT_byte_size, None, 0);
1285 // If we're a forward decl, say so.
1286 if (CTy.isForwardDecl())
1287 addFlag(&Buffer, dwarf::DW_AT_declaration);
1289 // Add source line info if available.
1290 if (!CTy.isForwardDecl())
1291 addSourceLine(&Buffer, CTy);
1293 // No harm in adding the runtime language to the declaration.
1294 unsigned RLang = CTy.getRunTimeLang();
1295 if (RLang)
1296 addUInt(&Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1297 RLang);
1298 }
1299 }
1301 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1302 /// DITemplateTypeParameter.
1303 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1304 DITemplateTypeParameter TP) {
1305 DIE *ParamDIE =
1306 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1307 // Add the type if it exists, it could be void and therefore no type.
1308 if (TP.getType())
1309 addType(ParamDIE, resolve(TP.getType()));
1310 if (!TP.getName().empty())
1311 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1312 }
1314 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1315 /// DITemplateValueParameter.
1316 void
1317 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1318 DITemplateValueParameter VP) {
1319 DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1321 // Add the type if there is one, template template and template parameter
1322 // packs will not have a type.
1323 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1324 addType(ParamDIE, resolve(VP.getType()));
1325 if (!VP.getName().empty())
1326 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1327 if (Value *Val = VP.getValue()) {
1328 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1329 addConstantValue(ParamDIE, CI,
1330 isUnsignedDIType(DD, resolve(VP.getType())));
1331 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1332 // For declaration non-type template parameters (such as global values and
1333 // functions)
1334 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1335 addOpAddress(Block, Asm->getSymbol(GV));
1336 // Emit DW_OP_stack_value to use the address as the immediate value of the
1337 // parameter, rather than a pointer to it.
1338 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1339 addBlock(ParamDIE, dwarf::DW_AT_location, Block);
1340 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1341 assert(isa<MDString>(Val));
1342 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1343 cast<MDString>(Val)->getString());
1344 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1345 assert(isa<MDNode>(Val));
1346 DIArray A(cast<MDNode>(Val));
1347 addTemplateParams(*ParamDIE, A);
1348 }
1349 }
1350 }
1352 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1353 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1354 // Construct the context before querying for the existence of the DIE in case
1355 // such construction creates the DIE.
1356 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1358 DIE *NDie = getDIE(NS);
1359 if (NDie)
1360 return NDie;
1361 NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1363 if (!NS.getName().empty()) {
1364 addString(NDie, dwarf::DW_AT_name, NS.getName());
1365 addAccelNamespace(NS.getName(), NDie);
1366 addGlobalName(NS.getName(), NDie, NS.getContext());
1367 } else
1368 addAccelNamespace("(anonymous namespace)", NDie);
1369 addSourceLine(NDie, NS);
1370 return NDie;
1371 }
1373 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1374 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1375 // Construct the context before querying for the existence of the DIE in case
1376 // such construction creates the DIE (as is the case for member function
1377 // declarations).
1378 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1380 DIE *SPDie = getDIE(SP);
1381 if (SPDie)
1382 return SPDie;
1384 DISubprogram SPDecl = SP.getFunctionDeclaration();
1385 if (SPDecl.isSubprogram())
1386 // Add subprogram definitions to the CU die directly.
1387 ContextDIE = UnitDie.get();
1389 // DW_TAG_inlined_subroutine may refer to this DIE.
1390 SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1392 DIE *DeclDie = NULL;
1393 if (SPDecl.isSubprogram())
1394 DeclDie = getOrCreateSubprogramDIE(SPDecl);
1396 // Add function template parameters.
1397 addTemplateParams(*SPDie, SP.getTemplateParams());
1399 // If this DIE is going to refer declaration info using AT_specification
1400 // then there is no need to add other attributes.
1401 if (DeclDie) {
1402 // Refer function declaration directly.
1403 addDIEEntry(SPDie, dwarf::DW_AT_specification, DeclDie);
1405 return SPDie;
1406 }
1408 // Add the linkage name if we have one.
1409 StringRef LinkageName = SP.getLinkageName();
1410 if (!LinkageName.empty())
1411 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1412 GlobalValue::getRealLinkageName(LinkageName));
1414 // Constructors and operators for anonymous aggregates do not have names.
1415 if (!SP.getName().empty())
1416 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1418 addSourceLine(SPDie, SP);
1420 // Add the prototype if we have a prototype and we have a C like
1421 // language.
1422 uint16_t Language = getLanguage();
1423 if (SP.isPrototyped() &&
1424 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1425 Language == dwarf::DW_LANG_ObjC))
1426 addFlag(SPDie, dwarf::DW_AT_prototyped);
1428 DICompositeType SPTy = SP.getType();
1429 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1430 "the type of a subprogram should be a subroutine");
1432 DIArray Args = SPTy.getTypeArray();
1433 // Add a return type. If this is a type like a C/C++ void type we don't add a
1434 // return type.
1435 if (Args.getElement(0))
1436 addType(SPDie, DIType(Args.getElement(0)));
1438 unsigned VK = SP.getVirtuality();
1439 if (VK) {
1440 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1441 DIEBlock *Block = getDIEBlock();
1442 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1443 addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1444 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1445 ContainingTypeMap.insert(
1446 std::make_pair(SPDie, resolve(SP.getContainingType())));
1447 }
1449 if (!SP.isDefinition()) {
1450 addFlag(SPDie, dwarf::DW_AT_declaration);
1452 // Add arguments. Do not add arguments for subprogram definition. They will
1453 // be handled while processing variables.
1454 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1455 DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, *SPDie);
1456 DIType ATy(Args.getElement(i));
1457 addType(Arg, ATy);
1458 if (ATy.isArtificial())
1459 addFlag(Arg, dwarf::DW_AT_artificial);
1460 }
1461 }
1463 if (SP.isArtificial())
1464 addFlag(SPDie, dwarf::DW_AT_artificial);
1466 if (!SP.isLocalToUnit())
1467 addFlag(SPDie, dwarf::DW_AT_external);
1469 if (SP.isOptimized())
1470 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1472 if (unsigned isa = Asm->getISAEncoding()) {
1473 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1474 }
1476 if (SP.isLValueReference())
1477 addFlag(SPDie, dwarf::DW_AT_reference);
1479 if (SP.isRValueReference())
1480 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1482 if (SP.isProtected())
1483 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1484 dwarf::DW_ACCESS_protected);
1485 else if (SP.isPrivate())
1486 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1487 dwarf::DW_ACCESS_private);
1488 else
1489 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1490 dwarf::DW_ACCESS_public);
1492 if (SP.isExplicit())
1493 addFlag(SPDie, dwarf::DW_AT_explicit);
1495 return SPDie;
1496 }
1498 // Return const expression if value is a GEP to access merged global
1499 // constant. e.g.
1500 // i8* getelementptr ({ i8, i8, i8, i8 }* @_MergedGlobals, i32 0, i32 0)
1501 static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
1502 const ConstantExpr *CE = dyn_cast_or_null<ConstantExpr>(V);
1503 if (!CE || CE->getNumOperands() != 3 ||
1504 CE->getOpcode() != Instruction::GetElementPtr)
1505 return NULL;
1507 // First operand points to a global struct.
1508 Value *Ptr = CE->getOperand(0);
1509 if (!isa<GlobalValue>(Ptr) ||
1510 !isa<StructType>(cast<PointerType>(Ptr->getType())->getElementType()))
1511 return NULL;
1513 // Second operand is zero.
1514 const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(CE->getOperand(1));
1515 if (!CI || !CI->isZero())
1516 return NULL;
1518 // Third operand is offset.
1519 if (!isa<ConstantInt>(CE->getOperand(2)))
1520 return NULL;
1522 return CE;
1523 }
1525 /// createGlobalVariableDIE - create global variable DIE.
1526 void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
1527 // Check for pre-existence.
1528 if (getDIE(GV))
1529 return;
1531 assert(GV.isGlobalVariable());
1533 DIScope GVContext = GV.getContext();
1534 DIType GTy = GV.getType();
1536 // If this is a static data member definition, some attributes belong
1537 // to the declaration DIE.
1538 DIE *VariableDIE = NULL;
1539 bool IsStaticMember = false;
1540 DIDerivedType SDMDecl = GV.getStaticDataMemberDeclaration();
1541 if (SDMDecl.Verify()) {
1542 assert(SDMDecl.isStaticMember() && "Expected static member decl");
1543 // We need the declaration DIE that is in the static member's class.
1544 VariableDIE = getOrCreateStaticMemberDIE(SDMDecl);
1545 IsStaticMember = true;
1546 }
1548 // If this is not a static data member definition, create the variable
1549 // DIE and add the initial set of attributes to it.
1550 if (!VariableDIE) {
1551 // Construct the context before querying for the existence of the DIE in
1552 // case such construction creates the DIE.
1553 DIE *ContextDIE = getOrCreateContextDIE(GVContext);
1555 // Add to map.
1556 VariableDIE = createAndAddDIE(GV.getTag(), *ContextDIE, GV);
1558 // Add name and type.
1559 addString(VariableDIE, dwarf::DW_AT_name, GV.getDisplayName());
1560 addType(VariableDIE, GTy);
1562 // Add scoping info.
1563 if (!GV.isLocalToUnit())
1564 addFlag(VariableDIE, dwarf::DW_AT_external);
1566 // Add line number info.
1567 addSourceLine(VariableDIE, GV);
1568 }
1570 // Add location.
1571 bool addToAccelTable = false;
1572 DIE *VariableSpecDIE = NULL;
1573 bool isGlobalVariable = GV.getGlobal() != NULL;
1574 if (isGlobalVariable) {
1575 addToAccelTable = true;
1576 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1577 const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
1578 if (GV.getGlobal()->isThreadLocal()) {
1579 // FIXME: Make this work with -gsplit-dwarf.
1580 unsigned PointerSize = Asm->getDataLayout().getPointerSize();
1581 assert((PointerSize == 4 || PointerSize == 8) &&
1582 "Add support for other sizes if necessary");
1583 // Based on GCC's support for TLS:
1584 if (!DD->useSplitDwarf()) {
1585 // 1) Start with a constNu of the appropriate pointer size
1586 addUInt(Block, dwarf::DW_FORM_data1,
1587 PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
1588 // 2) containing the (relocated) offset of the TLS variable
1589 // within the module's TLS block.
1590 addExpr(Block, dwarf::DW_FORM_udata,
1591 Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym));
1592 } else {
1593 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
1594 addUInt(Block, dwarf::DW_FORM_udata,
1595 DU->getAddrPoolIndex(Sym, /* TLS */ true));
1596 }
1597 // 3) followed by a custom OP to make the debugger do a TLS lookup.
1598 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
1599 } else {
1600 DD->addArangeLabel(SymbolCU(this, Sym));
1601 addOpAddress(Block, Sym);
1602 }
1603 // Do not create specification DIE if context is either compile unit
1604 // or a subprogram.
1605 if (GVContext && GV.isDefinition() && !GVContext.isCompileUnit() &&
1606 !GVContext.isFile() && !DD->isSubprogramContext(GVContext)) {
1607 // Create specification DIE.
1608 VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
1609 addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
1610 addBlock(VariableSpecDIE, dwarf::DW_AT_location, Block);
1611 // A static member's declaration is already flagged as such.
1612 if (!SDMDecl.Verify())
1613 addFlag(VariableDIE, dwarf::DW_AT_declaration);
1614 } else {
1615 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1616 }
1617 // Add the linkage name.
1618 StringRef LinkageName = GV.getLinkageName();
1619 if (!LinkageName.empty())
1620 // From DWARF4: DIEs to which DW_AT_linkage_name may apply include:
1621 // TAG_common_block, TAG_constant, TAG_entry_point, TAG_subprogram and
1622 // TAG_variable.
1623 addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
1624 : VariableDIE,
1625 dwarf::DW_AT_MIPS_linkage_name,
1626 GlobalValue::getRealLinkageName(LinkageName));
1627 } else if (const ConstantInt *CI =
1628 dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
1629 // AT_const_value was added when the static member was created. To avoid
1630 // emitting AT_const_value multiple times, we only add AT_const_value when
1631 // it is not a static member.
1632 if (!IsStaticMember)
1633 addConstantValue(VariableDIE, CI, isUnsignedDIType(DD, GTy));
1634 } else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
1635 addToAccelTable = true;
1636 // GV is a merged global.
1637 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
1638 Value *Ptr = CE->getOperand(0);
1639 MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
1640 DD->addArangeLabel(SymbolCU(this, Sym));
1641 addOpAddress(Block, Sym);
1642 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1643 SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
1644 addUInt(Block, dwarf::DW_FORM_udata,
1645 Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
1646 addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1647 addBlock(VariableDIE, dwarf::DW_AT_location, Block);
1648 }
1650 if (addToAccelTable) {
1651 DIE *AddrDIE = VariableSpecDIE ? VariableSpecDIE : VariableDIE;
1652 addAccelName(GV.getName(), AddrDIE);
1654 // If the linkage name is different than the name, go ahead and output
1655 // that as well into the name table.
1656 if (GV.getLinkageName() != "" && GV.getName() != GV.getLinkageName())
1657 addAccelName(GV.getLinkageName(), AddrDIE);
1658 }
1660 if (!GV.isLocalToUnit())
1661 addGlobalName(GV.getName(), VariableSpecDIE ? VariableSpecDIE : VariableDIE,
1662 GV.getContext());
1663 }
1665 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1666 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1667 DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1668 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
1670 // The LowerBound value defines the lower bounds which is typically zero for
1671 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1672 // Count == -1 then the array is unbounded and we do not emit
1673 // DW_AT_lower_bound and DW_AT_upper_bound attributes. If LowerBound == 0 and
1674 // Count == 0, then the array has zero elements in which case we do not emit
1675 // an upper bound.
1676 int64_t LowerBound = SR.getLo();
1677 int64_t DefaultLowerBound = getDefaultLowerBound();
1678 int64_t Count = SR.getCount();
1680 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1681 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1683 if (Count != -1 && Count != 0)
1684 // FIXME: An unbounded array should reference the expression that defines
1685 // the array.
1686 addUInt(DW_Subrange, dwarf::DW_AT_upper_bound, None,
1687 LowerBound + Count - 1);
1688 }
1690 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1691 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1692 if (CTy.isVector())
1693 addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
1695 // Emit the element type.
1696 addType(&Buffer, resolve(CTy.getTypeDerivedFrom()));
1698 // Get an anonymous type for index type.
1699 // FIXME: This type should be passed down from the front end
1700 // as different languages may have different sizes for indexes.
1701 DIE *IdxTy = getIndexTyDie();
1702 if (!IdxTy) {
1703 // Construct an anonymous type for index type.
1704 IdxTy = createAndAddDIE(dwarf::DW_TAG_base_type, *UnitDie);
1705 addString(IdxTy, dwarf::DW_AT_name, "int");
1706 addUInt(IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int32_t));
1707 addUInt(IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1708 dwarf::DW_ATE_signed);
1709 setIndexTyDie(IdxTy);
1710 }
1712 // Add subranges to array type.
1713 DIArray Elements = CTy.getTypeArray();
1714 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1715 DIDescriptor Element = Elements.getElement(i);
1716 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1717 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1718 }
1719 }
1721 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1722 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1723 DIArray Elements = CTy.getTypeArray();
1725 // Add enumerators to enumeration type.
1726 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1727 DIEnumerator Enum(Elements.getElement(i));
1728 if (Enum.isEnumerator()) {
1729 DIE *Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1730 StringRef Name = Enum.getName();
1731 addString(Enumerator, dwarf::DW_AT_name, Name);
1732 int64_t Value = Enum.getEnumValue();
1733 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1734 Value);
1735 }
1736 }
1737 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1738 if (DTy) {
1739 addType(&Buffer, DTy);
1740 addFlag(&Buffer, dwarf::DW_AT_enum_class);
1741 }
1742 }
1744 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1745 /// vtables.
1746 void DwarfUnit::constructContainingTypeDIEs() {
1747 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1748 CE = ContainingTypeMap.end();
1749 CI != CE; ++CI) {
1750 DIE *SPDie = CI->first;
1751 DIDescriptor D(CI->second);
1752 if (!D)
1753 continue;
1754 DIE *NDie = getDIE(D);
1755 if (!NDie)
1756 continue;
1757 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, NDie);
1758 }
1759 }
1761 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
1762 DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
1763 StringRef Name = DV.getName();
1765 // Define variable debug information entry.
1766 DIE *VariableDie = new DIE(DV.getTag());
1767 DbgVariable *AbsVar = DV.getAbstractVariable();
1768 DIE *AbsDIE = AbsVar ? AbsVar->getDIE() : NULL;
1769 if (AbsDIE)
1770 addDIEEntry(VariableDie, dwarf::DW_AT_abstract_origin, AbsDIE);
1771 else {
1772 if (!Name.empty())
1773 addString(VariableDie, dwarf::DW_AT_name, Name);
1774 addSourceLine(VariableDie, DV.getVariable());
1775 addType(VariableDie, DV.getType());
1776 }
1778 if (DV.isArtificial())
1779 addFlag(VariableDie, dwarf::DW_AT_artificial);
1781 if (isScopeAbstract) {
1782 DV.setDIE(VariableDie);
1783 return VariableDie;
1784 }
1786 // Add variable address.
1788 unsigned Offset = DV.getDotDebugLocOffset();
1789 if (Offset != ~0U) {
1790 addSectionLabel(VariableDie, dwarf::DW_AT_location,
1791 Asm->GetTempSymbol("debug_loc", Offset));
1792 DV.setDIE(VariableDie);
1793 return VariableDie;
1794 }
1796 // Check if variable is described by a DBG_VALUE instruction.
1797 if (const MachineInstr *DVInsn = DV.getMInsn()) {
1798 assert(DVInsn->getNumOperands() == 3);
1799 if (DVInsn->getOperand(0).isReg()) {
1800 const MachineOperand RegOp = DVInsn->getOperand(0);
1801 // If the second operand is an immediate, this is an indirect value.
1802 if (DVInsn->getOperand(1).isImm()) {
1803 MachineLocation Location(RegOp.getReg(),
1804 DVInsn->getOperand(1).getImm());
1805 addVariableAddress(DV, VariableDie, Location);
1806 } else if (RegOp.getReg())
1807 addVariableAddress(DV, VariableDie, MachineLocation(RegOp.getReg()));
1808 } else if (DVInsn->getOperand(0).isImm())
1809 addConstantValue(VariableDie, DVInsn->getOperand(0), DV.getType());
1810 else if (DVInsn->getOperand(0).isFPImm())
1811 addConstantFPValue(VariableDie, DVInsn->getOperand(0));
1812 else if (DVInsn->getOperand(0).isCImm())
1813 addConstantValue(VariableDie, DVInsn->getOperand(0).getCImm(),
1814 isUnsignedDIType(DD, DV.getType()));
1816 DV.setDIE(VariableDie);
1817 return VariableDie;
1818 } else {
1819 // .. else use frame index.
1820 int FI = DV.getFrameIndex();
1821 if (FI != ~0) {
1822 unsigned FrameReg = 0;
1823 const TargetFrameLowering *TFI = Asm->TM.getFrameLowering();
1824 int Offset = TFI->getFrameIndexReference(*Asm->MF, FI, FrameReg);
1825 MachineLocation Location(FrameReg, Offset);
1826 addVariableAddress(DV, VariableDie, Location);
1827 }
1828 }
1830 DV.setDIE(VariableDie);
1831 return VariableDie;
1832 }
1834 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1835 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1836 DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1837 StringRef Name = DT.getName();
1838 if (!Name.empty())
1839 addString(MemberDie, dwarf::DW_AT_name, Name);
1841 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1843 addSourceLine(MemberDie, DT);
1845 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1847 // For C++, virtual base classes are not at fixed offset. Use following
1848 // expression to extract appropriate offset from vtable.
1849 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1851 DIEBlock *VBaseLocationDie = new (DIEValueAllocator) DIEBlock();
1852 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1853 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1854 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1855 addUInt(VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1856 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1857 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1858 addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1860 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1861 } else {
1862 uint64_t Size = DT.getSizeInBits();
1863 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1864 uint64_t OffsetInBytes;
1866 if (Size != FieldSize) {
1867 // Handle bitfield.
1868 addUInt(MemberDie, dwarf::DW_AT_byte_size, None,
1869 getBaseTypeSize(DD, DT) >> 3);
1870 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, DT.getSizeInBits());
1872 uint64_t Offset = DT.getOffsetInBits();
1873 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1874 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1875 uint64_t FieldOffset = (HiMark - FieldSize);
1876 Offset -= FieldOffset;
1878 // Maybe we need to work from the other end.
1879 if (Asm->getDataLayout().isLittleEndian())
1880 Offset = FieldSize - (Offset + Size);
1881 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1883 // Here DW_AT_data_member_location points to the anonymous
1884 // field that includes this bit field.
1885 OffsetInBytes = FieldOffset >> 3;
1886 } else
1887 // This is not a bitfield.
1888 OffsetInBytes = DT.getOffsetInBits() >> 3;
1890 if (DD->getDwarfVersion() <= 2) {
1891 DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
1892 addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1893 addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1894 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1895 } else
1896 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1897 OffsetInBytes);
1898 }
1900 if (DT.isProtected())
1901 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1902 dwarf::DW_ACCESS_protected);
1903 else if (DT.isPrivate())
1904 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1905 dwarf::DW_ACCESS_private);
1906 // Otherwise C++ member and base classes are considered public.
1907 else
1908 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1909 dwarf::DW_ACCESS_public);
1910 if (DT.isVirtual())
1911 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1912 dwarf::DW_VIRTUALITY_virtual);
1914 // Objective-C properties.
1915 if (MDNode *PNode = DT.getObjCProperty())
1916 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1917 MemberDie->addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1918 PropertyDie);
1920 if (DT.isArtificial())
1921 addFlag(MemberDie, dwarf::DW_AT_artificial);
1922 }
1924 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1925 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1926 if (!DT.Verify())
1927 return NULL;
1929 // Construct the context before querying for the existence of the DIE in case
1930 // such construction creates the DIE.
1931 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1932 assert(dwarf::isType(ContextDIE->getTag()) &&
1933 "Static member should belong to a type.");
1935 DIE *StaticMemberDIE = getDIE(DT);
1936 if (StaticMemberDIE)
1937 return StaticMemberDIE;
1939 StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1941 DIType Ty = resolve(DT.getTypeDerivedFrom());
1943 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1944 addType(StaticMemberDIE, Ty);
1945 addSourceLine(StaticMemberDIE, DT);
1946 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1947 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1949 // FIXME: We could omit private if the parent is a class_type, and
1950 // public if the parent is something else.
1951 if (DT.isProtected())
1952 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1953 dwarf::DW_ACCESS_protected);
1954 else if (DT.isPrivate())
1955 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1956 dwarf::DW_ACCESS_private);
1957 else
1958 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1959 dwarf::DW_ACCESS_public);
1961 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1962 addConstantValue(StaticMemberDIE, CI, isUnsignedDIType(DD, Ty));
1963 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1964 addConstantFPValue(StaticMemberDIE, CFP);
1966 return StaticMemberDIE;
1967 }
1969 void DwarfUnit::emitHeader(const MCSection *ASection,
1970 const MCSymbol *ASectionSym) const {
1971 Asm->OutStreamer.AddComment("DWARF version number");
1972 Asm->EmitInt16(DD->getDwarfVersion());
1973 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1974 // We share one abbreviations table across all units so it's always at the
1975 // start of the section. Use a relocatable offset where needed to ensure
1976 // linking doesn't invalidate that offset.
1977 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1978 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1979 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1980 }
1982 void DwarfCompileUnit::initStmtList(MCSymbol *DwarfLineSectionSym) {
1983 // Define start line table label for each Compile Unit.
1984 MCSymbol *LineTableStartSym =
1985 Asm->GetTempSymbol("line_table_start", getUniqueID());
1986 Asm->OutStreamer.getContext().setMCLineTableSymbol(LineTableStartSym,
1987 getUniqueID());
1989 // Use a single line table if we are generating assembly.
1990 bool UseTheFirstCU =
1991 Asm->OutStreamer.hasRawTextSupport() || (getUniqueID() == 0);
1993 stmtListIndex = UnitDie->getValues().size();
1995 // DW_AT_stmt_list is a offset of line number information for this
1996 // compile unit in debug_line section. For split dwarf this is
1997 // left in the skeleton CU and so not included.
1998 // The line table entries are not always emitted in assembly, so it
1999 // is not okay to use line_table_start here.
2000 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
2001 addSectionLabel(UnitDie.get(), dwarf::DW_AT_stmt_list,
2002 UseTheFirstCU ? DwarfLineSectionSym : LineTableStartSym);
2003 else if (UseTheFirstCU)
2004 addSectionOffset(UnitDie.get(), dwarf::DW_AT_stmt_list, 0);
2005 else
2006 addSectionDelta(UnitDie.get(), dwarf::DW_AT_stmt_list, LineTableStartSym,
2007 DwarfLineSectionSym);
2008 }
2010 void DwarfCompileUnit::applyStmtList(DIE &D) {
2011 D.addValue(dwarf::DW_AT_stmt_list,
2012 UnitDie->getAbbrev().getData()[stmtListIndex].getForm(),
2013 UnitDie->getValues()[stmtListIndex]);
2014 }
2016 void DwarfTypeUnit::emitHeader(const MCSection *ASection,
2017 const MCSymbol *ASectionSym) const {
2018 DwarfUnit::emitHeader(ASection, ASectionSym);
2019 Asm->OutStreamer.AddComment("Type Signature");
2020 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
2021 Asm->OutStreamer.AddComment("Type DIE Offset");
2022 // In a skeleton type unit there is no type DIE so emit a zero offset.
2023 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
2024 sizeof(Ty->getOffset()));
2025 }
2027 void DwarfTypeUnit::initSection(const MCSection *Section) {
2028 assert(!this->Section);
2029 this->Section = Section;
2030 // Since each type unit is contained in its own COMDAT section, the begin
2031 // label and the section label are the same. Using the begin label emission in
2032 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
2033 // the only other alternative of lazily constructing start-of-section labels
2034 // and storing a mapping in DwarfDebug (or AsmPrinter).
2035 this->SectionSym = this->LabelBegin =
2036 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
2037 this->LabelEnd =
2038 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
2039 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
2040 }