1 //===-- llvm/CodeGen/DwarfUnit.cpp - Dwarf Type and Compile Units ---------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for constructing a dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "DwarfUnit.h"
16 #include "DwarfAccelTable.h"
17 #include "DwarfCompileUnit.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/APFloat.h"
20 #include "llvm/IR/Constants.h"
21 #include "llvm/IR/DIBuilder.h"
22 #include "llvm/IR/DataLayout.h"
23 #include "llvm/IR/GlobalVariable.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/Mangler.h"
26 #include "llvm/MC/MCAsmInfo.h"
27 #include "llvm/MC/MCContext.h"
28 #include "llvm/MC/MCSection.h"
29 #include "llvm/MC/MCStreamer.h"
30 #include "llvm/Support/CommandLine.h"
31 #include "llvm/Target/TargetFrameLowering.h"
32 #include "llvm/Target/TargetLoweringObjectFile.h"
33 #include "llvm/Target/TargetMachine.h"
34 #include "llvm/Target/TargetRegisterInfo.h"
35 #include "llvm/Target/TargetSubtargetInfo.h"
37 using namespace llvm;
39 #define DEBUG_TYPE "dwarfdebug"
41 static cl::opt<bool>
42 GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
43 cl::desc("Generate DWARF4 type units."),
44 cl::init(false));
46 /// Unit - Unit constructor.
47 DwarfUnit::DwarfUnit(unsigned UID, dwarf::Tag UnitTag, DICompileUnit Node,
48 AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
49 : UniqueID(UID), CUNode(Node), UnitDie(UnitTag), DebugInfoOffset(0), Asm(A),
50 DD(DW), DU(DWU), IndexTyDie(nullptr), Section(nullptr) {
51 assert(UnitTag == dwarf::DW_TAG_compile_unit ||
52 UnitTag == dwarf::DW_TAG_type_unit);
53 DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
54 }
56 DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A,
57 DwarfDebug *DW, DwarfFile *DWU,
58 MCDwarfDwoLineTable *SplitLineTable)
59 : DwarfUnit(UID, dwarf::DW_TAG_type_unit, CU.getCUNode(), A, DW, DWU),
60 CU(CU), SplitLineTable(SplitLineTable) {
61 if (SplitLineTable)
62 addSectionOffset(UnitDie, dwarf::DW_AT_stmt_list, 0);
63 }
65 /// ~Unit - Destructor for compile unit.
66 DwarfUnit::~DwarfUnit() {
67 for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
68 DIEBlocks[j]->~DIEBlock();
69 for (unsigned j = 0, M = DIELocs.size(); j < M; ++j)
70 DIELocs[j]->~DIELoc();
71 }
73 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
74 /// information entry.
75 DIEEntry *DwarfUnit::createDIEEntry(DIE &Entry) {
76 DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
77 return Value;
78 }
80 /// getDefaultLowerBound - Return the default lower bound for an array. If the
81 /// DWARF version doesn't handle the language, return -1.
82 int64_t DwarfUnit::getDefaultLowerBound() const {
83 switch (getLanguage()) {
84 default:
85 break;
87 case dwarf::DW_LANG_C89:
88 case dwarf::DW_LANG_C99:
89 case dwarf::DW_LANG_C:
90 case dwarf::DW_LANG_C_plus_plus:
91 case dwarf::DW_LANG_ObjC:
92 case dwarf::DW_LANG_ObjC_plus_plus:
93 return 0;
95 case dwarf::DW_LANG_Fortran77:
96 case dwarf::DW_LANG_Fortran90:
97 case dwarf::DW_LANG_Fortran95:
98 return 1;
100 // The languages below have valid values only if the DWARF version >= 4.
101 case dwarf::DW_LANG_Java:
102 case dwarf::DW_LANG_Python:
103 case dwarf::DW_LANG_UPC:
104 case dwarf::DW_LANG_D:
105 if (dwarf::DWARF_VERSION >= 4)
106 return 0;
107 break;
109 case dwarf::DW_LANG_Ada83:
110 case dwarf::DW_LANG_Ada95:
111 case dwarf::DW_LANG_Cobol74:
112 case dwarf::DW_LANG_Cobol85:
113 case dwarf::DW_LANG_Modula2:
114 case dwarf::DW_LANG_Pascal83:
115 case dwarf::DW_LANG_PLI:
116 if (dwarf::DWARF_VERSION >= 4)
117 return 1;
118 break;
119 }
121 return -1;
122 }
124 /// Check whether the DIE for this MDNode can be shared across CUs.
125 static bool isShareableAcrossCUs(DIDescriptor D) {
126 // When the MDNode can be part of the type system, the DIE can be shared
127 // across CUs.
128 // Combining type units and cross-CU DIE sharing is lower value (since
129 // cross-CU DIE sharing is used in LTO and removes type redundancy at that
130 // level already) but may be implementable for some value in projects
131 // building multiple independent libraries with LTO and then linking those
132 // together.
133 return (D.isType() ||
134 (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
135 !GenerateDwarfTypeUnits;
136 }
138 /// getDIE - Returns the debug information entry map slot for the
139 /// specified debug variable. We delegate the request to DwarfDebug
140 /// when the DIE for this MDNode can be shared across CUs. The mappings
141 /// will be kept in DwarfDebug for shareable DIEs.
142 DIE *DwarfUnit::getDIE(DIDescriptor D) const {
143 if (isShareableAcrossCUs(D))
144 return DD->getDIE(D);
145 return MDNodeToDieMap.lookup(D);
146 }
148 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
149 /// when the DIE for this MDNode can be shared across CUs. The mappings
150 /// will be kept in DwarfDebug for shareable DIEs.
151 void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
152 if (isShareableAcrossCUs(Desc)) {
153 DD->insertDIE(Desc, D);
154 return;
155 }
156 MDNodeToDieMap.insert(std::make_pair(Desc, D));
157 }
159 /// addFlag - Add a flag that is true.
160 void DwarfUnit::addFlag(DIE &Die, dwarf::Attribute Attribute) {
161 if (DD->getDwarfVersion() >= 4)
162 Die.addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
163 else
164 Die.addValue(Attribute, dwarf::DW_FORM_flag, DIEIntegerOne);
165 }
167 /// addUInt - Add an unsigned integer attribute data and value.
168 ///
169 void DwarfUnit::addUInt(DIE &Die, dwarf::Attribute Attribute,
170 Optional<dwarf::Form> Form, uint64_t Integer) {
171 if (!Form)
172 Form = DIEInteger::BestForm(false, Integer);
173 DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
174 DIEInteger(Integer);
175 Die.addValue(Attribute, *Form, Value);
176 }
178 void DwarfUnit::addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer) {
179 addUInt(Block, (dwarf::Attribute)0, Form, Integer);
180 }
182 /// addSInt - Add an signed integer attribute data and value.
183 ///
184 void DwarfUnit::addSInt(DIE &Die, dwarf::Attribute Attribute,
185 Optional<dwarf::Form> Form, int64_t Integer) {
186 if (!Form)
187 Form = DIEInteger::BestForm(true, Integer);
188 DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
189 Die.addValue(Attribute, *Form, Value);
190 }
192 void DwarfUnit::addSInt(DIELoc &Die, Optional<dwarf::Form> Form,
193 int64_t Integer) {
194 addSInt(Die, (dwarf::Attribute)0, Form, Integer);
195 }
197 /// addString - Add a string attribute data and value. We always emit a
198 /// reference to the string pool instead of immediate strings so that DIEs have
199 /// more predictable sizes. In the case of split dwarf we emit an index
200 /// into another table which gets us the static offset into the string
201 /// table.
202 void DwarfUnit::addString(DIE &Die, dwarf::Attribute Attribute,
203 StringRef String) {
205 if (!DD->useSplitDwarf())
206 return addLocalString(Die, Attribute, String);
208 unsigned idx = DU->getStringPool().getIndex(*Asm, String);
209 DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
210 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
211 Die.addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
212 }
214 /// addLocalString - Add a string attribute data and value. This is guaranteed
215 /// to be in the local string pool instead of indirected.
216 void DwarfUnit::addLocalString(DIE &Die, dwarf::Attribute Attribute,
217 StringRef String) {
218 MCSymbol *Symb = DU->getStringPool().getSymbol(*Asm, String);
219 DIEValue *Value;
220 if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
221 Value = new (DIEValueAllocator) DIELabel(Symb);
222 else
223 Value = new (DIEValueAllocator) DIEDelta(Symb, DD->getDebugStrSym());
224 DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
225 Die.addValue(Attribute, dwarf::DW_FORM_strp, Str);
226 }
228 /// addExpr - Add a Dwarf expression attribute data and value.
229 ///
230 void DwarfUnit::addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr) {
231 DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
232 Die.addValue((dwarf::Attribute)0, Form, Value);
233 }
235 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
236 ///
237 void DwarfUnit::addLocationList(DIE &Die, dwarf::Attribute Attribute,
238 unsigned Index) {
239 DIEValue *Value = new (DIEValueAllocator) DIELocList(Index);
240 dwarf::Form Form = DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
241 : dwarf::DW_FORM_data4;
242 Die.addValue(Attribute, Form, Value);
243 }
245 /// addLabel - Add a Dwarf label attribute data and value.
246 ///
247 void DwarfUnit::addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form,
248 const MCSymbol *Label) {
249 DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
250 Die.addValue(Attribute, Form, Value);
251 }
253 void DwarfUnit::addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label) {
254 addLabel(Die, (dwarf::Attribute)0, Form, Label);
255 }
257 /// addSectionOffset - Add an offset into a section attribute data and value.
258 ///
259 void DwarfUnit::addSectionOffset(DIE &Die, dwarf::Attribute Attribute,
260 uint64_t Integer) {
261 if (DD->getDwarfVersion() >= 4)
262 addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
263 else
264 addUInt(Die, Attribute, dwarf::DW_FORM_data4, Integer);
265 }
267 unsigned DwarfTypeUnit::getOrCreateSourceID(StringRef FileName, StringRef DirName) {
268 return SplitLineTable ? SplitLineTable->getFile(DirName, FileName)
269 : getCU().getOrCreateSourceID(FileName, DirName);
270 }
272 /// addOpAddress - Add a dwarf op address data and value using the
273 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
274 ///
275 void DwarfUnit::addOpAddress(DIELoc &Die, const MCSymbol *Sym) {
276 if (!DD->useSplitDwarf()) {
277 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
278 addLabel(Die, dwarf::DW_FORM_udata, Sym);
279 } else {
280 addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_addr_index);
281 addUInt(Die, dwarf::DW_FORM_GNU_addr_index,
282 DD->getAddressPool().getIndex(Sym));
283 }
284 }
286 void DwarfUnit::addLabelDelta(DIE &Die, dwarf::Attribute Attribute,
287 const MCSymbol *Hi, const MCSymbol *Lo) {
288 DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
289 Die.addValue(Attribute, dwarf::DW_FORM_data4, Value);
290 }
292 /// addDIEEntry - Add a DIE attribute data and value.
293 ///
294 void DwarfUnit::addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry) {
295 addDIEEntry(Die, Attribute, createDIEEntry(Entry));
296 }
298 void DwarfUnit::addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type) {
299 // Flag the type unit reference as a declaration so that if it contains
300 // members (implicit special members, static data member definitions, member
301 // declarations for definitions in this CU, etc) consumers don't get confused
302 // and think this is a full definition.
303 addFlag(Die, dwarf::DW_AT_declaration);
305 Die.addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
306 new (DIEValueAllocator) DIETypeSignature(Type));
307 }
309 void DwarfUnit::addDIEEntry(DIE &Die, dwarf::Attribute Attribute,
310 DIEEntry *Entry) {
311 const DIE *DieCU = Die.getUnitOrNull();
312 const DIE *EntryCU = Entry->getEntry().getUnitOrNull();
313 if (!DieCU)
314 // We assume that Die belongs to this CU, if it is not linked to any CU yet.
315 DieCU = &getUnitDie();
316 if (!EntryCU)
317 EntryCU = &getUnitDie();
318 Die.addValue(Attribute,
319 EntryCU == DieCU ? dwarf::DW_FORM_ref4 : dwarf::DW_FORM_ref_addr,
320 Entry);
321 }
323 /// Create a DIE with the given Tag, add the DIE to its parent, and
324 /// call insertDIE if MD is not null.
325 DIE &DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
326 assert(Tag != dwarf::DW_TAG_auto_variable &&
327 Tag != dwarf::DW_TAG_arg_variable);
328 Parent.addChild(make_unique<DIE>((dwarf::Tag)Tag));
329 DIE &Die = *Parent.getChildren().back();
330 if (N)
331 insertDIE(N, &Die);
332 return Die;
333 }
335 /// addBlock - Add block data.
336 ///
337 void DwarfUnit::addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Loc) {
338 Loc->ComputeSize(Asm);
339 DIELocs.push_back(Loc); // Memoize so we can call the destructor later on.
340 Die.addValue(Attribute, Loc->BestForm(DD->getDwarfVersion()), Loc);
341 }
343 void DwarfUnit::addBlock(DIE &Die, dwarf::Attribute Attribute,
344 DIEBlock *Block) {
345 Block->ComputeSize(Asm);
346 DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
347 Die.addValue(Attribute, Block->BestForm(), Block);
348 }
350 /// addSourceLine - Add location information to specified debug information
351 /// entry.
352 void DwarfUnit::addSourceLine(DIE &Die, unsigned Line, StringRef File,
353 StringRef Directory) {
354 if (Line == 0)
355 return;
357 unsigned FileID = getOrCreateSourceID(File, Directory);
358 assert(FileID && "Invalid file id");
359 addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
360 addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
361 }
363 /// addSourceLine - Add location information to specified debug information
364 /// entry.
365 void DwarfUnit::addSourceLine(DIE &Die, DIVariable V) {
366 assert(V.isVariable());
368 addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
369 V.getContext().getDirectory());
370 }
372 /// addSourceLine - Add location information to specified debug information
373 /// entry.
374 void DwarfUnit::addSourceLine(DIE &Die, DIGlobalVariable G) {
375 assert(G.isGlobalVariable());
377 addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
378 }
380 /// addSourceLine - Add location information to specified debug information
381 /// entry.
382 void DwarfUnit::addSourceLine(DIE &Die, DISubprogram SP) {
383 assert(SP.isSubprogram());
385 addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
386 }
388 /// addSourceLine - Add location information to specified debug information
389 /// entry.
390 void DwarfUnit::addSourceLine(DIE &Die, DIType Ty) {
391 assert(Ty.isType());
393 addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
394 }
396 /// addSourceLine - Add location information to specified debug information
397 /// entry.
398 void DwarfUnit::addSourceLine(DIE &Die, DIObjCProperty Ty) {
399 assert(Ty.isObjCProperty());
401 DIFile File = Ty.getFile();
402 addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
403 File.getDirectory());
404 }
406 /// addSourceLine - Add location information to specified debug information
407 /// entry.
408 void DwarfUnit::addSourceLine(DIE &Die, DINameSpace NS) {
409 assert(NS.Verify());
411 addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
412 }
414 /// addVariableAddress - Add DW_AT_location attribute for a
415 /// DbgVariable based on provided MachineLocation.
416 void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE &Die,
417 MachineLocation Location) {
418 if (DV.variableHasComplexAddress())
419 addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
420 else if (DV.isBlockByrefVariable())
421 addBlockByrefAddress(DV, Die, dwarf::DW_AT_location, Location);
422 else
423 addAddress(Die, dwarf::DW_AT_location, Location,
424 DV.getVariable().isIndirect());
425 }
427 /// addRegisterOp - Add register operand.
428 // FIXME: Ideally, this would share the implementation with
429 // AsmPrinter::EmitDwarfRegOpPiece.
430 void DwarfUnit::addRegisterOpPiece(DIELoc &TheDie, unsigned Reg,
431 unsigned SizeInBits, unsigned OffsetInBits) {
432 const TargetRegisterInfo *RI = Asm->TM.getSubtargetImpl()->getRegisterInfo();
433 int DWReg = RI->getDwarfRegNum(Reg, false);
434 bool isSubRegister = DWReg < 0;
436 unsigned Idx = 0;
438 // Go up the super-register chain until we hit a valid dwarf register number.
439 for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
440 DWReg = RI->getDwarfRegNum(*SR, false);
441 if (DWReg >= 0)
442 Idx = RI->getSubRegIndex(*SR, Reg);
443 }
445 if (DWReg < 0) {
446 DEBUG(dbgs() << "Invalid Dwarf register number.\n");
447 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
448 return;
449 }
451 // Emit register.
452 if (DWReg < 32)
453 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
454 else {
455 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
456 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
457 }
459 // Emit mask.
460 bool isPiece = SizeInBits > 0;
461 if (isSubRegister || isPiece) {
462 const unsigned SizeOfByte = 8;
463 unsigned RegSizeInBits = RI->getSubRegIdxSize(Idx);
464 unsigned RegOffsetInBits = RI->getSubRegIdxOffset(Idx);
465 unsigned PieceSizeInBits = std::max(SizeInBits, RegSizeInBits);
466 unsigned PieceOffsetInBits = OffsetInBits ? OffsetInBits : RegOffsetInBits;
467 assert(RegSizeInBits >= SizeInBits && "register smaller than value");
469 if (RegOffsetInBits != PieceOffsetInBits) {
470 // Manually shift the value into place, since the DW_OP_piece
471 // describes the part of the variable, not the position of the
472 // subregister.
473 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
474 addUInt(TheDie, dwarf::DW_FORM_data1, RegOffsetInBits);
475 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_shr);
476 }
478 if (PieceOffsetInBits > 0 || PieceSizeInBits % SizeOfByte) {
479 assert(PieceSizeInBits > 0 && "piece has zero size");
480 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
481 addUInt(TheDie, dwarf::DW_FORM_data1, PieceSizeInBits);
482 addUInt(TheDie, dwarf::DW_FORM_data1, PieceOffsetInBits);
483 } else {
484 assert(PieceSizeInBits > 0 && "piece has zero size");
485 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
486 addUInt(TheDie, dwarf::DW_FORM_data1, PieceSizeInBits/SizeOfByte);
487 }
488 }
489 }
491 /// addRegisterOffset - Add register offset.
492 void DwarfUnit::addRegisterOffset(DIELoc &TheDie, unsigned Reg,
493 int64_t Offset) {
494 const TargetRegisterInfo *RI = Asm->TM.getSubtargetImpl()->getRegisterInfo();
495 unsigned DWReg = RI->getDwarfRegNum(Reg, false);
496 const TargetRegisterInfo *TRI = Asm->TM.getSubtargetImpl()->getRegisterInfo();
497 if (Reg == TRI->getFrameRegister(*Asm->MF))
498 // If variable offset is based in frame register then use fbreg.
499 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_fbreg);
500 else if (DWReg < 32)
501 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_breg0 + DWReg);
502 else {
503 addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bregx);
504 addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
505 }
506 addSInt(TheDie, dwarf::DW_FORM_sdata, Offset);
507 }
509 /// addAddress - Add an address attribute to a die based on the location
510 /// provided.
511 void DwarfUnit::addAddress(DIE &Die, dwarf::Attribute Attribute,
512 const MachineLocation &Location, bool Indirect) {
513 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
515 if (Location.isReg() && !Indirect)
516 addRegisterOpPiece(*Loc, Location.getReg());
517 else {
518 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
519 if (Indirect && !Location.isReg()) {
520 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
521 }
522 }
524 // Now attach the location information to the DIE.
525 addBlock(Die, Attribute, Loc);
526 }
528 /// addComplexAddress - Start with the address based on the location provided,
529 /// and generate the DWARF information necessary to find the actual variable
530 /// given the extra address information encoded in the DbgVariable, starting
531 /// from the starting location. Add the DWARF information to the die.
532 ///
533 void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE &Die,
534 dwarf::Attribute Attribute,
535 const MachineLocation &Location) {
536 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
537 unsigned N = DV.getNumAddrElements();
538 unsigned i = 0;
539 if (Location.isReg()) {
540 if (N >= 2 && DV.getAddrElement(0) == dwarf::DW_OP_plus) {
541 assert(!DV.getVariable().isIndirect() &&
542 "double indirection not handled");
543 // If first address element is OpPlus then emit
544 // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
545 addRegisterOffset(*Loc, Location.getReg(), DV.getAddrElement(1));
546 i = 2;
547 } else if (N >= 2 && DV.getAddrElement(0) == dwarf::DW_OP_deref) {
548 assert(!DV.getVariable().isIndirect() &&
549 "double indirection not handled");
550 addRegisterOpPiece(*Loc, Location.getReg(),
551 DV.getExpression().getPieceSize(),
552 DV.getExpression().getPieceOffset());
553 i = 3;
554 } else
555 addRegisterOpPiece(*Loc, Location.getReg());
556 } else
557 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
559 for (; i < N; ++i) {
560 uint64_t Element = DV.getAddrElement(i);
561 if (Element == dwarf::DW_OP_plus) {
562 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
563 addUInt(*Loc, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
565 } else if (Element == dwarf::DW_OP_deref) {
566 if (!Location.isReg())
567 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
569 } else if (Element == dwarf::DW_OP_piece) {
570 const unsigned SizeOfByte = 8;
571 unsigned PieceOffsetInBits = DV.getAddrElement(++i)*SizeOfByte;
572 unsigned PieceSizeInBits = DV.getAddrElement(++i)*SizeOfByte;
573 // Emit DW_OP_bit_piece Size Offset.
574 assert(PieceSizeInBits > 0 && "piece has zero size");
575 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
576 addUInt(*Loc, dwarf::DW_FORM_udata, PieceSizeInBits);
577 addUInt(*Loc, dwarf::DW_FORM_udata, PieceOffsetInBits);
579 } else
580 llvm_unreachable("unknown DIBuilder Opcode");
581 }
583 // Now attach the location information to the DIE.
584 addBlock(Die, Attribute, Loc);
585 }
587 /* Byref variables, in Blocks, are declared by the programmer as "SomeType
588 VarName;", but the compiler creates a __Block_byref_x_VarName struct, and
589 gives the variable VarName either the struct, or a pointer to the struct, as
590 its type. This is necessary for various behind-the-scenes things the
591 compiler needs to do with by-reference variables in Blocks.
593 However, as far as the original *programmer* is concerned, the variable
594 should still have type 'SomeType', as originally declared.
596 The function getBlockByrefType dives into the __Block_byref_x_VarName
597 struct to find the original type of the variable, which is then assigned to
598 the variable's Debug Information Entry as its real type. So far, so good.
599 However now the debugger will expect the variable VarName to have the type
600 SomeType. So we need the location attribute for the variable to be an
601 expression that explains to the debugger how to navigate through the
602 pointers and struct to find the actual variable of type SomeType.
604 The following function does just that. We start by getting
605 the "normal" location for the variable. This will be the location
606 of either the struct __Block_byref_x_VarName or the pointer to the
607 struct __Block_byref_x_VarName.
609 The struct will look something like:
611 struct __Block_byref_x_VarName {
612 ... <various fields>
613 struct __Block_byref_x_VarName *forwarding;
614 ... <various other fields>
615 SomeType VarName;
616 ... <maybe more fields>
617 };
619 If we are given the struct directly (as our starting point) we
620 need to tell the debugger to:
622 1). Add the offset of the forwarding field.
624 2). Follow that pointer to get the real __Block_byref_x_VarName
625 struct to use (the real one may have been copied onto the heap).
627 3). Add the offset for the field VarName, to find the actual variable.
629 If we started with a pointer to the struct, then we need to
630 dereference that pointer first, before the other steps.
631 Translating this into DWARF ops, we will need to append the following
632 to the current location description for the variable:
634 DW_OP_deref -- optional, if we start with a pointer
635 DW_OP_plus_uconst <forward_fld_offset>
636 DW_OP_deref
637 DW_OP_plus_uconst <varName_fld_offset>
639 That is what this function does. */
641 /// addBlockByrefAddress - Start with the address based on the location
642 /// provided, and generate the DWARF information necessary to find the
643 /// actual Block variable (navigating the Block struct) based on the
644 /// starting location. Add the DWARF information to the die. For
645 /// more information, read large comment just above here.
646 ///
647 void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE &Die,
648 dwarf::Attribute Attribute,
649 const MachineLocation &Location) {
650 DIType Ty = DV.getType();
651 DIType TmpTy = Ty;
652 uint16_t Tag = Ty.getTag();
653 bool isPointer = false;
655 StringRef varName = DV.getName();
657 if (Tag == dwarf::DW_TAG_pointer_type) {
658 DIDerivedType DTy(Ty);
659 TmpTy = resolve(DTy.getTypeDerivedFrom());
660 isPointer = true;
661 }
663 DICompositeType blockStruct(TmpTy);
665 // Find the __forwarding field and the variable field in the __Block_byref
666 // struct.
667 DIArray Fields = blockStruct.getElements();
668 DIDerivedType varField;
669 DIDerivedType forwardingField;
671 for (unsigned i = 0, N = Fields.getNumElements(); i < N; ++i) {
672 DIDerivedType DT(Fields.getElement(i));
673 StringRef fieldName = DT.getName();
674 if (fieldName == "__forwarding")
675 forwardingField = DT;
676 else if (fieldName == varName)
677 varField = DT;
678 }
680 // Get the offsets for the forwarding field and the variable field.
681 unsigned forwardingFieldOffset = forwardingField.getOffsetInBits() >> 3;
682 unsigned varFieldOffset = varField.getOffsetInBits() >> 2;
684 // Decode the original location, and use that as the start of the byref
685 // variable's location.
686 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
688 if (Location.isReg())
689 addRegisterOpPiece(*Loc, Location.getReg());
690 else
691 addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
693 // If we started with a pointer to the __Block_byref... struct, then
694 // the first thing we need to do is dereference the pointer (DW_OP_deref).
695 if (isPointer)
696 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
698 // Next add the offset for the '__forwarding' field:
699 // DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
700 // adding the offset if it's 0.
701 if (forwardingFieldOffset > 0) {
702 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
703 addUInt(*Loc, dwarf::DW_FORM_udata, forwardingFieldOffset);
704 }
706 // Now dereference the __forwarding field to get to the real __Block_byref
707 // struct: DW_OP_deref.
708 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
710 // Now that we've got the real __Block_byref... struct, add the offset
711 // for the variable's field to get to the location of the actual variable:
712 // DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
713 if (varFieldOffset > 0) {
714 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
715 addUInt(*Loc, dwarf::DW_FORM_udata, varFieldOffset);
716 }
718 // Now attach the location information to the DIE.
719 addBlock(Die, Attribute, Loc);
720 }
722 /// Return true if type encoding is unsigned.
723 static bool isUnsignedDIType(DwarfDebug *DD, DIType Ty) {
724 DIDerivedType DTy(Ty);
725 if (DTy.isDerivedType()) {
726 dwarf::Tag T = (dwarf::Tag)Ty.getTag();
727 // Encode pointer constants as unsigned bytes. This is used at least for
728 // null pointer constant emission.
729 // FIXME: reference and rvalue_reference /probably/ shouldn't be allowed
730 // here, but accept them for now due to a bug in SROA producing bogus
731 // dbg.values.
732 if (T == dwarf::DW_TAG_pointer_type ||
733 T == dwarf::DW_TAG_ptr_to_member_type ||
734 T == dwarf::DW_TAG_reference_type ||
735 T == dwarf::DW_TAG_rvalue_reference_type)
736 return true;
737 assert(T == dwarf::DW_TAG_typedef || T == dwarf::DW_TAG_const_type ||
738 T == dwarf::DW_TAG_volatile_type ||
739 T == dwarf::DW_TAG_restrict_type ||
740 T == dwarf::DW_TAG_enumeration_type);
741 if (DITypeRef Deriv = DTy.getTypeDerivedFrom())
742 return isUnsignedDIType(DD, DD->resolve(Deriv));
743 // FIXME: Enums without a fixed underlying type have unknown signedness
744 // here, leading to incorrectly emitted constants.
745 assert(DTy.getTag() == dwarf::DW_TAG_enumeration_type);
746 return false;
747 }
749 DIBasicType BTy(Ty);
750 assert(BTy.isBasicType());
751 unsigned Encoding = BTy.getEncoding();
752 assert((Encoding == dwarf::DW_ATE_unsigned ||
753 Encoding == dwarf::DW_ATE_unsigned_char ||
754 Encoding == dwarf::DW_ATE_signed ||
755 Encoding == dwarf::DW_ATE_signed_char ||
756 Encoding == dwarf::DW_ATE_UTF || Encoding == dwarf::DW_ATE_boolean) &&
757 "Unsupported encoding");
758 return (Encoding == dwarf::DW_ATE_unsigned ||
759 Encoding == dwarf::DW_ATE_unsigned_char ||
760 Encoding == dwarf::DW_ATE_UTF || Encoding == dwarf::DW_ATE_boolean);
761 }
763 /// If this type is derived from a base type then return base type size.
764 static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
765 unsigned Tag = Ty.getTag();
767 if (Tag != dwarf::DW_TAG_member && Tag != dwarf::DW_TAG_typedef &&
768 Tag != dwarf::DW_TAG_const_type && Tag != dwarf::DW_TAG_volatile_type &&
769 Tag != dwarf::DW_TAG_restrict_type)
770 return Ty.getSizeInBits();
772 DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
774 // If this type is not derived from any type or the type is a declaration then
775 // take conservative approach.
776 if (!BaseType.isValid() || BaseType.isForwardDecl())
777 return Ty.getSizeInBits();
779 // If this is a derived type, go ahead and get the base type, unless it's a
780 // reference then it's just the size of the field. Pointer types have no need
781 // of this since they're a different type of qualification on the type.
782 if (BaseType.getTag() == dwarf::DW_TAG_reference_type ||
783 BaseType.getTag() == dwarf::DW_TAG_rvalue_reference_type)
784 return Ty.getSizeInBits();
786 if (BaseType.isDerivedType())
787 return getBaseTypeSize(DD, DIDerivedType(BaseType));
789 return BaseType.getSizeInBits();
790 }
792 /// addConstantFPValue - Add constant value entry in variable DIE.
793 void DwarfUnit::addConstantFPValue(DIE &Die, const MachineOperand &MO) {
794 assert(MO.isFPImm() && "Invalid machine operand!");
795 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
796 APFloat FPImm = MO.getFPImm()->getValueAPF();
798 // Get the raw data form of the floating point.
799 const APInt FltVal = FPImm.bitcastToAPInt();
800 const char *FltPtr = (const char *)FltVal.getRawData();
802 int NumBytes = FltVal.getBitWidth() / 8; // 8 bits per byte.
803 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
804 int Incr = (LittleEndian ? 1 : -1);
805 int Start = (LittleEndian ? 0 : NumBytes - 1);
806 int Stop = (LittleEndian ? NumBytes : -1);
808 // Output the constant to DWARF one byte at a time.
809 for (; Start != Stop; Start += Incr)
810 addUInt(*Block, dwarf::DW_FORM_data1, (unsigned char)0xFF & FltPtr[Start]);
812 addBlock(Die, dwarf::DW_AT_const_value, Block);
813 }
815 /// addConstantFPValue - Add constant value entry in variable DIE.
816 void DwarfUnit::addConstantFPValue(DIE &Die, const ConstantFP *CFP) {
817 // Pass this down to addConstantValue as an unsigned bag of bits.
818 addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
819 }
821 /// addConstantValue - Add constant value entry in variable DIE.
822 void DwarfUnit::addConstantValue(DIE &Die, const ConstantInt *CI, DIType Ty) {
823 addConstantValue(Die, CI->getValue(), Ty);
824 }
826 /// addConstantValue - Add constant value entry in variable DIE.
827 void DwarfUnit::addConstantValue(DIE &Die, const MachineOperand &MO,
828 DIType Ty) {
829 assert(MO.isImm() && "Invalid machine operand!");
831 addConstantValue(Die, isUnsignedDIType(DD, Ty), MO.getImm());
832 }
834 void DwarfUnit::addConstantValue(DIE &Die, bool Unsigned, uint64_t Val) {
835 // FIXME: This is a bit conservative/simple - it emits negative values always
836 // sign extended to 64 bits rather than minimizing the number of bytes.
837 addUInt(Die, dwarf::DW_AT_const_value,
838 Unsigned ? dwarf::DW_FORM_udata : dwarf::DW_FORM_sdata, Val);
839 }
841 void DwarfUnit::addConstantValue(DIE &Die, const APInt &Val, DIType Ty) {
842 addConstantValue(Die, Val, isUnsignedDIType(DD, Ty));
843 }
845 // addConstantValue - Add constant value entry in variable DIE.
846 void DwarfUnit::addConstantValue(DIE &Die, const APInt &Val, bool Unsigned) {
847 unsigned CIBitWidth = Val.getBitWidth();
848 if (CIBitWidth <= 64) {
849 addConstantValue(Die, Unsigned,
850 Unsigned ? Val.getZExtValue() : Val.getSExtValue());
851 return;
852 }
854 DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
856 // Get the raw data form of the large APInt.
857 const uint64_t *Ptr64 = Val.getRawData();
859 int NumBytes = Val.getBitWidth() / 8; // 8 bits per byte.
860 bool LittleEndian = Asm->getDataLayout().isLittleEndian();
862 // Output the constant to DWARF one byte at a time.
863 for (int i = 0; i < NumBytes; i++) {
864 uint8_t c;
865 if (LittleEndian)
866 c = Ptr64[i / 8] >> (8 * (i & 7));
867 else
868 c = Ptr64[(NumBytes - 1 - i) / 8] >> (8 * ((NumBytes - 1 - i) & 7));
869 addUInt(*Block, dwarf::DW_FORM_data1, c);
870 }
872 addBlock(Die, dwarf::DW_AT_const_value, Block);
873 }
875 /// addTemplateParams - Add template parameters into buffer.
876 void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
877 // Add template parameters.
878 for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
879 DIDescriptor Element = TParams.getElement(i);
880 if (Element.isTemplateTypeParameter())
881 constructTemplateTypeParameterDIE(Buffer,
882 DITemplateTypeParameter(Element));
883 else if (Element.isTemplateValueParameter())
884 constructTemplateValueParameterDIE(Buffer,
885 DITemplateValueParameter(Element));
886 }
887 }
889 /// getOrCreateContextDIE - Get context owner's DIE.
890 DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
891 if (!Context || Context.isFile())
892 return &getUnitDie();
893 if (Context.isType())
894 return getOrCreateTypeDIE(DIType(Context));
895 if (Context.isNameSpace())
896 return getOrCreateNameSpace(DINameSpace(Context));
897 if (Context.isSubprogram())
898 return getOrCreateSubprogramDIE(DISubprogram(Context));
899 return getDIE(Context);
900 }
902 DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
903 DIScope Context = resolve(Ty.getContext());
904 DIE *ContextDIE = getOrCreateContextDIE(Context);
906 if (DIE *TyDIE = getDIE(Ty))
907 return TyDIE;
909 // Create new type.
910 DIE &TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
912 constructTypeDIE(TyDIE, Ty);
914 updateAcceleratorTables(Context, Ty, TyDIE);
915 return &TyDIE;
916 }
918 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
919 /// given DIType.
920 DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
921 if (!TyNode)
922 return nullptr;
924 DIType Ty(TyNode);
925 assert(Ty.isType());
926 assert(Ty == resolve(Ty.getRef()) &&
927 "type was not uniqued, possible ODR violation.");
929 // DW_TAG_restrict_type is not supported in DWARF2
930 if (Ty.getTag() == dwarf::DW_TAG_restrict_type && DD->getDwarfVersion() <= 2)
931 return getOrCreateTypeDIE(resolve(DIDerivedType(Ty).getTypeDerivedFrom()));
933 // Construct the context before querying for the existence of the DIE in case
934 // such construction creates the DIE.
935 DIScope Context = resolve(Ty.getContext());
936 DIE *ContextDIE = getOrCreateContextDIE(Context);
937 assert(ContextDIE);
939 if (DIE *TyDIE = getDIE(Ty))
940 return TyDIE;
942 // Create new type.
943 DIE &TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
945 updateAcceleratorTables(Context, Ty, TyDIE);
947 if (Ty.isBasicType())
948 constructTypeDIE(TyDIE, DIBasicType(Ty));
949 else if (Ty.isCompositeType()) {
950 DICompositeType CTy(Ty);
951 if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
952 if (MDString *TypeId = CTy.getIdentifier()) {
953 DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
954 // Skip updating the accelerator tables since this is not the full type.
955 return &TyDIE;
956 }
957 constructTypeDIE(TyDIE, CTy);
958 } else {
959 assert(Ty.isDerivedType() && "Unknown kind of DIType");
960 constructTypeDIE(TyDIE, DIDerivedType(Ty));
961 }
963 return &TyDIE;
964 }
966 void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
967 const DIE &TyDIE) {
968 if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
969 bool IsImplementation = 0;
970 if (Ty.isCompositeType()) {
971 DICompositeType CT(Ty);
972 // A runtime language of 0 actually means C/C++ and that any
973 // non-negative value is some version of Objective-C/C++.
974 IsImplementation = (CT.getRunTimeLang() == 0) || CT.isObjcClassComplete();
975 }
976 unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
977 DD->addAccelType(Ty.getName(), TyDIE, Flags);
979 if ((!Context || Context.isCompileUnit() || Context.isFile() ||
980 Context.isNameSpace()) &&
981 getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
982 GlobalTypes[getParentContextString(Context) + Ty.getName().str()] =
983 &TyDIE;
984 }
985 }
987 /// addType - Add a new type attribute to the specified entity.
988 void DwarfUnit::addType(DIE &Entity, DIType Ty, dwarf::Attribute Attribute) {
989 assert(Ty && "Trying to add a type that doesn't exist?");
991 // Check for pre-existence.
992 DIEEntry *Entry = getDIEEntry(Ty);
993 // If it exists then use the existing value.
994 if (Entry) {
995 addDIEEntry(Entity, Attribute, Entry);
996 return;
997 }
999 // Construct type.
1000 DIE *Buffer = getOrCreateTypeDIE(Ty);
1002 // Set up proxy.
1003 Entry = createDIEEntry(*Buffer);
1004 insertDIEEntry(Ty, Entry);
1005 addDIEEntry(Entity, Attribute, Entry);
1006 }
1008 /// addGlobalName - Add a new global name to the compile unit.
1009 void DwarfUnit::addGlobalName(StringRef Name, DIE &Die, DIScope Context) {
1010 if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
1011 return;
1012 std::string FullName = getParentContextString(Context) + Name.str();
1013 GlobalNames[FullName] = &Die;
1014 }
1016 /// getParentContextString - Walks the metadata parent chain in a language
1017 /// specific manner (using the compile unit language) and returns
1018 /// it as a string. This is done at the metadata level because DIEs may
1019 /// not currently have been added to the parent context and walking the
1020 /// DIEs looking for names is more expensive than walking the metadata.
1021 std::string DwarfUnit::getParentContextString(DIScope Context) const {
1022 if (!Context)
1023 return "";
1025 // FIXME: Decide whether to implement this for non-C++ languages.
1026 if (getLanguage() != dwarf::DW_LANG_C_plus_plus)
1027 return "";
1029 std::string CS;
1030 SmallVector<DIScope, 1> Parents;
1031 while (!Context.isCompileUnit()) {
1032 Parents.push_back(Context);
1033 if (Context.getContext())
1034 Context = resolve(Context.getContext());
1035 else
1036 // Structure, etc types will have a NULL context if they're at the top
1037 // level.
1038 break;
1039 }
1041 // Reverse iterate over our list to go from the outermost construct to the
1042 // innermost.
1043 for (SmallVectorImpl<DIScope>::reverse_iterator I = Parents.rbegin(),
1044 E = Parents.rend();
1045 I != E; ++I) {
1046 DIScope Ctx = *I;
1047 StringRef Name = Ctx.getName();
1048 if (Name.empty() && Ctx.isNameSpace())
1049 Name = "(anonymous namespace)";
1050 if (!Name.empty()) {
1051 CS += Name;
1052 CS += "::";
1053 }
1054 }
1055 return CS;
1056 }
1058 /// constructTypeDIE - Construct basic type die from DIBasicType.
1059 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
1060 // Get core information.
1061 StringRef Name = BTy.getName();
1062 // Add name if not anonymous or intermediate type.
1063 if (!Name.empty())
1064 addString(Buffer, dwarf::DW_AT_name, Name);
1066 // An unspecified type only has a name attribute.
1067 if (BTy.getTag() == dwarf::DW_TAG_unspecified_type)
1068 return;
1070 addUInt(Buffer, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1071 BTy.getEncoding());
1073 uint64_t Size = BTy.getSizeInBits() >> 3;
1074 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1075 }
1077 /// constructTypeDIE - Construct derived type die from DIDerivedType.
1078 void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
1079 // Get core information.
1080 StringRef Name = DTy.getName();
1081 uint64_t Size = DTy.getSizeInBits() >> 3;
1082 uint16_t Tag = Buffer.getTag();
1084 // Map to main type, void will not have a type.
1085 DIType FromTy = resolve(DTy.getTypeDerivedFrom());
1086 if (FromTy)
1087 addType(Buffer, FromTy);
1089 // Add name if not anonymous or intermediate type.
1090 if (!Name.empty())
1091 addString(Buffer, dwarf::DW_AT_name, Name);
1093 // Add size if non-zero (derived types might be zero-sized.)
1094 if (Size && Tag != dwarf::DW_TAG_pointer_type)
1095 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1097 if (Tag == dwarf::DW_TAG_ptr_to_member_type)
1098 addDIEEntry(Buffer, dwarf::DW_AT_containing_type,
1099 *getOrCreateTypeDIE(resolve(DTy.getClassType())));
1100 // Add source line info if available and TyDesc is not a forward declaration.
1101 if (!DTy.isForwardDecl())
1102 addSourceLine(Buffer, DTy);
1103 }
1105 /// constructSubprogramArguments - Construct function argument DIEs.
1106 void DwarfUnit::constructSubprogramArguments(DIE &Buffer, DITypeArray Args) {
1107 for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
1108 DIType Ty = resolve(Args.getElement(i));
1109 if (!Ty) {
1110 assert(i == N-1 && "Unspecified parameter must be the last argument");
1111 createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
1112 } else {
1113 DIE &Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
1114 addType(Arg, Ty);
1115 if (Ty.isArtificial())
1116 addFlag(Arg, dwarf::DW_AT_artificial);
1117 }
1118 }
1119 }
1121 /// constructTypeDIE - Construct type DIE from DICompositeType.
1122 void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
1123 // Add name if not anonymous or intermediate type.
1124 StringRef Name = CTy.getName();
1126 uint64_t Size = CTy.getSizeInBits() >> 3;
1127 uint16_t Tag = Buffer.getTag();
1129 switch (Tag) {
1130 case dwarf::DW_TAG_array_type:
1131 constructArrayTypeDIE(Buffer, CTy);
1132 break;
1133 case dwarf::DW_TAG_enumeration_type:
1134 constructEnumTypeDIE(Buffer, CTy);
1135 break;
1136 case dwarf::DW_TAG_subroutine_type: {
1137 // Add return type. A void return won't have a type.
1138 DITypeArray Elements = DISubroutineType(CTy).getTypeArray();
1139 DIType RTy(resolve(Elements.getElement(0)));
1140 if (RTy)
1141 addType(Buffer, RTy);
1143 bool isPrototyped = true;
1144 if (Elements.getNumElements() == 2 &&
1145 !Elements.getElement(1))
1146 isPrototyped = false;
1148 constructSubprogramArguments(Buffer, Elements);
1150 // Add prototype flag if we're dealing with a C language and the
1151 // function has been prototyped.
1152 uint16_t Language = getLanguage();
1153 if (isPrototyped &&
1154 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1155 Language == dwarf::DW_LANG_ObjC))
1156 addFlag(Buffer, dwarf::DW_AT_prototyped);
1158 if (CTy.isLValueReference())
1159 addFlag(Buffer, dwarf::DW_AT_reference);
1161 if (CTy.isRValueReference())
1162 addFlag(Buffer, dwarf::DW_AT_rvalue_reference);
1163 } break;
1164 case dwarf::DW_TAG_structure_type:
1165 case dwarf::DW_TAG_union_type:
1166 case dwarf::DW_TAG_class_type: {
1167 // Add elements to structure type.
1168 DIArray Elements = CTy.getElements();
1169 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1170 DIDescriptor Element = Elements.getElement(i);
1171 if (Element.isSubprogram())
1172 getOrCreateSubprogramDIE(DISubprogram(Element));
1173 else if (Element.isDerivedType()) {
1174 DIDerivedType DDTy(Element);
1175 if (DDTy.getTag() == dwarf::DW_TAG_friend) {
1176 DIE &ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
1177 addType(ElemDie, resolve(DDTy.getTypeDerivedFrom()),
1178 dwarf::DW_AT_friend);
1179 } else if (DDTy.isStaticMember()) {
1180 getOrCreateStaticMemberDIE(DDTy);
1181 } else {
1182 constructMemberDIE(Buffer, DDTy);
1183 }
1184 } else if (Element.isObjCProperty()) {
1185 DIObjCProperty Property(Element);
1186 DIE &ElemDie = createAndAddDIE(Property.getTag(), Buffer);
1187 StringRef PropertyName = Property.getObjCPropertyName();
1188 addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
1189 if (Property.getType())
1190 addType(ElemDie, Property.getType());
1191 addSourceLine(ElemDie, Property);
1192 StringRef GetterName = Property.getObjCPropertyGetterName();
1193 if (!GetterName.empty())
1194 addString(ElemDie, dwarf::DW_AT_APPLE_property_getter, GetterName);
1195 StringRef SetterName = Property.getObjCPropertySetterName();
1196 if (!SetterName.empty())
1197 addString(ElemDie, dwarf::DW_AT_APPLE_property_setter, SetterName);
1198 unsigned PropertyAttributes = 0;
1199 if (Property.isReadOnlyObjCProperty())
1200 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readonly;
1201 if (Property.isReadWriteObjCProperty())
1202 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_readwrite;
1203 if (Property.isAssignObjCProperty())
1204 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_assign;
1205 if (Property.isRetainObjCProperty())
1206 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_retain;
1207 if (Property.isCopyObjCProperty())
1208 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_copy;
1209 if (Property.isNonAtomicObjCProperty())
1210 PropertyAttributes |= dwarf::DW_APPLE_PROPERTY_nonatomic;
1211 if (PropertyAttributes)
1212 addUInt(ElemDie, dwarf::DW_AT_APPLE_property_attribute, None,
1213 PropertyAttributes);
1215 DIEEntry *Entry = getDIEEntry(Element);
1216 if (!Entry) {
1217 Entry = createDIEEntry(ElemDie);
1218 insertDIEEntry(Element, Entry);
1219 }
1220 } else
1221 continue;
1222 }
1224 if (CTy.isAppleBlockExtension())
1225 addFlag(Buffer, dwarf::DW_AT_APPLE_block);
1227 DICompositeType ContainingType(resolve(CTy.getContainingType()));
1228 if (ContainingType)
1229 addDIEEntry(Buffer, dwarf::DW_AT_containing_type,
1230 *getOrCreateTypeDIE(ContainingType));
1232 if (CTy.isObjcClassComplete())
1233 addFlag(Buffer, dwarf::DW_AT_APPLE_objc_complete_type);
1235 // Add template parameters to a class, structure or union types.
1236 // FIXME: The support isn't in the metadata for this yet.
1237 if (Tag == dwarf::DW_TAG_class_type ||
1238 Tag == dwarf::DW_TAG_structure_type || Tag == dwarf::DW_TAG_union_type)
1239 addTemplateParams(Buffer, CTy.getTemplateParams());
1241 break;
1242 }
1243 default:
1244 break;
1245 }
1247 // Add name if not anonymous or intermediate type.
1248 if (!Name.empty())
1249 addString(Buffer, dwarf::DW_AT_name, Name);
1251 if (Tag == dwarf::DW_TAG_enumeration_type ||
1252 Tag == dwarf::DW_TAG_class_type || Tag == dwarf::DW_TAG_structure_type ||
1253 Tag == dwarf::DW_TAG_union_type) {
1254 // Add size if non-zero (derived types might be zero-sized.)
1255 // TODO: Do we care about size for enum forward declarations?
1256 if (Size)
1257 addUInt(Buffer, dwarf::DW_AT_byte_size, None, Size);
1258 else if (!CTy.isForwardDecl())
1259 // Add zero size if it is not a forward declaration.
1260 addUInt(Buffer, dwarf::DW_AT_byte_size, None, 0);
1262 // If we're a forward decl, say so.
1263 if (CTy.isForwardDecl())
1264 addFlag(Buffer, dwarf::DW_AT_declaration);
1266 // Add source line info if available.
1267 if (!CTy.isForwardDecl())
1268 addSourceLine(Buffer, CTy);
1270 // No harm in adding the runtime language to the declaration.
1271 unsigned RLang = CTy.getRunTimeLang();
1272 if (RLang)
1273 addUInt(Buffer, dwarf::DW_AT_APPLE_runtime_class, dwarf::DW_FORM_data1,
1274 RLang);
1275 }
1276 }
1278 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
1279 /// DITemplateTypeParameter.
1280 void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
1281 DITemplateTypeParameter TP) {
1282 DIE &ParamDIE =
1283 createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
1284 // Add the type if it exists, it could be void and therefore no type.
1285 if (TP.getType())
1286 addType(ParamDIE, resolve(TP.getType()));
1287 if (!TP.getName().empty())
1288 addString(ParamDIE, dwarf::DW_AT_name, TP.getName());
1289 }
1291 /// constructTemplateValueParameterDIE - Construct new DIE for the given
1292 /// DITemplateValueParameter.
1293 void
1294 DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
1295 DITemplateValueParameter VP) {
1296 DIE &ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
1298 // Add the type if there is one, template template and template parameter
1299 // packs will not have a type.
1300 if (VP.getTag() == dwarf::DW_TAG_template_value_parameter)
1301 addType(ParamDIE, resolve(VP.getType()));
1302 if (!VP.getName().empty())
1303 addString(ParamDIE, dwarf::DW_AT_name, VP.getName());
1304 if (Value *Val = VP.getValue()) {
1305 if (ConstantInt *CI = dyn_cast<ConstantInt>(Val))
1306 addConstantValue(ParamDIE, CI, resolve(VP.getType()));
1307 else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
1308 // For declaration non-type template parameters (such as global values and
1309 // functions)
1310 DIELoc *Loc = new (DIEValueAllocator) DIELoc();
1311 addOpAddress(*Loc, Asm->getSymbol(GV));
1312 // Emit DW_OP_stack_value to use the address as the immediate value of the
1313 // parameter, rather than a pointer to it.
1314 addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
1315 addBlock(ParamDIE, dwarf::DW_AT_location, Loc);
1316 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
1317 assert(isa<MDString>(Val));
1318 addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
1319 cast<MDString>(Val)->getString());
1320 } else if (VP.getTag() == dwarf::DW_TAG_GNU_template_parameter_pack) {
1321 assert(isa<MDNode>(Val));
1322 DIArray A(cast<MDNode>(Val));
1323 addTemplateParams(ParamDIE, A);
1324 }
1325 }
1326 }
1328 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
1329 DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
1330 // Construct the context before querying for the existence of the DIE in case
1331 // such construction creates the DIE.
1332 DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
1334 if (DIE *NDie = getDIE(NS))
1335 return NDie;
1336 DIE &NDie = createAndAddDIE(dwarf::DW_TAG_namespace, *ContextDIE, NS);
1338 StringRef Name = NS.getName();
1339 if (!Name.empty())
1340 addString(NDie, dwarf::DW_AT_name, NS.getName());
1341 else
1342 Name = "(anonymous namespace)";
1343 DD->addAccelNamespace(Name, NDie);
1344 addGlobalName(Name, NDie, NS.getContext());
1345 addSourceLine(NDie, NS);
1346 return &NDie;
1347 }
1349 /// getOrCreateSubprogramDIE - Create new DIE using SP.
1350 DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
1351 // Construct the context before querying for the existence of the DIE in case
1352 // such construction creates the DIE (as is the case for member function
1353 // declarations).
1354 DIE *ContextDIE = getOrCreateContextDIE(resolve(SP.getContext()));
1356 if (DIE *SPDie = getDIE(SP))
1357 return SPDie;
1359 if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
1360 // Add subprogram definitions to the CU die directly.
1361 ContextDIE = &getUnitDie();
1362 // Build the decl now to ensure it precedes the definition.
1363 getOrCreateSubprogramDIE(SPDecl);
1364 }
1366 // DW_TAG_inlined_subroutine may refer to this DIE.
1367 DIE &SPDie = createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, SP);
1369 // Stop here and fill this in later, depending on whether or not this
1370 // subprogram turns out to have inlined instances or not.
1371 if (SP.isDefinition())
1372 return &SPDie;
1374 applySubprogramAttributes(SP, SPDie);
1375 return &SPDie;
1376 }
1378 void DwarfUnit::applySubprogramAttributesToDefinition(DISubprogram SP, DIE &SPDie) {
1379 DISubprogram SPDecl = SP.getFunctionDeclaration();
1380 DIScope Context = resolve(SPDecl ? SPDecl.getContext() : SP.getContext());
1381 applySubprogramAttributes(SP, SPDie);
1382 addGlobalName(SP.getName(), SPDie, Context);
1383 }
1385 void DwarfUnit::applySubprogramAttributes(DISubprogram SP, DIE &SPDie) {
1386 DIE *DeclDie = nullptr;
1387 StringRef DeclLinkageName;
1388 if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
1389 DeclDie = getDIE(SPDecl);
1390 assert(DeclDie && "This DIE should've already been constructed when the "
1391 "definition DIE was created in "
1392 "getOrCreateSubprogramDIE");
1393 DeclLinkageName = SPDecl.getLinkageName();
1394 }
1396 // Add function template parameters.
1397 addTemplateParams(SPDie, SP.getTemplateParams());
1399 // Add the linkage name if we have one and it isn't in the Decl.
1400 StringRef LinkageName = SP.getLinkageName();
1401 assert(((LinkageName.empty() || DeclLinkageName.empty()) ||
1402 LinkageName == DeclLinkageName) &&
1403 "decl has a linkage name and it is different");
1404 if (!LinkageName.empty() && DeclLinkageName.empty())
1405 addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
1406 GlobalValue::getRealLinkageName(LinkageName));
1408 if (DeclDie) {
1409 // Refer to the function declaration where all the other attributes will be
1410 // found.
1411 addDIEEntry(SPDie, dwarf::DW_AT_specification, *DeclDie);
1412 return;
1413 }
1415 // Constructors and operators for anonymous aggregates do not have names.
1416 if (!SP.getName().empty())
1417 addString(SPDie, dwarf::DW_AT_name, SP.getName());
1419 // Skip the rest of the attributes under -gmlt to save space.
1420 if(getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
1421 return;
1423 addSourceLine(SPDie, SP);
1425 // Add the prototype if we have a prototype and we have a C like
1426 // language.
1427 uint16_t Language = getLanguage();
1428 if (SP.isPrototyped() &&
1429 (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
1430 Language == dwarf::DW_LANG_ObjC))
1431 addFlag(SPDie, dwarf::DW_AT_prototyped);
1433 DISubroutineType SPTy = SP.getType();
1434 assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
1435 "the type of a subprogram should be a subroutine");
1437 DITypeArray Args = SPTy.getTypeArray();
1438 // Add a return type. If this is a type like a C/C++ void type we don't add a
1439 // return type.
1440 if (resolve(Args.getElement(0)))
1441 addType(SPDie, DIType(resolve(Args.getElement(0))));
1443 unsigned VK = SP.getVirtuality();
1444 if (VK) {
1445 addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
1446 DIELoc *Block = getDIELoc();
1447 addUInt(*Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1448 addUInt(*Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
1449 addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
1450 ContainingTypeMap.insert(
1451 std::make_pair(&SPDie, resolve(SP.getContainingType())));
1452 }
1454 if (!SP.isDefinition()) {
1455 addFlag(SPDie, dwarf::DW_AT_declaration);
1457 // Add arguments. Do not add arguments for subprogram definition. They will
1458 // be handled while processing variables.
1459 constructSubprogramArguments(SPDie, Args);
1460 }
1462 if (SP.isArtificial())
1463 addFlag(SPDie, dwarf::DW_AT_artificial);
1465 if (!SP.isLocalToUnit())
1466 addFlag(SPDie, dwarf::DW_AT_external);
1468 if (SP.isOptimized())
1469 addFlag(SPDie, dwarf::DW_AT_APPLE_optimized);
1471 if (unsigned isa = Asm->getISAEncoding()) {
1472 addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
1473 }
1475 if (SP.isLValueReference())
1476 addFlag(SPDie, dwarf::DW_AT_reference);
1478 if (SP.isRValueReference())
1479 addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
1481 if (SP.isProtected())
1482 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1483 dwarf::DW_ACCESS_protected);
1484 else if (SP.isPrivate())
1485 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1486 dwarf::DW_ACCESS_private);
1487 else if (SP.isPublic())
1488 addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1489 dwarf::DW_ACCESS_public);
1491 if (SP.isExplicit())
1492 addFlag(SPDie, dwarf::DW_AT_explicit);
1493 }
1495 void DwarfUnit::applyVariableAttributes(const DbgVariable &Var,
1496 DIE &VariableDie) {
1497 StringRef Name = Var.getName();
1498 if (!Name.empty())
1499 addString(VariableDie, dwarf::DW_AT_name, Name);
1500 addSourceLine(VariableDie, Var.getVariable());
1501 addType(VariableDie, Var.getType());
1502 if (Var.isArtificial())
1503 addFlag(VariableDie, dwarf::DW_AT_artificial);
1504 }
1506 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
1507 void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
1508 DIE &DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
1509 addDIEEntry(DW_Subrange, dwarf::DW_AT_type, *IndexTy);
1511 // The LowerBound value defines the lower bounds which is typically zero for
1512 // C/C++. The Count value is the number of elements. Values are 64 bit. If
1513 // Count == -1 then the array is unbounded and we do not emit
1514 // DW_AT_lower_bound and DW_AT_count attributes.
1515 int64_t LowerBound = SR.getLo();
1516 int64_t DefaultLowerBound = getDefaultLowerBound();
1517 int64_t Count = SR.getCount();
1519 if (DefaultLowerBound == -1 || LowerBound != DefaultLowerBound)
1520 addUInt(DW_Subrange, dwarf::DW_AT_lower_bound, None, LowerBound);
1522 if (Count != -1)
1523 // FIXME: An unbounded array should reference the expression that defines
1524 // the array.
1525 addUInt(DW_Subrange, dwarf::DW_AT_count, None, Count);
1526 }
1528 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
1529 void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
1530 if (CTy.isVector())
1531 addFlag(Buffer, dwarf::DW_AT_GNU_vector);
1533 // Emit the element type.
1534 addType(Buffer, resolve(CTy.getTypeDerivedFrom()));
1536 // Get an anonymous type for index type.
1537 // FIXME: This type should be passed down from the front end
1538 // as different languages may have different sizes for indexes.
1539 DIE *IdxTy = getIndexTyDie();
1540 if (!IdxTy) {
1541 // Construct an integer type to use for indexes.
1542 IdxTy = &createAndAddDIE(dwarf::DW_TAG_base_type, UnitDie);
1543 addString(*IdxTy, dwarf::DW_AT_name, "sizetype");
1544 addUInt(*IdxTy, dwarf::DW_AT_byte_size, None, sizeof(int64_t));
1545 addUInt(*IdxTy, dwarf::DW_AT_encoding, dwarf::DW_FORM_data1,
1546 dwarf::DW_ATE_unsigned);
1547 setIndexTyDie(IdxTy);
1548 }
1550 // Add subranges to array type.
1551 DIArray Elements = CTy.getElements();
1552 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1553 DIDescriptor Element = Elements.getElement(i);
1554 if (Element.getTag() == dwarf::DW_TAG_subrange_type)
1555 constructSubrangeDIE(Buffer, DISubrange(Element), IdxTy);
1556 }
1557 }
1559 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
1560 void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
1561 DIArray Elements = CTy.getElements();
1563 // Add enumerators to enumeration type.
1564 for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
1565 DIEnumerator Enum(Elements.getElement(i));
1566 if (Enum.isEnumerator()) {
1567 DIE &Enumerator = createAndAddDIE(dwarf::DW_TAG_enumerator, Buffer);
1568 StringRef Name = Enum.getName();
1569 addString(Enumerator, dwarf::DW_AT_name, Name);
1570 int64_t Value = Enum.getEnumValue();
1571 addSInt(Enumerator, dwarf::DW_AT_const_value, dwarf::DW_FORM_sdata,
1572 Value);
1573 }
1574 }
1575 DIType DTy = resolve(CTy.getTypeDerivedFrom());
1576 if (DTy) {
1577 addType(Buffer, DTy);
1578 addFlag(Buffer, dwarf::DW_AT_enum_class);
1579 }
1580 }
1582 /// constructContainingTypeDIEs - Construct DIEs for types that contain
1583 /// vtables.
1584 void DwarfUnit::constructContainingTypeDIEs() {
1585 for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
1586 CE = ContainingTypeMap.end();
1587 CI != CE; ++CI) {
1588 DIE &SPDie = *CI->first;
1589 DIDescriptor D(CI->second);
1590 if (!D)
1591 continue;
1592 DIE *NDie = getDIE(D);
1593 if (!NDie)
1594 continue;
1595 addDIEEntry(SPDie, dwarf::DW_AT_containing_type, *NDie);
1596 }
1597 }
1599 /// constructMemberDIE - Construct member DIE from DIDerivedType.
1600 void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
1601 DIE &MemberDie = createAndAddDIE(DT.getTag(), Buffer);
1602 StringRef Name = DT.getName();
1603 if (!Name.empty())
1604 addString(MemberDie, dwarf::DW_AT_name, Name);
1606 addType(MemberDie, resolve(DT.getTypeDerivedFrom()));
1608 addSourceLine(MemberDie, DT);
1610 if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
1612 // For C++, virtual base classes are not at fixed offset. Use following
1613 // expression to extract appropriate offset from vtable.
1614 // BaseAddr = ObAddr + *((*ObAddr) - Offset)
1616 DIELoc *VBaseLocationDie = new (DIEValueAllocator) DIELoc();
1617 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
1618 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1619 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
1620 addUInt(*VBaseLocationDie, dwarf::DW_FORM_udata, DT.getOffsetInBits());
1621 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_minus);
1622 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
1623 addUInt(*VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
1625 addBlock(MemberDie, dwarf::DW_AT_data_member_location, VBaseLocationDie);
1626 } else {
1627 uint64_t Size = DT.getSizeInBits();
1628 uint64_t FieldSize = getBaseTypeSize(DD, DT);
1629 uint64_t OffsetInBytes;
1631 if (Size != FieldSize) {
1632 // Handle bitfield, assume bytes are 8 bits.
1633 addUInt(MemberDie, dwarf::DW_AT_byte_size, None, FieldSize/8);
1634 addUInt(MemberDie, dwarf::DW_AT_bit_size, None, Size);
1636 uint64_t Offset = DT.getOffsetInBits();
1637 uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
1638 uint64_t HiMark = (Offset + FieldSize) & AlignMask;
1639 uint64_t FieldOffset = (HiMark - FieldSize);
1640 Offset -= FieldOffset;
1642 // Maybe we need to work from the other end.
1643 if (Asm->getDataLayout().isLittleEndian())
1644 Offset = FieldSize - (Offset + Size);
1645 addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
1647 // Here DW_AT_data_member_location points to the anonymous
1648 // field that includes this bit field.
1649 OffsetInBytes = FieldOffset >> 3;
1650 } else
1651 // This is not a bitfield.
1652 OffsetInBytes = DT.getOffsetInBits() >> 3;
1654 if (DD->getDwarfVersion() <= 2) {
1655 DIELoc *MemLocationDie = new (DIEValueAllocator) DIELoc();
1656 addUInt(*MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
1657 addUInt(*MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
1658 addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
1659 } else
1660 addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
1661 OffsetInBytes);
1662 }
1664 if (DT.isProtected())
1665 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1666 dwarf::DW_ACCESS_protected);
1667 else if (DT.isPrivate())
1668 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1669 dwarf::DW_ACCESS_private);
1670 // Otherwise C++ member and base classes are considered public.
1671 else if (DT.isPublic())
1672 addUInt(MemberDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1673 dwarf::DW_ACCESS_public);
1674 if (DT.isVirtual())
1675 addUInt(MemberDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1,
1676 dwarf::DW_VIRTUALITY_virtual);
1678 // Objective-C properties.
1679 if (MDNode *PNode = DT.getObjCProperty())
1680 if (DIEEntry *PropertyDie = getDIEEntry(PNode))
1681 MemberDie.addValue(dwarf::DW_AT_APPLE_property, dwarf::DW_FORM_ref4,
1682 PropertyDie);
1684 if (DT.isArtificial())
1685 addFlag(MemberDie, dwarf::DW_AT_artificial);
1686 }
1688 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
1689 DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
1690 if (!DT.Verify())
1691 return nullptr;
1693 // Construct the context before querying for the existence of the DIE in case
1694 // such construction creates the DIE.
1695 DIE *ContextDIE = getOrCreateContextDIE(resolve(DT.getContext()));
1696 assert(dwarf::isType(ContextDIE->getTag()) &&
1697 "Static member should belong to a type.");
1699 if (DIE *StaticMemberDIE = getDIE(DT))
1700 return StaticMemberDIE;
1702 DIE &StaticMemberDIE = createAndAddDIE(DT.getTag(), *ContextDIE, DT);
1704 DIType Ty = resolve(DT.getTypeDerivedFrom());
1706 addString(StaticMemberDIE, dwarf::DW_AT_name, DT.getName());
1707 addType(StaticMemberDIE, Ty);
1708 addSourceLine(StaticMemberDIE, DT);
1709 addFlag(StaticMemberDIE, dwarf::DW_AT_external);
1710 addFlag(StaticMemberDIE, dwarf::DW_AT_declaration);
1712 // FIXME: We could omit private if the parent is a class_type, and
1713 // public if the parent is something else.
1714 if (DT.isProtected())
1715 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1716 dwarf::DW_ACCESS_protected);
1717 else if (DT.isPrivate())
1718 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1719 dwarf::DW_ACCESS_private);
1720 else if (DT.isPublic())
1721 addUInt(StaticMemberDIE, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
1722 dwarf::DW_ACCESS_public);
1724 if (const ConstantInt *CI = dyn_cast_or_null<ConstantInt>(DT.getConstant()))
1725 addConstantValue(StaticMemberDIE, CI, Ty);
1726 if (const ConstantFP *CFP = dyn_cast_or_null<ConstantFP>(DT.getConstant()))
1727 addConstantFPValue(StaticMemberDIE, CFP);
1729 return &StaticMemberDIE;
1730 }
1732 void DwarfUnit::emitHeader(const MCSymbol *ASectionSym) const {
1733 Asm->OutStreamer.AddComment("DWARF version number");
1734 Asm->EmitInt16(DD->getDwarfVersion());
1735 Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
1736 // We share one abbreviations table across all units so it's always at the
1737 // start of the section. Use a relocatable offset where needed to ensure
1738 // linking doesn't invalidate that offset.
1739 if (ASectionSym)
1740 Asm->EmitSectionOffset(ASectionSym, ASectionSym);
1741 else
1742 // Use a constant value when no symbol is provided.
1743 Asm->EmitInt32(0);
1744 Asm->OutStreamer.AddComment("Address Size (in bytes)");
1745 Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
1746 }
1748 void DwarfTypeUnit::emitHeader(const MCSymbol *ASectionSym) const {
1749 DwarfUnit::emitHeader(ASectionSym);
1750 Asm->OutStreamer.AddComment("Type Signature");
1751 Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
1752 Asm->OutStreamer.AddComment("Type DIE Offset");
1753 // In a skeleton type unit there is no type DIE so emit a zero offset.
1754 Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
1755 sizeof(Ty->getOffset()));
1756 }
1758 void DwarfTypeUnit::initSection(const MCSection *Section) {
1759 assert(!this->Section);
1760 this->Section = Section;
1761 // Since each type unit is contained in its own COMDAT section, the begin
1762 // label and the section label are the same. Using the begin label emission in
1763 // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
1764 // the only other alternative of lazily constructing start-of-section labels
1765 // and storing a mapping in DwarfDebug (or AsmPrinter).
1766 this->SectionSym = this->LabelBegin =
1767 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
1768 this->LabelEnd =
1769 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
1770 }