1 //===-- llvm/CodeGen/DwarfUnit.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_DWARFUNIT_H
15 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFUNIT_H
17 #include "DwarfDebug.h"
18 #include "llvm/ADT/DenseMap.h"
19 #include "llvm/ADT/Optional.h"
20 #include "llvm/ADT/StringMap.h"
21 #include "llvm/CodeGen/AsmPrinter.h"
22 #include "llvm/CodeGen/DIE.h"
23 #include "llvm/IR/DIBuilder.h"
24 #include "llvm/IR/DebugInfo.h"
25 #include "llvm/MC/MCDwarf.h"
26 #include "llvm/MC/MCExpr.h"
27 #include "llvm/MC/MCSection.h"
29 namespace llvm {
31 class MachineLocation;
32 class MachineOperand;
33 class ConstantInt;
34 class ConstantFP;
35 class DbgVariable;
36 class DwarfCompileUnit;
38 // Data structure to hold a range for range lists.
39 class RangeSpan {
40 public:
41 RangeSpan(MCSymbol *S, MCSymbol *E) : Start(S), End(E) {}
42 const MCSymbol *getStart() const { return Start; }
43 const MCSymbol *getEnd() const { return End; }
44 void setEnd(const MCSymbol *E) { End = E; }
46 private:
47 const MCSymbol *Start, *End;
48 };
50 class RangeSpanList {
51 private:
52 // Index for locating within the debug_range section this particular span.
53 MCSymbol *RangeSym;
54 // List of ranges.
55 SmallVector<RangeSpan, 2> Ranges;
57 public:
58 RangeSpanList(MCSymbol *Sym, SmallVector<RangeSpan, 2> Ranges)
59 : RangeSym(Sym), Ranges(std::move(Ranges)) {}
60 MCSymbol *getSym() const { return RangeSym; }
61 const SmallVectorImpl<RangeSpan> &getRanges() const { return Ranges; }
62 void addRange(RangeSpan Range) { Ranges.push_back(Range); }
63 };
65 //===----------------------------------------------------------------------===//
66 /// Unit - This dwarf writer support class manages information associated
67 /// with a source file.
68 class DwarfUnit {
69 protected:
70 /// UniqueID - a numeric ID unique among all CUs in the module
71 unsigned UniqueID;
73 /// Node - MDNode for the compile unit.
74 DICompileUnit CUNode;
76 /// Unit debug information entry.
77 DIE UnitDie;
79 /// Offset of the UnitDie from beginning of debug info section.
80 unsigned DebugInfoOffset;
82 /// Asm - Target of Dwarf emission.
83 AsmPrinter *Asm;
85 // Holders for some common dwarf information.
86 DwarfDebug *DD;
87 DwarfFile *DU;
89 /// IndexTyDie - An anonymous type for index type. Owned by UnitDie.
90 DIE *IndexTyDie;
92 /// MDNodeToDieMap - Tracks the mapping of unit level debug information
93 /// variables to debug information entries.
94 DenseMap<const MDNode *, DIE *> MDNodeToDieMap;
96 /// MDNodeToDIEEntryMap - Tracks the mapping of unit level debug information
97 /// descriptors to debug information entries using a DIEEntry proxy.
98 DenseMap<const MDNode *, DIEEntry *> MDNodeToDIEEntryMap;
100 /// DIEBlocks - A list of all the DIEBlocks in use.
101 std::vector<DIEBlock *> DIEBlocks;
103 /// DIELocs - A list of all the DIELocs in use.
104 std::vector<DIELoc *> DIELocs;
106 /// ContainingTypeMap - This map is used to keep track of subprogram DIEs that
107 /// need DW_AT_containing_type attribute. This attribute points to a DIE that
108 /// corresponds to the MDNode mapped with the subprogram DIE.
109 DenseMap<DIE *, const MDNode *> ContainingTypeMap;
111 // DIEValueAllocator - All DIEValues are allocated through this allocator.
112 BumpPtrAllocator DIEValueAllocator;
114 // DIEIntegerOne - A preallocated DIEValue because 1 is used frequently.
115 DIEInteger *DIEIntegerOne;
117 /// The section this unit will be emitted in.
118 const MCSection *Section;
120 DwarfUnit(unsigned UID, dwarf::Tag, DICompileUnit CU, AsmPrinter *A,
121 DwarfDebug *DW, DwarfFile *DWU);
123 void initSection(const MCSection *Section);
125 /// Add a string attribute data and value.
126 void addLocalString(DIE &Die, dwarf::Attribute Attribute, StringRef Str);
128 void addIndexedString(DIE &Die, dwarf::Attribute Attribute, StringRef Str);
130 bool applySubprogramDefinitionAttributes(DISubprogram SP, DIE &SPDie);
132 public:
133 virtual ~DwarfUnit();
135 const MCSection *getSection() const {
136 assert(Section);
137 return Section;
138 }
140 // Accessors.
141 AsmPrinter* getAsmPrinter() const { return Asm; }
142 unsigned getUniqueID() const { return UniqueID; }
143 uint16_t getLanguage() const { return CUNode.getLanguage(); }
144 DICompileUnit getCUNode() const { return CUNode; }
145 DIE &getUnitDie() { return UnitDie; }
147 unsigned getDebugInfoOffset() const { return DebugInfoOffset; }
148 void setDebugInfoOffset(unsigned DbgInfoOff) { DebugInfoOffset = DbgInfoOff; }
150 /// hasContent - Return true if this compile unit has something to write out.
151 bool hasContent() const { return !UnitDie.getChildren().empty(); }
153 /// getParentContextString - Get a string containing the language specific
154 /// context for a global name.
155 std::string getParentContextString(DIScope Context) const;
157 /// Add a new global name to the compile unit.
158 virtual void addGlobalName(StringRef Name, DIE &Die, DIScope Context) {}
160 /// Add a new global type to the compile unit.
161 virtual void addGlobalType(DIType Ty, const DIE &Die, DIScope Context) {}
163 /// addAccelNamespace - Add a new name to the namespace accelerator table.
164 void addAccelNamespace(StringRef Name, const DIE &Die);
166 /// getDIE - Returns the debug information entry map slot for the
167 /// specified debug variable. We delegate the request to DwarfDebug
168 /// when the MDNode can be part of the type system, since DIEs for
169 /// the type system can be shared across CUs and the mappings are
170 /// kept in DwarfDebug.
171 DIE *getDIE(DIDescriptor D) const;
173 /// getDIELoc - Returns a fresh newly allocated DIELoc.
174 DIELoc *getDIELoc() { return new (DIEValueAllocator) DIELoc(); }
176 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
177 /// when the MDNode can be part of the type system, since DIEs for
178 /// the type system can be shared across CUs and the mappings are
179 /// kept in DwarfDebug.
180 void insertDIE(DIDescriptor Desc, DIE *D);
182 /// addFlag - Add a flag that is true to the DIE.
183 void addFlag(DIE &Die, dwarf::Attribute Attribute);
185 /// addUInt - Add an unsigned integer attribute data and value.
186 void addUInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
187 uint64_t Integer);
189 void addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer);
191 /// addSInt - Add an signed integer attribute data and value.
192 void addSInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
193 int64_t Integer);
195 void addSInt(DIELoc &Die, Optional<dwarf::Form> Form, int64_t Integer);
197 /// addString - Add a string attribute data and value.
198 void addString(DIE &Die, dwarf::Attribute Attribute, StringRef Str);
200 /// addLabel - Add a Dwarf label attribute data and value.
201 void addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form,
202 const MCSymbol *Label);
204 void addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label);
206 /// addSectionOffset - Add an offset into a section attribute data and value.
207 ///
208 void addSectionOffset(DIE &Die, dwarf::Attribute Attribute, uint64_t Integer);
210 /// addOpAddress - Add a dwarf op address data and value using the
211 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
212 void addOpAddress(DIELoc &Die, const MCSymbol *Label);
214 /// addLabelDelta - Add a label delta attribute data and value.
215 void addLabelDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
216 const MCSymbol *Lo);
218 /// addDIEEntry - Add a DIE attribute data and value.
219 void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry);
221 /// addDIEEntry - Add a DIE attribute data and value.
222 void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIEEntry *Entry);
224 void addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type);
226 /// addBlock - Add block data.
227 void addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Block);
229 /// addBlock - Add block data.
230 void addBlock(DIE &Die, dwarf::Attribute Attribute, DIEBlock *Block);
232 /// addSourceLine - Add location information to specified debug information
233 /// entry.
234 void addSourceLine(DIE &Die, unsigned Line, StringRef File,
235 StringRef Directory);
236 void addSourceLine(DIE &Die, DIVariable V);
237 void addSourceLine(DIE &Die, DIGlobalVariable G);
238 void addSourceLine(DIE &Die, DISubprogram SP);
239 void addSourceLine(DIE &Die, DIType Ty);
240 void addSourceLine(DIE &Die, DINameSpace NS);
241 void addSourceLine(DIE &Die, DIObjCProperty Ty);
243 /// addConstantValue - Add constant value entry in variable DIE.
244 void addConstantValue(DIE &Die, const MachineOperand &MO, DIType Ty);
245 void addConstantValue(DIE &Die, const ConstantInt *CI, DIType Ty);
246 void addConstantValue(DIE &Die, const APInt &Val, DIType Ty);
247 void addConstantValue(DIE &Die, const APInt &Val, bool Unsigned);
248 void addConstantValue(DIE &Die, bool Unsigned, uint64_t Val);
250 /// addConstantFPValue - Add constant value entry in variable DIE.
251 void addConstantFPValue(DIE &Die, const MachineOperand &MO);
252 void addConstantFPValue(DIE &Die, const ConstantFP *CFP);
254 /// addTemplateParams - Add template parameters in buffer.
255 void addTemplateParams(DIE &Buffer, DIArray TParams);
257 /// \brief Add register operand.
258 /// \returns false if the register does not exist, e.g., because it was never
259 /// materialized.
260 bool addRegisterOpPiece(DIELoc &TheDie, unsigned Reg,
261 unsigned SizeInBits = 0, unsigned OffsetInBits = 0);
263 /// \brief Add register offset.
264 /// \returns false if the register does not exist, e.g., because it was never
265 /// materialized.
266 bool addRegisterOffset(DIELoc &TheDie, unsigned Reg, int64_t Offset);
268 // FIXME: Should be reformulated in terms of addComplexAddress.
269 /// addBlockByrefAddress - Start with the address based on the location
270 /// provided, and generate the DWARF information necessary to find the
271 /// actual Block variable (navigating the Block struct) based on the
272 /// starting location. Add the DWARF information to the die. Obsolete,
273 /// please use addComplexAddress instead.
274 void addBlockByrefAddress(const DbgVariable &DV, DIE &Die,
275 dwarf::Attribute Attribute,
276 const MachineLocation &Location);
278 /// addType - Add a new type attribute to the specified entity. This takes
279 /// and attribute parameter because DW_AT_friend attributes are also
280 /// type references.
281 void addType(DIE &Entity, DIType Ty,
282 dwarf::Attribute Attribute = dwarf::DW_AT_type);
284 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
285 DIE *getOrCreateNameSpace(DINameSpace NS);
287 /// getOrCreateSubprogramDIE - Create new DIE using SP.
288 DIE *getOrCreateSubprogramDIE(DISubprogram SP, bool Minimal = false);
290 void applySubprogramAttributes(DISubprogram SP, DIE &SPDie,
291 bool Minimal = false);
293 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
294 /// given DIType.
295 DIE *getOrCreateTypeDIE(const MDNode *N);
297 /// getOrCreateContextDIE - Get context owner's DIE.
298 DIE *createTypeDIE(DICompositeType Ty);
300 /// getOrCreateContextDIE - Get context owner's DIE.
301 DIE *getOrCreateContextDIE(DIScope Context);
303 /// constructContainingTypeDIEs - Construct DIEs for types that contain
304 /// vtables.
305 void constructContainingTypeDIEs();
307 /// constructSubprogramArguments - Construct function argument DIEs.
308 void constructSubprogramArguments(DIE &Buffer, DITypeArray Args);
310 /// Create a DIE with the given Tag, add the DIE to its parent, and
311 /// call insertDIE if MD is not null.
312 DIE &createAndAddDIE(unsigned Tag, DIE &Parent,
313 DIDescriptor N = DIDescriptor());
315 /// Compute the size of a header for this unit, not including the initial
316 /// length field.
317 virtual unsigned getHeaderSize() const {
318 return sizeof(int16_t) + // DWARF version number
319 sizeof(int32_t) + // Offset Into Abbrev. Section
320 sizeof(int8_t); // Pointer Size (in bytes)
321 }
323 /// Emit the header for this unit, not including the initial length field.
324 virtual void emitHeader(const MCSymbol *ASectionSym) const;
326 virtual DwarfCompileUnit &getCU() = 0;
328 /// constructTypeDIE - Construct type DIE from DICompositeType.
329 void constructTypeDIE(DIE &Buffer, DICompositeType CTy);
331 protected:
332 /// getOrCreateStaticMemberDIE - Create new static data member DIE.
333 DIE *getOrCreateStaticMemberDIE(DIDerivedType DT);
335 /// Look up the source ID with the given directory and source file names. If
336 /// none currently exists, create a new ID and insert it in the line table.
337 virtual unsigned getOrCreateSourceID(StringRef File, StringRef Directory) = 0;
339 /// resolve - Look in the DwarfDebug map for the MDNode that
340 /// corresponds to the reference.
341 template <typename T> T resolve(DIRef<T> Ref) const {
342 return DD->resolve(Ref);
343 }
345 private:
346 /// constructTypeDIE - Construct basic type die from DIBasicType.
347 void constructTypeDIE(DIE &Buffer, DIBasicType BTy);
349 /// constructTypeDIE - Construct derived type die from DIDerivedType.
350 void constructTypeDIE(DIE &Buffer, DIDerivedType DTy);
352 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
353 void constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy);
355 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
356 void constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy);
358 /// constructEnumTypeDIE - Construct enum type DIE from DIEnumerator.
359 void constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy);
361 /// constructMemberDIE - Construct member DIE from DIDerivedType.
362 void constructMemberDIE(DIE &Buffer, DIDerivedType DT);
364 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
365 /// DITemplateTypeParameter.
366 void constructTemplateTypeParameterDIE(DIE &Buffer,
367 DITemplateTypeParameter TP);
369 /// constructTemplateValueParameterDIE - Construct new DIE for the given
370 /// DITemplateValueParameter.
371 void constructTemplateValueParameterDIE(DIE &Buffer,
372 DITemplateValueParameter TVP);
374 /// getLowerBoundDefault - Return the default lower bound for an array. If the
375 /// DWARF version doesn't handle the language, return -1.
376 int64_t getDefaultLowerBound() const;
378 /// getDIEEntry - Returns the debug information entry for the specified
379 /// debug variable.
380 DIEEntry *getDIEEntry(const MDNode *N) const {
381 return MDNodeToDIEEntryMap.lookup(N);
382 }
384 /// insertDIEEntry - Insert debug information entry into the map.
385 void insertDIEEntry(const MDNode *N, DIEEntry *E) {
386 MDNodeToDIEEntryMap.insert(std::make_pair(N, E));
387 }
389 // getIndexTyDie - Get an anonymous type for index type.
390 DIE *getIndexTyDie();
392 // setIndexTyDie - Set D as anonymous type for index which can be reused
393 // later.
394 void setIndexTyDie(DIE *D) { IndexTyDie = D; }
396 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
397 /// information entry.
398 DIEEntry *createDIEEntry(DIE &Entry);
400 /// If this is a named finished type then include it in the list of types for
401 /// the accelerator tables.
402 void updateAcceleratorTables(DIScope Context, DIType Ty, const DIE &TyDIE);
404 virtual bool isDwoUnit() const = 0;
405 };
407 class DwarfTypeUnit : public DwarfUnit {
408 uint64_t TypeSignature;
409 const DIE *Ty;
410 DwarfCompileUnit &CU;
411 MCDwarfDwoLineTable *SplitLineTable;
413 unsigned getOrCreateSourceID(StringRef File, StringRef Directory) override;
414 bool isDwoUnit() const override;
416 public:
417 DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A,
418 DwarfDebug *DW, DwarfFile *DWU,
419 MCDwarfDwoLineTable *SplitLineTable = nullptr);
421 void setTypeSignature(uint64_t Signature) { TypeSignature = Signature; }
422 uint64_t getTypeSignature() const { return TypeSignature; }
423 void setType(const DIE *Ty) { this->Ty = Ty; }
425 /// Emit the header for this unit, not including the initial length field.
426 void emitHeader(const MCSymbol *ASectionSym) const override;
427 unsigned getHeaderSize() const override {
428 return DwarfUnit::getHeaderSize() + sizeof(uint64_t) + // Type Signature
429 sizeof(uint32_t); // Type DIE Offset
430 }
431 using DwarfUnit::initSection;
432 DwarfCompileUnit &getCU() override { return CU; }
433 };
434 } // end llvm namespace
435 #endif