1 //===-- llvm/CodeGen/DwarfUnit.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
15 #define CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
17 #include "DIE.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/DenseMap.h"
20 #include "llvm/ADT/Optional.h"
21 #include "llvm/ADT/StringMap.h"
22 #include "llvm/CodeGen/AsmPrinter.h"
23 #include "llvm/IR/DIBuilder.h"
24 #include "llvm/IR/DebugInfo.h"
25 #include "llvm/MC/MCExpr.h"
26 #include "llvm/MC/MCSection.h"
27 #include "llvm/MC/MCDwarf.h"
29 namespace llvm {
31 class MachineLocation;
32 class MachineOperand;
33 class ConstantInt;
34 class ConstantFP;
35 class DbgVariable;
36 class DwarfCompileUnit;
38 // Data structure to hold a range for range lists.
39 class RangeSpan {
40 public:
41 RangeSpan(MCSymbol *S, MCSymbol *E) : Start(S), End(E) {}
42 const MCSymbol *getStart() const { return Start; }
43 const MCSymbol *getEnd() const { return End; }
44 void setEnd(const MCSymbol *E) { End = E; }
46 private:
47 const MCSymbol *Start, *End;
48 };
50 class RangeSpanList {
51 private:
52 // Index for locating within the debug_range section this particular span.
53 MCSymbol *RangeSym;
54 // List of ranges.
55 SmallVector<RangeSpan, 2> Ranges;
57 public:
58 RangeSpanList(MCSymbol *Sym) : RangeSym(Sym) {}
59 MCSymbol *getSym() const { return RangeSym; }
60 const SmallVectorImpl<RangeSpan> &getRanges() const { return Ranges; }
61 void addRange(RangeSpan Range) { Ranges.push_back(Range); }
62 };
64 //===----------------------------------------------------------------------===//
65 /// Unit - This dwarf writer support class manages information associated
66 /// with a source file.
67 class DwarfUnit {
68 protected:
69 /// UniqueID - a numeric ID unique among all CUs in the module
70 unsigned UniqueID;
72 /// Node - MDNode for the compile unit.
73 DICompileUnit CUNode;
75 /// Unit debug information entry.
76 DIE UnitDie;
78 /// Offset of the UnitDie from beginning of debug info section.
79 unsigned DebugInfoOffset;
81 /// Asm - Target of Dwarf emission.
82 AsmPrinter *Asm;
84 // Holders for some common dwarf information.
85 DwarfDebug *DD;
86 DwarfFile *DU;
88 /// IndexTyDie - An anonymous type for index type. Owned by UnitDie.
89 DIE *IndexTyDie;
91 /// MDNodeToDieMap - Tracks the mapping of unit level debug information
92 /// variables to debug information entries.
93 DenseMap<const MDNode *, DIE *> MDNodeToDieMap;
95 /// MDNodeToDIEEntryMap - Tracks the mapping of unit level debug information
96 /// descriptors to debug information entries using a DIEEntry proxy.
97 DenseMap<const MDNode *, DIEEntry *> MDNodeToDIEEntryMap;
99 /// GlobalNames - A map of globally visible named entities for this unit.
100 StringMap<const DIE *> GlobalNames;
102 /// GlobalTypes - A map of globally visible types for this unit.
103 StringMap<const DIE *> GlobalTypes;
105 /// DIEBlocks - A list of all the DIEBlocks in use.
106 std::vector<DIEBlock *> DIEBlocks;
108 /// DIELocs - A list of all the DIELocs in use.
109 std::vector<DIELoc *> DIELocs;
111 /// ContainingTypeMap - This map is used to keep track of subprogram DIEs that
112 /// need DW_AT_containing_type attribute. This attribute points to a DIE that
113 /// corresponds to the MDNode mapped with the subprogram DIE.
114 DenseMap<DIE *, const MDNode *> ContainingTypeMap;
116 // List of ranges for a given compile unit.
117 SmallVector<RangeSpan, 1> CURanges;
119 // List of range lists for a given compile unit, separate from the ranges for
120 // the CU itself.
121 SmallVector<RangeSpanList, 1> CURangeLists;
123 // DIEValueAllocator - All DIEValues are allocated through this allocator.
124 BumpPtrAllocator DIEValueAllocator;
126 // DIEIntegerOne - A preallocated DIEValue because 1 is used frequently.
127 DIEInteger *DIEIntegerOne;
129 /// The section this unit will be emitted in.
130 const MCSection *Section;
132 /// A label at the start of the non-dwo section related to this unit.
133 MCSymbol *SectionSym;
135 /// The start of the unit within its section.
136 MCSymbol *LabelBegin;
138 /// The end of the unit within its section.
139 MCSymbol *LabelEnd;
141 /// Skeleton unit associated with this unit.
142 DwarfUnit *Skeleton;
144 DwarfUnit(unsigned UID, dwarf::Tag, DICompileUnit CU, AsmPrinter *A,
145 DwarfDebug *DW, DwarfFile *DWU);
147 public:
148 virtual ~DwarfUnit();
150 /// Set the skeleton unit associated with this unit.
151 void setSkeleton(DwarfUnit &Skel) { Skeleton = &Skel; }
153 /// Get the skeleton unit associated with this unit.
154 DwarfUnit *getSkeleton() const { return Skeleton; }
156 /// Pass in the SectionSym even though we could recreate it in every compile
157 /// unit (type units will have actually distinct symbols once they're in
158 /// comdat sections).
159 void initSection(const MCSection *Section, MCSymbol *SectionSym) {
160 assert(!this->Section);
161 this->Section = Section;
162 this->SectionSym = SectionSym;
163 this->LabelBegin =
164 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
165 this->LabelEnd =
166 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
167 }
169 const MCSection *getSection() const {
170 assert(Section);
171 return Section;
172 }
174 /// If there's a skeleton then return the section symbol for the skeleton
175 /// unit, otherwise return the section symbol for this unit.
176 MCSymbol *getLocalSectionSym() const {
177 if (Skeleton)
178 return Skeleton->getSectionSym();
179 return getSectionSym();
180 }
182 MCSymbol *getSectionSym() const {
183 assert(Section);
184 return SectionSym;
185 }
187 /// If there's a skeleton then return the begin label for the skeleton unit,
188 /// otherwise return the local label for this unit.
189 MCSymbol *getLocalLabelBegin() const {
190 if (Skeleton)
191 return Skeleton->getLabelBegin();
192 return getLabelBegin();
193 }
195 MCSymbol *getLabelBegin() const {
196 assert(Section);
197 return LabelBegin;
198 }
200 MCSymbol *getLabelEnd() const {
201 assert(Section);
202 return LabelEnd;
203 }
205 // Accessors.
206 unsigned getUniqueID() const { return UniqueID; }
207 uint16_t getLanguage() const { return CUNode.getLanguage(); }
208 DICompileUnit getCUNode() const { return CUNode; }
209 DIE &getUnitDie() { return UnitDie; }
210 const StringMap<const DIE *> &getGlobalNames() const { return GlobalNames; }
211 const StringMap<const DIE *> &getGlobalTypes() const { return GlobalTypes; }
213 unsigned getDebugInfoOffset() const { return DebugInfoOffset; }
214 void setDebugInfoOffset(unsigned DbgInfoOff) { DebugInfoOffset = DbgInfoOff; }
216 /// hasContent - Return true if this compile unit has something to write out.
217 bool hasContent() const { return !UnitDie.getChildren().empty(); }
219 /// addRange - Add an address range to the list of ranges for this unit.
220 void addRange(RangeSpan Range);
222 /// getRanges - Get the list of ranges for this unit.
223 const SmallVectorImpl<RangeSpan> &getRanges() const { return CURanges; }
224 SmallVectorImpl<RangeSpan> &getRanges() { return CURanges; }
226 /// addRangeList - Add an address range list to the list of range lists.
227 void addRangeList(RangeSpanList Ranges) { CURangeLists.push_back(Ranges); }
229 /// getRangeLists - Get the vector of range lists.
230 const SmallVectorImpl<RangeSpanList> &getRangeLists() const {
231 return CURangeLists;
232 }
233 SmallVectorImpl<RangeSpanList> &getRangeLists() { return CURangeLists; }
235 /// getParentContextString - Get a string containing the language specific
236 /// context for a global name.
237 std::string getParentContextString(DIScope Context) const;
239 /// addGlobalName - Add a new global entity to the compile unit.
240 ///
241 void addGlobalName(StringRef Name, DIE &Die, DIScope Context);
243 /// addAccelNamespace - Add a new name to the namespace accelerator table.
244 void addAccelNamespace(StringRef Name, const DIE &Die);
246 /// getDIE - Returns the debug information entry map slot for the
247 /// specified debug variable. We delegate the request to DwarfDebug
248 /// when the MDNode can be part of the type system, since DIEs for
249 /// the type system can be shared across CUs and the mappings are
250 /// kept in DwarfDebug.
251 DIE *getDIE(DIDescriptor D) const;
253 /// getDIELoc - Returns a fresh newly allocated DIELoc.
254 DIELoc *getDIELoc() { return new (DIEValueAllocator) DIELoc(); }
256 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
257 /// when the MDNode can be part of the type system, since DIEs for
258 /// the type system can be shared across CUs and the mappings are
259 /// kept in DwarfDebug.
260 void insertDIE(DIDescriptor Desc, DIE *D);
262 /// addFlag - Add a flag that is true to the DIE.
263 void addFlag(DIE &Die, dwarf::Attribute Attribute);
265 /// addUInt - Add an unsigned integer attribute data and value.
266 void addUInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
267 uint64_t Integer);
269 void addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer);
271 /// addSInt - Add an signed integer attribute data and value.
272 void addSInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
273 int64_t Integer);
275 void addSInt(DIELoc &Die, Optional<dwarf::Form> Form, int64_t Integer);
277 /// addString - Add a string attribute data and value.
278 void addString(DIE &Die, dwarf::Attribute Attribute, const StringRef Str);
280 /// addLocalString - Add a string attribute data and value.
281 void addLocalString(DIE &Die, dwarf::Attribute Attribute,
282 const StringRef Str);
284 /// addExpr - Add a Dwarf expression attribute data and value.
285 void addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr);
287 /// addLabel - Add a Dwarf label attribute data and value.
288 void addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form,
289 const MCSymbol *Label);
291 void addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label);
293 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
294 void addLocationList(DIE &Die, dwarf::Attribute Attribute, unsigned Index);
296 /// addSectionLabel - Add a Dwarf section label attribute data and value.
297 ///
298 void addSectionLabel(DIE &Die, dwarf::Attribute Attribute,
299 const MCSymbol *Label);
301 /// addSectionOffset - Add an offset into a section attribute data and value.
302 ///
303 void addSectionOffset(DIE &Die, dwarf::Attribute Attribute, uint64_t Integer);
305 /// addOpAddress - Add a dwarf op address data and value using the
306 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
307 void addOpAddress(DIELoc &Die, const MCSymbol *Label);
309 /// addSectionDelta - Add a label delta attribute data and value.
310 void addSectionDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
311 const MCSymbol *Lo);
313 /// addLabelDelta - Add a label delta attribute data and value.
314 void addLabelDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
315 const MCSymbol *Lo);
317 /// addDIEEntry - Add a DIE attribute data and value.
318 void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry);
320 /// addDIEEntry - Add a DIE attribute data and value.
321 void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIEEntry *Entry);
323 void addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type);
325 /// addBlock - Add block data.
326 void addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Block);
328 /// addBlock - Add block data.
329 void addBlock(DIE &Die, dwarf::Attribute Attribute, DIEBlock *Block);
331 /// addSourceLine - Add location information to specified debug information
332 /// entry.
333 void addSourceLine(DIE &Die, unsigned Line, StringRef File,
334 StringRef Directory);
335 void addSourceLine(DIE &Die, DIVariable V);
336 void addSourceLine(DIE &Die, DIGlobalVariable G);
337 void addSourceLine(DIE &Die, DISubprogram SP);
338 void addSourceLine(DIE &Die, DIType Ty);
339 void addSourceLine(DIE &Die, DINameSpace NS);
340 void addSourceLine(DIE &Die, DIObjCProperty Ty);
342 /// addAddress - Add an address attribute to a die based on the location
343 /// provided.
344 void addAddress(DIE &Die, dwarf::Attribute Attribute,
345 const MachineLocation &Location, bool Indirect = false);
347 /// addConstantValue - Add constant value entry in variable DIE.
348 void addConstantValue(DIE &Die, const MachineOperand &MO, DIType Ty);
349 void addConstantValue(DIE &Die, const ConstantInt *CI, DIType Ty);
350 void addConstantValue(DIE &Die, const APInt &Val, DIType Ty);
351 void addConstantValue(DIE &Die, const APInt &Val, bool Unsigned);
352 void addConstantValue(DIE &Die, bool Unsigned, uint64_t Val);
354 /// addConstantFPValue - Add constant value entry in variable DIE.
355 void addConstantFPValue(DIE &Die, const MachineOperand &MO);
356 void addConstantFPValue(DIE &Die, const ConstantFP *CFP);
358 /// addTemplateParams - Add template parameters in buffer.
359 void addTemplateParams(DIE &Buffer, DIArray TParams);
361 /// addRegisterOp - Add register operand.
362 void addRegisterOpPiece(DIELoc &TheDie, unsigned Reg,
363 unsigned SizeInBits = 0, unsigned OffsetInBits = 0);
365 /// addRegisterOffset - Add register offset.
366 void addRegisterOffset(DIELoc &TheDie, unsigned Reg, int64_t Offset);
368 /// addComplexAddress - Start with the address based on the location provided,
369 /// and generate the DWARF information necessary to find the actual variable
370 /// (navigating the extra location information encoded in the type) based on
371 /// the starting location. Add the DWARF information to the die.
372 void addComplexAddress(const DbgVariable &DV, DIE &Die,
373 dwarf::Attribute Attribute,
374 const MachineLocation &Location);
376 // FIXME: Should be reformulated in terms of addComplexAddress.
377 /// addBlockByrefAddress - Start with the address based on the location
378 /// provided, and generate the DWARF information necessary to find the
379 /// actual Block variable (navigating the Block struct) based on the
380 /// starting location. Add the DWARF information to the die. Obsolete,
381 /// please use addComplexAddress instead.
382 void addBlockByrefAddress(const DbgVariable &DV, DIE &Die,
383 dwarf::Attribute Attribute,
384 const MachineLocation &Location);
386 /// addVariableAddress - Add DW_AT_location attribute for a
387 /// DbgVariable based on provided MachineLocation.
388 void addVariableAddress(const DbgVariable &DV, DIE &Die,
389 MachineLocation Location);
391 /// addType - Add a new type attribute to the specified entity. This takes
392 /// and attribute parameter because DW_AT_friend attributes are also
393 /// type references.
394 void addType(DIE &Entity, DIType Ty,
395 dwarf::Attribute Attribute = dwarf::DW_AT_type);
397 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
398 DIE *getOrCreateNameSpace(DINameSpace NS);
400 /// getOrCreateSubprogramDIE - Create new DIE using SP.
401 DIE *getOrCreateSubprogramDIE(DISubprogram SP);
403 void applySubprogramAttributes(DISubprogram SP, DIE &SPDie);
404 void applySubprogramAttributesToDefinition(DISubprogram SP, DIE &SPDie);
405 void applyVariableAttributes(const DbgVariable &Var, DIE &VariableDie);
407 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
408 /// given DIType.
409 DIE *getOrCreateTypeDIE(const MDNode *N);
411 /// getOrCreateContextDIE - Get context owner's DIE.
412 DIE *createTypeDIE(DICompositeType Ty);
414 /// getOrCreateContextDIE - Get context owner's DIE.
415 DIE *getOrCreateContextDIE(DIScope Context);
417 /// constructContainingTypeDIEs - Construct DIEs for types that contain
418 /// vtables.
419 void constructContainingTypeDIEs();
421 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
422 std::unique_ptr<DIE> constructVariableDIE(DbgVariable &DV,
423 bool Abstract = false);
425 /// constructSubprogramArguments - Construct function argument DIEs.
426 void constructSubprogramArguments(DIE &Buffer, DITypeArray Args);
428 /// Create a DIE with the given Tag, add the DIE to its parent, and
429 /// call insertDIE if MD is not null.
430 DIE &createAndAddDIE(unsigned Tag, DIE &Parent,
431 DIDescriptor N = DIDescriptor());
433 /// Compute the size of a header for this unit, not including the initial
434 /// length field.
435 virtual unsigned getHeaderSize() const {
436 return sizeof(int16_t) + // DWARF version number
437 sizeof(int32_t) + // Offset Into Abbrev. Section
438 sizeof(int8_t); // Pointer Size (in bytes)
439 }
441 /// Emit the header for this unit, not including the initial length field.
442 virtual void emitHeader(const MCSymbol *ASectionSym) const;
444 virtual DwarfCompileUnit &getCU() = 0;
446 /// constructTypeDIE - Construct type DIE from DICompositeType.
447 void constructTypeDIE(DIE &Buffer, DICompositeType CTy);
449 protected:
450 /// getOrCreateStaticMemberDIE - Create new static data member DIE.
451 DIE *getOrCreateStaticMemberDIE(DIDerivedType DT);
453 /// Look up the source ID with the given directory and source file names. If
454 /// none currently exists, create a new ID and insert it in the line table.
455 virtual unsigned getOrCreateSourceID(StringRef File, StringRef Directory) = 0;
457 private:
458 /// \brief Construct a DIE for the given DbgVariable without initializing the
459 /// DbgVariable's DIE reference.
460 std::unique_ptr<DIE> constructVariableDIEImpl(const DbgVariable &DV,
461 bool Abstract);
463 /// constructTypeDIE - Construct basic type die from DIBasicType.
464 void constructTypeDIE(DIE &Buffer, DIBasicType BTy);
466 /// constructTypeDIE - Construct derived type die from DIDerivedType.
467 void constructTypeDIE(DIE &Buffer, DIDerivedType DTy);
469 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
470 void constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy);
472 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
473 void constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy);
475 /// constructEnumTypeDIE - Construct enum type DIE from DIEnumerator.
476 void constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy);
478 /// constructMemberDIE - Construct member DIE from DIDerivedType.
479 void constructMemberDIE(DIE &Buffer, DIDerivedType DT);
481 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
482 /// DITemplateTypeParameter.
483 void constructTemplateTypeParameterDIE(DIE &Buffer,
484 DITemplateTypeParameter TP);
486 /// constructTemplateValueParameterDIE - Construct new DIE for the given
487 /// DITemplateValueParameter.
488 void constructTemplateValueParameterDIE(DIE &Buffer,
489 DITemplateValueParameter TVP);
491 /// getLowerBoundDefault - Return the default lower bound for an array. If the
492 /// DWARF version doesn't handle the language, return -1.
493 int64_t getDefaultLowerBound() const;
495 /// getDIEEntry - Returns the debug information entry for the specified
496 /// debug variable.
497 DIEEntry *getDIEEntry(const MDNode *N) const {
498 return MDNodeToDIEEntryMap.lookup(N);
499 }
501 /// insertDIEEntry - Insert debug information entry into the map.
502 void insertDIEEntry(const MDNode *N, DIEEntry *E) {
503 MDNodeToDIEEntryMap.insert(std::make_pair(N, E));
504 }
506 // getIndexTyDie - Get an anonymous type for index type.
507 DIE *getIndexTyDie() { return IndexTyDie; }
509 // setIndexTyDie - Set D as anonymous type for index which can be reused
510 // later.
511 void setIndexTyDie(DIE *D) { IndexTyDie = D; }
513 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
514 /// information entry.
515 DIEEntry *createDIEEntry(DIE &Entry);
517 /// resolve - Look in the DwarfDebug map for the MDNode that
518 /// corresponds to the reference.
519 template <typename T> T resolve(DIRef<T> Ref) const {
520 return DD->resolve(Ref);
521 }
523 /// If this is a named finished type then include it in the list of types for
524 /// the accelerator tables.
525 void updateAcceleratorTables(DIScope Context, DIType Ty, const DIE &TyDIE);
526 };
528 class DwarfCompileUnit : public DwarfUnit {
529 /// The attribute index of DW_AT_stmt_list in the compile unit DIE, avoiding
530 /// the need to search for it in applyStmtList.
531 unsigned stmtListIndex;
533 public:
534 DwarfCompileUnit(unsigned UID, DICompileUnit Node, AsmPrinter *A,
535 DwarfDebug *DW, DwarfFile *DWU);
537 void initStmtList(MCSymbol *DwarfLineSectionSym);
539 /// Apply the DW_AT_stmt_list from this compile unit to the specified DIE.
540 void applyStmtList(DIE &D);
542 /// createGlobalVariableDIE - create global variable DIE.
543 void createGlobalVariableDIE(DIGlobalVariable GV);
545 /// addLabelAddress - Add a dwarf label attribute data and value using
546 /// either DW_FORM_addr or DW_FORM_GNU_addr_index.
547 void addLabelAddress(DIE &Die, dwarf::Attribute Attribute,
548 const MCSymbol *Label);
550 /// addLocalLabelAddress - Add a dwarf label attribute data and value using
551 /// DW_FORM_addr only.
552 void addLocalLabelAddress(DIE &Die, dwarf::Attribute Attribute,
553 const MCSymbol *Label);
555 DwarfCompileUnit &getCU() override { return *this; }
557 unsigned getOrCreateSourceID(StringRef FileName, StringRef DirName) override;
558 };
560 class DwarfTypeUnit : public DwarfUnit {
561 private:
562 uint64_t TypeSignature;
563 const DIE *Ty;
564 DwarfCompileUnit &CU;
565 MCDwarfDwoLineTable *SplitLineTable;
567 public:
568 DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A,
569 DwarfDebug *DW, DwarfFile *DWU,
570 MCDwarfDwoLineTable *SplitLineTable = nullptr);
572 void setTypeSignature(uint64_t Signature) { TypeSignature = Signature; }
573 uint64_t getTypeSignature() const { return TypeSignature; }
574 void setType(const DIE *Ty) { this->Ty = Ty; }
576 /// Emit the header for this unit, not including the initial length field.
577 void emitHeader(const MCSymbol *ASectionSym) const override;
578 unsigned getHeaderSize() const override {
579 return DwarfUnit::getHeaderSize() + sizeof(uint64_t) + // Type Signature
580 sizeof(uint32_t); // Type DIE Offset
581 }
582 void initSection(const MCSection *Section);
583 // Bring in the base function (taking two args, including the section symbol)
584 // for use when building DWO type units (they don't go in unique comdat
585 // sections)
586 using DwarfUnit::initSection;
587 DwarfCompileUnit &getCU() override { return CU; }
589 protected:
590 unsigned getOrCreateSourceID(StringRef File, StringRef Directory) override;
591 };
592 } // end llvm namespace
593 #endif