DebugInfo: Simplify solution to avoid DW_AT_artificial on inlined parameters.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfUnit.h
1 //===-- llvm/CodeGen/DwarfUnit.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
15 #define CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
17 #include "DIE.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/DenseMap.h"
20 #include "llvm/ADT/Optional.h"
21 #include "llvm/ADT/StringMap.h"
22 #include "llvm/CodeGen/AsmPrinter.h"
23 #include "llvm/IR/DIBuilder.h"
24 #include "llvm/IR/DebugInfo.h"
25 #include "llvm/MC/MCExpr.h"
26 #include "llvm/MC/MCSection.h"
27 #include "llvm/MC/MCDwarf.h"
29 namespace llvm {
31 class MachineLocation;
32 class MachineOperand;
33 class ConstantInt;
34 class ConstantFP;
35 class DbgVariable;
36 class DwarfCompileUnit;
38 // Data structure to hold a range for range lists.
39 class RangeSpan {
40 public:
41   RangeSpan(MCSymbol *S, MCSymbol *E) : Start(S), End(E) {}
42   const MCSymbol *getStart() const { return Start; }
43   const MCSymbol *getEnd() const { return End; }
44   void setEnd(const MCSymbol *E) { End = E; }
46 private:
47   const MCSymbol *Start, *End;
48 };
50 class RangeSpanList {
51 private:
52   // Index for locating within the debug_range section this particular span.
53   MCSymbol *RangeSym;
54   // List of ranges.
55   SmallVector<RangeSpan, 2> Ranges;
57 public:
58   RangeSpanList(MCSymbol *Sym) : RangeSym(Sym) {}
59   MCSymbol *getSym() const { return RangeSym; }
60   const SmallVectorImpl<RangeSpan> &getRanges() const { return Ranges; }
61   void addRange(RangeSpan Range) { Ranges.push_back(Range); }
62 };
64 //===----------------------------------------------------------------------===//
65 /// Unit - This dwarf writer support class manages information associated
66 /// with a source file.
67 class DwarfUnit {
68 protected:
69   /// UniqueID - a numeric ID unique among all CUs in the module
70   unsigned UniqueID;
72   /// Node - MDNode for the compile unit.
73   DICompileUnit CUNode;
75   /// Unit debug information entry.
76   DIE UnitDie;
78   /// Offset of the UnitDie from beginning of debug info section.
79   unsigned DebugInfoOffset;
81   /// Asm - Target of Dwarf emission.
82   AsmPrinter *Asm;
84   // Holders for some common dwarf information.
85   DwarfDebug *DD;
86   DwarfFile *DU;
88   /// IndexTyDie - An anonymous type for index type.  Owned by UnitDie.
89   DIE *IndexTyDie;
91   /// MDNodeToDieMap - Tracks the mapping of unit level debug information
92   /// variables to debug information entries.
93   DenseMap<const MDNode *, DIE *> MDNodeToDieMap;
95   /// MDNodeToDIEEntryMap - Tracks the mapping of unit level debug information
96   /// descriptors to debug information entries using a DIEEntry proxy.
97   DenseMap<const MDNode *, DIEEntry *> MDNodeToDIEEntryMap;
99   /// GlobalNames - A map of globally visible named entities for this unit.
100   StringMap<const DIE *> GlobalNames;
102   /// GlobalTypes - A map of globally visible types for this unit.
103   StringMap<const DIE *> GlobalTypes;
105   /// DIEBlocks - A list of all the DIEBlocks in use.
106   std::vector<DIEBlock *> DIEBlocks;
107   
108   /// DIELocs - A list of all the DIELocs in use.
109   std::vector<DIELoc *> DIELocs;
111   /// ContainingTypeMap - This map is used to keep track of subprogram DIEs that
112   /// need DW_AT_containing_type attribute. This attribute points to a DIE that
113   /// corresponds to the MDNode mapped with the subprogram DIE.
114   DenseMap<DIE *, const MDNode *> ContainingTypeMap;
116   // List of ranges for a given compile unit.
117   SmallVector<RangeSpan, 1> CURanges;
119   // List of range lists for a given compile unit, separate from the ranges for
120   // the CU itself.
121   SmallVector<RangeSpanList, 1> CURangeLists;
123   // DIEValueAllocator - All DIEValues are allocated through this allocator.
124   BumpPtrAllocator DIEValueAllocator;
126   // DIEIntegerOne - A preallocated DIEValue because 1 is used frequently.
127   DIEInteger *DIEIntegerOne;
129   /// The section this unit will be emitted in.
130   const MCSection *Section;
132   /// A label at the start of the non-dwo section related to this unit.
133   MCSymbol *SectionSym;
135   /// The start of the unit within its section.
136   MCSymbol *LabelBegin;
138   /// The end of the unit within its section.
139   MCSymbol *LabelEnd;
141   /// Skeleton unit associated with this unit.
142   DwarfUnit *Skeleton;
144   DwarfUnit(unsigned UID, dwarf::Tag, DICompileUnit CU, AsmPrinter *A,
145             DwarfDebug *DW, DwarfFile *DWU);
147 public:
148   virtual ~DwarfUnit();
150   /// Set the skeleton unit associated with this unit.
151   void setSkeleton(DwarfUnit &Skel) { Skeleton = &Skel; }
153   /// Get the skeleton unit associated with this unit.
154   DwarfUnit *getSkeleton() const { return Skeleton; }
156   /// Pass in the SectionSym even though we could recreate it in every compile
157   /// unit (type units will have actually distinct symbols once they're in
158   /// comdat sections).
159   void initSection(const MCSection *Section, MCSymbol *SectionSym) {
160     assert(!this->Section);
161     this->Section = Section;
162     this->SectionSym = SectionSym;
163     this->LabelBegin =
164         Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
165     this->LabelEnd =
166         Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
167   }
169   const MCSection *getSection() const {
170     assert(Section);
171     return Section;
172   }
174   /// If there's a skeleton then return the section symbol for the skeleton
175   /// unit, otherwise return the section symbol for this unit.
176   MCSymbol *getLocalSectionSym() const {
177     if (Skeleton)
178       return Skeleton->getSectionSym();
179     return getSectionSym();
180   }
182   MCSymbol *getSectionSym() const {
183     assert(Section);
184     return SectionSym;
185   }
187   /// If there's a skeleton then return the begin label for the skeleton unit,
188   /// otherwise return the local label for this unit.
189   MCSymbol *getLocalLabelBegin() const {
190     if (Skeleton)
191       return Skeleton->getLabelBegin();
192     return getLabelBegin();
193   }
195   MCSymbol *getLabelBegin() const {
196     assert(Section);
197     return LabelBegin;
198   }
200   MCSymbol *getLabelEnd() const {
201     assert(Section);
202     return LabelEnd;
203   }
205   // Accessors.
206   unsigned getUniqueID() const { return UniqueID; }
207   uint16_t getLanguage() const { return CUNode.getLanguage(); }
208   DICompileUnit getCUNode() const { return CUNode; }
209   DIE &getUnitDie() { return UnitDie; }
210   const StringMap<const DIE *> &getGlobalNames() const { return GlobalNames; }
211   const StringMap<const DIE *> &getGlobalTypes() const { return GlobalTypes; }
213   unsigned getDebugInfoOffset() const { return DebugInfoOffset; }
214   void setDebugInfoOffset(unsigned DbgInfoOff) { DebugInfoOffset = DbgInfoOff; }
216   /// hasContent - Return true if this compile unit has something to write out.
217   bool hasContent() const { return !UnitDie.getChildren().empty(); }
219   /// addRange - Add an address range to the list of ranges for this unit.
220   void addRange(RangeSpan Range);
222   /// getRanges - Get the list of ranges for this unit.
223   const SmallVectorImpl<RangeSpan> &getRanges() const { return CURanges; }
224   SmallVectorImpl<RangeSpan> &getRanges() { return CURanges; }
226   /// addRangeList - Add an address range list to the list of range lists.
227   void addRangeList(RangeSpanList Ranges) { CURangeLists.push_back(Ranges); }
229   /// getRangeLists - Get the vector of range lists.
230   const SmallVectorImpl<RangeSpanList> &getRangeLists() const {
231     return CURangeLists;
232   }
233   SmallVectorImpl<RangeSpanList> &getRangeLists() { return CURangeLists; }
235   /// getParentContextString - Get a string containing the language specific
236   /// context for a global name.
237   std::string getParentContextString(DIScope Context) const;
239   /// addGlobalName - Add a new global entity to the compile unit.
240   ///
241   void addGlobalName(StringRef Name, DIE &Die, DIScope Context);
243   /// addAccelNamespace - Add a new name to the namespace accelerator table.
244   void addAccelNamespace(StringRef Name, const DIE &Die);
246   /// getDIE - Returns the debug information entry map slot for the
247   /// specified debug variable. We delegate the request to DwarfDebug
248   /// when the MDNode can be part of the type system, since DIEs for
249   /// the type system can be shared across CUs and the mappings are
250   /// kept in DwarfDebug.
251   DIE *getDIE(DIDescriptor D) const;
253   /// getDIELoc - Returns a fresh newly allocated DIELoc.
254   DIELoc *getDIELoc() { return new (DIEValueAllocator) DIELoc(); }
256   /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
257   /// when the MDNode can be part of the type system, since DIEs for
258   /// the type system can be shared across CUs and the mappings are
259   /// kept in DwarfDebug.
260   void insertDIE(DIDescriptor Desc, DIE *D);
262   /// addFlag - Add a flag that is true to the DIE.
263   void addFlag(DIE &Die, dwarf::Attribute Attribute);
265   /// addUInt - Add an unsigned integer attribute data and value.
266   void addUInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
267                uint64_t Integer);
269   void addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer);
271   /// addSInt - Add an signed integer attribute data and value.
272   void addSInt(DIE &Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
273                int64_t Integer);
275   void addSInt(DIELoc &Die, Optional<dwarf::Form> Form, int64_t Integer);
277   /// addString - Add a string attribute data and value.
278   void addString(DIE &Die, dwarf::Attribute Attribute, const StringRef Str);
280   /// addLocalString - Add a string attribute data and value.
281   void addLocalString(DIE &Die, dwarf::Attribute Attribute,
282                       const StringRef Str);
284   /// addExpr - Add a Dwarf expression attribute data and value.
285   void addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr);
287   /// addLabel - Add a Dwarf label attribute data and value.
288   void addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form,
289                 const MCSymbol *Label);
291   void addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label);
293   /// addLocationList - Add a Dwarf loclistptr attribute data and value.
294   void addLocationList(DIE &Die, dwarf::Attribute Attribute, unsigned Index);
296   /// addSectionLabel - Add a Dwarf section label attribute data and value.
297   ///
298   void addSectionLabel(DIE &Die, dwarf::Attribute Attribute,
299                        const MCSymbol *Label);
301   /// addSectionOffset - Add an offset into a section attribute data and value.
302   ///
303   void addSectionOffset(DIE &Die, dwarf::Attribute Attribute, uint64_t Integer);
305   /// addOpAddress - Add a dwarf op address data and value using the
306   /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
307   void addOpAddress(DIELoc &Die, const MCSymbol *Label);
309   /// addSectionDelta - Add a label delta attribute data and value.
310   void addSectionDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
311                        const MCSymbol *Lo);
313   /// addLabelDelta - Add a label delta attribute data and value.
314   void addLabelDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
315                      const MCSymbol *Lo);
317   /// addDIEEntry - Add a DIE attribute data and value.
318   void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry);
320   /// addDIEEntry - Add a DIE attribute data and value.
321   void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIEEntry *Entry);
323   void addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type);
325   /// addBlock - Add block data.
326   void addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Block);
328   /// addBlock - Add block data.
329   void addBlock(DIE &Die, dwarf::Attribute Attribute, DIEBlock *Block);
331   /// addSourceLine - Add location information to specified debug information
332   /// entry.
333   void addSourceLine(DIE &Die, unsigned Line, StringRef File,
334                      StringRef Directory);
335   void addSourceLine(DIE &Die, DIVariable V);
336   void addSourceLine(DIE &Die, DIGlobalVariable G);
337   void addSourceLine(DIE &Die, DISubprogram SP);
338   void addSourceLine(DIE &Die, DIType Ty);
339   void addSourceLine(DIE &Die, DINameSpace NS);
340   void addSourceLine(DIE &Die, DIObjCProperty Ty);
342   /// addAddress - Add an address attribute to a die based on the location
343   /// provided.
344   void addAddress(DIE &Die, dwarf::Attribute Attribute,
345                   const MachineLocation &Location, bool Indirect = false);
347   /// addConstantValue - Add constant value entry in variable DIE.
348   void addConstantValue(DIE &Die, const MachineOperand &MO, DIType Ty);
349   void addConstantValue(DIE &Die, const ConstantInt *CI, DIType Ty);
350   void addConstantValue(DIE &Die, const APInt &Val, DIType Ty);
351   void addConstantValue(DIE &Die, const APInt &Val, bool Unsigned);
352   void addConstantValue(DIE &Die, bool Unsigned, uint64_t Val);
354   /// addConstantFPValue - Add constant value entry in variable DIE.
355   void addConstantFPValue(DIE &Die, const MachineOperand &MO);
356   void addConstantFPValue(DIE &Die, const ConstantFP *CFP);
358   /// addTemplateParams - Add template parameters in buffer.
359   void addTemplateParams(DIE &Buffer, DIArray TParams);
361   /// addRegisterOp - Add register operand.
362   void addRegisterOp(DIELoc &TheDie, unsigned Reg);
364   /// addRegisterOffset - Add register offset.
365   void addRegisterOffset(DIELoc &TheDie, unsigned Reg, int64_t Offset);
367   /// addComplexAddress - Start with the address based on the location provided,
368   /// and generate the DWARF information necessary to find the actual variable
369   /// (navigating the extra location information encoded in the type) based on
370   /// the starting location.  Add the DWARF information to the die.
371   void addComplexAddress(const DbgVariable &DV, DIE &Die,
372                          dwarf::Attribute Attribute,
373                          const MachineLocation &Location);
375   // FIXME: Should be reformulated in terms of addComplexAddress.
376   /// addBlockByrefAddress - Start with the address based on the location
377   /// provided, and generate the DWARF information necessary to find the
378   /// actual Block variable (navigating the Block struct) based on the
379   /// starting location.  Add the DWARF information to the die.  Obsolete,
380   /// please use addComplexAddress instead.
381   void addBlockByrefAddress(const DbgVariable &DV, DIE &Die,
382                             dwarf::Attribute Attribute,
383                             const MachineLocation &Location);
385   /// addVariableAddress - Add DW_AT_location attribute for a
386   /// DbgVariable based on provided MachineLocation.
387   void addVariableAddress(const DbgVariable &DV, DIE &Die,
388                           MachineLocation Location);
390   /// addType - Add a new type attribute to the specified entity. This takes
391   /// and attribute parameter because DW_AT_friend attributes are also
392   /// type references.
393   void addType(DIE &Entity, DIType Ty,
394                dwarf::Attribute Attribute = dwarf::DW_AT_type);
396   /// getOrCreateNameSpace - Create a DIE for DINameSpace.
397   DIE *getOrCreateNameSpace(DINameSpace NS);
399   /// getOrCreateSubprogramDIE - Create new DIE using SP.
400   DIE *getOrCreateSubprogramDIE(DISubprogram SP);
402   void applySubprogramAttributes(DISubprogram SP, DIE &SPDie);
404   /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
405   /// given DIType.
406   DIE *getOrCreateTypeDIE(const MDNode *N);
408   /// getOrCreateContextDIE - Get context owner's DIE.
409   DIE *createTypeDIE(DICompositeType Ty);
411   /// getOrCreateContextDIE - Get context owner's DIE.
412   DIE *getOrCreateContextDIE(DIScope Context);
414   /// constructContainingTypeDIEs - Construct DIEs for types that contain
415   /// vtables.
416   void constructContainingTypeDIEs();
418   /// constructVariableDIE - Construct a DIE for the given DbgVariable.
419   std::unique_ptr<DIE> constructVariableDIE(DbgVariable &DV,
420                                             bool Abstract = false);
422   /// constructSubprogramArguments - Construct function argument DIEs.
423   void constructSubprogramArguments(DIE &Buffer, DIArray Args);
425   /// Create a DIE with the given Tag, add the DIE to its parent, and
426   /// call insertDIE if MD is not null.
427   DIE &createAndAddDIE(unsigned Tag, DIE &Parent,
428                        DIDescriptor N = DIDescriptor());
430   /// Compute the size of a header for this unit, not including the initial
431   /// length field.
432   virtual unsigned getHeaderSize() const {
433     return sizeof(int16_t) + // DWARF version number
434            sizeof(int32_t) + // Offset Into Abbrev. Section
435            sizeof(int8_t);   // Pointer Size (in bytes)
436   }
438   /// Emit the header for this unit, not including the initial length field.
439   virtual void emitHeader(const MCSymbol *ASectionSym) const;
441   virtual DwarfCompileUnit &getCU() = 0;
443   /// constructTypeDIE - Construct type DIE from DICompositeType.
444   void constructTypeDIE(DIE &Buffer, DICompositeType CTy);
446 protected:
447   /// getOrCreateStaticMemberDIE - Create new static data member DIE.
448   DIE *getOrCreateStaticMemberDIE(DIDerivedType DT);
450   /// Look up the source ID with the given directory and source file names. If
451   /// none currently exists, create a new ID and insert it in the line table.
452   virtual unsigned getOrCreateSourceID(StringRef File, StringRef Directory) = 0;
454 private:
455   /// \brief Construct a DIE for the given DbgVariable without initializing the
456   /// DbgVariable's DIE reference.
457   std::unique_ptr<DIE> constructVariableDIEImpl(const DbgVariable &DV,
458                                                 bool Abstract);
460   /// constructTypeDIE - Construct basic type die from DIBasicType.
461   void constructTypeDIE(DIE &Buffer, DIBasicType BTy);
463   /// constructTypeDIE - Construct derived type die from DIDerivedType.
464   void constructTypeDIE(DIE &Buffer, DIDerivedType DTy);
466   /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
467   void constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy);
469   /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
470   void constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy);
472   /// constructEnumTypeDIE - Construct enum type DIE from DIEnumerator.
473   void constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy);
475   /// constructMemberDIE - Construct member DIE from DIDerivedType.
476   void constructMemberDIE(DIE &Buffer, DIDerivedType DT);
478   /// constructTemplateTypeParameterDIE - Construct new DIE for the given
479   /// DITemplateTypeParameter.
480   void constructTemplateTypeParameterDIE(DIE &Buffer,
481                                          DITemplateTypeParameter TP);
483   /// constructTemplateValueParameterDIE - Construct new DIE for the given
484   /// DITemplateValueParameter.
485   void constructTemplateValueParameterDIE(DIE &Buffer,
486                                           DITemplateValueParameter TVP);
488   /// getLowerBoundDefault - Return the default lower bound for an array. If the
489   /// DWARF version doesn't handle the language, return -1.
490   int64_t getDefaultLowerBound() const;
492   /// getDIEEntry - Returns the debug information entry for the specified
493   /// debug variable.
494   DIEEntry *getDIEEntry(const MDNode *N) const {
495     return MDNodeToDIEEntryMap.lookup(N);
496   }
498   /// insertDIEEntry - Insert debug information entry into the map.
499   void insertDIEEntry(const MDNode *N, DIEEntry *E) {
500     MDNodeToDIEEntryMap.insert(std::make_pair(N, E));
501   }
503   // getIndexTyDie - Get an anonymous type for index type.
504   DIE *getIndexTyDie() { return IndexTyDie; }
506   // setIndexTyDie - Set D as anonymous type for index which can be reused
507   // later.
508   void setIndexTyDie(DIE *D) { IndexTyDie = D; }
510   /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
511   /// information entry.
512   DIEEntry *createDIEEntry(DIE &Entry);
514   /// resolve - Look in the DwarfDebug map for the MDNode that
515   /// corresponds to the reference.
516   template <typename T> T resolve(DIRef<T> Ref) const {
517     return DD->resolve(Ref);
518   }
520   /// If this is a named finished type then include it in the list of types for
521   /// the accelerator tables.
522   void updateAcceleratorTables(DIScope Context, DIType Ty, const DIE &TyDIE);
523 };
525 class DwarfCompileUnit : public DwarfUnit {
526   /// The attribute index of DW_AT_stmt_list in the compile unit DIE, avoiding
527   /// the need to search for it in applyStmtList.
528   unsigned stmtListIndex;
530 public:
531   DwarfCompileUnit(unsigned UID, DICompileUnit Node, AsmPrinter *A,
532                    DwarfDebug *DW, DwarfFile *DWU);
534   void initStmtList(MCSymbol *DwarfLineSectionSym);
536   /// Apply the DW_AT_stmt_list from this compile unit to the specified DIE.
537   void applyStmtList(DIE &D);
539   /// createGlobalVariableDIE - create global variable DIE.
540   void createGlobalVariableDIE(DIGlobalVariable GV);
542   /// addLabelAddress - Add a dwarf label attribute data and value using
543   /// either DW_FORM_addr or DW_FORM_GNU_addr_index.
544   void addLabelAddress(DIE &Die, dwarf::Attribute Attribute,
545                        const MCSymbol *Label);
547   /// addLocalLabelAddress - Add a dwarf label attribute data and value using
548   /// DW_FORM_addr only.
549   void addLocalLabelAddress(DIE &Die, dwarf::Attribute Attribute,
550                             const MCSymbol *Label);
552   DwarfCompileUnit &getCU() override { return *this; }
554   unsigned getOrCreateSourceID(StringRef FileName, StringRef DirName) override;
555 };
557 class DwarfTypeUnit : public DwarfUnit {
558 private:
559   uint64_t TypeSignature;
560   const DIE *Ty;
561   DwarfCompileUnit &CU;
562   MCDwarfDwoLineTable *SplitLineTable;
564 public:
565   DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A,
566                 DwarfDebug *DW, DwarfFile *DWU,
567                 MCDwarfDwoLineTable *SplitLineTable = nullptr);
569   void setTypeSignature(uint64_t Signature) { TypeSignature = Signature; }
570   uint64_t getTypeSignature() const { return TypeSignature; }
571   void setType(const DIE *Ty) { this->Ty = Ty; }
573   /// Emit the header for this unit, not including the initial length field.
574   void emitHeader(const MCSymbol *ASectionSym) const override;
575   unsigned getHeaderSize() const override {
576     return DwarfUnit::getHeaderSize() + sizeof(uint64_t) + // Type Signature
577            sizeof(uint32_t);                               // Type DIE Offset
578   }
579   void initSection(const MCSection *Section);
580   DwarfCompileUnit &getCU() override { return CU; }
582 protected:
583   unsigned getOrCreateSourceID(StringRef File, StringRef Directory) override;
584 };
585 } // end llvm namespace
586 #endif