1 //===-- llvm/CodeGen/DwarfUnit.h - Dwarf Compile Unit ---*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing dwarf compile unit.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
15 #define CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H
17 #include "DIE.h"
18 #include "DwarfDebug.h"
19 #include "llvm/ADT/DenseMap.h"
20 #include "llvm/ADT/Optional.h"
21 #include "llvm/ADT/StringMap.h"
22 #include "llvm/CodeGen/AsmPrinter.h"
23 #include "llvm/IR/DIBuilder.h"
24 #include "llvm/IR/DebugInfo.h"
25 #include "llvm/MC/MCExpr.h"
26 #include "llvm/MC/MCSection.h"
27 #include "llvm/MC/MCDwarf.h"
29 namespace llvm {
31 class MachineLocation;
32 class MachineOperand;
33 class ConstantInt;
34 class ConstantFP;
35 class DbgVariable;
36 class DwarfCompileUnit;
38 // Data structure to hold a range for range lists.
39 class RangeSpan {
40 public:
41 RangeSpan(MCSymbol *S, MCSymbol *E) : Start(S), End(E) {}
42 const MCSymbol *getStart() const { return Start; }
43 const MCSymbol *getEnd() const { return End; }
44 void setEnd(const MCSymbol *E) { End = E; }
46 private:
47 const MCSymbol *Start, *End;
48 };
50 class RangeSpanList {
51 private:
52 // Index for locating within the debug_range section this particular span.
53 MCSymbol *RangeSym;
54 // List of ranges.
55 SmallVector<RangeSpan, 2> Ranges;
57 public:
58 RangeSpanList(MCSymbol *Sym) : RangeSym(Sym) {}
59 MCSymbol *getSym() const { return RangeSym; }
60 const SmallVectorImpl<RangeSpan> &getRanges() const { return Ranges; }
61 void addRange(RangeSpan Range) { Ranges.push_back(Range); }
62 };
64 //===----------------------------------------------------------------------===//
65 /// Unit - This dwarf writer support class manages information associated
66 /// with a source file.
67 class DwarfUnit {
68 protected:
69 /// UniqueID - a numeric ID unique among all CUs in the module
70 unsigned UniqueID;
72 /// Node - MDNode for the compile unit.
73 DICompileUnit CUNode;
75 /// Unit debug information entry.
76 const std::unique_ptr<DIE> UnitDie;
78 /// Offset of the UnitDie from beginning of debug info section.
79 unsigned DebugInfoOffset;
81 /// Asm - Target of Dwarf emission.
82 AsmPrinter *Asm;
84 // Holders for some common dwarf information.
85 DwarfDebug *DD;
86 DwarfFile *DU;
88 /// IndexTyDie - An anonymous type for index type. Owned by UnitDie.
89 DIE *IndexTyDie;
91 /// MDNodeToDieMap - Tracks the mapping of unit level debug information
92 /// variables to debug information entries.
93 DenseMap<const MDNode *, DIE *> MDNodeToDieMap;
95 /// MDNodeToDIEEntryMap - Tracks the mapping of unit level debug information
96 /// descriptors to debug information entries using a DIEEntry proxy.
97 DenseMap<const MDNode *, DIEEntry *> MDNodeToDIEEntryMap;
99 /// GlobalNames - A map of globally visible named entities for this unit.
100 StringMap<const DIE *> GlobalNames;
102 /// GlobalTypes - A map of globally visible types for this unit.
103 StringMap<const DIE *> GlobalTypes;
105 /// DIEBlocks - A list of all the DIEBlocks in use.
106 std::vector<DIEBlock *> DIEBlocks;
108 /// DIELocs - A list of all the DIELocs in use.
109 std::vector<DIELoc *> DIELocs;
111 /// ContainingTypeMap - This map is used to keep track of subprogram DIEs that
112 /// need DW_AT_containing_type attribute. This attribute points to a DIE that
113 /// corresponds to the MDNode mapped with the subprogram DIE.
114 DenseMap<DIE *, const MDNode *> ContainingTypeMap;
116 // List of ranges for a given compile unit.
117 SmallVector<RangeSpan, 1> CURanges;
119 // List of range lists for a given compile unit, separate from the ranges for
120 // the CU itself.
121 SmallVector<RangeSpanList, 1> CURangeLists;
123 // DIEValueAllocator - All DIEValues are allocated through this allocator.
124 BumpPtrAllocator DIEValueAllocator;
126 // DIEIntegerOne - A preallocated DIEValue because 1 is used frequently.
127 DIEInteger *DIEIntegerOne;
129 /// The section this unit will be emitted in.
130 const MCSection *Section;
132 /// A label at the start of the non-dwo section related to this unit.
133 MCSymbol *SectionSym;
135 /// The start of the unit within its section.
136 MCSymbol *LabelBegin;
138 /// The end of the unit within its section.
139 MCSymbol *LabelEnd;
141 /// The label for the start of the range sets for the elements of this unit.
142 MCSymbol *LabelRange;
144 /// Skeleton unit associated with this unit.
145 DwarfUnit *Skeleton;
147 DwarfUnit(unsigned UID, DIE *D, DICompileUnit CU, AsmPrinter *A,
148 DwarfDebug *DW, DwarfFile *DWU);
150 public:
151 virtual ~DwarfUnit();
153 /// Set the skeleton unit associated with this unit.
154 void setSkeleton(DwarfUnit &Skel) { Skeleton = &Skel; }
156 /// Get the skeleton unit associated with this unit.
157 DwarfUnit *getSkeleton() const { return Skeleton; }
159 /// Pass in the SectionSym even though we could recreate it in every compile
160 /// unit (type units will have actually distinct symbols once they're in
161 /// comdat sections).
162 void initSection(const MCSection *Section, MCSymbol *SectionSym) {
163 assert(!this->Section);
164 this->Section = Section;
165 this->SectionSym = SectionSym;
166 this->LabelBegin =
167 Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
168 this->LabelEnd =
169 Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
170 this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
171 }
173 const MCSection *getSection() const {
174 assert(Section);
175 return Section;
176 }
178 /// If there's a skeleton then return the section symbol for the skeleton
179 /// unit, otherwise return the section symbol for this unit.
180 MCSymbol *getLocalSectionSym() const {
181 if (Skeleton)
182 return Skeleton->getSectionSym();
183 return getSectionSym();
184 }
186 MCSymbol *getSectionSym() const {
187 assert(Section);
188 return SectionSym;
189 }
191 /// If there's a skeleton then return the begin label for the skeleton unit,
192 /// otherwise return the local label for this unit.
193 MCSymbol *getLocalLabelBegin() const {
194 if (Skeleton)
195 return Skeleton->getLabelBegin();
196 return getLabelBegin();
197 }
199 MCSymbol *getLabelBegin() const {
200 assert(Section);
201 return LabelBegin;
202 }
204 MCSymbol *getLabelEnd() const {
205 assert(Section);
206 return LabelEnd;
207 }
209 MCSymbol *getLabelRange() const {
210 assert(Section);
211 return LabelRange;
212 }
214 // Accessors.
215 unsigned getUniqueID() const { return UniqueID; }
216 uint16_t getLanguage() const { return CUNode.getLanguage(); }
217 DICompileUnit getCUNode() const { return CUNode; }
218 DIE *getUnitDie() const { return UnitDie.get(); }
219 const StringMap<const DIE *> &getGlobalNames() const { return GlobalNames; }
220 const StringMap<const DIE *> &getGlobalTypes() const { return GlobalTypes; }
222 unsigned getDebugInfoOffset() const { return DebugInfoOffset; }
223 void setDebugInfoOffset(unsigned DbgInfoOff) { DebugInfoOffset = DbgInfoOff; }
225 /// hasContent - Return true if this compile unit has something to write out.
226 bool hasContent() const { return !UnitDie->getChildren().empty(); }
228 /// addRange - Add an address range to the list of ranges for this unit.
229 void addRange(RangeSpan Range);
231 /// getRanges - Get the list of ranges for this unit.
232 const SmallVectorImpl<RangeSpan> &getRanges() const { return CURanges; }
233 SmallVectorImpl<RangeSpan> &getRanges() { return CURanges; }
235 /// addRangeList - Add an address range list to the list of range lists.
236 void addRangeList(RangeSpanList Ranges) { CURangeLists.push_back(Ranges); }
238 /// getRangeLists - Get the vector of range lists.
239 const SmallVectorImpl<RangeSpanList> &getRangeLists() const {
240 return CURangeLists;
241 }
242 SmallVectorImpl<RangeSpanList> &getRangeLists() { return CURangeLists; }
244 /// getParentContextString - Get a string containing the language specific
245 /// context for a global name.
246 std::string getParentContextString(DIScope Context) const;
248 /// addGlobalName - Add a new global entity to the compile unit.
249 ///
250 void addGlobalName(StringRef Name, DIE *Die, DIScope Context);
252 /// addAccelNamespace - Add a new name to the namespace accelerator table.
253 void addAccelNamespace(StringRef Name, const DIE *Die);
255 /// getDIE - Returns the debug information entry map slot for the
256 /// specified debug variable. We delegate the request to DwarfDebug
257 /// when the MDNode can be part of the type system, since DIEs for
258 /// the type system can be shared across CUs and the mappings are
259 /// kept in DwarfDebug.
260 DIE *getDIE(DIDescriptor D) const;
262 /// getDIELoc - Returns a fresh newly allocated DIELoc.
263 DIELoc *getDIELoc() { return new (DIEValueAllocator) DIELoc(); }
265 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
266 /// when the MDNode can be part of the type system, since DIEs for
267 /// the type system can be shared across CUs and the mappings are
268 /// kept in DwarfDebug.
269 void insertDIE(DIDescriptor Desc, DIE *D);
271 /// addDie - Adds or interns the DIE to the compile unit.
272 ///
273 void addDie(DIE *Buffer) { UnitDie->addChild(Buffer); }
275 /// addFlag - Add a flag that is true to the DIE.
276 void addFlag(DIE *Die, dwarf::Attribute Attribute);
278 /// addUInt - Add an unsigned integer attribute data and value.
279 void addUInt(DIE *Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
280 uint64_t Integer);
282 void addUInt(DIE *Block, dwarf::Form Form, uint64_t Integer);
284 /// addSInt - Add an signed integer attribute data and value.
285 void addSInt(DIE *Die, dwarf::Attribute Attribute, Optional<dwarf::Form> Form,
286 int64_t Integer);
288 void addSInt(DIELoc *Die, Optional<dwarf::Form> Form, int64_t Integer);
290 /// addString - Add a string attribute data and value.
291 void addString(DIE *Die, dwarf::Attribute Attribute, const StringRef Str);
293 /// addLocalString - Add a string attribute data and value.
294 void addLocalString(DIE *Die, dwarf::Attribute Attribute,
295 const StringRef Str);
297 /// addExpr - Add a Dwarf expression attribute data and value.
298 void addExpr(DIELoc *Die, dwarf::Form Form, const MCExpr *Expr);
300 /// addLabel - Add a Dwarf label attribute data and value.
301 void addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
302 const MCSymbol *Label);
304 void addLabel(DIELoc *Die, dwarf::Form Form, const MCSymbol *Label);
306 /// addLocationList - Add a Dwarf loclistptr attribute data and value.
307 void addLocationList(DIE *Die, dwarf::Attribute Attribute, unsigned Index);
309 /// addSectionLabel - Add a Dwarf section label attribute data and value.
310 ///
311 void addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
312 const MCSymbol *Label);
314 /// addSectionOffset - Add an offset into a section attribute data and value.
315 ///
316 void addSectionOffset(DIE *Die, dwarf::Attribute Attribute, uint64_t Integer);
318 /// addOpAddress - Add a dwarf op address data and value using the
319 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
320 void addOpAddress(DIELoc *Die, const MCSymbol *Label);
322 /// addSectionDelta - Add a label delta attribute data and value.
323 void addSectionDelta(DIE *Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
324 const MCSymbol *Lo);
326 /// addLabelDelta - Add a label delta attribute data and value.
327 void addLabelDelta(DIE *Die, dwarf::Attribute Attribute, const MCSymbol *Hi,
328 const MCSymbol *Lo);
330 /// addDIEEntry - Add a DIE attribute data and value.
331 void addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry);
333 /// addDIEEntry - Add a DIE attribute data and value.
334 void addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIEEntry *Entry);
336 void addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type);
338 /// addBlock - Add block data.
339 void addBlock(DIE *Die, dwarf::Attribute Attribute, DIELoc *Block);
341 /// addBlock - Add block data.
342 void addBlock(DIE *Die, dwarf::Attribute Attribute, DIEBlock *Block);
344 /// addSourceLine - Add location information to specified debug information
345 /// entry.
346 void addSourceLine(DIE *Die, unsigned Line, StringRef File,
347 StringRef Directory);
348 void addSourceLine(DIE *Die, DIVariable V);
349 void addSourceLine(DIE *Die, DIGlobalVariable G);
350 void addSourceLine(DIE *Die, DISubprogram SP);
351 void addSourceLine(DIE *Die, DIType Ty);
352 void addSourceLine(DIE *Die, DINameSpace NS);
353 void addSourceLine(DIE *Die, DIObjCProperty Ty);
355 /// addAddress - Add an address attribute to a die based on the location
356 /// provided.
357 void addAddress(DIE *Die, dwarf::Attribute Attribute,
358 const MachineLocation &Location, bool Indirect = false);
360 /// addConstantValue - Add constant value entry in variable DIE.
361 void addConstantValue(DIE *Die, const MachineOperand &MO, DIType Ty);
362 void addConstantValue(DIE *Die, const ConstantInt *CI, bool Unsigned);
363 void addConstantValue(DIE *Die, const APInt &Val, bool Unsigned);
365 /// addConstantFPValue - Add constant value entry in variable DIE.
366 void addConstantFPValue(DIE *Die, const MachineOperand &MO);
367 void addConstantFPValue(DIE *Die, const ConstantFP *CFP);
369 /// addTemplateParams - Add template parameters in buffer.
370 void addTemplateParams(DIE &Buffer, DIArray TParams);
372 /// addRegisterOp - Add register operand.
373 void addRegisterOp(DIELoc *TheDie, unsigned Reg);
375 /// addRegisterOffset - Add register offset.
376 void addRegisterOffset(DIELoc *TheDie, unsigned Reg, int64_t Offset);
378 /// addComplexAddress - Start with the address based on the location provided,
379 /// and generate the DWARF information necessary to find the actual variable
380 /// (navigating the extra location information encoded in the type) based on
381 /// the starting location. Add the DWARF information to the die.
382 void addComplexAddress(const DbgVariable &DV, DIE *Die,
383 dwarf::Attribute Attribute,
384 const MachineLocation &Location);
386 // FIXME: Should be reformulated in terms of addComplexAddress.
387 /// addBlockByrefAddress - Start with the address based on the location
388 /// provided, and generate the DWARF information necessary to find the
389 /// actual Block variable (navigating the Block struct) based on the
390 /// starting location. Add the DWARF information to the die. Obsolete,
391 /// please use addComplexAddress instead.
392 void addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
393 dwarf::Attribute Attribute,
394 const MachineLocation &Location);
396 /// addVariableAddress - Add DW_AT_location attribute for a
397 /// DbgVariable based on provided MachineLocation.
398 void addVariableAddress(const DbgVariable &DV, DIE *Die,
399 MachineLocation Location);
401 /// addType - Add a new type attribute to the specified entity. This takes
402 /// and attribute parameter because DW_AT_friend attributes are also
403 /// type references.
404 void addType(DIE *Entity, DIType Ty,
405 dwarf::Attribute Attribute = dwarf::DW_AT_type);
407 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
408 DIE *getOrCreateNameSpace(DINameSpace NS);
410 /// getOrCreateSubprogramDIE - Create new DIE using SP.
411 DIE *getOrCreateSubprogramDIE(DISubprogram SP);
413 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
414 /// given DIType.
415 DIE *getOrCreateTypeDIE(const MDNode *N);
417 /// getOrCreateContextDIE - Get context owner's DIE.
418 DIE *createTypeDIE(DICompositeType Ty);
420 /// getOrCreateContextDIE - Get context owner's DIE.
421 DIE *getOrCreateContextDIE(DIScope Context);
423 /// constructContainingTypeDIEs - Construct DIEs for types that contain
424 /// vtables.
425 void constructContainingTypeDIEs();
427 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
428 DIE *constructVariableDIE(DbgVariable &DV, bool isScopeAbstract);
430 /// constructSubprogramArguments - Construct function argument DIEs.
431 void constructSubprogramArguments(DIE &Buffer, DIArray Args);
433 /// Create a DIE with the given Tag, add the DIE to its parent, and
434 /// call insertDIE if MD is not null.
435 DIE *createAndAddDIE(unsigned Tag, DIE &Parent,
436 DIDescriptor N = DIDescriptor());
438 /// Compute the size of a header for this unit, not including the initial
439 /// length field.
440 virtual unsigned getHeaderSize() const {
441 return sizeof(int16_t) + // DWARF version number
442 sizeof(int32_t) + // Offset Into Abbrev. Section
443 sizeof(int8_t); // Pointer Size (in bytes)
444 }
446 /// Emit the header for this unit, not including the initial length field.
447 virtual void emitHeader(const MCSymbol *ASectionSym) const;
449 virtual DwarfCompileUnit &getCU() = 0;
451 protected:
452 /// getOrCreateStaticMemberDIE - Create new static data member DIE.
453 DIE *getOrCreateStaticMemberDIE(DIDerivedType DT);
455 /// Look up the source ID with the given directory and source file names. If
456 /// none currently exists, create a new ID and insert it in the line table.
457 virtual unsigned getOrCreateSourceID(StringRef File, StringRef Directory) = 0;
459 private:
460 /// \brief Construct a DIE for the given DbgVariable without initializing the
461 /// DbgVariable's DIE reference.
462 DIE *constructVariableDIEImpl(const DbgVariable &DV, bool isScopeAbstract);
464 /// constructTypeDIE - Construct basic type die from DIBasicType.
465 void constructTypeDIE(DIE &Buffer, DIBasicType BTy);
467 /// constructTypeDIE - Construct derived type die from DIDerivedType.
468 void constructTypeDIE(DIE &Buffer, DIDerivedType DTy);
470 /// constructTypeDIE - Construct type DIE from DICompositeType.
471 void constructTypeDIE(DIE &Buffer, DICompositeType CTy);
473 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
474 void constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy);
476 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
477 void constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy);
479 /// constructEnumTypeDIE - Construct enum type DIE from DIEnumerator.
480 void constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy);
482 /// constructMemberDIE - Construct member DIE from DIDerivedType.
483 void constructMemberDIE(DIE &Buffer, DIDerivedType DT);
485 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
486 /// DITemplateTypeParameter.
487 void constructTemplateTypeParameterDIE(DIE &Buffer,
488 DITemplateTypeParameter TP);
490 /// constructTemplateValueParameterDIE - Construct new DIE for the given
491 /// DITemplateValueParameter.
492 void constructTemplateValueParameterDIE(DIE &Buffer,
493 DITemplateValueParameter TVP);
495 /// getLowerBoundDefault - Return the default lower bound for an array. If the
496 /// DWARF version doesn't handle the language, return -1.
497 int64_t getDefaultLowerBound() const;
499 /// getDIEEntry - Returns the debug information entry for the specified
500 /// debug variable.
501 DIEEntry *getDIEEntry(const MDNode *N) const {
502 return MDNodeToDIEEntryMap.lookup(N);
503 }
505 /// insertDIEEntry - Insert debug information entry into the map.
506 void insertDIEEntry(const MDNode *N, DIEEntry *E) {
507 MDNodeToDIEEntryMap.insert(std::make_pair(N, E));
508 }
510 // getIndexTyDie - Get an anonymous type for index type.
511 DIE *getIndexTyDie() { return IndexTyDie; }
513 // setIndexTyDie - Set D as anonymous type for index which can be reused
514 // later.
515 void setIndexTyDie(DIE *D) { IndexTyDie = D; }
517 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
518 /// information entry.
519 DIEEntry *createDIEEntry(DIE *Entry);
521 /// resolve - Look in the DwarfDebug map for the MDNode that
522 /// corresponds to the reference.
523 template <typename T> T resolve(DIRef<T> Ref) const {
524 return DD->resolve(Ref);
525 }
527 /// If this is a named finished type then include it in the list of types for
528 /// the accelerator tables.
529 void updateAcceleratorTables(DIScope Context, DIType Ty, const DIE *TyDIE);
530 };
532 class DwarfCompileUnit : public DwarfUnit {
533 /// The attribute index of DW_AT_stmt_list in the compile unit DIE, avoiding
534 /// the need to search for it in applyStmtList.
535 unsigned stmtListIndex;
537 public:
538 DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
539 DwarfDebug *DW, DwarfFile *DWU);
541 void initStmtList(MCSymbol *DwarfLineSectionSym);
543 /// Apply the DW_AT_stmt_list from this compile unit to the specified DIE.
544 void applyStmtList(DIE &D);
546 /// createGlobalVariableDIE - create global variable DIE.
547 void createGlobalVariableDIE(DIGlobalVariable GV);
549 /// addLabelAddress - Add a dwarf label attribute data and value using
550 /// either DW_FORM_addr or DW_FORM_GNU_addr_index.
551 void addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
552 const MCSymbol *Label);
554 /// addLocalLabelAddress - Add a dwarf label attribute data and value using
555 /// DW_FORM_addr only.
556 void addLocalLabelAddress(DIE *Die, dwarf::Attribute Attribute,
557 const MCSymbol *Label);
559 DwarfCompileUnit &getCU() override { return *this; }
561 unsigned getOrCreateSourceID(StringRef FileName, StringRef DirName) override;
562 };
564 class DwarfTypeUnit : public DwarfUnit {
565 private:
566 uint64_t TypeSignature;
567 const DIE *Ty;
568 DwarfCompileUnit &CU;
569 MCDwarfDwoLineTable *SplitLineTable;
571 public:
572 DwarfTypeUnit(unsigned UID, DIE *D, DwarfCompileUnit &CU, AsmPrinter *A,
573 DwarfDebug *DW, DwarfFile *DWU,
574 MCDwarfDwoLineTable *SplitLineTable = nullptr);
576 void setTypeSignature(uint64_t Signature) { TypeSignature = Signature; }
577 uint64_t getTypeSignature() const { return TypeSignature; }
578 void setType(const DIE *Ty) { this->Ty = Ty; }
580 /// Emit the header for this unit, not including the initial length field.
581 void emitHeader(const MCSymbol *ASectionSym) const override;
582 unsigned getHeaderSize() const override {
583 return DwarfUnit::getHeaderSize() + sizeof(uint64_t) + // Type Signature
584 sizeof(uint32_t); // Type DIE Offset
585 }
586 void initSection(const MCSection *Section);
587 DwarfCompileUnit &getCU() override { return CU; }
589 protected:
590 unsigned getOrCreateSourceID(StringRef File, StringRef Directory) override;
591 };
592 } // end llvm namespace
593 #endif