1 //===-- OcamlGCPrinter.cpp - Ocaml frametable emitter ---------------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements printing the assembly code for an Ocaml frametable.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "llvm/CodeGen/GCs.h"
15 #include "llvm/ADT/SmallString.h"
16 #include "llvm/CodeGen/AsmPrinter.h"
17 #include "llvm/CodeGen/GCMetadataPrinter.h"
18 #include "llvm/IR/DataLayout.h"
19 #include "llvm/IR/Mangler.h"
20 #include "llvm/IR/Module.h"
21 #include "llvm/MC/MCAsmInfo.h"
22 #include "llvm/MC/MCContext.h"
23 #include "llvm/MC/MCStreamer.h"
24 #include "llvm/MC/MCSymbol.h"
25 #include "llvm/Support/ErrorHandling.h"
26 #include "llvm/Support/FormattedStream.h"
27 #include "llvm/Target/TargetLoweringObjectFile.h"
28 #include "llvm/Target/TargetMachine.h"
29 #include <cctype>
30 using namespace llvm;
32 namespace {
34 class OcamlGCMetadataPrinter : public GCMetadataPrinter {
35 public:
36 void beginAssembly(AsmPrinter &AP) override;
37 void finishAssembly(AsmPrinter &AP) override;
38 };
40 }
42 static GCMetadataPrinterRegistry::Add<OcamlGCMetadataPrinter>
43 Y("ocaml", "ocaml 3.10-compatible collector");
45 void llvm::linkOcamlGCPrinter() { }
47 static void EmitCamlGlobal(const Module &M, AsmPrinter &AP, const char *Id) {
48 const std::string &MId = M.getModuleIdentifier();
50 std::string SymName;
51 SymName += "caml";
52 size_t Letter = SymName.size();
53 SymName.append(MId.begin(), std::find(MId.begin(), MId.end(), '.'));
54 SymName += "__";
55 SymName += Id;
57 // Capitalize the first letter of the module name.
58 SymName[Letter] = toupper(SymName[Letter]);
60 SmallString<128> TmpStr;
61 AP.Mang->getNameWithPrefix(TmpStr, SymName);
63 MCSymbol *Sym = AP.OutContext.GetOrCreateSymbol(TmpStr);
65 AP.OutStreamer.EmitSymbolAttribute(Sym, MCSA_Global);
66 AP.OutStreamer.EmitLabel(Sym);
67 }
69 void OcamlGCMetadataPrinter::beginAssembly(AsmPrinter &AP) {
70 AP.OutStreamer.SwitchSection(AP.getObjFileLowering().getTextSection());
71 EmitCamlGlobal(getModule(), AP, "code_begin");
73 AP.OutStreamer.SwitchSection(AP.getObjFileLowering().getDataSection());
74 EmitCamlGlobal(getModule(), AP, "data_begin");
75 }
77 /// emitAssembly - Print the frametable. The ocaml frametable format is thus:
78 ///
79 /// extern "C" struct align(sizeof(intptr_t)) {
80 /// uint16_t NumDescriptors;
81 /// struct align(sizeof(intptr_t)) {
82 /// void *ReturnAddress;
83 /// uint16_t FrameSize;
84 /// uint16_t NumLiveOffsets;
85 /// uint16_t LiveOffsets[NumLiveOffsets];
86 /// } Descriptors[NumDescriptors];
87 /// } caml${module}__frametable;
88 ///
89 /// Note that this precludes programs from stack frames larger than 64K
90 /// (FrameSize and LiveOffsets would overflow). FrameTablePrinter will abort if
91 /// either condition is detected in a function which uses the GC.
92 ///
93 void OcamlGCMetadataPrinter::finishAssembly(AsmPrinter &AP) {
94 unsigned IntPtrSize = AP.TM.getDataLayout()->getPointerSize();
96 AP.OutStreamer.SwitchSection(AP.getObjFileLowering().getTextSection());
97 EmitCamlGlobal(getModule(), AP, "code_end");
99 AP.OutStreamer.SwitchSection(AP.getObjFileLowering().getDataSection());
100 EmitCamlGlobal(getModule(), AP, "data_end");
102 // FIXME: Why does ocaml emit this??
103 AP.OutStreamer.EmitIntValue(0, IntPtrSize);
105 AP.OutStreamer.SwitchSection(AP.getObjFileLowering().getDataSection());
106 EmitCamlGlobal(getModule(), AP, "frametable");
108 int NumDescriptors = 0;
109 for (iterator I = begin(), IE = end(); I != IE; ++I) {
110 GCFunctionInfo &FI = **I;
111 for (GCFunctionInfo::iterator J = FI.begin(), JE = FI.end(); J != JE; ++J) {
112 NumDescriptors++;
113 }
114 }
116 if (NumDescriptors >= 1<<16) {
117 // Very rude!
118 report_fatal_error(" Too much descriptor for ocaml GC");
119 }
120 AP.EmitInt16(NumDescriptors);
121 AP.EmitAlignment(IntPtrSize == 4 ? 2 : 3);
123 for (iterator I = begin(), IE = end(); I != IE; ++I) {
124 GCFunctionInfo &FI = **I;
126 uint64_t FrameSize = FI.getFrameSize();
127 if (FrameSize >= 1<<16) {
128 // Very rude!
129 report_fatal_error("Function '" + FI.getFunction().getName() +
130 "' is too large for the ocaml GC! "
131 "Frame size " + Twine(FrameSize) + ">= 65536.\n"
132 "(" + Twine(uintptr_t(&FI)) + ")");
133 }
135 AP.OutStreamer.AddComment("live roots for " +
136 Twine(FI.getFunction().getName()));
137 AP.OutStreamer.AddBlankLine();
139 for (GCFunctionInfo::iterator J = FI.begin(), JE = FI.end(); J != JE; ++J) {
140 size_t LiveCount = FI.live_size(J);
141 if (LiveCount >= 1<<16) {
142 // Very rude!
143 report_fatal_error("Function '" + FI.getFunction().getName() +
144 "' is too large for the ocaml GC! "
145 "Live root count "+Twine(LiveCount)+" >= 65536.");
146 }
148 AP.OutStreamer.EmitSymbolValue(J->Label, IntPtrSize);
149 AP.EmitInt16(FrameSize);
150 AP.EmitInt16(LiveCount);
152 for (GCFunctionInfo::live_iterator K = FI.live_begin(J),
153 KE = FI.live_end(J); K != KE; ++K) {
154 if (K->StackOffset >= 1<<16) {
155 // Very rude!
156 report_fatal_error(
157 "GC root stack offset is outside of fixed stack frame and out "
158 "of range for ocaml GC!");
159 }
160 AP.EmitInt16(K->StackOffset);
161 }
163 AP.EmitAlignment(IntPtrSize == 4 ? 2 : 3);
164 }
165 }
166 }