]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/AsmPrinter/WinCodeViewLineTables.cpp
Convert more loops to range-based equivalents
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / WinCodeViewLineTables.cpp
1 //===-- llvm/lib/CodeGen/AsmPrinter/WinCodeViewLineTables.cpp --*- C++ -*--===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing line tables info into COFF files.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "WinCodeViewLineTables.h"
15 #include "llvm/MC/MCExpr.h"
16 #include "llvm/MC/MCSymbol.h"
17 #include "llvm/Support/COFF.h"
19 namespace llvm {
21 StringRef WinCodeViewLineTables::getFullFilepath(const MDNode *S) {
22   assert(S);
23   DIDescriptor D(S);
24   assert((D.isCompileUnit() || D.isFile() || D.isSubprogram() ||
25           D.isLexicalBlockFile() || D.isLexicalBlock()) &&
26          "Unexpected scope info");
28   DIScope Scope(S);
29   StringRef Dir = Scope.getDirectory(),
30             Filename = Scope.getFilename();
31   char *&Result = DirAndFilenameToFilepathMap[std::make_pair(Dir, Filename)];
32   if (Result)
33     return Result;
35   // Clang emits directory and relative filename info into the IR, but CodeView
36   // operates on full paths.  We could change Clang to emit full paths too, but
37   // that would increase the IR size and probably not needed for other users.
38   // For now, just concatenate and canonicalize the path here.
39   std::string Filepath;
40   if (Filename.find(':') == 1)
41     Filepath = Filename;
42   else
43     Filepath = (Dir + Twine("\\") + Filename).str();
45   // Canonicalize the path.  We have to do it textually because we may no longer
46   // have access the file in the filesystem.
47   // First, replace all slashes with backslashes.
48   std::replace(Filepath.begin(), Filepath.end(), '/', '\\');
50   // Remove all "\.\" with "\".
51   size_t Cursor = 0;
52   while ((Cursor = Filepath.find("\\.\\", Cursor)) != std::string::npos)
53     Filepath.erase(Cursor, 2);
55   // Replace all "\XXX\..\" with "\".  Don't try too hard though as the original
56   // path should be well-formatted, e.g. start with a drive letter, etc.
57   Cursor = 0;
58   while ((Cursor = Filepath.find("\\..\\", Cursor)) != std::string::npos) {
59     // Something's wrong if the path starts with "\..\", abort.
60     if (Cursor == 0)
61       break;
63     size_t PrevSlash = Filepath.rfind('\\', Cursor - 1);
64     if (PrevSlash == std::string::npos)
65       // Something's wrong, abort.
66       break;
68     Filepath.erase(PrevSlash, Cursor + 3 - PrevSlash);
69     // The next ".." might be following the one we've just erased.
70     Cursor = PrevSlash;
71   }
73   // Remove all duplicate backslashes.
74   Cursor = 0;
75   while ((Cursor = Filepath.find("\\\\", Cursor)) != std::string::npos)
76     Filepath.erase(Cursor, 1);
78   Result = strdup(Filepath.c_str());
79   return StringRef(Result);
80 }
82 void WinCodeViewLineTables::maybeRecordLocation(DebugLoc DL,
83                                                 const MachineFunction *MF) {
84   const MDNode *Scope = DL.getScope(MF->getFunction()->getContext());
85   if (!Scope)
86     return;
87   StringRef Filename = getFullFilepath(Scope);
89   // Skip this instruction if it has the same file:line as the previous one.
90   assert(CurFn);
91   if (!CurFn->Instrs.empty()) {
92     const InstrInfoTy &LastInstr = InstrInfo[CurFn->Instrs.back()];
93     if (LastInstr.Filename == Filename && LastInstr.LineNumber == DL.getLine())
94       return;
95   }
96   FileNameRegistry.add(Filename);
98   MCSymbol *MCL = Asm->MMI->getContext().CreateTempSymbol();
99   Asm->OutStreamer.EmitLabel(MCL);
100   CurFn->Instrs.push_back(MCL);
101   InstrInfo[MCL] = InstrInfoTy(Filename, DL.getLine());
104 WinCodeViewLineTables::WinCodeViewLineTables(AsmPrinter *AP)
105     : Asm(nullptr), CurFn(nullptr) {
106   MachineModuleInfo *MMI = AP->MMI;
108   // If module doesn't have named metadata anchors or COFF debug section
109   // is not available, skip any debug info related stuff.
110   if (!MMI->getModule()->getNamedMetadata("llvm.dbg.cu") ||
111       !AP->getObjFileLowering().getCOFFDebugSymbolsSection())
112     return;
114   // Tell MMI that we have debug info.
115   MMI->setDebugInfoAvailability(true);
116   Asm = AP;
119 static void EmitLabelDiff(MCStreamer &Streamer,
120                           const MCSymbol *From, const MCSymbol *To) {
121   MCSymbolRefExpr::VariantKind Variant = MCSymbolRefExpr::VK_None;
122   MCContext &Context = Streamer.getContext();
123   const MCExpr *FromRef = MCSymbolRefExpr::Create(From, Variant, Context),
124                *ToRef   = MCSymbolRefExpr::Create(To, Variant, Context);
125   const MCExpr *AddrDelta =
126       MCBinaryExpr::Create(MCBinaryExpr::Sub, ToRef, FromRef, Context);
127   Streamer.EmitValue(AddrDelta, 4);
130 void WinCodeViewLineTables::emitDebugInfoForFunction(const Function *GV) {
131   // For each function there is a separate subsection
132   // which holds the PC to file:line table.
133   const MCSymbol *Fn = Asm->getSymbol(GV);
134   assert(Fn);
136   const FunctionInfo &FI = FnDebugInfo[GV];
137   if (FI.Instrs.empty())
138     return;
139   assert(FI.End && "Don't know where the function ends?");
141   // PCs/Instructions are grouped into segments sharing the same filename.
142   // Pre-calculate the lengths (in instructions) of these segments and store
143   // them in a map for convenience.  Each index in the map is the sequential
144   // number of the respective instruction that starts a new segment.
145   DenseMap<size_t, size_t> FilenameSegmentLengths;
146   size_t LastSegmentEnd = 0;
147   StringRef PrevFilename = InstrInfo[FI.Instrs[0]].Filename;
148   for (size_t J = 1, F = FI.Instrs.size(); J != F; ++J) {
149     if (PrevFilename == InstrInfo[FI.Instrs[J]].Filename)
150       continue;
151     FilenameSegmentLengths[LastSegmentEnd] = J - LastSegmentEnd;
152     LastSegmentEnd = J;
153     PrevFilename = InstrInfo[FI.Instrs[J]].Filename;
154   }
155   FilenameSegmentLengths[LastSegmentEnd] = FI.Instrs.size() - LastSegmentEnd;
157   // Emit the control code of the subsection followed by the payload size.
158   Asm->OutStreamer.AddComment(
159       "Linetable subsection for " + Twine(Fn->getName()));
160   Asm->EmitInt32(COFF::DEBUG_LINE_TABLE_SUBSECTION);
161   MCSymbol *SubsectionBegin = Asm->MMI->getContext().CreateTempSymbol(),
162            *SubsectionEnd = Asm->MMI->getContext().CreateTempSymbol();
163   EmitLabelDiff(Asm->OutStreamer, SubsectionBegin, SubsectionEnd);
164   Asm->OutStreamer.EmitLabel(SubsectionBegin);
166   // Identify the function this subsection is for.
167   Asm->OutStreamer.EmitCOFFSecRel32(Fn);
168   Asm->OutStreamer.EmitCOFFSectionIndex(Fn);
170   // Length of the function's code, in bytes.
171   EmitLabelDiff(Asm->OutStreamer, Fn, FI.End);
173   // PC-to-linenumber lookup table:
174   MCSymbol *FileSegmentEnd = nullptr;
175   for (size_t J = 0, F = FI.Instrs.size(); J != F; ++J) {
176     MCSymbol *Instr = FI.Instrs[J];
177     assert(InstrInfo.count(Instr));
179     if (FilenameSegmentLengths.count(J)) {
180       // We came to a beginning of a new filename segment.
181       if (FileSegmentEnd)
182         Asm->OutStreamer.EmitLabel(FileSegmentEnd);
183       StringRef CurFilename = InstrInfo[FI.Instrs[J]].Filename;
184       assert(FileNameRegistry.Infos.count(CurFilename));
185       size_t IndexInStringTable =
186           FileNameRegistry.Infos[CurFilename].FilenameID;
187       // Each segment starts with the offset of the filename
188       // in the string table.
189       Asm->OutStreamer.AddComment(
190           "Segment for file '" + Twine(CurFilename) + "' begins");
191       MCSymbol *FileSegmentBegin = Asm->MMI->getContext().CreateTempSymbol();
192       Asm->OutStreamer.EmitLabel(FileSegmentBegin);
193       Asm->EmitInt32(8 * IndexInStringTable);
195       // Number of PC records in the lookup table.
196       size_t SegmentLength = FilenameSegmentLengths[J];
197       Asm->EmitInt32(SegmentLength);
199       // Full size of the segment for this filename, including the prev two
200       // records.
201       FileSegmentEnd = Asm->MMI->getContext().CreateTempSymbol();
202       EmitLabelDiff(Asm->OutStreamer, FileSegmentBegin, FileSegmentEnd);
203     }
205     // The first PC with the given linenumber and the linenumber itself.
206     EmitLabelDiff(Asm->OutStreamer, Fn, Instr);
207     Asm->EmitInt32(InstrInfo[Instr].LineNumber);
208   }
210   if (FileSegmentEnd)
211     Asm->OutStreamer.EmitLabel(FileSegmentEnd);
212   Asm->OutStreamer.EmitLabel(SubsectionEnd);
215 void WinCodeViewLineTables::endModule() {
216   if (FnDebugInfo.empty())
217     return;
219   assert(Asm != nullptr);
220   Asm->OutStreamer.SwitchSection(
221       Asm->getObjFileLowering().getCOFFDebugSymbolsSection());
222   Asm->EmitInt32(COFF::DEBUG_SECTION_MAGIC);
224   // The COFF .debug$S section consists of several subsections, each starting
225   // with a 4-byte control code (e.g. 0xF1, 0xF2, etc) and then a 4-byte length
226   // of the payload followed by the payload itself.  The subsections are 4-byte
227   // aligned.
229   for (size_t I = 0, E = VisitedFunctions.size(); I != E; ++I)
230     emitDebugInfoForFunction(VisitedFunctions[I]);
232   // This subsection holds a file index to offset in string table table.
233   Asm->OutStreamer.AddComment("File index to string table offset subsection");
234   Asm->EmitInt32(COFF::DEBUG_INDEX_SUBSECTION);
235   size_t NumFilenames = FileNameRegistry.Infos.size();
236   Asm->EmitInt32(8 * NumFilenames);
237   for (size_t I = 0, E = FileNameRegistry.Filenames.size(); I != E; ++I) {
238     StringRef Filename = FileNameRegistry.Filenames[I];
239     // For each unique filename, just write it's offset in the string table.
240     Asm->EmitInt32(FileNameRegistry.Infos[Filename].StartOffset);
241     // The function name offset is not followed by any additional data.
242     Asm->EmitInt32(0);
243   }
245   // This subsection holds the string table.
246   Asm->OutStreamer.AddComment("String table");
247   Asm->EmitInt32(COFF::DEBUG_STRING_TABLE_SUBSECTION);
248   Asm->EmitInt32(FileNameRegistry.LastOffset);
249   // The payload starts with a null character.
250   Asm->EmitInt8(0);
252   for (size_t I = 0, E = FileNameRegistry.Filenames.size(); I != E; ++I) {
253     // Just emit unique filenames one by one, separated by a null character.
254     Asm->OutStreamer.EmitBytes(FileNameRegistry.Filenames[I]);
255     Asm->EmitInt8(0);
256   }
258   // No more subsections. Fill with zeros to align the end of the section by 4.
259   Asm->OutStreamer.EmitFill((-FileNameRegistry.LastOffset) % 4, 0);
261   clear();
264 void WinCodeViewLineTables::beginFunction(const MachineFunction *MF) {
265   assert(!CurFn && "Can't process two functions at once!");
267   if (!Asm || !Asm->MMI->hasDebugInfo())
268     return;
270   const Function *GV = MF->getFunction();
271   assert(FnDebugInfo.count(GV) == false);
272   VisitedFunctions.push_back(GV);
273   CurFn = &FnDebugInfo[GV];
275   // Find the end of the function prolog.
276   // FIXME: is there a simpler a way to do this? Can we just search
277   // for the first instruction of the function, not the last of the prolog?
278   DebugLoc PrologEndLoc;
279   bool EmptyPrologue = true;
280   for (const auto &MBB : *MF) {
281     if (!PrologEndLoc.isUnknown())
282       break;
283     for (const auto &MI : MBB) {
284       if (MI.isDebugValue())
285         continue;
287       // First known non-DBG_VALUE and non-frame setup location marks
288       // the beginning of the function body.
289       // FIXME: do we need the first subcondition?
290       if (!MI.getFlag(MachineInstr::FrameSetup) &&
291           (!MI.getDebugLoc().isUnknown())) {
292         PrologEndLoc = MI.getDebugLoc();
293         break;
294       }
295       EmptyPrologue = false;
296     }
297   }
298   // Record beginning of function if we have a non-empty prologue.
299   if (!PrologEndLoc.isUnknown() && !EmptyPrologue) {
300     DebugLoc FnStartDL =
301         PrologEndLoc.getFnDebugLoc(MF->getFunction()->getContext());
302     maybeRecordLocation(FnStartDL, MF);
303   }
306 void WinCodeViewLineTables::endFunction(const MachineFunction *MF) {
307   if (!Asm || !CurFn)  // We haven't created any debug info for this function.
308     return;
310   const Function *GV = MF->getFunction();
311   assert(FnDebugInfo.count(GV) == true);
312   assert(CurFn == &FnDebugInfo[GV]);
314   if (CurFn->Instrs.empty()) {
315     FnDebugInfo.erase(GV);
316     VisitedFunctions.pop_back();
317   } else {
318     // Define end label for subprogram.
319     MCSymbol *FunctionEndSym = Asm->OutStreamer.getContext().CreateTempSymbol();
320     Asm->OutStreamer.EmitLabel(FunctionEndSym);
321     CurFn->End = FunctionEndSym;
322   }
323   CurFn = nullptr;
326 void WinCodeViewLineTables::beginInstruction(const MachineInstr *MI) {
327   // Ignore DBG_VALUE locations and function prologue.
328   if (!Asm || MI->isDebugValue() || MI->getFlag(MachineInstr::FrameSetup))
329     return;
330   DebugLoc DL = MI->getDebugLoc();
331   if (DL == PrevInstLoc || DL.isUnknown())
332     return;
333   maybeRecordLocation(DL, Asm->MF);