1 //===-- llvm/lib/CodeGen/AsmPrinter/WinCodeViewLineTables.cpp --*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains support for writing line tables info into COFF files.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "WinCodeViewLineTables.h"
15 #include "llvm/MC/MCExpr.h"
16 #include "llvm/MC/MCSymbol.h"
17 #include "llvm/Support/COFF.h"
19 namespace llvm {
21 StringRef WinCodeViewLineTables::getFullFilepath(const MDNode *S) {
22 assert(S);
23 DIDescriptor D(S);
24 assert((D.isCompileUnit() || D.isFile() || D.isSubprogram() ||
25 D.isLexicalBlockFile() || D.isLexicalBlock()) &&
26 "Unexpected scope info");
28 DIScope Scope(S);
29 StringRef Dir = Scope.getDirectory(),
30 Filename = Scope.getFilename();
31 char *&Result = DirAndFilenameToFilepathMap[std::make_pair(Dir, Filename)];
32 if (Result)
33 return Result;
35 // Clang emits directory and relative filename info into the IR, but CodeView
36 // operates on full paths. We could change Clang to emit full paths too, but
37 // that would increase the IR size and probably not needed for other users.
38 // For now, just concatenate and canonicalize the path here.
39 std::string Filepath;
40 if (Filename.find(':') == 1)
41 Filepath = Filename;
42 else
43 Filepath = (Dir + Twine("\\") + Filename).str();
45 // Canonicalize the path. We have to do it textually because we may no longer
46 // have access the file in the filesystem.
47 // First, replace all slashes with backslashes.
48 std::replace(Filepath.begin(), Filepath.end(), '/', '\\');
50 // Remove all "\.\" with "\".
51 size_t Cursor = 0;
52 while ((Cursor = Filepath.find("\\.\\", Cursor)) != std::string::npos)
53 Filepath.erase(Cursor, 2);
55 // Replace all "\XXX\..\" with "\". Don't try too hard though as the original
56 // path should be well-formatted, e.g. start with a drive letter, etc.
57 Cursor = 0;
58 while ((Cursor = Filepath.find("\\..\\", Cursor)) != std::string::npos) {
59 // Something's wrong if the path starts with "\..\", abort.
60 if (Cursor == 0)
61 break;
63 size_t PrevSlash = Filepath.rfind('\\', Cursor - 1);
64 if (PrevSlash == std::string::npos)
65 // Something's wrong, abort.
66 break;
68 Filepath.erase(PrevSlash, Cursor + 3 - PrevSlash);
69 // The next ".." might be following the one we've just erased.
70 Cursor = PrevSlash;
71 }
73 // Remove all duplicate backslashes.
74 Cursor = 0;
75 while ((Cursor = Filepath.find("\\\\", Cursor)) != std::string::npos)
76 Filepath.erase(Cursor, 1);
78 Result = strdup(Filepath.c_str());
79 return StringRef(Result);
80 }
82 void WinCodeViewLineTables::maybeRecordLocation(DebugLoc DL,
83 const MachineFunction *MF) {
84 const MDNode *Scope = DL.getScope(MF->getFunction()->getContext());
85 if (!Scope)
86 return;
87 StringRef Filename = getFullFilepath(Scope);
89 // Skip this instruction if it has the same file:line as the previous one.
90 assert(CurFn);
91 if (!CurFn->Instrs.empty()) {
92 const InstrInfoTy &LastInstr = InstrInfo[CurFn->Instrs.back()];
93 if (LastInstr.Filename == Filename && LastInstr.LineNumber == DL.getLine())
94 return;
95 }
96 FileNameRegistry.add(Filename);
98 MCSymbol *MCL = Asm->MMI->getContext().CreateTempSymbol();
99 Asm->OutStreamer.EmitLabel(MCL);
100 CurFn->Instrs.push_back(MCL);
101 InstrInfo[MCL] = InstrInfoTy(Filename, DL.getLine());
102 }
104 WinCodeViewLineTables::WinCodeViewLineTables(AsmPrinter *AP)
105 : Asm(nullptr), CurFn(nullptr) {
106 MachineModuleInfo *MMI = AP->MMI;
108 // If module doesn't have named metadata anchors or COFF debug section
109 // is not available, skip any debug info related stuff.
110 if (!MMI->getModule()->getNamedMetadata("llvm.dbg.cu") ||
111 !AP->getObjFileLowering().getCOFFDebugSymbolsSection())
112 return;
114 // Tell MMI that we have debug info.
115 MMI->setDebugInfoAvailability(true);
116 Asm = AP;
117 }
119 static void EmitLabelDiff(MCStreamer &Streamer,
120 const MCSymbol *From, const MCSymbol *To) {
121 MCSymbolRefExpr::VariantKind Variant = MCSymbolRefExpr::VK_None;
122 MCContext &Context = Streamer.getContext();
123 const MCExpr *FromRef = MCSymbolRefExpr::Create(From, Variant, Context),
124 *ToRef = MCSymbolRefExpr::Create(To, Variant, Context);
125 const MCExpr *AddrDelta =
126 MCBinaryExpr::Create(MCBinaryExpr::Sub, ToRef, FromRef, Context);
127 Streamer.EmitValue(AddrDelta, 4);
128 }
130 void WinCodeViewLineTables::emitDebugInfoForFunction(const Function *GV) {
131 // For each function there is a separate subsection
132 // which holds the PC to file:line table.
133 const MCSymbol *Fn = Asm->getSymbol(GV);
134 assert(Fn);
136 const FunctionInfo &FI = FnDebugInfo[GV];
137 if (FI.Instrs.empty())
138 return;
139 assert(FI.End && "Don't know where the function ends?");
141 // PCs/Instructions are grouped into segments sharing the same filename.
142 // Pre-calculate the lengths (in instructions) of these segments and store
143 // them in a map for convenience. Each index in the map is the sequential
144 // number of the respective instruction that starts a new segment.
145 DenseMap<size_t, size_t> FilenameSegmentLengths;
146 size_t LastSegmentEnd = 0;
147 StringRef PrevFilename = InstrInfo[FI.Instrs[0]].Filename;
148 for (size_t J = 1, F = FI.Instrs.size(); J != F; ++J) {
149 if (PrevFilename == InstrInfo[FI.Instrs[J]].Filename)
150 continue;
151 FilenameSegmentLengths[LastSegmentEnd] = J - LastSegmentEnd;
152 LastSegmentEnd = J;
153 PrevFilename = InstrInfo[FI.Instrs[J]].Filename;
154 }
155 FilenameSegmentLengths[LastSegmentEnd] = FI.Instrs.size() - LastSegmentEnd;
157 // Emit the control code of the subsection followed by the payload size.
158 Asm->OutStreamer.AddComment(
159 "Linetable subsection for " + Twine(Fn->getName()));
160 Asm->EmitInt32(COFF::DEBUG_LINE_TABLE_SUBSECTION);
161 MCSymbol *SubsectionBegin = Asm->MMI->getContext().CreateTempSymbol(),
162 *SubsectionEnd = Asm->MMI->getContext().CreateTempSymbol();
163 EmitLabelDiff(Asm->OutStreamer, SubsectionBegin, SubsectionEnd);
164 Asm->OutStreamer.EmitLabel(SubsectionBegin);
166 // Identify the function this subsection is for.
167 Asm->OutStreamer.EmitCOFFSecRel32(Fn);
168 Asm->OutStreamer.EmitCOFFSectionIndex(Fn);
170 // Length of the function's code, in bytes.
171 EmitLabelDiff(Asm->OutStreamer, Fn, FI.End);
173 // PC-to-linenumber lookup table:
174 MCSymbol *FileSegmentEnd = nullptr;
175 for (size_t J = 0, F = FI.Instrs.size(); J != F; ++J) {
176 MCSymbol *Instr = FI.Instrs[J];
177 assert(InstrInfo.count(Instr));
179 if (FilenameSegmentLengths.count(J)) {
180 // We came to a beginning of a new filename segment.
181 if (FileSegmentEnd)
182 Asm->OutStreamer.EmitLabel(FileSegmentEnd);
183 StringRef CurFilename = InstrInfo[FI.Instrs[J]].Filename;
184 assert(FileNameRegistry.Infos.count(CurFilename));
185 size_t IndexInStringTable =
186 FileNameRegistry.Infos[CurFilename].FilenameID;
187 // Each segment starts with the offset of the filename
188 // in the string table.
189 Asm->OutStreamer.AddComment(
190 "Segment for file '" + Twine(CurFilename) + "' begins");
191 MCSymbol *FileSegmentBegin = Asm->MMI->getContext().CreateTempSymbol();
192 Asm->OutStreamer.EmitLabel(FileSegmentBegin);
193 Asm->EmitInt32(8 * IndexInStringTable);
195 // Number of PC records in the lookup table.
196 size_t SegmentLength = FilenameSegmentLengths[J];
197 Asm->EmitInt32(SegmentLength);
199 // Full size of the segment for this filename, including the prev two
200 // records.
201 FileSegmentEnd = Asm->MMI->getContext().CreateTempSymbol();
202 EmitLabelDiff(Asm->OutStreamer, FileSegmentBegin, FileSegmentEnd);
203 }
205 // The first PC with the given linenumber and the linenumber itself.
206 EmitLabelDiff(Asm->OutStreamer, Fn, Instr);
207 Asm->EmitInt32(InstrInfo[Instr].LineNumber);
208 }
210 if (FileSegmentEnd)
211 Asm->OutStreamer.EmitLabel(FileSegmentEnd);
212 Asm->OutStreamer.EmitLabel(SubsectionEnd);
213 }
215 void WinCodeViewLineTables::endModule() {
216 if (FnDebugInfo.empty())
217 return;
219 assert(Asm != nullptr);
220 Asm->OutStreamer.SwitchSection(
221 Asm->getObjFileLowering().getCOFFDebugSymbolsSection());
222 Asm->EmitInt32(COFF::DEBUG_SECTION_MAGIC);
224 // The COFF .debug$S section consists of several subsections, each starting
225 // with a 4-byte control code (e.g. 0xF1, 0xF2, etc) and then a 4-byte length
226 // of the payload followed by the payload itself. The subsections are 4-byte
227 // aligned.
229 for (size_t I = 0, E = VisitedFunctions.size(); I != E; ++I)
230 emitDebugInfoForFunction(VisitedFunctions[I]);
232 // This subsection holds a file index to offset in string table table.
233 Asm->OutStreamer.AddComment("File index to string table offset subsection");
234 Asm->EmitInt32(COFF::DEBUG_INDEX_SUBSECTION);
235 size_t NumFilenames = FileNameRegistry.Infos.size();
236 Asm->EmitInt32(8 * NumFilenames);
237 for (size_t I = 0, E = FileNameRegistry.Filenames.size(); I != E; ++I) {
238 StringRef Filename = FileNameRegistry.Filenames[I];
239 // For each unique filename, just write it's offset in the string table.
240 Asm->EmitInt32(FileNameRegistry.Infos[Filename].StartOffset);
241 // The function name offset is not followed by any additional data.
242 Asm->EmitInt32(0);
243 }
245 // This subsection holds the string table.
246 Asm->OutStreamer.AddComment("String table");
247 Asm->EmitInt32(COFF::DEBUG_STRING_TABLE_SUBSECTION);
248 Asm->EmitInt32(FileNameRegistry.LastOffset);
249 // The payload starts with a null character.
250 Asm->EmitInt8(0);
252 for (size_t I = 0, E = FileNameRegistry.Filenames.size(); I != E; ++I) {
253 // Just emit unique filenames one by one, separated by a null character.
254 Asm->OutStreamer.EmitBytes(FileNameRegistry.Filenames[I]);
255 Asm->EmitInt8(0);
256 }
258 // No more subsections. Fill with zeros to align the end of the section by 4.
259 Asm->OutStreamer.EmitFill((-FileNameRegistry.LastOffset) % 4, 0);
261 clear();
262 }
264 void WinCodeViewLineTables::beginFunction(const MachineFunction *MF) {
265 assert(!CurFn && "Can't process two functions at once!");
267 if (!Asm || !Asm->MMI->hasDebugInfo())
268 return;
270 const Function *GV = MF->getFunction();
271 assert(FnDebugInfo.count(GV) == false);
272 VisitedFunctions.push_back(GV);
273 CurFn = &FnDebugInfo[GV];
275 // Find the end of the function prolog.
276 // FIXME: is there a simpler a way to do this? Can we just search
277 // for the first instruction of the function, not the last of the prolog?
278 DebugLoc PrologEndLoc;
279 bool EmptyPrologue = true;
280 for (const auto &MBB : *MF) {
281 if (!PrologEndLoc.isUnknown())
282 break;
283 for (const auto &MI : MBB) {
284 if (MI.isDebugValue())
285 continue;
287 // First known non-DBG_VALUE and non-frame setup location marks
288 // the beginning of the function body.
289 // FIXME: do we need the first subcondition?
290 if (!MI.getFlag(MachineInstr::FrameSetup) &&
291 (!MI.getDebugLoc().isUnknown())) {
292 PrologEndLoc = MI.getDebugLoc();
293 break;
294 }
295 EmptyPrologue = false;
296 }
297 }
298 // Record beginning of function if we have a non-empty prologue.
299 if (!PrologEndLoc.isUnknown() && !EmptyPrologue) {
300 DebugLoc FnStartDL =
301 PrologEndLoc.getFnDebugLoc(MF->getFunction()->getContext());
302 maybeRecordLocation(FnStartDL, MF);
303 }
304 }
306 void WinCodeViewLineTables::endFunction(const MachineFunction *MF) {
307 if (!Asm || !CurFn) // We haven't created any debug info for this function.
308 return;
310 const Function *GV = MF->getFunction();
311 assert(FnDebugInfo.count(GV));
312 assert(CurFn == &FnDebugInfo[GV]);
314 if (CurFn->Instrs.empty()) {
315 FnDebugInfo.erase(GV);
316 VisitedFunctions.pop_back();
317 } else {
318 // Define end label for subprogram.
319 MCSymbol *FunctionEndSym = Asm->OutStreamer.getContext().CreateTempSymbol();
320 Asm->OutStreamer.EmitLabel(FunctionEndSym);
321 CurFn->End = FunctionEndSym;
322 }
323 CurFn = nullptr;
324 }
326 void WinCodeViewLineTables::beginInstruction(const MachineInstr *MI) {
327 // Ignore DBG_VALUE locations and function prologue.
328 if (!Asm || MI->isDebugValue() || MI->getFlag(MachineInstr::FrameSetup))
329 return;
330 DebugLoc DL = MI->getDebugLoc();
331 if (DL == PrevInstLoc || DL.isUnknown())
332 return;
333 maybeRecordLocation(DL, Asm->MF);
334 }
335 }