]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/BranchFolding.cpp
Replace the dangling context hotfix with an assertion.
[opencl/llvm.git] / lib / CodeGen / BranchFolding.cpp
1 //===-- BranchFolding.cpp - Fold machine code branch instructions ---------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass forwards branches to unconditional branches to make them branch
11 // directly to the target block.  This pass often results in dead MBB's, which
12 // it then removes.
13 //
14 // Note that this pass must be run after register allocation, it cannot handle
15 // SSA form.
16 //
17 //===----------------------------------------------------------------------===//
19 #define DEBUG_TYPE "branchfolding"
20 #include "BranchFolding.h"
21 #include "llvm/ADT/STLExtras.h"
22 #include "llvm/ADT/SmallSet.h"
23 #include "llvm/ADT/Statistic.h"
24 #include "llvm/CodeGen/MachineFunctionPass.h"
25 #include "llvm/CodeGen/MachineJumpTableInfo.h"
26 #include "llvm/CodeGen/MachineModuleInfo.h"
27 #include "llvm/CodeGen/MachineRegisterInfo.h"
28 #include "llvm/CodeGen/Passes.h"
29 #include "llvm/CodeGen/RegisterScavenging.h"
30 #include "llvm/IR/Function.h"
31 #include "llvm/Support/CommandLine.h"
32 #include "llvm/Support/Debug.h"
33 #include "llvm/Support/ErrorHandling.h"
34 #include "llvm/Support/raw_ostream.h"
35 #include "llvm/Target/TargetInstrInfo.h"
36 #include "llvm/Target/TargetMachine.h"
37 #include "llvm/Target/TargetRegisterInfo.h"
38 #include <algorithm>
39 using namespace llvm;
41 STATISTIC(NumDeadBlocks, "Number of dead blocks removed");
42 STATISTIC(NumBranchOpts, "Number of branches optimized");
43 STATISTIC(NumTailMerge , "Number of block tails merged");
44 STATISTIC(NumHoist     , "Number of times common instructions are hoisted");
46 static cl::opt<cl::boolOrDefault> FlagEnableTailMerge("enable-tail-merge",
47                               cl::init(cl::BOU_UNSET), cl::Hidden);
49 // Throttle for huge numbers of predecessors (compile speed problems)
50 static cl::opt<unsigned>
51 TailMergeThreshold("tail-merge-threshold",
52           cl::desc("Max number of predecessors to consider tail merging"),
53           cl::init(150), cl::Hidden);
55 // Heuristic for tail merging (and, inversely, tail duplication).
56 // TODO: This should be replaced with a target query.
57 static cl::opt<unsigned>
58 TailMergeSize("tail-merge-size",
59           cl::desc("Min number of instructions to consider tail merging"),
60                               cl::init(3), cl::Hidden);
62 namespace {
63   /// BranchFolderPass - Wrap branch folder in a machine function pass.
64   class BranchFolderPass : public MachineFunctionPass {
65   public:
66     static char ID;
67     explicit BranchFolderPass(): MachineFunctionPass(ID) {}
69     virtual bool runOnMachineFunction(MachineFunction &MF);
71     virtual void getAnalysisUsage(AnalysisUsage &AU) const {
72       AU.addRequired<TargetPassConfig>();
73       MachineFunctionPass::getAnalysisUsage(AU);
74     }
75   };
76 }
78 char BranchFolderPass::ID = 0;
79 char &llvm::BranchFolderPassID = BranchFolderPass::ID;
81 INITIALIZE_PASS(BranchFolderPass, "branch-folder",
82                 "Control Flow Optimizer", false, false)
84 bool BranchFolderPass::runOnMachineFunction(MachineFunction &MF) {
85   TargetPassConfig *PassConfig = &getAnalysis<TargetPassConfig>();
86   BranchFolder Folder(PassConfig->getEnableTailMerge(), /*CommonHoist=*/true);
87   return Folder.OptimizeFunction(MF,
88                                  MF.getTarget().getInstrInfo(),
89                                  MF.getTarget().getRegisterInfo(),
90                                  getAnalysisIfAvailable<MachineModuleInfo>());
91 }
94 BranchFolder::BranchFolder(bool defaultEnableTailMerge, bool CommonHoist) {
95   switch (FlagEnableTailMerge) {
96   case cl::BOU_UNSET: EnableTailMerge = defaultEnableTailMerge; break;
97   case cl::BOU_TRUE: EnableTailMerge = true; break;
98   case cl::BOU_FALSE: EnableTailMerge = false; break;
99   }
101   EnableHoistCommonCode = CommonHoist;
104 /// RemoveDeadBlock - Remove the specified dead machine basic block from the
105 /// function, updating the CFG.
106 void BranchFolder::RemoveDeadBlock(MachineBasicBlock *MBB) {
107   assert(MBB->pred_empty() && "MBB must be dead!");
108   DEBUG(dbgs() << "\nRemoving MBB: " << *MBB);
110   MachineFunction *MF = MBB->getParent();
111   // drop all successors.
112   while (!MBB->succ_empty())
113     MBB->removeSuccessor(MBB->succ_end()-1);
115   // Avoid matching if this pointer gets reused.
116   TriedMerging.erase(MBB);
118   // Remove the block.
119   MF->erase(MBB);
122 /// OptimizeImpDefsBlock - If a basic block is just a bunch of implicit_def
123 /// followed by terminators, and if the implicitly defined registers are not
124 /// used by the terminators, remove those implicit_def's. e.g.
125 /// BB1:
126 ///   r0 = implicit_def
127 ///   r1 = implicit_def
128 ///   br
129 /// This block can be optimized away later if the implicit instructions are
130 /// removed.
131 bool BranchFolder::OptimizeImpDefsBlock(MachineBasicBlock *MBB) {
132   SmallSet<unsigned, 4> ImpDefRegs;
133   MachineBasicBlock::iterator I = MBB->begin();
134   while (I != MBB->end()) {
135     if (!I->isImplicitDef())
136       break;
137     unsigned Reg = I->getOperand(0).getReg();
138     for (MCSubRegIterator SubRegs(Reg, TRI, /*IncludeSelf=*/true);
139          SubRegs.isValid(); ++SubRegs)
140       ImpDefRegs.insert(*SubRegs);
141     ++I;
142   }
143   if (ImpDefRegs.empty())
144     return false;
146   MachineBasicBlock::iterator FirstTerm = I;
147   while (I != MBB->end()) {
148     if (!TII->isUnpredicatedTerminator(I))
149       return false;
150     // See if it uses any of the implicitly defined registers.
151     for (unsigned i = 0, e = I->getNumOperands(); i != e; ++i) {
152       MachineOperand &MO = I->getOperand(i);
153       if (!MO.isReg() || !MO.isUse())
154         continue;
155       unsigned Reg = MO.getReg();
156       if (ImpDefRegs.count(Reg))
157         return false;
158     }
159     ++I;
160   }
162   I = MBB->begin();
163   while (I != FirstTerm) {
164     MachineInstr *ImpDefMI = &*I;
165     ++I;
166     MBB->erase(ImpDefMI);
167   }
169   return true;
172 /// OptimizeFunction - Perhaps branch folding, tail merging and other
173 /// CFG optimizations on the given function.
174 bool BranchFolder::OptimizeFunction(MachineFunction &MF,
175                                     const TargetInstrInfo *tii,
176                                     const TargetRegisterInfo *tri,
177                                     MachineModuleInfo *mmi) {
178   if (!tii) return false;
180   TriedMerging.clear();
182   TII = tii;
183   TRI = tri;
184   MMI = mmi;
185   RS = NULL;
187   // Use a RegScavenger to help update liveness when required.
188   MachineRegisterInfo &MRI = MF.getRegInfo();
189   if (MRI.tracksLiveness() && TRI->trackLivenessAfterRegAlloc(MF))
190     RS = new RegScavenger();
191   else
192     MRI.invalidateLiveness();
194   // Fix CFG.  The later algorithms expect it to be right.
195   bool MadeChange = false;
196   for (MachineFunction::iterator I = MF.begin(), E = MF.end(); I != E; I++) {
197     MachineBasicBlock *MBB = I, *TBB = 0, *FBB = 0;
198     SmallVector<MachineOperand, 4> Cond;
199     if (!TII->AnalyzeBranch(*MBB, TBB, FBB, Cond, true))
200       MadeChange |= MBB->CorrectExtraCFGEdges(TBB, FBB, !Cond.empty());
201     MadeChange |= OptimizeImpDefsBlock(MBB);
202   }
204   bool MadeChangeThisIteration = true;
205   while (MadeChangeThisIteration) {
206     MadeChangeThisIteration    = TailMergeBlocks(MF);
207     MadeChangeThisIteration   |= OptimizeBranches(MF);
208     if (EnableHoistCommonCode)
209       MadeChangeThisIteration |= HoistCommonCode(MF);
210     MadeChange |= MadeChangeThisIteration;
211   }
213   // See if any jump tables have become dead as the code generator
214   // did its thing.
215   MachineJumpTableInfo *JTI = MF.getJumpTableInfo();
216   if (JTI == 0) {
217     delete RS;
218     return MadeChange;
219   }
221   // Walk the function to find jump tables that are live.
222   BitVector JTIsLive(JTI->getJumpTables().size());
223   for (MachineFunction::iterator BB = MF.begin(), E = MF.end();
224        BB != E; ++BB) {
225     for (MachineBasicBlock::iterator I = BB->begin(), E = BB->end();
226          I != E; ++I)
227       for (unsigned op = 0, e = I->getNumOperands(); op != e; ++op) {
228         MachineOperand &Op = I->getOperand(op);
229         if (!Op.isJTI()) continue;
231         // Remember that this JT is live.
232         JTIsLive.set(Op.getIndex());
233       }
234   }
236   // Finally, remove dead jump tables.  This happens when the
237   // indirect jump was unreachable (and thus deleted).
238   for (unsigned i = 0, e = JTIsLive.size(); i != e; ++i)
239     if (!JTIsLive.test(i)) {
240       JTI->RemoveJumpTable(i);
241       MadeChange = true;
242     }
244   delete RS;
245   return MadeChange;
248 //===----------------------------------------------------------------------===//
249 //  Tail Merging of Blocks
250 //===----------------------------------------------------------------------===//
252 /// HashMachineInstr - Compute a hash value for MI and its operands.
253 static unsigned HashMachineInstr(const MachineInstr *MI) {
254   unsigned Hash = MI->getOpcode();
255   for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
256     const MachineOperand &Op = MI->getOperand(i);
258     // Merge in bits from the operand if easy.
259     unsigned OperandHash = 0;
260     switch (Op.getType()) {
261     case MachineOperand::MO_Register:          OperandHash = Op.getReg(); break;
262     case MachineOperand::MO_Immediate:         OperandHash = Op.getImm(); break;
263     case MachineOperand::MO_MachineBasicBlock:
264       OperandHash = Op.getMBB()->getNumber();
265       break;
266     case MachineOperand::MO_FrameIndex:
267     case MachineOperand::MO_ConstantPoolIndex:
268     case MachineOperand::MO_JumpTableIndex:
269       OperandHash = Op.getIndex();
270       break;
271     case MachineOperand::MO_GlobalAddress:
272     case MachineOperand::MO_ExternalSymbol:
273       // Global address / external symbol are too hard, don't bother, but do
274       // pull in the offset.
275       OperandHash = Op.getOffset();
276       break;
277     default: break;
278     }
280     Hash += ((OperandHash << 3) | Op.getType()) << (i&31);
281   }
282   return Hash;
285 /// HashEndOfMBB - Hash the last instruction in the MBB.
286 static unsigned HashEndOfMBB(const MachineBasicBlock *MBB) {
287   MachineBasicBlock::const_iterator I = MBB->end();
288   if (I == MBB->begin())
289     return 0;   // Empty MBB.
291   --I;
292   // Skip debug info so it will not affect codegen.
293   while (I->isDebugValue()) {
294     if (I==MBB->begin())
295       return 0;      // MBB empty except for debug info.
296     --I;
297   }
299   return HashMachineInstr(I);
302 /// ComputeCommonTailLength - Given two machine basic blocks, compute the number
303 /// of instructions they actually have in common together at their end.  Return
304 /// iterators for the first shared instruction in each block.
305 static unsigned ComputeCommonTailLength(MachineBasicBlock *MBB1,
306                                         MachineBasicBlock *MBB2,
307                                         MachineBasicBlock::iterator &I1,
308                                         MachineBasicBlock::iterator &I2) {
309   I1 = MBB1->end();
310   I2 = MBB2->end();
312   unsigned TailLen = 0;
313   while (I1 != MBB1->begin() && I2 != MBB2->begin()) {
314     --I1; --I2;
315     // Skip debugging pseudos; necessary to avoid changing the code.
316     while (I1->isDebugValue()) {
317       if (I1==MBB1->begin()) {
318         while (I2->isDebugValue()) {
319           if (I2==MBB2->begin())
320             // I1==DBG at begin; I2==DBG at begin
321             return TailLen;
322           --I2;
323         }
324         ++I2;
325         // I1==DBG at begin; I2==non-DBG, or first of DBGs not at begin
326         return TailLen;
327       }
328       --I1;
329     }
330     // I1==first (untested) non-DBG preceding known match
331     while (I2->isDebugValue()) {
332       if (I2==MBB2->begin()) {
333         ++I1;
334         // I1==non-DBG, or first of DBGs not at begin; I2==DBG at begin
335         return TailLen;
336       }
337       --I2;
338     }
339     // I1, I2==first (untested) non-DBGs preceding known match
340     if (!I1->isIdenticalTo(I2) ||
341         // FIXME: This check is dubious. It's used to get around a problem where
342         // people incorrectly expect inline asm directives to remain in the same
343         // relative order. This is untenable because normal compiler
344         // optimizations (like this one) may reorder and/or merge these
345         // directives.
346         I1->isInlineAsm()) {
347       ++I1; ++I2;
348       break;
349     }
350     ++TailLen;
351   }
352   // Back past possible debugging pseudos at beginning of block.  This matters
353   // when one block differs from the other only by whether debugging pseudos
354   // are present at the beginning.  (This way, the various checks later for
355   // I1==MBB1->begin() work as expected.)
356   if (I1 == MBB1->begin() && I2 != MBB2->begin()) {
357     --I2;
358     while (I2->isDebugValue()) {
359       if (I2 == MBB2->begin())
360         return TailLen;
361       --I2;
362     }
363     ++I2;
364   }
365   if (I2 == MBB2->begin() && I1 != MBB1->begin()) {
366     --I1;
367     while (I1->isDebugValue()) {
368       if (I1 == MBB1->begin())
369         return TailLen;
370       --I1;
371     }
372     ++I1;
373   }
374   return TailLen;
377 void BranchFolder::MaintainLiveIns(MachineBasicBlock *CurMBB,
378                                    MachineBasicBlock *NewMBB) {
379   if (RS) {
380     RS->enterBasicBlock(CurMBB);
381     if (!CurMBB->empty())
382       RS->forward(prior(CurMBB->end()));
383     BitVector RegsLiveAtExit(TRI->getNumRegs());
384     RS->getRegsUsed(RegsLiveAtExit, false);
385     for (unsigned int i = 0, e = TRI->getNumRegs(); i != e; i++)
386       if (RegsLiveAtExit[i])
387         NewMBB->addLiveIn(i);
388   }
391 /// ReplaceTailWithBranchTo - Delete the instruction OldInst and everything
392 /// after it, replacing it with an unconditional branch to NewDest.
393 void BranchFolder::ReplaceTailWithBranchTo(MachineBasicBlock::iterator OldInst,
394                                            MachineBasicBlock *NewDest) {
395   MachineBasicBlock *CurMBB = OldInst->getParent();
397   TII->ReplaceTailWithBranchTo(OldInst, NewDest);
399   // For targets that use the register scavenger, we must maintain LiveIns.
400   MaintainLiveIns(CurMBB, NewDest);
402   ++NumTailMerge;
405 /// SplitMBBAt - Given a machine basic block and an iterator into it, split the
406 /// MBB so that the part before the iterator falls into the part starting at the
407 /// iterator.  This returns the new MBB.
408 MachineBasicBlock *BranchFolder::SplitMBBAt(MachineBasicBlock &CurMBB,
409                                             MachineBasicBlock::iterator BBI1,
410                                             const BasicBlock *BB) {
411   if (!TII->isLegalToSplitMBBAt(CurMBB, BBI1))
412     return 0;
414   MachineFunction &MF = *CurMBB.getParent();
416   // Create the fall-through block.
417   MachineFunction::iterator MBBI = &CurMBB;
418   MachineBasicBlock *NewMBB =MF.CreateMachineBasicBlock(BB);
419   CurMBB.getParent()->insert(++MBBI, NewMBB);
421   // Move all the successors of this block to the specified block.
422   NewMBB->transferSuccessors(&CurMBB);
424   // Add an edge from CurMBB to NewMBB for the fall-through.
425   CurMBB.addSuccessor(NewMBB);
427   // Splice the code over.
428   NewMBB->splice(NewMBB->end(), &CurMBB, BBI1, CurMBB.end());
430   // For targets that use the register scavenger, we must maintain LiveIns.
431   MaintainLiveIns(&CurMBB, NewMBB);
433   return NewMBB;
436 /// EstimateRuntime - Make a rough estimate for how long it will take to run
437 /// the specified code.
438 static unsigned EstimateRuntime(MachineBasicBlock::iterator I,
439                                 MachineBasicBlock::iterator E) {
440   unsigned Time = 0;
441   for (; I != E; ++I) {
442     if (I->isDebugValue())
443       continue;
444     if (I->isCall())
445       Time += 10;
446     else if (I->mayLoad() || I->mayStore())
447       Time += 2;
448     else
449       ++Time;
450   }
451   return Time;
454 // CurMBB needs to add an unconditional branch to SuccMBB (we removed these
455 // branches temporarily for tail merging).  In the case where CurMBB ends
456 // with a conditional branch to the next block, optimize by reversing the
457 // test and conditionally branching to SuccMBB instead.
458 static void FixTail(MachineBasicBlock *CurMBB, MachineBasicBlock *SuccBB,
459                     const TargetInstrInfo *TII) {
460   MachineFunction *MF = CurMBB->getParent();
461   MachineFunction::iterator I = llvm::next(MachineFunction::iterator(CurMBB));
462   MachineBasicBlock *TBB = 0, *FBB = 0;
463   SmallVector<MachineOperand, 4> Cond;
464   DebugLoc dl;  // FIXME: this is nowhere
465   if (I != MF->end() &&
466       !TII->AnalyzeBranch(*CurMBB, TBB, FBB, Cond, true)) {
467     MachineBasicBlock *NextBB = I;
468     if (TBB == NextBB && !Cond.empty() && !FBB) {
469       if (!TII->ReverseBranchCondition(Cond)) {
470         TII->RemoveBranch(*CurMBB);
471         TII->InsertBranch(*CurMBB, SuccBB, NULL, Cond, dl);
472         return;
473       }
474     }
475   }
476   TII->InsertBranch(*CurMBB, SuccBB, NULL,
477                     SmallVector<MachineOperand, 0>(), dl);
480 bool
481 BranchFolder::MergePotentialsElt::operator<(const MergePotentialsElt &o) const {
482   if (getHash() < o.getHash())
483     return true;
484   if (getHash() > o.getHash())
485     return false;
486   if (getBlock()->getNumber() < o.getBlock()->getNumber())
487     return true;
488   if (getBlock()->getNumber() > o.getBlock()->getNumber())
489     return false;
490   // _GLIBCXX_DEBUG checks strict weak ordering, which involves comparing
491   // an object with itself.
492 #ifndef _GLIBCXX_DEBUG
493   llvm_unreachable("Predecessor appears twice");
494 #else
495   return false;
496 #endif
499 /// CountTerminators - Count the number of terminators in the given
500 /// block and set I to the position of the first non-terminator, if there
501 /// is one, or MBB->end() otherwise.
502 static unsigned CountTerminators(MachineBasicBlock *MBB,
503                                  MachineBasicBlock::iterator &I) {
504   I = MBB->end();
505   unsigned NumTerms = 0;
506   for (;;) {
507     if (I == MBB->begin()) {
508       I = MBB->end();
509       break;
510     }
511     --I;
512     if (!I->isTerminator()) break;
513     ++NumTerms;
514   }
515   return NumTerms;
518 /// ProfitableToMerge - Check if two machine basic blocks have a common tail
519 /// and decide if it would be profitable to merge those tails.  Return the
520 /// length of the common tail and iterators to the first common instruction
521 /// in each block.
522 static bool ProfitableToMerge(MachineBasicBlock *MBB1,
523                               MachineBasicBlock *MBB2,
524                               unsigned minCommonTailLength,
525                               unsigned &CommonTailLen,
526                               MachineBasicBlock::iterator &I1,
527                               MachineBasicBlock::iterator &I2,
528                               MachineBasicBlock *SuccBB,
529                               MachineBasicBlock *PredBB) {
530   CommonTailLen = ComputeCommonTailLength(MBB1, MBB2, I1, I2);
531   if (CommonTailLen == 0)
532     return false;
533   DEBUG(dbgs() << "Common tail length of BB#" << MBB1->getNumber()
534                << " and BB#" << MBB2->getNumber() << " is " << CommonTailLen
535                << '\n');
537   // It's almost always profitable to merge any number of non-terminator
538   // instructions with the block that falls through into the common successor.
539   if (MBB1 == PredBB || MBB2 == PredBB) {
540     MachineBasicBlock::iterator I;
541     unsigned NumTerms = CountTerminators(MBB1 == PredBB ? MBB2 : MBB1, I);
542     if (CommonTailLen > NumTerms)
543       return true;
544   }
546   // If one of the blocks can be completely merged and happens to be in
547   // a position where the other could fall through into it, merge any number
548   // of instructions, because it can be done without a branch.
549   // TODO: If the blocks are not adjacent, move one of them so that they are?
550   if (MBB1->isLayoutSuccessor(MBB2) && I2 == MBB2->begin())
551     return true;
552   if (MBB2->isLayoutSuccessor(MBB1) && I1 == MBB1->begin())
553     return true;
555   // If both blocks have an unconditional branch temporarily stripped out,
556   // count that as an additional common instruction for the following
557   // heuristics.
558   unsigned EffectiveTailLen = CommonTailLen;
559   if (SuccBB && MBB1 != PredBB && MBB2 != PredBB &&
560       !MBB1->back().isBarrier() &&
561       !MBB2->back().isBarrier())
562     ++EffectiveTailLen;
564   // Check if the common tail is long enough to be worthwhile.
565   if (EffectiveTailLen >= minCommonTailLength)
566     return true;
568   // If we are optimizing for code size, 2 instructions in common is enough if
569   // we don't have to split a block.  At worst we will be introducing 1 new
570   // branch instruction, which is likely to be smaller than the 2
571   // instructions that would be deleted in the merge.
572   MachineFunction *MF = MBB1->getParent();
573   if (EffectiveTailLen >= 2 &&
574       MF->getFunction()->getAttributes().
575         hasAttribute(AttributeSet::FunctionIndex, Attribute::OptimizeForSize) &&
576       (I1 == MBB1->begin() || I2 == MBB2->begin()))
577     return true;
579   return false;
582 /// ComputeSameTails - Look through all the blocks in MergePotentials that have
583 /// hash CurHash (guaranteed to match the last element).  Build the vector
584 /// SameTails of all those that have the (same) largest number of instructions
585 /// in common of any pair of these blocks.  SameTails entries contain an
586 /// iterator into MergePotentials (from which the MachineBasicBlock can be
587 /// found) and a MachineBasicBlock::iterator into that MBB indicating the
588 /// instruction where the matching code sequence begins.
589 /// Order of elements in SameTails is the reverse of the order in which
590 /// those blocks appear in MergePotentials (where they are not necessarily
591 /// consecutive).
592 unsigned BranchFolder::ComputeSameTails(unsigned CurHash,
593                                         unsigned minCommonTailLength,
594                                         MachineBasicBlock *SuccBB,
595                                         MachineBasicBlock *PredBB) {
596   unsigned maxCommonTailLength = 0U;
597   SameTails.clear();
598   MachineBasicBlock::iterator TrialBBI1, TrialBBI2;
599   MPIterator HighestMPIter = prior(MergePotentials.end());
600   for (MPIterator CurMPIter = prior(MergePotentials.end()),
601                   B = MergePotentials.begin();
602        CurMPIter != B && CurMPIter->getHash() == CurHash;
603        --CurMPIter) {
604     for (MPIterator I = prior(CurMPIter); I->getHash() == CurHash ; --I) {
605       unsigned CommonTailLen;
606       if (ProfitableToMerge(CurMPIter->getBlock(), I->getBlock(),
607                             minCommonTailLength,
608                             CommonTailLen, TrialBBI1, TrialBBI2,
609                             SuccBB, PredBB)) {
610         if (CommonTailLen > maxCommonTailLength) {
611           SameTails.clear();
612           maxCommonTailLength = CommonTailLen;
613           HighestMPIter = CurMPIter;
614           SameTails.push_back(SameTailElt(CurMPIter, TrialBBI1));
615         }
616         if (HighestMPIter == CurMPIter &&
617             CommonTailLen == maxCommonTailLength)
618           SameTails.push_back(SameTailElt(I, TrialBBI2));
619       }
620       if (I == B)
621         break;
622     }
623   }
624   return maxCommonTailLength;
627 /// RemoveBlocksWithHash - Remove all blocks with hash CurHash from
628 /// MergePotentials, restoring branches at ends of blocks as appropriate.
629 void BranchFolder::RemoveBlocksWithHash(unsigned CurHash,
630                                         MachineBasicBlock *SuccBB,
631                                         MachineBasicBlock *PredBB) {
632   MPIterator CurMPIter, B;
633   for (CurMPIter = prior(MergePotentials.end()), B = MergePotentials.begin();
634        CurMPIter->getHash() == CurHash;
635        --CurMPIter) {
636     // Put the unconditional branch back, if we need one.
637     MachineBasicBlock *CurMBB = CurMPIter->getBlock();
638     if (SuccBB && CurMBB != PredBB)
639       FixTail(CurMBB, SuccBB, TII);
640     if (CurMPIter == B)
641       break;
642   }
643   if (CurMPIter->getHash() != CurHash)
644     CurMPIter++;
645   MergePotentials.erase(CurMPIter, MergePotentials.end());
648 /// CreateCommonTailOnlyBlock - None of the blocks to be tail-merged consist
649 /// only of the common tail.  Create a block that does by splitting one.
650 bool BranchFolder::CreateCommonTailOnlyBlock(MachineBasicBlock *&PredBB,
651                                              MachineBasicBlock *SuccBB,
652                                              unsigned maxCommonTailLength,
653                                              unsigned &commonTailIndex) {
654   commonTailIndex = 0;
655   unsigned TimeEstimate = ~0U;
656   for (unsigned i = 0, e = SameTails.size(); i != e; ++i) {
657     // Use PredBB if possible; that doesn't require a new branch.
658     if (SameTails[i].getBlock() == PredBB) {
659       commonTailIndex = i;
660       break;
661     }
662     // Otherwise, make a (fairly bogus) choice based on estimate of
663     // how long it will take the various blocks to execute.
664     unsigned t = EstimateRuntime(SameTails[i].getBlock()->begin(),
665                                  SameTails[i].getTailStartPos());
666     if (t <= TimeEstimate) {
667       TimeEstimate = t;
668       commonTailIndex = i;
669     }
670   }
672   MachineBasicBlock::iterator BBI =
673     SameTails[commonTailIndex].getTailStartPos();
674   MachineBasicBlock *MBB = SameTails[commonTailIndex].getBlock();
676   // If the common tail includes any debug info we will take it pretty
677   // randomly from one of the inputs.  Might be better to remove it?
678   DEBUG(dbgs() << "\nSplitting BB#" << MBB->getNumber() << ", size "
679                << maxCommonTailLength);
681   // If the split block unconditionally falls-thru to SuccBB, it will be
682   // merged. In control flow terms it should then take SuccBB's name. e.g. If
683   // SuccBB is an inner loop, the common tail is still part of the inner loop.
684   const BasicBlock *BB = (SuccBB && MBB->succ_size() == 1) ?
685     SuccBB->getBasicBlock() : MBB->getBasicBlock();
686   MachineBasicBlock *newMBB = SplitMBBAt(*MBB, BBI, BB);
687   if (!newMBB) {
688     DEBUG(dbgs() << "... failed!");
689     return false;
690   }
692   SameTails[commonTailIndex].setBlock(newMBB);
693   SameTails[commonTailIndex].setTailStartPos(newMBB->begin());
695   // If we split PredBB, newMBB is the new predecessor.
696   if (PredBB == MBB)
697     PredBB = newMBB;
699   return true;
702 // See if any of the blocks in MergePotentials (which all have a common single
703 // successor, or all have no successor) can be tail-merged.  If there is a
704 // successor, any blocks in MergePotentials that are not tail-merged and
705 // are not immediately before Succ must have an unconditional branch to
706 // Succ added (but the predecessor/successor lists need no adjustment).
707 // The lone predecessor of Succ that falls through into Succ,
708 // if any, is given in PredBB.
710 bool BranchFolder::TryTailMergeBlocks(MachineBasicBlock *SuccBB,
711                                       MachineBasicBlock *PredBB) {
712   bool MadeChange = false;
714   // Except for the special cases below, tail-merge if there are at least
715   // this many instructions in common.
716   unsigned minCommonTailLength = TailMergeSize;
718   DEBUG(dbgs() << "\nTryTailMergeBlocks: ";
719         for (unsigned i = 0, e = MergePotentials.size(); i != e; ++i)
720           dbgs() << "BB#" << MergePotentials[i].getBlock()->getNumber()
721                  << (i == e-1 ? "" : ", ");
722         dbgs() << "\n";
723         if (SuccBB) {
724           dbgs() << "  with successor BB#" << SuccBB->getNumber() << '\n';
725           if (PredBB)
726             dbgs() << "  which has fall-through from BB#"
727                    << PredBB->getNumber() << "\n";
728         }
729         dbgs() << "Looking for common tails of at least "
730                << minCommonTailLength << " instruction"
731                << (minCommonTailLength == 1 ? "" : "s") << '\n';
732        );
734   // Sort by hash value so that blocks with identical end sequences sort
735   // together.
736   std::stable_sort(MergePotentials.begin(), MergePotentials.end());
738   // Walk through equivalence sets looking for actual exact matches.
739   while (MergePotentials.size() > 1) {
740     unsigned CurHash = MergePotentials.back().getHash();
742     // Build SameTails, identifying the set of blocks with this hash code
743     // and with the maximum number of instructions in common.
744     unsigned maxCommonTailLength = ComputeSameTails(CurHash,
745                                                     minCommonTailLength,
746                                                     SuccBB, PredBB);
748     // If we didn't find any pair that has at least minCommonTailLength
749     // instructions in common, remove all blocks with this hash code and retry.
750     if (SameTails.empty()) {
751       RemoveBlocksWithHash(CurHash, SuccBB, PredBB);
752       continue;
753     }
755     // If one of the blocks is the entire common tail (and not the entry
756     // block, which we can't jump to), we can treat all blocks with this same
757     // tail at once.  Use PredBB if that is one of the possibilities, as that
758     // will not introduce any extra branches.
759     MachineBasicBlock *EntryBB = MergePotentials.begin()->getBlock()->
760                                  getParent()->begin();
761     unsigned commonTailIndex = SameTails.size();
762     // If there are two blocks, check to see if one can be made to fall through
763     // into the other.
764     if (SameTails.size() == 2 &&
765         SameTails[0].getBlock()->isLayoutSuccessor(SameTails[1].getBlock()) &&
766         SameTails[1].tailIsWholeBlock())
767       commonTailIndex = 1;
768     else if (SameTails.size() == 2 &&
769              SameTails[1].getBlock()->isLayoutSuccessor(
770                                                      SameTails[0].getBlock()) &&
771              SameTails[0].tailIsWholeBlock())
772       commonTailIndex = 0;
773     else {
774       // Otherwise just pick one, favoring the fall-through predecessor if
775       // there is one.
776       for (unsigned i = 0, e = SameTails.size(); i != e; ++i) {
777         MachineBasicBlock *MBB = SameTails[i].getBlock();
778         if (MBB == EntryBB && SameTails[i].tailIsWholeBlock())
779           continue;
780         if (MBB == PredBB) {
781           commonTailIndex = i;
782           break;
783         }
784         if (SameTails[i].tailIsWholeBlock())
785           commonTailIndex = i;
786       }
787     }
789     if (commonTailIndex == SameTails.size() ||
790         (SameTails[commonTailIndex].getBlock() == PredBB &&
791          !SameTails[commonTailIndex].tailIsWholeBlock())) {
792       // None of the blocks consist entirely of the common tail.
793       // Split a block so that one does.
794       if (!CreateCommonTailOnlyBlock(PredBB, SuccBB,
795                                      maxCommonTailLength, commonTailIndex)) {
796         RemoveBlocksWithHash(CurHash, SuccBB, PredBB);
797         continue;
798       }
799     }
801     MachineBasicBlock *MBB = SameTails[commonTailIndex].getBlock();
802     // MBB is common tail.  Adjust all other BB's to jump to this one.
803     // Traversal must be forwards so erases work.
804     DEBUG(dbgs() << "\nUsing common tail in BB#" << MBB->getNumber()
805                  << " for ");
806     for (unsigned int i=0, e = SameTails.size(); i != e; ++i) {
807       if (commonTailIndex == i)
808         continue;
809       DEBUG(dbgs() << "BB#" << SameTails[i].getBlock()->getNumber()
810                    << (i == e-1 ? "" : ", "));
811       // Hack the end off BB i, making it jump to BB commonTailIndex instead.
812       ReplaceTailWithBranchTo(SameTails[i].getTailStartPos(), MBB);
813       // BB i is no longer a predecessor of SuccBB; remove it from the worklist.
814       MergePotentials.erase(SameTails[i].getMPIter());
815     }
816     DEBUG(dbgs() << "\n");
817     // We leave commonTailIndex in the worklist in case there are other blocks
818     // that match it with a smaller number of instructions.
819     MadeChange = true;
820   }
821   return MadeChange;
824 bool BranchFolder::TailMergeBlocks(MachineFunction &MF) {
825   bool MadeChange = false;
826   if (!EnableTailMerge) return MadeChange;
828   // First find blocks with no successors.
829   MergePotentials.clear();
830   for (MachineFunction::iterator I = MF.begin(), E = MF.end();
831        I != E && MergePotentials.size() < TailMergeThreshold; ++I) {
832     if (TriedMerging.count(I))
833       continue;
834     if (I->succ_empty())
835       MergePotentials.push_back(MergePotentialsElt(HashEndOfMBB(I), I));
836   }
838   // If this is a large problem, avoid visiting the same basic blocks
839   // multiple times.
840   if (MergePotentials.size() == TailMergeThreshold)
841     for (unsigned i = 0, e = MergePotentials.size(); i != e; ++i)
842       TriedMerging.insert(MergePotentials[i].getBlock());
844   // See if we can do any tail merging on those.
845   if (MergePotentials.size() >= 2)
846     MadeChange |= TryTailMergeBlocks(NULL, NULL);
848   // Look at blocks (IBB) with multiple predecessors (PBB).
849   // We change each predecessor to a canonical form, by
850   // (1) temporarily removing any unconditional branch from the predecessor
851   // to IBB, and
852   // (2) alter conditional branches so they branch to the other block
853   // not IBB; this may require adding back an unconditional branch to IBB
854   // later, where there wasn't one coming in.  E.g.
855   //   Bcc IBB
856   //   fallthrough to QBB
857   // here becomes
858   //   Bncc QBB
859   // with a conceptual B to IBB after that, which never actually exists.
860   // With those changes, we see whether the predecessors' tails match,
861   // and merge them if so.  We change things out of canonical form and
862   // back to the way they were later in the process.  (OptimizeBranches
863   // would undo some of this, but we can't use it, because we'd get into
864   // a compile-time infinite loop repeatedly doing and undoing the same
865   // transformations.)
867   for (MachineFunction::iterator I = llvm::next(MF.begin()), E = MF.end();
868        I != E; ++I) {
869     if (I->pred_size() < 2) continue;
870     SmallPtrSet<MachineBasicBlock *, 8> UniquePreds;
871     MachineBasicBlock *IBB = I;
872     MachineBasicBlock *PredBB = prior(I);
873     MergePotentials.clear();
874     for (MachineBasicBlock::pred_iterator P = I->pred_begin(),
875            E2 = I->pred_end();
876          P != E2 && MergePotentials.size() < TailMergeThreshold; ++P) {
877       MachineBasicBlock *PBB = *P;
878       if (TriedMerging.count(PBB))
879         continue;
881       // Skip blocks that loop to themselves, can't tail merge these.
882       if (PBB == IBB)
883         continue;
885       // Visit each predecessor only once.
886       if (!UniquePreds.insert(PBB))
887         continue;
889       // Skip blocks which may jump to a landing pad. Can't tail merge these.
890       if (PBB->getLandingPadSuccessor())
891         continue;
893       MachineBasicBlock *TBB = 0, *FBB = 0;
894       SmallVector<MachineOperand, 4> Cond;
895       if (!TII->AnalyzeBranch(*PBB, TBB, FBB, Cond, true)) {
896         // Failing case: IBB is the target of a cbr, and we cannot reverse the
897         // branch.
898         SmallVector<MachineOperand, 4> NewCond(Cond);
899         if (!Cond.empty() && TBB == IBB) {
900           if (TII->ReverseBranchCondition(NewCond))
901             continue;
902           // This is the QBB case described above
903           if (!FBB)
904             FBB = llvm::next(MachineFunction::iterator(PBB));
905         }
907         // Failing case: the only way IBB can be reached from PBB is via
908         // exception handling.  Happens for landing pads.  Would be nice to have
909         // a bit in the edge so we didn't have to do all this.
910         if (IBB->isLandingPad()) {
911           MachineFunction::iterator IP = PBB;  IP++;
912           MachineBasicBlock *PredNextBB = NULL;
913           if (IP != MF.end())
914             PredNextBB = IP;
915           if (TBB == NULL) {
916             if (IBB != PredNextBB)      // fallthrough
917               continue;
918           } else if (FBB) {
919             if (TBB != IBB && FBB != IBB)   // cbr then ubr
920               continue;
921           } else if (Cond.empty()) {
922             if (TBB != IBB)               // ubr
923               continue;
924           } else {
925             if (TBB != IBB && IBB != PredNextBB)  // cbr
926               continue;
927           }
928         }
930         // Remove the unconditional branch at the end, if any.
931         if (TBB && (Cond.empty() || FBB)) {
932           DebugLoc dl;  // FIXME: this is nowhere
933           TII->RemoveBranch(*PBB);
934           if (!Cond.empty())
935             // reinsert conditional branch only, for now
936             TII->InsertBranch(*PBB, (TBB == IBB) ? FBB : TBB, 0, NewCond, dl);
937         }
939         MergePotentials.push_back(MergePotentialsElt(HashEndOfMBB(PBB), *P));
940       }
941     }
943     // If this is a large problem, avoid visiting the same basic blocks multiple
944     // times.
945     if (MergePotentials.size() == TailMergeThreshold)
946       for (unsigned i = 0, e = MergePotentials.size(); i != e; ++i)
947         TriedMerging.insert(MergePotentials[i].getBlock());
949     if (MergePotentials.size() >= 2)
950       MadeChange |= TryTailMergeBlocks(IBB, PredBB);
952     // Reinsert an unconditional branch if needed. The 1 below can occur as a
953     // result of removing blocks in TryTailMergeBlocks.
954     PredBB = prior(I);     // this may have been changed in TryTailMergeBlocks
955     if (MergePotentials.size() == 1 &&
956         MergePotentials.begin()->getBlock() != PredBB)
957       FixTail(MergePotentials.begin()->getBlock(), IBB, TII);
958   }
960   return MadeChange;
963 //===----------------------------------------------------------------------===//
964 //  Branch Optimization
965 //===----------------------------------------------------------------------===//
967 bool BranchFolder::OptimizeBranches(MachineFunction &MF) {
968   bool MadeChange = false;
970   // Make sure blocks are numbered in order
971   MF.RenumberBlocks();
973   for (MachineFunction::iterator I = llvm::next(MF.begin()), E = MF.end();
974        I != E; ) {
975     MachineBasicBlock *MBB = I++;
976     MadeChange |= OptimizeBlock(MBB);
978     // If it is dead, remove it.
979     if (MBB->pred_empty()) {
980       RemoveDeadBlock(MBB);
981       MadeChange = true;
982       ++NumDeadBlocks;
983     }
984   }
985   return MadeChange;
988 // Blocks should be considered empty if they contain only debug info;
989 // else the debug info would affect codegen.
990 static bool IsEmptyBlock(MachineBasicBlock *MBB) {
991   if (MBB->empty())
992     return true;
993   for (MachineBasicBlock::iterator MBBI = MBB->begin(), MBBE = MBB->end();
994        MBBI!=MBBE; ++MBBI) {
995     if (!MBBI->isDebugValue())
996       return false;
997   }
998   return true;
1001 // Blocks with only debug info and branches should be considered the same
1002 // as blocks with only branches.
1003 static bool IsBranchOnlyBlock(MachineBasicBlock *MBB) {
1004   MachineBasicBlock::iterator MBBI, MBBE;
1005   for (MBBI = MBB->begin(), MBBE = MBB->end(); MBBI!=MBBE; ++MBBI) {
1006     if (!MBBI->isDebugValue())
1007       break;
1008   }
1009   return (MBBI->isBranch());
1012 /// IsBetterFallthrough - Return true if it would be clearly better to
1013 /// fall-through to MBB1 than to fall through into MBB2.  This has to return
1014 /// a strict ordering, returning true for both (MBB1,MBB2) and (MBB2,MBB1) will
1015 /// result in infinite loops.
1016 static bool IsBetterFallthrough(MachineBasicBlock *MBB1,
1017                                 MachineBasicBlock *MBB2) {
1018   // Right now, we use a simple heuristic.  If MBB2 ends with a call, and
1019   // MBB1 doesn't, we prefer to fall through into MBB1.  This allows us to
1020   // optimize branches that branch to either a return block or an assert block
1021   // into a fallthrough to the return.
1022   if (IsEmptyBlock(MBB1) || IsEmptyBlock(MBB2)) return false;
1024   // If there is a clear successor ordering we make sure that one block
1025   // will fall through to the next
1026   if (MBB1->isSuccessor(MBB2)) return true;
1027   if (MBB2->isSuccessor(MBB1)) return false;
1029   // Neither block consists entirely of debug info (per IsEmptyBlock check),
1030   // so we needn't test for falling off the beginning here.
1031   MachineBasicBlock::iterator MBB1I = --MBB1->end();
1032   while (MBB1I->isDebugValue())
1033     --MBB1I;
1034   MachineBasicBlock::iterator MBB2I = --MBB2->end();
1035   while (MBB2I->isDebugValue())
1036     --MBB2I;
1037   return MBB2I->isCall() && !MBB1I->isCall();
1040 /// getBranchDebugLoc - Find and return, if any, the DebugLoc of the branch
1041 /// instructions on the block. Always use the DebugLoc of the first
1042 /// branching instruction found unless its absent, in which case use the
1043 /// DebugLoc of the second if present.
1044 static DebugLoc getBranchDebugLoc(MachineBasicBlock &MBB) {
1045   MachineBasicBlock::iterator I = MBB.end();
1046   if (I == MBB.begin())
1047     return DebugLoc();
1048   --I;
1049   while (I->isDebugValue() && I != MBB.begin())
1050     --I;
1051   if (I->isBranch())
1052     return I->getDebugLoc();
1053   return DebugLoc();
1056 /// OptimizeBlock - Analyze and optimize control flow related to the specified
1057 /// block.  This is never called on the entry block.
1058 bool BranchFolder::OptimizeBlock(MachineBasicBlock *MBB) {
1059   bool MadeChange = false;
1060   MachineFunction &MF = *MBB->getParent();
1061 ReoptimizeBlock:
1063   MachineFunction::iterator FallThrough = MBB;
1064   ++FallThrough;
1066   // If this block is empty, make everyone use its fall-through, not the block
1067   // explicitly.  Landing pads should not do this since the landing-pad table
1068   // points to this block.  Blocks with their addresses taken shouldn't be
1069   // optimized away.
1070   if (IsEmptyBlock(MBB) && !MBB->isLandingPad() && !MBB->hasAddressTaken()) {
1071     // Dead block?  Leave for cleanup later.
1072     if (MBB->pred_empty()) return MadeChange;
1074     if (FallThrough == MF.end()) {
1075       // TODO: Simplify preds to not branch here if possible!
1076     } else {
1077       // Rewrite all predecessors of the old block to go to the fallthrough
1078       // instead.
1079       while (!MBB->pred_empty()) {
1080         MachineBasicBlock *Pred = *(MBB->pred_end()-1);
1081         Pred->ReplaceUsesOfBlockWith(MBB, FallThrough);
1082       }
1083       // If MBB was the target of a jump table, update jump tables to go to the
1084       // fallthrough instead.
1085       if (MachineJumpTableInfo *MJTI = MF.getJumpTableInfo())
1086         MJTI->ReplaceMBBInJumpTables(MBB, FallThrough);
1087       MadeChange = true;
1088     }
1089     return MadeChange;
1090   }
1092   // Check to see if we can simplify the terminator of the block before this
1093   // one.
1094   MachineBasicBlock &PrevBB = *prior(MachineFunction::iterator(MBB));
1096   MachineBasicBlock *PriorTBB = 0, *PriorFBB = 0;
1097   SmallVector<MachineOperand, 4> PriorCond;
1098   bool PriorUnAnalyzable =
1099     TII->AnalyzeBranch(PrevBB, PriorTBB, PriorFBB, PriorCond, true);
1100   if (!PriorUnAnalyzable) {
1101     // If the CFG for the prior block has extra edges, remove them.
1102     MadeChange |= PrevBB.CorrectExtraCFGEdges(PriorTBB, PriorFBB,
1103                                               !PriorCond.empty());
1105     // If the previous branch is conditional and both conditions go to the same
1106     // destination, remove the branch, replacing it with an unconditional one or
1107     // a fall-through.
1108     if (PriorTBB && PriorTBB == PriorFBB) {
1109       DebugLoc dl = getBranchDebugLoc(PrevBB);
1110       TII->RemoveBranch(PrevBB);
1111       PriorCond.clear();
1112       if (PriorTBB != MBB)
1113         TII->InsertBranch(PrevBB, PriorTBB, 0, PriorCond, dl);
1114       MadeChange = true;
1115       ++NumBranchOpts;
1116       goto ReoptimizeBlock;
1117     }
1119     // If the previous block unconditionally falls through to this block and
1120     // this block has no other predecessors, move the contents of this block
1121     // into the prior block. This doesn't usually happen when SimplifyCFG
1122     // has been used, but it can happen if tail merging splits a fall-through
1123     // predecessor of a block.
1124     // This has to check PrevBB->succ_size() because EH edges are ignored by
1125     // AnalyzeBranch.
1126     if (PriorCond.empty() && !PriorTBB && MBB->pred_size() == 1 &&
1127         PrevBB.succ_size() == 1 &&
1128         !MBB->hasAddressTaken() && !MBB->isLandingPad()) {
1129       DEBUG(dbgs() << "\nMerging into block: " << PrevBB
1130                    << "From MBB: " << *MBB);
1131       // Remove redundant DBG_VALUEs first.
1132       if (PrevBB.begin() != PrevBB.end()) {
1133         MachineBasicBlock::iterator PrevBBIter = PrevBB.end();
1134         --PrevBBIter;
1135         MachineBasicBlock::iterator MBBIter = MBB->begin();
1136         // Check if DBG_VALUE at the end of PrevBB is identical to the
1137         // DBG_VALUE at the beginning of MBB.
1138         while (PrevBBIter != PrevBB.begin() && MBBIter != MBB->end()
1139                && PrevBBIter->isDebugValue() && MBBIter->isDebugValue()) {
1140           if (!MBBIter->isIdenticalTo(PrevBBIter))
1141             break;
1142           MachineInstr *DuplicateDbg = MBBIter;
1143           ++MBBIter; -- PrevBBIter;
1144           DuplicateDbg->eraseFromParent();
1145         }
1146       }
1147       PrevBB.splice(PrevBB.end(), MBB, MBB->begin(), MBB->end());
1148       PrevBB.removeSuccessor(PrevBB.succ_begin());
1149       assert(PrevBB.succ_empty());
1150       PrevBB.transferSuccessors(MBB);
1151       MadeChange = true;
1152       return MadeChange;
1153     }
1155     // If the previous branch *only* branches to *this* block (conditional or
1156     // not) remove the branch.
1157     if (PriorTBB == MBB && PriorFBB == 0) {
1158       TII->RemoveBranch(PrevBB);
1159       MadeChange = true;
1160       ++NumBranchOpts;
1161       goto ReoptimizeBlock;
1162     }
1164     // If the prior block branches somewhere else on the condition and here if
1165     // the condition is false, remove the uncond second branch.
1166     if (PriorFBB == MBB) {
1167       DebugLoc dl = getBranchDebugLoc(PrevBB);
1168       TII->RemoveBranch(PrevBB);
1169       TII->InsertBranch(PrevBB, PriorTBB, 0, PriorCond, dl);
1170       MadeChange = true;
1171       ++NumBranchOpts;
1172       goto ReoptimizeBlock;
1173     }
1175     // If the prior block branches here on true and somewhere else on false, and
1176     // if the branch condition is reversible, reverse the branch to create a
1177     // fall-through.
1178     if (PriorTBB == MBB) {
1179       SmallVector<MachineOperand, 4> NewPriorCond(PriorCond);
1180       if (!TII->ReverseBranchCondition(NewPriorCond)) {
1181         DebugLoc dl = getBranchDebugLoc(PrevBB);
1182         TII->RemoveBranch(PrevBB);
1183         TII->InsertBranch(PrevBB, PriorFBB, 0, NewPriorCond, dl);
1184         MadeChange = true;
1185         ++NumBranchOpts;
1186         goto ReoptimizeBlock;
1187       }
1188     }
1190     // If this block has no successors (e.g. it is a return block or ends with
1191     // a call to a no-return function like abort or __cxa_throw) and if the pred
1192     // falls through into this block, and if it would otherwise fall through
1193     // into the block after this, move this block to the end of the function.
1194     //
1195     // We consider it more likely that execution will stay in the function (e.g.
1196     // due to loops) than it is to exit it.  This asserts in loops etc, moving
1197     // the assert condition out of the loop body.
1198     if (MBB->succ_empty() && !PriorCond.empty() && PriorFBB == 0 &&
1199         MachineFunction::iterator(PriorTBB) == FallThrough &&
1200         !MBB->canFallThrough()) {
1201       bool DoTransform = true;
1203       // We have to be careful that the succs of PredBB aren't both no-successor
1204       // blocks.  If neither have successors and if PredBB is the second from
1205       // last block in the function, we'd just keep swapping the two blocks for
1206       // last.  Only do the swap if one is clearly better to fall through than
1207       // the other.
1208       if (FallThrough == --MF.end() &&
1209           !IsBetterFallthrough(PriorTBB, MBB))
1210         DoTransform = false;
1212       if (DoTransform) {
1213         // Reverse the branch so we will fall through on the previous true cond.
1214         SmallVector<MachineOperand, 4> NewPriorCond(PriorCond);
1215         if (!TII->ReverseBranchCondition(NewPriorCond)) {
1216           DEBUG(dbgs() << "\nMoving MBB: " << *MBB
1217                        << "To make fallthrough to: " << *PriorTBB << "\n");
1219           DebugLoc dl = getBranchDebugLoc(PrevBB);
1220           TII->RemoveBranch(PrevBB);
1221           TII->InsertBranch(PrevBB, MBB, 0, NewPriorCond, dl);
1223           // Move this block to the end of the function.
1224           MBB->moveAfter(--MF.end());
1225           MadeChange = true;
1226           ++NumBranchOpts;
1227           return MadeChange;
1228         }
1229       }
1230     }
1231   }
1233   // Analyze the branch in the current block.
1234   MachineBasicBlock *CurTBB = 0, *CurFBB = 0;
1235   SmallVector<MachineOperand, 4> CurCond;
1236   bool CurUnAnalyzable= TII->AnalyzeBranch(*MBB, CurTBB, CurFBB, CurCond, true);
1237   if (!CurUnAnalyzable) {
1238     // If the CFG for the prior block has extra edges, remove them.
1239     MadeChange |= MBB->CorrectExtraCFGEdges(CurTBB, CurFBB, !CurCond.empty());
1241     // If this is a two-way branch, and the FBB branches to this block, reverse
1242     // the condition so the single-basic-block loop is faster.  Instead of:
1243     //    Loop: xxx; jcc Out; jmp Loop
1244     // we want:
1245     //    Loop: xxx; jncc Loop; jmp Out
1246     if (CurTBB && CurFBB && CurFBB == MBB && CurTBB != MBB) {
1247       SmallVector<MachineOperand, 4> NewCond(CurCond);
1248       if (!TII->ReverseBranchCondition(NewCond)) {
1249         DebugLoc dl = getBranchDebugLoc(*MBB);
1250         TII->RemoveBranch(*MBB);
1251         TII->InsertBranch(*MBB, CurFBB, CurTBB, NewCond, dl);
1252         MadeChange = true;
1253         ++NumBranchOpts;
1254         goto ReoptimizeBlock;
1255       }
1256     }
1258     // If this branch is the only thing in its block, see if we can forward
1259     // other blocks across it.
1260     if (CurTBB && CurCond.empty() && CurFBB == 0 &&
1261         IsBranchOnlyBlock(MBB) && CurTBB != MBB &&
1262         !MBB->hasAddressTaken()) {
1263       DebugLoc dl = getBranchDebugLoc(*MBB);
1264       // This block may contain just an unconditional branch.  Because there can
1265       // be 'non-branch terminators' in the block, try removing the branch and
1266       // then seeing if the block is empty.
1267       TII->RemoveBranch(*MBB);
1268       // If the only things remaining in the block are debug info, remove these
1269       // as well, so this will behave the same as an empty block in non-debug
1270       // mode.
1271       if (!MBB->empty()) {
1272         bool NonDebugInfoFound = false;
1273         for (MachineBasicBlock::iterator I = MBB->begin(), E = MBB->end();
1274              I != E; ++I) {
1275           if (!I->isDebugValue()) {
1276             NonDebugInfoFound = true;
1277             break;
1278           }
1279         }
1280         if (!NonDebugInfoFound)
1281           // Make the block empty, losing the debug info (we could probably
1282           // improve this in some cases.)
1283           MBB->erase(MBB->begin(), MBB->end());
1284       }
1285       // If this block is just an unconditional branch to CurTBB, we can
1286       // usually completely eliminate the block.  The only case we cannot
1287       // completely eliminate the block is when the block before this one
1288       // falls through into MBB and we can't understand the prior block's branch
1289       // condition.
1290       if (MBB->empty()) {
1291         bool PredHasNoFallThrough = !PrevBB.canFallThrough();
1292         if (PredHasNoFallThrough || !PriorUnAnalyzable ||
1293             !PrevBB.isSuccessor(MBB)) {
1294           // If the prior block falls through into us, turn it into an
1295           // explicit branch to us to make updates simpler.
1296           if (!PredHasNoFallThrough && PrevBB.isSuccessor(MBB) &&
1297               PriorTBB != MBB && PriorFBB != MBB) {
1298             if (PriorTBB == 0) {
1299               assert(PriorCond.empty() && PriorFBB == 0 &&
1300                      "Bad branch analysis");
1301               PriorTBB = MBB;
1302             } else {
1303               assert(PriorFBB == 0 && "Machine CFG out of date!");
1304               PriorFBB = MBB;
1305             }
1306             DebugLoc pdl = getBranchDebugLoc(PrevBB);
1307             TII->RemoveBranch(PrevBB);
1308             TII->InsertBranch(PrevBB, PriorTBB, PriorFBB, PriorCond, pdl);
1309           }
1311           // Iterate through all the predecessors, revectoring each in-turn.
1312           size_t PI = 0;
1313           bool DidChange = false;
1314           bool HasBranchToSelf = false;
1315           while(PI != MBB->pred_size()) {
1316             MachineBasicBlock *PMBB = *(MBB->pred_begin() + PI);
1317             if (PMBB == MBB) {
1318               // If this block has an uncond branch to itself, leave it.
1319               ++PI;
1320               HasBranchToSelf = true;
1321             } else {
1322               DidChange = true;
1323               PMBB->ReplaceUsesOfBlockWith(MBB, CurTBB);
1324               // If this change resulted in PMBB ending in a conditional
1325               // branch where both conditions go to the same destination,
1326               // change this to an unconditional branch (and fix the CFG).
1327               MachineBasicBlock *NewCurTBB = 0, *NewCurFBB = 0;
1328               SmallVector<MachineOperand, 4> NewCurCond;
1329               bool NewCurUnAnalyzable = TII->AnalyzeBranch(*PMBB, NewCurTBB,
1330                       NewCurFBB, NewCurCond, true);
1331               if (!NewCurUnAnalyzable && NewCurTBB && NewCurTBB == NewCurFBB) {
1332                 DebugLoc pdl = getBranchDebugLoc(*PMBB);
1333                 TII->RemoveBranch(*PMBB);
1334                 NewCurCond.clear();
1335                 TII->InsertBranch(*PMBB, NewCurTBB, 0, NewCurCond, pdl);
1336                 MadeChange = true;
1337                 ++NumBranchOpts;
1338                 PMBB->CorrectExtraCFGEdges(NewCurTBB, 0, false);
1339               }
1340             }
1341           }
1343           // Change any jumptables to go to the new MBB.
1344           if (MachineJumpTableInfo *MJTI = MF.getJumpTableInfo())
1345             MJTI->ReplaceMBBInJumpTables(MBB, CurTBB);
1346           if (DidChange) {
1347             ++NumBranchOpts;
1348             MadeChange = true;
1349             if (!HasBranchToSelf) return MadeChange;
1350           }
1351         }
1352       }
1354       // Add the branch back if the block is more than just an uncond branch.
1355       TII->InsertBranch(*MBB, CurTBB, 0, CurCond, dl);
1356     }
1357   }
1359   // If the prior block doesn't fall through into this block, and if this
1360   // block doesn't fall through into some other block, see if we can find a
1361   // place to move this block where a fall-through will happen.
1362   if (!PrevBB.canFallThrough()) {
1364     // Now we know that there was no fall-through into this block, check to
1365     // see if it has a fall-through into its successor.
1366     bool CurFallsThru = MBB->canFallThrough();
1368     if (!MBB->isLandingPad()) {
1369       // Check all the predecessors of this block.  If one of them has no fall
1370       // throughs, move this block right after it.
1371       for (MachineBasicBlock::pred_iterator PI = MBB->pred_begin(),
1372            E = MBB->pred_end(); PI != E; ++PI) {
1373         // Analyze the branch at the end of the pred.
1374         MachineBasicBlock *PredBB = *PI;
1375         MachineFunction::iterator PredFallthrough = PredBB; ++PredFallthrough;
1376         MachineBasicBlock *PredTBB = 0, *PredFBB = 0;
1377         SmallVector<MachineOperand, 4> PredCond;
1378         if (PredBB != MBB && !PredBB->canFallThrough() &&
1379             !TII->AnalyzeBranch(*PredBB, PredTBB, PredFBB, PredCond, true)
1380             && (!CurFallsThru || !CurTBB || !CurFBB)
1381             && (!CurFallsThru || MBB->getNumber() >= PredBB->getNumber())) {
1382           // If the current block doesn't fall through, just move it.
1383           // If the current block can fall through and does not end with a
1384           // conditional branch, we need to append an unconditional jump to
1385           // the (current) next block.  To avoid a possible compile-time
1386           // infinite loop, move blocks only backward in this case.
1387           // Also, if there are already 2 branches here, we cannot add a third;
1388           // this means we have the case
1389           // Bcc next
1390           // B elsewhere
1391           // next:
1392           if (CurFallsThru) {
1393             MachineBasicBlock *NextBB = llvm::next(MachineFunction::iterator(MBB));
1394             CurCond.clear();
1395             TII->InsertBranch(*MBB, NextBB, 0, CurCond, DebugLoc());
1396           }
1397           MBB->moveAfter(PredBB);
1398           MadeChange = true;
1399           goto ReoptimizeBlock;
1400         }
1401       }
1402     }
1404     if (!CurFallsThru) {
1405       // Check all successors to see if we can move this block before it.
1406       for (MachineBasicBlock::succ_iterator SI = MBB->succ_begin(),
1407            E = MBB->succ_end(); SI != E; ++SI) {
1408         // Analyze the branch at the end of the block before the succ.
1409         MachineBasicBlock *SuccBB = *SI;
1410         MachineFunction::iterator SuccPrev = SuccBB; --SuccPrev;
1412         // If this block doesn't already fall-through to that successor, and if
1413         // the succ doesn't already have a block that can fall through into it,
1414         // and if the successor isn't an EH destination, we can arrange for the
1415         // fallthrough to happen.
1416         if (SuccBB != MBB && &*SuccPrev != MBB &&
1417             !SuccPrev->canFallThrough() && !CurUnAnalyzable &&
1418             !SuccBB->isLandingPad()) {
1419           MBB->moveBefore(SuccBB);
1420           MadeChange = true;
1421           goto ReoptimizeBlock;
1422         }
1423       }
1425       // Okay, there is no really great place to put this block.  If, however,
1426       // the block before this one would be a fall-through if this block were
1427       // removed, move this block to the end of the function.
1428       MachineBasicBlock *PrevTBB = 0, *PrevFBB = 0;
1429       SmallVector<MachineOperand, 4> PrevCond;
1430       if (FallThrough != MF.end() &&
1431           !TII->AnalyzeBranch(PrevBB, PrevTBB, PrevFBB, PrevCond, true) &&
1432           PrevBB.isSuccessor(FallThrough)) {
1433         MBB->moveAfter(--MF.end());
1434         MadeChange = true;
1435         return MadeChange;
1436       }
1437     }
1438   }
1440   return MadeChange;
1443 //===----------------------------------------------------------------------===//
1444 //  Hoist Common Code
1445 //===----------------------------------------------------------------------===//
1447 /// HoistCommonCode - Hoist common instruction sequences at the start of basic
1448 /// blocks to their common predecessor.
1449 bool BranchFolder::HoistCommonCode(MachineFunction &MF) {
1450   bool MadeChange = false;
1451   for (MachineFunction::iterator I = MF.begin(), E = MF.end(); I != E; ) {
1452     MachineBasicBlock *MBB = I++;
1453     MadeChange |= HoistCommonCodeInSuccs(MBB);
1454   }
1456   return MadeChange;
1459 /// findFalseBlock - BB has a fallthrough. Find its 'false' successor given
1460 /// its 'true' successor.
1461 static MachineBasicBlock *findFalseBlock(MachineBasicBlock *BB,
1462                                          MachineBasicBlock *TrueBB) {
1463   for (MachineBasicBlock::succ_iterator SI = BB->succ_begin(),
1464          E = BB->succ_end(); SI != E; ++SI) {
1465     MachineBasicBlock *SuccBB = *SI;
1466     if (SuccBB != TrueBB)
1467       return SuccBB;
1468   }
1469   return NULL;
1472 /// findHoistingInsertPosAndDeps - Find the location to move common instructions
1473 /// in successors to. The location is usually just before the terminator,
1474 /// however if the terminator is a conditional branch and its previous
1475 /// instruction is the flag setting instruction, the previous instruction is
1476 /// the preferred location. This function also gathers uses and defs of the
1477 /// instructions from the insertion point to the end of the block. The data is
1478 /// used by HoistCommonCodeInSuccs to ensure safety.
1479 static
1480 MachineBasicBlock::iterator findHoistingInsertPosAndDeps(MachineBasicBlock *MBB,
1481                                                   const TargetInstrInfo *TII,
1482                                                   const TargetRegisterInfo *TRI,
1483                                                   SmallSet<unsigned,4> &Uses,
1484                                                   SmallSet<unsigned,4> &Defs) {
1485   MachineBasicBlock::iterator Loc = MBB->getFirstTerminator();
1486   if (!TII->isUnpredicatedTerminator(Loc))
1487     return MBB->end();
1489   for (unsigned i = 0, e = Loc->getNumOperands(); i != e; ++i) {
1490     const MachineOperand &MO = Loc->getOperand(i);
1491     if (!MO.isReg())
1492       continue;
1493     unsigned Reg = MO.getReg();
1494     if (!Reg)
1495       continue;
1496     if (MO.isUse()) {
1497       for (MCRegAliasIterator AI(Reg, TRI, true); AI.isValid(); ++AI)
1498         Uses.insert(*AI);
1499     } else if (!MO.isDead())
1500       // Don't try to hoist code in the rare case the terminator defines a
1501       // register that is later used.
1502       return MBB->end();
1503   }
1505   if (Uses.empty())
1506     return Loc;
1507   if (Loc == MBB->begin())
1508     return MBB->end();
1510   // The terminator is probably a conditional branch, try not to separate the
1511   // branch from condition setting instruction.
1512   MachineBasicBlock::iterator PI = Loc;
1513   --PI;
1514   while (PI != MBB->begin() && Loc->isDebugValue())
1515     --PI;
1517   bool IsDef = false;
1518   for (unsigned i = 0, e = PI->getNumOperands(); !IsDef && i != e; ++i) {
1519     const MachineOperand &MO = PI->getOperand(i);
1520     // If PI has a regmask operand, it is probably a call. Separate away.
1521     if (MO.isRegMask())
1522       return Loc;
1523     if (!MO.isReg() || MO.isUse())
1524       continue;
1525     unsigned Reg = MO.getReg();
1526     if (!Reg)
1527       continue;
1528     if (Uses.count(Reg))
1529       IsDef = true;
1530   }
1531   if (!IsDef)
1532     // The condition setting instruction is not just before the conditional
1533     // branch.
1534     return Loc;
1536   // Be conservative, don't insert instruction above something that may have
1537   // side-effects. And since it's potentially bad to separate flag setting
1538   // instruction from the conditional branch, just abort the optimization
1539   // completely.
1540   // Also avoid moving code above predicated instruction since it's hard to
1541   // reason about register liveness with predicated instruction.
1542   bool DontMoveAcrossStore = true;
1543   if (!PI->isSafeToMove(TII, 0, DontMoveAcrossStore) ||
1544       TII->isPredicated(PI))
1545     return MBB->end();
1548   // Find out what registers are live. Note this routine is ignoring other live
1549   // registers which are only used by instructions in successor blocks.
1550   for (unsigned i = 0, e = PI->getNumOperands(); i != e; ++i) {
1551     const MachineOperand &MO = PI->getOperand(i);
1552     if (!MO.isReg())
1553       continue;
1554     unsigned Reg = MO.getReg();
1555     if (!Reg)
1556       continue;
1557     if (MO.isUse()) {
1558       for (MCRegAliasIterator AI(Reg, TRI, true); AI.isValid(); ++AI)
1559         Uses.insert(*AI);
1560     } else {
1561       if (Uses.erase(Reg)) {
1562         for (MCSubRegIterator SubRegs(Reg, TRI); SubRegs.isValid(); ++SubRegs)
1563           Uses.erase(*SubRegs); // Use sub-registers to be conservative
1564       }
1565       for (MCRegAliasIterator AI(Reg, TRI, true); AI.isValid(); ++AI)
1566         Defs.insert(*AI);
1567     }
1568   }
1570   return PI;
1573 /// HoistCommonCodeInSuccs - If the successors of MBB has common instruction
1574 /// sequence at the start of the function, move the instructions before MBB
1575 /// terminator if it's legal.
1576 bool BranchFolder::HoistCommonCodeInSuccs(MachineBasicBlock *MBB) {
1577   MachineBasicBlock *TBB = 0, *FBB = 0;
1578   SmallVector<MachineOperand, 4> Cond;
1579   if (TII->AnalyzeBranch(*MBB, TBB, FBB, Cond, true) || !TBB || Cond.empty())
1580     return false;
1582   if (!FBB) FBB = findFalseBlock(MBB, TBB);
1583   if (!FBB)
1584     // Malformed bcc? True and false blocks are the same?
1585     return false;
1587   // Restrict the optimization to cases where MBB is the only predecessor,
1588   // it is an obvious win.
1589   if (TBB->pred_size() > 1 || FBB->pred_size() > 1)
1590     return false;
1592   // Find a suitable position to hoist the common instructions to. Also figure
1593   // out which registers are used or defined by instructions from the insertion
1594   // point to the end of the block.
1595   SmallSet<unsigned, 4> Uses, Defs;
1596   MachineBasicBlock::iterator Loc =
1597     findHoistingInsertPosAndDeps(MBB, TII, TRI, Uses, Defs);
1598   if (Loc == MBB->end())
1599     return false;
1601   bool HasDups = false;
1602   SmallVector<unsigned, 4> LocalDefs;
1603   SmallSet<unsigned, 4> LocalDefsSet;
1604   MachineBasicBlock::iterator TIB = TBB->begin();
1605   MachineBasicBlock::iterator FIB = FBB->begin();
1606   MachineBasicBlock::iterator TIE = TBB->end();
1607   MachineBasicBlock::iterator FIE = FBB->end();
1608   while (TIB != TIE && FIB != FIE) {
1609     // Skip dbg_value instructions. These do not count.
1610     if (TIB->isDebugValue()) {
1611       while (TIB != TIE && TIB->isDebugValue())
1612         ++TIB;
1613       if (TIB == TIE)
1614         break;
1615     }
1616     if (FIB->isDebugValue()) {
1617       while (FIB != FIE && FIB->isDebugValue())
1618         ++FIB;
1619       if (FIB == FIE)
1620         break;
1621     }
1622     if (!TIB->isIdenticalTo(FIB, MachineInstr::CheckKillDead))
1623       break;
1625     if (TII->isPredicated(TIB))
1626       // Hard to reason about register liveness with predicated instruction.
1627       break;
1629     bool IsSafe = true;
1630     for (unsigned i = 0, e = TIB->getNumOperands(); i != e; ++i) {
1631       MachineOperand &MO = TIB->getOperand(i);
1632       // Don't attempt to hoist instructions with register masks.
1633       if (MO.isRegMask()) {
1634         IsSafe = false;
1635         break;
1636       }
1637       if (!MO.isReg())
1638         continue;
1639       unsigned Reg = MO.getReg();
1640       if (!Reg)
1641         continue;
1642       if (MO.isDef()) {
1643         if (Uses.count(Reg)) {
1644           // Avoid clobbering a register that's used by the instruction at
1645           // the point of insertion.
1646           IsSafe = false;
1647           break;
1648         }
1650         if (Defs.count(Reg) && !MO.isDead()) {
1651           // Don't hoist the instruction if the def would be clobber by the
1652           // instruction at the point insertion. FIXME: This is overly
1653           // conservative. It should be possible to hoist the instructions
1654           // in BB2 in the following example:
1655           // BB1:
1656           // r1, eflag = op1 r2, r3
1657           // brcc eflag
1658           //
1659           // BB2:
1660           // r1 = op2, ...
1661           //    = op3, r1<kill>
1662           IsSafe = false;
1663           break;
1664         }
1665       } else if (!LocalDefsSet.count(Reg)) {
1666         if (Defs.count(Reg)) {
1667           // Use is defined by the instruction at the point of insertion.
1668           IsSafe = false;
1669           break;
1670         }
1672         if (MO.isKill() && Uses.count(Reg))
1673           // Kills a register that's read by the instruction at the point of
1674           // insertion. Remove the kill marker.
1675           MO.setIsKill(false);
1676       }
1677     }
1678     if (!IsSafe)
1679       break;
1681     bool DontMoveAcrossStore = true;
1682     if (!TIB->isSafeToMove(TII, 0, DontMoveAcrossStore))
1683       break;
1685     // Remove kills from LocalDefsSet, these registers had short live ranges.
1686     for (unsigned i = 0, e = TIB->getNumOperands(); i != e; ++i) {
1687       MachineOperand &MO = TIB->getOperand(i);
1688       if (!MO.isReg() || !MO.isUse() || !MO.isKill())
1689         continue;
1690       unsigned Reg = MO.getReg();
1691       if (!Reg || !LocalDefsSet.count(Reg))
1692         continue;
1693       for (MCRegAliasIterator AI(Reg, TRI, true); AI.isValid(); ++AI)
1694         LocalDefsSet.erase(*AI);
1695     }
1697     // Track local defs so we can update liveins.
1698     for (unsigned i = 0, e = TIB->getNumOperands(); i != e; ++i) {
1699       MachineOperand &MO = TIB->getOperand(i);
1700       if (!MO.isReg() || !MO.isDef() || MO.isDead())
1701         continue;
1702       unsigned Reg = MO.getReg();
1703       if (!Reg)
1704         continue;
1705       LocalDefs.push_back(Reg);
1706       for (MCRegAliasIterator AI(Reg, TRI, true); AI.isValid(); ++AI)
1707         LocalDefsSet.insert(*AI);
1708     }
1710     HasDups = true;
1711     ++TIB;
1712     ++FIB;
1713   }
1715   if (!HasDups)
1716     return false;
1718   MBB->splice(Loc, TBB, TBB->begin(), TIB);
1719   FBB->erase(FBB->begin(), FIB);
1721   // Update livein's.
1722   for (unsigned i = 0, e = LocalDefs.size(); i != e; ++i) {
1723     unsigned Def = LocalDefs[i];
1724     if (LocalDefsSet.count(Def)) {
1725       TBB->addLiveIn(Def);
1726       FBB->addLiveIn(Def);
1727     }
1728   }
1730   ++NumHoist;
1731   return true;