1 //=- llvm/CodeGen/DFAPacketizer.cpp - DFA Packetizer for VLIW -*- C++ -*-=====//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 // This class implements a deterministic finite automaton (DFA) based
10 // packetizing mechanism for VLIW architectures. It provides APIs to
11 // determine whether there exists a legal mapping of instructions to
12 // functional unit assignments in a packet. The DFA is auto-generated from
13 // the target's Schedule.td file.
14 //
15 // A DFA consists of 3 major elements: states, inputs, and transitions. For
16 // the packetizing mechanism, the input is the set of instruction classes for
17 // a target. The state models all possible combinations of functional unit
18 // consumption for a given set of instructions in a packet. A transition
19 // models the addition of an instruction to a packet. In the DFA constructed
20 // by this class, if an instruction can be added to a packet, then a valid
21 // transition exists from the corresponding state. Invalid transitions
22 // indicate that the instruction cannot be added to the current packet.
23 //
24 //===----------------------------------------------------------------------===//
26 #include "llvm/CodeGen/DFAPacketizer.h"
27 #include "llvm/CodeGen/MachineInstr.h"
28 #include "llvm/CodeGen/MachineInstrBundle.h"
29 #include "llvm/CodeGen/ScheduleDAGInstrs.h"
30 #include "llvm/MC/MCInstrItineraries.h"
31 #include "llvm/Target/TargetInstrInfo.h"
32 using namespace llvm;
34 DFAPacketizer::DFAPacketizer(const InstrItineraryData *I, const int (*SIT)[2],
35 const unsigned *SET):
36 InstrItins(I), CurrentState(0), DFAStateInputTable(SIT),
37 DFAStateEntryTable(SET) {}
40 //
41 // ReadTable - Read the DFA transition table and update CachedTable.
42 //
43 // Format of the transition tables:
44 // DFAStateInputTable[][2] = pairs of <Input, Transition> for all valid
45 // transitions
46 // DFAStateEntryTable[i] = Index of the first entry in DFAStateInputTable
47 // for the ith state
48 //
49 void DFAPacketizer::ReadTable(unsigned int state) {
50 unsigned ThisState = DFAStateEntryTable[state];
51 unsigned NextStateInTable = DFAStateEntryTable[state+1];
52 // Early exit in case CachedTable has already contains this
53 // state's transitions.
54 if (CachedTable.count(UnsignPair(state,
55 DFAStateInputTable[ThisState][0])))
56 return;
58 for (unsigned i = ThisState; i < NextStateInTable; i++)
59 CachedTable[UnsignPair(state, DFAStateInputTable[i][0])] =
60 DFAStateInputTable[i][1];
61 }
64 // canReserveResources - Check if the resources occupied by a MCInstrDesc
65 // are available in the current state.
66 bool DFAPacketizer::canReserveResources(const llvm::MCInstrDesc *MID) {
67 unsigned InsnClass = MID->getSchedClass();
68 const llvm::InstrStage *IS = InstrItins->beginStage(InsnClass);
69 unsigned FuncUnits = IS->getUnits();
70 UnsignPair StateTrans = UnsignPair(CurrentState, FuncUnits);
71 ReadTable(CurrentState);
72 return (CachedTable.count(StateTrans) != 0);
73 }
76 // reserveResources - Reserve the resources occupied by a MCInstrDesc and
77 // change the current state to reflect that change.
78 void DFAPacketizer::reserveResources(const llvm::MCInstrDesc *MID) {
79 unsigned InsnClass = MID->getSchedClass();
80 const llvm::InstrStage *IS = InstrItins->beginStage(InsnClass);
81 unsigned FuncUnits = IS->getUnits();
82 UnsignPair StateTrans = UnsignPair(CurrentState, FuncUnits);
83 ReadTable(CurrentState);
84 assert(CachedTable.count(StateTrans) != 0);
85 CurrentState = CachedTable[StateTrans];
86 }
89 // canReserveResources - Check if the resources occupied by a machine
90 // instruction are available in the current state.
91 bool DFAPacketizer::canReserveResources(llvm::MachineInstr *MI) {
92 const llvm::MCInstrDesc &MID = MI->getDesc();
93 return canReserveResources(&MID);
94 }
96 // reserveResources - Reserve the resources occupied by a machine
97 // instruction and change the current state to reflect that change.
98 void DFAPacketizer::reserveResources(llvm::MachineInstr *MI) {
99 const llvm::MCInstrDesc &MID = MI->getDesc();
100 reserveResources(&MID);
101 }
103 namespace llvm {
104 // DefaultVLIWScheduler - This class extends ScheduleDAGInstrs and overrides
105 // Schedule method to build the dependence graph.
106 class DefaultVLIWScheduler : public ScheduleDAGInstrs {
107 public:
108 DefaultVLIWScheduler(MachineFunction &MF, MachineLoopInfo &MLI,
109 bool IsPostRA);
110 // Schedule - Actual scheduling work.
111 void schedule() override;
112 };
113 }
115 DefaultVLIWScheduler::DefaultVLIWScheduler(MachineFunction &MF,
116 MachineLoopInfo &MLI, bool IsPostRA)
117 : ScheduleDAGInstrs(MF, &MLI, IsPostRA) {
118 CanHandleTerminators = true;
119 }
121 void DefaultVLIWScheduler::schedule() {
122 // Build the scheduling graph.
123 buildSchedGraph(nullptr);
124 }
126 // VLIWPacketizerList Ctor
127 VLIWPacketizerList::VLIWPacketizerList(MachineFunction &MF,
128 MachineLoopInfo &MLI, bool IsPostRA)
129 : TM(MF.getTarget()), MF(MF) {
130 TII = TM.getSubtargetImpl()->getInstrInfo();
131 ResourceTracker = TII->CreateTargetScheduleState(MF.getSubtarget());
132 VLIWScheduler = new DefaultVLIWScheduler(MF, MLI, IsPostRA);
133 }
135 // VLIWPacketizerList Dtor
136 VLIWPacketizerList::~VLIWPacketizerList() {
137 if (VLIWScheduler)
138 delete VLIWScheduler;
140 if (ResourceTracker)
141 delete ResourceTracker;
142 }
144 // endPacket - End the current packet, bundle packet instructions and reset
145 // DFA state.
146 void VLIWPacketizerList::endPacket(MachineBasicBlock *MBB,
147 MachineInstr *MI) {
148 if (CurrentPacketMIs.size() > 1) {
149 MachineInstr *MIFirst = CurrentPacketMIs.front();
150 finalizeBundle(*MBB, MIFirst, MI);
151 }
152 CurrentPacketMIs.clear();
153 ResourceTracker->clearResources();
154 }
156 // PacketizeMIs - Bundle machine instructions into packets.
157 void VLIWPacketizerList::PacketizeMIs(MachineBasicBlock *MBB,
158 MachineBasicBlock::iterator BeginItr,
159 MachineBasicBlock::iterator EndItr) {
160 assert(VLIWScheduler && "VLIW Scheduler is not initialized!");
161 VLIWScheduler->startBlock(MBB);
162 VLIWScheduler->enterRegion(MBB, BeginItr, EndItr,
163 std::distance(BeginItr, EndItr));
164 VLIWScheduler->schedule();
166 // Generate MI -> SU map.
167 MIToSUnit.clear();
168 for (unsigned i = 0, e = VLIWScheduler->SUnits.size(); i != e; ++i) {
169 SUnit *SU = &VLIWScheduler->SUnits[i];
170 MIToSUnit[SU->getInstr()] = SU;
171 }
173 // The main packetizer loop.
174 for (; BeginItr != EndItr; ++BeginItr) {
175 MachineInstr *MI = BeginItr;
177 this->initPacketizerState();
179 // End the current packet if needed.
180 if (this->isSoloInstruction(MI)) {
181 endPacket(MBB, MI);
182 continue;
183 }
185 // Ignore pseudo instructions.
186 if (this->ignorePseudoInstruction(MI, MBB))
187 continue;
189 SUnit *SUI = MIToSUnit[MI];
190 assert(SUI && "Missing SUnit Info!");
192 // Ask DFA if machine resource is available for MI.
193 bool ResourceAvail = ResourceTracker->canReserveResources(MI);
194 if (ResourceAvail) {
195 // Dependency check for MI with instructions in CurrentPacketMIs.
196 for (std::vector<MachineInstr*>::iterator VI = CurrentPacketMIs.begin(),
197 VE = CurrentPacketMIs.end(); VI != VE; ++VI) {
198 MachineInstr *MJ = *VI;
199 SUnit *SUJ = MIToSUnit[MJ];
200 assert(SUJ && "Missing SUnit Info!");
202 // Is it legal to packetize SUI and SUJ together.
203 if (!this->isLegalToPacketizeTogether(SUI, SUJ)) {
204 // Allow packetization if dependency can be pruned.
205 if (!this->isLegalToPruneDependencies(SUI, SUJ)) {
206 // End the packet if dependency cannot be pruned.
207 endPacket(MBB, MI);
208 break;
209 } // !isLegalToPruneDependencies.
210 } // !isLegalToPacketizeTogether.
211 } // For all instructions in CurrentPacketMIs.
212 } else {
213 // End the packet if resource is not available.
214 endPacket(MBB, MI);
215 }
217 // Add MI to the current packet.
218 BeginItr = this->addToPacket(MI);
219 } // For all instructions in BB.
221 // End any packet left behind.
222 endPacket(MBB, EndItr);
223 VLIWScheduler->exitRegion();
224 VLIWScheduler->finishBlock();
225 }