]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/GCStrategy.cpp
Replace the dangling context hotfix with an assertion.
[opencl/llvm.git] / lib / CodeGen / GCStrategy.cpp
1 //===-- GCStrategy.cpp - Garbage collection infrastructure -----------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements target- and collector-independent garbage collection
11 // infrastructure.
12 //
13 // GCMachineCodeAnalysis identifies the GC safe points in the machine code.
14 // Roots are identified in SelectionDAGISel.
15 //
16 //===----------------------------------------------------------------------===//
18 #include "llvm/CodeGen/GCStrategy.h"
19 #include "llvm/Analysis/DominatorInternals.h"
20 #include "llvm/Analysis/Dominators.h"
21 #include "llvm/CodeGen/MachineFrameInfo.h"
22 #include "llvm/CodeGen/MachineFunctionPass.h"
23 #include "llvm/CodeGen/MachineInstrBuilder.h"
24 #include "llvm/CodeGen/MachineModuleInfo.h"
25 #include "llvm/CodeGen/Passes.h"
26 #include "llvm/IR/IntrinsicInst.h"
27 #include "llvm/IR/Module.h"
28 #include "llvm/Support/Debug.h"
29 #include "llvm/Support/ErrorHandling.h"
30 #include "llvm/Support/raw_ostream.h"
31 #include "llvm/Target/TargetFrameLowering.h"
32 #include "llvm/Target/TargetInstrInfo.h"
33 #include "llvm/Target/TargetMachine.h"
34 #include "llvm/Target/TargetRegisterInfo.h"
36 using namespace llvm;
38 namespace {
40   /// LowerIntrinsics - This pass rewrites calls to the llvm.gcread or
41   /// llvm.gcwrite intrinsics, replacing them with simple loads and stores as
42   /// directed by the GCStrategy. It also performs automatic root initialization
43   /// and custom intrinsic lowering.
44   class LowerIntrinsics : public FunctionPass {
45     static bool NeedsDefaultLoweringPass(const GCStrategy &C);
46     static bool NeedsCustomLoweringPass(const GCStrategy &C);
47     static bool CouldBecomeSafePoint(Instruction *I);
48     bool PerformDefaultLowering(Function &F, GCStrategy &Coll);
49     static bool InsertRootInitializers(Function &F,
50                                        AllocaInst **Roots, unsigned Count);
52   public:
53     static char ID;
55     LowerIntrinsics();
56     const char *getPassName() const;
57     void getAnalysisUsage(AnalysisUsage &AU) const;
59     bool doInitialization(Module &M);
60     bool runOnFunction(Function &F);
61   };
64   /// GCMachineCodeAnalysis - This is a target-independent pass over the machine
65   /// function representation to identify safe points for the garbage collector
66   /// in the machine code. It inserts labels at safe points and populates a
67   /// GCMetadata record for each function.
68   class GCMachineCodeAnalysis : public MachineFunctionPass {
69     const TargetMachine *TM;
70     GCFunctionInfo *FI;
71     MachineModuleInfo *MMI;
72     const TargetInstrInfo *TII;
74     void FindSafePoints(MachineFunction &MF);
75     void VisitCallPoint(MachineBasicBlock::iterator MI);
76     MCSymbol *InsertLabel(MachineBasicBlock &MBB,
77                           MachineBasicBlock::iterator MI,
78                           DebugLoc DL) const;
80     void FindStackOffsets(MachineFunction &MF);
82   public:
83     static char ID;
85     GCMachineCodeAnalysis();
86     void getAnalysisUsage(AnalysisUsage &AU) const;
88     bool runOnMachineFunction(MachineFunction &MF);
89   };
91 }
93 // -----------------------------------------------------------------------------
95 GCStrategy::GCStrategy() :
96   NeededSafePoints(0),
97   CustomReadBarriers(false),
98   CustomWriteBarriers(false),
99   CustomRoots(false),
100   CustomSafePoints(false),
101   InitRoots(true),
102   UsesMetadata(false)
103 {}
105 GCStrategy::~GCStrategy() {
106   for (iterator I = begin(), E = end(); I != E; ++I)
107     delete *I;
109   Functions.clear();
112 bool GCStrategy::initializeCustomLowering(Module &M) { return false; }
114 bool GCStrategy::performCustomLowering(Function &F) {
115   dbgs() << "gc " << getName() << " must override performCustomLowering.\n";
116   llvm_unreachable("must override performCustomLowering");
120 bool GCStrategy::findCustomSafePoints(GCFunctionInfo& FI, MachineFunction &F) {
121   dbgs() << "gc " << getName() << " must override findCustomSafePoints.\n";
122   llvm_unreachable(0);
126 GCFunctionInfo *GCStrategy::insertFunctionInfo(const Function &F) {
127   GCFunctionInfo *FI = new GCFunctionInfo(F, *this);
128   Functions.push_back(FI);
129   return FI;
132 // -----------------------------------------------------------------------------
134 INITIALIZE_PASS_BEGIN(LowerIntrinsics, "gc-lowering", "GC Lowering",
135                       false, false)
136 INITIALIZE_PASS_DEPENDENCY(GCModuleInfo)
137 INITIALIZE_PASS_END(LowerIntrinsics, "gc-lowering", "GC Lowering", false, false)
139 FunctionPass *llvm::createGCLoweringPass() {
140   return new LowerIntrinsics();
143 char LowerIntrinsics::ID = 0;
145 LowerIntrinsics::LowerIntrinsics()
146   : FunctionPass(ID) {
147     initializeLowerIntrinsicsPass(*PassRegistry::getPassRegistry());
148   }
150 const char *LowerIntrinsics::getPassName() const {
151   return "Lower Garbage Collection Instructions";
154 void LowerIntrinsics::getAnalysisUsage(AnalysisUsage &AU) const {
155   FunctionPass::getAnalysisUsage(AU);
156   AU.addRequired<GCModuleInfo>();
157   AU.addPreserved<DominatorTree>();
160 /// doInitialization - If this module uses the GC intrinsics, find them now.
161 bool LowerIntrinsics::doInitialization(Module &M) {
162   // FIXME: This is rather antisocial in the context of a JIT since it performs
163   //        work against the entire module. But this cannot be done at
164   //        runFunction time (initializeCustomLowering likely needs to change
165   //        the module).
166   GCModuleInfo *MI = getAnalysisIfAvailable<GCModuleInfo>();
167   assert(MI && "LowerIntrinsics didn't require GCModuleInfo!?");
168   for (Module::iterator I = M.begin(), E = M.end(); I != E; ++I)
169     if (!I->isDeclaration() && I->hasGC())
170       MI->getFunctionInfo(*I); // Instantiate the GC strategy.
172   bool MadeChange = false;
173   for (GCModuleInfo::iterator I = MI->begin(), E = MI->end(); I != E; ++I)
174     if (NeedsCustomLoweringPass(**I))
175       if ((*I)->initializeCustomLowering(M))
176         MadeChange = true;
178   return MadeChange;
181 bool LowerIntrinsics::InsertRootInitializers(Function &F, AllocaInst **Roots,
182                                                           unsigned Count) {
183   // Scroll past alloca instructions.
184   BasicBlock::iterator IP = F.getEntryBlock().begin();
185   while (isa<AllocaInst>(IP)) ++IP;
187   // Search for initializers in the initial BB.
188   SmallPtrSet<AllocaInst*,16> InitedRoots;
189   for (; !CouldBecomeSafePoint(IP); ++IP)
190     if (StoreInst *SI = dyn_cast<StoreInst>(IP))
191       if (AllocaInst *AI =
192           dyn_cast<AllocaInst>(SI->getOperand(1)->stripPointerCasts()))
193         InitedRoots.insert(AI);
195   // Add root initializers.
196   bool MadeChange = false;
198   for (AllocaInst **I = Roots, **E = Roots + Count; I != E; ++I)
199     if (!InitedRoots.count(*I)) {
200       StoreInst* SI = new StoreInst(ConstantPointerNull::get(cast<PointerType>(
201                         cast<PointerType>((*I)->getType())->getElementType())),
202                         *I);
203       SI->insertAfter(*I);
204       MadeChange = true;
205     }
207   return MadeChange;
210 bool LowerIntrinsics::NeedsDefaultLoweringPass(const GCStrategy &C) {
211   // Default lowering is necessary only if read or write barriers have a default
212   // action. The default for roots is no action.
213   return !C.customWriteBarrier()
214       || !C.customReadBarrier()
215       || C.initializeRoots();
218 bool LowerIntrinsics::NeedsCustomLoweringPass(const GCStrategy &C) {
219   // Custom lowering is only necessary if enabled for some action.
220   return C.customWriteBarrier()
221       || C.customReadBarrier()
222       || C.customRoots();
225 /// CouldBecomeSafePoint - Predicate to conservatively determine whether the
226 /// instruction could introduce a safe point.
227 bool LowerIntrinsics::CouldBecomeSafePoint(Instruction *I) {
228   // The natural definition of instructions which could introduce safe points
229   // are:
230   //
231   //   - call, invoke (AfterCall, BeforeCall)
232   //   - phis (Loops)
233   //   - invoke, ret, unwind (Exit)
234   //
235   // However, instructions as seemingly inoccuous as arithmetic can become
236   // libcalls upon lowering (e.g., div i64 on a 32-bit platform), so instead
237   // it is necessary to take a conservative approach.
239   if (isa<AllocaInst>(I) || isa<GetElementPtrInst>(I) ||
240       isa<StoreInst>(I) || isa<LoadInst>(I))
241     return false;
243   // llvm.gcroot is safe because it doesn't do anything at runtime.
244   if (CallInst *CI = dyn_cast<CallInst>(I))
245     if (Function *F = CI->getCalledFunction())
246       if (unsigned IID = F->getIntrinsicID())
247         if (IID == Intrinsic::gcroot)
248           return false;
250   return true;
253 /// runOnFunction - Replace gcread/gcwrite intrinsics with loads and stores.
254 /// Leave gcroot intrinsics; the code generator needs to see those.
255 bool LowerIntrinsics::runOnFunction(Function &F) {
256   // Quick exit for functions that do not use GC.
257   if (!F.hasGC())
258     return false;
260   GCFunctionInfo &FI = getAnalysis<GCModuleInfo>().getFunctionInfo(F);
261   GCStrategy &S = FI.getStrategy();
263   bool MadeChange = false;
265   if (NeedsDefaultLoweringPass(S))
266     MadeChange |= PerformDefaultLowering(F, S);
268   bool UseCustomLoweringPass = NeedsCustomLoweringPass(S);
269   if (UseCustomLoweringPass)
270     MadeChange |= S.performCustomLowering(F);
272   // Custom lowering may modify the CFG, so dominators must be recomputed.
273   if (UseCustomLoweringPass) {
274     if (DominatorTree *DT = getAnalysisIfAvailable<DominatorTree>())
275       DT->DT->recalculate(F);
276   }
278   return MadeChange;
281 bool LowerIntrinsics::PerformDefaultLowering(Function &F, GCStrategy &S) {
282   bool LowerWr = !S.customWriteBarrier();
283   bool LowerRd = !S.customReadBarrier();
284   bool InitRoots = S.initializeRoots();
286   SmallVector<AllocaInst*, 32> Roots;
288   bool MadeChange = false;
289   for (Function::iterator BB = F.begin(), E = F.end(); BB != E; ++BB) {
290     for (BasicBlock::iterator II = BB->begin(), E = BB->end(); II != E;) {
291       if (IntrinsicInst *CI = dyn_cast<IntrinsicInst>(II++)) {
292         Function *F = CI->getCalledFunction();
293         switch (F->getIntrinsicID()) {
294         case Intrinsic::gcwrite:
295           if (LowerWr) {
296             // Replace a write barrier with a simple store.
297             Value *St = new StoreInst(CI->getArgOperand(0),
298                                       CI->getArgOperand(2), CI);
299             CI->replaceAllUsesWith(St);
300             CI->eraseFromParent();
301           }
302           break;
303         case Intrinsic::gcread:
304           if (LowerRd) {
305             // Replace a read barrier with a simple load.
306             Value *Ld = new LoadInst(CI->getArgOperand(1), "", CI);
307             Ld->takeName(CI);
308             CI->replaceAllUsesWith(Ld);
309             CI->eraseFromParent();
310           }
311           break;
312         case Intrinsic::gcroot:
313           if (InitRoots) {
314             // Initialize the GC root, but do not delete the intrinsic. The
315             // backend needs the intrinsic to flag the stack slot.
316             Roots.push_back(cast<AllocaInst>(
317                               CI->getArgOperand(0)->stripPointerCasts()));
318           }
319           break;
320         default:
321           continue;
322         }
324         MadeChange = true;
325       }
326     }
327   }
329   if (Roots.size())
330     MadeChange |= InsertRootInitializers(F, Roots.begin(), Roots.size());
332   return MadeChange;
335 // -----------------------------------------------------------------------------
337 char GCMachineCodeAnalysis::ID = 0;
338 char &llvm::GCMachineCodeAnalysisID = GCMachineCodeAnalysis::ID;
340 INITIALIZE_PASS(GCMachineCodeAnalysis, "gc-analysis",
341                 "Analyze Machine Code For Garbage Collection", false, false)
343 GCMachineCodeAnalysis::GCMachineCodeAnalysis()
344   : MachineFunctionPass(ID) {}
346 void GCMachineCodeAnalysis::getAnalysisUsage(AnalysisUsage &AU) const {
347   MachineFunctionPass::getAnalysisUsage(AU);
348   AU.setPreservesAll();
349   AU.addRequired<MachineModuleInfo>();
350   AU.addRequired<GCModuleInfo>();
353 MCSymbol *GCMachineCodeAnalysis::InsertLabel(MachineBasicBlock &MBB,
354                                              MachineBasicBlock::iterator MI,
355                                              DebugLoc DL) const {
356   MCSymbol *Label = MBB.getParent()->getContext().CreateTempSymbol();
357   BuildMI(MBB, MI, DL, TII->get(TargetOpcode::GC_LABEL)).addSym(Label);
358   return Label;
361 void GCMachineCodeAnalysis::VisitCallPoint(MachineBasicBlock::iterator CI) {
362   // Find the return address (next instruction), too, so as to bracket the call
363   // instruction.
364   MachineBasicBlock::iterator RAI = CI;
365   ++RAI;
367   if (FI->getStrategy().needsSafePoint(GC::PreCall)) {
368     MCSymbol* Label = InsertLabel(*CI->getParent(), CI, CI->getDebugLoc());
369     FI->addSafePoint(GC::PreCall, Label, CI->getDebugLoc());
370   }
372   if (FI->getStrategy().needsSafePoint(GC::PostCall)) {
373     MCSymbol* Label = InsertLabel(*CI->getParent(), RAI, CI->getDebugLoc());
374     FI->addSafePoint(GC::PostCall, Label, CI->getDebugLoc());
375   }
378 void GCMachineCodeAnalysis::FindSafePoints(MachineFunction &MF) {
379   for (MachineFunction::iterator BBI = MF.begin(),
380                                  BBE = MF.end(); BBI != BBE; ++BBI)
381     for (MachineBasicBlock::iterator MI = BBI->begin(),
382                                      ME = BBI->end(); MI != ME; ++MI)
383       if (MI->isCall())
384         VisitCallPoint(MI);
387 void GCMachineCodeAnalysis::FindStackOffsets(MachineFunction &MF) {
388   const TargetFrameLowering *TFI = TM->getFrameLowering();
389   assert(TFI && "TargetRegisterInfo not available!");
391   for (GCFunctionInfo::roots_iterator RI = FI->roots_begin();
392        RI != FI->roots_end();) {
393     // If the root references a dead object, no need to keep it.
394     if (MF.getFrameInfo()->isDeadObjectIndex(RI->Num)) {
395       RI = FI->removeStackRoot(RI);
396     } else {
397       RI->StackOffset = TFI->getFrameIndexOffset(MF, RI->Num);
398       ++RI;
399     }
400   }
403 bool GCMachineCodeAnalysis::runOnMachineFunction(MachineFunction &MF) {
404   // Quick exit for functions that do not use GC.
405   if (!MF.getFunction()->hasGC())
406     return false;
408   FI = &getAnalysis<GCModuleInfo>().getFunctionInfo(*MF.getFunction());
409   if (!FI->getStrategy().needsSafePoints())
410     return false;
412   TM = &MF.getTarget();
413   MMI = &getAnalysis<MachineModuleInfo>();
414   TII = TM->getInstrInfo();
416   // Find the size of the stack frame.
417   FI->setFrameSize(MF.getFrameInfo()->getStackSize());
419   // Find all safe points.
420   if (FI->getStrategy().customSafePoints()) {
421     FI->getStrategy().findCustomSafePoints(*FI, MF);
422   } else {
423     FindSafePoints(MF);
424   }
426   // Find the stack offsets for all roots.
427   FindStackOffsets(MF);
429   return false;