1 //===-- InterferenceCache.h - Caching per-block interference ---*- C++ -*--===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // InterferenceCache remembers per-block interference from LiveIntervalUnions,
11 // fixed RegUnit interference, and register masks.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_CODEGEN_INTERFERENCECACHE
16 #define LLVM_CODEGEN_INTERFERENCECACHE
18 #include "llvm/CodeGen/LiveIntervalUnion.h"
20 namespace llvm {
22 class LiveIntervals;
24 class InterferenceCache {
25 const TargetRegisterInfo *TRI;
26 LiveIntervalUnion *LIUArray;
27 MachineFunction *MF;
29 /// BlockInterference - information about the interference in a single basic
30 /// block.
31 struct BlockInterference {
32 BlockInterference() : Tag(0) {}
33 unsigned Tag;
34 SlotIndex First;
35 SlotIndex Last;
36 };
38 /// Entry - A cache entry containing interference information for all aliases
39 /// of PhysReg in all basic blocks.
40 class Entry {
41 /// PhysReg - The register currently represented.
42 unsigned PhysReg;
44 /// Tag - Cache tag is changed when any of the underlying LiveIntervalUnions
45 /// change.
46 unsigned Tag;
48 /// RefCount - The total number of Cursor instances referring to this Entry.
49 unsigned RefCount;
51 /// MF - The current function.
52 MachineFunction *MF;
54 /// Indexes - Mapping block numbers to SlotIndex ranges.
55 SlotIndexes *Indexes;
57 /// LIS - Used for accessing register mask interference maps.
58 LiveIntervals *LIS;
60 /// PrevPos - The previous position the iterators were moved to.
61 SlotIndex PrevPos;
63 /// RegUnitInfo - Information tracked about each RegUnit in PhysReg.
64 /// When PrevPos is set, the iterators are valid as if advanceTo(PrevPos)
65 /// had just been called.
66 struct RegUnitInfo {
67 /// Iterator pointing into the LiveIntervalUnion containing virtual
68 /// register interference.
69 LiveIntervalUnion::SegmentIter VirtI;
71 /// Tag of the LIU last time we looked.
72 unsigned VirtTag;
74 /// Fixed interference in RegUnit.
75 LiveRange *Fixed;
77 /// Iterator pointing into the fixed RegUnit interference.
78 LiveInterval::iterator FixedI;
80 RegUnitInfo(LiveIntervalUnion &LIU) : VirtTag(LIU.getTag()), Fixed(0) {
81 VirtI.setMap(LIU.getMap());
82 }
83 };
85 /// Info for each RegUnit in PhysReg. It is very rare ofr a PHysReg to have
86 /// more than 4 RegUnits.
87 SmallVector<RegUnitInfo, 4> RegUnits;
89 /// Blocks - Interference for each block in the function.
90 SmallVector<BlockInterference, 8> Blocks;
92 /// update - Recompute Blocks[MBBNum]
93 void update(unsigned MBBNum);
95 public:
96 Entry() : PhysReg(0), Tag(0), RefCount(0), Indexes(0), LIS(0) {}
98 void clear(MachineFunction *mf, SlotIndexes *indexes, LiveIntervals *lis) {
99 assert(!hasRefs() && "Cannot clear cache entry with references");
100 PhysReg = 0;
101 MF = mf;
102 Indexes = indexes;
103 LIS = lis;
104 }
106 unsigned getPhysReg() const { return PhysReg; }
108 void addRef(int Delta) { RefCount += Delta; }
110 bool hasRefs() const { return RefCount > 0; }
112 void revalidate(LiveIntervalUnion *LIUArray, const TargetRegisterInfo *TRI);
114 /// valid - Return true if this is a valid entry for physReg.
115 bool valid(LiveIntervalUnion *LIUArray, const TargetRegisterInfo *TRI);
117 /// reset - Initialize entry to represent physReg's aliases.
118 void reset(unsigned physReg,
119 LiveIntervalUnion *LIUArray,
120 const TargetRegisterInfo *TRI,
121 const MachineFunction *MF);
123 /// get - Return an up to date BlockInterference.
124 BlockInterference *get(unsigned MBBNum) {
125 if (Blocks[MBBNum].Tag != Tag)
126 update(MBBNum);
127 return &Blocks[MBBNum];
128 }
129 };
131 // We don't keep a cache entry for every physical register, that would use too
132 // much memory. Instead, a fixed number of cache entries are used in a round-
133 // robin manner.
134 enum { CacheEntries = 32 };
136 // Point to an entry for each physreg. The entry pointed to may not be up to
137 // date, and it may have been reused for a different physreg.
138 SmallVector<unsigned char, 2> PhysRegEntries;
140 // Next round-robin entry to be picked.
141 unsigned RoundRobin;
143 // The actual cache entries.
144 Entry Entries[CacheEntries];
146 // get - Get a valid entry for PhysReg.
147 Entry *get(unsigned PhysReg);
149 public:
150 InterferenceCache() : TRI(0), LIUArray(0), MF(0), RoundRobin(0) {}
152 /// init - Prepare cache for a new function.
153 void init(MachineFunction*, LiveIntervalUnion*, SlotIndexes*, LiveIntervals*,
154 const TargetRegisterInfo *);
156 /// getMaxCursors - Return the maximum number of concurrent cursors that can
157 /// be supported.
158 unsigned getMaxCursors() const { return CacheEntries; }
160 /// Cursor - The primary query interface for the block interference cache.
161 class Cursor {
162 Entry *CacheEntry;
163 BlockInterference *Current;
164 static BlockInterference NoInterference;
166 void setEntry(Entry *E) {
167 Current = 0;
168 // Update reference counts. Nothing happens when RefCount reaches 0, so
169 // we don't have to check for E == CacheEntry etc.
170 if (CacheEntry)
171 CacheEntry->addRef(-1);
172 CacheEntry = E;
173 if (CacheEntry)
174 CacheEntry->addRef(+1);
175 }
177 public:
178 /// Cursor - Create a dangling cursor.
179 Cursor() : CacheEntry(0), Current(0) {}
180 ~Cursor() { setEntry(0); }
182 Cursor(const Cursor &O) : CacheEntry(0), Current(0) {
183 setEntry(O.CacheEntry);
184 }
186 Cursor &operator=(const Cursor &O) {
187 setEntry(O.CacheEntry);
188 return *this;
189 }
191 /// setPhysReg - Point this cursor to PhysReg's interference.
192 void setPhysReg(InterferenceCache &Cache, unsigned PhysReg) {
193 // Release reference before getting a new one. That guarantees we can
194 // actually have CacheEntries live cursors.
195 setEntry(0);
196 if (PhysReg)
197 setEntry(Cache.get(PhysReg));
198 }
200 /// moveTo - Move cursor to basic block MBBNum.
201 void moveToBlock(unsigned MBBNum) {
202 Current = CacheEntry ? CacheEntry->get(MBBNum) : &NoInterference;
203 }
205 /// hasInterference - Return true if the current block has any interference.
206 bool hasInterference() {
207 return Current->First.isValid();
208 }
210 /// first - Return the starting index of the first interfering range in the
211 /// current block.
212 SlotIndex first() {
213 return Current->First;
214 }
216 /// last - Return the ending index of the last interfering range in the
217 /// current block.
218 SlotIndex last() {
219 return Current->Last;
220 }
221 };
223 friend class Cursor;
224 };
226 } // namespace llvm
228 #endif