]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/LiveInterval.cpp
remove extra semicolon
[opencl/llvm.git] / lib / CodeGen / LiveInterval.cpp
1 //===-- LiveInterval.cpp - Live Interval Representation -------------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the LiveRange and LiveInterval classes.  Given some
11 // numbering of each the machine instructions an interval [i, j) is said to be a
12 // live range for register v if there is no instruction with number j' >= j
13 // such that v is live at j' and there is no instruction with number i' < i such
14 // that v is live at i'. In this implementation ranges can have holes,
15 // i.e. a range might look like [1,20), [50,65), [1000,1001).  Each
16 // individual segment is represented as an instance of LiveRange::Segment,
17 // and the whole range is represented as an instance of LiveRange.
18 //
19 //===----------------------------------------------------------------------===//
21 #include "llvm/CodeGen/LiveInterval.h"
22 #include "RegisterCoalescer.h"
23 #include "llvm/ADT/DenseMap.h"
24 #include "llvm/ADT/STLExtras.h"
25 #include "llvm/ADT/SmallSet.h"
26 #include "llvm/CodeGen/LiveIntervalAnalysis.h"
27 #include "llvm/CodeGen/MachineRegisterInfo.h"
28 #include "llvm/Support/Debug.h"
29 #include "llvm/Support/Format.h"
30 #include "llvm/Support/raw_ostream.h"
31 #include "llvm/Target/TargetRegisterInfo.h"
32 #include <algorithm>
33 using namespace llvm;
35 LiveRange::iterator LiveRange::find(SlotIndex Pos) {
36   // This algorithm is basically std::upper_bound.
37   // Unfortunately, std::upper_bound cannot be used with mixed types until we
38   // adopt C++0x. Many libraries can do it, but not all.
39   if (empty() || Pos >= endIndex())
40     return end();
41   iterator I = begin();
42   size_t Len = size();
43   do {
44     size_t Mid = Len >> 1;
45     if (Pos < I[Mid].end)
46       Len = Mid;
47     else
48       I += Mid + 1, Len -= Mid + 1;
49   } while (Len);
50   return I;
51 }
53 VNInfo *LiveRange::createDeadDef(SlotIndex Def,
54                                   VNInfo::Allocator &VNInfoAllocator) {
55   assert(!Def.isDead() && "Cannot define a value at the dead slot");
56   iterator I = find(Def);
57   if (I == end()) {
58     VNInfo *VNI = getNextValue(Def, VNInfoAllocator);
59     segments.push_back(Segment(Def, Def.getDeadSlot(), VNI));
60     return VNI;
61   }
62   if (SlotIndex::isSameInstr(Def, I->start)) {
63     assert(I->valno->def == I->start && "Inconsistent existing value def");
65     // It is possible to have both normal and early-clobber defs of the same
66     // register on an instruction. It doesn't make a lot of sense, but it is
67     // possible to specify in inline assembly.
68     //
69     // Just convert everything to early-clobber.
70     Def = std::min(Def, I->start);
71     if (Def != I->start)
72       I->start = I->valno->def = Def;
73     return I->valno;
74   }
75   assert(SlotIndex::isEarlierInstr(Def, I->start) && "Already live at def");
76   VNInfo *VNI = getNextValue(Def, VNInfoAllocator);
77   segments.insert(I, Segment(Def, Def.getDeadSlot(), VNI));
78   return VNI;
79 }
81 // overlaps - Return true if the intersection of the two live ranges is
82 // not empty.
83 //
84 // An example for overlaps():
85 //
86 // 0: A = ...
87 // 4: B = ...
88 // 8: C = A + B ;; last use of A
89 //
90 // The live ranges should look like:
91 //
92 // A = [3, 11)
93 // B = [7, x)
94 // C = [11, y)
95 //
96 // A->overlaps(C) should return false since we want to be able to join
97 // A and C.
98 //
99 bool LiveRange::overlapsFrom(const LiveRange& other,
100                              const_iterator StartPos) const {
101   assert(!empty() && "empty range");
102   const_iterator i = begin();
103   const_iterator ie = end();
104   const_iterator j = StartPos;
105   const_iterator je = other.end();
107   assert((StartPos->start <= i->start || StartPos == other.begin()) &&
108          StartPos != other.end() && "Bogus start position hint!");
110   if (i->start < j->start) {
111     i = std::upper_bound(i, ie, j->start);
112     if (i != begin()) --i;
113   } else if (j->start < i->start) {
114     ++StartPos;
115     if (StartPos != other.end() && StartPos->start <= i->start) {
116       assert(StartPos < other.end() && i < end());
117       j = std::upper_bound(j, je, i->start);
118       if (j != other.begin()) --j;
119     }
120   } else {
121     return true;
122   }
124   if (j == je) return false;
126   while (i != ie) {
127     if (i->start > j->start) {
128       std::swap(i, j);
129       std::swap(ie, je);
130     }
132     if (i->end > j->start)
133       return true;
134     ++i;
135   }
137   return false;
140 bool LiveRange::overlaps(const LiveRange &Other, const CoalescerPair &CP,
141                          const SlotIndexes &Indexes) const {
142   assert(!empty() && "empty range");
143   if (Other.empty())
144     return false;
146   // Use binary searches to find initial positions.
147   const_iterator I = find(Other.beginIndex());
148   const_iterator IE = end();
149   if (I == IE)
150     return false;
151   const_iterator J = Other.find(I->start);
152   const_iterator JE = Other.end();
153   if (J == JE)
154     return false;
156   for (;;) {
157     // J has just been advanced to satisfy:
158     assert(J->end >= I->start);
159     // Check for an overlap.
160     if (J->start < I->end) {
161       // I and J are overlapping. Find the later start.
162       SlotIndex Def = std::max(I->start, J->start);
163       // Allow the overlap if Def is a coalescable copy.
164       if (Def.isBlock() ||
165           !CP.isCoalescable(Indexes.getInstructionFromIndex(Def)))
166         return true;
167     }
168     // Advance the iterator that ends first to check for more overlaps.
169     if (J->end > I->end) {
170       std::swap(I, J);
171       std::swap(IE, JE);
172     }
173     // Advance J until J->end >= I->start.
174     do
175       if (++J == JE)
176         return false;
177     while (J->end < I->start);
178   }
181 /// overlaps - Return true if the live range overlaps an interval specified
182 /// by [Start, End).
183 bool LiveRange::overlaps(SlotIndex Start, SlotIndex End) const {
184   assert(Start < End && "Invalid range");
185   const_iterator I = std::lower_bound(begin(), end(), End);
186   return I != begin() && (--I)->end > Start;
189 bool LiveRange::covers(const LiveRange &Other) const {
190   if (empty())
191     return Other.empty();
193   const_iterator I = begin();
194   for (const Segment &O : Other.segments) {
195     I = advanceTo(I, O.start);
196     if (I == end() || I->start > O.start)
197       return false;
199     // Check adjacent live segments and see if we can get behind O.end.
200     while (I->end < O.end) {
201       const_iterator Last = I;
202       // Get next segment and abort if it was not adjacent.
203       ++I;
204       if (I == end() || Last->end != I->start)
205         return false;
206     }
207   }
208   return true;
211 /// ValNo is dead, remove it.  If it is the largest value number, just nuke it
212 /// (and any other deleted values neighboring it), otherwise mark it as ~1U so
213 /// it can be nuked later.
214 void LiveRange::markValNoForDeletion(VNInfo *ValNo) {
215   if (ValNo->id == getNumValNums()-1) {
216     do {
217       valnos.pop_back();
218     } while (!valnos.empty() && valnos.back()->isUnused());
219   } else {
220     ValNo->markUnused();
221   }
224 /// RenumberValues - Renumber all values in order of appearance and delete the
225 /// remaining unused values.
226 void LiveRange::RenumberValues() {
227   SmallPtrSet<VNInfo*, 8> Seen;
228   valnos.clear();
229   for (const Segment &S : segments) {
230     VNInfo *VNI = S.valno;
231     if (!Seen.insert(VNI).second)
232       continue;
233     assert(!VNI->isUnused() && "Unused valno used by live segment");
234     VNI->id = (unsigned)valnos.size();
235     valnos.push_back(VNI);
236   }
239 /// This method is used when we want to extend the segment specified by I to end
240 /// at the specified endpoint.  To do this, we should merge and eliminate all
241 /// segments that this will overlap with.  The iterator is not invalidated.
242 void LiveRange::extendSegmentEndTo(iterator I, SlotIndex NewEnd) {
243   assert(I != end() && "Not a valid segment!");
244   VNInfo *ValNo = I->valno;
246   // Search for the first segment that we can't merge with.
247   iterator MergeTo = std::next(I);
248   for (; MergeTo != end() && NewEnd >= MergeTo->end; ++MergeTo) {
249     assert(MergeTo->valno == ValNo && "Cannot merge with differing values!");
250   }
252   // If NewEnd was in the middle of a segment, make sure to get its endpoint.
253   I->end = std::max(NewEnd, std::prev(MergeTo)->end);
255   // If the newly formed segment now touches the segment after it and if they
256   // have the same value number, merge the two segments into one segment.
257   if (MergeTo != end() && MergeTo->start <= I->end &&
258       MergeTo->valno == ValNo) {
259     I->end = MergeTo->end;
260     ++MergeTo;
261   }
263   // Erase any dead segments.
264   segments.erase(std::next(I), MergeTo);
268 /// This method is used when we want to extend the segment specified by I to
269 /// start at the specified endpoint.  To do this, we should merge and eliminate
270 /// all segments that this will overlap with.
271 LiveRange::iterator
272 LiveRange::extendSegmentStartTo(iterator I, SlotIndex NewStart) {
273   assert(I != end() && "Not a valid segment!");
274   VNInfo *ValNo = I->valno;
276   // Search for the first segment that we can't merge with.
277   iterator MergeTo = I;
278   do {
279     if (MergeTo == begin()) {
280       I->start = NewStart;
281       segments.erase(MergeTo, I);
282       return I;
283     }
284     assert(MergeTo->valno == ValNo && "Cannot merge with differing values!");
285     --MergeTo;
286   } while (NewStart <= MergeTo->start);
288   // If we start in the middle of another segment, just delete a range and
289   // extend that segment.
290   if (MergeTo->end >= NewStart && MergeTo->valno == ValNo) {
291     MergeTo->end = I->end;
292   } else {
293     // Otherwise, extend the segment right after.
294     ++MergeTo;
295     MergeTo->start = NewStart;
296     MergeTo->end = I->end;
297   }
299   segments.erase(std::next(MergeTo), std::next(I));
300   return MergeTo;
303 void LiveRange::append(const Segment S) {
304   // Check that the segment belongs to the back of the list.
305   assert(segments.empty() || segments.back().end <= S.start);
306   segments.push_back(S);
309 LiveRange::iterator LiveRange::addSegmentFrom(Segment S, iterator From) {
310   SlotIndex Start = S.start, End = S.end;
311   iterator it = std::upper_bound(From, end(), Start);
313   // If the inserted segment starts in the middle or right at the end of
314   // another segment, just extend that segment to contain the segment of S.
315   if (it != begin()) {
316     iterator B = std::prev(it);
317     if (S.valno == B->valno) {
318       if (B->start <= Start && B->end >= Start) {
319         extendSegmentEndTo(B, End);
320         return B;
321       }
322     } else {
323       // Check to make sure that we are not overlapping two live segments with
324       // different valno's.
325       assert(B->end <= Start &&
326              "Cannot overlap two segments with differing ValID's"
327              " (did you def the same reg twice in a MachineInstr?)");
328     }
329   }
331   // Otherwise, if this segment ends in the middle of, or right next to, another
332   // segment, merge it into that segment.
333   if (it != end()) {
334     if (S.valno == it->valno) {
335       if (it->start <= End) {
336         it = extendSegmentStartTo(it, Start);
338         // If S is a complete superset of a segment, we may need to grow its
339         // endpoint as well.
340         if (End > it->end)
341           extendSegmentEndTo(it, End);
342         return it;
343       }
344     } else {
345       // Check to make sure that we are not overlapping two live segments with
346       // different valno's.
347       assert(it->start >= End &&
348              "Cannot overlap two segments with differing ValID's");
349     }
350   }
352   // Otherwise, this is just a new segment that doesn't interact with anything.
353   // Insert it.
354   return segments.insert(it, S);
357 /// extendInBlock - If this range is live before Kill in the basic
358 /// block that starts at StartIdx, extend it to be live up to Kill and return
359 /// the value. If there is no live range before Kill, return NULL.
360 VNInfo *LiveRange::extendInBlock(SlotIndex StartIdx, SlotIndex Kill) {
361   if (empty())
362     return nullptr;
363   iterator I = std::upper_bound(begin(), end(), Kill.getPrevSlot());
364   if (I == begin())
365     return nullptr;
366   --I;
367   if (I->end <= StartIdx)
368     return nullptr;
369   if (I->end < Kill)
370     extendSegmentEndTo(I, Kill);
371   return I->valno;
374 /// Remove the specified segment from this range.  Note that the segment must
375 /// be in a single Segment in its entirety.
376 void LiveRange::removeSegment(SlotIndex Start, SlotIndex End,
377                               bool RemoveDeadValNo) {
378   // Find the Segment containing this span.
379   iterator I = find(Start);
380   assert(I != end() && "Segment is not in range!");
381   assert(I->containsInterval(Start, End)
382          && "Segment is not entirely in range!");
384   // If the span we are removing is at the start of the Segment, adjust it.
385   VNInfo *ValNo = I->valno;
386   if (I->start == Start) {
387     if (I->end == End) {
388       if (RemoveDeadValNo) {
389         // Check if val# is dead.
390         bool isDead = true;
391         for (const_iterator II = begin(), EE = end(); II != EE; ++II)
392           if (II != I && II->valno == ValNo) {
393             isDead = false;
394             break;
395           }
396         if (isDead) {
397           // Now that ValNo is dead, remove it.
398           markValNoForDeletion(ValNo);
399         }
400       }
402       segments.erase(I);  // Removed the whole Segment.
403     } else
404       I->start = End;
405     return;
406   }
408   // Otherwise if the span we are removing is at the end of the Segment,
409   // adjust the other way.
410   if (I->end == End) {
411     I->end = Start;
412     return;
413   }
415   // Otherwise, we are splitting the Segment into two pieces.
416   SlotIndex OldEnd = I->end;
417   I->end = Start;   // Trim the old segment.
419   // Insert the new one.
420   segments.insert(std::next(I), Segment(End, OldEnd, ValNo));
423 /// removeValNo - Remove all the segments defined by the specified value#.
424 /// Also remove the value# from value# list.
425 void LiveRange::removeValNo(VNInfo *ValNo) {
426   if (empty()) return;
427   iterator I = end();
428   iterator E = begin();
429   do {
430     --I;
431     if (I->valno == ValNo)
432       segments.erase(I);
433   } while (I != E);
434   // Now that ValNo is dead, remove it.
435   markValNoForDeletion(ValNo);
438 void LiveRange::join(LiveRange &Other,
439                      const int *LHSValNoAssignments,
440                      const int *RHSValNoAssignments,
441                      SmallVectorImpl<VNInfo *> &NewVNInfo) {
442   verify();
444   // Determine if any of our values are mapped.  This is uncommon, so we want
445   // to avoid the range scan if not.
446   bool MustMapCurValNos = false;
447   unsigned NumVals = getNumValNums();
448   unsigned NumNewVals = NewVNInfo.size();
449   for (unsigned i = 0; i != NumVals; ++i) {
450     unsigned LHSValID = LHSValNoAssignments[i];
451     if (i != LHSValID ||
452         (NewVNInfo[LHSValID] && NewVNInfo[LHSValID] != getValNumInfo(i))) {
453       MustMapCurValNos = true;
454       break;
455     }
456   }
458   // If we have to apply a mapping to our base range assignment, rewrite it now.
459   if (MustMapCurValNos && !empty()) {
460     // Map the first live range.
462     iterator OutIt = begin();
463     OutIt->valno = NewVNInfo[LHSValNoAssignments[OutIt->valno->id]];
464     for (iterator I = std::next(OutIt), E = end(); I != E; ++I) {
465       VNInfo* nextValNo = NewVNInfo[LHSValNoAssignments[I->valno->id]];
466       assert(nextValNo && "Huh?");
468       // If this live range has the same value # as its immediate predecessor,
469       // and if they are neighbors, remove one Segment.  This happens when we
470       // have [0,4:0)[4,7:1) and map 0/1 onto the same value #.
471       if (OutIt->valno == nextValNo && OutIt->end == I->start) {
472         OutIt->end = I->end;
473       } else {
474         // Didn't merge. Move OutIt to the next segment,
475         ++OutIt;
476         OutIt->valno = nextValNo;
477         if (OutIt != I) {
478           OutIt->start = I->start;
479           OutIt->end = I->end;
480         }
481       }
482     }
483     // If we merge some segments, chop off the end.
484     ++OutIt;
485     segments.erase(OutIt, end());
486   }
488   // Rewrite Other values before changing the VNInfo ids.
489   // This can leave Other in an invalid state because we're not coalescing
490   // touching segments that now have identical values. That's OK since Other is
491   // not supposed to be valid after calling join();
492   for (Segment &S : Other.segments)
493     S.valno = NewVNInfo[RHSValNoAssignments[S.valno->id]];
495   // Update val# info. Renumber them and make sure they all belong to this
496   // LiveRange now. Also remove dead val#'s.
497   unsigned NumValNos = 0;
498   for (unsigned i = 0; i < NumNewVals; ++i) {
499     VNInfo *VNI = NewVNInfo[i];
500     if (VNI) {
501       if (NumValNos >= NumVals)
502         valnos.push_back(VNI);
503       else
504         valnos[NumValNos] = VNI;
505       VNI->id = NumValNos++;  // Renumber val#.
506     }
507   }
508   if (NumNewVals < NumVals)
509     valnos.resize(NumNewVals);  // shrinkify
511   // Okay, now insert the RHS live segments into the LHS.
512   LiveRangeUpdater Updater(this);
513   for (Segment &S : Other.segments)
514     Updater.add(S);
517 /// Merge all of the segments in RHS into this live range as the specified
518 /// value number.  The segments in RHS are allowed to overlap with segments in
519 /// the current range, but only if the overlapping segments have the
520 /// specified value number.
521 void LiveRange::MergeSegmentsInAsValue(const LiveRange &RHS,
522                                        VNInfo *LHSValNo) {
523   LiveRangeUpdater Updater(this);
524   for (const Segment &S : RHS.segments)
525     Updater.add(S.start, S.end, LHSValNo);
528 /// MergeValueInAsValue - Merge all of the live segments of a specific val#
529 /// in RHS into this live range as the specified value number.
530 /// The segments in RHS are allowed to overlap with segments in the
531 /// current range, it will replace the value numbers of the overlaped
532 /// segments with the specified value number.
533 void LiveRange::MergeValueInAsValue(const LiveRange &RHS,
534                                     const VNInfo *RHSValNo,
535                                     VNInfo *LHSValNo) {
536   LiveRangeUpdater Updater(this);
537   for (const Segment &S : RHS.segments)
538     if (S.valno == RHSValNo)
539       Updater.add(S.start, S.end, LHSValNo);
542 /// MergeValueNumberInto - This method is called when two value nubmers
543 /// are found to be equivalent.  This eliminates V1, replacing all
544 /// segments with the V1 value number with the V2 value number.  This can
545 /// cause merging of V1/V2 values numbers and compaction of the value space.
546 VNInfo *LiveRange::MergeValueNumberInto(VNInfo *V1, VNInfo *V2) {
547   assert(V1 != V2 && "Identical value#'s are always equivalent!");
549   // This code actually merges the (numerically) larger value number into the
550   // smaller value number, which is likely to allow us to compactify the value
551   // space.  The only thing we have to be careful of is to preserve the
552   // instruction that defines the result value.
554   // Make sure V2 is smaller than V1.
555   if (V1->id < V2->id) {
556     V1->copyFrom(*V2);
557     std::swap(V1, V2);
558   }
560   // Merge V1 segments into V2.
561   for (iterator I = begin(); I != end(); ) {
562     iterator S = I++;
563     if (S->valno != V1) continue;  // Not a V1 Segment.
565     // Okay, we found a V1 live range.  If it had a previous, touching, V2 live
566     // range, extend it.
567     if (S != begin()) {
568       iterator Prev = S-1;
569       if (Prev->valno == V2 && Prev->end == S->start) {
570         Prev->end = S->end;
572         // Erase this live-range.
573         segments.erase(S);
574         I = Prev+1;
575         S = Prev;
576       }
577     }
579     // Okay, now we have a V1 or V2 live range that is maximally merged forward.
580     // Ensure that it is a V2 live-range.
581     S->valno = V2;
583     // If we can merge it into later V2 segments, do so now.  We ignore any
584     // following V1 segments, as they will be merged in subsequent iterations
585     // of the loop.
586     if (I != end()) {
587       if (I->start == S->end && I->valno == V2) {
588         S->end = I->end;
589         segments.erase(I);
590         I = S+1;
591       }
592     }
593   }
595   // Now that V1 is dead, remove it.
596   markValNoForDeletion(V1);
598   return V2;
601 void LiveInterval::removeEmptySubRanges() {
602   SubRange **NextPtr = &SubRanges;
603   SubRange *I = *NextPtr;
604   while (I != nullptr) {
605     if (!I->empty()) {
606       NextPtr = &I->Next;
607       I = *NextPtr;
608       continue;
609     }
610     // Skip empty subranges until we find the first nonempty one.
611     do {
612       I = I->Next;
613     } while (I != nullptr && I->empty());
614     *NextPtr = I;
615   }
618 /// Helper function for constructMainRangeFromSubranges(): Search the CFG
619 /// backwards until we find a place covered by a LiveRange segment that actually
620 /// has a valno set.
621 static VNInfo *searchForVNI(const SlotIndexes &Indexes, LiveRange &LR,
622     const MachineBasicBlock *MBB,
623     SmallPtrSetImpl<const MachineBasicBlock*> &Visited) {
624   // We start the search at the end of MBB.
625   SlotIndex EndIdx = Indexes.getMBBEndIdx(MBB);
626   // In our use case we can't live the area covered by the live segments without
627   // finding an actual VNI def.
628   LiveRange::iterator I = LR.find(EndIdx.getPrevSlot());
629   assert(I != LR.end());
630   LiveRange::Segment &S = *I;
631   if (S.valno != nullptr)
632     return S.valno;
634   VNInfo *VNI = nullptr;
635   // Continue at predecessors (we could even go to idom with domtree available).
636   for (const MachineBasicBlock *Pred : MBB->predecessors()) {
637     // Avoid going in circles.
638     if (!Visited.insert(Pred).second)
639       continue;
641     VNI = searchForVNI(Indexes, LR, Pred, Visited);
642     if (VNI != nullptr) {
643       S.valno = VNI;
644       break;
645     }
646   }
648   return VNI;
651 static void determineMissingVNIs(const SlotIndexes &Indexes, LiveInterval &LI) {
652   SmallPtrSet<const MachineBasicBlock*, 5> Visited;
653   for (LiveRange::Segment &S : LI.segments) {
654     if (S.valno != nullptr)
655       continue;
656     // This can only happen at the begin of a basic block.
657     assert(S.start.isBlock() && "valno should only be missing at block begin");
659     Visited.clear();
660     const MachineBasicBlock *MBB = Indexes.getMBBFromIndex(S.start);
661     for (const MachineBasicBlock *Pred : MBB->predecessors()) {
662       VNInfo *VNI = searchForVNI(Indexes, LI, Pred, Visited);
663       if (VNI != nullptr) {
664         S.valno = VNI;
665         break;
666       }
667     }
668     assert(S.valno != nullptr && "could not determine valno");
669   }
672 void LiveInterval::constructMainRangeFromSubranges(
673     const SlotIndexes &Indexes, VNInfo::Allocator &VNIAllocator) {
674   // The basic observations on which this algorithm is based:
675   // - Each Def/ValNo in a subrange must have a corresponding def on the main
676   //   range, but not further defs/valnos are necessary.
677   // - If any of the subranges is live at a point the main liverange has to be
678   //   live too, conversily if no subrange is live the main range mustn't be
679   //   live either.
680   // We do this by scannig through all the subranges simultaneously creating new
681   // segments in the main range as segments start/ends come up in the subranges.
682   assert(hasSubRanges() && "expected subranges to be present");
683   assert(segments.empty() && valnos.empty() && "expected empty main range");
685   // Collect subrange, iterator pairs for the walk and determine first and last
686   // SlotIndex involved.
687   SmallVector<std::pair<const SubRange*, const_iterator>, 4> SRs;
688   SlotIndex First;
689   SlotIndex Last;
690   for (const SubRange &SR : subranges()) {
691     if (SR.empty())
692       continue;
693     SRs.push_back(std::make_pair(&SR, SR.begin()));
694     if (!First.isValid() || SR.segments.front().start < First)
695       First = SR.segments.front().start;
696     if (!Last.isValid() || SR.segments.back().end > Last)
697       Last = SR.segments.back().end;
698   }
700   // Walk over all subranges simultaneously.
701   Segment CurrentSegment;
702   bool ConstructingSegment = false;
703   bool NeedVNIFixup = false;
704   unsigned ActiveMask = 0;
705   SlotIndex Pos = First;
706   while (true) {
707     SlotIndex NextPos = Last;
708     enum {
709       NOTHING,
710       BEGIN_SEGMENT,
711       END_SEGMENT,
712     } Event = NOTHING;
713     // Which subregister lanes are affected by the current event.
714     unsigned EventMask = 0;
715     // Whether a BEGIN_SEGMENT is also a valno definition point.
716     bool IsDef = false;
717     // Find the next begin or end of a subrange segment. Combine masks if we
718     // have multiple begins/ends at the same position. Ends take precedence over
719     // Begins.
720     for (auto &SRP : SRs) {
721       const SubRange &SR = *SRP.first;
722       const_iterator &I = SRP.second;
723       // Advance iterator of subrange to a segment involving Pos; the earlier
724       // segments are already merged at this point.
725       while (I != SR.end() &&
726              (I->end < Pos ||
727               (I->end == Pos && (ActiveMask & SR.LaneMask) == 0)))
728         ++I;
729       if (I == SR.end())
730         continue;
731       if ((ActiveMask & SR.LaneMask) == 0 &&
732           Pos <= I->start && I->start <= NextPos) {
733         // Merge multiple begins at the same position.
734         if (I->start == NextPos && Event == BEGIN_SEGMENT) {
735           EventMask |= SR.LaneMask;
736           IsDef |= I->valno->def == I->start;
737         } else if (I->start < NextPos || Event != END_SEGMENT) {
738           Event = BEGIN_SEGMENT;
739           NextPos = I->start;
740           EventMask = SR.LaneMask;
741           IsDef = I->valno->def == I->start;
742         }
743       }
744       if ((ActiveMask & SR.LaneMask) != 0 &&
745           Pos <= I->end && I->end <= NextPos) {
746         // Merge multiple ends at the same position.
747         if (I->end == NextPos && Event == END_SEGMENT)
748           EventMask |= SR.LaneMask;
749         else {
750           Event = END_SEGMENT;
751           NextPos = I->end;
752           EventMask = SR.LaneMask;
753         }
754       }
755     }
757     // Advance scan position.
758     Pos = NextPos;
759     if (Event == BEGIN_SEGMENT) {
760       if (ConstructingSegment && IsDef) {
761         // Finish previous segment because we have to start a new one.
762         CurrentSegment.end = Pos;
763         append(CurrentSegment);
764         ConstructingSegment = false;
765       }
767       // Start a new segment if necessary.
768       if (!ConstructingSegment) {
769         // Determine value number for the segment.
770         VNInfo *VNI;
771         if (IsDef) {
772           VNI = getNextValue(Pos, VNIAllocator);
773         } else {
774           // We have to reuse an existing value number, if we are lucky
775           // then we already passed one of the predecessor blocks and determined
776           // its value number (with blocks in reverse postorder this would be
777           // always true but we have no such guarantee).
778           assert(Pos.isBlock());
779           const MachineBasicBlock *MBB = Indexes.getMBBFromIndex(Pos);
780           // See if any of the predecessor blocks has a lower number and a VNI
781           for (const MachineBasicBlock *Pred : MBB->predecessors()) {
782             SlotIndex PredEnd = Indexes.getMBBEndIdx(Pred);
783             VNI = getVNInfoBefore(PredEnd);
784             if (VNI != nullptr)
785               break;
786           }
787           // Def will come later: We have to do an extra fixup pass.
788           if (VNI == nullptr)
789             NeedVNIFixup = true;
790         }
792         CurrentSegment.start = Pos;
793         CurrentSegment.valno = VNI;
794         ConstructingSegment = true;
795       }
796       ActiveMask |= EventMask;
797     } else if (Event == END_SEGMENT) {
798       assert(ConstructingSegment);
799       // Finish segment if no lane is active anymore.
800       ActiveMask &= ~EventMask;
801       if (ActiveMask == 0) {
802         CurrentSegment.end = Pos;
803         append(CurrentSegment);
804         ConstructingSegment = false;
805       }
806     } else {
807       // We reached the end of the last subranges and can stop.
808       assert(Event == NOTHING);
809       break;
810     }
811   }
813   // We might not be able to assign new valnos for all segments if the basic
814   // block containing the definition comes after a segment using the valno.
815   // Do a fixup pass for this uncommon case.
816   if (NeedVNIFixup)
817     determineMissingVNIs(Indexes, *this);
819   assert(ActiveMask == 0 && !ConstructingSegment && "all segments ended");
820   verify();
823 unsigned LiveInterval::getSize() const {
824   unsigned Sum = 0;
825   for (const Segment &S : segments)
826     Sum += S.start.distance(S.end);
827   return Sum;
830 raw_ostream& llvm::operator<<(raw_ostream& os, const LiveRange::Segment &S) {
831   return os << '[' << S.start << ',' << S.end << ':' << S.valno->id << ")";
834 #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
835 void LiveRange::Segment::dump() const {
836   dbgs() << *this << "\n";
838 #endif
840 void LiveRange::print(raw_ostream &OS) const {
841   if (empty())
842     OS << "EMPTY";
843   else {
844     for (const Segment &S : segments) {
845       OS << S;
846       assert(S.valno == getValNumInfo(S.valno->id) && "Bad VNInfo");
847     }
848   }
850   // Print value number info.
851   if (getNumValNums()) {
852     OS << "  ";
853     unsigned vnum = 0;
854     for (const_vni_iterator i = vni_begin(), e = vni_end(); i != e;
855          ++i, ++vnum) {
856       const VNInfo *vni = *i;
857       if (vnum) OS << " ";
858       OS << vnum << "@";
859       if (vni->isUnused()) {
860         OS << "x";
861       } else {
862         OS << vni->def;
863         if (vni->isPHIDef())
864           OS << "-phi";
865       }
866     }
867   }
870 void LiveInterval::print(raw_ostream &OS) const {
871   OS << PrintReg(reg) << ' ';
872   super::print(OS);
873   // Print subranges
874   for (const SubRange &SR : subranges()) {
875     OS << format(" L%04X ", SR.LaneMask) << SR;
876   }
879 #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
880 void LiveRange::dump() const {
881   dbgs() << *this << "\n";
884 void LiveInterval::dump() const {
885   dbgs() << *this << "\n";
887 #endif
889 #ifndef NDEBUG
890 void LiveRange::verify() const {
891   for (const_iterator I = begin(), E = end(); I != E; ++I) {
892     assert(I->start.isValid());
893     assert(I->end.isValid());
894     assert(I->start < I->end);
895     assert(I->valno != nullptr);
896     assert(I->valno->id < valnos.size());
897     assert(I->valno == valnos[I->valno->id]);
898     if (std::next(I) != E) {
899       assert(I->end <= std::next(I)->start);
900       if (I->end == std::next(I)->start)
901         assert(I->valno != std::next(I)->valno);
902     }
903   }
906 void LiveInterval::verify(const MachineRegisterInfo *MRI) const {
907   super::verify();
909   // Make sure SubRanges are fine and LaneMasks are disjunct.
910   unsigned Mask = 0;
911   unsigned MaxMask = MRI != nullptr ? MRI->getMaxLaneMaskForVReg(reg) : ~0u;
912   for (const SubRange &SR : subranges()) {
913     // Subrange lanemask should be disjunct to any previous subrange masks.
914     assert((Mask & SR.LaneMask) == 0);
915     Mask |= SR.LaneMask;
917     // subrange mask should not contained in maximum lane mask for the vreg.
918     assert((Mask & ~MaxMask) == 0);
920     SR.verify();
921     // Main liverange should cover subrange.
922     assert(covers(SR));
923   }
925 #endif
928 //===----------------------------------------------------------------------===//
929 //                           LiveRangeUpdater class
930 //===----------------------------------------------------------------------===//
931 //
932 // The LiveRangeUpdater class always maintains these invariants:
933 //
934 // - When LastStart is invalid, Spills is empty and the iterators are invalid.
935 //   This is the initial state, and the state created by flush().
936 //   In this state, isDirty() returns false.
937 //
938 // Otherwise, segments are kept in three separate areas:
939 //
940 // 1. [begin; WriteI) at the front of LR.
941 // 2. [ReadI; end) at the back of LR.
942 // 3. Spills.
943 //
944 // - LR.begin() <= WriteI <= ReadI <= LR.end().
945 // - Segments in all three areas are fully ordered and coalesced.
946 // - Segments in area 1 precede and can't coalesce with segments in area 2.
947 // - Segments in Spills precede and can't coalesce with segments in area 2.
948 // - No coalescing is possible between segments in Spills and segments in area
949 //   1, and there are no overlapping segments.
950 //
951 // The segments in Spills are not ordered with respect to the segments in area
952 // 1. They need to be merged.
953 //
954 // When they exist, Spills.back().start <= LastStart,
955 //                 and WriteI[-1].start <= LastStart.
957 void LiveRangeUpdater::print(raw_ostream &OS) const {
958   if (!isDirty()) {
959     if (LR)
960       OS << "Clean updater: " << *LR << '\n';
961     else
962       OS << "Null updater.\n";
963     return;
964   }
965   assert(LR && "Can't have null LR in dirty updater.");
966   OS << " updater with gap = " << (ReadI - WriteI)
967      << ", last start = " << LastStart
968      << ":\n  Area 1:";
969   for (const auto &S : make_range(LR->begin(), WriteI))
970     OS << ' ' << S;
971   OS << "\n  Spills:";
972   for (unsigned I = 0, E = Spills.size(); I != E; ++I)
973     OS << ' ' << Spills[I];
974   OS << "\n  Area 2:";
975   for (const auto &S : make_range(ReadI, LR->end()))
976     OS << ' ' << S;
977   OS << '\n';
980 void LiveRangeUpdater::dump() const
982   print(errs());
985 // Determine if A and B should be coalesced.
986 static inline bool coalescable(const LiveRange::Segment &A,
987                                const LiveRange::Segment &B) {
988   assert(A.start <= B.start && "Unordered live segments.");
989   if (A.end == B.start)
990     return A.valno == B.valno;
991   if (A.end < B.start)
992     return false;
993   assert(A.valno == B.valno && "Cannot overlap different values");
994   return true;
997 void LiveRangeUpdater::add(LiveRange::Segment Seg) {
998   assert(LR && "Cannot add to a null destination");
1000   // Flush the state if Start moves backwards.
1001   if (!LastStart.isValid() || LastStart > Seg.start) {
1002     if (isDirty())
1003       flush();
1004     // This brings us to an uninitialized state. Reinitialize.
1005     assert(Spills.empty() && "Leftover spilled segments");
1006     WriteI = ReadI = LR->begin();
1007   }
1009   // Remember start for next time.
1010   LastStart = Seg.start;
1012   // Advance ReadI until it ends after Seg.start.
1013   LiveRange::iterator E = LR->end();
1014   if (ReadI != E && ReadI->end <= Seg.start) {
1015     // First try to close the gap between WriteI and ReadI with spills.
1016     if (ReadI != WriteI)
1017       mergeSpills();
1018     // Then advance ReadI.
1019     if (ReadI == WriteI)
1020       ReadI = WriteI = LR->find(Seg.start);
1021     else
1022       while (ReadI != E && ReadI->end <= Seg.start)
1023         *WriteI++ = *ReadI++;
1024   }
1026   assert(ReadI == E || ReadI->end > Seg.start);
1028   // Check if the ReadI segment begins early.
1029   if (ReadI != E && ReadI->start <= Seg.start) {
1030     assert(ReadI->valno == Seg.valno && "Cannot overlap different values");
1031     // Bail if Seg is completely contained in ReadI.
1032     if (ReadI->end >= Seg.end)
1033       return;
1034     // Coalesce into Seg.
1035     Seg.start = ReadI->start;
1036     ++ReadI;
1037   }
1039   // Coalesce as much as possible from ReadI into Seg.
1040   while (ReadI != E && coalescable(Seg, *ReadI)) {
1041     Seg.end = std::max(Seg.end, ReadI->end);
1042     ++ReadI;
1043   }
1045   // Try coalescing Spills.back() into Seg.
1046   if (!Spills.empty() && coalescable(Spills.back(), Seg)) {
1047     Seg.start = Spills.back().start;
1048     Seg.end = std::max(Spills.back().end, Seg.end);
1049     Spills.pop_back();
1050   }
1052   // Try coalescing Seg into WriteI[-1].
1053   if (WriteI != LR->begin() && coalescable(WriteI[-1], Seg)) {
1054     WriteI[-1].end = std::max(WriteI[-1].end, Seg.end);
1055     return;
1056   }
1058   // Seg doesn't coalesce with anything, and needs to be inserted somewhere.
1059   if (WriteI != ReadI) {
1060     *WriteI++ = Seg;
1061     return;
1062   }
1064   // Finally, append to LR or Spills.
1065   if (WriteI == E) {
1066     LR->segments.push_back(Seg);
1067     WriteI = ReadI = LR->end();
1068   } else
1069     Spills.push_back(Seg);
1072 // Merge as many spilled segments as possible into the gap between WriteI
1073 // and ReadI. Advance WriteI to reflect the inserted instructions.
1074 void LiveRangeUpdater::mergeSpills() {
1075   // Perform a backwards merge of Spills and [SpillI;WriteI).
1076   size_t GapSize = ReadI - WriteI;
1077   size_t NumMoved = std::min(Spills.size(), GapSize);
1078   LiveRange::iterator Src = WriteI;
1079   LiveRange::iterator Dst = Src + NumMoved;
1080   LiveRange::iterator SpillSrc = Spills.end();
1081   LiveRange::iterator B = LR->begin();
1083   // This is the new WriteI position after merging spills.
1084   WriteI = Dst;
1086   // Now merge Src and Spills backwards.
1087   while (Src != Dst) {
1088     if (Src != B && Src[-1].start > SpillSrc[-1].start)
1089       *--Dst = *--Src;
1090     else
1091       *--Dst = *--SpillSrc;
1092   }
1093   assert(NumMoved == size_t(Spills.end() - SpillSrc));
1094   Spills.erase(SpillSrc, Spills.end());
1097 void LiveRangeUpdater::flush() {
1098   if (!isDirty())
1099     return;
1100   // Clear the dirty state.
1101   LastStart = SlotIndex();
1103   assert(LR && "Cannot add to a null destination");
1105   // Nothing to merge?
1106   if (Spills.empty()) {
1107     LR->segments.erase(WriteI, ReadI);
1108     LR->verify();
1109     return;
1110   }
1112   // Resize the WriteI - ReadI gap to match Spills.
1113   size_t GapSize = ReadI - WriteI;
1114   if (GapSize < Spills.size()) {
1115     // The gap is too small. Make some room.
1116     size_t WritePos = WriteI - LR->begin();
1117     LR->segments.insert(ReadI, Spills.size() - GapSize, LiveRange::Segment());
1118     // This also invalidated ReadI, but it is recomputed below.
1119     WriteI = LR->begin() + WritePos;
1120   } else {
1121     // Shrink the gap if necessary.
1122     LR->segments.erase(WriteI + Spills.size(), ReadI);
1123   }
1124   ReadI = WriteI + Spills.size();
1125   mergeSpills();
1126   LR->verify();
1129 unsigned ConnectedVNInfoEqClasses::Classify(const LiveInterval *LI) {
1130   // Create initial equivalence classes.
1131   EqClass.clear();
1132   EqClass.grow(LI->getNumValNums());
1134   const VNInfo *used = nullptr, *unused = nullptr;
1136   // Determine connections.
1137   for (const VNInfo *VNI : LI->valnos) {
1138     // Group all unused values into one class.
1139     if (VNI->isUnused()) {
1140       if (unused)
1141         EqClass.join(unused->id, VNI->id);
1142       unused = VNI;
1143       continue;
1144     }
1145     used = VNI;
1146     if (VNI->isPHIDef()) {
1147       const MachineBasicBlock *MBB = LIS.getMBBFromIndex(VNI->def);
1148       assert(MBB && "Phi-def has no defining MBB");
1149       // Connect to values live out of predecessors.
1150       for (MachineBasicBlock::const_pred_iterator PI = MBB->pred_begin(),
1151            PE = MBB->pred_end(); PI != PE; ++PI)
1152         if (const VNInfo *PVNI = LI->getVNInfoBefore(LIS.getMBBEndIdx(*PI)))
1153           EqClass.join(VNI->id, PVNI->id);
1154     } else {
1155       // Normal value defined by an instruction. Check for two-addr redef.
1156       // FIXME: This could be coincidental. Should we really check for a tied
1157       // operand constraint?
1158       // Note that VNI->def may be a use slot for an early clobber def.
1159       if (const VNInfo *UVNI = LI->getVNInfoBefore(VNI->def))
1160         EqClass.join(VNI->id, UVNI->id);
1161     }
1162   }
1164   // Lump all the unused values in with the last used value.
1165   if (used && unused)
1166     EqClass.join(used->id, unused->id);
1168   EqClass.compress();
1169   return EqClass.getNumClasses();
1172 void ConnectedVNInfoEqClasses::Distribute(LiveInterval *LIV[],
1173                                           MachineRegisterInfo &MRI) {
1174   assert(LIV[0] && "LIV[0] must be set");
1175   LiveInterval &LI = *LIV[0];
1177   // Rewrite instructions.
1178   for (MachineRegisterInfo::reg_iterator RI = MRI.reg_begin(LI.reg),
1179        RE = MRI.reg_end(); RI != RE;) {
1180     MachineOperand &MO = *RI;
1181     MachineInstr *MI = RI->getParent();
1182     ++RI;
1183     // DBG_VALUE instructions don't have slot indexes, so get the index of the
1184     // instruction before them.
1185     // Normally, DBG_VALUE instructions are removed before this function is
1186     // called, but it is not a requirement.
1187     SlotIndex Idx;
1188     if (MI->isDebugValue())
1189       Idx = LIS.getSlotIndexes()->getIndexBefore(MI);
1190     else
1191       Idx = LIS.getInstructionIndex(MI);
1192     LiveQueryResult LRQ = LI.Query(Idx);
1193     const VNInfo *VNI = MO.readsReg() ? LRQ.valueIn() : LRQ.valueDefined();
1194     // In the case of an <undef> use that isn't tied to any def, VNI will be
1195     // NULL. If the use is tied to a def, VNI will be the defined value.
1196     if (!VNI)
1197       continue;
1198     MO.setReg(LIV[getEqClass(VNI)]->reg);
1199   }
1201   // Move runs to new intervals.
1202   LiveInterval::iterator J = LI.begin(), E = LI.end();
1203   while (J != E && EqClass[J->valno->id] == 0)
1204     ++J;
1205   for (LiveInterval::iterator I = J; I != E; ++I) {
1206     if (unsigned eq = EqClass[I->valno->id]) {
1207       assert((LIV[eq]->empty() || LIV[eq]->expiredAt(I->start)) &&
1208              "New intervals should be empty");
1209       LIV[eq]->segments.push_back(*I);
1210     } else
1211       *J++ = *I;
1212   }
1213   // TODO: do not cheat anymore by simply cleaning all subranges
1214   LI.clearSubRanges();
1215   LI.segments.erase(J, E);
1217   // Transfer VNInfos to their new owners and renumber them.
1218   unsigned j = 0, e = LI.getNumValNums();
1219   while (j != e && EqClass[j] == 0)
1220     ++j;
1221   for (unsigned i = j; i != e; ++i) {
1222     VNInfo *VNI = LI.getValNumInfo(i);
1223     if (unsigned eq = EqClass[i]) {
1224       VNI->id = LIV[eq]->getNumValNums();
1225       LIV[eq]->valnos.push_back(VNI);
1226     } else {
1227       VNI->id = j;
1228       LI.valnos[j++] = VNI;
1229     }
1230   }
1231   LI.valnos.resize(j);