]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/LiveInterval.cpp
constify the getters in SDNodeDbgValue.
[opencl/llvm.git] / lib / CodeGen / LiveInterval.cpp
1 //===-- LiveInterval.cpp - Live Interval Representation -------------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the LiveRange and LiveInterval classes.  Given some
11 // numbering of each the machine instructions an interval [i, j) is said to be a
12 // live range for register v if there is no instruction with number j' >= j
13 // such that v is live at j' and there is no instruction with number i' < i such
14 // that v is live at i'. In this implementation ranges can have holes,
15 // i.e. a range might look like [1,20), [50,65), [1000,1001).  Each
16 // individual segment is represented as an instance of LiveRange::Segment,
17 // and the whole range is represented as an instance of LiveRange.
18 //
19 //===----------------------------------------------------------------------===//
21 #include "llvm/CodeGen/LiveInterval.h"
22 #include "RegisterCoalescer.h"
23 #include "llvm/ADT/DenseMap.h"
24 #include "llvm/ADT/STLExtras.h"
25 #include "llvm/ADT/SmallSet.h"
26 #include "llvm/CodeGen/LiveIntervalAnalysis.h"
27 #include "llvm/CodeGen/MachineRegisterInfo.h"
28 #include "llvm/Support/Debug.h"
29 #include "llvm/Support/raw_ostream.h"
30 #include "llvm/Target/TargetRegisterInfo.h"
31 #include <algorithm>
32 using namespace llvm;
34 LiveRange::iterator LiveRange::find(SlotIndex Pos) {
35   // This algorithm is basically std::upper_bound.
36   // Unfortunately, std::upper_bound cannot be used with mixed types until we
37   // adopt C++0x. Many libraries can do it, but not all.
38   if (empty() || Pos >= endIndex())
39     return end();
40   iterator I = begin();
41   size_t Len = size();
42   do {
43     size_t Mid = Len >> 1;
44     if (Pos < I[Mid].end)
45       Len = Mid;
46     else
47       I += Mid + 1, Len -= Mid + 1;
48   } while (Len);
49   return I;
50 }
52 VNInfo *LiveRange::createDeadDef(SlotIndex Def,
53                                   VNInfo::Allocator &VNInfoAllocator) {
54   assert(!Def.isDead() && "Cannot define a value at the dead slot");
55   iterator I = find(Def);
56   if (I == end()) {
57     VNInfo *VNI = getNextValue(Def, VNInfoAllocator);
58     segments.push_back(Segment(Def, Def.getDeadSlot(), VNI));
59     return VNI;
60   }
61   if (SlotIndex::isSameInstr(Def, I->start)) {
62     assert(I->valno->def == I->start && "Inconsistent existing value def");
64     // It is possible to have both normal and early-clobber defs of the same
65     // register on an instruction. It doesn't make a lot of sense, but it is
66     // possible to specify in inline assembly.
67     //
68     // Just convert everything to early-clobber.
69     Def = std::min(Def, I->start);
70     if (Def != I->start)
71       I->start = I->valno->def = Def;
72     return I->valno;
73   }
74   assert(SlotIndex::isEarlierInstr(Def, I->start) && "Already live at def");
75   VNInfo *VNI = getNextValue(Def, VNInfoAllocator);
76   segments.insert(I, Segment(Def, Def.getDeadSlot(), VNI));
77   return VNI;
78 }
80 // overlaps - Return true if the intersection of the two live ranges is
81 // not empty.
82 //
83 // An example for overlaps():
84 //
85 // 0: A = ...
86 // 4: B = ...
87 // 8: C = A + B ;; last use of A
88 //
89 // The live ranges should look like:
90 //
91 // A = [3, 11)
92 // B = [7, x)
93 // C = [11, y)
94 //
95 // A->overlaps(C) should return false since we want to be able to join
96 // A and C.
97 //
98 bool LiveRange::overlapsFrom(const LiveRange& other,
99                              const_iterator StartPos) const {
100   assert(!empty() && "empty range");
101   const_iterator i = begin();
102   const_iterator ie = end();
103   const_iterator j = StartPos;
104   const_iterator je = other.end();
106   assert((StartPos->start <= i->start || StartPos == other.begin()) &&
107          StartPos != other.end() && "Bogus start position hint!");
109   if (i->start < j->start) {
110     i = std::upper_bound(i, ie, j->start);
111     if (i != begin()) --i;
112   } else if (j->start < i->start) {
113     ++StartPos;
114     if (StartPos != other.end() && StartPos->start <= i->start) {
115       assert(StartPos < other.end() && i < end());
116       j = std::upper_bound(j, je, i->start);
117       if (j != other.begin()) --j;
118     }
119   } else {
120     return true;
121   }
123   if (j == je) return false;
125   while (i != ie) {
126     if (i->start > j->start) {
127       std::swap(i, j);
128       std::swap(ie, je);
129     }
131     if (i->end > j->start)
132       return true;
133     ++i;
134   }
136   return false;
139 bool LiveRange::overlaps(const LiveRange &Other, const CoalescerPair &CP,
140                          const SlotIndexes &Indexes) const {
141   assert(!empty() && "empty range");
142   if (Other.empty())
143     return false;
145   // Use binary searches to find initial positions.
146   const_iterator I = find(Other.beginIndex());
147   const_iterator IE = end();
148   if (I == IE)
149     return false;
150   const_iterator J = Other.find(I->start);
151   const_iterator JE = Other.end();
152   if (J == JE)
153     return false;
155   for (;;) {
156     // J has just been advanced to satisfy:
157     assert(J->end >= I->start);
158     // Check for an overlap.
159     if (J->start < I->end) {
160       // I and J are overlapping. Find the later start.
161       SlotIndex Def = std::max(I->start, J->start);
162       // Allow the overlap if Def is a coalescable copy.
163       if (Def.isBlock() ||
164           !CP.isCoalescable(Indexes.getInstructionFromIndex(Def)))
165         return true;
166     }
167     // Advance the iterator that ends first to check for more overlaps.
168     if (J->end > I->end) {
169       std::swap(I, J);
170       std::swap(IE, JE);
171     }
172     // Advance J until J->end >= I->start.
173     do
174       if (++J == JE)
175         return false;
176     while (J->end < I->start);
177   }
180 /// overlaps - Return true if the live range overlaps an interval specified
181 /// by [Start, End).
182 bool LiveRange::overlaps(SlotIndex Start, SlotIndex End) const {
183   assert(Start < End && "Invalid range");
184   const_iterator I = std::lower_bound(begin(), end(), End);
185   return I != begin() && (--I)->end > Start;
189 /// ValNo is dead, remove it.  If it is the largest value number, just nuke it
190 /// (and any other deleted values neighboring it), otherwise mark it as ~1U so
191 /// it can be nuked later.
192 void LiveRange::markValNoForDeletion(VNInfo *ValNo) {
193   if (ValNo->id == getNumValNums()-1) {
194     do {
195       valnos.pop_back();
196     } while (!valnos.empty() && valnos.back()->isUnused());
197   } else {
198     ValNo->markUnused();
199   }
202 /// RenumberValues - Renumber all values in order of appearance and delete the
203 /// remaining unused values.
204 void LiveRange::RenumberValues() {
205   SmallPtrSet<VNInfo*, 8> Seen;
206   valnos.clear();
207   for (const_iterator I = begin(), E = end(); I != E; ++I) {
208     VNInfo *VNI = I->valno;
209     if (!Seen.insert(VNI))
210       continue;
211     assert(!VNI->isUnused() && "Unused valno used by live segment");
212     VNI->id = (unsigned)valnos.size();
213     valnos.push_back(VNI);
214   }
217 /// This method is used when we want to extend the segment specified by I to end
218 /// at the specified endpoint.  To do this, we should merge and eliminate all
219 /// segments that this will overlap with.  The iterator is not invalidated.
220 void LiveRange::extendSegmentEndTo(iterator I, SlotIndex NewEnd) {
221   assert(I != end() && "Not a valid segment!");
222   VNInfo *ValNo = I->valno;
224   // Search for the first segment that we can't merge with.
225   iterator MergeTo = std::next(I);
226   for (; MergeTo != end() && NewEnd >= MergeTo->end; ++MergeTo) {
227     assert(MergeTo->valno == ValNo && "Cannot merge with differing values!");
228   }
230   // If NewEnd was in the middle of a segment, make sure to get its endpoint.
231   I->end = std::max(NewEnd, std::prev(MergeTo)->end);
233   // If the newly formed segment now touches the segment after it and if they
234   // have the same value number, merge the two segments into one segment.
235   if (MergeTo != end() && MergeTo->start <= I->end &&
236       MergeTo->valno == ValNo) {
237     I->end = MergeTo->end;
238     ++MergeTo;
239   }
241   // Erase any dead segments.
242   segments.erase(std::next(I), MergeTo);
246 /// This method is used when we want to extend the segment specified by I to
247 /// start at the specified endpoint.  To do this, we should merge and eliminate
248 /// all segments that this will overlap with.
249 LiveRange::iterator
250 LiveRange::extendSegmentStartTo(iterator I, SlotIndex NewStart) {
251   assert(I != end() && "Not a valid segment!");
252   VNInfo *ValNo = I->valno;
254   // Search for the first segment that we can't merge with.
255   iterator MergeTo = I;
256   do {
257     if (MergeTo == begin()) {
258       I->start = NewStart;
259       segments.erase(MergeTo, I);
260       return I;
261     }
262     assert(MergeTo->valno == ValNo && "Cannot merge with differing values!");
263     --MergeTo;
264   } while (NewStart <= MergeTo->start);
266   // If we start in the middle of another segment, just delete a range and
267   // extend that segment.
268   if (MergeTo->end >= NewStart && MergeTo->valno == ValNo) {
269     MergeTo->end = I->end;
270   } else {
271     // Otherwise, extend the segment right after.
272     ++MergeTo;
273     MergeTo->start = NewStart;
274     MergeTo->end = I->end;
275   }
277   segments.erase(std::next(MergeTo), std::next(I));
278   return MergeTo;
281 LiveRange::iterator LiveRange::addSegmentFrom(Segment S, iterator From) {
282   SlotIndex Start = S.start, End = S.end;
283   iterator it = std::upper_bound(From, end(), Start);
285   // If the inserted segment starts in the middle or right at the end of
286   // another segment, just extend that segment to contain the segment of S.
287   if (it != begin()) {
288     iterator B = std::prev(it);
289     if (S.valno == B->valno) {
290       if (B->start <= Start && B->end >= Start) {
291         extendSegmentEndTo(B, End);
292         return B;
293       }
294     } else {
295       // Check to make sure that we are not overlapping two live segments with
296       // different valno's.
297       assert(B->end <= Start &&
298              "Cannot overlap two segments with differing ValID's"
299              " (did you def the same reg twice in a MachineInstr?)");
300     }
301   }
303   // Otherwise, if this segment ends in the middle of, or right next to, another
304   // segment, merge it into that segment.
305   if (it != end()) {
306     if (S.valno == it->valno) {
307       if (it->start <= End) {
308         it = extendSegmentStartTo(it, Start);
310         // If S is a complete superset of a segment, we may need to grow its
311         // endpoint as well.
312         if (End > it->end)
313           extendSegmentEndTo(it, End);
314         return it;
315       }
316     } else {
317       // Check to make sure that we are not overlapping two live segments with
318       // different valno's.
319       assert(it->start >= End &&
320              "Cannot overlap two segments with differing ValID's");
321     }
322   }
324   // Otherwise, this is just a new segment that doesn't interact with anything.
325   // Insert it.
326   return segments.insert(it, S);
329 /// extendInBlock - If this range is live before Kill in the basic
330 /// block that starts at StartIdx, extend it to be live up to Kill and return
331 /// the value. If there is no live range before Kill, return NULL.
332 VNInfo *LiveRange::extendInBlock(SlotIndex StartIdx, SlotIndex Kill) {
333   if (empty())
334     return nullptr;
335   iterator I = std::upper_bound(begin(), end(), Kill.getPrevSlot());
336   if (I == begin())
337     return nullptr;
338   --I;
339   if (I->end <= StartIdx)
340     return nullptr;
341   if (I->end < Kill)
342     extendSegmentEndTo(I, Kill);
343   return I->valno;
346 /// Remove the specified segment from this range.  Note that the segment must
347 /// be in a single Segment in its entirety.
348 void LiveRange::removeSegment(SlotIndex Start, SlotIndex End,
349                               bool RemoveDeadValNo) {
350   // Find the Segment containing this span.
351   iterator I = find(Start);
352   assert(I != end() && "Segment is not in range!");
353   assert(I->containsInterval(Start, End)
354          && "Segment is not entirely in range!");
356   // If the span we are removing is at the start of the Segment, adjust it.
357   VNInfo *ValNo = I->valno;
358   if (I->start == Start) {
359     if (I->end == End) {
360       if (RemoveDeadValNo) {
361         // Check if val# is dead.
362         bool isDead = true;
363         for (const_iterator II = begin(), EE = end(); II != EE; ++II)
364           if (II != I && II->valno == ValNo) {
365             isDead = false;
366             break;
367           }
368         if (isDead) {
369           // Now that ValNo is dead, remove it.
370           markValNoForDeletion(ValNo);
371         }
372       }
374       segments.erase(I);  // Removed the whole Segment.
375     } else
376       I->start = End;
377     return;
378   }
380   // Otherwise if the span we are removing is at the end of the Segment,
381   // adjust the other way.
382   if (I->end == End) {
383     I->end = Start;
384     return;
385   }
387   // Otherwise, we are splitting the Segment into two pieces.
388   SlotIndex OldEnd = I->end;
389   I->end = Start;   // Trim the old segment.
391   // Insert the new one.
392   segments.insert(std::next(I), Segment(End, OldEnd, ValNo));
395 /// removeValNo - Remove all the segments defined by the specified value#.
396 /// Also remove the value# from value# list.
397 void LiveRange::removeValNo(VNInfo *ValNo) {
398   if (empty()) return;
399   iterator I = end();
400   iterator E = begin();
401   do {
402     --I;
403     if (I->valno == ValNo)
404       segments.erase(I);
405   } while (I != E);
406   // Now that ValNo is dead, remove it.
407   markValNoForDeletion(ValNo);
410 void LiveRange::join(LiveRange &Other,
411                      const int *LHSValNoAssignments,
412                      const int *RHSValNoAssignments,
413                      SmallVectorImpl<VNInfo *> &NewVNInfo) {
414   verify();
416   // Determine if any of our values are mapped.  This is uncommon, so we want
417   // to avoid the range scan if not.
418   bool MustMapCurValNos = false;
419   unsigned NumVals = getNumValNums();
420   unsigned NumNewVals = NewVNInfo.size();
421   for (unsigned i = 0; i != NumVals; ++i) {
422     unsigned LHSValID = LHSValNoAssignments[i];
423     if (i != LHSValID ||
424         (NewVNInfo[LHSValID] && NewVNInfo[LHSValID] != getValNumInfo(i))) {
425       MustMapCurValNos = true;
426       break;
427     }
428   }
430   // If we have to apply a mapping to our base range assignment, rewrite it now.
431   if (MustMapCurValNos && !empty()) {
432     // Map the first live range.
434     iterator OutIt = begin();
435     OutIt->valno = NewVNInfo[LHSValNoAssignments[OutIt->valno->id]];
436     for (iterator I = std::next(OutIt), E = end(); I != E; ++I) {
437       VNInfo* nextValNo = NewVNInfo[LHSValNoAssignments[I->valno->id]];
438       assert(nextValNo && "Huh?");
440       // If this live range has the same value # as its immediate predecessor,
441       // and if they are neighbors, remove one Segment.  This happens when we
442       // have [0,4:0)[4,7:1) and map 0/1 onto the same value #.
443       if (OutIt->valno == nextValNo && OutIt->end == I->start) {
444         OutIt->end = I->end;
445       } else {
446         // Didn't merge. Move OutIt to the next segment,
447         ++OutIt;
448         OutIt->valno = nextValNo;
449         if (OutIt != I) {
450           OutIt->start = I->start;
451           OutIt->end = I->end;
452         }
453       }
454     }
455     // If we merge some segments, chop off the end.
456     ++OutIt;
457     segments.erase(OutIt, end());
458   }
460   // Rewrite Other values before changing the VNInfo ids.
461   // This can leave Other in an invalid state because we're not coalescing
462   // touching segments that now have identical values. That's OK since Other is
463   // not supposed to be valid after calling join();
464   for (iterator I = Other.begin(), E = Other.end(); I != E; ++I)
465     I->valno = NewVNInfo[RHSValNoAssignments[I->valno->id]];
467   // Update val# info. Renumber them and make sure they all belong to this
468   // LiveRange now. Also remove dead val#'s.
469   unsigned NumValNos = 0;
470   for (unsigned i = 0; i < NumNewVals; ++i) {
471     VNInfo *VNI = NewVNInfo[i];
472     if (VNI) {
473       if (NumValNos >= NumVals)
474         valnos.push_back(VNI);
475       else
476         valnos[NumValNos] = VNI;
477       VNI->id = NumValNos++;  // Renumber val#.
478     }
479   }
480   if (NumNewVals < NumVals)
481     valnos.resize(NumNewVals);  // shrinkify
483   // Okay, now insert the RHS live segments into the LHS.
484   LiveRangeUpdater Updater(this);
485   for (iterator I = Other.begin(), E = Other.end(); I != E; ++I)
486     Updater.add(*I);
489 /// Merge all of the segments in RHS into this live range as the specified
490 /// value number.  The segments in RHS are allowed to overlap with segments in
491 /// the current range, but only if the overlapping segments have the
492 /// specified value number.
493 void LiveRange::MergeSegmentsInAsValue(const LiveRange &RHS,
494                                        VNInfo *LHSValNo) {
495   LiveRangeUpdater Updater(this);
496   for (const_iterator I = RHS.begin(), E = RHS.end(); I != E; ++I)
497     Updater.add(I->start, I->end, LHSValNo);
500 /// MergeValueInAsValue - Merge all of the live segments of a specific val#
501 /// in RHS into this live range as the specified value number.
502 /// The segments in RHS are allowed to overlap with segments in the
503 /// current range, it will replace the value numbers of the overlaped
504 /// segments with the specified value number.
505 void LiveRange::MergeValueInAsValue(const LiveRange &RHS,
506                                     const VNInfo *RHSValNo,
507                                     VNInfo *LHSValNo) {
508   LiveRangeUpdater Updater(this);
509   for (const_iterator I = RHS.begin(), E = RHS.end(); I != E; ++I)
510     if (I->valno == RHSValNo)
511       Updater.add(I->start, I->end, LHSValNo);
514 /// MergeValueNumberInto - This method is called when two value nubmers
515 /// are found to be equivalent.  This eliminates V1, replacing all
516 /// segments with the V1 value number with the V2 value number.  This can
517 /// cause merging of V1/V2 values numbers and compaction of the value space.
518 VNInfo *LiveRange::MergeValueNumberInto(VNInfo *V1, VNInfo *V2) {
519   assert(V1 != V2 && "Identical value#'s are always equivalent!");
521   // This code actually merges the (numerically) larger value number into the
522   // smaller value number, which is likely to allow us to compactify the value
523   // space.  The only thing we have to be careful of is to preserve the
524   // instruction that defines the result value.
526   // Make sure V2 is smaller than V1.
527   if (V1->id < V2->id) {
528     V1->copyFrom(*V2);
529     std::swap(V1, V2);
530   }
532   // Merge V1 segments into V2.
533   for (iterator I = begin(); I != end(); ) {
534     iterator S = I++;
535     if (S->valno != V1) continue;  // Not a V1 Segment.
537     // Okay, we found a V1 live range.  If it had a previous, touching, V2 live
538     // range, extend it.
539     if (S != begin()) {
540       iterator Prev = S-1;
541       if (Prev->valno == V2 && Prev->end == S->start) {
542         Prev->end = S->end;
544         // Erase this live-range.
545         segments.erase(S);
546         I = Prev+1;
547         S = Prev;
548       }
549     }
551     // Okay, now we have a V1 or V2 live range that is maximally merged forward.
552     // Ensure that it is a V2 live-range.
553     S->valno = V2;
555     // If we can merge it into later V2 segments, do so now.  We ignore any
556     // following V1 segments, as they will be merged in subsequent iterations
557     // of the loop.
558     if (I != end()) {
559       if (I->start == S->end && I->valno == V2) {
560         S->end = I->end;
561         segments.erase(I);
562         I = S+1;
563       }
564     }
565   }
567   // Now that V1 is dead, remove it.
568   markValNoForDeletion(V1);
570   return V2;
573 unsigned LiveInterval::getSize() const {
574   unsigned Sum = 0;
575   for (const_iterator I = begin(), E = end(); I != E; ++I)
576     Sum += I->start.distance(I->end);
577   return Sum;
580 raw_ostream& llvm::operator<<(raw_ostream& os, const LiveRange::Segment &S) {
581   return os << '[' << S.start << ',' << S.end << ':' << S.valno->id << ")";
584 #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
585 void LiveRange::Segment::dump() const {
586   dbgs() << *this << "\n";
588 #endif
590 void LiveRange::print(raw_ostream &OS) const {
591   if (empty())
592     OS << "EMPTY";
593   else {
594     for (const_iterator I = begin(), E = end(); I != E; ++I) {
595       OS << *I;
596       assert(I->valno == getValNumInfo(I->valno->id) && "Bad VNInfo");
597     }
598   }
600   // Print value number info.
601   if (getNumValNums()) {
602     OS << "  ";
603     unsigned vnum = 0;
604     for (const_vni_iterator i = vni_begin(), e = vni_end(); i != e;
605          ++i, ++vnum) {
606       const VNInfo *vni = *i;
607       if (vnum) OS << " ";
608       OS << vnum << "@";
609       if (vni->isUnused()) {
610         OS << "x";
611       } else {
612         OS << vni->def;
613         if (vni->isPHIDef())
614           OS << "-phi";
615       }
616     }
617   }
620 void LiveInterval::print(raw_ostream &OS) const {
621   OS << PrintReg(reg) << ' ';
622   super::print(OS);
625 #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
626 void LiveRange::dump() const {
627   dbgs() << *this << "\n";
630 void LiveInterval::dump() const {
631   dbgs() << *this << "\n";
633 #endif
635 #ifndef NDEBUG
636 void LiveRange::verify() const {
637   for (const_iterator I = begin(), E = end(); I != E; ++I) {
638     assert(I->start.isValid());
639     assert(I->end.isValid());
640     assert(I->start < I->end);
641     assert(I->valno != nullptr);
642     assert(I->valno->id < valnos.size());
643     assert(I->valno == valnos[I->valno->id]);
644     if (std::next(I) != E) {
645       assert(I->end <= std::next(I)->start);
646       if (I->end == std::next(I)->start)
647         assert(I->valno != std::next(I)->valno);
648     }
649   }
651 #endif
654 //===----------------------------------------------------------------------===//
655 //                           LiveRangeUpdater class
656 //===----------------------------------------------------------------------===//
657 //
658 // The LiveRangeUpdater class always maintains these invariants:
659 //
660 // - When LastStart is invalid, Spills is empty and the iterators are invalid.
661 //   This is the initial state, and the state created by flush().
662 //   In this state, isDirty() returns false.
663 //
664 // Otherwise, segments are kept in three separate areas:
665 //
666 // 1. [begin; WriteI) at the front of LR.
667 // 2. [ReadI; end) at the back of LR.
668 // 3. Spills.
669 //
670 // - LR.begin() <= WriteI <= ReadI <= LR.end().
671 // - Segments in all three areas are fully ordered and coalesced.
672 // - Segments in area 1 precede and can't coalesce with segments in area 2.
673 // - Segments in Spills precede and can't coalesce with segments in area 2.
674 // - No coalescing is possible between segments in Spills and segments in area
675 //   1, and there are no overlapping segments.
676 //
677 // The segments in Spills are not ordered with respect to the segments in area
678 // 1. They need to be merged.
679 //
680 // When they exist, Spills.back().start <= LastStart,
681 //                 and WriteI[-1].start <= LastStart.
683 void LiveRangeUpdater::print(raw_ostream &OS) const {
684   if (!isDirty()) {
685     if (LR)
686       OS << "Clean updater: " << *LR << '\n';
687     else
688       OS << "Null updater.\n";
689     return;
690   }
691   assert(LR && "Can't have null LR in dirty updater.");
692   OS << " updater with gap = " << (ReadI - WriteI)
693      << ", last start = " << LastStart
694      << ":\n  Area 1:";
695   for (LiveRange::const_iterator I = LR->begin(); I != WriteI; ++I)
696     OS << ' ' << *I;
697   OS << "\n  Spills:";
698   for (unsigned I = 0, E = Spills.size(); I != E; ++I)
699     OS << ' ' << Spills[I];
700   OS << "\n  Area 2:";
701   for (LiveRange::const_iterator I = ReadI, E = LR->end(); I != E; ++I)
702     OS << ' ' << *I;
703   OS << '\n';
706 void LiveRangeUpdater::dump() const
708   print(errs());
711 // Determine if A and B should be coalesced.
712 static inline bool coalescable(const LiveRange::Segment &A,
713                                const LiveRange::Segment &B) {
714   assert(A.start <= B.start && "Unordered live segments.");
715   if (A.end == B.start)
716     return A.valno == B.valno;
717   if (A.end < B.start)
718     return false;
719   assert(A.valno == B.valno && "Cannot overlap different values");
720   return true;
723 void LiveRangeUpdater::add(LiveRange::Segment Seg) {
724   assert(LR && "Cannot add to a null destination");
726   // Flush the state if Start moves backwards.
727   if (!LastStart.isValid() || LastStart > Seg.start) {
728     if (isDirty())
729       flush();
730     // This brings us to an uninitialized state. Reinitialize.
731     assert(Spills.empty() && "Leftover spilled segments");
732     WriteI = ReadI = LR->begin();
733   }
735   // Remember start for next time.
736   LastStart = Seg.start;
738   // Advance ReadI until it ends after Seg.start.
739   LiveRange::iterator E = LR->end();
740   if (ReadI != E && ReadI->end <= Seg.start) {
741     // First try to close the gap between WriteI and ReadI with spills.
742     if (ReadI != WriteI)
743       mergeSpills();
744     // Then advance ReadI.
745     if (ReadI == WriteI)
746       ReadI = WriteI = LR->find(Seg.start);
747     else
748       while (ReadI != E && ReadI->end <= Seg.start)
749         *WriteI++ = *ReadI++;
750   }
752   assert(ReadI == E || ReadI->end > Seg.start);
754   // Check if the ReadI segment begins early.
755   if (ReadI != E && ReadI->start <= Seg.start) {
756     assert(ReadI->valno == Seg.valno && "Cannot overlap different values");
757     // Bail if Seg is completely contained in ReadI.
758     if (ReadI->end >= Seg.end)
759       return;
760     // Coalesce into Seg.
761     Seg.start = ReadI->start;
762     ++ReadI;
763   }
765   // Coalesce as much as possible from ReadI into Seg.
766   while (ReadI != E && coalescable(Seg, *ReadI)) {
767     Seg.end = std::max(Seg.end, ReadI->end);
768     ++ReadI;
769   }
771   // Try coalescing Spills.back() into Seg.
772   if (!Spills.empty() && coalescable(Spills.back(), Seg)) {
773     Seg.start = Spills.back().start;
774     Seg.end = std::max(Spills.back().end, Seg.end);
775     Spills.pop_back();
776   }
778   // Try coalescing Seg into WriteI[-1].
779   if (WriteI != LR->begin() && coalescable(WriteI[-1], Seg)) {
780     WriteI[-1].end = std::max(WriteI[-1].end, Seg.end);
781     return;
782   }
784   // Seg doesn't coalesce with anything, and needs to be inserted somewhere.
785   if (WriteI != ReadI) {
786     *WriteI++ = Seg;
787     return;
788   }
790   // Finally, append to LR or Spills.
791   if (WriteI == E) {
792     LR->segments.push_back(Seg);
793     WriteI = ReadI = LR->end();
794   } else
795     Spills.push_back(Seg);
798 // Merge as many spilled segments as possible into the gap between WriteI
799 // and ReadI. Advance WriteI to reflect the inserted instructions.
800 void LiveRangeUpdater::mergeSpills() {
801   // Perform a backwards merge of Spills and [SpillI;WriteI).
802   size_t GapSize = ReadI - WriteI;
803   size_t NumMoved = std::min(Spills.size(), GapSize);
804   LiveRange::iterator Src = WriteI;
805   LiveRange::iterator Dst = Src + NumMoved;
806   LiveRange::iterator SpillSrc = Spills.end();
807   LiveRange::iterator B = LR->begin();
809   // This is the new WriteI position after merging spills.
810   WriteI = Dst;
812   // Now merge Src and Spills backwards.
813   while (Src != Dst) {
814     if (Src != B && Src[-1].start > SpillSrc[-1].start)
815       *--Dst = *--Src;
816     else
817       *--Dst = *--SpillSrc;
818   }
819   assert(NumMoved == size_t(Spills.end() - SpillSrc));
820   Spills.erase(SpillSrc, Spills.end());
823 void LiveRangeUpdater::flush() {
824   if (!isDirty())
825     return;
826   // Clear the dirty state.
827   LastStart = SlotIndex();
829   assert(LR && "Cannot add to a null destination");
831   // Nothing to merge?
832   if (Spills.empty()) {
833     LR->segments.erase(WriteI, ReadI);
834     LR->verify();
835     return;
836   }
838   // Resize the WriteI - ReadI gap to match Spills.
839   size_t GapSize = ReadI - WriteI;
840   if (GapSize < Spills.size()) {
841     // The gap is too small. Make some room.
842     size_t WritePos = WriteI - LR->begin();
843     LR->segments.insert(ReadI, Spills.size() - GapSize, LiveRange::Segment());
844     // This also invalidated ReadI, but it is recomputed below.
845     WriteI = LR->begin() + WritePos;
846   } else {
847     // Shrink the gap if necessary.
848     LR->segments.erase(WriteI + Spills.size(), ReadI);
849   }
850   ReadI = WriteI + Spills.size();
851   mergeSpills();
852   LR->verify();
855 unsigned ConnectedVNInfoEqClasses::Classify(const LiveInterval *LI) {
856   // Create initial equivalence classes.
857   EqClass.clear();
858   EqClass.grow(LI->getNumValNums());
860   const VNInfo *used = nullptr, *unused = nullptr;
862   // Determine connections.
863   for (LiveInterval::const_vni_iterator I = LI->vni_begin(), E = LI->vni_end();
864        I != E; ++I) {
865     const VNInfo *VNI = *I;
866     // Group all unused values into one class.
867     if (VNI->isUnused()) {
868       if (unused)
869         EqClass.join(unused->id, VNI->id);
870       unused = VNI;
871       continue;
872     }
873     used = VNI;
874     if (VNI->isPHIDef()) {
875       const MachineBasicBlock *MBB = LIS.getMBBFromIndex(VNI->def);
876       assert(MBB && "Phi-def has no defining MBB");
877       // Connect to values live out of predecessors.
878       for (MachineBasicBlock::const_pred_iterator PI = MBB->pred_begin(),
879            PE = MBB->pred_end(); PI != PE; ++PI)
880         if (const VNInfo *PVNI = LI->getVNInfoBefore(LIS.getMBBEndIdx(*PI)))
881           EqClass.join(VNI->id, PVNI->id);
882     } else {
883       // Normal value defined by an instruction. Check for two-addr redef.
884       // FIXME: This could be coincidental. Should we really check for a tied
885       // operand constraint?
886       // Note that VNI->def may be a use slot for an early clobber def.
887       if (const VNInfo *UVNI = LI->getVNInfoBefore(VNI->def))
888         EqClass.join(VNI->id, UVNI->id);
889     }
890   }
892   // Lump all the unused values in with the last used value.
893   if (used && unused)
894     EqClass.join(used->id, unused->id);
896   EqClass.compress();
897   return EqClass.getNumClasses();
900 void ConnectedVNInfoEqClasses::Distribute(LiveInterval *LIV[],
901                                           MachineRegisterInfo &MRI) {
902   assert(LIV[0] && "LIV[0] must be set");
903   LiveInterval &LI = *LIV[0];
905   // Rewrite instructions.
906   for (MachineRegisterInfo::reg_iterator RI = MRI.reg_begin(LI.reg),
907        RE = MRI.reg_end(); RI != RE;) {
908     MachineOperand &MO = *RI;
909     MachineInstr *MI = RI->getParent();
910     ++RI;
911     // DBG_VALUE instructions don't have slot indexes, so get the index of the
912     // instruction before them.
913     // Normally, DBG_VALUE instructions are removed before this function is
914     // called, but it is not a requirement.
915     SlotIndex Idx;
916     if (MI->isDebugValue())
917       Idx = LIS.getSlotIndexes()->getIndexBefore(MI);
918     else
919       Idx = LIS.getInstructionIndex(MI);
920     LiveQueryResult LRQ = LI.Query(Idx);
921     const VNInfo *VNI = MO.readsReg() ? LRQ.valueIn() : LRQ.valueDefined();
922     // In the case of an <undef> use that isn't tied to any def, VNI will be
923     // NULL. If the use is tied to a def, VNI will be the defined value.
924     if (!VNI)
925       continue;
926     MO.setReg(LIV[getEqClass(VNI)]->reg);
927   }
929   // Move runs to new intervals.
930   LiveInterval::iterator J = LI.begin(), E = LI.end();
931   while (J != E && EqClass[J->valno->id] == 0)
932     ++J;
933   for (LiveInterval::iterator I = J; I != E; ++I) {
934     if (unsigned eq = EqClass[I->valno->id]) {
935       assert((LIV[eq]->empty() || LIV[eq]->expiredAt(I->start)) &&
936              "New intervals should be empty");
937       LIV[eq]->segments.push_back(*I);
938     } else
939       *J++ = *I;
940   }
941   LI.segments.erase(J, E);
943   // Transfer VNInfos to their new owners and renumber them.
944   unsigned j = 0, e = LI.getNumValNums();
945   while (j != e && EqClass[j] == 0)
946     ++j;
947   for (unsigned i = j; i != e; ++i) {
948     VNInfo *VNI = LI.getValNumInfo(i);
949     if (unsigned eq = EqClass[i]) {
950       VNI->id = LIV[eq]->getNumValNums();
951       LIV[eq]->valnos.push_back(VNI);
952     } else {
953       VNI->id = j;
954       LI.valnos[j++] = VNI;
955     }
956   }
957   LI.valnos.resize(j);