1 //===---- LiveRangeCalc.h - Calculate live ranges ---------------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // The LiveRangeCalc class can be used to compute live ranges from scratch. It
11 // caches information about values in the CFG to speed up repeated operations
12 // on the same live range. The cache can be shared by non-overlapping live
13 // ranges. SplitKit uses that when computing the live range of split products.
14 //
15 // A low-level interface is available to clients that know where a variable is
16 // live, but don't know which value it has as every point. LiveRangeCalc will
17 // propagate values down the dominator tree, and even insert PHI-defs where
18 // needed. SplitKit uses this faster interface when possible.
19 //
20 //===----------------------------------------------------------------------===//
22 #ifndef LLVM_CODEGEN_LIVERANGECALC_H
23 #define LLVM_CODEGEN_LIVERANGECALC_H
25 #include "llvm/ADT/BitVector.h"
26 #include "llvm/ADT/IndexedMap.h"
27 #include "llvm/CodeGen/LiveInterval.h"
29 namespace llvm {
31 /// Forward declarations for MachineDominators.h:
32 class MachineDominatorTree;
33 template <class NodeT> class DomTreeNodeBase;
34 typedef DomTreeNodeBase<MachineBasicBlock> MachineDomTreeNode;
36 class LiveRangeCalc {
37 const MachineFunction *MF;
38 const MachineRegisterInfo *MRI;
39 SlotIndexes *Indexes;
40 MachineDominatorTree *DomTree;
41 VNInfo::Allocator *Alloc;
43 /// Seen - Bit vector of active entries in LiveOut, also used as a visited
44 /// set by findReachingDefs. One entry per basic block, indexed by block
45 /// number. This is kept as a separate bit vector because it can be cleared
46 /// quickly when switching live ranges.
47 BitVector Seen;
49 /// LiveOutPair - A value and the block that defined it. The domtree node is
50 /// redundant, it can be computed as: MDT[Indexes.getMBBFromIndex(VNI->def)].
51 typedef std::pair<VNInfo*, MachineDomTreeNode*> LiveOutPair;
53 /// LiveOutMap - Map basic blocks to the value leaving the block.
54 typedef IndexedMap<LiveOutPair, MBB2NumberFunctor> LiveOutMap;
56 /// LiveOut - Map each basic block where a live range is live out to the
57 /// live-out value and its defining block.
58 ///
59 /// For every basic block, MBB, one of these conditions shall be true:
60 ///
61 /// 1. !Seen.count(MBB->getNumber())
62 /// Blocks without a Seen bit are ignored.
63 /// 2. LiveOut[MBB].second.getNode() == MBB
64 /// The live-out value is defined in MBB.
65 /// 3. forall P in preds(MBB): LiveOut[P] == LiveOut[MBB]
66 /// The live-out value passses through MBB. All predecessors must carry
67 /// the same value.
68 ///
69 /// The domtree node may be null, it can be computed.
70 ///
71 /// The map can be shared by multiple live ranges as long as no two are
72 /// live-out of the same block.
73 LiveOutMap LiveOut;
75 /// LiveInBlock - Information about a basic block where a live range is known
76 /// to be live-in, but the value has not yet been determined.
77 struct LiveInBlock {
78 // The live range set that is live-in to this block. The algorithms can
79 // handle multiple non-overlapping live ranges simultaneously.
80 LiveRange &LR;
82 // DomNode - Dominator tree node for the block.
83 // Cleared when the final value has been determined and LI has been updated.
84 MachineDomTreeNode *DomNode;
86 // Position in block where the live-in range ends, or SlotIndex() if the
87 // range passes through the block. When the final value has been
88 // determined, the range from the block start to Kill will be added to LI.
89 SlotIndex Kill;
91 // Live-in value filled in by updateSSA once it is known.
92 VNInfo *Value;
94 LiveInBlock(LiveRange &LR, MachineDomTreeNode *node, SlotIndex kill)
95 : LR(LR), DomNode(node), Kill(kill), Value(nullptr) {}
96 };
98 /// LiveIn - Work list of blocks where the live-in value has yet to be
99 /// determined. This list is typically computed by findReachingDefs() and
100 /// used as a work list by updateSSA(). The low-level interface may also be
101 /// used to add entries directly.
102 SmallVector<LiveInBlock, 16> LiveIn;
104 /// Assuming that LI is live-in to KillMBB and killed at Kill, find the set
105 /// of defs that can reach it.
106 ///
107 /// If only one def can reach Kill, all paths from the def to kill are added
108 /// to LI, and the function returns true.
109 ///
110 /// If multiple values can reach Kill, the blocks that need LI to be live in
111 /// are added to the LiveIn array, and the function returns false.
112 ///
113 /// PhysReg, when set, is used to verify live-in lists on basic blocks.
114 bool findReachingDefs(LiveRange &LR, MachineBasicBlock &KillMBB,
115 SlotIndex Kill, unsigned PhysReg);
117 /// updateSSA - Compute the values that will be live in to all requested
118 /// blocks in LiveIn. Create PHI-def values as required to preserve SSA form.
119 ///
120 /// Every live-in block must be jointly dominated by the added live-out
121 /// blocks. No values are read from the live ranges.
122 void updateSSA();
124 /// Add liveness as specified in the LiveIn vector.
125 void updateLiveIns();
127 public:
128 LiveRangeCalc() : MF(nullptr), MRI(nullptr), Indexes(nullptr),
129 DomTree(nullptr), Alloc(nullptr) {}
131 //===--------------------------------------------------------------------===//
132 // High-level interface.
133 //===--------------------------------------------------------------------===//
134 //
135 // Calculate live ranges from scratch.
136 //
138 /// reset - Prepare caches for a new set of non-overlapping live ranges. The
139 /// caches must be reset before attempting calculations with a live range
140 /// that may overlap a previously computed live range, and before the first
141 /// live range in a function. If live ranges are not known to be
142 /// non-overlapping, call reset before each.
143 void reset(const MachineFunction *MF,
144 SlotIndexes*,
145 MachineDominatorTree*,
146 VNInfo::Allocator*);
148 //===--------------------------------------------------------------------===//
149 // Mid-level interface.
150 //===--------------------------------------------------------------------===//
151 //
152 // Modify existing live ranges.
153 //
155 /// extend - Extend the live range of LI to reach Kill.
156 ///
157 /// The existing values in LI must be live so they jointly dominate Kill. If
158 /// Kill is not dominated by a single existing value, PHI-defs are inserted
159 /// as required to preserve SSA form. If Kill is known to be dominated by a
160 /// single existing value, Alloc may be null.
161 ///
162 /// PhysReg, when set, is used to verify live-in lists on basic blocks.
163 void extend(LiveRange &LR, SlotIndex Kill, unsigned PhysReg = 0);
165 /// createDeadDefs - Create a dead def in LI for every def operand of Reg.
166 /// Each instruction defining Reg gets a new VNInfo with a corresponding
167 /// minimal live range.
168 void createDeadDefs(LiveRange &LR, unsigned Reg);
170 /// createDeadDefs - Create a dead def in LI for every def of LI->reg.
171 void createDeadDefs(LiveInterval &LI) {
172 createDeadDefs(LI, LI.reg);
173 }
175 /// extendToUses - Extend the live range of LI to reach all uses of Reg.
176 ///
177 /// All uses must be jointly dominated by existing liveness. PHI-defs are
178 /// inserted as needed to preserve SSA form.
179 void extendToUses(LiveRange &LR, unsigned Reg);
181 /// extendToUses - Extend the live range of LI to reach all uses of LI->reg.
182 void extendToUses(LiveInterval &LI) {
183 extendToUses(LI, LI.reg);
184 }
186 //===--------------------------------------------------------------------===//
187 // Low-level interface.
188 //===--------------------------------------------------------------------===//
189 //
190 // These functions can be used to compute live ranges where the live-in and
191 // live-out blocks are already known, but the SSA value in each block is
192 // unknown.
193 //
194 // After calling reset(), add known live-out values and known live-in blocks.
195 // Then call calculateValues() to compute the actual value that is
196 // live-in to each block, and add liveness to the live ranges.
197 //
199 /// setLiveOutValue - Indicate that VNI is live out from MBB. The
200 /// calculateValues() function will not add liveness for MBB, the caller
201 /// should take care of that.
202 ///
203 /// VNI may be null only if MBB is a live-through block also passed to
204 /// addLiveInBlock().
205 void setLiveOutValue(MachineBasicBlock *MBB, VNInfo *VNI) {
206 Seen.set(MBB->getNumber());
207 LiveOut[MBB] = LiveOutPair(VNI, nullptr);
208 }
210 /// addLiveInBlock - Add a block with an unknown live-in value. This
211 /// function can only be called once per basic block. Once the live-in value
212 /// has been determined, calculateValues() will add liveness to LI.
213 ///
214 /// @param LR The live range that is live-in to the block.
215 /// @param DomNode The domtree node for the block.
216 /// @param Kill Index in block where LI is killed. If the value is
217 /// live-through, set Kill = SLotIndex() and also call
218 /// setLiveOutValue(MBB, 0).
219 void addLiveInBlock(LiveRange &LR,
220 MachineDomTreeNode *DomNode,
221 SlotIndex Kill = SlotIndex()) {
222 LiveIn.push_back(LiveInBlock(LR, DomNode, Kill));
223 }
225 /// calculateValues - Calculate the value that will be live-in to each block
226 /// added with addLiveInBlock. Add PHI-def values as needed to preserve SSA
227 /// form. Add liveness to all live-in blocks up to the Kill point, or the
228 /// whole block for live-through blocks.
229 ///
230 /// Every predecessor of a live-in block must have been given a value with
231 /// setLiveOutValue, the value may be null for live-trough blocks.
232 void calculateValues();
233 };
235 } // end namespace llvm
237 #endif