]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/OptimizePHIs.cpp
Add a couple of convenience accessors to DebugLocEntry::Value to further
[opencl/llvm.git] / lib / CodeGen / OptimizePHIs.cpp
1 //===-- OptimizePHIs.cpp - Optimize machine instruction PHIs --------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass optimizes machine instruction PHIs to take advantage of
11 // opportunities created during DAG legalization.
12 //
13 //===----------------------------------------------------------------------===//
15 #include "llvm/CodeGen/Passes.h"
16 #include "llvm/ADT/SmallPtrSet.h"
17 #include "llvm/ADT/Statistic.h"
18 #include "llvm/CodeGen/MachineFunctionPass.h"
19 #include "llvm/CodeGen/MachineInstr.h"
20 #include "llvm/CodeGen/MachineRegisterInfo.h"
21 #include "llvm/IR/Function.h"
22 #include "llvm/Target/TargetInstrInfo.h"
23 #include "llvm/Target/TargetSubtargetInfo.h"
24 using namespace llvm;
26 #define DEBUG_TYPE "phi-opt"
28 STATISTIC(NumPHICycles, "Number of PHI cycles replaced");
29 STATISTIC(NumDeadPHICycles, "Number of dead PHI cycles");
31 namespace {
32   class OptimizePHIs : public MachineFunctionPass {
33     MachineRegisterInfo *MRI;
34     const TargetInstrInfo *TII;
36   public:
37     static char ID; // Pass identification
38     OptimizePHIs() : MachineFunctionPass(ID) {
39       initializeOptimizePHIsPass(*PassRegistry::getPassRegistry());
40     }
42     bool runOnMachineFunction(MachineFunction &MF) override;
44     void getAnalysisUsage(AnalysisUsage &AU) const override {
45       AU.setPreservesCFG();
46       MachineFunctionPass::getAnalysisUsage(AU);
47     }
49   private:
50     typedef SmallPtrSet<MachineInstr*, 16> InstrSet;
51     typedef SmallPtrSetIterator<MachineInstr*> InstrSetIterator;
53     bool IsSingleValuePHICycle(MachineInstr *MI, unsigned &SingleValReg,
54                                InstrSet &PHIsInCycle);
55     bool IsDeadPHICycle(MachineInstr *MI, InstrSet &PHIsInCycle);
56     bool OptimizeBB(MachineBasicBlock &MBB);
57   };
58 }
60 char OptimizePHIs::ID = 0;
61 char &llvm::OptimizePHIsID = OptimizePHIs::ID;
62 INITIALIZE_PASS(OptimizePHIs, "opt-phis",
63                 "Optimize machine instruction PHIs", false, false)
65 bool OptimizePHIs::runOnMachineFunction(MachineFunction &Fn) {
66   if (skipOptnoneFunction(*Fn.getFunction()))
67     return false;
69   MRI = &Fn.getRegInfo();
70   TII = Fn.getSubtarget().getInstrInfo();
72   // Find dead PHI cycles and PHI cycles that can be replaced by a single
73   // value.  InstCombine does these optimizations, but DAG legalization may
74   // introduce new opportunities, e.g., when i64 values are split up for
75   // 32-bit targets.
76   bool Changed = false;
77   for (MachineFunction::iterator I = Fn.begin(), E = Fn.end(); I != E; ++I)
78     Changed |= OptimizeBB(*I);
80   return Changed;
81 }
83 /// IsSingleValuePHICycle - Check if MI is a PHI where all the source operands
84 /// are copies of SingleValReg, possibly via copies through other PHIs.  If
85 /// SingleValReg is zero on entry, it is set to the register with the single
86 /// non-copy value.  PHIsInCycle is a set used to keep track of the PHIs that
87 /// have been scanned.
88 bool OptimizePHIs::IsSingleValuePHICycle(MachineInstr *MI,
89                                          unsigned &SingleValReg,
90                                          InstrSet &PHIsInCycle) {
91   assert(MI->isPHI() && "IsSingleValuePHICycle expects a PHI instruction");
92   unsigned DstReg = MI->getOperand(0).getReg();
94   // See if we already saw this register.
95   if (!PHIsInCycle.insert(MI))
96     return true;
98   // Don't scan crazily complex things.
99   if (PHIsInCycle.size() == 16)
100     return false;
102   // Scan the PHI operands.
103   for (unsigned i = 1; i != MI->getNumOperands(); i += 2) {
104     unsigned SrcReg = MI->getOperand(i).getReg();
105     if (SrcReg == DstReg)
106       continue;
107     MachineInstr *SrcMI = MRI->getVRegDef(SrcReg);
109     // Skip over register-to-register moves.
110     if (SrcMI && SrcMI->isCopy() &&
111         !SrcMI->getOperand(0).getSubReg() &&
112         !SrcMI->getOperand(1).getSubReg() &&
113         TargetRegisterInfo::isVirtualRegister(SrcMI->getOperand(1).getReg()))
114       SrcMI = MRI->getVRegDef(SrcMI->getOperand(1).getReg());
115     if (!SrcMI)
116       return false;
118     if (SrcMI->isPHI()) {
119       if (!IsSingleValuePHICycle(SrcMI, SingleValReg, PHIsInCycle))
120         return false;
121     } else {
122       // Fail if there is more than one non-phi/non-move register.
123       if (SingleValReg != 0)
124         return false;
125       SingleValReg = SrcReg;
126     }
127   }
128   return true;
131 /// IsDeadPHICycle - Check if the register defined by a PHI is only used by
132 /// other PHIs in a cycle.
133 bool OptimizePHIs::IsDeadPHICycle(MachineInstr *MI, InstrSet &PHIsInCycle) {
134   assert(MI->isPHI() && "IsDeadPHICycle expects a PHI instruction");
135   unsigned DstReg = MI->getOperand(0).getReg();
136   assert(TargetRegisterInfo::isVirtualRegister(DstReg) &&
137          "PHI destination is not a virtual register");
139   // See if we already saw this register.
140   if (!PHIsInCycle.insert(MI))
141     return true;
143   // Don't scan crazily complex things.
144   if (PHIsInCycle.size() == 16)
145     return false;
147   for (MachineInstr &UseMI : MRI->use_instructions(DstReg)) {
148     if (!UseMI.isPHI() || !IsDeadPHICycle(&UseMI, PHIsInCycle))
149       return false;
150   }
152   return true;
155 /// OptimizeBB - Remove dead PHI cycles and PHI cycles that can be replaced by
156 /// a single value.
157 bool OptimizePHIs::OptimizeBB(MachineBasicBlock &MBB) {
158   bool Changed = false;
159   for (MachineBasicBlock::iterator
160          MII = MBB.begin(), E = MBB.end(); MII != E; ) {
161     MachineInstr *MI = &*MII++;
162     if (!MI->isPHI())
163       break;
165     // Check for single-value PHI cycles.
166     unsigned SingleValReg = 0;
167     InstrSet PHIsInCycle;
168     if (IsSingleValuePHICycle(MI, SingleValReg, PHIsInCycle) &&
169         SingleValReg != 0) {
170       unsigned OldReg = MI->getOperand(0).getReg();
171       if (!MRI->constrainRegClass(SingleValReg, MRI->getRegClass(OldReg)))
172         continue;
174       MRI->replaceRegWith(OldReg, SingleValReg);
175       MI->eraseFromParent();
176       ++NumPHICycles;
177       Changed = true;
178       continue;
179     }
181     // Check for dead PHI cycles.
182     PHIsInCycle.clear();
183     if (IsDeadPHICycle(MI, PHIsInCycle)) {
184       for (InstrSetIterator PI = PHIsInCycle.begin(), PE = PHIsInCycle.end();
185            PI != PE; ++PI) {
186         MachineInstr *PhiMI = *PI;
187         if (&*MII == PhiMI)
188           ++MII;
189         PhiMI->eraseFromParent();
190       }
191       ++NumDeadPHICycles;
192       Changed = true;
193     }
194   }
195   return Changed;