1 //===-- PrologEpilogInserter.cpp - Insert Prolog/Epilog code in function --===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass is responsible for finalizing the functions frame layout, saving
11 // callee saved registers, and for emitting prolog & epilog code for the
12 // function.
13 //
14 // This pass must be run after register allocation. After this pass is
15 // executed, it is illegal to construct MO_FrameIndex operands.
16 //
17 //===----------------------------------------------------------------------===//
19 #include "PrologEpilogInserter.h"
20 #include "llvm/ADT/IndexedMap.h"
21 #include "llvm/ADT/STLExtras.h"
22 #include "llvm/ADT/SetVector.h"
23 #include "llvm/ADT/SmallSet.h"
24 #include "llvm/ADT/Statistic.h"
25 #include "llvm/CodeGen/MachineDominators.h"
26 #include "llvm/CodeGen/MachineFrameInfo.h"
27 #include "llvm/CodeGen/MachineInstr.h"
28 #include "llvm/CodeGen/MachineLoopInfo.h"
29 #include "llvm/CodeGen/MachineModuleInfo.h"
30 #include "llvm/CodeGen/MachineRegisterInfo.h"
31 #include "llvm/CodeGen/RegisterScavenging.h"
32 #include "llvm/CodeGen/StackProtector.h"
33 #include "llvm/IR/DiagnosticInfo.h"
34 #include "llvm/IR/InlineAsm.h"
35 #include "llvm/IR/LLVMContext.h"
36 #include "llvm/Support/CommandLine.h"
37 #include "llvm/Support/Compiler.h"
38 #include "llvm/Support/Debug.h"
39 #include "llvm/Support/raw_ostream.h"
40 #include "llvm/Target/TargetFrameLowering.h"
41 #include "llvm/Target/TargetInstrInfo.h"
42 #include "llvm/Target/TargetMachine.h"
43 #include "llvm/Target/TargetRegisterInfo.h"
44 #include <climits>
46 using namespace llvm;
48 #define DEBUG_TYPE "pei"
50 char PEI::ID = 0;
51 char &llvm::PrologEpilogCodeInserterID = PEI::ID;
53 static cl::opt<unsigned>
54 WarnStackSize("warn-stack-size", cl::Hidden, cl::init((unsigned)-1),
55 cl::desc("Warn for stack size bigger than the given"
56 " number"));
58 INITIALIZE_PASS_BEGIN(PEI, "prologepilog",
59 "Prologue/Epilogue Insertion", false, false)
60 INITIALIZE_PASS_DEPENDENCY(MachineLoopInfo)
61 INITIALIZE_PASS_DEPENDENCY(MachineDominatorTree)
62 INITIALIZE_PASS_DEPENDENCY(StackProtector)
63 INITIALIZE_PASS_DEPENDENCY(TargetPassConfig)
64 INITIALIZE_PASS_END(PEI, "prologepilog",
65 "Prologue/Epilogue Insertion & Frame Finalization",
66 false, false)
68 STATISTIC(NumScavengedRegs, "Number of frame index regs scavenged");
69 STATISTIC(NumBytesStackSpace,
70 "Number of bytes used for stack in all functions");
72 void PEI::getAnalysisUsage(AnalysisUsage &AU) const {
73 AU.setPreservesCFG();
74 AU.addPreserved<MachineLoopInfo>();
75 AU.addPreserved<MachineDominatorTree>();
76 AU.addRequired<StackProtector>();
77 AU.addRequired<TargetPassConfig>();
78 MachineFunctionPass::getAnalysisUsage(AU);
79 }
81 bool PEI::isReturnBlock(MachineBasicBlock* MBB) {
82 return (MBB && !MBB->empty() && MBB->back().isReturn());
83 }
85 /// Compute the set of return blocks
86 void PEI::calculateSets(MachineFunction &Fn) {
87 // Sets used to compute spill, restore placement sets.
88 const std::vector<CalleeSavedInfo> &CSI =
89 Fn.getFrameInfo()->getCalleeSavedInfo();
91 // If no CSRs used, we are done.
92 if (CSI.empty())
93 return;
95 // Save refs to entry and return blocks.
96 EntryBlock = Fn.begin();
97 for (MachineFunction::iterator MBB = Fn.begin(), E = Fn.end();
98 MBB != E; ++MBB)
99 if (isReturnBlock(MBB))
100 ReturnBlocks.push_back(MBB);
102 return;
103 }
105 /// StackObjSet - A set of stack object indexes
106 typedef SmallSetVector<int, 8> StackObjSet;
108 /// runOnMachineFunction - Insert prolog/epilog code and replace abstract
109 /// frame indexes with appropriate references.
110 ///
111 bool PEI::runOnMachineFunction(MachineFunction &Fn) {
112 const Function* F = Fn.getFunction();
113 const TargetRegisterInfo *TRI = Fn.getTarget().getRegisterInfo();
114 const TargetFrameLowering *TFI = Fn.getTarget().getFrameLowering();
116 assert(!Fn.getRegInfo().getNumVirtRegs() && "Regalloc must assign all vregs");
118 RS = TRI->requiresRegisterScavenging(Fn) ? new RegScavenger() : nullptr;
119 FrameIndexVirtualScavenging = TRI->requiresFrameIndexScavenging(Fn);
121 // Calculate the MaxCallFrameSize and AdjustsStack variables for the
122 // function's frame information. Also eliminates call frame pseudo
123 // instructions.
124 calculateCallsInformation(Fn);
126 // Allow the target machine to make some adjustments to the function
127 // e.g. UsedPhysRegs before calculateCalleeSavedRegisters.
128 TFI->processFunctionBeforeCalleeSavedScan(Fn, RS);
130 // Scan the function for modified callee saved registers and insert spill code
131 // for any callee saved registers that are modified.
132 calculateCalleeSavedRegisters(Fn);
134 // Determine placement of CSR spill/restore code:
135 // place all spills in the entry block, all restores in return blocks.
136 calculateSets(Fn);
138 // Add the code to save and restore the callee saved registers
139 if (!F->hasFnAttribute(Attribute::Naked))
140 insertCSRSpillsAndRestores(Fn);
142 // Allow the target machine to make final modifications to the function
143 // before the frame layout is finalized.
144 TFI->processFunctionBeforeFrameFinalized(Fn, RS);
146 // Calculate actual frame offsets for all abstract stack objects...
147 calculateFrameObjectOffsets(Fn);
149 // Add prolog and epilog code to the function. This function is required
150 // to align the stack frame as necessary for any stack variables or
151 // called functions. Because of this, calculateCalleeSavedRegisters()
152 // must be called before this function in order to set the AdjustsStack
153 // and MaxCallFrameSize variables.
154 if (!F->hasFnAttribute(Attribute::Naked))
155 insertPrologEpilogCode(Fn);
157 // Replace all MO_FrameIndex operands with physical register references
158 // and actual offsets.
159 //
160 replaceFrameIndices(Fn);
162 // If register scavenging is needed, as we've enabled doing it as a
163 // post-pass, scavenge the virtual registers that frame index elimiation
164 // inserted.
165 if (TRI->requiresRegisterScavenging(Fn) && FrameIndexVirtualScavenging)
166 scavengeFrameVirtualRegs(Fn);
168 // Clear any vregs created by virtual scavenging.
169 Fn.getRegInfo().clearVirtRegs();
171 // Warn on stack size when we exceeds the given limit.
172 MachineFrameInfo *MFI = Fn.getFrameInfo();
173 uint64_t StackSize = MFI->getStackSize();
174 if (WarnStackSize.getNumOccurrences() > 0 && WarnStackSize < StackSize) {
175 DiagnosticInfoStackSize DiagStackSize(*F, StackSize);
176 F->getContext().diagnose(DiagStackSize);
177 }
179 delete RS;
180 ReturnBlocks.clear();
181 return true;
182 }
184 /// calculateCallsInformation - Calculate the MaxCallFrameSize and AdjustsStack
185 /// variables for the function's frame information and eliminate call frame
186 /// pseudo instructions.
187 void PEI::calculateCallsInformation(MachineFunction &Fn) {
188 const TargetInstrInfo &TII = *Fn.getTarget().getInstrInfo();
189 const TargetFrameLowering *TFI = Fn.getTarget().getFrameLowering();
190 MachineFrameInfo *MFI = Fn.getFrameInfo();
192 unsigned MaxCallFrameSize = 0;
193 bool AdjustsStack = MFI->adjustsStack();
195 // Get the function call frame set-up and tear-down instruction opcode
196 int FrameSetupOpcode = TII.getCallFrameSetupOpcode();
197 int FrameDestroyOpcode = TII.getCallFrameDestroyOpcode();
199 // Early exit for targets which have no call frame setup/destroy pseudo
200 // instructions.
201 if (FrameSetupOpcode == -1 && FrameDestroyOpcode == -1)
202 return;
204 std::vector<MachineBasicBlock::iterator> FrameSDOps;
205 for (MachineFunction::iterator BB = Fn.begin(), E = Fn.end(); BB != E; ++BB)
206 for (MachineBasicBlock::iterator I = BB->begin(); I != BB->end(); ++I)
207 if (I->getOpcode() == FrameSetupOpcode ||
208 I->getOpcode() == FrameDestroyOpcode) {
209 assert(I->getNumOperands() >= 1 && "Call Frame Setup/Destroy Pseudo"
210 " instructions should have a single immediate argument!");
211 unsigned Size = I->getOperand(0).getImm();
212 if (Size > MaxCallFrameSize) MaxCallFrameSize = Size;
213 AdjustsStack = true;
214 FrameSDOps.push_back(I);
215 } else if (I->isInlineAsm()) {
216 // Some inline asm's need a stack frame, as indicated by operand 1.
217 unsigned ExtraInfo = I->getOperand(InlineAsm::MIOp_ExtraInfo).getImm();
218 if (ExtraInfo & InlineAsm::Extra_IsAlignStack)
219 AdjustsStack = true;
220 }
222 MFI->setAdjustsStack(AdjustsStack);
223 MFI->setMaxCallFrameSize(MaxCallFrameSize);
225 for (std::vector<MachineBasicBlock::iterator>::iterator
226 i = FrameSDOps.begin(), e = FrameSDOps.end(); i != e; ++i) {
227 MachineBasicBlock::iterator I = *i;
229 // If call frames are not being included as part of the stack frame, and
230 // the target doesn't indicate otherwise, remove the call frame pseudos
231 // here. The sub/add sp instruction pairs are still inserted, but we don't
232 // need to track the SP adjustment for frame index elimination.
233 if (TFI->canSimplifyCallFramePseudos(Fn))
234 TFI->eliminateCallFramePseudoInstr(Fn, *I->getParent(), I);
235 }
236 }
239 /// calculateCalleeSavedRegisters - Scan the function for modified callee saved
240 /// registers.
241 void PEI::calculateCalleeSavedRegisters(MachineFunction &F) {
242 const TargetRegisterInfo *RegInfo = F.getTarget().getRegisterInfo();
243 const TargetFrameLowering *TFI = F.getTarget().getFrameLowering();
244 MachineFrameInfo *MFI = F.getFrameInfo();
246 // Get the callee saved register list...
247 const MCPhysReg *CSRegs = RegInfo->getCalleeSavedRegs(&F);
249 // These are used to keep track the callee-save area. Initialize them.
250 MinCSFrameIndex = INT_MAX;
251 MaxCSFrameIndex = 0;
253 // Early exit for targets which have no callee saved registers.
254 if (!CSRegs || CSRegs[0] == 0)
255 return;
257 // In Naked functions we aren't going to save any registers.
258 if (F.getFunction()->hasFnAttribute(Attribute::Naked))
259 return;
261 std::vector<CalleeSavedInfo> CSI;
262 for (unsigned i = 0; CSRegs[i]; ++i) {
263 unsigned Reg = CSRegs[i];
264 // Functions which call __builtin_unwind_init get all their registers saved.
265 if (F.getRegInfo().isPhysRegUsed(Reg) || F.getMMI().callsUnwindInit()) {
266 // If the reg is modified, save it!
267 CSI.push_back(CalleeSavedInfo(Reg));
268 }
269 }
271 if (CSI.empty())
272 return; // Early exit if no callee saved registers are modified!
274 unsigned NumFixedSpillSlots;
275 const TargetFrameLowering::SpillSlot *FixedSpillSlots =
276 TFI->getCalleeSavedSpillSlots(NumFixedSpillSlots);
278 // Now that we know which registers need to be saved and restored, allocate
279 // stack slots for them.
280 for (std::vector<CalleeSavedInfo>::iterator
281 I = CSI.begin(), E = CSI.end(); I != E; ++I) {
282 unsigned Reg = I->getReg();
283 const TargetRegisterClass *RC = RegInfo->getMinimalPhysRegClass(Reg);
285 int FrameIdx;
286 if (RegInfo->hasReservedSpillSlot(F, Reg, FrameIdx)) {
287 I->setFrameIdx(FrameIdx);
288 continue;
289 }
291 // Check to see if this physreg must be spilled to a particular stack slot
292 // on this target.
293 const TargetFrameLowering::SpillSlot *FixedSlot = FixedSpillSlots;
294 while (FixedSlot != FixedSpillSlots+NumFixedSpillSlots &&
295 FixedSlot->Reg != Reg)
296 ++FixedSlot;
298 if (FixedSlot == FixedSpillSlots + NumFixedSpillSlots) {
299 // Nope, just spill it anywhere convenient.
300 unsigned Align = RC->getAlignment();
301 unsigned StackAlign = TFI->getStackAlignment();
303 // We may not be able to satisfy the desired alignment specification of
304 // the TargetRegisterClass if the stack alignment is smaller. Use the
305 // min.
306 Align = std::min(Align, StackAlign);
307 FrameIdx = MFI->CreateStackObject(RC->getSize(), Align, true);
308 if ((unsigned)FrameIdx < MinCSFrameIndex) MinCSFrameIndex = FrameIdx;
309 if ((unsigned)FrameIdx > MaxCSFrameIndex) MaxCSFrameIndex = FrameIdx;
310 } else {
311 // Spill it to the stack where we must.
312 FrameIdx = MFI->CreateFixedObject(RC->getSize(), FixedSlot->Offset, true);
313 }
315 I->setFrameIdx(FrameIdx);
316 }
318 MFI->setCalleeSavedInfo(CSI);
319 }
321 /// insertCSRSpillsAndRestores - Insert spill and restore code for
322 /// callee saved registers used in the function.
323 ///
324 void PEI::insertCSRSpillsAndRestores(MachineFunction &Fn) {
325 // Get callee saved register information.
326 MachineFrameInfo *MFI = Fn.getFrameInfo();
327 const std::vector<CalleeSavedInfo> &CSI = MFI->getCalleeSavedInfo();
329 MFI->setCalleeSavedInfoValid(true);
331 // Early exit if no callee saved registers are modified!
332 if (CSI.empty())
333 return;
335 const TargetInstrInfo &TII = *Fn.getTarget().getInstrInfo();
336 const TargetFrameLowering *TFI = Fn.getTarget().getFrameLowering();
337 const TargetRegisterInfo *TRI = Fn.getTarget().getRegisterInfo();
338 MachineBasicBlock::iterator I;
340 // Spill using target interface.
341 I = EntryBlock->begin();
342 if (!TFI->spillCalleeSavedRegisters(*EntryBlock, I, CSI, TRI)) {
343 for (unsigned i = 0, e = CSI.size(); i != e; ++i) {
344 // Add the callee-saved register as live-in.
345 // It's killed at the spill.
346 EntryBlock->addLiveIn(CSI[i].getReg());
348 // Insert the spill to the stack frame.
349 unsigned Reg = CSI[i].getReg();
350 const TargetRegisterClass *RC = TRI->getMinimalPhysRegClass(Reg);
351 TII.storeRegToStackSlot(*EntryBlock, I, Reg, true, CSI[i].getFrameIdx(),
352 RC, TRI);
353 }
354 }
356 // Restore using target interface.
357 for (unsigned ri = 0, re = ReturnBlocks.size(); ri != re; ++ri) {
358 MachineBasicBlock *MBB = ReturnBlocks[ri];
359 I = MBB->end();
360 --I;
362 // Skip over all terminator instructions, which are part of the return
363 // sequence.
364 MachineBasicBlock::iterator I2 = I;
365 while (I2 != MBB->begin() && (--I2)->isTerminator())
366 I = I2;
368 bool AtStart = I == MBB->begin();
369 MachineBasicBlock::iterator BeforeI = I;
370 if (!AtStart)
371 --BeforeI;
373 // Restore all registers immediately before the return and any
374 // terminators that precede it.
375 if (!TFI->restoreCalleeSavedRegisters(*MBB, I, CSI, TRI)) {
376 for (unsigned i = 0, e = CSI.size(); i != e; ++i) {
377 unsigned Reg = CSI[i].getReg();
378 const TargetRegisterClass *RC = TRI->getMinimalPhysRegClass(Reg);
379 TII.loadRegFromStackSlot(*MBB, I, Reg, CSI[i].getFrameIdx(), RC, TRI);
380 assert(I != MBB->begin() &&
381 "loadRegFromStackSlot didn't insert any code!");
382 // Insert in reverse order. loadRegFromStackSlot can insert
383 // multiple instructions.
384 if (AtStart)
385 I = MBB->begin();
386 else {
387 I = BeforeI;
388 ++I;
389 }
390 }
391 }
392 }
393 }
395 /// AdjustStackOffset - Helper function used to adjust the stack frame offset.
396 static inline void
397 AdjustStackOffset(MachineFrameInfo *MFI, int FrameIdx,
398 bool StackGrowsDown, int64_t &Offset,
399 unsigned &MaxAlign) {
400 // If the stack grows down, add the object size to find the lowest address.
401 if (StackGrowsDown)
402 Offset += MFI->getObjectSize(FrameIdx);
404 unsigned Align = MFI->getObjectAlignment(FrameIdx);
406 // If the alignment of this object is greater than that of the stack, then
407 // increase the stack alignment to match.
408 MaxAlign = std::max(MaxAlign, Align);
410 // Adjust to alignment boundary.
411 Offset = (Offset + Align - 1) / Align * Align;
413 if (StackGrowsDown) {
414 DEBUG(dbgs() << "alloc FI(" << FrameIdx << ") at SP[" << -Offset << "]\n");
415 MFI->setObjectOffset(FrameIdx, -Offset); // Set the computed offset
416 } else {
417 DEBUG(dbgs() << "alloc FI(" << FrameIdx << ") at SP[" << Offset << "]\n");
418 MFI->setObjectOffset(FrameIdx, Offset);
419 Offset += MFI->getObjectSize(FrameIdx);
420 }
421 }
423 /// AssignProtectedObjSet - Helper function to assign large stack objects (i.e.,
424 /// those required to be close to the Stack Protector) to stack offsets.
425 static void
426 AssignProtectedObjSet(const StackObjSet &UnassignedObjs,
427 SmallSet<int, 16> &ProtectedObjs,
428 MachineFrameInfo *MFI, bool StackGrowsDown,
429 int64_t &Offset, unsigned &MaxAlign) {
431 for (StackObjSet::const_iterator I = UnassignedObjs.begin(),
432 E = UnassignedObjs.end(); I != E; ++I) {
433 int i = *I;
434 AdjustStackOffset(MFI, i, StackGrowsDown, Offset, MaxAlign);
435 ProtectedObjs.insert(i);
436 }
437 }
439 /// calculateFrameObjectOffsets - Calculate actual frame offsets for all of the
440 /// abstract stack objects.
441 ///
442 void PEI::calculateFrameObjectOffsets(MachineFunction &Fn) {
443 const TargetFrameLowering &TFI = *Fn.getTarget().getFrameLowering();
444 StackProtector *SP = &getAnalysis<StackProtector>();
446 bool StackGrowsDown =
447 TFI.getStackGrowthDirection() == TargetFrameLowering::StackGrowsDown;
449 // Loop over all of the stack objects, assigning sequential addresses...
450 MachineFrameInfo *MFI = Fn.getFrameInfo();
452 // Start at the beginning of the local area.
453 // The Offset is the distance from the stack top in the direction
454 // of stack growth -- so it's always nonnegative.
455 int LocalAreaOffset = TFI.getOffsetOfLocalArea();
456 if (StackGrowsDown)
457 LocalAreaOffset = -LocalAreaOffset;
458 assert(LocalAreaOffset >= 0
459 && "Local area offset should be in direction of stack growth");
460 int64_t Offset = LocalAreaOffset;
462 // If there are fixed sized objects that are preallocated in the local area,
463 // non-fixed objects can't be allocated right at the start of local area.
464 // We currently don't support filling in holes in between fixed sized
465 // objects, so we adjust 'Offset' to point to the end of last fixed sized
466 // preallocated object.
467 for (int i = MFI->getObjectIndexBegin(); i != 0; ++i) {
468 int64_t FixedOff;
469 if (StackGrowsDown) {
470 // The maximum distance from the stack pointer is at lower address of
471 // the object -- which is given by offset. For down growing stack
472 // the offset is negative, so we negate the offset to get the distance.
473 FixedOff = -MFI->getObjectOffset(i);
474 } else {
475 // The maximum distance from the start pointer is at the upper
476 // address of the object.
477 FixedOff = MFI->getObjectOffset(i) + MFI->getObjectSize(i);
478 }
479 if (FixedOff > Offset) Offset = FixedOff;
480 }
482 // First assign frame offsets to stack objects that are used to spill
483 // callee saved registers.
484 if (StackGrowsDown) {
485 for (unsigned i = MinCSFrameIndex; i <= MaxCSFrameIndex; ++i) {
486 // If the stack grows down, we need to add the size to find the lowest
487 // address of the object.
488 Offset += MFI->getObjectSize(i);
490 unsigned Align = MFI->getObjectAlignment(i);
491 // Adjust to alignment boundary
492 Offset = (Offset+Align-1)/Align*Align;
494 MFI->setObjectOffset(i, -Offset); // Set the computed offset
495 }
496 } else {
497 int MaxCSFI = MaxCSFrameIndex, MinCSFI = MinCSFrameIndex;
498 for (int i = MaxCSFI; i >= MinCSFI ; --i) {
499 unsigned Align = MFI->getObjectAlignment(i);
500 // Adjust to alignment boundary
501 Offset = (Offset+Align-1)/Align*Align;
503 MFI->setObjectOffset(i, Offset);
504 Offset += MFI->getObjectSize(i);
505 }
506 }
508 unsigned MaxAlign = MFI->getMaxAlignment();
510 // Make sure the special register scavenging spill slot is closest to the
511 // incoming stack pointer if a frame pointer is required and is closer
512 // to the incoming rather than the final stack pointer.
513 const TargetRegisterInfo *RegInfo = Fn.getTarget().getRegisterInfo();
514 bool EarlyScavengingSlots = (TFI.hasFP(Fn) &&
515 TFI.isFPCloseToIncomingSP() &&
516 RegInfo->useFPForScavengingIndex(Fn) &&
517 !RegInfo->needsStackRealignment(Fn));
518 if (RS && EarlyScavengingSlots) {
519 SmallVector<int, 2> SFIs;
520 RS->getScavengingFrameIndices(SFIs);
521 for (SmallVectorImpl<int>::iterator I = SFIs.begin(),
522 IE = SFIs.end(); I != IE; ++I)
523 AdjustStackOffset(MFI, *I, StackGrowsDown, Offset, MaxAlign);
524 }
526 // FIXME: Once this is working, then enable flag will change to a target
527 // check for whether the frame is large enough to want to use virtual
528 // frame index registers. Functions which don't want/need this optimization
529 // will continue to use the existing code path.
530 if (MFI->getUseLocalStackAllocationBlock()) {
531 unsigned Align = MFI->getLocalFrameMaxAlign();
533 // Adjust to alignment boundary.
534 Offset = (Offset + Align - 1) / Align * Align;
536 DEBUG(dbgs() << "Local frame base offset: " << Offset << "\n");
538 // Resolve offsets for objects in the local block.
539 for (unsigned i = 0, e = MFI->getLocalFrameObjectCount(); i != e; ++i) {
540 std::pair<int, int64_t> Entry = MFI->getLocalFrameObjectMap(i);
541 int64_t FIOffset = (StackGrowsDown ? -Offset : Offset) + Entry.second;
542 DEBUG(dbgs() << "alloc FI(" << Entry.first << ") at SP[" <<
543 FIOffset << "]\n");
544 MFI->setObjectOffset(Entry.first, FIOffset);
545 }
546 // Allocate the local block
547 Offset += MFI->getLocalFrameSize();
549 MaxAlign = std::max(Align, MaxAlign);
550 }
552 // Make sure that the stack protector comes before the local variables on the
553 // stack.
554 SmallSet<int, 16> ProtectedObjs;
555 if (MFI->getStackProtectorIndex() >= 0) {
556 StackObjSet LargeArrayObjs;
557 StackObjSet SmallArrayObjs;
558 StackObjSet AddrOfObjs;
560 AdjustStackOffset(MFI, MFI->getStackProtectorIndex(), StackGrowsDown,
561 Offset, MaxAlign);
563 // Assign large stack objects first.
564 for (unsigned i = 0, e = MFI->getObjectIndexEnd(); i != e; ++i) {
565 if (MFI->isObjectPreAllocated(i) &&
566 MFI->getUseLocalStackAllocationBlock())
567 continue;
568 if (i >= MinCSFrameIndex && i <= MaxCSFrameIndex)
569 continue;
570 if (RS && RS->isScavengingFrameIndex((int)i))
571 continue;
572 if (MFI->isDeadObjectIndex(i))
573 continue;
574 if (MFI->getStackProtectorIndex() == (int)i)
575 continue;
577 switch (SP->getSSPLayout(MFI->getObjectAllocation(i))) {
578 case StackProtector::SSPLK_None:
579 continue;
580 case StackProtector::SSPLK_SmallArray:
581 SmallArrayObjs.insert(i);
582 continue;
583 case StackProtector::SSPLK_AddrOf:
584 AddrOfObjs.insert(i);
585 continue;
586 case StackProtector::SSPLK_LargeArray:
587 LargeArrayObjs.insert(i);
588 continue;
589 }
590 llvm_unreachable("Unexpected SSPLayoutKind.");
591 }
593 AssignProtectedObjSet(LargeArrayObjs, ProtectedObjs, MFI, StackGrowsDown,
594 Offset, MaxAlign);
595 AssignProtectedObjSet(SmallArrayObjs, ProtectedObjs, MFI, StackGrowsDown,
596 Offset, MaxAlign);
597 AssignProtectedObjSet(AddrOfObjs, ProtectedObjs, MFI, StackGrowsDown,
598 Offset, MaxAlign);
599 }
601 // Then assign frame offsets to stack objects that are not used to spill
602 // callee saved registers.
603 for (unsigned i = 0, e = MFI->getObjectIndexEnd(); i != e; ++i) {
604 if (MFI->isObjectPreAllocated(i) &&
605 MFI->getUseLocalStackAllocationBlock())
606 continue;
607 if (i >= MinCSFrameIndex && i <= MaxCSFrameIndex)
608 continue;
609 if (RS && RS->isScavengingFrameIndex((int)i))
610 continue;
611 if (MFI->isDeadObjectIndex(i))
612 continue;
613 if (MFI->getStackProtectorIndex() == (int)i)
614 continue;
615 if (ProtectedObjs.count(i))
616 continue;
618 AdjustStackOffset(MFI, i, StackGrowsDown, Offset, MaxAlign);
619 }
621 // Make sure the special register scavenging spill slot is closest to the
622 // stack pointer.
623 if (RS && !EarlyScavengingSlots) {
624 SmallVector<int, 2> SFIs;
625 RS->getScavengingFrameIndices(SFIs);
626 for (SmallVectorImpl<int>::iterator I = SFIs.begin(),
627 IE = SFIs.end(); I != IE; ++I)
628 AdjustStackOffset(MFI, *I, StackGrowsDown, Offset, MaxAlign);
629 }
631 if (!TFI.targetHandlesStackFrameRounding()) {
632 // If we have reserved argument space for call sites in the function
633 // immediately on entry to the current function, count it as part of the
634 // overall stack size.
635 if (MFI->adjustsStack() && TFI.hasReservedCallFrame(Fn))
636 Offset += MFI->getMaxCallFrameSize();
638 // Round up the size to a multiple of the alignment. If the function has
639 // any calls or alloca's, align to the target's StackAlignment value to
640 // ensure that the callee's frame or the alloca data is suitably aligned;
641 // otherwise, for leaf functions, align to the TransientStackAlignment
642 // value.
643 unsigned StackAlign;
644 if (MFI->adjustsStack() || MFI->hasVarSizedObjects() ||
645 (RegInfo->needsStackRealignment(Fn) && MFI->getObjectIndexEnd() != 0))
646 StackAlign = TFI.getStackAlignment();
647 else
648 StackAlign = TFI.getTransientStackAlignment();
650 // If the frame pointer is eliminated, all frame offsets will be relative to
651 // SP not FP. Align to MaxAlign so this works.
652 StackAlign = std::max(StackAlign, MaxAlign);
653 unsigned AlignMask = StackAlign - 1;
654 Offset = (Offset + AlignMask) & ~uint64_t(AlignMask);
655 }
657 // Update frame info to pretend that this is part of the stack...
658 int64_t StackSize = Offset - LocalAreaOffset;
659 MFI->setStackSize(StackSize);
660 NumBytesStackSpace += StackSize;
661 }
663 /// insertPrologEpilogCode - Scan the function for modified callee saved
664 /// registers, insert spill code for these callee saved registers, then add
665 /// prolog and epilog code to the function.
666 ///
667 void PEI::insertPrologEpilogCode(MachineFunction &Fn) {
668 const TargetFrameLowering &TFI = *Fn.getTarget().getFrameLowering();
670 // Add prologue to the function...
671 TFI.emitPrologue(Fn);
673 // Add epilogue to restore the callee-save registers in each exiting block
674 for (MachineFunction::iterator I = Fn.begin(), E = Fn.end(); I != E; ++I) {
675 // If last instruction is a return instruction, add an epilogue
676 if (!I->empty() && I->back().isReturn())
677 TFI.emitEpilogue(Fn, *I);
678 }
680 // Emit additional code that is required to support segmented stacks, if
681 // we've been asked for it. This, when linked with a runtime with support
682 // for segmented stacks (libgcc is one), will result in allocating stack
683 // space in small chunks instead of one large contiguous block.
684 if (Fn.shouldSplitStack())
685 TFI.adjustForSegmentedStacks(Fn);
687 // Emit additional code that is required to explicitly handle the stack in
688 // HiPE native code (if needed) when loaded in the Erlang/OTP runtime. The
689 // approach is rather similar to that of Segmented Stacks, but it uses a
690 // different conditional check and another BIF for allocating more stack
691 // space.
692 if (Fn.getFunction()->getCallingConv() == CallingConv::HiPE)
693 TFI.adjustForHiPEPrologue(Fn);
694 }
696 /// replaceFrameIndices - Replace all MO_FrameIndex operands with physical
697 /// register references and actual offsets.
698 ///
699 void PEI::replaceFrameIndices(MachineFunction &Fn) {
700 if (!Fn.getFrameInfo()->hasStackObjects()) return; // Nothing to do?
702 // Store SPAdj at exit of a basic block.
703 SmallVector<int, 8> SPState;
704 SPState.resize(Fn.getNumBlockIDs());
705 SmallPtrSet<MachineBasicBlock*, 8> Reachable;
707 // Iterate over the reachable blocks in DFS order.
708 for (df_ext_iterator<MachineFunction*, SmallPtrSet<MachineBasicBlock*, 8> >
709 DFI = df_ext_begin(&Fn, Reachable), DFE = df_ext_end(&Fn, Reachable);
710 DFI != DFE; ++DFI) {
711 int SPAdj = 0;
712 // Check the exit state of the DFS stack predecessor.
713 if (DFI.getPathLength() >= 2) {
714 MachineBasicBlock *StackPred = DFI.getPath(DFI.getPathLength() - 2);
715 assert(Reachable.count(StackPred) &&
716 "DFS stack predecessor is already visited.\n");
717 SPAdj = SPState[StackPred->getNumber()];
718 }
719 MachineBasicBlock *BB = *DFI;
720 replaceFrameIndices(BB, Fn, SPAdj);
721 SPState[BB->getNumber()] = SPAdj;
722 }
724 // Handle the unreachable blocks.
725 for (MachineFunction::iterator BB = Fn.begin(), E = Fn.end(); BB != E; ++BB) {
726 if (Reachable.count(BB))
727 // Already handled in DFS traversal.
728 continue;
729 int SPAdj = 0;
730 replaceFrameIndices(BB, Fn, SPAdj);
731 }
732 }
734 void PEI::replaceFrameIndices(MachineBasicBlock *BB, MachineFunction &Fn,
735 int &SPAdj) {
736 const TargetMachine &TM = Fn.getTarget();
737 assert(TM.getRegisterInfo() && "TM::getRegisterInfo() must be implemented!");
738 const TargetInstrInfo &TII = *Fn.getTarget().getInstrInfo();
739 const TargetRegisterInfo &TRI = *TM.getRegisterInfo();
740 const TargetFrameLowering *TFI = TM.getFrameLowering();
741 bool StackGrowsDown =
742 TFI->getStackGrowthDirection() == TargetFrameLowering::StackGrowsDown;
743 int FrameSetupOpcode = TII.getCallFrameSetupOpcode();
744 int FrameDestroyOpcode = TII.getCallFrameDestroyOpcode();
746 if (RS && !FrameIndexVirtualScavenging) RS->enterBasicBlock(BB);
748 for (MachineBasicBlock::iterator I = BB->begin(); I != BB->end(); ) {
750 if (I->getOpcode() == FrameSetupOpcode ||
751 I->getOpcode() == FrameDestroyOpcode) {
752 // Remember how much SP has been adjusted to create the call
753 // frame.
754 int Size = I->getOperand(0).getImm();
756 if ((!StackGrowsDown && I->getOpcode() == FrameSetupOpcode) ||
757 (StackGrowsDown && I->getOpcode() == FrameDestroyOpcode))
758 Size = -Size;
760 SPAdj += Size;
762 MachineBasicBlock::iterator PrevI = BB->end();
763 if (I != BB->begin()) PrevI = std::prev(I);
764 TFI->eliminateCallFramePseudoInstr(Fn, *BB, I);
766 // Visit the instructions created by eliminateCallFramePseudoInstr().
767 if (PrevI == BB->end())
768 I = BB->begin(); // The replaced instr was the first in the block.
769 else
770 I = std::next(PrevI);
771 continue;
772 }
774 MachineInstr *MI = I;
775 bool DoIncr = true;
776 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
777 if (!MI->getOperand(i).isFI())
778 continue;
780 // Frame indicies in debug values are encoded in a target independent
781 // way with simply the frame index and offset rather than any
782 // target-specific addressing mode.
783 if (MI->isDebugValue()) {
784 assert(i == 0 && "Frame indicies can only appear as the first "
785 "operand of a DBG_VALUE machine instruction");
786 unsigned Reg;
787 MachineOperand &Offset = MI->getOperand(1);
788 Offset.setImm(Offset.getImm() +
789 TFI->getFrameIndexReference(
790 Fn, MI->getOperand(0).getIndex(), Reg));
791 MI->getOperand(0).ChangeToRegister(Reg, false /*isDef*/);
792 continue;
793 }
795 // Some instructions (e.g. inline asm instructions) can have
796 // multiple frame indices and/or cause eliminateFrameIndex
797 // to insert more than one instruction. We need the register
798 // scavenger to go through all of these instructions so that
799 // it can update its register information. We keep the
800 // iterator at the point before insertion so that we can
801 // revisit them in full.
802 bool AtBeginning = (I == BB->begin());
803 if (!AtBeginning) --I;
805 // If this instruction has a FrameIndex operand, we need to
806 // use that target machine register info object to eliminate
807 // it.
808 TRI.eliminateFrameIndex(MI, SPAdj, i,
809 FrameIndexVirtualScavenging ? nullptr : RS);
811 // Reset the iterator if we were at the beginning of the BB.
812 if (AtBeginning) {
813 I = BB->begin();
814 DoIncr = false;
815 }
817 MI = nullptr;
818 break;
819 }
821 if (DoIncr && I != BB->end()) ++I;
823 // Update register states.
824 if (RS && !FrameIndexVirtualScavenging && MI) RS->forward(MI);
825 }
826 }
828 /// scavengeFrameVirtualRegs - Replace all frame index virtual registers
829 /// with physical registers. Use the register scavenger to find an
830 /// appropriate register to use.
831 ///
832 /// FIXME: Iterating over the instruction stream is unnecessary. We can simply
833 /// iterate over the vreg use list, which at this point only contains machine
834 /// operands for which eliminateFrameIndex need a new scratch reg.
835 void PEI::scavengeFrameVirtualRegs(MachineFunction &Fn) {
836 // Run through the instructions and find any virtual registers.
837 for (MachineFunction::iterator BB = Fn.begin(),
838 E = Fn.end(); BB != E; ++BB) {
839 RS->enterBasicBlock(BB);
841 int SPAdj = 0;
843 // The instruction stream may change in the loop, so check BB->end()
844 // directly.
845 for (MachineBasicBlock::iterator I = BB->begin(); I != BB->end(); ) {
846 // We might end up here again with a NULL iterator if we scavenged a
847 // register for which we inserted spill code for definition by what was
848 // originally the first instruction in BB.
849 if (I == MachineBasicBlock::iterator(nullptr))
850 I = BB->begin();
852 MachineInstr *MI = I;
853 MachineBasicBlock::iterator J = std::next(I);
854 MachineBasicBlock::iterator P =
855 I == BB->begin() ? MachineBasicBlock::iterator(nullptr)
856 : std::prev(I);
858 // RS should process this instruction before we might scavenge at this
859 // location. This is because we might be replacing a virtual register
860 // defined by this instruction, and if so, registers killed by this
861 // instruction are available, and defined registers are not.
862 RS->forward(I);
864 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
865 if (MI->getOperand(i).isReg()) {
866 MachineOperand &MO = MI->getOperand(i);
867 unsigned Reg = MO.getReg();
868 if (Reg == 0)
869 continue;
870 if (!TargetRegisterInfo::isVirtualRegister(Reg))
871 continue;
873 // When we first encounter a new virtual register, it
874 // must be a definition.
875 assert(MI->getOperand(i).isDef() &&
876 "frame index virtual missing def!");
877 // Scavenge a new scratch register
878 const TargetRegisterClass *RC = Fn.getRegInfo().getRegClass(Reg);
879 unsigned ScratchReg = RS->scavengeRegister(RC, J, SPAdj);
881 ++NumScavengedRegs;
883 // Replace this reference to the virtual register with the
884 // scratch register.
885 assert (ScratchReg && "Missing scratch register!");
886 Fn.getRegInfo().replaceRegWith(Reg, ScratchReg);
888 // Because this instruction was processed by the RS before this
889 // register was allocated, make sure that the RS now records the
890 // register as being used.
891 RS->setUsed(ScratchReg);
892 }
893 }
895 // If the scavenger needed to use one of its spill slots, the
896 // spill code will have been inserted in between I and J. This is a
897 // problem because we need the spill code before I: Move I to just
898 // prior to J.
899 if (I != std::prev(J)) {
900 BB->splice(J, BB, I);
902 // Before we move I, we need to prepare the RS to visit I again.
903 // Specifically, RS will assert if it sees uses of registers that
904 // it believes are undefined. Because we have already processed
905 // register kills in I, when it visits I again, it will believe that
906 // those registers are undefined. To avoid this situation, unprocess
907 // the instruction I.
908 assert(RS->getCurrentPosition() == I &&
909 "The register scavenger has an unexpected position");
910 I = P;
911 RS->unprocess(P);
912 } else
913 ++I;
914 }
915 }
916 }