1 //===-- RegAllocBase.h - basic regalloc interface and driver --*- C++ -*---===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the RegAllocBase class, which is the skeleton of a basic
11 // register allocation algorithm and interface for extending it. It provides the
12 // building blocks on which to construct other experimental allocators and test
13 // the validity of two principles:
14 //
15 // - If virtual and physical register liveness is modeled using intervals, then
16 // on-the-fly interference checking is cheap. Furthermore, interferences can be
17 // lazily cached and reused.
18 //
19 // - Register allocation complexity, and generated code performance is
20 // determined by the effectiveness of live range splitting rather than optimal
21 // coloring.
22 //
23 // Following the first principle, interfering checking revolves around the
24 // LiveIntervalUnion data structure.
25 //
26 // To fulfill the second principle, the basic allocator provides a driver for
27 // incremental splitting. It essentially punts on the problem of register
28 // coloring, instead driving the assignment of virtual to physical registers by
29 // the cost of splitting. The basic allocator allows for heuristic reassignment
30 // of registers, if a more sophisticated allocator chooses to do that.
31 //
32 // This framework provides a way to engineer the compile time vs. code
33 // quality trade-off without relying on a particular theoretical solver.
34 //
35 //===----------------------------------------------------------------------===//
37 #ifndef LLVM_CODEGEN_REGALLOCBASE
38 #define LLVM_CODEGEN_REGALLOCBASE
40 #include "llvm/CodeGen/LiveInterval.h"
41 #include "llvm/CodeGen/RegisterClassInfo.h"
43 namespace llvm {
45 template<typename T> class SmallVectorImpl;
46 class TargetRegisterInfo;
47 class VirtRegMap;
48 class LiveIntervals;
49 class LiveRegMatrix;
50 class Spiller;
52 /// RegAllocBase provides the register allocation driver and interface that can
53 /// be extended to add interesting heuristics.
54 ///
55 /// Register allocators must override the selectOrSplit() method to implement
56 /// live range splitting. They must also override enqueue/dequeue to provide an
57 /// assignment order.
58 class RegAllocBase {
59 virtual void anchor();
60 protected:
61 const TargetRegisterInfo *TRI;
62 MachineRegisterInfo *MRI;
63 VirtRegMap *VRM;
64 LiveIntervals *LIS;
65 LiveRegMatrix *Matrix;
66 RegisterClassInfo RegClassInfo;
68 RegAllocBase()
69 : TRI(nullptr), MRI(nullptr), VRM(nullptr), LIS(nullptr), Matrix(nullptr) {}
71 virtual ~RegAllocBase() {}
73 // A RegAlloc pass should call this before allocatePhysRegs.
74 void init(VirtRegMap &vrm, LiveIntervals &lis, LiveRegMatrix &mat);
76 // The top-level driver. The output is a VirtRegMap that us updated with
77 // physical register assignments.
78 void allocatePhysRegs();
80 // Get a temporary reference to a Spiller instance.
81 virtual Spiller &spiller() = 0;
83 /// enqueue - Add VirtReg to the priority queue of unassigned registers.
84 virtual void enqueue(LiveInterval *LI) = 0;
86 /// dequeue - Return the next unassigned register, or NULL.
87 virtual LiveInterval *dequeue() = 0;
89 // A RegAlloc pass should override this to provide the allocation heuristics.
90 // Each call must guarantee forward progess by returning an available PhysReg
91 // or new set of split live virtual registers. It is up to the splitter to
92 // converge quickly toward fully spilled live ranges.
93 virtual unsigned selectOrSplit(LiveInterval &VirtReg,
94 SmallVectorImpl<unsigned> &splitLVRs) = 0;
96 // Use this group name for NamedRegionTimer.
97 static const char TimerGroupName[];
99 public:
100 /// VerifyEnabled - True when -verify-regalloc is given.
101 static bool VerifyEnabled;
103 private:
104 void seedLiveRegs();
105 };
107 } // end namespace llvm
109 #endif // !defined(LLVM_CODEGEN_REGALLOCBASE)