1 //===---- ScheduleDAGInstrs.cpp - MachineInstr Rescheduling ---------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This implements the ScheduleDAGInstrs class, which implements re-scheduling
11 // of MachineInstrs.
12 //
13 //===----------------------------------------------------------------------===//
15 #include "llvm/CodeGen/ScheduleDAGInstrs.h"
16 #include "llvm/ADT/MapVector.h"
17 #include "llvm/ADT/SmallPtrSet.h"
18 #include "llvm/ADT/SmallSet.h"
19 #include "llvm/Analysis/AliasAnalysis.h"
20 #include "llvm/Analysis/ValueTracking.h"
21 #include "llvm/CodeGen/LiveIntervalAnalysis.h"
22 #include "llvm/CodeGen/MachineFunctionPass.h"
23 #include "llvm/CodeGen/MachineInstrBuilder.h"
24 #include "llvm/CodeGen/MachineMemOperand.h"
25 #include "llvm/CodeGen/MachineRegisterInfo.h"
26 #include "llvm/CodeGen/PseudoSourceValue.h"
27 #include "llvm/CodeGen/RegisterPressure.h"
28 #include "llvm/CodeGen/ScheduleDFS.h"
29 #include "llvm/IR/Operator.h"
30 #include "llvm/MC/MCInstrItineraries.h"
31 #include "llvm/Support/CommandLine.h"
32 #include "llvm/Support/Debug.h"
33 #include "llvm/Support/Format.h"
34 #include "llvm/Support/raw_ostream.h"
35 #include "llvm/Target/TargetInstrInfo.h"
36 #include "llvm/Target/TargetMachine.h"
37 #include "llvm/Target/TargetRegisterInfo.h"
38 #include "llvm/Target/TargetSubtargetInfo.h"
39 #include <queue>
41 using namespace llvm;
43 #define DEBUG_TYPE "misched"
45 static cl::opt<bool> EnableAASchedMI("enable-aa-sched-mi", cl::Hidden,
46 cl::ZeroOrMore, cl::init(false),
47 cl::desc("Enable use of AA during MI DAG construction"));
49 static cl::opt<bool> UseTBAA("use-tbaa-in-sched-mi", cl::Hidden,
50 cl::init(true), cl::desc("Enable use of TBAA during MI DAG construction"));
52 ScheduleDAGInstrs::ScheduleDAGInstrs(MachineFunction &mf,
53 const MachineLoopInfo *mli,
54 bool IsPostRAFlag,
55 bool RemoveKillFlags,
56 LiveIntervals *lis)
57 : ScheduleDAG(mf), MLI(mli), MFI(mf.getFrameInfo()), LIS(lis),
58 IsPostRA(IsPostRAFlag), RemoveKillFlags(RemoveKillFlags),
59 CanHandleTerminators(false), FirstDbgValue(nullptr) {
60 assert((IsPostRA || LIS) && "PreRA scheduling requires LiveIntervals");
61 DbgValues.clear();
62 assert(!(IsPostRA && MRI.getNumVirtRegs()) &&
63 "Virtual registers must be removed prior to PostRA scheduling");
65 const TargetSubtargetInfo &ST = TM.getSubtarget<TargetSubtargetInfo>();
66 SchedModel.init(ST.getSchedModel(), &ST, TII);
67 }
69 /// getUnderlyingObjectFromInt - This is the function that does the work of
70 /// looking through basic ptrtoint+arithmetic+inttoptr sequences.
71 static const Value *getUnderlyingObjectFromInt(const Value *V) {
72 do {
73 if (const Operator *U = dyn_cast<Operator>(V)) {
74 // If we find a ptrtoint, we can transfer control back to the
75 // regular getUnderlyingObjectFromInt.
76 if (U->getOpcode() == Instruction::PtrToInt)
77 return U->getOperand(0);
78 // If we find an add of a constant, a multiplied value, or a phi, it's
79 // likely that the other operand will lead us to the base
80 // object. We don't have to worry about the case where the
81 // object address is somehow being computed by the multiply,
82 // because our callers only care when the result is an
83 // identifiable object.
84 if (U->getOpcode() != Instruction::Add ||
85 (!isa<ConstantInt>(U->getOperand(1)) &&
86 Operator::getOpcode(U->getOperand(1)) != Instruction::Mul &&
87 !isa<PHINode>(U->getOperand(1))))
88 return V;
89 V = U->getOperand(0);
90 } else {
91 return V;
92 }
93 assert(V->getType()->isIntegerTy() && "Unexpected operand type!");
94 } while (1);
95 }
97 /// getUnderlyingObjects - This is a wrapper around GetUnderlyingObjects
98 /// and adds support for basic ptrtoint+arithmetic+inttoptr sequences.
99 static void getUnderlyingObjects(const Value *V,
100 SmallVectorImpl<Value *> &Objects) {
101 SmallPtrSet<const Value *, 16> Visited;
102 SmallVector<const Value *, 4> Working(1, V);
103 do {
104 V = Working.pop_back_val();
106 SmallVector<Value *, 4> Objs;
107 GetUnderlyingObjects(const_cast<Value *>(V), Objs);
109 for (SmallVectorImpl<Value *>::iterator I = Objs.begin(), IE = Objs.end();
110 I != IE; ++I) {
111 V = *I;
112 if (!Visited.insert(V).second)
113 continue;
114 if (Operator::getOpcode(V) == Instruction::IntToPtr) {
115 const Value *O =
116 getUnderlyingObjectFromInt(cast<User>(V)->getOperand(0));
117 if (O->getType()->isPointerTy()) {
118 Working.push_back(O);
119 continue;
120 }
121 }
122 Objects.push_back(const_cast<Value *>(V));
123 }
124 } while (!Working.empty());
125 }
127 typedef PointerUnion<const Value *, const PseudoSourceValue *> ValueType;
128 typedef SmallVector<PointerIntPair<ValueType, 1, bool>, 4>
129 UnderlyingObjectsVector;
131 /// getUnderlyingObjectsForInstr - If this machine instr has memory reference
132 /// information and it can be tracked to a normal reference to a known
133 /// object, return the Value for that object.
134 static void getUnderlyingObjectsForInstr(const MachineInstr *MI,
135 const MachineFrameInfo *MFI,
136 UnderlyingObjectsVector &Objects) {
137 if (!MI->hasOneMemOperand() ||
138 (!(*MI->memoperands_begin())->getValue() &&
139 !(*MI->memoperands_begin())->getPseudoValue()) ||
140 (*MI->memoperands_begin())->isVolatile())
141 return;
143 if (const PseudoSourceValue *PSV =
144 (*MI->memoperands_begin())->getPseudoValue()) {
145 // For now, ignore PseudoSourceValues which may alias LLVM IR values
146 // because the code that uses this function has no way to cope with
147 // such aliases.
148 if (!PSV->isAliased(MFI)) {
149 bool MayAlias = PSV->mayAlias(MFI);
150 Objects.push_back(UnderlyingObjectsVector::value_type(PSV, MayAlias));
151 }
152 return;
153 }
155 const Value *V = (*MI->memoperands_begin())->getValue();
156 if (!V)
157 return;
159 SmallVector<Value *, 4> Objs;
160 getUnderlyingObjects(V, Objs);
162 for (SmallVectorImpl<Value *>::iterator I = Objs.begin(), IE = Objs.end();
163 I != IE; ++I) {
164 V = *I;
166 if (!isIdentifiedObject(V)) {
167 Objects.clear();
168 return;
169 }
171 Objects.push_back(UnderlyingObjectsVector::value_type(V, true));
172 }
173 }
175 void ScheduleDAGInstrs::startBlock(MachineBasicBlock *bb) {
176 BB = bb;
177 }
179 void ScheduleDAGInstrs::finishBlock() {
180 // Subclasses should no longer refer to the old block.
181 BB = nullptr;
182 }
184 /// Initialize the DAG and common scheduler state for the current scheduling
185 /// region. This does not actually create the DAG, only clears it. The
186 /// scheduling driver may call BuildSchedGraph multiple times per scheduling
187 /// region.
188 void ScheduleDAGInstrs::enterRegion(MachineBasicBlock *bb,
189 MachineBasicBlock::iterator begin,
190 MachineBasicBlock::iterator end,
191 unsigned regioninstrs) {
192 assert(bb == BB && "startBlock should set BB");
193 RegionBegin = begin;
194 RegionEnd = end;
195 NumRegionInstrs = regioninstrs;
196 }
198 /// Close the current scheduling region. Don't clear any state in case the
199 /// driver wants to refer to the previous scheduling region.
200 void ScheduleDAGInstrs::exitRegion() {
201 // Nothing to do.
202 }
204 /// addSchedBarrierDeps - Add dependencies from instructions in the current
205 /// list of instructions being scheduled to scheduling barrier by adding
206 /// the exit SU to the register defs and use list. This is because we want to
207 /// make sure instructions which define registers that are either used by
208 /// the terminator or are live-out are properly scheduled. This is
209 /// especially important when the definition latency of the return value(s)
210 /// are too high to be hidden by the branch or when the liveout registers
211 /// used by instructions in the fallthrough block.
212 void ScheduleDAGInstrs::addSchedBarrierDeps() {
213 MachineInstr *ExitMI = RegionEnd != BB->end() ? &*RegionEnd : nullptr;
214 ExitSU.setInstr(ExitMI);
215 bool AllDepKnown = ExitMI &&
216 (ExitMI->isCall() || ExitMI->isBarrier());
217 if (ExitMI && AllDepKnown) {
218 // If it's a call or a barrier, add dependencies on the defs and uses of
219 // instruction.
220 for (unsigned i = 0, e = ExitMI->getNumOperands(); i != e; ++i) {
221 const MachineOperand &MO = ExitMI->getOperand(i);
222 if (!MO.isReg() || MO.isDef()) continue;
223 unsigned Reg = MO.getReg();
224 if (Reg == 0) continue;
226 if (TRI->isPhysicalRegister(Reg))
227 Uses.insert(PhysRegSUOper(&ExitSU, -1, Reg));
228 else {
229 assert(!IsPostRA && "Virtual register encountered after regalloc.");
230 if (MO.readsReg()) // ignore undef operands
231 addVRegUseDeps(&ExitSU, i);
232 }
233 }
234 } else {
235 // For others, e.g. fallthrough, conditional branch, assume the exit
236 // uses all the registers that are livein to the successor blocks.
237 assert(Uses.empty() && "Uses in set before adding deps?");
238 for (MachineBasicBlock::succ_iterator SI = BB->succ_begin(),
239 SE = BB->succ_end(); SI != SE; ++SI)
240 for (MachineBasicBlock::livein_iterator I = (*SI)->livein_begin(),
241 E = (*SI)->livein_end(); I != E; ++I) {
242 unsigned Reg = *I;
243 if (!Uses.contains(Reg))
244 Uses.insert(PhysRegSUOper(&ExitSU, -1, Reg));
245 }
246 }
247 }
249 /// MO is an operand of SU's instruction that defines a physical register. Add
250 /// data dependencies from SU to any uses of the physical register.
251 void ScheduleDAGInstrs::addPhysRegDataDeps(SUnit *SU, unsigned OperIdx) {
252 const MachineOperand &MO = SU->getInstr()->getOperand(OperIdx);
253 assert(MO.isDef() && "expect physreg def");
255 // Ask the target if address-backscheduling is desirable, and if so how much.
256 const TargetSubtargetInfo &ST = TM.getSubtarget<TargetSubtargetInfo>();
258 for (MCRegAliasIterator Alias(MO.getReg(), TRI, true);
259 Alias.isValid(); ++Alias) {
260 if (!Uses.contains(*Alias))
261 continue;
262 for (Reg2SUnitsMap::iterator I = Uses.find(*Alias); I != Uses.end(); ++I) {
263 SUnit *UseSU = I->SU;
264 if (UseSU == SU)
265 continue;
267 // Adjust the dependence latency using operand def/use information,
268 // then allow the target to perform its own adjustments.
269 int UseOp = I->OpIdx;
270 MachineInstr *RegUse = nullptr;
271 SDep Dep;
272 if (UseOp < 0)
273 Dep = SDep(SU, SDep::Artificial);
274 else {
275 // Set the hasPhysRegDefs only for physreg defs that have a use within
276 // the scheduling region.
277 SU->hasPhysRegDefs = true;
278 Dep = SDep(SU, SDep::Data, *Alias);
279 RegUse = UseSU->getInstr();
280 }
281 Dep.setLatency(
282 SchedModel.computeOperandLatency(SU->getInstr(), OperIdx, RegUse,
283 UseOp));
285 ST.adjustSchedDependency(SU, UseSU, Dep);
286 UseSU->addPred(Dep);
287 }
288 }
289 }
291 /// addPhysRegDeps - Add register dependencies (data, anti, and output) from
292 /// this SUnit to following instructions in the same scheduling region that
293 /// depend the physical register referenced at OperIdx.
294 void ScheduleDAGInstrs::addPhysRegDeps(SUnit *SU, unsigned OperIdx) {
295 MachineInstr *MI = SU->getInstr();
296 MachineOperand &MO = MI->getOperand(OperIdx);
298 // Optionally add output and anti dependencies. For anti
299 // dependencies we use a latency of 0 because for a multi-issue
300 // target we want to allow the defining instruction to issue
301 // in the same cycle as the using instruction.
302 // TODO: Using a latency of 1 here for output dependencies assumes
303 // there's no cost for reusing registers.
304 SDep::Kind Kind = MO.isUse() ? SDep::Anti : SDep::Output;
305 for (MCRegAliasIterator Alias(MO.getReg(), TRI, true);
306 Alias.isValid(); ++Alias) {
307 if (!Defs.contains(*Alias))
308 continue;
309 for (Reg2SUnitsMap::iterator I = Defs.find(*Alias); I != Defs.end(); ++I) {
310 SUnit *DefSU = I->SU;
311 if (DefSU == &ExitSU)
312 continue;
313 if (DefSU != SU &&
314 (Kind != SDep::Output || !MO.isDead() ||
315 !DefSU->getInstr()->registerDefIsDead(*Alias))) {
316 if (Kind == SDep::Anti)
317 DefSU->addPred(SDep(SU, Kind, /*Reg=*/*Alias));
318 else {
319 SDep Dep(SU, Kind, /*Reg=*/*Alias);
320 Dep.setLatency(
321 SchedModel.computeOutputLatency(MI, OperIdx, DefSU->getInstr()));
322 DefSU->addPred(Dep);
323 }
324 }
325 }
326 }
328 if (!MO.isDef()) {
329 SU->hasPhysRegUses = true;
330 // Either insert a new Reg2SUnits entry with an empty SUnits list, or
331 // retrieve the existing SUnits list for this register's uses.
332 // Push this SUnit on the use list.
333 Uses.insert(PhysRegSUOper(SU, OperIdx, MO.getReg()));
334 if (RemoveKillFlags)
335 MO.setIsKill(false);
336 }
337 else {
338 addPhysRegDataDeps(SU, OperIdx);
339 unsigned Reg = MO.getReg();
341 // clear this register's use list
342 if (Uses.contains(Reg))
343 Uses.eraseAll(Reg);
345 if (!MO.isDead()) {
346 Defs.eraseAll(Reg);
347 } else if (SU->isCall) {
348 // Calls will not be reordered because of chain dependencies (see
349 // below). Since call operands are dead, calls may continue to be added
350 // to the DefList making dependence checking quadratic in the size of
351 // the block. Instead, we leave only one call at the back of the
352 // DefList.
353 Reg2SUnitsMap::RangePair P = Defs.equal_range(Reg);
354 Reg2SUnitsMap::iterator B = P.first;
355 Reg2SUnitsMap::iterator I = P.second;
356 for (bool isBegin = I == B; !isBegin; /* empty */) {
357 isBegin = (--I) == B;
358 if (!I->SU->isCall)
359 break;
360 I = Defs.erase(I);
361 }
362 }
364 // Defs are pushed in the order they are visited and never reordered.
365 Defs.insert(PhysRegSUOper(SU, OperIdx, Reg));
366 }
367 }
369 /// addVRegDefDeps - Add register output and data dependencies from this SUnit
370 /// to instructions that occur later in the same scheduling region if they read
371 /// from or write to the virtual register defined at OperIdx.
372 ///
373 /// TODO: Hoist loop induction variable increments. This has to be
374 /// reevaluated. Generally, IV scheduling should be done before coalescing.
375 void ScheduleDAGInstrs::addVRegDefDeps(SUnit *SU, unsigned OperIdx) {
376 const MachineInstr *MI = SU->getInstr();
377 unsigned Reg = MI->getOperand(OperIdx).getReg();
379 // Singly defined vregs do not have output/anti dependencies.
380 // The current operand is a def, so we have at least one.
381 // Check here if there are any others...
382 if (MRI.hasOneDef(Reg))
383 return;
385 // Add output dependence to the next nearest def of this vreg.
386 //
387 // Unless this definition is dead, the output dependence should be
388 // transitively redundant with antidependencies from this definition's
389 // uses. We're conservative for now until we have a way to guarantee the uses
390 // are not eliminated sometime during scheduling. The output dependence edge
391 // is also useful if output latency exceeds def-use latency.
392 VReg2SUnitMap::iterator DefI = VRegDefs.find(Reg);
393 if (DefI == VRegDefs.end())
394 VRegDefs.insert(VReg2SUnit(Reg, SU));
395 else {
396 SUnit *DefSU = DefI->SU;
397 if (DefSU != SU && DefSU != &ExitSU) {
398 SDep Dep(SU, SDep::Output, Reg);
399 Dep.setLatency(
400 SchedModel.computeOutputLatency(MI, OperIdx, DefSU->getInstr()));
401 DefSU->addPred(Dep);
402 }
403 DefI->SU = SU;
404 }
405 }
407 /// addVRegUseDeps - Add a register data dependency if the instruction that
408 /// defines the virtual register used at OperIdx is mapped to an SUnit. Add a
409 /// register antidependency from this SUnit to instructions that occur later in
410 /// the same scheduling region if they write the virtual register.
411 ///
412 /// TODO: Handle ExitSU "uses" properly.
413 void ScheduleDAGInstrs::addVRegUseDeps(SUnit *SU, unsigned OperIdx) {
414 MachineInstr *MI = SU->getInstr();
415 unsigned Reg = MI->getOperand(OperIdx).getReg();
417 // Record this local VReg use.
418 VReg2UseMap::iterator UI = VRegUses.find(Reg);
419 for (; UI != VRegUses.end(); ++UI) {
420 if (UI->SU == SU)
421 break;
422 }
423 if (UI == VRegUses.end())
424 VRegUses.insert(VReg2SUnit(Reg, SU));
426 // Lookup this operand's reaching definition.
427 assert(LIS && "vreg dependencies requires LiveIntervals");
428 LiveQueryResult LRQ
429 = LIS->getInterval(Reg).Query(LIS->getInstructionIndex(MI));
430 VNInfo *VNI = LRQ.valueIn();
432 // VNI will be valid because MachineOperand::readsReg() is checked by caller.
433 assert(VNI && "No value to read by operand");
434 MachineInstr *Def = LIS->getInstructionFromIndex(VNI->def);
435 // Phis and other noninstructions (after coalescing) have a NULL Def.
436 if (Def) {
437 SUnit *DefSU = getSUnit(Def);
438 if (DefSU) {
439 // The reaching Def lives within this scheduling region.
440 // Create a data dependence.
441 SDep dep(DefSU, SDep::Data, Reg);
442 // Adjust the dependence latency using operand def/use information, then
443 // allow the target to perform its own adjustments.
444 int DefOp = Def->findRegisterDefOperandIdx(Reg);
445 dep.setLatency(SchedModel.computeOperandLatency(Def, DefOp, MI, OperIdx));
447 const TargetSubtargetInfo &ST = TM.getSubtarget<TargetSubtargetInfo>();
448 ST.adjustSchedDependency(DefSU, SU, const_cast<SDep &>(dep));
449 SU->addPred(dep);
450 }
451 }
453 // Add antidependence to the following def of the vreg it uses.
454 VReg2SUnitMap::iterator DefI = VRegDefs.find(Reg);
455 if (DefI != VRegDefs.end() && DefI->SU != SU)
456 DefI->SU->addPred(SDep(SU, SDep::Anti, Reg));
457 }
459 /// Return true if MI is an instruction we are unable to reason about
460 /// (like a call or something with unmodeled side effects).
461 static inline bool isGlobalMemoryObject(AliasAnalysis *AA, MachineInstr *MI) {
462 if (MI->isCall() || MI->hasUnmodeledSideEffects() ||
463 (MI->hasOrderedMemoryRef() &&
464 (!MI->mayLoad() || !MI->isInvariantLoad(AA))))
465 return true;
466 return false;
467 }
469 // This MI might have either incomplete info, or known to be unsafe
470 // to deal with (i.e. volatile object).
471 static inline bool isUnsafeMemoryObject(MachineInstr *MI,
472 const MachineFrameInfo *MFI) {
473 if (!MI || MI->memoperands_empty())
474 return true;
475 // We purposefully do no check for hasOneMemOperand() here
476 // in hope to trigger an assert downstream in order to
477 // finish implementation.
478 if ((*MI->memoperands_begin())->isVolatile() ||
479 MI->hasUnmodeledSideEffects())
480 return true;
482 if ((*MI->memoperands_begin())->getPseudoValue()) {
483 // Similarly to getUnderlyingObjectForInstr:
484 // For now, ignore PseudoSourceValues which may alias LLVM IR values
485 // because the code that uses this function has no way to cope with
486 // such aliases.
487 return true;
488 }
490 const Value *V = (*MI->memoperands_begin())->getValue();
491 if (!V)
492 return true;
494 SmallVector<Value *, 4> Objs;
495 getUnderlyingObjects(V, Objs);
496 for (SmallVectorImpl<Value *>::iterator I = Objs.begin(),
497 IE = Objs.end(); I != IE; ++I) {
498 // Does this pointer refer to a distinct and identifiable object?
499 if (!isIdentifiedObject(*I))
500 return true;
501 }
503 return false;
504 }
506 /// This returns true if the two MIs need a chain edge betwee them.
507 /// If these are not even memory operations, we still may need
508 /// chain deps between them. The question really is - could
509 /// these two MIs be reordered during scheduling from memory dependency
510 /// point of view.
511 static bool MIsNeedChainEdge(AliasAnalysis *AA, const MachineFrameInfo *MFI,
512 MachineInstr *MIa,
513 MachineInstr *MIb) {
514 const MachineFunction *MF = MIa->getParent()->getParent();
515 const TargetInstrInfo *TII = MF->getSubtarget().getInstrInfo();
517 // Cover a trivial case - no edge is need to itself.
518 if (MIa == MIb)
519 return false;
521 // Let the target decide if memory accesses cannot possibly overlap.
522 if ((MIa->mayLoad() || MIa->mayStore()) &&
523 (MIb->mayLoad() || MIb->mayStore()))
524 if (TII->areMemAccessesTriviallyDisjoint(MIa, MIb, AA))
525 return false;
527 // FIXME: Need to handle multiple memory operands to support all targets.
528 if (!MIa->hasOneMemOperand() || !MIb->hasOneMemOperand())
529 return true;
531 if (isUnsafeMemoryObject(MIa, MFI) || isUnsafeMemoryObject(MIb, MFI))
532 return true;
534 // If we are dealing with two "normal" loads, we do not need an edge
535 // between them - they could be reordered.
536 if (!MIa->mayStore() && !MIb->mayStore())
537 return false;
539 // To this point analysis is generic. From here on we do need AA.
540 if (!AA)
541 return true;
543 MachineMemOperand *MMOa = *MIa->memoperands_begin();
544 MachineMemOperand *MMOb = *MIb->memoperands_begin();
546 if (!MMOa->getValue() || !MMOb->getValue())
547 return true;
549 // The following interface to AA is fashioned after DAGCombiner::isAlias
550 // and operates with MachineMemOperand offset with some important
551 // assumptions:
552 // - LLVM fundamentally assumes flat address spaces.
553 // - MachineOperand offset can *only* result from legalization and
554 // cannot affect queries other than the trivial case of overlap
555 // checking.
556 // - These offsets never wrap and never step outside
557 // of allocated objects.
558 // - There should never be any negative offsets here.
559 //
560 // FIXME: Modify API to hide this math from "user"
561 // FIXME: Even before we go to AA we can reason locally about some
562 // memory objects. It can save compile time, and possibly catch some
563 // corner cases not currently covered.
565 assert ((MMOa->getOffset() >= 0) && "Negative MachineMemOperand offset");
566 assert ((MMOb->getOffset() >= 0) && "Negative MachineMemOperand offset");
568 int64_t MinOffset = std::min(MMOa->getOffset(), MMOb->getOffset());
569 int64_t Overlapa = MMOa->getSize() + MMOa->getOffset() - MinOffset;
570 int64_t Overlapb = MMOb->getSize() + MMOb->getOffset() - MinOffset;
572 AliasAnalysis::AliasResult AAResult = AA->alias(
573 AliasAnalysis::Location(MMOa->getValue(), Overlapa,
574 UseTBAA ? MMOa->getAAInfo() : AAMDNodes()),
575 AliasAnalysis::Location(MMOb->getValue(), Overlapb,
576 UseTBAA ? MMOb->getAAInfo() : AAMDNodes()));
578 return (AAResult != AliasAnalysis::NoAlias);
579 }
581 /// This recursive function iterates over chain deps of SUb looking for
582 /// "latest" node that needs a chain edge to SUa.
583 static unsigned
584 iterateChainSucc(AliasAnalysis *AA, const MachineFrameInfo *MFI,
585 SUnit *SUa, SUnit *SUb, SUnit *ExitSU, unsigned *Depth,
586 SmallPtrSetImpl<const SUnit*> &Visited) {
587 if (!SUa || !SUb || SUb == ExitSU)
588 return *Depth;
590 // Remember visited nodes.
591 if (!Visited.insert(SUb).second)
592 return *Depth;
593 // If there is _some_ dependency already in place, do not
594 // descend any further.
595 // TODO: Need to make sure that if that dependency got eliminated or ignored
596 // for any reason in the future, we would not violate DAG topology.
597 // Currently it does not happen, but makes an implicit assumption about
598 // future implementation.
599 //
600 // Independently, if we encounter node that is some sort of global
601 // object (like a call) we already have full set of dependencies to it
602 // and we can stop descending.
603 if (SUa->isSucc(SUb) ||
604 isGlobalMemoryObject(AA, SUb->getInstr()))
605 return *Depth;
607 // If we do need an edge, or we have exceeded depth budget,
608 // add that edge to the predecessors chain of SUb,
609 // and stop descending.
610 if (*Depth > 200 ||
611 MIsNeedChainEdge(AA, MFI, SUa->getInstr(), SUb->getInstr())) {
612 SUb->addPred(SDep(SUa, SDep::MayAliasMem));
613 return *Depth;
614 }
615 // Track current depth.
616 (*Depth)++;
617 // Iterate over memory dependencies only.
618 for (SUnit::const_succ_iterator I = SUb->Succs.begin(), E = SUb->Succs.end();
619 I != E; ++I)
620 if (I->isNormalMemoryOrBarrier())
621 iterateChainSucc (AA, MFI, SUa, I->getSUnit(), ExitSU, Depth, Visited);
622 return *Depth;
623 }
625 /// This function assumes that "downward" from SU there exist
626 /// tail/leaf of already constructed DAG. It iterates downward and
627 /// checks whether SU can be aliasing any node dominated
628 /// by it.
629 static void adjustChainDeps(AliasAnalysis *AA, const MachineFrameInfo *MFI,
630 SUnit *SU, SUnit *ExitSU, std::set<SUnit *> &CheckList,
631 unsigned LatencyToLoad) {
632 if (!SU)
633 return;
635 SmallPtrSet<const SUnit*, 16> Visited;
636 unsigned Depth = 0;
638 for (std::set<SUnit *>::iterator I = CheckList.begin(), IE = CheckList.end();
639 I != IE; ++I) {
640 if (SU == *I)
641 continue;
642 if (MIsNeedChainEdge(AA, MFI, SU->getInstr(), (*I)->getInstr())) {
643 SDep Dep(SU, SDep::MayAliasMem);
644 Dep.setLatency(((*I)->getInstr()->mayLoad()) ? LatencyToLoad : 0);
645 (*I)->addPred(Dep);
646 }
648 // Iterate recursively over all previously added memory chain
649 // successors. Keep track of visited nodes.
650 for (SUnit::const_succ_iterator J = (*I)->Succs.begin(),
651 JE = (*I)->Succs.end(); J != JE; ++J)
652 if (J->isNormalMemoryOrBarrier())
653 iterateChainSucc (AA, MFI, SU, J->getSUnit(),
654 ExitSU, &Depth, Visited);
655 }
656 }
658 /// Check whether two objects need a chain edge, if so, add it
659 /// otherwise remember the rejected SU.
660 static inline
661 void addChainDependency (AliasAnalysis *AA, const MachineFrameInfo *MFI,
662 SUnit *SUa, SUnit *SUb,
663 std::set<SUnit *> &RejectList,
664 unsigned TrueMemOrderLatency = 0,
665 bool isNormalMemory = false) {
666 // If this is a false dependency,
667 // do not add the edge, but rememeber the rejected node.
668 if (MIsNeedChainEdge(AA, MFI, SUa->getInstr(), SUb->getInstr())) {
669 SDep Dep(SUa, isNormalMemory ? SDep::MayAliasMem : SDep::Barrier);
670 Dep.setLatency(TrueMemOrderLatency);
671 SUb->addPred(Dep);
672 }
673 else {
674 // Duplicate entries should be ignored.
675 RejectList.insert(SUb);
676 DEBUG(dbgs() << "\tReject chain dep between SU("
677 << SUa->NodeNum << ") and SU("
678 << SUb->NodeNum << ")\n");
679 }
680 }
682 /// Create an SUnit for each real instruction, numbered in top-down toplological
683 /// order. The instruction order A < B, implies that no edge exists from B to A.
684 ///
685 /// Map each real instruction to its SUnit.
686 ///
687 /// After initSUnits, the SUnits vector cannot be resized and the scheduler may
688 /// hang onto SUnit pointers. We may relax this in the future by using SUnit IDs
689 /// instead of pointers.
690 ///
691 /// MachineScheduler relies on initSUnits numbering the nodes by their order in
692 /// the original instruction list.
693 void ScheduleDAGInstrs::initSUnits() {
694 // We'll be allocating one SUnit for each real instruction in the region,
695 // which is contained within a basic block.
696 SUnits.reserve(NumRegionInstrs);
698 for (MachineBasicBlock::iterator I = RegionBegin; I != RegionEnd; ++I) {
699 MachineInstr *MI = I;
700 if (MI->isDebugValue())
701 continue;
703 SUnit *SU = newSUnit(MI);
704 MISUnitMap[MI] = SU;
706 SU->isCall = MI->isCall();
707 SU->isCommutable = MI->isCommutable();
709 // Assign the Latency field of SU using target-provided information.
710 SU->Latency = SchedModel.computeInstrLatency(SU->getInstr());
712 // If this SUnit uses a reserved or unbuffered resource, mark it as such.
713 //
714 // Reserved resources block an instruction from issuing and stall the
715 // entire pipeline. These are identified by BufferSize=0.
716 //
717 // Unbuffered resources prevent execution of subsequent instructions that
718 // require the same resources. This is used for in-order execution pipelines
719 // within an out-of-order core. These are identified by BufferSize=1.
720 if (SchedModel.hasInstrSchedModel()) {
721 const MCSchedClassDesc *SC = getSchedClass(SU);
722 for (TargetSchedModel::ProcResIter
723 PI = SchedModel.getWriteProcResBegin(SC),
724 PE = SchedModel.getWriteProcResEnd(SC); PI != PE; ++PI) {
725 switch (SchedModel.getProcResource(PI->ProcResourceIdx)->BufferSize) {
726 case 0:
727 SU->hasReservedResource = true;
728 break;
729 case 1:
730 SU->isUnbuffered = true;
731 break;
732 default:
733 break;
734 }
735 }
736 }
737 }
738 }
740 /// If RegPressure is non-null, compute register pressure as a side effect. The
741 /// DAG builder is an efficient place to do it because it already visits
742 /// operands.
743 void ScheduleDAGInstrs::buildSchedGraph(AliasAnalysis *AA,
744 RegPressureTracker *RPTracker,
745 PressureDiffs *PDiffs) {
746 const TargetSubtargetInfo &ST = TM.getSubtarget<TargetSubtargetInfo>();
747 bool UseAA = EnableAASchedMI.getNumOccurrences() > 0 ? EnableAASchedMI
748 : ST.useAA();
749 AliasAnalysis *AAForDep = UseAA ? AA : nullptr;
751 MISUnitMap.clear();
752 ScheduleDAG::clearDAG();
754 // Create an SUnit for each real instruction.
755 initSUnits();
757 if (PDiffs)
758 PDiffs->init(SUnits.size());
760 // We build scheduling units by walking a block's instruction list from bottom
761 // to top.
763 // Remember where a generic side-effecting instruction is as we procede.
764 SUnit *BarrierChain = nullptr, *AliasChain = nullptr;
766 // Memory references to specific known memory locations are tracked
767 // so that they can be given more precise dependencies. We track
768 // separately the known memory locations that may alias and those
769 // that are known not to alias
770 MapVector<ValueType, std::vector<SUnit *> > AliasMemDefs, NonAliasMemDefs;
771 MapVector<ValueType, std::vector<SUnit *> > AliasMemUses, NonAliasMemUses;
772 std::set<SUnit*> RejectMemNodes;
774 // Remove any stale debug info; sometimes BuildSchedGraph is called again
775 // without emitting the info from the previous call.
776 DbgValues.clear();
777 FirstDbgValue = nullptr;
779 assert(Defs.empty() && Uses.empty() &&
780 "Only BuildGraph should update Defs/Uses");
781 Defs.setUniverse(TRI->getNumRegs());
782 Uses.setUniverse(TRI->getNumRegs());
784 assert(VRegDefs.empty() && "Only BuildSchedGraph may access VRegDefs");
785 VRegUses.clear();
786 VRegDefs.setUniverse(MRI.getNumVirtRegs());
787 VRegUses.setUniverse(MRI.getNumVirtRegs());
789 // Model data dependencies between instructions being scheduled and the
790 // ExitSU.
791 addSchedBarrierDeps();
793 // Walk the list of instructions, from bottom moving up.
794 MachineInstr *DbgMI = nullptr;
795 for (MachineBasicBlock::iterator MII = RegionEnd, MIE = RegionBegin;
796 MII != MIE; --MII) {
797 MachineInstr *MI = std::prev(MII);
798 if (MI && DbgMI) {
799 DbgValues.push_back(std::make_pair(DbgMI, MI));
800 DbgMI = nullptr;
801 }
803 if (MI->isDebugValue()) {
804 DbgMI = MI;
805 continue;
806 }
807 SUnit *SU = MISUnitMap[MI];
808 assert(SU && "No SUnit mapped to this MI");
810 if (RPTracker) {
811 PressureDiff *PDiff = PDiffs ? &(*PDiffs)[SU->NodeNum] : nullptr;
812 RPTracker->recede(/*LiveUses=*/nullptr, PDiff);
813 assert(RPTracker->getPos() == std::prev(MII) &&
814 "RPTracker can't find MI");
815 }
817 assert(
818 (CanHandleTerminators || (!MI->isTerminator() && !MI->isPosition())) &&
819 "Cannot schedule terminators or labels!");
821 // Add register-based dependencies (data, anti, and output).
822 bool HasVRegDef = false;
823 for (unsigned j = 0, n = MI->getNumOperands(); j != n; ++j) {
824 const MachineOperand &MO = MI->getOperand(j);
825 if (!MO.isReg()) continue;
826 unsigned Reg = MO.getReg();
827 if (Reg == 0) continue;
829 if (TRI->isPhysicalRegister(Reg))
830 addPhysRegDeps(SU, j);
831 else {
832 assert(!IsPostRA && "Virtual register encountered!");
833 if (MO.isDef()) {
834 HasVRegDef = true;
835 addVRegDefDeps(SU, j);
836 }
837 else if (MO.readsReg()) // ignore undef operands
838 addVRegUseDeps(SU, j);
839 }
840 }
841 // If we haven't seen any uses in this scheduling region, create a
842 // dependence edge to ExitSU to model the live-out latency. This is required
843 // for vreg defs with no in-region use, and prefetches with no vreg def.
844 //
845 // FIXME: NumDataSuccs would be more precise than NumSuccs here. This
846 // check currently relies on being called before adding chain deps.
847 if (SU->NumSuccs == 0 && SU->Latency > 1
848 && (HasVRegDef || MI->mayLoad())) {
849 SDep Dep(SU, SDep::Artificial);
850 Dep.setLatency(SU->Latency - 1);
851 ExitSU.addPred(Dep);
852 }
854 // Add chain dependencies.
855 // Chain dependencies used to enforce memory order should have
856 // latency of 0 (except for true dependency of Store followed by
857 // aliased Load... we estimate that with a single cycle of latency
858 // assuming the hardware will bypass)
859 // Note that isStoreToStackSlot and isLoadFromStackSLot are not usable
860 // after stack slots are lowered to actual addresses.
861 // TODO: Use an AliasAnalysis and do real alias-analysis queries, and
862 // produce more precise dependence information.
863 unsigned TrueMemOrderLatency = MI->mayStore() ? 1 : 0;
864 if (isGlobalMemoryObject(AA, MI)) {
865 // Be conservative with these and add dependencies on all memory
866 // references, even those that are known to not alias.
867 for (MapVector<ValueType, std::vector<SUnit *> >::iterator I =
868 NonAliasMemDefs.begin(), E = NonAliasMemDefs.end(); I != E; ++I) {
869 for (unsigned i = 0, e = I->second.size(); i != e; ++i) {
870 I->second[i]->addPred(SDep(SU, SDep::Barrier));
871 }
872 }
873 for (MapVector<ValueType, std::vector<SUnit *> >::iterator I =
874 NonAliasMemUses.begin(), E = NonAliasMemUses.end(); I != E; ++I) {
875 for (unsigned i = 0, e = I->second.size(); i != e; ++i) {
876 SDep Dep(SU, SDep::Barrier);
877 Dep.setLatency(TrueMemOrderLatency);
878 I->second[i]->addPred(Dep);
879 }
880 }
881 // Add SU to the barrier chain.
882 if (BarrierChain)
883 BarrierChain->addPred(SDep(SU, SDep::Barrier));
884 BarrierChain = SU;
885 // This is a barrier event that acts as a pivotal node in the DAG,
886 // so it is safe to clear list of exposed nodes.
887 adjustChainDeps(AA, MFI, SU, &ExitSU, RejectMemNodes,
888 TrueMemOrderLatency);
889 RejectMemNodes.clear();
890 NonAliasMemDefs.clear();
891 NonAliasMemUses.clear();
893 // fall-through
894 new_alias_chain:
895 // Chain all possibly aliasing memory references through SU.
896 if (AliasChain) {
897 unsigned ChainLatency = 0;
898 if (AliasChain->getInstr()->mayLoad())
899 ChainLatency = TrueMemOrderLatency;
900 addChainDependency(AAForDep, MFI, SU, AliasChain, RejectMemNodes,
901 ChainLatency);
902 }
903 AliasChain = SU;
904 for (unsigned k = 0, m = PendingLoads.size(); k != m; ++k)
905 addChainDependency(AAForDep, MFI, SU, PendingLoads[k], RejectMemNodes,
906 TrueMemOrderLatency);
907 for (MapVector<ValueType, std::vector<SUnit *> >::iterator I =
908 AliasMemDefs.begin(), E = AliasMemDefs.end(); I != E; ++I) {
909 for (unsigned i = 0, e = I->second.size(); i != e; ++i)
910 addChainDependency(AAForDep, MFI, SU, I->second[i], RejectMemNodes);
911 }
912 for (MapVector<ValueType, std::vector<SUnit *> >::iterator I =
913 AliasMemUses.begin(), E = AliasMemUses.end(); I != E; ++I) {
914 for (unsigned i = 0, e = I->second.size(); i != e; ++i)
915 addChainDependency(AAForDep, MFI, SU, I->second[i], RejectMemNodes,
916 TrueMemOrderLatency);
917 }
918 adjustChainDeps(AA, MFI, SU, &ExitSU, RejectMemNodes,
919 TrueMemOrderLatency);
920 PendingLoads.clear();
921 AliasMemDefs.clear();
922 AliasMemUses.clear();
923 } else if (MI->mayStore()) {
924 // Add dependence on barrier chain, if needed.
925 // There is no point to check aliasing on barrier event. Even if
926 // SU and barrier _could_ be reordered, they should not. In addition,
927 // we have lost all RejectMemNodes below barrier.
928 if (BarrierChain)
929 BarrierChain->addPred(SDep(SU, SDep::Barrier));
931 UnderlyingObjectsVector Objs;
932 getUnderlyingObjectsForInstr(MI, MFI, Objs);
934 if (Objs.empty()) {
935 // Treat all other stores conservatively.
936 goto new_alias_chain;
937 }
939 bool MayAlias = false;
940 for (UnderlyingObjectsVector::iterator K = Objs.begin(), KE = Objs.end();
941 K != KE; ++K) {
942 ValueType V = K->getPointer();
943 bool ThisMayAlias = K->getInt();
944 if (ThisMayAlias)
945 MayAlias = true;
947 // A store to a specific PseudoSourceValue. Add precise dependencies.
948 // Record the def in MemDefs, first adding a dep if there is
949 // an existing def.
950 MapVector<ValueType, std::vector<SUnit *> >::iterator I =
951 ((ThisMayAlias) ? AliasMemDefs.find(V) : NonAliasMemDefs.find(V));
952 MapVector<ValueType, std::vector<SUnit *> >::iterator IE =
953 ((ThisMayAlias) ? AliasMemDefs.end() : NonAliasMemDefs.end());
954 if (I != IE) {
955 for (unsigned i = 0, e = I->second.size(); i != e; ++i)
956 addChainDependency(AAForDep, MFI, SU, I->second[i], RejectMemNodes,
957 0, true);
959 // If we're not using AA, then we only need one store per object.
960 if (!AAForDep)
961 I->second.clear();
962 I->second.push_back(SU);
963 } else {
964 if (ThisMayAlias) {
965 if (!AAForDep)
966 AliasMemDefs[V].clear();
967 AliasMemDefs[V].push_back(SU);
968 } else {
969 if (!AAForDep)
970 NonAliasMemDefs[V].clear();
971 NonAliasMemDefs[V].push_back(SU);
972 }
973 }
974 // Handle the uses in MemUses, if there are any.
975 MapVector<ValueType, std::vector<SUnit *> >::iterator J =
976 ((ThisMayAlias) ? AliasMemUses.find(V) : NonAliasMemUses.find(V));
977 MapVector<ValueType, std::vector<SUnit *> >::iterator JE =
978 ((ThisMayAlias) ? AliasMemUses.end() : NonAliasMemUses.end());
979 if (J != JE) {
980 for (unsigned i = 0, e = J->second.size(); i != e; ++i)
981 addChainDependency(AAForDep, MFI, SU, J->second[i], RejectMemNodes,
982 TrueMemOrderLatency, true);
983 J->second.clear();
984 }
985 }
986 if (MayAlias) {
987 // Add dependencies from all the PendingLoads, i.e. loads
988 // with no underlying object.
989 for (unsigned k = 0, m = PendingLoads.size(); k != m; ++k)
990 addChainDependency(AAForDep, MFI, SU, PendingLoads[k], RejectMemNodes,
991 TrueMemOrderLatency);
992 // Add dependence on alias chain, if needed.
993 if (AliasChain)
994 addChainDependency(AAForDep, MFI, SU, AliasChain, RejectMemNodes);
995 // But we also should check dependent instructions for the
996 // SU in question.
997 adjustChainDeps(AA, MFI, SU, &ExitSU, RejectMemNodes,
998 TrueMemOrderLatency);
999 }
1000 } else if (MI->mayLoad()) {
1001 bool MayAlias = true;
1002 if (MI->isInvariantLoad(AA)) {
1003 // Invariant load, no chain dependencies needed!
1004 } else {
1005 UnderlyingObjectsVector Objs;
1006 getUnderlyingObjectsForInstr(MI, MFI, Objs);
1008 if (Objs.empty()) {
1009 // A load with no underlying object. Depend on all
1010 // potentially aliasing stores.
1011 for (MapVector<ValueType, std::vector<SUnit *> >::iterator I =
1012 AliasMemDefs.begin(), E = AliasMemDefs.end(); I != E; ++I)
1013 for (unsigned i = 0, e = I->second.size(); i != e; ++i)
1014 addChainDependency(AAForDep, MFI, SU, I->second[i],
1015 RejectMemNodes);
1017 PendingLoads.push_back(SU);
1018 MayAlias = true;
1019 } else {
1020 MayAlias = false;
1021 }
1023 for (UnderlyingObjectsVector::iterator
1024 J = Objs.begin(), JE = Objs.end(); J != JE; ++J) {
1025 ValueType V = J->getPointer();
1026 bool ThisMayAlias = J->getInt();
1028 if (ThisMayAlias)
1029 MayAlias = true;
1031 // A load from a specific PseudoSourceValue. Add precise dependencies.
1032 MapVector<ValueType, std::vector<SUnit *> >::iterator I =
1033 ((ThisMayAlias) ? AliasMemDefs.find(V) : NonAliasMemDefs.find(V));
1034 MapVector<ValueType, std::vector<SUnit *> >::iterator IE =
1035 ((ThisMayAlias) ? AliasMemDefs.end() : NonAliasMemDefs.end());
1036 if (I != IE)
1037 for (unsigned i = 0, e = I->second.size(); i != e; ++i)
1038 addChainDependency(AAForDep, MFI, SU, I->second[i],
1039 RejectMemNodes, 0, true);
1040 if (ThisMayAlias)
1041 AliasMemUses[V].push_back(SU);
1042 else
1043 NonAliasMemUses[V].push_back(SU);
1044 }
1045 if (MayAlias)
1046 adjustChainDeps(AA, MFI, SU, &ExitSU, RejectMemNodes, /*Latency=*/0);
1047 // Add dependencies on alias and barrier chains, if needed.
1048 if (MayAlias && AliasChain)
1049 addChainDependency(AAForDep, MFI, SU, AliasChain, RejectMemNodes);
1050 if (BarrierChain)
1051 BarrierChain->addPred(SDep(SU, SDep::Barrier));
1052 }
1053 }
1054 }
1055 if (DbgMI)
1056 FirstDbgValue = DbgMI;
1058 Defs.clear();
1059 Uses.clear();
1060 VRegDefs.clear();
1061 PendingLoads.clear();
1062 }
1064 /// \brief Initialize register live-range state for updating kills.
1065 void ScheduleDAGInstrs::startBlockForKills(MachineBasicBlock *BB) {
1066 // Start with no live registers.
1067 LiveRegs.reset();
1069 // Examine the live-in regs of all successors.
1070 for (MachineBasicBlock::succ_iterator SI = BB->succ_begin(),
1071 SE = BB->succ_end(); SI != SE; ++SI) {
1072 for (MachineBasicBlock::livein_iterator I = (*SI)->livein_begin(),
1073 E = (*SI)->livein_end(); I != E; ++I) {
1074 unsigned Reg = *I;
1075 // Repeat, for reg and all subregs.
1076 for (MCSubRegIterator SubRegs(Reg, TRI, /*IncludeSelf=*/true);
1077 SubRegs.isValid(); ++SubRegs)
1078 LiveRegs.set(*SubRegs);
1079 }
1080 }
1081 }
1083 bool ScheduleDAGInstrs::toggleKillFlag(MachineInstr *MI, MachineOperand &MO) {
1084 // Setting kill flag...
1085 if (!MO.isKill()) {
1086 MO.setIsKill(true);
1087 return false;
1088 }
1090 // If MO itself is live, clear the kill flag...
1091 if (LiveRegs.test(MO.getReg())) {
1092 MO.setIsKill(false);
1093 return false;
1094 }
1096 // If any subreg of MO is live, then create an imp-def for that
1097 // subreg and keep MO marked as killed.
1098 MO.setIsKill(false);
1099 bool AllDead = true;
1100 const unsigned SuperReg = MO.getReg();
1101 MachineInstrBuilder MIB(MF, MI);
1102 for (MCSubRegIterator SubRegs(SuperReg, TRI); SubRegs.isValid(); ++SubRegs) {
1103 if (LiveRegs.test(*SubRegs)) {
1104 MIB.addReg(*SubRegs, RegState::ImplicitDefine);
1105 AllDead = false;
1106 }
1107 }
1109 if(AllDead)
1110 MO.setIsKill(true);
1111 return false;
1112 }
1114 // FIXME: Reuse the LivePhysRegs utility for this.
1115 void ScheduleDAGInstrs::fixupKills(MachineBasicBlock *MBB) {
1116 DEBUG(dbgs() << "Fixup kills for BB#" << MBB->getNumber() << '\n');
1118 LiveRegs.resize(TRI->getNumRegs());
1119 BitVector killedRegs(TRI->getNumRegs());
1121 startBlockForKills(MBB);
1123 // Examine block from end to start...
1124 unsigned Count = MBB->size();
1125 for (MachineBasicBlock::iterator I = MBB->end(), E = MBB->begin();
1126 I != E; --Count) {
1127 MachineInstr *MI = --I;
1128 if (MI->isDebugValue())
1129 continue;
1131 // Update liveness. Registers that are defed but not used in this
1132 // instruction are now dead. Mark register and all subregs as they
1133 // are completely defined.
1134 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
1135 MachineOperand &MO = MI->getOperand(i);
1136 if (MO.isRegMask())
1137 LiveRegs.clearBitsNotInMask(MO.getRegMask());
1138 if (!MO.isReg()) continue;
1139 unsigned Reg = MO.getReg();
1140 if (Reg == 0) continue;
1141 if (!MO.isDef()) continue;
1142 // Ignore two-addr defs.
1143 if (MI->isRegTiedToUseOperand(i)) continue;
1145 // Repeat for reg and all subregs.
1146 for (MCSubRegIterator SubRegs(Reg, TRI, /*IncludeSelf=*/true);
1147 SubRegs.isValid(); ++SubRegs)
1148 LiveRegs.reset(*SubRegs);
1149 }
1151 // Examine all used registers and set/clear kill flag. When a
1152 // register is used multiple times we only set the kill flag on
1153 // the first use. Don't set kill flags on undef operands.
1154 killedRegs.reset();
1155 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
1156 MachineOperand &MO = MI->getOperand(i);
1157 if (!MO.isReg() || !MO.isUse() || MO.isUndef()) continue;
1158 unsigned Reg = MO.getReg();
1159 if ((Reg == 0) || MRI.isReserved(Reg)) continue;
1161 bool kill = false;
1162 if (!killedRegs.test(Reg)) {
1163 kill = true;
1164 // A register is not killed if any subregs are live...
1165 for (MCSubRegIterator SubRegs(Reg, TRI); SubRegs.isValid(); ++SubRegs) {
1166 if (LiveRegs.test(*SubRegs)) {
1167 kill = false;
1168 break;
1169 }
1170 }
1172 // If subreg is not live, then register is killed if it became
1173 // live in this instruction
1174 if (kill)
1175 kill = !LiveRegs.test(Reg);
1176 }
1178 if (MO.isKill() != kill) {
1179 DEBUG(dbgs() << "Fixing " << MO << " in ");
1180 // Warning: toggleKillFlag may invalidate MO.
1181 toggleKillFlag(MI, MO);
1182 DEBUG(MI->dump());
1183 }
1185 killedRegs.set(Reg);
1186 }
1188 // Mark any used register (that is not using undef) and subregs as
1189 // now live...
1190 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
1191 MachineOperand &MO = MI->getOperand(i);
1192 if (!MO.isReg() || !MO.isUse() || MO.isUndef()) continue;
1193 unsigned Reg = MO.getReg();
1194 if ((Reg == 0) || MRI.isReserved(Reg)) continue;
1196 for (MCSubRegIterator SubRegs(Reg, TRI, /*IncludeSelf=*/true);
1197 SubRegs.isValid(); ++SubRegs)
1198 LiveRegs.set(*SubRegs);
1199 }
1200 }
1201 }
1203 void ScheduleDAGInstrs::dumpNode(const SUnit *SU) const {
1204 #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
1205 SU->getInstr()->dump();
1206 #endif
1207 }
1209 std::string ScheduleDAGInstrs::getGraphNodeLabel(const SUnit *SU) const {
1210 std::string s;
1211 raw_string_ostream oss(s);
1212 if (SU == &EntrySU)
1213 oss << "<entry>";
1214 else if (SU == &ExitSU)
1215 oss << "<exit>";
1216 else
1217 SU->getInstr()->print(oss, &TM, /*SkipOpers=*/true);
1218 return oss.str();
1219 }
1221 /// Return the basic block label. It is not necessarilly unique because a block
1222 /// contains multiple scheduling regions. But it is fine for visualization.
1223 std::string ScheduleDAGInstrs::getDAGName() const {
1224 return "dag." + BB->getFullName();
1225 }
1227 //===----------------------------------------------------------------------===//
1228 // SchedDFSResult Implementation
1229 //===----------------------------------------------------------------------===//
1231 namespace llvm {
1232 /// \brief Internal state used to compute SchedDFSResult.
1233 class SchedDFSImpl {
1234 SchedDFSResult &R;
1236 /// Join DAG nodes into equivalence classes by their subtree.
1237 IntEqClasses SubtreeClasses;
1238 /// List PredSU, SuccSU pairs that represent data edges between subtrees.
1239 std::vector<std::pair<const SUnit*, const SUnit*> > ConnectionPairs;
1241 struct RootData {
1242 unsigned NodeID;
1243 unsigned ParentNodeID; // Parent node (member of the parent subtree).
1244 unsigned SubInstrCount; // Instr count in this tree only, not children.
1246 RootData(unsigned id): NodeID(id),
1247 ParentNodeID(SchedDFSResult::InvalidSubtreeID),
1248 SubInstrCount(0) {}
1250 unsigned getSparseSetIndex() const { return NodeID; }
1251 };
1253 SparseSet<RootData> RootSet;
1255 public:
1256 SchedDFSImpl(SchedDFSResult &r): R(r), SubtreeClasses(R.DFSNodeData.size()) {
1257 RootSet.setUniverse(R.DFSNodeData.size());
1258 }
1260 /// Return true if this node been visited by the DFS traversal.
1261 ///
1262 /// During visitPostorderNode the Node's SubtreeID is assigned to the Node
1263 /// ID. Later, SubtreeID is updated but remains valid.
1264 bool isVisited(const SUnit *SU) const {
1265 return R.DFSNodeData[SU->NodeNum].SubtreeID
1266 != SchedDFSResult::InvalidSubtreeID;
1267 }
1269 /// Initialize this node's instruction count. We don't need to flag the node
1270 /// visited until visitPostorder because the DAG cannot have cycles.
1271 void visitPreorder(const SUnit *SU) {
1272 R.DFSNodeData[SU->NodeNum].InstrCount =
1273 SU->getInstr()->isTransient() ? 0 : 1;
1274 }
1276 /// Called once for each node after all predecessors are visited. Revisit this
1277 /// node's predecessors and potentially join them now that we know the ILP of
1278 /// the other predecessors.
1279 void visitPostorderNode(const SUnit *SU) {
1280 // Mark this node as the root of a subtree. It may be joined with its
1281 // successors later.
1282 R.DFSNodeData[SU->NodeNum].SubtreeID = SU->NodeNum;
1283 RootData RData(SU->NodeNum);
1284 RData.SubInstrCount = SU->getInstr()->isTransient() ? 0 : 1;
1286 // If any predecessors are still in their own subtree, they either cannot be
1287 // joined or are large enough to remain separate. If this parent node's
1288 // total instruction count is not greater than a child subtree by at least
1289 // the subtree limit, then try to join it now since splitting subtrees is
1290 // only useful if multiple high-pressure paths are possible.
1291 unsigned InstrCount = R.DFSNodeData[SU->NodeNum].InstrCount;
1292 for (SUnit::const_pred_iterator
1293 PI = SU->Preds.begin(), PE = SU->Preds.end(); PI != PE; ++PI) {
1294 if (PI->getKind() != SDep::Data)
1295 continue;
1296 unsigned PredNum = PI->getSUnit()->NodeNum;
1297 if ((InstrCount - R.DFSNodeData[PredNum].InstrCount) < R.SubtreeLimit)
1298 joinPredSubtree(*PI, SU, /*CheckLimit=*/false);
1300 // Either link or merge the TreeData entry from the child to the parent.
1301 if (R.DFSNodeData[PredNum].SubtreeID == PredNum) {
1302 // If the predecessor's parent is invalid, this is a tree edge and the
1303 // current node is the parent.
1304 if (RootSet[PredNum].ParentNodeID == SchedDFSResult::InvalidSubtreeID)
1305 RootSet[PredNum].ParentNodeID = SU->NodeNum;
1306 }
1307 else if (RootSet.count(PredNum)) {
1308 // The predecessor is not a root, but is still in the root set. This
1309 // must be the new parent that it was just joined to. Note that
1310 // RootSet[PredNum].ParentNodeID may either be invalid or may still be
1311 // set to the original parent.
1312 RData.SubInstrCount += RootSet[PredNum].SubInstrCount;
1313 RootSet.erase(PredNum);
1314 }
1315 }
1316 RootSet[SU->NodeNum] = RData;
1317 }
1319 /// Called once for each tree edge after calling visitPostOrderNode on the
1320 /// predecessor. Increment the parent node's instruction count and
1321 /// preemptively join this subtree to its parent's if it is small enough.
1322 void visitPostorderEdge(const SDep &PredDep, const SUnit *Succ) {
1323 R.DFSNodeData[Succ->NodeNum].InstrCount
1324 += R.DFSNodeData[PredDep.getSUnit()->NodeNum].InstrCount;
1325 joinPredSubtree(PredDep, Succ);
1326 }
1328 /// Add a connection for cross edges.
1329 void visitCrossEdge(const SDep &PredDep, const SUnit *Succ) {
1330 ConnectionPairs.push_back(std::make_pair(PredDep.getSUnit(), Succ));
1331 }
1333 /// Set each node's subtree ID to the representative ID and record connections
1334 /// between trees.
1335 void finalize() {
1336 SubtreeClasses.compress();
1337 R.DFSTreeData.resize(SubtreeClasses.getNumClasses());
1338 assert(SubtreeClasses.getNumClasses() == RootSet.size()
1339 && "number of roots should match trees");
1340 for (SparseSet<RootData>::const_iterator
1341 RI = RootSet.begin(), RE = RootSet.end(); RI != RE; ++RI) {
1342 unsigned TreeID = SubtreeClasses[RI->NodeID];
1343 if (RI->ParentNodeID != SchedDFSResult::InvalidSubtreeID)
1344 R.DFSTreeData[TreeID].ParentTreeID = SubtreeClasses[RI->ParentNodeID];
1345 R.DFSTreeData[TreeID].SubInstrCount = RI->SubInstrCount;
1346 // Note that SubInstrCount may be greater than InstrCount if we joined
1347 // subtrees across a cross edge. InstrCount will be attributed to the
1348 // original parent, while SubInstrCount will be attributed to the joined
1349 // parent.
1350 }
1351 R.SubtreeConnections.resize(SubtreeClasses.getNumClasses());
1352 R.SubtreeConnectLevels.resize(SubtreeClasses.getNumClasses());
1353 DEBUG(dbgs() << R.getNumSubtrees() << " subtrees:\n");
1354 for (unsigned Idx = 0, End = R.DFSNodeData.size(); Idx != End; ++Idx) {
1355 R.DFSNodeData[Idx].SubtreeID = SubtreeClasses[Idx];
1356 DEBUG(dbgs() << " SU(" << Idx << ") in tree "
1357 << R.DFSNodeData[Idx].SubtreeID << '\n');
1358 }
1359 for (std::vector<std::pair<const SUnit*, const SUnit*> >::const_iterator
1360 I = ConnectionPairs.begin(), E = ConnectionPairs.end();
1361 I != E; ++I) {
1362 unsigned PredTree = SubtreeClasses[I->first->NodeNum];
1363 unsigned SuccTree = SubtreeClasses[I->second->NodeNum];
1364 if (PredTree == SuccTree)
1365 continue;
1366 unsigned Depth = I->first->getDepth();
1367 addConnection(PredTree, SuccTree, Depth);
1368 addConnection(SuccTree, PredTree, Depth);
1369 }
1370 }
1372 protected:
1373 /// Join the predecessor subtree with the successor that is its DFS
1374 /// parent. Apply some heuristics before joining.
1375 bool joinPredSubtree(const SDep &PredDep, const SUnit *Succ,
1376 bool CheckLimit = true) {
1377 assert(PredDep.getKind() == SDep::Data && "Subtrees are for data edges");
1379 // Check if the predecessor is already joined.
1380 const SUnit *PredSU = PredDep.getSUnit();
1381 unsigned PredNum = PredSU->NodeNum;
1382 if (R.DFSNodeData[PredNum].SubtreeID != PredNum)
1383 return false;
1385 // Four is the magic number of successors before a node is considered a
1386 // pinch point.
1387 unsigned NumDataSucs = 0;
1388 for (SUnit::const_succ_iterator SI = PredSU->Succs.begin(),
1389 SE = PredSU->Succs.end(); SI != SE; ++SI) {
1390 if (SI->getKind() == SDep::Data) {
1391 if (++NumDataSucs >= 4)
1392 return false;
1393 }
1394 }
1395 if (CheckLimit && R.DFSNodeData[PredNum].InstrCount > R.SubtreeLimit)
1396 return false;
1397 R.DFSNodeData[PredNum].SubtreeID = Succ->NodeNum;
1398 SubtreeClasses.join(Succ->NodeNum, PredNum);
1399 return true;
1400 }
1402 /// Called by finalize() to record a connection between trees.
1403 void addConnection(unsigned FromTree, unsigned ToTree, unsigned Depth) {
1404 if (!Depth)
1405 return;
1407 do {
1408 SmallVectorImpl<SchedDFSResult::Connection> &Connections =
1409 R.SubtreeConnections[FromTree];
1410 for (SmallVectorImpl<SchedDFSResult::Connection>::iterator
1411 I = Connections.begin(), E = Connections.end(); I != E; ++I) {
1412 if (I->TreeID == ToTree) {
1413 I->Level = std::max(I->Level, Depth);
1414 return;
1415 }
1416 }
1417 Connections.push_back(SchedDFSResult::Connection(ToTree, Depth));
1418 FromTree = R.DFSTreeData[FromTree].ParentTreeID;
1419 } while (FromTree != SchedDFSResult::InvalidSubtreeID);
1420 }
1421 };
1422 } // namespace llvm
1424 namespace {
1425 /// \brief Manage the stack used by a reverse depth-first search over the DAG.
1426 class SchedDAGReverseDFS {
1427 std::vector<std::pair<const SUnit*, SUnit::const_pred_iterator> > DFSStack;
1428 public:
1429 bool isComplete() const { return DFSStack.empty(); }
1431 void follow(const SUnit *SU) {
1432 DFSStack.push_back(std::make_pair(SU, SU->Preds.begin()));
1433 }
1434 void advance() { ++DFSStack.back().second; }
1436 const SDep *backtrack() {
1437 DFSStack.pop_back();
1438 return DFSStack.empty() ? nullptr : std::prev(DFSStack.back().second);
1439 }
1441 const SUnit *getCurr() const { return DFSStack.back().first; }
1443 SUnit::const_pred_iterator getPred() const { return DFSStack.back().second; }
1445 SUnit::const_pred_iterator getPredEnd() const {
1446 return getCurr()->Preds.end();
1447 }
1448 };
1449 } // anonymous
1451 static bool hasDataSucc(const SUnit *SU) {
1452 for (SUnit::const_succ_iterator
1453 SI = SU->Succs.begin(), SE = SU->Succs.end(); SI != SE; ++SI) {
1454 if (SI->getKind() == SDep::Data && !SI->getSUnit()->isBoundaryNode())
1455 return true;
1456 }
1457 return false;
1458 }
1460 /// Compute an ILP metric for all nodes in the subDAG reachable via depth-first
1461 /// search from this root.
1462 void SchedDFSResult::compute(ArrayRef<SUnit> SUnits) {
1463 if (!IsBottomUp)
1464 llvm_unreachable("Top-down ILP metric is unimplemnted");
1466 SchedDFSImpl Impl(*this);
1467 for (ArrayRef<SUnit>::const_iterator
1468 SI = SUnits.begin(), SE = SUnits.end(); SI != SE; ++SI) {
1469 const SUnit *SU = &*SI;
1470 if (Impl.isVisited(SU) || hasDataSucc(SU))
1471 continue;
1473 SchedDAGReverseDFS DFS;
1474 Impl.visitPreorder(SU);
1475 DFS.follow(SU);
1476 for (;;) {
1477 // Traverse the leftmost path as far as possible.
1478 while (DFS.getPred() != DFS.getPredEnd()) {
1479 const SDep &PredDep = *DFS.getPred();
1480 DFS.advance();
1481 // Ignore non-data edges.
1482 if (PredDep.getKind() != SDep::Data
1483 || PredDep.getSUnit()->isBoundaryNode()) {
1484 continue;
1485 }
1486 // An already visited edge is a cross edge, assuming an acyclic DAG.
1487 if (Impl.isVisited(PredDep.getSUnit())) {
1488 Impl.visitCrossEdge(PredDep, DFS.getCurr());
1489 continue;
1490 }
1491 Impl.visitPreorder(PredDep.getSUnit());
1492 DFS.follow(PredDep.getSUnit());
1493 }
1494 // Visit the top of the stack in postorder and backtrack.
1495 const SUnit *Child = DFS.getCurr();
1496 const SDep *PredDep = DFS.backtrack();
1497 Impl.visitPostorderNode(Child);
1498 if (PredDep)
1499 Impl.visitPostorderEdge(*PredDep, DFS.getCurr());
1500 if (DFS.isComplete())
1501 break;
1502 }
1503 }
1504 Impl.finalize();
1505 }
1507 /// The root of the given SubtreeID was just scheduled. For all subtrees
1508 /// connected to this tree, record the depth of the connection so that the
1509 /// nearest connected subtrees can be prioritized.
1510 void SchedDFSResult::scheduleTree(unsigned SubtreeID) {
1511 for (SmallVectorImpl<Connection>::const_iterator
1512 I = SubtreeConnections[SubtreeID].begin(),
1513 E = SubtreeConnections[SubtreeID].end(); I != E; ++I) {
1514 SubtreeConnectLevels[I->TreeID] =
1515 std::max(SubtreeConnectLevels[I->TreeID], I->Level);
1516 DEBUG(dbgs() << " Tree: " << I->TreeID
1517 << " @" << SubtreeConnectLevels[I->TreeID] << '\n');
1518 }
1519 }
1521 LLVM_DUMP_METHOD
1522 void ILPValue::print(raw_ostream &OS) const {
1523 OS << InstrCount << " / " << Length << " = ";
1524 if (!Length)
1525 OS << "BADILP";
1526 else
1527 OS << format("%g", ((double)InstrCount / Length));
1528 }
1530 LLVM_DUMP_METHOD
1531 void ILPValue::dump() const {
1532 dbgs() << *this << '\n';
1533 }
1535 namespace llvm {
1537 LLVM_DUMP_METHOD
1538 raw_ostream &operator<<(raw_ostream &OS, const ILPValue &Val) {
1539 Val.print(OS);
1540 return OS;
1541 }
1543 } // namespace llvm