Revert "This reapplies r207130 with an additional testcase+and a missing check for"
[opencl/llvm.git] / lib / CodeGen / SelectionDAG / SDNodeDbgValue.h
1 //===-- llvm/CodeGen/SDNodeDbgValue.h - SelectionDAG dbg_value --*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file declares the SDDbgValue class.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_CODEGEN_SDNODEDBGVALUE_H
15 #define LLVM_CODEGEN_SDNODEDBGVALUE_H
17 #include "llvm/ADT/SmallVector.h"
18 #include "llvm/IR/DebugLoc.h"
19 #include "llvm/Support/DataTypes.h"
21 namespace llvm {
23 class MDNode;
24 class SDNode;
25 class Value;
27 /// SDDbgValue - Holds the information from a dbg_value node through SDISel.
28 /// We do not use SDValue here to avoid including its header.
30 class SDDbgValue {
31 public:
32   enum DbgValueKind {
33     SDNODE = 0,             // value is the result of an expression
34     CONST = 1,              // value is a constant
35     FRAMEIX = 2             // value is contents of a stack location
36   };
37 private:
38   enum DbgValueKind kind;
39   union {
40     struct {
41       SDNode *Node;         // valid for expressions
42       unsigned ResNo;       // valid for expressions
43     } s;
44     const Value *Const;     // valid for constants
45     unsigned FrameIx;       // valid for stack objects
46   } u;
47   MDNode *mdPtr;
48   uint64_t Offset;
49   DebugLoc DL;
50   unsigned Order;
51   bool Invalid;
52 public:
53   // Constructor for non-constants.
54   SDDbgValue(MDNode *mdP, SDNode *N, unsigned R, uint64_t off, DebugLoc dl,
55              unsigned O) : mdPtr(mdP), Offset(off), DL(dl), Order(O),
56                            Invalid(false) {
57     kind = SDNODE;
58     u.s.Node = N;
59     u.s.ResNo = R;
60   }
62   // Constructor for constants.
63   SDDbgValue(MDNode *mdP, const Value *C, uint64_t off, DebugLoc dl,
64              unsigned O) : 
65     mdPtr(mdP), Offset(off), DL(dl), Order(O), Invalid(false) {
66     kind = CONST;
67     u.Const = C;
68   }
70   // Constructor for frame indices.
71   SDDbgValue(MDNode *mdP, unsigned FI, uint64_t off, DebugLoc dl, unsigned O) : 
72     mdPtr(mdP), Offset(off), DL(dl), Order(O), Invalid(false) {
73     kind = FRAMEIX;
74     u.FrameIx = FI;
75   }
77   // Returns the kind.
78   DbgValueKind getKind() { return kind; }
80   // Returns the MDNode pointer.
81   MDNode *getMDPtr() { return mdPtr; }
83   // Returns the SDNode* for a register ref
84   SDNode *getSDNode() { assert (kind==SDNODE); return u.s.Node; }
86   // Returns the ResNo for a register ref
87   unsigned getResNo() { assert (kind==SDNODE); return u.s.ResNo; }
89   // Returns the Value* for a constant
90   const Value *getConst() { assert (kind==CONST); return u.Const; }
92   // Returns the FrameIx for a stack object
93   unsigned getFrameIx() { assert (kind==FRAMEIX); return u.FrameIx; }
95   // Returns the offset.
96   uint64_t getOffset() { return Offset; }
98   // Returns the DebugLoc.
99   DebugLoc getDebugLoc() { return DL; }
101   // Returns the SDNodeOrder.  This is the order of the preceding node in the
102   // input.
103   unsigned getOrder() { return Order; }
105   // setIsInvalidated / isInvalidated - Setter / getter of the "Invalidated"
106   // property. A SDDbgValue is invalid if the SDNode that produces the value is
107   // deleted.
108   void setIsInvalidated() { Invalid = true; }
109   bool isInvalidated() { return Invalid; }
110 };
112 } // end llvm namespace
114 #endif