c8bb3d8831c4ebb29434786f9726ecdccc9f412f
1 //===-- llvm/CodeGen/SDNodeDbgValue.h - SelectionDAG dbg_value --*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file declares the SDDbgValue class.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_LIB_CODEGEN_SELECTIONDAG_SDNODEDBGVALUE_H
15 #define LLVM_LIB_CODEGEN_SELECTIONDAG_SDNODEDBGVALUE_H
17 #include "llvm/ADT/SmallVector.h"
18 #include "llvm/IR/DebugLoc.h"
19 #include "llvm/Support/DataTypes.h"
21 namespace llvm {
23 class MDNode;
24 class SDNode;
25 class Value;
27 /// SDDbgValue - Holds the information from a dbg_value node through SDISel.
28 /// We do not use SDValue here to avoid including its header.
30 class SDDbgValue {
31 public:
32 enum DbgValueKind {
33 SDNODE = 0, // value is the result of an expression
34 CONST = 1, // value is a constant
35 FRAMEIX = 2 // value is contents of a stack location
36 };
37 private:
38 enum DbgValueKind kind;
39 union {
40 struct {
41 SDNode *Node; // valid for expressions
42 unsigned ResNo; // valid for expressions
43 } s;
44 const Value *Const; // valid for constants
45 unsigned FrameIx; // valid for stack objects
46 } u;
47 MDNode *Var;
48 MDNode *Expr;
49 bool IsIndirect;
50 uint64_t Offset;
51 DebugLoc DL;
52 unsigned Order;
53 bool Invalid;
54 public:
55 // Constructor for non-constants.
56 SDDbgValue(MDNode *Var, MDNode *Expr, SDNode *N, unsigned R, bool indir,
57 uint64_t off, DebugLoc dl, unsigned O)
58 : Var(Var), Expr(Expr), IsIndirect(indir), Offset(off), DL(dl), Order(O),
59 Invalid(false) {
60 kind = SDNODE;
61 u.s.Node = N;
62 u.s.ResNo = R;
63 }
65 // Constructor for constants.
66 SDDbgValue(MDNode *Var, MDNode *Expr, const Value *C, uint64_t off,
67 DebugLoc dl, unsigned O)
68 : Var(Var), Expr(Expr), IsIndirect(false), Offset(off), DL(dl), Order(O),
69 Invalid(false) {
70 kind = CONST;
71 u.Const = C;
72 }
74 // Constructor for frame indices.
75 SDDbgValue(MDNode *Var, MDNode *Expr, unsigned FI, uint64_t off, DebugLoc dl,
76 unsigned O)
77 : Var(Var), Expr(Expr), IsIndirect(false), Offset(off), DL(dl), Order(O),
78 Invalid(false) {
79 kind = FRAMEIX;
80 u.FrameIx = FI;
81 }
83 // Returns the kind.
84 DbgValueKind getKind() { return kind; }
86 // Returns the MDNode pointer for the variable.
87 MDNode *getVariable() { return Var; }
89 // Returns the MDNode pointer for the expression.
90 MDNode *getExpression() { return Expr; }
92 // Returns the SDNode* for a register ref
93 SDNode *getSDNode() { assert (kind==SDNODE); return u.s.Node; }
95 // Returns the ResNo for a register ref
96 unsigned getResNo() { assert (kind==SDNODE); return u.s.ResNo; }
98 // Returns the Value* for a constant
99 const Value *getConst() { assert (kind==CONST); return u.Const; }
101 // Returns the FrameIx for a stack object
102 unsigned getFrameIx() { assert (kind==FRAMEIX); return u.FrameIx; }
104 // Returns whether this is an indirect value.
105 bool isIndirect() { return IsIndirect; }
107 // Returns the offset.
108 uint64_t getOffset() { return Offset; }
110 // Returns the DebugLoc.
111 DebugLoc getDebugLoc() { return DL; }
113 // Returns the SDNodeOrder. This is the order of the preceding node in the
114 // input.
115 unsigned getOrder() { return Order; }
117 // setIsInvalidated / isInvalidated - Setter / getter of the "Invalidated"
118 // property. A SDDbgValue is invalid if the SDNode that produces the value is
119 // deleted.
120 void setIsInvalidated() { Invalid = true; }
121 bool isInvalidated() { return Invalid; }
122 };
124 } // end llvm namespace
126 #endif