Revert "This reapplies r207130 with an additional testcase+and a missing check for"
[opencl/llvm.git] / lib / CodeGen / SelectionDAG / SelectionDAGBuilder.h
1 //===-- SelectionDAGBuilder.h - Selection-DAG building --------*- C++ -*---===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This implements routines for translating from LLVM IR into SelectionDAG IR.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef SELECTIONDAGBUILDER_H
15 #define SELECTIONDAGBUILDER_H
17 #include "llvm/ADT/APInt.h"
18 #include "llvm/ADT/DenseMap.h"
19 #include "llvm/CodeGen/SelectionDAG.h"
20 #include "llvm/CodeGen/SelectionDAGNodes.h"
21 #include "llvm/IR/CallSite.h"
22 #include "llvm/IR/Constants.h"
23 #include "llvm/Support/ErrorHandling.h"
24 #include <vector>
26 namespace llvm {
28 class AddrSpaceCastInst;
29 class AliasAnalysis;
30 class AllocaInst;
31 class BasicBlock;
32 class BitCastInst;
33 class BranchInst;
34 class CallInst;
35 class DbgValueInst;
36 class ExtractElementInst;
37 class ExtractValueInst;
38 class FCmpInst;
39 class FPExtInst;
40 class FPToSIInst;
41 class FPToUIInst;
42 class FPTruncInst;
43 class Function;
44 class FunctionLoweringInfo;
45 class GetElementPtrInst;
46 class GCFunctionInfo;
47 class ICmpInst;
48 class IntToPtrInst;
49 class IndirectBrInst;
50 class InvokeInst;
51 class InsertElementInst;
52 class InsertValueInst;
53 class Instruction;
54 class LoadInst;
55 class MachineBasicBlock;
56 class MachineInstr;
57 class MachineRegisterInfo;
58 class MDNode;
59 class MVT;
60 class PHINode;
61 class PtrToIntInst;
62 class ReturnInst;
63 class SDDbgValue;
64 class SExtInst;
65 class SelectInst;
66 class ShuffleVectorInst;
67 class SIToFPInst;
68 class StoreInst;
69 class SwitchInst;
70 class DataLayout;
71 class TargetLibraryInfo;
72 class TargetLowering;
73 class TruncInst;
74 class UIToFPInst;
75 class UnreachableInst;
76 class VAArgInst;
77 class ZExtInst;
79 //===----------------------------------------------------------------------===//
80 /// SelectionDAGBuilder - This is the common target-independent lowering
81 /// implementation that is parameterized by a TargetLowering object.
82 ///
83 class SelectionDAGBuilder {
84   /// CurInst - The current instruction being visited
85   const Instruction *CurInst;
87   DenseMap<const Value*, SDValue> NodeMap;
89   /// UnusedArgNodeMap - Maps argument value for unused arguments. This is used
90   /// to preserve debug information for incoming arguments.
91   DenseMap<const Value*, SDValue> UnusedArgNodeMap;
93   /// DanglingDebugInfo - Helper type for DanglingDebugInfoMap.
94   class DanglingDebugInfo {
95     const DbgValueInst* DI;
96     DebugLoc dl;
97     unsigned SDNodeOrder;
98   public:
99     DanglingDebugInfo() : DI(nullptr), dl(DebugLoc()), SDNodeOrder(0) { }
100     DanglingDebugInfo(const DbgValueInst *di, DebugLoc DL, unsigned SDNO) :
101       DI(di), dl(DL), SDNodeOrder(SDNO) { }
102     const DbgValueInst* getDI() { return DI; }
103     DebugLoc getdl() { return dl; }
104     unsigned getSDNodeOrder() { return SDNodeOrder; }
105   };
107   /// DanglingDebugInfoMap - Keeps track of dbg_values for which we have not
108   /// yet seen the referent.  We defer handling these until we do see it.
109   DenseMap<const Value*, DanglingDebugInfo> DanglingDebugInfoMap;
111 public:
112   /// PendingLoads - Loads are not emitted to the program immediately.  We bunch
113   /// them up and then emit token factor nodes when possible.  This allows us to
114   /// get simple disambiguation between loads without worrying about alias
115   /// analysis.
116   SmallVector<SDValue, 8> PendingLoads;
117 private:
119   /// PendingExports - CopyToReg nodes that copy values to virtual registers
120   /// for export to other blocks need to be emitted before any terminator
121   /// instruction, but they have no other ordering requirements. We bunch them
122   /// up and the emit a single tokenfactor for them just before terminator
123   /// instructions.
124   SmallVector<SDValue, 8> PendingExports;
126   /// SDNodeOrder - A unique monotonically increasing number used to order the
127   /// SDNodes we create.
128   unsigned SDNodeOrder;
130   /// Case - A struct to record the Value for a switch case, and the
131   /// case's target basic block.
132   struct Case {
133     const Constant *Low;
134     const Constant *High;
135     MachineBasicBlock* BB;
136     uint32_t ExtraWeight;
138     Case() : Low(nullptr), High(nullptr), BB(nullptr), ExtraWeight(0) { }
139     Case(const Constant *low, const Constant *high, MachineBasicBlock *bb,
140          uint32_t extraweight) : Low(low), High(high), BB(bb),
141          ExtraWeight(extraweight) { }
143     APInt size() const {
144       const APInt &rHigh = cast<ConstantInt>(High)->getValue();
145       const APInt &rLow  = cast<ConstantInt>(Low)->getValue();
146       return (rHigh - rLow + 1ULL);
147     }
148   };
150   struct CaseBits {
151     uint64_t Mask;
152     MachineBasicBlock* BB;
153     unsigned Bits;
154     uint32_t ExtraWeight;
156     CaseBits(uint64_t mask, MachineBasicBlock* bb, unsigned bits,
157              uint32_t Weight):
158       Mask(mask), BB(bb), Bits(bits), ExtraWeight(Weight) { }
159   };
161   typedef std::vector<Case>           CaseVector;
162   typedef std::vector<CaseBits>       CaseBitsVector;
163   typedef CaseVector::iterator        CaseItr;
164   typedef std::pair<CaseItr, CaseItr> CaseRange;
166   /// CaseRec - A struct with ctor used in lowering switches to a binary tree
167   /// of conditional branches.
168   struct CaseRec {
169     CaseRec(MachineBasicBlock *bb, const Constant *lt, const Constant *ge,
170             CaseRange r) :
171     CaseBB(bb), LT(lt), GE(ge), Range(r) {}
173     /// CaseBB - The MBB in which to emit the compare and branch
174     MachineBasicBlock *CaseBB;
175     /// LT, GE - If nonzero, we know the current case value must be less-than or
176     /// greater-than-or-equal-to these Constants.
177     const Constant *LT;
178     const Constant *GE;
179     /// Range - A pair of iterators representing the range of case values to be
180     /// processed at this point in the binary search tree.
181     CaseRange Range;
182   };
184   typedef std::vector<CaseRec> CaseRecVector;
186   /// The comparison function for sorting the switch case values in the vector.
187   /// WARNING: Case ranges should be disjoint!
188   struct CaseCmp {
189     bool operator()(const Case &C1, const Case &C2) {
190       assert(isa<ConstantInt>(C1.Low) && isa<ConstantInt>(C2.High));
191       const ConstantInt* CI1 = cast<const ConstantInt>(C1.Low);
192       const ConstantInt* CI2 = cast<const ConstantInt>(C2.High);
193       return CI1->getValue().slt(CI2->getValue());
194     }
195   };
197   struct CaseBitsCmp {
198     bool operator()(const CaseBits &C1, const CaseBits &C2) {
199       return C1.Bits > C2.Bits;
200     }
201   };
203   size_t Clusterify(CaseVector &Cases, const SwitchInst &SI);
205   /// CaseBlock - This structure is used to communicate between
206   /// SelectionDAGBuilder and SDISel for the code generation of additional basic
207   /// blocks needed by multi-case switch statements.
208   struct CaseBlock {
209     CaseBlock(ISD::CondCode cc, const Value *cmplhs, const Value *cmprhs,
210               const Value *cmpmiddle,
211               MachineBasicBlock *truebb, MachineBasicBlock *falsebb,
212               MachineBasicBlock *me,
213               uint32_t trueweight = 0, uint32_t falseweight = 0)
214       : CC(cc), CmpLHS(cmplhs), CmpMHS(cmpmiddle), CmpRHS(cmprhs),
215         TrueBB(truebb), FalseBB(falsebb), ThisBB(me),
216         TrueWeight(trueweight), FalseWeight(falseweight) { }
218     // CC - the condition code to use for the case block's setcc node
219     ISD::CondCode CC;
221     // CmpLHS/CmpRHS/CmpMHS - The LHS/MHS/RHS of the comparison to emit.
222     // Emit by default LHS op RHS. MHS is used for range comparisons:
223     // If MHS is not null: (LHS <= MHS) and (MHS <= RHS).
224     const Value *CmpLHS, *CmpMHS, *CmpRHS;
226     // TrueBB/FalseBB - the block to branch to if the setcc is true/false.
227     MachineBasicBlock *TrueBB, *FalseBB;
229     // ThisBB - the block into which to emit the code for the setcc and branches
230     MachineBasicBlock *ThisBB;
232     // TrueWeight/FalseWeight - branch weights.
233     uint32_t TrueWeight, FalseWeight;
234   };
236   struct JumpTable {
237     JumpTable(unsigned R, unsigned J, MachineBasicBlock *M,
238               MachineBasicBlock *D): Reg(R), JTI(J), MBB(M), Default(D) {}
240     /// Reg - the virtual register containing the index of the jump table entry
241     //. to jump to.
242     unsigned Reg;
243     /// JTI - the JumpTableIndex for this jump table in the function.
244     unsigned JTI;
245     /// MBB - the MBB into which to emit the code for the indirect jump.
246     MachineBasicBlock *MBB;
247     /// Default - the MBB of the default bb, which is a successor of the range
248     /// check MBB.  This is when updating PHI nodes in successors.
249     MachineBasicBlock *Default;
250   };
251   struct JumpTableHeader {
252     JumpTableHeader(APInt F, APInt L, const Value *SV, MachineBasicBlock *H,
253                     bool E = false):
254       First(F), Last(L), SValue(SV), HeaderBB(H), Emitted(E) {}
255     APInt First;
256     APInt Last;
257     const Value *SValue;
258     MachineBasicBlock *HeaderBB;
259     bool Emitted;
260   };
261   typedef std::pair<JumpTableHeader, JumpTable> JumpTableBlock;
263   struct BitTestCase {
264     BitTestCase(uint64_t M, MachineBasicBlock* T, MachineBasicBlock* Tr,
265                 uint32_t Weight):
266       Mask(M), ThisBB(T), TargetBB(Tr), ExtraWeight(Weight) { }
267     uint64_t Mask;
268     MachineBasicBlock *ThisBB;
269     MachineBasicBlock *TargetBB;
270     uint32_t ExtraWeight;
271   };
273   typedef SmallVector<BitTestCase, 3> BitTestInfo;
275   struct BitTestBlock {
276     BitTestBlock(APInt F, APInt R, const Value* SV,
277                  unsigned Rg, MVT RgVT, bool E,
278                  MachineBasicBlock* P, MachineBasicBlock* D,
279                  const BitTestInfo& C):
280       First(F), Range(R), SValue(SV), Reg(Rg), RegVT(RgVT), Emitted(E),
281       Parent(P), Default(D), Cases(C) { }
282     APInt First;
283     APInt Range;
284     const Value *SValue;
285     unsigned Reg;
286     MVT RegVT;
287     bool Emitted;
288     MachineBasicBlock *Parent;
289     MachineBasicBlock *Default;
290     BitTestInfo Cases;
291   };
293   /// A class which encapsulates all of the information needed to generate a
294   /// stack protector check and signals to isel via its state being initialized
295   /// that a stack protector needs to be generated.
296   ///
297   /// *NOTE* The following is a high level documentation of SelectionDAG Stack
298   /// Protector Generation. The reason that it is placed here is for a lack of
299   /// other good places to stick it.
300   ///
301   /// High Level Overview of SelectionDAG Stack Protector Generation:
302   ///
303   /// Previously, generation of stack protectors was done exclusively in the
304   /// pre-SelectionDAG Codegen LLVM IR Pass "Stack Protector". This necessitated
305   /// splitting basic blocks at the IR level to create the success/failure basic
306   /// blocks in the tail of the basic block in question. As a result of this,
307   /// calls that would have qualified for the sibling call optimization were no
308   /// longer eligible for optimization since said calls were no longer right in
309   /// the "tail position" (i.e. the immediate predecessor of a ReturnInst
310   /// instruction).
311   ///
312   /// Then it was noticed that since the sibling call optimization causes the
313   /// callee to reuse the caller's stack, if we could delay the generation of
314   /// the stack protector check until later in CodeGen after the sibling call
315   /// decision was made, we get both the tail call optimization and the stack
316   /// protector check!
317   ///
318   /// A few goals in solving this problem were:
319   ///
320   ///   1. Preserve the architecture independence of stack protector generation.
321   ///
322   ///   2. Preserve the normal IR level stack protector check for platforms like
323   ///      OpenBSD for which we support platform specific stack protector
324   ///      generation.
325   ///
326   /// The main problem that guided the present solution is that one can not
327   /// solve this problem in an architecture independent manner at the IR level
328   /// only. This is because:
329   ///
330   ///   1. The decision on whether or not to perform a sibling call on certain
331   ///      platforms (for instance i386) requires lower level information
332   ///      related to available registers that can not be known at the IR level.
333   ///
334   ///   2. Even if the previous point were not true, the decision on whether to
335   ///      perform a tail call is done in LowerCallTo in SelectionDAG which
336   ///      occurs after the Stack Protector Pass. As a result, one would need to
337   ///      put the relevant callinst into the stack protector check success
338   ///      basic block (where the return inst is placed) and then move it back
339   ///      later at SelectionDAG/MI time before the stack protector check if the
340   ///      tail call optimization failed. The MI level option was nixed
341   ///      immediately since it would require platform specific pattern
342   ///      matching. The SelectionDAG level option was nixed because
343   ///      SelectionDAG only processes one IR level basic block at a time
344   ///      implying one could not create a DAG Combine to move the callinst.
345   ///
346   /// To get around this problem a few things were realized:
347   ///
348   ///   1. While one can not handle multiple IR level basic blocks at the
349   ///      SelectionDAG Level, one can generate multiple machine basic blocks
350   ///      for one IR level basic block. This is how we handle bit tests and
351   ///      switches.
352   ///
353   ///   2. At the MI level, tail calls are represented via a special return
354   ///      MIInst called "tcreturn". Thus if we know the basic block in which we
355   ///      wish to insert the stack protector check, we get the correct behavior
356   ///      by always inserting the stack protector check right before the return
357   ///      statement. This is a "magical transformation" since no matter where
358   ///      the stack protector check intrinsic is, we always insert the stack
359   ///      protector check code at the end of the BB.
360   ///
361   /// Given the aforementioned constraints, the following solution was devised:
362   ///
363   ///   1. On platforms that do not support SelectionDAG stack protector check
364   ///      generation, allow for the normal IR level stack protector check
365   ///      generation to continue.
366   ///
367   ///   2. On platforms that do support SelectionDAG stack protector check
368   ///      generation:
369   ///
370   ///     a. Use the IR level stack protector pass to decide if a stack
371   ///        protector is required/which BB we insert the stack protector check
372   ///        in by reusing the logic already therein. If we wish to generate a
373   ///        stack protector check in a basic block, we place a special IR
374   ///        intrinsic called llvm.stackprotectorcheck right before the BB's
375   ///        returninst or if there is a callinst that could potentially be
376   ///        sibling call optimized, before the call inst.
377   ///
378   ///     b. Then when a BB with said intrinsic is processed, we codegen the BB
379   ///        normally via SelectBasicBlock. In said process, when we visit the
380   ///        stack protector check, we do not actually emit anything into the
381   ///        BB. Instead, we just initialize the stack protector descriptor
382   ///        class (which involves stashing information/creating the success
383   ///        mbbb and the failure mbb if we have not created one for this
384   ///        function yet) and export the guard variable that we are going to
385   ///        compare.
386   ///
387   ///     c. After we finish selecting the basic block, in FinishBasicBlock if
388   ///        the StackProtectorDescriptor attached to the SelectionDAGBuilder is
389   ///        initialized, we first find a splice point in the parent basic block
390   ///        before the terminator and then splice the terminator of said basic
391   ///        block into the success basic block. Then we code-gen a new tail for
392   ///        the parent basic block consisting of the two loads, the comparison,
393   ///        and finally two branches to the success/failure basic blocks. We
394   ///        conclude by code-gening the failure basic block if we have not
395   ///        code-gened it already (all stack protector checks we generate in
396   ///        the same function, use the same failure basic block).
397   class StackProtectorDescriptor {
398   public:
399     StackProtectorDescriptor() : ParentMBB(nullptr), SuccessMBB(nullptr),
400                                  FailureMBB(nullptr), Guard(nullptr) { }
401     ~StackProtectorDescriptor() { }
403     /// Returns true if all fields of the stack protector descriptor are
404     /// initialized implying that we should/are ready to emit a stack protector.
405     bool shouldEmitStackProtector() const {
406       return ParentMBB && SuccessMBB && FailureMBB && Guard;
407     }
409     /// Initialize the stack protector descriptor structure for a new basic
410     /// block.
411     void initialize(const BasicBlock *BB,
412                     MachineBasicBlock *MBB,
413                     const CallInst &StackProtCheckCall) {
414       // Make sure we are not initialized yet.
415       assert(!shouldEmitStackProtector() && "Stack Protector Descriptor is "
416              "already initialized!");
417       ParentMBB = MBB;
418       SuccessMBB = AddSuccessorMBB(BB, MBB);
419       FailureMBB = AddSuccessorMBB(BB, MBB, FailureMBB);
420       if (!Guard)
421         Guard = StackProtCheckCall.getArgOperand(0);
422     }
424     /// Reset state that changes when we handle different basic blocks.
425     ///
426     /// This currently includes:
427     ///
428     /// 1. The specific basic block we are generating a
429     /// stack protector for (ParentMBB).
430     ///
431     /// 2. The successor machine basic block that will contain the tail of
432     /// parent mbb after we create the stack protector check (SuccessMBB). This
433     /// BB is visited only on stack protector check success.
434     void resetPerBBState() {
435       ParentMBB = nullptr;
436       SuccessMBB = nullptr;
437     }
439     /// Reset state that only changes when we switch functions.
440     ///
441     /// This currently includes:
442     ///
443     /// 1. FailureMBB since we reuse the failure code path for all stack
444     /// protector checks created in an individual function.
445     ///
446     /// 2.The guard variable since the guard variable we are checking against is
447     /// always the same.
448     void resetPerFunctionState() {
449       FailureMBB = nullptr;
450       Guard = nullptr;
451     }
453     MachineBasicBlock *getParentMBB() { return ParentMBB; }
454     MachineBasicBlock *getSuccessMBB() { return SuccessMBB; }
455     MachineBasicBlock *getFailureMBB() { return FailureMBB; }
456     const Value *getGuard() { return Guard; }
458   private:
459     /// The basic block for which we are generating the stack protector.
460     ///
461     /// As a result of stack protector generation, we will splice the
462     /// terminators of this basic block into the successor mbb SuccessMBB and
463     /// replace it with a compare/branch to the successor mbbs
464     /// SuccessMBB/FailureMBB depending on whether or not the stack protector
465     /// was violated.
466     MachineBasicBlock *ParentMBB;
468     /// A basic block visited on stack protector check success that contains the
469     /// terminators of ParentMBB.
470     MachineBasicBlock *SuccessMBB;
472     /// This basic block visited on stack protector check failure that will
473     /// contain a call to __stack_chk_fail().
474     MachineBasicBlock *FailureMBB;
476     /// The guard variable which we will compare against the stored value in the
477     /// stack protector stack slot.
478     const Value *Guard;
480     /// Add a successor machine basic block to ParentMBB. If the successor mbb
481     /// has not been created yet (i.e. if SuccMBB = 0), then the machine basic
482     /// block will be created.
483     MachineBasicBlock *AddSuccessorMBB(const BasicBlock *BB,
484                                        MachineBasicBlock *ParentMBB,
485                                        MachineBasicBlock *SuccMBB = nullptr);
486   };
488 private:
489   const TargetMachine &TM;
490 public:
491   /// Lowest valid SDNodeOrder. The special case 0 is reserved for scheduling
492   /// nodes without a corresponding SDNode.
493   static const unsigned LowestSDNodeOrder = 1;
495   SelectionDAG &DAG;
496   const DataLayout *DL;
497   AliasAnalysis *AA;
498   const TargetLibraryInfo *LibInfo;
500   /// SwitchCases - Vector of CaseBlock structures used to communicate
501   /// SwitchInst code generation information.
502   std::vector<CaseBlock> SwitchCases;
503   /// JTCases - Vector of JumpTable structures used to communicate
504   /// SwitchInst code generation information.
505   std::vector<JumpTableBlock> JTCases;
506   /// BitTestCases - Vector of BitTestBlock structures used to communicate
507   /// SwitchInst code generation information.
508   std::vector<BitTestBlock> BitTestCases;
509   /// A StackProtectorDescriptor structure used to communicate stack protector
510   /// information in between SelectBasicBlock and FinishBasicBlock.
511   StackProtectorDescriptor SPDescriptor;
513   // Emit PHI-node-operand constants only once even if used by multiple
514   // PHI nodes.
515   DenseMap<const Constant *, unsigned> ConstantsOut;
517   /// FuncInfo - Information about the function as a whole.
518   ///
519   FunctionLoweringInfo &FuncInfo;
521   /// OptLevel - What optimization level we're generating code for.
522   ///
523   CodeGenOpt::Level OptLevel;
525   /// GFI - Garbage collection metadata for the function.
526   GCFunctionInfo *GFI;
528   /// LPadToCallSiteMap - Map a landing pad to the call site indexes.
529   DenseMap<MachineBasicBlock*, SmallVector<unsigned, 4> > LPadToCallSiteMap;
531   /// HasTailCall - This is set to true if a call in the current
532   /// block has been translated as a tail call. In this case,
533   /// no subsequent DAG nodes should be created.
534   ///
535   bool HasTailCall;
537   LLVMContext *Context;
539   SelectionDAGBuilder(SelectionDAG &dag, FunctionLoweringInfo &funcinfo,
540                       CodeGenOpt::Level ol)
541     : CurInst(nullptr), SDNodeOrder(LowestSDNodeOrder), TM(dag.getTarget()),
542       DAG(dag), FuncInfo(funcinfo), OptLevel(ol),
543       HasTailCall(false) {
544   }
546   void init(GCFunctionInfo *gfi, AliasAnalysis &aa,
547             const TargetLibraryInfo *li);
549   /// clear - Clear out the current SelectionDAG and the associated
550   /// state and prepare this SelectionDAGBuilder object to be used
551   /// for a new block. This doesn't clear out information about
552   /// additional blocks that are needed to complete switch lowering
553   /// or PHI node updating; that information is cleared out as it is
554   /// consumed.
555   void clear();
557   /// clearDanglingDebugInfo - Clear the dangling debug information
558   /// map. This function is separated from the clear so that debug
559   /// information that is dangling in a basic block can be properly
560   /// resolved in a different basic block. This allows the
561   /// SelectionDAG to resolve dangling debug information attached
562   /// to PHI nodes.
563   void clearDanglingDebugInfo();
565   /// getRoot - Return the current virtual root of the Selection DAG,
566   /// flushing any PendingLoad items. This must be done before emitting
567   /// a store or any other node that may need to be ordered after any
568   /// prior load instructions.
569   ///
570   SDValue getRoot();
572   /// getControlRoot - Similar to getRoot, but instead of flushing all the
573   /// PendingLoad items, flush all the PendingExports items. It is necessary
574   /// to do this before emitting a terminator instruction.
575   ///
576   SDValue getControlRoot();
578   SDLoc getCurSDLoc() const {
579     return SDLoc(CurInst, SDNodeOrder);
580   }
582   DebugLoc getCurDebugLoc() const {
583     return CurInst ? CurInst->getDebugLoc() : DebugLoc();
584   }
586   unsigned getSDNodeOrder() const { return SDNodeOrder; }
588   void CopyValueToVirtualRegister(const Value *V, unsigned Reg);
590   void visit(const Instruction &I);
592   void visit(unsigned Opcode, const User &I);
594   // resolveDanglingDebugInfo - if we saw an earlier dbg_value referring to V,
595   // generate the debug data structures now that we've seen its definition.
596   void resolveDanglingDebugInfo(const Value *V, SDValue Val);
597   SDValue getValue(const Value *V);
598   SDValue getNonRegisterValue(const Value *V);
599   SDValue getValueImpl(const Value *V);
601   void setValue(const Value *V, SDValue NewN) {
602     SDValue &N = NodeMap[V];
603     assert(!N.getNode() && "Already set a value for this node!");
604     N = NewN;
605   }
607   void setUnusedArgValue(const Value *V, SDValue NewN) {
608     SDValue &N = UnusedArgNodeMap[V];
609     assert(!N.getNode() && "Already set a value for this node!");
610     N = NewN;
611   }
613   void FindMergedConditions(const Value *Cond, MachineBasicBlock *TBB,
614                             MachineBasicBlock *FBB, MachineBasicBlock *CurBB,
615                             MachineBasicBlock *SwitchBB, unsigned Opc,
616                             uint32_t TW, uint32_t FW);
617   void EmitBranchForMergedCondition(const Value *Cond, MachineBasicBlock *TBB,
618                                     MachineBasicBlock *FBB,
619                                     MachineBasicBlock *CurBB,
620                                     MachineBasicBlock *SwitchBB,
621                                     uint32_t TW, uint32_t FW);
622   bool ShouldEmitAsBranches(const std::vector<CaseBlock> &Cases);
623   bool isExportableFromCurrentBlock(const Value *V, const BasicBlock *FromBB);
624   void CopyToExportRegsIfNeeded(const Value *V);
625   void ExportFromCurrentBlock(const Value *V);
626   void LowerCallTo(ImmutableCallSite CS, SDValue Callee, bool IsTailCall,
627                    MachineBasicBlock *LandingPad = nullptr);
629   std::pair<SDValue, SDValue> LowerCallOperands(const CallInst &CI,
630                                                 unsigned ArgIdx,
631                                                 unsigned NumArgs,
632                                                 SDValue Callee,
633                                                 bool useVoidTy = false);
635   /// UpdateSplitBlock - When an MBB was split during scheduling, update the
636   /// references that need to refer to the last resulting block.
637   void UpdateSplitBlock(MachineBasicBlock *First, MachineBasicBlock *Last);
639 private:
640   // Terminator instructions.
641   void visitRet(const ReturnInst &I);
642   void visitBr(const BranchInst &I);
643   void visitSwitch(const SwitchInst &I);
644   void visitIndirectBr(const IndirectBrInst &I);
645   void visitUnreachable(const UnreachableInst &I);
647   // Helpers for visitSwitch
648   bool handleSmallSwitchRange(CaseRec& CR,
649                               CaseRecVector& WorkList,
650                               const Value* SV,
651                               MachineBasicBlock* Default,
652                               MachineBasicBlock *SwitchBB);
653   bool handleJTSwitchCase(CaseRec& CR,
654                           CaseRecVector& WorkList,
655                           const Value* SV,
656                           MachineBasicBlock* Default,
657                           MachineBasicBlock *SwitchBB);
658   bool handleBTSplitSwitchCase(CaseRec& CR,
659                                CaseRecVector& WorkList,
660                                const Value* SV,
661                                MachineBasicBlock* Default,
662                                MachineBasicBlock *SwitchBB);
663   bool handleBitTestsSwitchCase(CaseRec& CR,
664                                 CaseRecVector& WorkList,
665                                 const Value* SV,
666                                 MachineBasicBlock* Default,
667                                 MachineBasicBlock *SwitchBB);
669   uint32_t getEdgeWeight(const MachineBasicBlock *Src,
670                          const MachineBasicBlock *Dst) const;
671   void addSuccessorWithWeight(MachineBasicBlock *Src, MachineBasicBlock *Dst,
672                               uint32_t Weight = 0);
673 public:
674   void visitSwitchCase(CaseBlock &CB,
675                        MachineBasicBlock *SwitchBB);
676   void visitSPDescriptorParent(StackProtectorDescriptor &SPD,
677                                MachineBasicBlock *ParentBB);
678   void visitSPDescriptorFailure(StackProtectorDescriptor &SPD);
679   void visitBitTestHeader(BitTestBlock &B, MachineBasicBlock *SwitchBB);
680   void visitBitTestCase(BitTestBlock &BB,
681                         MachineBasicBlock* NextMBB,
682                         uint32_t BranchWeightToNext,
683                         unsigned Reg,
684                         BitTestCase &B,
685                         MachineBasicBlock *SwitchBB);
686   void visitJumpTable(JumpTable &JT);
687   void visitJumpTableHeader(JumpTable &JT, JumpTableHeader &JTH,
688                             MachineBasicBlock *SwitchBB);
690 private:
691   // These all get lowered before this pass.
692   void visitInvoke(const InvokeInst &I);
693   void visitResume(const ResumeInst &I);
695   void visitBinary(const User &I, unsigned OpCode);
696   void visitShift(const User &I, unsigned Opcode);
697   void visitAdd(const User &I)  { visitBinary(I, ISD::ADD); }
698   void visitFAdd(const User &I) { visitBinary(I, ISD::FADD); }
699   void visitSub(const User &I)  { visitBinary(I, ISD::SUB); }
700   void visitFSub(const User &I);
701   void visitMul(const User &I)  { visitBinary(I, ISD::MUL); }
702   void visitFMul(const User &I) { visitBinary(I, ISD::FMUL); }
703   void visitURem(const User &I) { visitBinary(I, ISD::UREM); }
704   void visitSRem(const User &I) { visitBinary(I, ISD::SREM); }
705   void visitFRem(const User &I) { visitBinary(I, ISD::FREM); }
706   void visitUDiv(const User &I) { visitBinary(I, ISD::UDIV); }
707   void visitSDiv(const User &I);
708   void visitFDiv(const User &I) { visitBinary(I, ISD::FDIV); }
709   void visitAnd (const User &I) { visitBinary(I, ISD::AND); }
710   void visitOr  (const User &I) { visitBinary(I, ISD::OR); }
711   void visitXor (const User &I) { visitBinary(I, ISD::XOR); }
712   void visitShl (const User &I) { visitShift(I, ISD::SHL); }
713   void visitLShr(const User &I) { visitShift(I, ISD::SRL); }
714   void visitAShr(const User &I) { visitShift(I, ISD::SRA); }
715   void visitICmp(const User &I);
716   void visitFCmp(const User &I);
717   // Visit the conversion instructions
718   void visitTrunc(const User &I);
719   void visitZExt(const User &I);
720   void visitSExt(const User &I);
721   void visitFPTrunc(const User &I);
722   void visitFPExt(const User &I);
723   void visitFPToUI(const User &I);
724   void visitFPToSI(const User &I);
725   void visitUIToFP(const User &I);
726   void visitSIToFP(const User &I);
727   void visitPtrToInt(const User &I);
728   void visitIntToPtr(const User &I);
729   void visitBitCast(const User &I);
730   void visitAddrSpaceCast(const User &I);
732   void visitExtractElement(const User &I);
733   void visitInsertElement(const User &I);
734   void visitShuffleVector(const User &I);
736   void visitExtractValue(const ExtractValueInst &I);
737   void visitInsertValue(const InsertValueInst &I);
738   void visitLandingPad(const LandingPadInst &I);
740   void visitGetElementPtr(const User &I);
741   void visitSelect(const User &I);
743   void visitAlloca(const AllocaInst &I);
744   void visitLoad(const LoadInst &I);
745   void visitStore(const StoreInst &I);
746   void visitAtomicCmpXchg(const AtomicCmpXchgInst &I);
747   void visitAtomicRMW(const AtomicRMWInst &I);
748   void visitFence(const FenceInst &I);
749   void visitPHI(const PHINode &I);
750   void visitCall(const CallInst &I);
751   bool visitMemCmpCall(const CallInst &I);
752   bool visitMemChrCall(const CallInst &I);
753   bool visitStrCpyCall(const CallInst &I, bool isStpcpy);
754   bool visitStrCmpCall(const CallInst &I);
755   bool visitStrLenCall(const CallInst &I);
756   bool visitStrNLenCall(const CallInst &I);
757   bool visitUnaryFloatCall(const CallInst &I, unsigned Opcode);
758   void visitAtomicLoad(const LoadInst &I);
759   void visitAtomicStore(const StoreInst &I);
761   void visitInlineAsm(ImmutableCallSite CS);
762   const char *visitIntrinsicCall(const CallInst &I, unsigned Intrinsic);
763   void visitTargetIntrinsic(const CallInst &I, unsigned Intrinsic);
765   void visitVAStart(const CallInst &I);
766   void visitVAArg(const VAArgInst &I);
767   void visitVAEnd(const CallInst &I);
768   void visitVACopy(const CallInst &I);
769   void visitStackmap(const CallInst &I);
770   void visitPatchpoint(const CallInst &I);
772   void visitUserOp1(const Instruction &I) {
773     llvm_unreachable("UserOp1 should not exist at instruction selection time!");
774   }
775   void visitUserOp2(const Instruction &I) {
776     llvm_unreachable("UserOp2 should not exist at instruction selection time!");
777   }
779   void processIntegerCallValue(const Instruction &I,
780                                SDValue Value, bool IsSigned);
782   void HandlePHINodesInSuccessorBlocks(const BasicBlock *LLVMBB);
784   /// EmitFuncArgumentDbgValue - If V is an function argument then create
785   /// corresponding DBG_VALUE machine instruction for it now. At the end of
786   /// instruction selection, they will be inserted to the entry BB.
787   bool EmitFuncArgumentDbgValue(const Value *V, MDNode *Variable,
788                                 int64_t Offset, const SDValue &N);
789 };
791 } // end namespace llvm
793 #endif