1 //===-- SelectionDAGBuilder.h - Selection-DAG building --------------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This implements routines for translating from LLVM IR into SelectionDAG IR.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef SELECTIONDAGBUILDER_H
15 #define SELECTIONDAGBUILDER_H
17 #include "llvm/ADT/APInt.h"
18 #include "llvm/ADT/DenseMap.h"
19 #include "llvm/CodeGen/SelectionDAG.h"
20 #include "llvm/CodeGen/SelectionDAGNodes.h"
21 #include "llvm/CodeGen/ValueTypes.h"
22 #include "llvm/Constants.h"
23 #include "llvm/Support/CallSite.h"
24 #include "llvm/Support/ErrorHandling.h"
25 #include <vector>
27 namespace llvm {
29 class AliasAnalysis;
30 class AllocaInst;
31 class BasicBlock;
32 class BitCastInst;
33 class BranchInst;
34 class CallInst;
35 class DbgValueInst;
36 class ExtractElementInst;
37 class ExtractValueInst;
38 class FCmpInst;
39 class FPExtInst;
40 class FPToSIInst;
41 class FPToUIInst;
42 class FPTruncInst;
43 class Function;
44 class FunctionLoweringInfo;
45 class GetElementPtrInst;
46 class GCFunctionInfo;
47 class ICmpInst;
48 class IntToPtrInst;
49 class IndirectBrInst;
50 class InvokeInst;
51 class InsertElementInst;
52 class InsertValueInst;
53 class Instruction;
54 class LoadInst;
55 class MachineBasicBlock;
56 class MachineInstr;
57 class MachineRegisterInfo;
58 class MDNode;
59 class PHINode;
60 class PtrToIntInst;
61 class ReturnInst;
62 class SDDbgValue;
63 class SExtInst;
64 class SelectInst;
65 class ShuffleVectorInst;
66 class SIToFPInst;
67 class StoreInst;
68 class SwitchInst;
69 class DataLayout;
70 class TargetLibraryInfo;
71 class TargetLowering;
72 class TruncInst;
73 class UIToFPInst;
74 class UnreachableInst;
75 class VAArgInst;
76 class ZExtInst;
78 //===----------------------------------------------------------------------===//
79 /// SelectionDAGBuilder - This is the common target-independent lowering
80 /// implementation that is parameterized by a TargetLowering object.
81 ///
82 class SelectionDAGBuilder {
83 /// CurDebugLoc - current file + line number. Changes as we build the DAG.
84 DebugLoc CurDebugLoc;
86 DenseMap<const Value*, SDValue> NodeMap;
88 /// UnusedArgNodeMap - Maps argument value for unused arguments. This is used
89 /// to preserve debug information for incoming arguments.
90 DenseMap<const Value*, SDValue> UnusedArgNodeMap;
92 /// DanglingDebugInfo - Helper type for DanglingDebugInfoMap.
93 class DanglingDebugInfo {
94 const DbgValueInst* DI;
95 DebugLoc dl;
96 unsigned SDNodeOrder;
97 public:
98 DanglingDebugInfo() : DI(0), dl(DebugLoc()), SDNodeOrder(0) { }
99 DanglingDebugInfo(const DbgValueInst *di, DebugLoc DL, unsigned SDNO) :
100 DI(di), dl(DL), SDNodeOrder(SDNO) { }
101 const DbgValueInst* getDI() { return DI; }
102 DebugLoc getdl() { return dl; }
103 unsigned getSDNodeOrder() { return SDNodeOrder; }
104 };
106 /// DanglingDebugInfoMap - Keeps track of dbg_values for which we have not
107 /// yet seen the referent. We defer handling these until we do see it.
108 DenseMap<const Value*, DanglingDebugInfo> DanglingDebugInfoMap;
110 public:
111 /// PendingLoads - Loads are not emitted to the program immediately. We bunch
112 /// them up and then emit token factor nodes when possible. This allows us to
113 /// get simple disambiguation between loads without worrying about alias
114 /// analysis.
115 SmallVector<SDValue, 8> PendingLoads;
116 private:
118 /// PendingExports - CopyToReg nodes that copy values to virtual registers
119 /// for export to other blocks need to be emitted before any terminator
120 /// instruction, but they have no other ordering requirements. We bunch them
121 /// up and the emit a single tokenfactor for them just before terminator
122 /// instructions.
123 SmallVector<SDValue, 8> PendingExports;
125 /// SDNodeOrder - A unique monotonically increasing number used to order the
126 /// SDNodes we create.
127 unsigned SDNodeOrder;
129 /// Case - A struct to record the Value for a switch case, and the
130 /// case's target basic block.
131 struct Case {
132 const Constant *Low;
133 const Constant *High;
134 MachineBasicBlock* BB;
135 uint32_t ExtraWeight;
137 Case() : Low(0), High(0), BB(0), ExtraWeight(0) { }
138 Case(const Constant *low, const Constant *high, MachineBasicBlock *bb,
139 uint32_t extraweight) : Low(low), High(high), BB(bb),
140 ExtraWeight(extraweight) { }
142 APInt size() const {
143 const APInt &rHigh = cast<ConstantInt>(High)->getValue();
144 const APInt &rLow = cast<ConstantInt>(Low)->getValue();
145 return (rHigh - rLow + 1ULL);
146 }
147 };
149 struct CaseBits {
150 uint64_t Mask;
151 MachineBasicBlock* BB;
152 unsigned Bits;
153 uint32_t ExtraWeight;
155 CaseBits(uint64_t mask, MachineBasicBlock* bb, unsigned bits,
156 uint32_t Weight):
157 Mask(mask), BB(bb), Bits(bits), ExtraWeight(Weight) { }
158 };
160 typedef std::vector<Case> CaseVector;
161 typedef std::vector<CaseBits> CaseBitsVector;
162 typedef CaseVector::iterator CaseItr;
163 typedef std::pair<CaseItr, CaseItr> CaseRange;
165 /// CaseRec - A struct with ctor used in lowering switches to a binary tree
166 /// of conditional branches.
167 struct CaseRec {
168 CaseRec(MachineBasicBlock *bb, const Constant *lt, const Constant *ge,
169 CaseRange r) :
170 CaseBB(bb), LT(lt), GE(ge), Range(r) {}
172 /// CaseBB - The MBB in which to emit the compare and branch
173 MachineBasicBlock *CaseBB;
174 /// LT, GE - If nonzero, we know the current case value must be less-than or
175 /// greater-than-or-equal-to these Constants.
176 const Constant *LT;
177 const Constant *GE;
178 /// Range - A pair of iterators representing the range of case values to be
179 /// processed at this point in the binary search tree.
180 CaseRange Range;
181 };
183 typedef std::vector<CaseRec> CaseRecVector;
185 struct CaseBitsCmp {
186 bool operator()(const CaseBits &C1, const CaseBits &C2) {
187 return C1.Bits > C2.Bits;
188 }
189 };
191 size_t Clusterify(CaseVector &Cases, const SwitchInst &SI);
193 /// CaseBlock - This structure is used to communicate between
194 /// SelectionDAGBuilder and SDISel for the code generation of additional basic
195 /// blocks needed by multi-case switch statements.
196 struct CaseBlock {
197 CaseBlock(ISD::CondCode cc, const Value *cmplhs, const Value *cmprhs,
198 const Value *cmpmiddle,
199 MachineBasicBlock *truebb, MachineBasicBlock *falsebb,
200 MachineBasicBlock *me,
201 uint32_t trueweight = 0, uint32_t falseweight = 0)
202 : CC(cc), CmpLHS(cmplhs), CmpMHS(cmpmiddle), CmpRHS(cmprhs),
203 TrueBB(truebb), FalseBB(falsebb), ThisBB(me),
204 TrueWeight(trueweight), FalseWeight(falseweight) { }
206 // CC - the condition code to use for the case block's setcc node
207 ISD::CondCode CC;
209 // CmpLHS/CmpRHS/CmpMHS - The LHS/MHS/RHS of the comparison to emit.
210 // Emit by default LHS op RHS. MHS is used for range comparisons:
211 // If MHS is not null: (LHS <= MHS) and (MHS <= RHS).
212 const Value *CmpLHS, *CmpMHS, *CmpRHS;
214 // TrueBB/FalseBB - the block to branch to if the setcc is true/false.
215 MachineBasicBlock *TrueBB, *FalseBB;
217 // ThisBB - the block into which to emit the code for the setcc and branches
218 MachineBasicBlock *ThisBB;
220 // TrueWeight/FalseWeight - branch weights.
221 uint32_t TrueWeight, FalseWeight;
222 };
224 struct JumpTable {
225 JumpTable(unsigned R, unsigned J, MachineBasicBlock *M,
226 MachineBasicBlock *D): Reg(R), JTI(J), MBB(M), Default(D) {}
228 /// Reg - the virtual register containing the index of the jump table entry
229 //. to jump to.
230 unsigned Reg;
231 /// JTI - the JumpTableIndex for this jump table in the function.
232 unsigned JTI;
233 /// MBB - the MBB into which to emit the code for the indirect jump.
234 MachineBasicBlock *MBB;
235 /// Default - the MBB of the default bb, which is a successor of the range
236 /// check MBB. This is when updating PHI nodes in successors.
237 MachineBasicBlock *Default;
238 };
239 struct JumpTableHeader {
240 JumpTableHeader(APInt F, APInt L, const Value *SV, MachineBasicBlock *H,
241 bool E = false):
242 First(F), Last(L), SValue(SV), HeaderBB(H), Emitted(E) {}
243 APInt First;
244 APInt Last;
245 const Value *SValue;
246 MachineBasicBlock *HeaderBB;
247 bool Emitted;
248 };
249 typedef std::pair<JumpTableHeader, JumpTable> JumpTableBlock;
251 struct BitTestCase {
252 BitTestCase(uint64_t M, MachineBasicBlock* T, MachineBasicBlock* Tr,
253 uint32_t Weight):
254 Mask(M), ThisBB(T), TargetBB(Tr), ExtraWeight(Weight) { }
255 uint64_t Mask;
256 MachineBasicBlock *ThisBB;
257 MachineBasicBlock *TargetBB;
258 uint32_t ExtraWeight;
259 };
261 typedef SmallVector<BitTestCase, 3> BitTestInfo;
263 struct BitTestBlock {
264 BitTestBlock(APInt F, APInt R, const Value* SV,
265 unsigned Rg, EVT RgVT, bool E,
266 MachineBasicBlock* P, MachineBasicBlock* D,
267 const BitTestInfo& C):
268 First(F), Range(R), SValue(SV), Reg(Rg), RegVT(RgVT), Emitted(E),
269 Parent(P), Default(D), Cases(C) { }
270 APInt First;
271 APInt Range;
272 const Value *SValue;
273 unsigned Reg;
274 EVT RegVT;
275 bool Emitted;
276 MachineBasicBlock *Parent;
277 MachineBasicBlock *Default;
278 BitTestInfo Cases;
279 };
281 public:
282 // TLI - This is information that describes the available target features we
283 // need for lowering. This indicates when operations are unavailable,
284 // implemented with a libcall, etc.
285 const TargetMachine &TM;
286 const TargetLowering &TLI;
287 SelectionDAG &DAG;
288 const DataLayout *TD;
289 AliasAnalysis *AA;
290 const TargetLibraryInfo *LibInfo;
292 /// SwitchCases - Vector of CaseBlock structures used to communicate
293 /// SwitchInst code generation information.
294 std::vector<CaseBlock> SwitchCases;
295 /// JTCases - Vector of JumpTable structures used to communicate
296 /// SwitchInst code generation information.
297 std::vector<JumpTableBlock> JTCases;
298 /// BitTestCases - Vector of BitTestBlock structures used to communicate
299 /// SwitchInst code generation information.
300 std::vector<BitTestBlock> BitTestCases;
302 // Emit PHI-node-operand constants only once even if used by multiple
303 // PHI nodes.
304 DenseMap<const Constant *, unsigned> ConstantsOut;
306 /// FuncInfo - Information about the function as a whole.
307 ///
308 FunctionLoweringInfo &FuncInfo;
310 /// OptLevel - What optimization level we're generating code for.
311 ///
312 CodeGenOpt::Level OptLevel;
314 /// GFI - Garbage collection metadata for the function.
315 GCFunctionInfo *GFI;
317 /// LPadToCallSiteMap - Map a landing pad to the call site indexes.
318 DenseMap<MachineBasicBlock*, SmallVector<unsigned, 4> > LPadToCallSiteMap;
320 /// HasTailCall - This is set to true if a call in the current
321 /// block has been translated as a tail call. In this case,
322 /// no subsequent DAG nodes should be created.
323 ///
324 bool HasTailCall;
326 LLVMContext *Context;
328 SelectionDAGBuilder(SelectionDAG &dag, FunctionLoweringInfo &funcinfo,
329 CodeGenOpt::Level ol)
330 : SDNodeOrder(0), TM(dag.getTarget()), TLI(dag.getTargetLoweringInfo()),
331 DAG(dag), FuncInfo(funcinfo), OptLevel(ol),
332 HasTailCall(false) {
333 }
335 void init(GCFunctionInfo *gfi, AliasAnalysis &aa,
336 const TargetLibraryInfo *li);
338 /// clear - Clear out the current SelectionDAG and the associated
339 /// state and prepare this SelectionDAGBuilder object to be used
340 /// for a new block. This doesn't clear out information about
341 /// additional blocks that are needed to complete switch lowering
342 /// or PHI node updating; that information is cleared out as it is
343 /// consumed.
344 void clear();
346 /// clearDanglingDebugInfo - Clear the dangling debug information
347 /// map. This function is separated from the clear so that debug
348 /// information that is dangling in a basic block can be properly
349 /// resolved in a different basic block. This allows the
350 /// SelectionDAG to resolve dangling debug information attached
351 /// to PHI nodes.
352 void clearDanglingDebugInfo();
354 /// getRoot - Return the current virtual root of the Selection DAG,
355 /// flushing any PendingLoad items. This must be done before emitting
356 /// a store or any other node that may need to be ordered after any
357 /// prior load instructions.
358 ///
359 SDValue getRoot();
361 /// getControlRoot - Similar to getRoot, but instead of flushing all the
362 /// PendingLoad items, flush all the PendingExports items. It is necessary
363 /// to do this before emitting a terminator instruction.
364 ///
365 SDValue getControlRoot();
367 DebugLoc getCurDebugLoc() const { return CurDebugLoc; }
369 unsigned getSDNodeOrder() const { return SDNodeOrder; }
371 void CopyValueToVirtualRegister(const Value *V, unsigned Reg);
373 /// AssignOrderingToNode - Assign an ordering to the node. The order is gotten
374 /// from how the code appeared in the source. The ordering is used by the
375 /// scheduler to effectively turn off scheduling.
376 void AssignOrderingToNode(const SDNode *Node);
378 void visit(const Instruction &I);
380 void visit(unsigned Opcode, const User &I);
382 // resolveDanglingDebugInfo - if we saw an earlier dbg_value referring to V,
383 // generate the debug data structures now that we've seen its definition.
384 void resolveDanglingDebugInfo(const Value *V, SDValue Val);
385 SDValue getValue(const Value *V);
386 SDValue getNonRegisterValue(const Value *V);
387 SDValue getValueImpl(const Value *V);
389 void setValue(const Value *V, SDValue NewN) {
390 SDValue &N = NodeMap[V];
391 assert(N.getNode() == 0 && "Already set a value for this node!");
392 N = NewN;
393 }
395 void setUnusedArgValue(const Value *V, SDValue NewN) {
396 SDValue &N = UnusedArgNodeMap[V];
397 assert(N.getNode() == 0 && "Already set a value for this node!");
398 N = NewN;
399 }
401 void FindMergedConditions(const Value *Cond, MachineBasicBlock *TBB,
402 MachineBasicBlock *FBB, MachineBasicBlock *CurBB,
403 MachineBasicBlock *SwitchBB, unsigned Opc);
404 void EmitBranchForMergedCondition(const Value *Cond, MachineBasicBlock *TBB,
405 MachineBasicBlock *FBB,
406 MachineBasicBlock *CurBB,
407 MachineBasicBlock *SwitchBB);
408 bool ShouldEmitAsBranches(const std::vector<CaseBlock> &Cases);
409 bool isExportableFromCurrentBlock(const Value *V, const BasicBlock *FromBB);
410 void CopyToExportRegsIfNeeded(const Value *V);
411 void ExportFromCurrentBlock(const Value *V);
412 void LowerCallTo(ImmutableCallSite CS, SDValue Callee, bool IsTailCall,
413 MachineBasicBlock *LandingPad = NULL);
415 /// UpdateSplitBlock - When an MBB was split during scheduling, update the
416 /// references that ned to refer to the last resulting block.
417 void UpdateSplitBlock(MachineBasicBlock *First, MachineBasicBlock *Last);
419 private:
420 // Terminator instructions.
421 void visitRet(const ReturnInst &I);
422 void visitBr(const BranchInst &I);
423 void visitSwitch(const SwitchInst &I);
424 void visitIndirectBr(const IndirectBrInst &I);
425 void visitUnreachable(const UnreachableInst &I) { /* noop */ }
427 // Helpers for visitSwitch
428 bool handleSmallSwitchRange(CaseRec& CR,
429 CaseRecVector& WorkList,
430 const Value* SV,
431 MachineBasicBlock* Default,
432 MachineBasicBlock *SwitchBB);
433 bool handleJTSwitchCase(CaseRec& CR,
434 CaseRecVector& WorkList,
435 const Value* SV,
436 MachineBasicBlock* Default,
437 MachineBasicBlock *SwitchBB);
438 bool handleBTSplitSwitchCase(CaseRec& CR,
439 CaseRecVector& WorkList,
440 const Value* SV,
441 MachineBasicBlock* Default,
442 MachineBasicBlock *SwitchBB);
443 bool handleBitTestsSwitchCase(CaseRec& CR,
444 CaseRecVector& WorkList,
445 const Value* SV,
446 MachineBasicBlock* Default,
447 MachineBasicBlock *SwitchBB);
449 uint32_t getEdgeWeight(const MachineBasicBlock *Src,
450 const MachineBasicBlock *Dst) const;
451 void addSuccessorWithWeight(MachineBasicBlock *Src, MachineBasicBlock *Dst,
452 uint32_t Weight = 0);
453 public:
454 void visitSwitchCase(CaseBlock &CB,
455 MachineBasicBlock *SwitchBB);
456 void visitBitTestHeader(BitTestBlock &B, MachineBasicBlock *SwitchBB);
457 void visitBitTestCase(BitTestBlock &BB,
458 MachineBasicBlock* NextMBB,
459 uint32_t BranchWeightToNext,
460 unsigned Reg,
461 BitTestCase &B,
462 MachineBasicBlock *SwitchBB);
463 void visitJumpTable(JumpTable &JT);
464 void visitJumpTableHeader(JumpTable &JT, JumpTableHeader &JTH,
465 MachineBasicBlock *SwitchBB);
467 private:
468 // These all get lowered before this pass.
469 void visitInvoke(const InvokeInst &I);
470 void visitResume(const ResumeInst &I);
472 void visitBinary(const User &I, unsigned OpCode);
473 void visitShift(const User &I, unsigned Opcode);
474 void visitAdd(const User &I) { visitBinary(I, ISD::ADD); }
475 void visitFAdd(const User &I) { visitBinary(I, ISD::FADD); }
476 void visitSub(const User &I) { visitBinary(I, ISD::SUB); }
477 void visitFSub(const User &I);
478 void visitMul(const User &I) { visitBinary(I, ISD::MUL); }
479 void visitFMul(const User &I) { visitBinary(I, ISD::FMUL); }
480 void visitURem(const User &I) { visitBinary(I, ISD::UREM); }
481 void visitSRem(const User &I) { visitBinary(I, ISD::SREM); }
482 void visitFRem(const User &I) { visitBinary(I, ISD::FREM); }
483 void visitUDiv(const User &I) { visitBinary(I, ISD::UDIV); }
484 void visitSDiv(const User &I);
485 void visitFDiv(const User &I) { visitBinary(I, ISD::FDIV); }
486 void visitAnd (const User &I) { visitBinary(I, ISD::AND); }
487 void visitOr (const User &I) { visitBinary(I, ISD::OR); }
488 void visitXor (const User &I) { visitBinary(I, ISD::XOR); }
489 void visitShl (const User &I) { visitShift(I, ISD::SHL); }
490 void visitLShr(const User &I) { visitShift(I, ISD::SRL); }
491 void visitAShr(const User &I) { visitShift(I, ISD::SRA); }
492 void visitICmp(const User &I);
493 void visitFCmp(const User &I);
494 // Visit the conversion instructions
495 void visitTrunc(const User &I);
496 void visitZExt(const User &I);
497 void visitSExt(const User &I);
498 void visitFPTrunc(const User &I);
499 void visitFPExt(const User &I);
500 void visitFPToUI(const User &I);
501 void visitFPToSI(const User &I);
502 void visitUIToFP(const User &I);
503 void visitSIToFP(const User &I);
504 void visitPtrToInt(const User &I);
505 void visitIntToPtr(const User &I);
506 void visitBitCast(const User &I);
508 void visitExtractElement(const User &I);
509 void visitInsertElement(const User &I);
510 void visitShuffleVector(const User &I);
512 void visitExtractValue(const ExtractValueInst &I);
513 void visitInsertValue(const InsertValueInst &I);
514 void visitLandingPad(const LandingPadInst &I);
516 void visitGetElementPtr(const User &I);
517 void visitSelect(const User &I);
519 void visitAlloca(const AllocaInst &I);
520 void visitLoad(const LoadInst &I);
521 void visitStore(const StoreInst &I);
522 void visitAtomicCmpXchg(const AtomicCmpXchgInst &I);
523 void visitAtomicRMW(const AtomicRMWInst &I);
524 void visitFence(const FenceInst &I);
525 void visitPHI(const PHINode &I);
526 void visitCall(const CallInst &I);
527 bool visitMemCmpCall(const CallInst &I);
528 bool visitUnaryFloatCall(const CallInst &I, unsigned Opcode);
529 void visitAtomicLoad(const LoadInst &I);
530 void visitAtomicStore(const StoreInst &I);
532 void visitInlineAsm(ImmutableCallSite CS);
533 const char *visitIntrinsicCall(const CallInst &I, unsigned Intrinsic);
534 void visitTargetIntrinsic(const CallInst &I, unsigned Intrinsic);
536 void visitVAStart(const CallInst &I);
537 void visitVAArg(const VAArgInst &I);
538 void visitVAEnd(const CallInst &I);
539 void visitVACopy(const CallInst &I);
541 void visitUserOp1(const Instruction &I) {
542 llvm_unreachable("UserOp1 should not exist at instruction selection time!");
543 }
544 void visitUserOp2(const Instruction &I) {
545 llvm_unreachable("UserOp2 should not exist at instruction selection time!");
546 }
548 void HandlePHINodesInSuccessorBlocks(const BasicBlock *LLVMBB);
550 /// EmitFuncArgumentDbgValue - If V is an function argument then create
551 /// corresponding DBG_VALUE machine instruction for it now. At the end of
552 /// instruction selection, they will be inserted to the entry BB.
553 bool EmitFuncArgumentDbgValue(const Value *V, MDNode *Variable,
554 int64_t Offset, const SDValue &N);
555 };
557 } // end namespace llvm
559 #endif