]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/CodeGen/TargetSchedule.cpp
Add a couple of convenience accessors to DebugLocEntry::Value to further
[opencl/llvm.git] / lib / CodeGen / TargetSchedule.cpp
1 //===-- llvm/Target/TargetSchedule.cpp - Sched Machine Model ----*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements a wrapper around MCSchedModel that allows the interface
11 // to benefit from information currently only available in TargetInstrInfo.
12 //
13 //===----------------------------------------------------------------------===//
15 #include "llvm/CodeGen/TargetSchedule.h"
16 #include "llvm/Support/CommandLine.h"
17 #include "llvm/Support/raw_ostream.h"
18 #include "llvm/Target/TargetInstrInfo.h"
19 #include "llvm/Target/TargetMachine.h"
20 #include "llvm/Target/TargetRegisterInfo.h"
21 #include "llvm/Target/TargetSubtargetInfo.h"
23 using namespace llvm;
25 static cl::opt<bool> EnableSchedModel("schedmodel", cl::Hidden, cl::init(true),
26   cl::desc("Use TargetSchedModel for latency lookup"));
28 static cl::opt<bool> EnableSchedItins("scheditins", cl::Hidden, cl::init(true),
29   cl::desc("Use InstrItineraryData for latency lookup"));
31 bool TargetSchedModel::hasInstrSchedModel() const {
32   return EnableSchedModel && SchedModel.hasInstrSchedModel();
33 }
35 bool TargetSchedModel::hasInstrItineraries() const {
36   return EnableSchedItins && !InstrItins.isEmpty();
37 }
39 static unsigned gcd(unsigned Dividend, unsigned Divisor) {
40   // Dividend and Divisor will be naturally swapped as needed.
41   while(Divisor) {
42     unsigned Rem = Dividend % Divisor;
43     Dividend = Divisor;
44     Divisor = Rem;
45   };
46   return Dividend;
47 }
48 static unsigned lcm(unsigned A, unsigned B) {
49   unsigned LCM = (uint64_t(A) * B) / gcd(A, B);
50   assert((LCM >= A && LCM >= B) && "LCM overflow");
51   return LCM;
52 }
54 void TargetSchedModel::init(const MCSchedModel &sm,
55                             const TargetSubtargetInfo *sti,
56                             const TargetInstrInfo *tii) {
57   SchedModel = sm;
58   STI = sti;
59   TII = tii;
60   STI->initInstrItins(InstrItins);
62   unsigned NumRes = SchedModel.getNumProcResourceKinds();
63   ResourceFactors.resize(NumRes);
64   ResourceLCM = SchedModel.IssueWidth;
65   for (unsigned Idx = 0; Idx < NumRes; ++Idx) {
66     unsigned NumUnits = SchedModel.getProcResource(Idx)->NumUnits;
67     if (NumUnits > 0)
68       ResourceLCM = lcm(ResourceLCM, NumUnits);
69   }
70   MicroOpFactor = ResourceLCM / SchedModel.IssueWidth;
71   for (unsigned Idx = 0; Idx < NumRes; ++Idx) {
72     unsigned NumUnits = SchedModel.getProcResource(Idx)->NumUnits;
73     ResourceFactors[Idx] = NumUnits ? (ResourceLCM / NumUnits) : 0;
74   }
75 }
77 unsigned TargetSchedModel::getNumMicroOps(const MachineInstr *MI,
78                                           const MCSchedClassDesc *SC) const {
79   if (hasInstrItineraries()) {
80     int UOps = InstrItins.getNumMicroOps(MI->getDesc().getSchedClass());
81     return (UOps >= 0) ? UOps : TII->getNumMicroOps(&InstrItins, MI);
82   }
83   if (hasInstrSchedModel()) {
84     if (!SC)
85       SC = resolveSchedClass(MI);
86     if (SC->isValid())
87       return SC->NumMicroOps;
88   }
89   return MI->isTransient() ? 0 : 1;
90 }
92 // The machine model may explicitly specify an invalid latency, which
93 // effectively means infinite latency. Since users of the TargetSchedule API
94 // don't know how to handle this, we convert it to a very large latency that is
95 // easy to distinguish when debugging the DAG but won't induce overflow.
96 static unsigned capLatency(int Cycles) {
97   return Cycles >= 0 ? Cycles : 1000;
98 }
100 /// Return the MCSchedClassDesc for this instruction. Some SchedClasses require
101 /// evaluation of predicates that depend on instruction operands or flags.
102 const MCSchedClassDesc *TargetSchedModel::
103 resolveSchedClass(const MachineInstr *MI) const {
105   // Get the definition's scheduling class descriptor from this machine model.
106   unsigned SchedClass = MI->getDesc().getSchedClass();
107   const MCSchedClassDesc *SCDesc = SchedModel.getSchedClassDesc(SchedClass);
108   if (!SCDesc->isValid())
109     return SCDesc;
111 #ifndef NDEBUG
112   unsigned NIter = 0;
113 #endif
114   while (SCDesc->isVariant()) {
115     assert(++NIter < 6 && "Variants are nested deeper than the magic number");
117     SchedClass = STI->resolveSchedClass(SchedClass, MI, this);
118     SCDesc = SchedModel.getSchedClassDesc(SchedClass);
119   }
120   return SCDesc;
123 /// Find the def index of this operand. This index maps to the machine model and
124 /// is independent of use operands. Def operands may be reordered with uses or
125 /// merged with uses without affecting the def index (e.g. before/after
126 /// regalloc). However, an instruction's def operands must never be reordered
127 /// with respect to each other.
128 static unsigned findDefIdx(const MachineInstr *MI, unsigned DefOperIdx) {
129   unsigned DefIdx = 0;
130   for (unsigned i = 0; i != DefOperIdx; ++i) {
131     const MachineOperand &MO = MI->getOperand(i);
132     if (MO.isReg() && MO.isDef())
133       ++DefIdx;
134   }
135   return DefIdx;
138 /// Find the use index of this operand. This is independent of the instruction's
139 /// def operands.
140 ///
141 /// Note that uses are not determined by the operand's isUse property, which
142 /// is simply the inverse of isDef. Here we consider any readsReg operand to be
143 /// a "use". The machine model allows an operand to be both a Def and Use.
144 static unsigned findUseIdx(const MachineInstr *MI, unsigned UseOperIdx) {
145   unsigned UseIdx = 0;
146   for (unsigned i = 0; i != UseOperIdx; ++i) {
147     const MachineOperand &MO = MI->getOperand(i);
148     if (MO.isReg() && MO.readsReg())
149       ++UseIdx;
150   }
151   return UseIdx;
154 // Top-level API for clients that know the operand indices.
155 unsigned TargetSchedModel::computeOperandLatency(
156   const MachineInstr *DefMI, unsigned DefOperIdx,
157   const MachineInstr *UseMI, unsigned UseOperIdx) const {
159   if (!hasInstrSchedModel() && !hasInstrItineraries())
160     return TII->defaultDefLatency(&SchedModel, DefMI);
162   if (hasInstrItineraries()) {
163     int OperLatency = 0;
164     if (UseMI) {
165       OperLatency = TII->getOperandLatency(&InstrItins, DefMI, DefOperIdx,
166                                            UseMI, UseOperIdx);
167     }
168     else {
169       unsigned DefClass = DefMI->getDesc().getSchedClass();
170       OperLatency = InstrItins.getOperandCycle(DefClass, DefOperIdx);
171     }
172     if (OperLatency >= 0)
173       return OperLatency;
175     // No operand latency was found.
176     unsigned InstrLatency = TII->getInstrLatency(&InstrItins, DefMI);
178     // Expected latency is the max of the stage latency and itinerary props.
179     // Rather than directly querying InstrItins stage latency, we call a TII
180     // hook to allow subtargets to specialize latency. This hook is only
181     // applicable to the InstrItins model. InstrSchedModel should model all
182     // special cases without TII hooks.
183     InstrLatency = std::max(InstrLatency,
184                             TII->defaultDefLatency(&SchedModel, DefMI));
185     return InstrLatency;
186   }
187   // hasInstrSchedModel()
188   const MCSchedClassDesc *SCDesc = resolveSchedClass(DefMI);
189   unsigned DefIdx = findDefIdx(DefMI, DefOperIdx);
190   if (DefIdx < SCDesc->NumWriteLatencyEntries) {
191     // Lookup the definition's write latency in SubtargetInfo.
192     const MCWriteLatencyEntry *WLEntry =
193       STI->getWriteLatencyEntry(SCDesc, DefIdx);
194     unsigned WriteID = WLEntry->WriteResourceID;
195     unsigned Latency = capLatency(WLEntry->Cycles);
196     if (!UseMI)
197       return Latency;
199     // Lookup the use's latency adjustment in SubtargetInfo.
200     const MCSchedClassDesc *UseDesc = resolveSchedClass(UseMI);
201     if (UseDesc->NumReadAdvanceEntries == 0)
202       return Latency;
203     unsigned UseIdx = findUseIdx(UseMI, UseOperIdx);
204     int Advance = STI->getReadAdvanceCycles(UseDesc, UseIdx, WriteID);
205     if (Advance > 0 && (unsigned)Advance > Latency) // unsigned wrap
206       return 0;
207     return Latency - Advance;
208   }
209   // If DefIdx does not exist in the model (e.g. implicit defs), then return
210   // unit latency (defaultDefLatency may be too conservative).
211 #ifndef NDEBUG
212   if (SCDesc->isValid() && !DefMI->getOperand(DefOperIdx).isImplicit()
213       && !DefMI->getDesc().OpInfo[DefOperIdx].isOptionalDef()
214       && SchedModel.isComplete()) {
215     std::string Err;
216     raw_string_ostream ss(Err);
217     ss << "DefIdx " << DefIdx << " exceeds machine model writes for "
218        << *DefMI;
219     report_fatal_error(ss.str());
220   }
221 #endif
222   // FIXME: Automatically giving all implicit defs defaultDefLatency is
223   // undesirable. We should only do it for defs that are known to the MC
224   // desc like flags. Truly implicit defs should get 1 cycle latency.
225   return DefMI->isTransient() ? 0 : TII->defaultDefLatency(&SchedModel, DefMI);
228 unsigned TargetSchedModel::computeInstrLatency(unsigned Opcode) const {
229   assert(hasInstrSchedModel() && "Only call this function with a SchedModel");
231   unsigned SCIdx = TII->get(Opcode).getSchedClass();
232   const MCSchedClassDesc *SCDesc = SchedModel.getSchedClassDesc(SCIdx);
233   unsigned Latency = 0;
235   if (SCDesc->isValid() && !SCDesc->isVariant()) {
236     for (unsigned DefIdx = 0, DefEnd = SCDesc->NumWriteLatencyEntries;
237          DefIdx != DefEnd; ++DefIdx) {
238       // Lookup the definition's write latency in SubtargetInfo.
239       const MCWriteLatencyEntry *WLEntry =
240           STI->getWriteLatencyEntry(SCDesc, DefIdx);
241       Latency = std::max(Latency, capLatency(WLEntry->Cycles));
242     }
243     return Latency;
244   }
246   assert(Latency && "No MI sched latency");
247   return 0;
250 unsigned
251 TargetSchedModel::computeInstrLatency(const MachineInstr *MI,
252                                       bool UseDefaultDefLatency) const {
253   // For the itinerary model, fall back to the old subtarget hook.
254   // Allow subtargets to compute Bundle latencies outside the machine model.
255   if (hasInstrItineraries() || MI->isBundle() ||
256       (!hasInstrSchedModel() && !UseDefaultDefLatency))
257     return TII->getInstrLatency(&InstrItins, MI);
259   if (hasInstrSchedModel()) {
260     const MCSchedClassDesc *SCDesc = resolveSchedClass(MI);
261     if (SCDesc->isValid()) {
262       unsigned Latency = 0;
263       for (unsigned DefIdx = 0, DefEnd = SCDesc->NumWriteLatencyEntries;
264            DefIdx != DefEnd; ++DefIdx) {
265         // Lookup the definition's write latency in SubtargetInfo.
266         const MCWriteLatencyEntry *WLEntry =
267           STI->getWriteLatencyEntry(SCDesc, DefIdx);
268         Latency = std::max(Latency, capLatency(WLEntry->Cycles));
269       }
270       return Latency;
271     }
272   }
273   return TII->defaultDefLatency(&SchedModel, MI);
276 unsigned TargetSchedModel::
277 computeOutputLatency(const MachineInstr *DefMI, unsigned DefOperIdx,
278                      const MachineInstr *DepMI) const {
279   if (SchedModel.MicroOpBufferSize <= 1)
280     return 1;
282   // MicroOpBufferSize > 1 indicates an out-of-order processor that can dispatch
283   // WAW dependencies in the same cycle.
285   // Treat predication as a data dependency for out-of-order cpus. In-order
286   // cpus do not need to treat predicated writes specially.
287   //
288   // TODO: The following hack exists because predication passes do not
289   // correctly append imp-use operands, and readsReg() strangely returns false
290   // for predicated defs.
291   unsigned Reg = DefMI->getOperand(DefOperIdx).getReg();
292   const MachineFunction &MF = *DefMI->getParent()->getParent();
293   const TargetRegisterInfo *TRI = MF.getSubtarget().getRegisterInfo();
294   if (!DepMI->readsRegister(Reg, TRI) && TII->isPredicated(DepMI))
295     return computeInstrLatency(DefMI);
297   // If we have a per operand scheduling model, check if this def is writing
298   // an unbuffered resource. If so, it treated like an in-order cpu.
299   if (hasInstrSchedModel()) {
300     const MCSchedClassDesc *SCDesc = resolveSchedClass(DefMI);
301     if (SCDesc->isValid()) {
302       for (const MCWriteProcResEntry *PRI = STI->getWriteProcResBegin(SCDesc),
303              *PRE = STI->getWriteProcResEnd(SCDesc); PRI != PRE; ++PRI) {
304         if (!SchedModel.getProcResource(PRI->ProcResourceIdx)->BufferSize)
305           return 1;
306       }
307     }
308   }
309   return 0;