1 //===-- BasicBlock.cpp - Implement BasicBlock related methods -------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the BasicBlock class for the IR library.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "llvm/IR/BasicBlock.h"
15 #include "SymbolTableListTraitsImpl.h"
16 #include "llvm/ADT/STLExtras.h"
17 #include "llvm/IR/Constants.h"
18 #include "llvm/IR/Instructions.h"
19 #include "llvm/IR/IntrinsicInst.h"
20 #include "llvm/IR/LLVMContext.h"
21 #include "llvm/IR/Type.h"
22 #include "llvm/Support/CFG.h"
23 #include "llvm/Support/LeakDetector.h"
24 #include <algorithm>
25 using namespace llvm;
27 ValueSymbolTable *BasicBlock::getValueSymbolTable() {
28 if (Function *F = getParent())
29 return &F->getValueSymbolTable();
30 return 0;
31 }
33 LLVMContext &BasicBlock::getContext() const {
34 return getType()->getContext();
35 }
37 // Explicit instantiation of SymbolTableListTraits since some of the methods
38 // are not in the public header file...
39 template class llvm::SymbolTableListTraits<Instruction, BasicBlock>;
42 BasicBlock::BasicBlock(LLVMContext &C, const Twine &Name, Function *NewParent,
43 BasicBlock *InsertBefore)
44 : Value(Type::getLabelTy(C), Value::BasicBlockVal), Parent(0) {
46 // Make sure that we get added to a function
47 LeakDetector::addGarbageObject(this);
49 if (InsertBefore) {
50 assert(NewParent &&
51 "Cannot insert block before another block with no function!");
52 NewParent->getBasicBlockList().insert(InsertBefore, this);
53 } else if (NewParent) {
54 NewParent->getBasicBlockList().push_back(this);
55 }
57 setName(Name);
58 }
61 BasicBlock::~BasicBlock() {
62 // If the address of the block is taken and it is being deleted (e.g. because
63 // it is dead), this means that there is either a dangling constant expr
64 // hanging off the block, or an undefined use of the block (source code
65 // expecting the address of a label to keep the block alive even though there
66 // is no indirect branch). Handle these cases by zapping the BlockAddress
67 // nodes. There are no other possible uses at this point.
68 if (hasAddressTaken()) {
69 assert(!use_empty() && "There should be at least one blockaddress!");
70 Constant *Replacement =
71 ConstantInt::get(llvm::Type::getInt32Ty(getContext()), 1);
72 while (!use_empty()) {
73 BlockAddress *BA = cast<BlockAddress>(use_back());
74 BA->replaceAllUsesWith(ConstantExpr::getIntToPtr(Replacement,
75 BA->getType()));
76 BA->destroyConstant();
77 }
78 }
80 assert(getParent() == 0 && "BasicBlock still linked into the program!");
81 dropAllReferences();
82 InstList.clear();
83 }
85 void BasicBlock::setParent(Function *parent) {
86 if (getParent())
87 LeakDetector::addGarbageObject(this);
89 // Set Parent=parent, updating instruction symtab entries as appropriate.
90 InstList.setSymTabObject(&Parent, parent);
92 if (getParent())
93 LeakDetector::removeGarbageObject(this);
94 }
96 void BasicBlock::removeFromParent() {
97 getParent()->getBasicBlockList().remove(this);
98 }
100 void BasicBlock::eraseFromParent() {
101 getParent()->getBasicBlockList().erase(this);
102 }
104 /// moveBefore - Unlink this basic block from its current function and
105 /// insert it into the function that MovePos lives in, right before MovePos.
106 void BasicBlock::moveBefore(BasicBlock *MovePos) {
107 MovePos->getParent()->getBasicBlockList().splice(MovePos,
108 getParent()->getBasicBlockList(), this);
109 }
111 /// moveAfter - Unlink this basic block from its current function and
112 /// insert it into the function that MovePos lives in, right after MovePos.
113 void BasicBlock::moveAfter(BasicBlock *MovePos) {
114 Function::iterator I = MovePos;
115 MovePos->getParent()->getBasicBlockList().splice(++I,
116 getParent()->getBasicBlockList(), this);
117 }
120 TerminatorInst *BasicBlock::getTerminator() {
121 if (InstList.empty()) return 0;
122 return dyn_cast<TerminatorInst>(&InstList.back());
123 }
125 const TerminatorInst *BasicBlock::getTerminator() const {
126 if (InstList.empty()) return 0;
127 return dyn_cast<TerminatorInst>(&InstList.back());
128 }
130 Instruction* BasicBlock::getFirstNonPHI() {
131 BasicBlock::iterator i = begin();
132 // All valid basic blocks should have a terminator,
133 // which is not a PHINode. If we have an invalid basic
134 // block we'll get an assertion failure when dereferencing
135 // a past-the-end iterator.
136 while (isa<PHINode>(i)) ++i;
137 return &*i;
138 }
140 Instruction* BasicBlock::getFirstNonPHIOrDbg() {
141 BasicBlock::iterator i = begin();
142 // All valid basic blocks should have a terminator,
143 // which is not a PHINode. If we have an invalid basic
144 // block we'll get an assertion failure when dereferencing
145 // a past-the-end iterator.
146 while (isa<PHINode>(i) || isa<DbgInfoIntrinsic>(i)) ++i;
147 return &*i;
148 }
150 Instruction* BasicBlock::getFirstNonPHIOrDbgOrLifetime() {
151 // All valid basic blocks should have a terminator,
152 // which is not a PHINode. If we have an invalid basic
153 // block we'll get an assertion failure when dereferencing
154 // a past-the-end iterator.
155 BasicBlock::iterator i = begin();
156 for (;; ++i) {
157 if (isa<PHINode>(i) || isa<DbgInfoIntrinsic>(i))
158 continue;
160 const IntrinsicInst *II = dyn_cast<IntrinsicInst>(i);
161 if (!II)
162 break;
163 if (II->getIntrinsicID() != Intrinsic::lifetime_start &&
164 II->getIntrinsicID() != Intrinsic::lifetime_end)
165 break;
166 }
167 return &*i;
168 }
170 BasicBlock::iterator BasicBlock::getFirstInsertionPt() {
171 iterator InsertPt = getFirstNonPHI();
172 if (isa<LandingPadInst>(InsertPt)) ++InsertPt;
173 return InsertPt;
174 }
176 void BasicBlock::dropAllReferences() {
177 for(iterator I = begin(), E = end(); I != E; ++I)
178 I->dropAllReferences();
179 }
181 /// getSinglePredecessor - If this basic block has a single predecessor block,
182 /// return the block, otherwise return a null pointer.
183 BasicBlock *BasicBlock::getSinglePredecessor() {
184 pred_iterator PI = pred_begin(this), E = pred_end(this);
185 if (PI == E) return 0; // No preds.
186 BasicBlock *ThePred = *PI;
187 ++PI;
188 return (PI == E) ? ThePred : 0 /*multiple preds*/;
189 }
191 /// getUniquePredecessor - If this basic block has a unique predecessor block,
192 /// return the block, otherwise return a null pointer.
193 /// Note that unique predecessor doesn't mean single edge, there can be
194 /// multiple edges from the unique predecessor to this block (for example
195 /// a switch statement with multiple cases having the same destination).
196 BasicBlock *BasicBlock::getUniquePredecessor() {
197 pred_iterator PI = pred_begin(this), E = pred_end(this);
198 if (PI == E) return 0; // No preds.
199 BasicBlock *PredBB = *PI;
200 ++PI;
201 for (;PI != E; ++PI) {
202 if (*PI != PredBB)
203 return 0;
204 // The same predecessor appears multiple times in the predecessor list.
205 // This is OK.
206 }
207 return PredBB;
208 }
210 /// removePredecessor - This method is used to notify a BasicBlock that the
211 /// specified Predecessor of the block is no longer able to reach it. This is
212 /// actually not used to update the Predecessor list, but is actually used to
213 /// update the PHI nodes that reside in the block. Note that this should be
214 /// called while the predecessor still refers to this block.
215 ///
216 void BasicBlock::removePredecessor(BasicBlock *Pred,
217 bool DontDeleteUselessPHIs) {
218 assert((hasNUsesOrMore(16)||// Reduce cost of this assertion for complex CFGs.
219 find(pred_begin(this), pred_end(this), Pred) != pred_end(this)) &&
220 "removePredecessor: BB is not a predecessor!");
222 if (InstList.empty()) return;
223 PHINode *APN = dyn_cast<PHINode>(&front());
224 if (!APN) return; // Quick exit.
226 // If there are exactly two predecessors, then we want to nuke the PHI nodes
227 // altogether. However, we cannot do this, if this in this case:
228 //
229 // Loop:
230 // %x = phi [X, Loop]
231 // %x2 = add %x, 1 ;; This would become %x2 = add %x2, 1
232 // br Loop ;; %x2 does not dominate all uses
233 //
234 // This is because the PHI node input is actually taken from the predecessor
235 // basic block. The only case this can happen is with a self loop, so we
236 // check for this case explicitly now.
237 //
238 unsigned max_idx = APN->getNumIncomingValues();
239 assert(max_idx != 0 && "PHI Node in block with 0 predecessors!?!?!");
240 if (max_idx == 2) {
241 BasicBlock *Other = APN->getIncomingBlock(APN->getIncomingBlock(0) == Pred);
243 // Disable PHI elimination!
244 if (this == Other) max_idx = 3;
245 }
247 // <= Two predecessors BEFORE I remove one?
248 if (max_idx <= 2 && !DontDeleteUselessPHIs) {
249 // Yup, loop through and nuke the PHI nodes
250 while (PHINode *PN = dyn_cast<PHINode>(&front())) {
251 // Remove the predecessor first.
252 PN->removeIncomingValue(Pred, !DontDeleteUselessPHIs);
254 // If the PHI _HAD_ two uses, replace PHI node with its now *single* value
255 if (max_idx == 2) {
256 if (PN->getIncomingValue(0) != PN)
257 PN->replaceAllUsesWith(PN->getIncomingValue(0));
258 else
259 // We are left with an infinite loop with no entries: kill the PHI.
260 PN->replaceAllUsesWith(UndefValue::get(PN->getType()));
261 getInstList().pop_front(); // Remove the PHI node
262 }
264 // If the PHI node already only had one entry, it got deleted by
265 // removeIncomingValue.
266 }
267 } else {
268 // Okay, now we know that we need to remove predecessor #pred_idx from all
269 // PHI nodes. Iterate over each PHI node fixing them up
270 PHINode *PN;
271 for (iterator II = begin(); (PN = dyn_cast<PHINode>(II)); ) {
272 ++II;
273 PN->removeIncomingValue(Pred, false);
274 // If all incoming values to the Phi are the same, we can replace the Phi
275 // with that value.
276 Value* PNV = 0;
277 if (!DontDeleteUselessPHIs && (PNV = PN->hasConstantValue()))
278 if (PNV != PN) {
279 PN->replaceAllUsesWith(PNV);
280 PN->eraseFromParent();
281 }
282 }
283 }
284 }
287 /// splitBasicBlock - This splits a basic block into two at the specified
288 /// instruction. Note that all instructions BEFORE the specified iterator stay
289 /// as part of the original basic block, an unconditional branch is added to
290 /// the new BB, and the rest of the instructions in the BB are moved to the new
291 /// BB, including the old terminator. This invalidates the iterator.
292 ///
293 /// Note that this only works on well formed basic blocks (must have a
294 /// terminator), and 'I' must not be the end of instruction list (which would
295 /// cause a degenerate basic block to be formed, having a terminator inside of
296 /// the basic block).
297 ///
298 BasicBlock *BasicBlock::splitBasicBlock(iterator I, const Twine &BBName) {
299 assert(getTerminator() && "Can't use splitBasicBlock on degenerate BB!");
300 assert(I != InstList.end() &&
301 "Trying to get me to create degenerate basic block!");
303 BasicBlock *InsertBefore = llvm::next(Function::iterator(this))
304 .getNodePtrUnchecked();
305 BasicBlock *New = BasicBlock::Create(getContext(), BBName,
306 getParent(), InsertBefore);
308 // Move all of the specified instructions from the original basic block into
309 // the new basic block.
310 New->getInstList().splice(New->end(), this->getInstList(), I, end());
312 // Add a branch instruction to the newly formed basic block.
313 BranchInst::Create(New, this);
315 // Now we must loop through all of the successors of the New block (which
316 // _were_ the successors of the 'this' block), and update any PHI nodes in
317 // successors. If there were PHI nodes in the successors, then they need to
318 // know that incoming branches will be from New, not from Old.
319 //
320 for (succ_iterator I = succ_begin(New), E = succ_end(New); I != E; ++I) {
321 // Loop over any phi nodes in the basic block, updating the BB field of
322 // incoming values...
323 BasicBlock *Successor = *I;
324 PHINode *PN;
325 for (BasicBlock::iterator II = Successor->begin();
326 (PN = dyn_cast<PHINode>(II)); ++II) {
327 int IDX = PN->getBasicBlockIndex(this);
328 while (IDX != -1) {
329 PN->setIncomingBlock((unsigned)IDX, New);
330 IDX = PN->getBasicBlockIndex(this);
331 }
332 }
333 }
334 return New;
335 }
337 void BasicBlock::replaceSuccessorsPhiUsesWith(BasicBlock *New) {
338 TerminatorInst *TI = getTerminator();
339 if (!TI)
340 // Cope with being called on a BasicBlock that doesn't have a terminator
341 // yet. Clang's CodeGenFunction::EmitReturnBlock() likes to do this.
342 return;
343 for (unsigned i = 0, e = TI->getNumSuccessors(); i != e; ++i) {
344 BasicBlock *Succ = TI->getSuccessor(i);
345 // N.B. Succ might not be a complete BasicBlock, so don't assume
346 // that it ends with a non-phi instruction.
347 for (iterator II = Succ->begin(), IE = Succ->end(); II != IE; ++II) {
348 PHINode *PN = dyn_cast<PHINode>(II);
349 if (!PN)
350 break;
351 int i;
352 while ((i = PN->getBasicBlockIndex(this)) >= 0)
353 PN->setIncomingBlock(i, New);
354 }
355 }
356 }
358 /// isLandingPad - Return true if this basic block is a landing pad. I.e., it's
359 /// the destination of the 'unwind' edge of an invoke instruction.
360 bool BasicBlock::isLandingPad() const {
361 return isa<LandingPadInst>(getFirstNonPHI());
362 }
364 /// getLandingPadInst() - Return the landingpad instruction associated with
365 /// the landing pad.
366 LandingPadInst *BasicBlock::getLandingPadInst() {
367 return dyn_cast<LandingPadInst>(getFirstNonPHI());
368 }
369 const LandingPadInst *BasicBlock::getLandingPadInst() const {
370 return dyn_cast<LandingPadInst>(getFirstNonPHI());
371 }