1 //===- Pass.cpp - LLVM Pass Infrastructure Implementation -----------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the LLVM Pass infrastructure. It is primarily
11 // responsible with ensuring that passes are executed and batched together
12 // optimally.
13 //
14 //===----------------------------------------------------------------------===//
16 #include "llvm/Pass.h"
17 #include "llvm/IR/Function.h"
18 #include "llvm/IR/IRPrintingPasses.h"
19 #include "llvm/IR/LegacyPassNameParser.h"
20 #include "llvm/PassRegistry.h"
21 #include "llvm/Support/Debug.h"
22 #include "llvm/Support/raw_ostream.h"
23 using namespace llvm;
25 #define DEBUG_TYPE "ir"
27 //===----------------------------------------------------------------------===//
28 // Pass Implementation
29 //
31 // Force out-of-line virtual method.
32 Pass::~Pass() {
33 delete Resolver;
34 }
36 // Force out-of-line virtual method.
37 ModulePass::~ModulePass() { }
39 Pass *ModulePass::createPrinterPass(raw_ostream &O,
40 const std::string &Banner) const {
41 return createPrintModulePass(O, Banner);
42 }
44 PassManagerType ModulePass::getPotentialPassManagerType() const {
45 return PMT_ModulePassManager;
46 }
48 bool Pass::mustPreserveAnalysisID(char &AID) const {
49 return Resolver->getAnalysisIfAvailable(&AID, true) != nullptr;
50 }
52 // dumpPassStructure - Implement the -debug-pass=Structure option
53 void Pass::dumpPassStructure(unsigned Offset) {
54 dbgs().indent(Offset*2) << getPassName() << "\n";
55 }
57 /// getPassName - Return a nice clean name for a pass. This usually
58 /// implemented in terms of the name that is registered by one of the
59 /// Registration templates, but can be overloaded directly.
60 ///
61 const char *Pass::getPassName() const {
62 AnalysisID AID = getPassID();
63 const PassInfo *PI = PassRegistry::getPassRegistry()->getPassInfo(AID);
64 if (PI)
65 return PI->getPassName();
66 return "Unnamed pass: implement Pass::getPassName()";
67 }
69 void Pass::preparePassManager(PMStack &) {
70 // By default, don't do anything.
71 }
73 PassManagerType Pass::getPotentialPassManagerType() const {
74 // Default implementation.
75 return PMT_Unknown;
76 }
78 void Pass::getAnalysisUsage(AnalysisUsage &) const {
79 // By default, no analysis results are used, all are invalidated.
80 }
82 void Pass::releaseMemory() {
83 // By default, don't do anything.
84 }
86 void Pass::verifyAnalysis() const {
87 // By default, don't do anything.
88 }
90 void *Pass::getAdjustedAnalysisPointer(AnalysisID AID) {
91 return this;
92 }
94 ImmutablePass *Pass::getAsImmutablePass() {
95 return nullptr;
96 }
98 PMDataManager *Pass::getAsPMDataManager() {
99 return nullptr;
100 }
102 void Pass::setResolver(AnalysisResolver *AR) {
103 assert(!Resolver && "Resolver is already set");
104 Resolver = AR;
105 }
107 // print - Print out the internal state of the pass. This is called by Analyze
108 // to print out the contents of an analysis. Otherwise it is not necessary to
109 // implement this method.
110 //
111 void Pass::print(raw_ostream &O,const Module*) const {
112 O << "Pass::print not implemented for pass: '" << getPassName() << "'!\n";
113 }
115 // dump - call print(cerr);
116 void Pass::dump() const {
117 print(dbgs(), nullptr);
118 }
120 //===----------------------------------------------------------------------===//
121 // ImmutablePass Implementation
122 //
123 // Force out-of-line virtual method.
124 ImmutablePass::~ImmutablePass() { }
126 void ImmutablePass::initializePass() {
127 // By default, don't do anything.
128 }
130 //===----------------------------------------------------------------------===//
131 // FunctionPass Implementation
132 //
134 Pass *FunctionPass::createPrinterPass(raw_ostream &O,
135 const std::string &Banner) const {
136 return createPrintFunctionPass(O, Banner);
137 }
139 PassManagerType FunctionPass::getPotentialPassManagerType() const {
140 return PMT_FunctionPassManager;
141 }
143 bool FunctionPass::skipOptnoneFunction(const Function &F) const {
144 if (F.hasFnAttribute(Attribute::OptimizeNone)) {
145 DEBUG(dbgs() << "Skipping pass '" << getPassName()
146 << "' on function " << F.getName() << "\n");
147 return true;
148 }
149 return false;
150 }
152 //===----------------------------------------------------------------------===//
153 // BasicBlockPass Implementation
154 //
156 Pass *BasicBlockPass::createPrinterPass(raw_ostream &O,
157 const std::string &Banner) const {
158 return createPrintBasicBlockPass(O, Banner);
159 }
161 bool BasicBlockPass::doInitialization(Function &) {
162 // By default, don't do anything.
163 return false;
164 }
166 bool BasicBlockPass::doFinalization(Function &) {
167 // By default, don't do anything.
168 return false;
169 }
171 bool BasicBlockPass::skipOptnoneFunction(const BasicBlock &BB) const {
172 const Function *F = BB.getParent();
173 if (F && F->hasFnAttribute(Attribute::OptimizeNone)) {
174 // Report this only once per function.
175 if (&BB == &F->getEntryBlock())
176 DEBUG(dbgs() << "Skipping pass '" << getPassName()
177 << "' on function " << F->getName() << "\n");
178 return true;
179 }
180 return false;
181 }
183 PassManagerType BasicBlockPass::getPotentialPassManagerType() const {
184 return PMT_BasicBlockPassManager;
185 }
187 const PassInfo *Pass::lookupPassInfo(const void *TI) {
188 return PassRegistry::getPassRegistry()->getPassInfo(TI);
189 }
191 const PassInfo *Pass::lookupPassInfo(StringRef Arg) {
192 return PassRegistry::getPassRegistry()->getPassInfo(Arg);
193 }
195 Pass *Pass::createPass(AnalysisID ID) {
196 const PassInfo *PI = PassRegistry::getPassRegistry()->getPassInfo(ID);
197 if (!PI)
198 return nullptr;
199 return PI->createPass();
200 }
202 //===----------------------------------------------------------------------===//
203 // Analysis Group Implementation Code
204 //===----------------------------------------------------------------------===//
206 // RegisterAGBase implementation
207 //
208 RegisterAGBase::RegisterAGBase(const char *Name, const void *InterfaceID,
209 const void *PassID, bool isDefault)
210 : PassInfo(Name, InterfaceID) {
211 PassRegistry::getPassRegistry()->registerAnalysisGroup(InterfaceID, PassID,
212 *this, isDefault);
213 }
215 //===----------------------------------------------------------------------===//
216 // PassRegistrationListener implementation
217 //
219 // enumeratePasses - Iterate over the registered passes, calling the
220 // passEnumerate callback on each PassInfo object.
221 //
222 void PassRegistrationListener::enumeratePasses() {
223 PassRegistry::getPassRegistry()->enumerateWith(this);
224 }
226 PassNameParser::PassNameParser()
227 : Opt(nullptr) {
228 PassRegistry::getPassRegistry()->addRegistrationListener(this);
229 }
231 PassNameParser::~PassNameParser() {
232 // This only gets called during static destruction, in which case the
233 // PassRegistry will have already been destroyed by llvm_shutdown(). So
234 // attempting to remove the registration listener is an error.
235 }
237 //===----------------------------------------------------------------------===//
238 // AnalysisUsage Class Implementation
239 //
241 namespace {
242 struct GetCFGOnlyPasses : public PassRegistrationListener {
243 typedef AnalysisUsage::VectorType VectorType;
244 VectorType &CFGOnlyList;
245 GetCFGOnlyPasses(VectorType &L) : CFGOnlyList(L) {}
247 void passEnumerate(const PassInfo *P) override {
248 if (P->isCFGOnlyPass())
249 CFGOnlyList.push_back(P->getTypeInfo());
250 }
251 };
252 }
254 // setPreservesCFG - This function should be called to by the pass, iff they do
255 // not:
256 //
257 // 1. Add or remove basic blocks from the function
258 // 2. Modify terminator instructions in any way.
259 //
260 // This function annotates the AnalysisUsage info object to say that analyses
261 // that only depend on the CFG are preserved by this pass.
262 //
263 void AnalysisUsage::setPreservesCFG() {
264 // Since this transformation doesn't modify the CFG, it preserves all analyses
265 // that only depend on the CFG (like dominators, loop info, etc...)
266 GetCFGOnlyPasses(Preserved).enumeratePasses();
267 }
269 AnalysisUsage &AnalysisUsage::addPreserved(StringRef Arg) {
270 const PassInfo *PI = Pass::lookupPassInfo(Arg);
271 // If the pass exists, preserve it. Otherwise silently do nothing.
272 if (PI) Preserved.push_back(PI->getTypeInfo());
273 return *this;
274 }
276 AnalysisUsage &AnalysisUsage::addRequiredID(const void *ID) {
277 Required.push_back(ID);
278 return *this;
279 }
281 AnalysisUsage &AnalysisUsage::addRequiredID(char &ID) {
282 Required.push_back(&ID);
283 return *this;
284 }
286 AnalysisUsage &AnalysisUsage::addRequiredTransitiveID(char &ID) {
287 Required.push_back(&ID);
288 RequiredTransitive.push_back(&ID);
289 return *this;
290 }