]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Linker/LinkModules.cpp
738791d7e5691378abe0af6c9b3a76ad6ab04ee8
[opencl/llvm.git] / lib / Linker / LinkModules.cpp
1 //===- lib/Linker/LinkModules.cpp - Module Linker Implementation ----------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements the LLVM module linker.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "llvm/Linker/Linker.h"
15 #include "llvm-c/Linker.h"
16 #include "llvm/ADT/Hashing.h"
17 #include "llvm/ADT/Optional.h"
18 #include "llvm/ADT/SetVector.h"
19 #include "llvm/ADT/SmallString.h"
20 #include "llvm/ADT/Statistic.h"
21 #include "llvm/IR/Constants.h"
22 #include "llvm/IR/DiagnosticInfo.h"
23 #include "llvm/IR/DiagnosticPrinter.h"
24 #include "llvm/IR/LLVMContext.h"
25 #include "llvm/IR/Module.h"
26 #include "llvm/IR/TypeFinder.h"
27 #include "llvm/Support/CommandLine.h"
28 #include "llvm/Support/Debug.h"
29 #include "llvm/Support/raw_ostream.h"
30 #include "llvm/Transforms/Utils/Cloning.h"
31 #include <cctype>
32 #include <tuple>
33 using namespace llvm;
36 //===----------------------------------------------------------------------===//
37 // TypeMap implementation.
38 //===----------------------------------------------------------------------===//
40 namespace {
41 class TypeMapTy : public ValueMapTypeRemapper {
42   /// This is a mapping from a source type to a destination type to use.
43   DenseMap<Type*, Type*> MappedTypes;
45   /// When checking to see if two subgraphs are isomorphic, we speculatively
46   /// add types to MappedTypes, but keep track of them here in case we need to
47   /// roll back.
48   SmallVector<Type*, 16> SpeculativeTypes;
50   SmallVector<StructType*, 16> SpeculativeDstOpaqueTypes;
52   /// This is a list of non-opaque structs in the source module that are mapped
53   /// to an opaque struct in the destination module.
54   SmallVector<StructType*, 16> SrcDefinitionsToResolve;
56   /// This is the set of opaque types in the destination modules who are
57   /// getting a body from the source module.
58   SmallPtrSet<StructType*, 16> DstResolvedOpaqueTypes;
60 public:
61   TypeMapTy(Linker::IdentifiedStructTypeSet &DstStructTypesSet)
62       : DstStructTypesSet(DstStructTypesSet) {}
64   Linker::IdentifiedStructTypeSet &DstStructTypesSet;
65   /// Indicate that the specified type in the destination module is conceptually
66   /// equivalent to the specified type in the source module.
67   void addTypeMapping(Type *DstTy, Type *SrcTy);
69   /// Produce a body for an opaque type in the dest module from a type
70   /// definition in the source module.
71   void linkDefinedTypeBodies();
73   /// Return the mapped type to use for the specified input type from the
74   /// source module.
75   Type *get(Type *SrcTy);
76   Type *get(Type *SrcTy, SmallPtrSet<StructType *, 8> &Visited);
78   void finishType(StructType *DTy, StructType *STy, ArrayRef<Type *> ETypes);
80   FunctionType *get(FunctionType *T) {
81     return cast<FunctionType>(get((Type *)T));
82   }
84   /// Dump out the type map for debugging purposes.
85   void dump() const {
86     for (auto &Pair : MappedTypes) {
87       dbgs() << "TypeMap: ";
88       Pair.first->print(dbgs());
89       dbgs() << " => ";
90       Pair.second->print(dbgs());
91       dbgs() << '\n';
92     }
93   }
95 private:
96   Type *remapType(Type *SrcTy) override { return get(SrcTy); }
98   bool areTypesIsomorphic(Type *DstTy, Type *SrcTy);
99 };
102 void TypeMapTy::addTypeMapping(Type *DstTy, Type *SrcTy) {
103   assert(SpeculativeTypes.empty());
104   assert(SpeculativeDstOpaqueTypes.empty());
106   // Check to see if these types are recursively isomorphic and establish a
107   // mapping between them if so.
108   if (!areTypesIsomorphic(DstTy, SrcTy)) {
109     // Oops, they aren't isomorphic.  Just discard this request by rolling out
110     // any speculative mappings we've established.
111     for (Type *Ty : SpeculativeTypes)
112       MappedTypes.erase(Ty);
114     SrcDefinitionsToResolve.resize(SrcDefinitionsToResolve.size() -
115                                    SpeculativeDstOpaqueTypes.size());
116     for (StructType *Ty : SpeculativeDstOpaqueTypes)
117       DstResolvedOpaqueTypes.erase(Ty);
118   } else {
119     for (Type *Ty : SpeculativeTypes)
120       if (auto *STy = dyn_cast<StructType>(Ty))
121         if (STy->hasName())
122           STy->setName("");
123   }
124   SpeculativeTypes.clear();
125   SpeculativeDstOpaqueTypes.clear();
128 /// Recursively walk this pair of types, returning true if they are isomorphic,
129 /// false if they are not.
130 bool TypeMapTy::areTypesIsomorphic(Type *DstTy, Type *SrcTy) {
131   // Two types with differing kinds are clearly not isomorphic.
132   if (DstTy->getTypeID() != SrcTy->getTypeID())
133     return false;
135   // If we have an entry in the MappedTypes table, then we have our answer.
136   Type *&Entry = MappedTypes[SrcTy];
137   if (Entry)
138     return Entry == DstTy;
140   // Two identical types are clearly isomorphic.  Remember this
141   // non-speculatively.
142   if (DstTy == SrcTy) {
143     Entry = DstTy;
144     return true;
145   }
147   // Okay, we have two types with identical kinds that we haven't seen before.
149   // If this is an opaque struct type, special case it.
150   if (StructType *SSTy = dyn_cast<StructType>(SrcTy)) {
151     // Mapping an opaque type to any struct, just keep the dest struct.
152     if (SSTy->isOpaque()) {
153       Entry = DstTy;
154       SpeculativeTypes.push_back(SrcTy);
155       return true;
156     }
158     // Mapping a non-opaque source type to an opaque dest.  If this is the first
159     // type that we're mapping onto this destination type then we succeed.  Keep
160     // the dest, but fill it in later. If this is the second (different) type
161     // that we're trying to map onto the same opaque type then we fail.
162     if (cast<StructType>(DstTy)->isOpaque()) {
163       // We can only map one source type onto the opaque destination type.
164       if (!DstResolvedOpaqueTypes.insert(cast<StructType>(DstTy)).second)
165         return false;
166       SrcDefinitionsToResolve.push_back(SSTy);
167       SpeculativeTypes.push_back(SrcTy);
168       SpeculativeDstOpaqueTypes.push_back(cast<StructType>(DstTy));
169       Entry = DstTy;
170       return true;
171     }
172   }
174   // If the number of subtypes disagree between the two types, then we fail.
175   if (SrcTy->getNumContainedTypes() != DstTy->getNumContainedTypes())
176     return false;
178   // Fail if any of the extra properties (e.g. array size) of the type disagree.
179   if (isa<IntegerType>(DstTy))
180     return false;  // bitwidth disagrees.
181   if (PointerType *PT = dyn_cast<PointerType>(DstTy)) {
182     if (PT->getAddressSpace() != cast<PointerType>(SrcTy)->getAddressSpace())
183       return false;
185   } else if (FunctionType *FT = dyn_cast<FunctionType>(DstTy)) {
186     if (FT->isVarArg() != cast<FunctionType>(SrcTy)->isVarArg())
187       return false;
188   } else if (StructType *DSTy = dyn_cast<StructType>(DstTy)) {
189     StructType *SSTy = cast<StructType>(SrcTy);
190     if (DSTy->isLiteral() != SSTy->isLiteral() ||
191         DSTy->isPacked() != SSTy->isPacked())
192       return false;
193   } else if (ArrayType *DATy = dyn_cast<ArrayType>(DstTy)) {
194     if (DATy->getNumElements() != cast<ArrayType>(SrcTy)->getNumElements())
195       return false;
196   } else if (VectorType *DVTy = dyn_cast<VectorType>(DstTy)) {
197     if (DVTy->getNumElements() != cast<VectorType>(SrcTy)->getNumElements())
198       return false;
199   }
201   // Otherwise, we speculate that these two types will line up and recursively
202   // check the subelements.
203   Entry = DstTy;
204   SpeculativeTypes.push_back(SrcTy);
206   for (unsigned I = 0, E = SrcTy->getNumContainedTypes(); I != E; ++I)
207     if (!areTypesIsomorphic(DstTy->getContainedType(I),
208                             SrcTy->getContainedType(I)))
209       return false;
211   // If everything seems to have lined up, then everything is great.
212   return true;
215 void TypeMapTy::linkDefinedTypeBodies() {
216   SmallVector<Type*, 16> Elements;
217   for (StructType *SrcSTy : SrcDefinitionsToResolve) {
218     StructType *DstSTy = cast<StructType>(MappedTypes[SrcSTy]);
219     assert(DstSTy->isOpaque());
221     // Map the body of the source type over to a new body for the dest type.
222     Elements.resize(SrcSTy->getNumElements());
223     for (unsigned I = 0, E = Elements.size(); I != E; ++I)
224       Elements[I] = get(SrcSTy->getElementType(I));
226     DstSTy->setBody(Elements, SrcSTy->isPacked());
227   }
228   SrcDefinitionsToResolve.clear();
229   DstResolvedOpaqueTypes.clear();
232 void TypeMapTy::finishType(StructType *DTy, StructType *STy,
233                            ArrayRef<Type *> ETypes) {
234   DTy->setBody(ETypes, STy->isPacked());
236   // Steal STy's name.
237   if (STy->hasName()) {
238     SmallString<16> TmpName = STy->getName();
239     STy->setName("");
240     DTy->setName(TmpName);
241   }
243   DstStructTypesSet.addNonOpaque(DTy);
246 Type *TypeMapTy::get(Type *Ty) {
247   SmallPtrSet<StructType *, 8> Visited;
248   return get(Ty, Visited);
251 Type *TypeMapTy::get(Type *Ty, SmallPtrSet<StructType *, 8> &Visited) {
252   // If we already have an entry for this type, return it.
253   Type **Entry = &MappedTypes[Ty];
254   if (*Entry)
255     return *Entry;
257   // These are types that LLVM itself will unique.
258   bool IsUniqued = !isa<StructType>(Ty) || cast<StructType>(Ty)->isLiteral();
260 #ifndef NDEBUG
261   if (!IsUniqued) {
262     for (auto &Pair : MappedTypes) {
263       assert(!(Pair.first != Ty && Pair.second == Ty) &&
264              "mapping to a source type");
265     }
266   }
267 #endif
269   if (!IsUniqued && !Visited.insert(cast<StructType>(Ty)).second) {
270     StructType *DTy = StructType::create(Ty->getContext());
271     return *Entry = DTy;
272   }
274   // If this is not a recursive type, then just map all of the elements and
275   // then rebuild the type from inside out.
276   SmallVector<Type *, 4> ElementTypes;
278   // If there are no element types to map, then the type is itself.  This is
279   // true for the anonymous {} struct, things like 'float', integers, etc.
280   if (Ty->getNumContainedTypes() == 0 && IsUniqued)
281     return *Entry = Ty;
283   // Remap all of the elements, keeping track of whether any of them change.
284   bool AnyChange = false;
285   ElementTypes.resize(Ty->getNumContainedTypes());
286   for (unsigned I = 0, E = Ty->getNumContainedTypes(); I != E; ++I) {
287     ElementTypes[I] = get(Ty->getContainedType(I), Visited);
288     AnyChange |= ElementTypes[I] != Ty->getContainedType(I);
289   }
291   // If we found our type while recursively processing stuff, just use it.
292   Entry = &MappedTypes[Ty];
293   if (*Entry) {
294     if (auto *DTy = dyn_cast<StructType>(*Entry)) {
295       if (DTy->isOpaque()) {
296         auto *STy = cast<StructType>(Ty);
297         finishType(DTy, STy, ElementTypes);
298       }
299     }
300     return *Entry;
301   }
303   // If all of the element types mapped directly over and the type is not
304   // a nomed struct, then the type is usable as-is.
305   if (!AnyChange && IsUniqued)
306     return *Entry = Ty;
308   // Otherwise, rebuild a modified type.
309   switch (Ty->getTypeID()) {
310   default:
311     llvm_unreachable("unknown derived type to remap");
312   case Type::ArrayTyID:
313     return *Entry = ArrayType::get(ElementTypes[0],
314                                    cast<ArrayType>(Ty)->getNumElements());
315   case Type::VectorTyID:
316     return *Entry = VectorType::get(ElementTypes[0],
317                                     cast<VectorType>(Ty)->getNumElements());
318   case Type::PointerTyID:
319     return *Entry = PointerType::get(ElementTypes[0],
320                                      cast<PointerType>(Ty)->getAddressSpace());
321   case Type::FunctionTyID:
322     return *Entry = FunctionType::get(ElementTypes[0],
323                                       makeArrayRef(ElementTypes).slice(1),
324                                       cast<FunctionType>(Ty)->isVarArg());
325   case Type::StructTyID: {
326     auto *STy = cast<StructType>(Ty);
327     bool IsPacked = STy->isPacked();
328     if (IsUniqued)
329       return *Entry = StructType::get(Ty->getContext(), ElementTypes, IsPacked);
331     // If the type is opaque, we can just use it directly.
332     if (STy->isOpaque()) {
333       DstStructTypesSet.addOpaque(STy);
334       return *Entry = Ty;
335     }
337     if (StructType *OldT =
338             DstStructTypesSet.findNonOpaque(ElementTypes, IsPacked)) {
339       STy->setName("");
340       return *Entry = OldT;
341     }
343     if (!AnyChange) {
344       DstStructTypesSet.addNonOpaque(STy);
345       return *Entry = Ty;
346     }
348     StructType *DTy = StructType::create(Ty->getContext());
349     finishType(DTy, STy, ElementTypes);
350     return *Entry = DTy;
351   }
352   }
355 //===----------------------------------------------------------------------===//
356 // ModuleLinker implementation.
357 //===----------------------------------------------------------------------===//
359 namespace {
360 class ModuleLinker;
362 /// Creates prototypes for functions that are lazily linked on the fly. This
363 /// speeds up linking for modules with many/ lazily linked functions of which
364 /// few get used.
365 class ValueMaterializerTy : public ValueMaterializer {
366   TypeMapTy &TypeMap;
367   Module *DstM;
368   std::vector<Function *> &LazilyLinkFunctions;
370 public:
371   ValueMaterializerTy(TypeMapTy &TypeMap, Module *DstM,
372                       std::vector<Function *> &LazilyLinkFunctions)
373       : ValueMaterializer(), TypeMap(TypeMap), DstM(DstM),
374         LazilyLinkFunctions(LazilyLinkFunctions) {}
376   Value *materializeValueFor(Value *V) override;
377 };
379 class LinkDiagnosticInfo : public DiagnosticInfo {
380   const Twine &Msg;
382 public:
383   LinkDiagnosticInfo(DiagnosticSeverity Severity, const Twine &Msg);
384   void print(DiagnosticPrinter &DP) const override;
385 };
386 LinkDiagnosticInfo::LinkDiagnosticInfo(DiagnosticSeverity Severity,
387                                        const Twine &Msg)
388     : DiagnosticInfo(DK_Linker, Severity), Msg(Msg) {}
389 void LinkDiagnosticInfo::print(DiagnosticPrinter &DP) const { DP << Msg; }
391 /// This is an implementation class for the LinkModules function, which is the
392 /// entrypoint for this file.
393 class ModuleLinker {
394   Module *DstM, *SrcM;
396   TypeMapTy TypeMap;
397   ValueMaterializerTy ValMaterializer;
399   /// Mapping of values from what they used to be in Src, to what they are now
400   /// in DstM.  ValueToValueMapTy is a ValueMap, which involves some overhead
401   /// due to the use of Value handles which the Linker doesn't actually need,
402   /// but this allows us to reuse the ValueMapper code.
403   ValueToValueMapTy ValueMap;
405   struct AppendingVarInfo {
406     GlobalVariable *NewGV;   // New aggregate global in dest module.
407     const Constant *DstInit; // Old initializer from dest module.
408     const Constant *SrcInit; // Old initializer from src module.
409   };
411   std::vector<AppendingVarInfo> AppendingVars;
413   // Set of items not to link in from source.
414   SmallPtrSet<const Value *, 16> DoNotLinkFromSource;
416   // Vector of functions to lazily link in.
417   std::vector<Function *> LazilyLinkFunctions;
419   Linker::DiagnosticHandlerFunction DiagnosticHandler;
421 public:
422   ModuleLinker(Module *dstM, Linker::IdentifiedStructTypeSet &Set, Module *srcM,
423                Linker::DiagnosticHandlerFunction DiagnosticHandler)
424       : DstM(dstM), SrcM(srcM), TypeMap(Set),
425         ValMaterializer(TypeMap, DstM, LazilyLinkFunctions),
426         DiagnosticHandler(DiagnosticHandler) {}
428   bool run();
430 private:
431   bool shouldLinkFromSource(bool &LinkFromSrc, const GlobalValue &Dest,
432                             const GlobalValue &Src);
434   /// Helper method for setting a message and returning an error code.
435   bool emitError(const Twine &Message) {
436     DiagnosticHandler(LinkDiagnosticInfo(DS_Error, Message));
437     return true;
438   }
440   void emitWarning(const Twine &Message) {
441     DiagnosticHandler(LinkDiagnosticInfo(DS_Warning, Message));
442   }
444   bool getComdatLeader(Module *M, StringRef ComdatName,
445                        const GlobalVariable *&GVar);
446   bool computeResultingSelectionKind(StringRef ComdatName,
447                                      Comdat::SelectionKind Src,
448                                      Comdat::SelectionKind Dst,
449                                      Comdat::SelectionKind &Result,
450                                      bool &LinkFromSrc);
451   std::map<const Comdat *, std::pair<Comdat::SelectionKind, bool>>
452       ComdatsChosen;
453   bool getComdatResult(const Comdat *SrcC, Comdat::SelectionKind &SK,
454                        bool &LinkFromSrc);
456   /// Given a global in the source module, return the global in the
457   /// destination module that is being linked to, if any.
458   GlobalValue *getLinkedToGlobal(const GlobalValue *SrcGV) {
459     // If the source has no name it can't link.  If it has local linkage,
460     // there is no name match-up going on.
461     if (!SrcGV->hasName() || SrcGV->hasLocalLinkage())
462       return nullptr;
464     // Otherwise see if we have a match in the destination module's symtab.
465     GlobalValue *DGV = DstM->getNamedValue(SrcGV->getName());
466     if (!DGV)
467       return nullptr;
469     // If we found a global with the same name in the dest module, but it has
470     // internal linkage, we are really not doing any linkage here.
471     if (DGV->hasLocalLinkage())
472       return nullptr;
474     // Otherwise, we do in fact link to the destination global.
475     return DGV;
476   }
478   void computeTypeMapping();
480   void upgradeMismatchedGlobalArray(StringRef Name);
481   void upgradeMismatchedGlobals();
483   bool linkAppendingVarProto(GlobalVariable *DstGV,
484                              const GlobalVariable *SrcGV);
486   bool linkGlobalValueProto(GlobalValue *GV);
487   GlobalValue *linkGlobalVariableProto(const GlobalVariable *SGVar,
488                                        GlobalValue *DGV, bool LinkFromSrc);
489   GlobalValue *linkFunctionProto(const Function *SF, GlobalValue *DGV,
490                                  bool LinkFromSrc);
491   GlobalValue *linkGlobalAliasProto(const GlobalAlias *SGA, GlobalValue *DGV,
492                                     bool LinkFromSrc);
494   bool linkModuleFlagsMetadata();
496   void linkAppendingVarInit(const AppendingVarInfo &AVI);
497   void linkGlobalInits();
498   void linkFunctionBody(Function *Dst, Function *Src);
499   void linkAliasBodies();
500   void linkNamedMDNodes();
501 };
504 /// The LLVM SymbolTable class autorenames globals that conflict in the symbol
505 /// table. This is good for all clients except for us. Go through the trouble
506 /// to force this back.
507 static void forceRenaming(GlobalValue *GV, StringRef Name) {
508   // If the global doesn't force its name or if it already has the right name,
509   // there is nothing for us to do.
510   if (GV->hasLocalLinkage() || GV->getName() == Name)
511     return;
513   Module *M = GV->getParent();
515   // If there is a conflict, rename the conflict.
516   if (GlobalValue *ConflictGV = M->getNamedValue(Name)) {
517     GV->takeName(ConflictGV);
518     ConflictGV->setName(Name);    // This will cause ConflictGV to get renamed
519     assert(ConflictGV->getName() != Name && "forceRenaming didn't work");
520   } else {
521     GV->setName(Name);              // Force the name back
522   }
525 /// copy additional attributes (those not needed to construct a GlobalValue)
526 /// from the SrcGV to the DestGV.
527 static void copyGVAttributes(GlobalValue *DestGV, const GlobalValue *SrcGV) {
528   DestGV->copyAttributesFrom(SrcGV);
529   forceRenaming(DestGV, SrcGV->getName());
532 static bool isLessConstraining(GlobalValue::VisibilityTypes a,
533                                GlobalValue::VisibilityTypes b) {
534   if (a == GlobalValue::HiddenVisibility)
535     return false;
536   if (b == GlobalValue::HiddenVisibility)
537     return true;
538   if (a == GlobalValue::ProtectedVisibility)
539     return false;
540   if (b == GlobalValue::ProtectedVisibility)
541     return true;
542   return false;
545 Value *ValueMaterializerTy::materializeValueFor(Value *V) {
546   Function *SF = dyn_cast<Function>(V);
547   if (!SF)
548     return nullptr;
550   Function *DF = Function::Create(TypeMap.get(SF->getFunctionType()),
551                                   SF->getLinkage(), SF->getName(), DstM);
552   copyGVAttributes(DF, SF);
554   if (Comdat *SC = SF->getComdat()) {
555     Comdat *DC = DstM->getOrInsertComdat(SC->getName());
556     DF->setComdat(DC);
557   }
559   LazilyLinkFunctions.push_back(SF);
560   return DF;
563 bool ModuleLinker::getComdatLeader(Module *M, StringRef ComdatName,
564                                    const GlobalVariable *&GVar) {
565   const GlobalValue *GVal = M->getNamedValue(ComdatName);
566   if (const auto *GA = dyn_cast_or_null<GlobalAlias>(GVal)) {
567     GVal = GA->getBaseObject();
568     if (!GVal)
569       // We cannot resolve the size of the aliasee yet.
570       return emitError("Linking COMDATs named '" + ComdatName +
571                        "': COMDAT key involves incomputable alias size.");
572   }
574   GVar = dyn_cast_or_null<GlobalVariable>(GVal);
575   if (!GVar)
576     return emitError(
577         "Linking COMDATs named '" + ComdatName +
578         "': GlobalVariable required for data dependent selection!");
580   return false;
583 bool ModuleLinker::computeResultingSelectionKind(StringRef ComdatName,
584                                                  Comdat::SelectionKind Src,
585                                                  Comdat::SelectionKind Dst,
586                                                  Comdat::SelectionKind &Result,
587                                                  bool &LinkFromSrc) {
588   // The ability to mix Comdat::SelectionKind::Any with
589   // Comdat::SelectionKind::Largest is a behavior that comes from COFF.
590   bool DstAnyOrLargest = Dst == Comdat::SelectionKind::Any ||
591                          Dst == Comdat::SelectionKind::Largest;
592   bool SrcAnyOrLargest = Src == Comdat::SelectionKind::Any ||
593                          Src == Comdat::SelectionKind::Largest;
594   if (DstAnyOrLargest && SrcAnyOrLargest) {
595     if (Dst == Comdat::SelectionKind::Largest ||
596         Src == Comdat::SelectionKind::Largest)
597       Result = Comdat::SelectionKind::Largest;
598     else
599       Result = Comdat::SelectionKind::Any;
600   } else if (Src == Dst) {
601     Result = Dst;
602   } else {
603     return emitError("Linking COMDATs named '" + ComdatName +
604                      "': invalid selection kinds!");
605   }
607   switch (Result) {
608   case Comdat::SelectionKind::Any:
609     // Go with Dst.
610     LinkFromSrc = false;
611     break;
612   case Comdat::SelectionKind::NoDuplicates:
613     return emitError("Linking COMDATs named '" + ComdatName +
614                      "': noduplicates has been violated!");
615   case Comdat::SelectionKind::ExactMatch:
616   case Comdat::SelectionKind::Largest:
617   case Comdat::SelectionKind::SameSize: {
618     const GlobalVariable *DstGV;
619     const GlobalVariable *SrcGV;
620     if (getComdatLeader(DstM, ComdatName, DstGV) ||
621         getComdatLeader(SrcM, ComdatName, SrcGV))
622       return true;
624     const DataLayout *DstDL = DstM->getDataLayout();
625     const DataLayout *SrcDL = SrcM->getDataLayout();
626     if (!DstDL || !SrcDL) {
627       return emitError(
628           "Linking COMDATs named '" + ComdatName +
629           "': can't do size dependent selection without DataLayout!");
630     }
631     uint64_t DstSize =
632         DstDL->getTypeAllocSize(DstGV->getType()->getPointerElementType());
633     uint64_t SrcSize =
634         SrcDL->getTypeAllocSize(SrcGV->getType()->getPointerElementType());
635     if (Result == Comdat::SelectionKind::ExactMatch) {
636       if (SrcGV->getInitializer() != DstGV->getInitializer())
637         return emitError("Linking COMDATs named '" + ComdatName +
638                          "': ExactMatch violated!");
639       LinkFromSrc = false;
640     } else if (Result == Comdat::SelectionKind::Largest) {
641       LinkFromSrc = SrcSize > DstSize;
642     } else if (Result == Comdat::SelectionKind::SameSize) {
643       if (SrcSize != DstSize)
644         return emitError("Linking COMDATs named '" + ComdatName +
645                          "': SameSize violated!");
646       LinkFromSrc = false;
647     } else {
648       llvm_unreachable("unknown selection kind");
649     }
650     break;
651   }
652   }
654   return false;
657 bool ModuleLinker::getComdatResult(const Comdat *SrcC,
658                                    Comdat::SelectionKind &Result,
659                                    bool &LinkFromSrc) {
660   Comdat::SelectionKind SSK = SrcC->getSelectionKind();
661   StringRef ComdatName = SrcC->getName();
662   Module::ComdatSymTabType &ComdatSymTab = DstM->getComdatSymbolTable();
663   Module::ComdatSymTabType::iterator DstCI = ComdatSymTab.find(ComdatName);
665   if (DstCI == ComdatSymTab.end()) {
666     // Use the comdat if it is only available in one of the modules.
667     LinkFromSrc = true;
668     Result = SSK;
669     return false;
670   }
672   const Comdat *DstC = &DstCI->second;
673   Comdat::SelectionKind DSK = DstC->getSelectionKind();
674   return computeResultingSelectionKind(ComdatName, SSK, DSK, Result,
675                                        LinkFromSrc);
678 bool ModuleLinker::shouldLinkFromSource(bool &LinkFromSrc,
679                                         const GlobalValue &Dest,
680                                         const GlobalValue &Src) {
681   // We always have to add Src if it has appending linkage.
682   if (Src.hasAppendingLinkage()) {
683     LinkFromSrc = true;
684     return false;
685   }
687   bool SrcIsDeclaration = Src.isDeclarationForLinker();
688   bool DestIsDeclaration = Dest.isDeclarationForLinker();
690   if (SrcIsDeclaration) {
691     // If Src is external or if both Src & Dest are external..  Just link the
692     // external globals, we aren't adding anything.
693     if (Src.hasDLLImportStorageClass()) {
694       // If one of GVs is marked as DLLImport, result should be dllimport'ed.
695       LinkFromSrc = DestIsDeclaration;
696       return false;
697     }
698     // If the Dest is weak, use the source linkage.
699     LinkFromSrc = Dest.hasExternalWeakLinkage();
700     return false;
701   }
703   if (DestIsDeclaration) {
704     // If Dest is external but Src is not:
705     LinkFromSrc = true;
706     return false;
707   }
709   if (Src.hasCommonLinkage()) {
710     if (Dest.hasLinkOnceLinkage() || Dest.hasWeakLinkage()) {
711       LinkFromSrc = true;
712       return false;
713     }
715     if (!Dest.hasCommonLinkage()) {
716       LinkFromSrc = false;
717       return false;
718     }
720     // FIXME: Make datalayout mandatory and just use getDataLayout().
721     DataLayout DL(Dest.getParent());
723     uint64_t DestSize = DL.getTypeAllocSize(Dest.getType()->getElementType());
724     uint64_t SrcSize = DL.getTypeAllocSize(Src.getType()->getElementType());
725     LinkFromSrc = SrcSize > DestSize;
726     return false;
727   }
729   if (Src.isWeakForLinker()) {
730     assert(!Dest.hasExternalWeakLinkage());
731     assert(!Dest.hasAvailableExternallyLinkage());
733     if (Dest.hasLinkOnceLinkage() && Src.hasWeakLinkage()) {
734       LinkFromSrc = true;
735       return false;
736     }
738     LinkFromSrc = false;
739     return false;
740   }
742   if (Dest.isWeakForLinker()) {
743     assert(Src.hasExternalLinkage());
744     LinkFromSrc = true;
745     return false;
746   }
748   assert(!Src.hasExternalWeakLinkage());
749   assert(!Dest.hasExternalWeakLinkage());
750   assert(Dest.hasExternalLinkage() && Src.hasExternalLinkage() &&
751          "Unexpected linkage type!");
752   return emitError("Linking globals named '" + Src.getName() +
753                    "': symbol multiply defined!");
756 /// Loop over all of the linked values to compute type mappings.  For example,
757 /// if we link "extern Foo *x" and "Foo *x = NULL", then we have two struct
758 /// types 'Foo' but one got renamed when the module was loaded into the same
759 /// LLVMContext.
760 void ModuleLinker::computeTypeMapping() {
761   for (GlobalValue &SGV : SrcM->globals()) {
762     GlobalValue *DGV = getLinkedToGlobal(&SGV);
763     if (!DGV)
764       continue;
766     if (!DGV->hasAppendingLinkage() || !SGV.hasAppendingLinkage()) {
767       TypeMap.addTypeMapping(DGV->getType(), SGV.getType());
768       continue;
769     }
771     // Unify the element type of appending arrays.
772     ArrayType *DAT = cast<ArrayType>(DGV->getType()->getElementType());
773     ArrayType *SAT = cast<ArrayType>(SGV.getType()->getElementType());
774     TypeMap.addTypeMapping(DAT->getElementType(), SAT->getElementType());
775   }
777   for (GlobalValue &SGV : *SrcM) {
778     if (GlobalValue *DGV = getLinkedToGlobal(&SGV))
779       TypeMap.addTypeMapping(DGV->getType(), SGV.getType());
780   }
782   for (GlobalValue &SGV : SrcM->aliases()) {
783     if (GlobalValue *DGV = getLinkedToGlobal(&SGV))
784       TypeMap.addTypeMapping(DGV->getType(), SGV.getType());
785   }
787   // Incorporate types by name, scanning all the types in the source module.
788   // At this point, the destination module may have a type "%foo = { i32 }" for
789   // example.  When the source module got loaded into the same LLVMContext, if
790   // it had the same type, it would have been renamed to "%foo.42 = { i32 }".
791   std::vector<StructType *> Types = SrcM->getIdentifiedStructTypes();
792   for (StructType *ST : Types) {
793     if (!ST->hasName())
794       continue;
796     // Check to see if there is a dot in the name followed by a digit.
797     size_t DotPos = ST->getName().rfind('.');
798     if (DotPos == 0 || DotPos == StringRef::npos ||
799         ST->getName().back() == '.' ||
800         !isdigit(static_cast<unsigned char>(ST->getName()[DotPos + 1])))
801       continue;
803     // Check to see if the destination module has a struct with the prefix name.
804     StructType *DST = DstM->getTypeByName(ST->getName().substr(0, DotPos));
805     if (!DST)
806       continue;
808     // Don't use it if this actually came from the source module. They're in
809     // the same LLVMContext after all. Also don't use it unless the type is
810     // actually used in the destination module. This can happen in situations
811     // like this:
812     //
813     //      Module A                         Module B
814     //      --------                         --------
815     //   %Z = type { %A }                %B = type { %C.1 }
816     //   %A = type { %B.1, [7 x i8] }    %C.1 = type { i8* }
817     //   %B.1 = type { %C }              %A.2 = type { %B.3, [5 x i8] }
818     //   %C = type { i8* }               %B.3 = type { %C.1 }
819     //
820     // When we link Module B with Module A, the '%B' in Module B is
821     // used. However, that would then use '%C.1'. But when we process '%C.1',
822     // we prefer to take the '%C' version. So we are then left with both
823     // '%C.1' and '%C' being used for the same types. This leads to some
824     // variables using one type and some using the other.
825     if (TypeMap.DstStructTypesSet.hasType(DST))
826       TypeMap.addTypeMapping(DST, ST);
827   }
829   // Now that we have discovered all of the type equivalences, get a body for
830   // any 'opaque' types in the dest module that are now resolved.
831   TypeMap.linkDefinedTypeBodies();
834 static void upgradeGlobalArray(GlobalVariable *GV) {
835   ArrayType *ATy = cast<ArrayType>(GV->getType()->getElementType());
836   StructType *OldTy = cast<StructType>(ATy->getElementType());
837   assert(OldTy->getNumElements() == 2 && "Expected to upgrade from 2 elements");
839   // Get the upgraded 3 element type.
840   PointerType *VoidPtrTy = Type::getInt8Ty(GV->getContext())->getPointerTo();
841   Type *Tys[3] = {OldTy->getElementType(0), OldTy->getElementType(1),
842                   VoidPtrTy};
843   StructType *NewTy = StructType::get(GV->getContext(), Tys, false);
845   // Build new constants with a null third field filled in.
846   Constant *OldInitC = GV->getInitializer();
847   ConstantArray *OldInit = dyn_cast<ConstantArray>(OldInitC);
848   if (!OldInit && !isa<ConstantAggregateZero>(OldInitC))
849     // Invalid initializer; give up.
850     return;
851   std::vector<Constant *> Initializers;
852   if (OldInit && OldInit->getNumOperands()) {
853     Value *Null = Constant::getNullValue(VoidPtrTy);
854     for (Use &U : OldInit->operands()) {
855       ConstantStruct *Init = cast<ConstantStruct>(U.get());
856       Initializers.push_back(ConstantStruct::get(
857           NewTy, Init->getOperand(0), Init->getOperand(1), Null, nullptr));
858     }
859   }
860   assert(Initializers.size() == ATy->getNumElements() &&
861          "Failed to copy all array elements");
863   // Replace the old GV with a new one.
864   ATy = ArrayType::get(NewTy, Initializers.size());
865   Constant *NewInit = ConstantArray::get(ATy, Initializers);
866   GlobalVariable *NewGV = new GlobalVariable(
867       *GV->getParent(), ATy, GV->isConstant(), GV->getLinkage(), NewInit, "",
868       GV, GV->getThreadLocalMode(), GV->getType()->getAddressSpace(),
869       GV->isExternallyInitialized());
870   NewGV->copyAttributesFrom(GV);
871   NewGV->takeName(GV);
872   assert(GV->use_empty() && "program cannot use initializer list");
873   GV->eraseFromParent();
876 void ModuleLinker::upgradeMismatchedGlobalArray(StringRef Name) {
877   // Look for the global arrays.
878   auto *DstGV = dyn_cast_or_null<GlobalVariable>(DstM->getNamedValue(Name));
879   if (!DstGV)
880     return;
881   auto *SrcGV = dyn_cast_or_null<GlobalVariable>(SrcM->getNamedValue(Name));
882   if (!SrcGV)
883     return;
885   // Check if the types already match.
886   auto *DstTy = cast<ArrayType>(DstGV->getType()->getElementType());
887   auto *SrcTy =
888       cast<ArrayType>(TypeMap.get(SrcGV->getType()->getElementType()));
889   if (DstTy == SrcTy)
890     return;
892   // Grab the element types.  We can only upgrade an array of a two-field
893   // struct.  Only bother if the other one has three-fields.
894   auto *DstEltTy = cast<StructType>(DstTy->getElementType());
895   auto *SrcEltTy = cast<StructType>(SrcTy->getElementType());
896   if (DstEltTy->getNumElements() == 2 && SrcEltTy->getNumElements() == 3) {
897     upgradeGlobalArray(DstGV);
898     return;
899   }
900   if (DstEltTy->getNumElements() == 3 && SrcEltTy->getNumElements() == 2)
901     upgradeGlobalArray(SrcGV);
903   // We can't upgrade any other differences.
906 void ModuleLinker::upgradeMismatchedGlobals() {
907   upgradeMismatchedGlobalArray("llvm.global_ctors");
908   upgradeMismatchedGlobalArray("llvm.global_dtors");
911 /// If there were any appending global variables, link them together now.
912 /// Return true on error.
913 bool ModuleLinker::linkAppendingVarProto(GlobalVariable *DstGV,
914                                          const GlobalVariable *SrcGV) {
916   if (!SrcGV->hasAppendingLinkage() || !DstGV->hasAppendingLinkage())
917     return emitError("Linking globals named '" + SrcGV->getName() +
918            "': can only link appending global with another appending global!");
920   ArrayType *DstTy = cast<ArrayType>(DstGV->getType()->getElementType());
921   ArrayType *SrcTy =
922     cast<ArrayType>(TypeMap.get(SrcGV->getType()->getElementType()));
923   Type *EltTy = DstTy->getElementType();
925   // Check to see that they two arrays agree on type.
926   if (EltTy != SrcTy->getElementType())
927     return emitError("Appending variables with different element types!");
928   if (DstGV->isConstant() != SrcGV->isConstant())
929     return emitError("Appending variables linked with different const'ness!");
931   if (DstGV->getAlignment() != SrcGV->getAlignment())
932     return emitError(
933              "Appending variables with different alignment need to be linked!");
935   if (DstGV->getVisibility() != SrcGV->getVisibility())
936     return emitError(
937             "Appending variables with different visibility need to be linked!");
939   if (DstGV->hasUnnamedAddr() != SrcGV->hasUnnamedAddr())
940     return emitError(
941         "Appending variables with different unnamed_addr need to be linked!");
943   if (StringRef(DstGV->getSection()) != SrcGV->getSection())
944     return emitError(
945           "Appending variables with different section name need to be linked!");
947   uint64_t NewSize = DstTy->getNumElements() + SrcTy->getNumElements();
948   ArrayType *NewType = ArrayType::get(EltTy, NewSize);
950   // Create the new global variable.
951   GlobalVariable *NG =
952     new GlobalVariable(*DstGV->getParent(), NewType, SrcGV->isConstant(),
953                        DstGV->getLinkage(), /*init*/nullptr, /*name*/"", DstGV,
954                        DstGV->getThreadLocalMode(),
955                        DstGV->getType()->getAddressSpace());
957   // Propagate alignment, visibility and section info.
958   copyGVAttributes(NG, DstGV);
960   AppendingVarInfo AVI;
961   AVI.NewGV = NG;
962   AVI.DstInit = DstGV->getInitializer();
963   AVI.SrcInit = SrcGV->getInitializer();
964   AppendingVars.push_back(AVI);
966   // Replace any uses of the two global variables with uses of the new
967   // global.
968   ValueMap[SrcGV] = ConstantExpr::getBitCast(NG, TypeMap.get(SrcGV->getType()));
970   DstGV->replaceAllUsesWith(ConstantExpr::getBitCast(NG, DstGV->getType()));
971   DstGV->eraseFromParent();
973   // Track the source variable so we don't try to link it.
974   DoNotLinkFromSource.insert(SrcGV);
976   return false;
979 bool ModuleLinker::linkGlobalValueProto(GlobalValue *SGV) {
980   GlobalValue *DGV = getLinkedToGlobal(SGV);
982   // Handle the ultra special appending linkage case first.
983   if (DGV && DGV->hasAppendingLinkage())
984     return linkAppendingVarProto(cast<GlobalVariable>(DGV),
985                                  cast<GlobalVariable>(SGV));
987   bool LinkFromSrc = true;
988   Comdat *C = nullptr;
989   GlobalValue::VisibilityTypes Visibility = SGV->getVisibility();
990   bool HasUnnamedAddr = SGV->hasUnnamedAddr();
992   if (const Comdat *SC = SGV->getComdat()) {
993     Comdat::SelectionKind SK;
994     std::tie(SK, LinkFromSrc) = ComdatsChosen[SC];
995     C = DstM->getOrInsertComdat(SC->getName());
996     C->setSelectionKind(SK);
997   } else if (DGV) {
998     if (shouldLinkFromSource(LinkFromSrc, *DGV, *SGV))
999       return true;
1000   }
1002   if (!LinkFromSrc) {
1003     // Track the source global so that we don't attempt to copy it over when
1004     // processing global initializers.
1005     DoNotLinkFromSource.insert(SGV);
1007     if (DGV)
1008       // Make sure to remember this mapping.
1009       ValueMap[SGV] =
1010           ConstantExpr::getBitCast(DGV, TypeMap.get(SGV->getType()));
1011   }
1013   if (DGV) {
1014     Visibility = isLessConstraining(Visibility, DGV->getVisibility())
1015                      ? DGV->getVisibility()
1016                      : Visibility;
1017     HasUnnamedAddr = HasUnnamedAddr && DGV->hasUnnamedAddr();
1018   }
1020   if (!LinkFromSrc && !DGV)
1021     return false;
1023   GlobalValue *NewGV;
1024   if (auto *SGVar = dyn_cast<GlobalVariable>(SGV)) {
1025     NewGV = linkGlobalVariableProto(SGVar, DGV, LinkFromSrc);
1026     if (!NewGV)
1027       return true;
1028   } else if (auto *SF = dyn_cast<Function>(SGV)) {
1029     NewGV = linkFunctionProto(SF, DGV, LinkFromSrc);
1030   } else {
1031     NewGV = linkGlobalAliasProto(cast<GlobalAlias>(SGV), DGV, LinkFromSrc);
1032   }
1034   if (NewGV) {
1035     if (NewGV != DGV)
1036       copyGVAttributes(NewGV, SGV);
1038     NewGV->setUnnamedAddr(HasUnnamedAddr);
1039     NewGV->setVisibility(Visibility);
1041     if (auto *NewGO = dyn_cast<GlobalObject>(NewGV)) {
1042       if (C)
1043         NewGO->setComdat(C);
1045       if (DGV && DGV->hasCommonLinkage() && SGV->hasCommonLinkage())
1046         NewGO->setAlignment(std::max(DGV->getAlignment(), SGV->getAlignment()));
1047     }
1049     // Make sure to remember this mapping.
1050     if (NewGV != DGV) {
1051       if (DGV) {
1052         DGV->replaceAllUsesWith(
1053             ConstantExpr::getBitCast(NewGV, DGV->getType()));
1054         DGV->eraseFromParent();
1055       }
1056       ValueMap[SGV] = NewGV;
1057     }
1058   }
1060   return false;
1063 /// Loop through the global variables in the src module and merge them into the
1064 /// dest module.
1065 GlobalValue *ModuleLinker::linkGlobalVariableProto(const GlobalVariable *SGVar,
1066                                                    GlobalValue *DGV,
1067                                                    bool LinkFromSrc) {
1068   bool ClearConstant = false;
1070   if (DGV) {
1071     auto *DGVar = dyn_cast<GlobalVariable>(DGV);
1072     if (!SGVar->isConstant() || (DGVar && !DGVar->isConstant()))
1073       ClearConstant = true;
1074   }
1076   if (!LinkFromSrc) {
1077     if (auto *NewGVar = dyn_cast<GlobalVariable>(DGV)) {
1078       if (NewGVar->isDeclaration() && ClearConstant)
1079         NewGVar->setConstant(false);
1080     }
1081     return DGV;
1082   }
1084   // No linking to be performed or linking from the source: simply create an
1085   // identical version of the symbol over in the dest module... the
1086   // initializer will be filled in later by LinkGlobalInits.
1087   GlobalVariable *NewDGV = new GlobalVariable(
1088       *DstM, TypeMap.get(SGVar->getType()->getElementType()),
1089       SGVar->isConstant(), SGVar->getLinkage(), /*init*/ nullptr,
1090       SGVar->getName(), /*insertbefore*/ nullptr, SGVar->getThreadLocalMode(),
1091       SGVar->getType()->getAddressSpace());
1093   return NewDGV;
1096 /// Link the function in the source module into the destination module if
1097 /// needed, setting up mapping information.
1098 GlobalValue *ModuleLinker::linkFunctionProto(const Function *SF,
1099                                              GlobalValue *DGV,
1100                                              bool LinkFromSrc) {
1101   if (!LinkFromSrc)
1102     return DGV;
1104   // If the function is to be lazily linked, don't create it just yet.
1105   // The ValueMaterializerTy will deal with creating it if it's used.
1106   if (!DGV && (SF->hasLocalLinkage() || SF->hasLinkOnceLinkage() ||
1107                SF->hasAvailableExternallyLinkage())) {
1108     DoNotLinkFromSource.insert(SF);
1109     return nullptr;
1110   }
1112   // If there is no linkage to be performed or we are linking from the source,
1113   // bring SF over.
1114   return Function::Create(TypeMap.get(SF->getFunctionType()), SF->getLinkage(),
1115                           SF->getName(), DstM);
1118 /// Set up prototypes for any aliases that come over from the source module.
1119 GlobalValue *ModuleLinker::linkGlobalAliasProto(const GlobalAlias *SGA,
1120                                                 GlobalValue *DGV,
1121                                                 bool LinkFromSrc) {
1122   if (!LinkFromSrc)
1123     return DGV;
1125   // If there is no linkage to be performed or we're linking from the source,
1126   // bring over SGA.
1127   auto *PTy = cast<PointerType>(TypeMap.get(SGA->getType()));
1128   return GlobalAlias::create(PTy->getElementType(), PTy->getAddressSpace(),
1129                              SGA->getLinkage(), SGA->getName(), DstM);
1132 static void getArrayElements(const Constant *C,
1133                              SmallVectorImpl<Constant *> &Dest) {
1134   unsigned NumElements = cast<ArrayType>(C->getType())->getNumElements();
1136   for (unsigned i = 0; i != NumElements; ++i)
1137     Dest.push_back(C->getAggregateElement(i));
1140 void ModuleLinker::linkAppendingVarInit(const AppendingVarInfo &AVI) {
1141   // Merge the initializer.
1142   SmallVector<Constant *, 16> DstElements;
1143   getArrayElements(AVI.DstInit, DstElements);
1145   SmallVector<Constant *, 16> SrcElements;
1146   getArrayElements(AVI.SrcInit, SrcElements);
1148   ArrayType *NewType = cast<ArrayType>(AVI.NewGV->getType()->getElementType());
1150   StringRef Name = AVI.NewGV->getName();
1151   bool IsNewStructor =
1152       (Name == "llvm.global_ctors" || Name == "llvm.global_dtors") &&
1153       cast<StructType>(NewType->getElementType())->getNumElements() == 3;
1155   for (auto *V : SrcElements) {
1156     if (IsNewStructor) {
1157       Constant *Key = V->getAggregateElement(2);
1158       if (DoNotLinkFromSource.count(Key))
1159         continue;
1160     }
1161     DstElements.push_back(
1162         MapValue(V, ValueMap, RF_None, &TypeMap, &ValMaterializer));
1163   }
1164   if (IsNewStructor) {
1165     NewType = ArrayType::get(NewType->getElementType(), DstElements.size());
1166     AVI.NewGV->mutateType(PointerType::get(NewType, 0));
1167   }
1169   AVI.NewGV->setInitializer(ConstantArray::get(NewType, DstElements));
1172 /// Update the initializers in the Dest module now that all globals that may be
1173 /// referenced are in Dest.
1174 void ModuleLinker::linkGlobalInits() {
1175   // Loop over all of the globals in the src module, mapping them over as we go
1176   for (Module::const_global_iterator I = SrcM->global_begin(),
1177        E = SrcM->global_end(); I != E; ++I) {
1179     // Only process initialized GV's or ones not already in dest.
1180     if (!I->hasInitializer() || DoNotLinkFromSource.count(I)) continue;
1182     // Grab destination global variable.
1183     GlobalVariable *DGV = cast<GlobalVariable>(ValueMap[I]);
1184     // Figure out what the initializer looks like in the dest module.
1185     DGV->setInitializer(MapValue(I->getInitializer(), ValueMap,
1186                                  RF_None, &TypeMap, &ValMaterializer));
1187   }
1190 /// Copy the source function over into the dest function and fix up references
1191 /// to values. At this point we know that Dest is an external function, and
1192 /// that Src is not.
1193 void ModuleLinker::linkFunctionBody(Function *Dst, Function *Src) {
1194   assert(Src && Dst && Dst->isDeclaration() && !Src->isDeclaration());
1196   // Go through and convert function arguments over, remembering the mapping.
1197   Function::arg_iterator DI = Dst->arg_begin();
1198   for (Function::arg_iterator I = Src->arg_begin(), E = Src->arg_end();
1199        I != E; ++I, ++DI) {
1200     DI->setName(I->getName());  // Copy the name over.
1202     // Add a mapping to our mapping.
1203     ValueMap[I] = DI;
1204   }
1206   // Splice the body of the source function into the dest function.
1207   Dst->getBasicBlockList().splice(Dst->end(), Src->getBasicBlockList());
1209   // At this point, all of the instructions and values of the function are now
1210   // copied over.  The only problem is that they are still referencing values in
1211   // the Source function as operands.  Loop through all of the operands of the
1212   // functions and patch them up to point to the local versions.
1213   for (Function::iterator BB = Dst->begin(), BE = Dst->end(); BB != BE; ++BB)
1214     for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
1215       RemapInstruction(I, ValueMap, RF_IgnoreMissingEntries, &TypeMap,
1216                        &ValMaterializer);
1218   // There is no need to map the arguments anymore.
1219   for (Function::arg_iterator I = Src->arg_begin(), E = Src->arg_end();
1220        I != E; ++I)
1221     ValueMap.erase(I);
1225 /// Insert all of the aliases in Src into the Dest module.
1226 void ModuleLinker::linkAliasBodies() {
1227   for (Module::alias_iterator I = SrcM->alias_begin(), E = SrcM->alias_end();
1228        I != E; ++I) {
1229     if (DoNotLinkFromSource.count(I))
1230       continue;
1231     if (Constant *Aliasee = I->getAliasee()) {
1232       GlobalAlias *DA = cast<GlobalAlias>(ValueMap[I]);
1233       Constant *Val =
1234           MapValue(Aliasee, ValueMap, RF_None, &TypeMap, &ValMaterializer);
1235       DA->setAliasee(Val);
1236     }
1237   }
1240 /// Insert all of the named MDNodes in Src into the Dest module.
1241 void ModuleLinker::linkNamedMDNodes() {
1242   const NamedMDNode *SrcModFlags = SrcM->getModuleFlagsMetadata();
1243   for (Module::const_named_metadata_iterator I = SrcM->named_metadata_begin(),
1244        E = SrcM->named_metadata_end(); I != E; ++I) {
1245     // Don't link module flags here. Do them separately.
1246     if (&*I == SrcModFlags) continue;
1247     NamedMDNode *DestNMD = DstM->getOrInsertNamedMetadata(I->getName());
1248     // Add Src elements into Dest node.
1249     for (unsigned i = 0, e = I->getNumOperands(); i != e; ++i)
1250       DestNMD->addOperand(MapValue(I->getOperand(i), ValueMap,
1251                                    RF_None, &TypeMap, &ValMaterializer));
1252   }
1255 /// Merge the linker flags in Src into the Dest module.
1256 bool ModuleLinker::linkModuleFlagsMetadata() {
1257   // If the source module has no module flags, we are done.
1258   const NamedMDNode *SrcModFlags = SrcM->getModuleFlagsMetadata();
1259   if (!SrcModFlags) return false;
1261   // If the destination module doesn't have module flags yet, then just copy
1262   // over the source module's flags.
1263   NamedMDNode *DstModFlags = DstM->getOrInsertModuleFlagsMetadata();
1264   if (DstModFlags->getNumOperands() == 0) {
1265     for (unsigned I = 0, E = SrcModFlags->getNumOperands(); I != E; ++I)
1266       DstModFlags->addOperand(SrcModFlags->getOperand(I));
1268     return false;
1269   }
1271   // First build a map of the existing module flags and requirements.
1272   DenseMap<MDString*, MDNode*> Flags;
1273   SmallSetVector<MDNode*, 16> Requirements;
1274   for (unsigned I = 0, E = DstModFlags->getNumOperands(); I != E; ++I) {
1275     MDNode *Op = DstModFlags->getOperand(I);
1276     ConstantInt *Behavior = cast<ConstantInt>(Op->getOperand(0));
1277     MDString *ID = cast<MDString>(Op->getOperand(1));
1279     if (Behavior->getZExtValue() == Module::Require) {
1280       Requirements.insert(cast<MDNode>(Op->getOperand(2)));
1281     } else {
1282       Flags[ID] = Op;
1283     }
1284   }
1286   // Merge in the flags from the source module, and also collect its set of
1287   // requirements.
1288   bool HasErr = false;
1289   for (unsigned I = 0, E = SrcModFlags->getNumOperands(); I != E; ++I) {
1290     MDNode *SrcOp = SrcModFlags->getOperand(I);
1291     ConstantInt *SrcBehavior = cast<ConstantInt>(SrcOp->getOperand(0));
1292     MDString *ID = cast<MDString>(SrcOp->getOperand(1));
1293     MDNode *DstOp = Flags.lookup(ID);
1294     unsigned SrcBehaviorValue = SrcBehavior->getZExtValue();
1296     // If this is a requirement, add it and continue.
1297     if (SrcBehaviorValue == Module::Require) {
1298       // If the destination module does not already have this requirement, add
1299       // it.
1300       if (Requirements.insert(cast<MDNode>(SrcOp->getOperand(2)))) {
1301         DstModFlags->addOperand(SrcOp);
1302       }
1303       continue;
1304     }
1306     // If there is no existing flag with this ID, just add it.
1307     if (!DstOp) {
1308       Flags[ID] = SrcOp;
1309       DstModFlags->addOperand(SrcOp);
1310       continue;
1311     }
1313     // Otherwise, perform a merge.
1314     ConstantInt *DstBehavior = cast<ConstantInt>(DstOp->getOperand(0));
1315     unsigned DstBehaviorValue = DstBehavior->getZExtValue();
1317     // If either flag has override behavior, handle it first.
1318     if (DstBehaviorValue == Module::Override) {
1319       // Diagnose inconsistent flags which both have override behavior.
1320       if (SrcBehaviorValue == Module::Override &&
1321           SrcOp->getOperand(2) != DstOp->getOperand(2)) {
1322         HasErr |= emitError("linking module flags '" + ID->getString() +
1323                             "': IDs have conflicting override values");
1324       }
1325       continue;
1326     } else if (SrcBehaviorValue == Module::Override) {
1327       // Update the destination flag to that of the source.
1328       DstOp->replaceOperandWith(0, SrcBehavior);
1329       DstOp->replaceOperandWith(2, SrcOp->getOperand(2));
1330       continue;
1331     }
1333     // Diagnose inconsistent merge behavior types.
1334     if (SrcBehaviorValue != DstBehaviorValue) {
1335       HasErr |= emitError("linking module flags '" + ID->getString() +
1336                           "': IDs have conflicting behaviors");
1337       continue;
1338     }
1340     // Perform the merge for standard behavior types.
1341     switch (SrcBehaviorValue) {
1342     case Module::Require:
1343     case Module::Override: llvm_unreachable("not possible");
1344     case Module::Error: {
1345       // Emit an error if the values differ.
1346       if (SrcOp->getOperand(2) != DstOp->getOperand(2)) {
1347         HasErr |= emitError("linking module flags '" + ID->getString() +
1348                             "': IDs have conflicting values");
1349       }
1350       continue;
1351     }
1352     case Module::Warning: {
1353       // Emit a warning if the values differ.
1354       if (SrcOp->getOperand(2) != DstOp->getOperand(2)) {
1355         emitWarning("linking module flags '" + ID->getString() +
1356                     "': IDs have conflicting values");
1357       }
1358       continue;
1359     }
1360     case Module::Append: {
1361       MDNode *DstValue = cast<MDNode>(DstOp->getOperand(2));
1362       MDNode *SrcValue = cast<MDNode>(SrcOp->getOperand(2));
1363       unsigned NumOps = DstValue->getNumOperands() + SrcValue->getNumOperands();
1364       Value **VP, **Values = VP = new Value*[NumOps];
1365       for (unsigned i = 0, e = DstValue->getNumOperands(); i != e; ++i, ++VP)
1366         *VP = DstValue->getOperand(i);
1367       for (unsigned i = 0, e = SrcValue->getNumOperands(); i != e; ++i, ++VP)
1368         *VP = SrcValue->getOperand(i);
1369       DstOp->replaceOperandWith(2, MDNode::get(DstM->getContext(),
1370                                                ArrayRef<Value*>(Values,
1371                                                                 NumOps)));
1372       delete[] Values;
1373       break;
1374     }
1375     case Module::AppendUnique: {
1376       SmallSetVector<Value*, 16> Elts;
1377       MDNode *DstValue = cast<MDNode>(DstOp->getOperand(2));
1378       MDNode *SrcValue = cast<MDNode>(SrcOp->getOperand(2));
1379       for (unsigned i = 0, e = DstValue->getNumOperands(); i != e; ++i)
1380         Elts.insert(DstValue->getOperand(i));
1381       for (unsigned i = 0, e = SrcValue->getNumOperands(); i != e; ++i)
1382         Elts.insert(SrcValue->getOperand(i));
1383       DstOp->replaceOperandWith(2, MDNode::get(DstM->getContext(),
1384                                                ArrayRef<Value*>(Elts.begin(),
1385                                                                 Elts.end())));
1386       break;
1387     }
1388     }
1389   }
1391   // Check all of the requirements.
1392   for (unsigned I = 0, E = Requirements.size(); I != E; ++I) {
1393     MDNode *Requirement = Requirements[I];
1394     MDString *Flag = cast<MDString>(Requirement->getOperand(0));
1395     Value *ReqValue = Requirement->getOperand(1);
1397     MDNode *Op = Flags[Flag];
1398     if (!Op || Op->getOperand(2) != ReqValue) {
1399       HasErr |= emitError("linking module flags '" + Flag->getString() +
1400                           "': does not have the required value");
1401       continue;
1402     }
1403   }
1405   return HasErr;
1408 bool ModuleLinker::run() {
1409   assert(DstM && "Null destination module");
1410   assert(SrcM && "Null source module");
1412   // Inherit the target data from the source module if the destination module
1413   // doesn't have one already.
1414   if (!DstM->getDataLayout() && SrcM->getDataLayout())
1415     DstM->setDataLayout(SrcM->getDataLayout());
1417   // Copy the target triple from the source to dest if the dest's is empty.
1418   if (DstM->getTargetTriple().empty() && !SrcM->getTargetTriple().empty())
1419     DstM->setTargetTriple(SrcM->getTargetTriple());
1421   if (SrcM->getDataLayout() && DstM->getDataLayout() &&
1422       *SrcM->getDataLayout() != *DstM->getDataLayout()) {
1423     emitWarning("Linking two modules of different data layouts: '" +
1424                 SrcM->getModuleIdentifier() + "' is '" +
1425                 SrcM->getDataLayoutStr() + "' whereas '" +
1426                 DstM->getModuleIdentifier() + "' is '" +
1427                 DstM->getDataLayoutStr() + "'\n");
1428   }
1429   if (!SrcM->getTargetTriple().empty() &&
1430       DstM->getTargetTriple() != SrcM->getTargetTriple()) {
1431     emitWarning("Linking two modules of different target triples: " +
1432                 SrcM->getModuleIdentifier() + "' is '" +
1433                 SrcM->getTargetTriple() + "' whereas '" +
1434                 DstM->getModuleIdentifier() + "' is '" +
1435                 DstM->getTargetTriple() + "'\n");
1436   }
1438   // Append the module inline asm string.
1439   if (!SrcM->getModuleInlineAsm().empty()) {
1440     if (DstM->getModuleInlineAsm().empty())
1441       DstM->setModuleInlineAsm(SrcM->getModuleInlineAsm());
1442     else
1443       DstM->setModuleInlineAsm(DstM->getModuleInlineAsm()+"\n"+
1444                                SrcM->getModuleInlineAsm());
1445   }
1447   // Loop over all of the linked values to compute type mappings.
1448   computeTypeMapping();
1450   ComdatsChosen.clear();
1451   for (const auto &SMEC : SrcM->getComdatSymbolTable()) {
1452     const Comdat &C = SMEC.getValue();
1453     if (ComdatsChosen.count(&C))
1454       continue;
1455     Comdat::SelectionKind SK;
1456     bool LinkFromSrc;
1457     if (getComdatResult(&C, SK, LinkFromSrc))
1458       return true;
1459     ComdatsChosen[&C] = std::make_pair(SK, LinkFromSrc);
1460   }
1462   // Upgrade mismatched global arrays.
1463   upgradeMismatchedGlobals();
1465   // Insert all of the globals in src into the DstM module... without linking
1466   // initializers (which could refer to functions not yet mapped over).
1467   for (Module::global_iterator I = SrcM->global_begin(),
1468        E = SrcM->global_end(); I != E; ++I)
1469     if (linkGlobalValueProto(I))
1470       return true;
1472   // Link the functions together between the two modules, without doing function
1473   // bodies... this just adds external function prototypes to the DstM
1474   // function...  We do this so that when we begin processing function bodies,
1475   // all of the global values that may be referenced are available in our
1476   // ValueMap.
1477   for (Module::iterator I = SrcM->begin(), E = SrcM->end(); I != E; ++I)
1478     if (linkGlobalValueProto(I))
1479       return true;
1481   // If there were any aliases, link them now.
1482   for (Module::alias_iterator I = SrcM->alias_begin(),
1483        E = SrcM->alias_end(); I != E; ++I)
1484     if (linkGlobalValueProto(I))
1485       return true;
1487   for (unsigned i = 0, e = AppendingVars.size(); i != e; ++i)
1488     linkAppendingVarInit(AppendingVars[i]);
1490   // Link in the function bodies that are defined in the source module into
1491   // DstM.
1492   for (Module::iterator SF = SrcM->begin(), E = SrcM->end(); SF != E; ++SF) {
1493     // Skip if not linking from source.
1494     if (DoNotLinkFromSource.count(SF)) continue;
1496     Function *DF = cast<Function>(ValueMap[SF]);
1498     // Link in the prefix data.
1499     if (SF->hasPrefixData())
1500       DF->setPrefixData(MapValue(
1501           SF->getPrefixData(), ValueMap, RF_None, &TypeMap, &ValMaterializer));
1503     // Link in the prologue data.
1504     if (SF->hasPrologueData())
1505       DF->setPrologueData(MapValue(
1506           SF->getPrologueData(), ValueMap, RF_None, &TypeMap, &ValMaterializer));
1508     // Materialize if needed.
1509     if (std::error_code EC = SF->materialize())
1510       return emitError(EC.message());
1512     // Skip if no body (function is external).
1513     if (SF->isDeclaration())
1514       continue;
1516     linkFunctionBody(DF, SF);
1517     SF->Dematerialize();
1518   }
1520   // Resolve all uses of aliases with aliasees.
1521   linkAliasBodies();
1523   // Remap all of the named MDNodes in Src into the DstM module. We do this
1524   // after linking GlobalValues so that MDNodes that reference GlobalValues
1525   // are properly remapped.
1526   linkNamedMDNodes();
1528   // Merge the module flags into the DstM module.
1529   if (linkModuleFlagsMetadata())
1530     return true;
1532   // Update the initializers in the DstM module now that all globals that may
1533   // be referenced are in DstM.
1534   linkGlobalInits();
1536   // Process vector of lazily linked in functions.
1537   bool LinkedInAnyFunctions;
1538   do {
1539     LinkedInAnyFunctions = false;
1541     for(std::vector<Function*>::iterator I = LazilyLinkFunctions.begin(),
1542         E = LazilyLinkFunctions.end(); I != E; ++I) {
1543       Function *SF = *I;
1544       if (!SF)
1545         continue;
1547       Function *DF = cast<Function>(ValueMap[SF]);
1548       if (SF->hasPrefixData()) {
1549         // Link in the prefix data.
1550         DF->setPrefixData(MapValue(SF->getPrefixData(),
1551                                    ValueMap,
1552                                    RF_None,
1553                                    &TypeMap,
1554                                    &ValMaterializer));
1555       }
1557       // Materialize if needed.
1558       if (std::error_code EC = SF->materialize())
1559         return emitError(EC.message());
1561       // Skip if no body (function is external).
1562       if (SF->isDeclaration())
1563         continue;
1565       // Erase from vector *before* the function body is linked - linkFunctionBody could
1566       // invalidate I.
1567       LazilyLinkFunctions.erase(I);
1569       // Link in function body.
1570       linkFunctionBody(DF, SF);
1571       SF->Dematerialize();
1573       // Set flag to indicate we may have more functions to lazily link in
1574       // since we linked in a function.
1575       LinkedInAnyFunctions = true;
1576       break;
1577     }
1578   } while (LinkedInAnyFunctions);
1580   return false;
1583 Linker::StructTypeKeyInfo::KeyTy::KeyTy(ArrayRef<Type *> E, bool P)
1584     : ETypes(E), IsPacked(P) {}
1586 Linker::StructTypeKeyInfo::KeyTy::KeyTy(const StructType *ST)
1587     : ETypes(ST->elements()), IsPacked(ST->isPacked()) {}
1589 bool Linker::StructTypeKeyInfo::KeyTy::operator==(const KeyTy &That) const {
1590   if (IsPacked != That.IsPacked)
1591     return false;
1592   if (ETypes != That.ETypes)
1593     return false;
1594   return true;
1597 bool Linker::StructTypeKeyInfo::KeyTy::operator!=(const KeyTy &That) const {
1598   return !this->operator==(That);
1601 StructType *Linker::StructTypeKeyInfo::getEmptyKey() {
1602   return DenseMapInfo<StructType *>::getEmptyKey();
1605 StructType *Linker::StructTypeKeyInfo::getTombstoneKey() {
1606   return DenseMapInfo<StructType *>::getTombstoneKey();
1609 unsigned Linker::StructTypeKeyInfo::getHashValue(const KeyTy &Key) {
1610   return hash_combine(hash_combine_range(Key.ETypes.begin(), Key.ETypes.end()),
1611                       Key.IsPacked);
1614 unsigned Linker::StructTypeKeyInfo::getHashValue(const StructType *ST) {
1615   return getHashValue(KeyTy(ST));
1618 bool Linker::StructTypeKeyInfo::isEqual(const KeyTy &LHS,
1619                                         const StructType *RHS) {
1620   if (RHS == getEmptyKey() || RHS == getTombstoneKey())
1621     return false;
1622   return LHS == KeyTy(RHS);
1625 bool Linker::StructTypeKeyInfo::isEqual(const StructType *LHS,
1626                                         const StructType *RHS) {
1627   if (RHS == getEmptyKey())
1628     return LHS == getEmptyKey();
1630   if (RHS == getTombstoneKey())
1631     return LHS == getTombstoneKey();
1633   return KeyTy(LHS) == KeyTy(RHS);
1636 void Linker::IdentifiedStructTypeSet::addNonOpaque(StructType *Ty) {
1637   assert(!Ty->isOpaque());
1638   bool &Entry = NonOpaqueStructTypes[Ty];
1639   Entry = true;
1642 void Linker::IdentifiedStructTypeSet::addOpaque(StructType *Ty) {
1643   assert(Ty->isOpaque());
1644   OpaqueStructTypes.insert(Ty);
1647 StructType *
1648 Linker::IdentifiedStructTypeSet::findNonOpaque(ArrayRef<Type *> ETypes,
1649                                                bool IsPacked) {
1650   Linker::StructTypeKeyInfo::KeyTy Key(ETypes, IsPacked);
1651   auto I = NonOpaqueStructTypes.find_as(Key);
1652   if (I == NonOpaqueStructTypes.end())
1653     return nullptr;
1654   return I->first;
1657 bool Linker::IdentifiedStructTypeSet::hasType(StructType *Ty) {
1658   if (Ty->isOpaque())
1659     return OpaqueStructTypes.count(Ty);
1660   auto I = NonOpaqueStructTypes.find(Ty);
1661   if (I == NonOpaqueStructTypes.end())
1662     return false;
1663   return I->first == Ty;
1666 void Linker::init(Module *M, DiagnosticHandlerFunction DiagnosticHandler) {
1667   this->Composite = M;
1668   this->DiagnosticHandler = DiagnosticHandler;
1670   TypeFinder StructTypes;
1671   StructTypes.run(*M, true);
1672   for (StructType *Ty : StructTypes) {
1673     if (Ty->isOpaque())
1674       IdentifiedStructTypes.addOpaque(Ty);
1675     else
1676       IdentifiedStructTypes.addNonOpaque(Ty);
1677   }
1680 Linker::Linker(Module *M, DiagnosticHandlerFunction DiagnosticHandler) {
1681   init(M, DiagnosticHandler);
1684 Linker::Linker(Module *M) {
1685   init(M, [this](const DiagnosticInfo &DI) {
1686     Composite->getContext().diagnose(DI);
1687   });
1690 Linker::~Linker() {
1693 void Linker::deleteModule() {
1694   delete Composite;
1695   Composite = nullptr;
1698 bool Linker::linkInModule(Module *Src) {
1699   ModuleLinker TheLinker(Composite, IdentifiedStructTypes, Src,
1700                          DiagnosticHandler);
1701   return TheLinker.run();
1704 //===----------------------------------------------------------------------===//
1705 // LinkModules entrypoint.
1706 //===----------------------------------------------------------------------===//
1708 /// This function links two modules together, with the resulting Dest module
1709 /// modified to be the composite of the two input modules. If an error occurs,
1710 /// true is returned and ErrorMsg (if not null) is set to indicate the problem.
1711 /// Upon failure, the Dest module could be in a modified state, and shouldn't be
1712 /// relied on to be consistent.
1713 bool Linker::LinkModules(Module *Dest, Module *Src,
1714                          DiagnosticHandlerFunction DiagnosticHandler) {
1715   Linker L(Dest, DiagnosticHandler);
1716   return L.linkInModule(Src);
1719 bool Linker::LinkModules(Module *Dest, Module *Src) {
1720   Linker L(Dest);
1721   return L.linkInModule(Src);
1724 //===----------------------------------------------------------------------===//
1725 // C API.
1726 //===----------------------------------------------------------------------===//
1728 LLVMBool LLVMLinkModules(LLVMModuleRef Dest, LLVMModuleRef Src,
1729                          LLVMLinkerMode Mode, char **OutMessages) {
1730   Module *D = unwrap(Dest);
1731   std::string Message;
1732   raw_string_ostream Stream(Message);
1733   DiagnosticPrinterRawOStream DP(Stream);
1735   LLVMBool Result = Linker::LinkModules(
1736       D, unwrap(Src), [&](const DiagnosticInfo &DI) { DI.print(DP); });
1738   if (OutMessages && Result)
1739     *OutMessages = strdup(Message.c_str());
1740   return Result;