1 //===- lib/MC/MCWinEH.cpp - Windows EH implementation ---------------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #include "llvm/ADT/StringRef.h"
11 #include "llvm/MC/MCContext.h"
12 #include "llvm/MC/MCObjectFileInfo.h"
13 #include "llvm/MC/MCSectionCOFF.h"
14 #include "llvm/MC/MCSymbol.h"
15 #include "llvm/MC/MCWinEH.h"
16 #include "llvm/Support/COFF.h"
18 namespace llvm {
19 namespace WinEH {
21 /// We can't have one section for all .pdata or .xdata because the Microsoft
22 /// linker seems to want all code relocations to refer to the same object file
23 /// section. If the code described is comdat, create a new comdat section
24 /// associated with that comdat. If the code described is not in the main .text
25 /// section, make a new section for it. Otherwise use the main unwind info
26 /// section.
27 static const MCSection *getUnwindInfoSection(
28 StringRef SecName, const MCSectionCOFF *UnwindSec, const MCSymbol *Function,
29 MCContext &Context) {
30 if (Function && Function->isInSection()) {
31 // If Function is in a COMDAT, get or create an unwind info section in that
32 // COMDAT group.
33 const MCSectionCOFF *FunctionSection =
34 cast<MCSectionCOFF>(&Function->getSection());
35 if (FunctionSection->getCharacteristics() & COFF::IMAGE_SCN_LNK_COMDAT) {
36 return Context.getAssociativeCOFFSection(
37 UnwindSec, FunctionSection->getCOMDATSymbol());
38 }
40 // If Function is in a section other than .text, create a new .pdata section.
41 // Otherwise use the plain .pdata section.
42 if (const auto *Section = dyn_cast<MCSectionCOFF>(FunctionSection)) {
43 StringRef CodeSecName = Section->getSectionName();
44 if (CodeSecName == ".text")
45 return UnwindSec;
47 if (CodeSecName.startswith(".text$"))
48 CodeSecName = CodeSecName.substr(6);
50 return Context.getCOFFSection(
51 (SecName + Twine('$') + CodeSecName).str(),
52 COFF::IMAGE_SCN_CNT_INITIALIZED_DATA | COFF::IMAGE_SCN_MEM_READ,
53 SectionKind::getDataRel());
54 }
55 }
57 return UnwindSec;
59 }
61 const MCSection *UnwindEmitter::getPDataSection(const MCSymbol *Function,
62 MCContext &Context) {
63 const MCSectionCOFF *PData =
64 cast<MCSectionCOFF>(Context.getObjectFileInfo()->getPDataSection());
65 return getUnwindInfoSection(".pdata", PData, Function, Context);
66 }
68 const MCSection *UnwindEmitter::getXDataSection(const MCSymbol *Function,
69 MCContext &Context) {
70 const MCSectionCOFF *XData =
71 cast<MCSectionCOFF>(Context.getObjectFileInfo()->getXDataSection());
72 return getUnwindInfoSection(".xdata", XData, Function, Context);
73 }
75 }
76 }