d4c742bb4494c2a032f3f48bf73d836fe8c5ca34
1 //===-- AArch64A57FPLoadBalancing.cpp - Balance FP ops statically on A57---===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 // For best-case performance on Cortex-A57, we should try to use a balanced
10 // mix of odd and even D-registers when performing a critical sequence of
11 // independent, non-quadword FP/ASIMD floating-point multiply or
12 // multiply-accumulate operations.
13 //
14 // This pass attempts to detect situations where the register allocation may
15 // adversely affect this load balancing and to change the registers used so as
16 // to better utilize the CPU.
17 //
18 // Ideally we'd just take each multiply or multiply-accumulate in turn and
19 // allocate it alternating even or odd registers. However, multiply-accumulates
20 // are most efficiently performed in the same functional unit as their
21 // accumulation operand. Therefore this pass tries to find maximal sequences
22 // ("Chains") of multiply-accumulates linked via their accumulation operand,
23 // and assign them all the same "color" (oddness/evenness).
24 //
25 // This optimization affects S-register and D-register floating point
26 // multiplies and FMADD/FMAs, as well as vector (floating point only) muls and
27 // FMADD/FMA. Q register instructions (and 128-bit vector instructions) are
28 // not affected.
29 //===----------------------------------------------------------------------===//
31 #include "AArch64.h"
32 #include "AArch64InstrInfo.h"
33 #include "AArch64Subtarget.h"
34 #include "llvm/ADT/BitVector.h"
35 #include "llvm/ADT/EquivalenceClasses.h"
36 #include "llvm/CodeGen/MachineFunction.h"
37 #include "llvm/CodeGen/MachineFunctionPass.h"
38 #include "llvm/CodeGen/MachineInstr.h"
39 #include "llvm/CodeGen/MachineInstrBuilder.h"
40 #include "llvm/CodeGen/MachineRegisterInfo.h"
41 #include "llvm/CodeGen/RegisterScavenging.h"
42 #include "llvm/CodeGen/RegisterClassInfo.h"
43 #include "llvm/Support/CommandLine.h"
44 #include "llvm/Support/Debug.h"
45 #include "llvm/Support/raw_ostream.h"
46 #include <list>
47 using namespace llvm;
49 #define DEBUG_TYPE "aarch64-a57-fp-load-balancing"
51 // Enforce the algorithm to use the scavenged register even when the original
52 // destination register is the correct color. Used for testing.
53 static cl::opt<bool>
54 TransformAll("aarch64-a57-fp-load-balancing-force-all",
55 cl::desc("Always modify dest registers regardless of color"),
56 cl::init(false), cl::Hidden);
58 // Never use the balance information obtained from chains - return a specific
59 // color always. Used for testing.
60 static cl::opt<unsigned>
61 OverrideBalance("aarch64-a57-fp-load-balancing-override",
62 cl::desc("Ignore balance information, always return "
63 "(1: Even, 2: Odd)."),
64 cl::init(0), cl::Hidden);
66 //===----------------------------------------------------------------------===//
67 // Helper functions
69 // Is the instruction a type of multiply on 64-bit (or 32-bit) FPRs?
70 static bool isMul(MachineInstr *MI) {
71 switch (MI->getOpcode()) {
72 case AArch64::FMULSrr:
73 case AArch64::FNMULSrr:
74 case AArch64::FMULDrr:
75 case AArch64::FNMULDrr:
76 return true;
77 default:
78 return false;
79 }
80 }
82 // Is the instruction a type of FP multiply-accumulate on 64-bit (or 32-bit) FPRs?
83 static bool isMla(MachineInstr *MI) {
84 switch (MI->getOpcode()) {
85 case AArch64::FMSUBSrrr:
86 case AArch64::FMADDSrrr:
87 case AArch64::FNMSUBSrrr:
88 case AArch64::FNMADDSrrr:
89 case AArch64::FMSUBDrrr:
90 case AArch64::FMADDDrrr:
91 case AArch64::FNMSUBDrrr:
92 case AArch64::FNMADDDrrr:
93 return true;
94 default:
95 return false;
96 }
97 }
99 //===----------------------------------------------------------------------===//
101 namespace {
102 /// A "color", which is either even or odd. Yes, these aren't really colors
103 /// but the algorithm is conceptually doing two-color graph coloring.
104 enum class Color { Even, Odd };
105 #ifndef NDEBUG
106 static const char *ColorNames[2] = { "Even", "Odd" };
107 #endif
109 class Chain;
111 class AArch64A57FPLoadBalancing : public MachineFunctionPass {
112 const AArch64InstrInfo *TII;
113 MachineRegisterInfo *MRI;
114 const TargetRegisterInfo *TRI;
115 RegisterClassInfo RCI;
117 public:
118 static char ID;
119 explicit AArch64A57FPLoadBalancing() : MachineFunctionPass(ID) {}
121 bool runOnMachineFunction(MachineFunction &F) override;
123 const char *getPassName() const override {
124 return "A57 FP Anti-dependency breaker";
125 }
127 void getAnalysisUsage(AnalysisUsage &AU) const override {
128 AU.setPreservesCFG();
129 MachineFunctionPass::getAnalysisUsage(AU);
130 }
132 private:
133 bool runOnBasicBlock(MachineBasicBlock &MBB);
134 bool colorChainSet(std::vector<Chain*> GV, MachineBasicBlock &MBB,
135 int &Balance);
136 bool colorChain(Chain *G, Color C, MachineBasicBlock &MBB);
137 int scavengeRegister(Chain *G, Color C, MachineBasicBlock &MBB);
138 void scanInstruction(MachineInstr *MI, unsigned Idx,
139 std::map<unsigned, Chain*> &Active,
140 std::set<std::unique_ptr<Chain>> &AllChains);
141 void maybeKillChain(MachineOperand &MO, unsigned Idx,
142 std::map<unsigned, Chain*> &RegChains);
143 Color getColor(unsigned Register);
144 Chain *getAndEraseNext(Color PreferredColor, std::vector<Chain*> &L);
145 };
146 char AArch64A57FPLoadBalancing::ID = 0;
148 /// A Chain is a sequence of instructions that are linked together by
149 /// an accumulation operand. For example:
150 ///
151 /// fmul d0<def>, ?
152 /// fmla d1<def>, ?, ?, d0<kill>
153 /// fmla d2<def>, ?, ?, d1<kill>
154 ///
155 /// There may be other instructions interleaved in the sequence that
156 /// do not belong to the chain. These other instructions must not use
157 /// the "chain" register at any point.
158 ///
159 /// We currently only support chains where the "chain" operand is killed
160 /// at each link in the chain for simplicity.
161 /// A chain has three important instructions - Start, Last and Kill.
162 /// * The start instruction is the first instruction in the chain.
163 /// * Last is the final instruction in the chain.
164 /// * Kill may or may not be defined. If defined, Kill is the instruction
165 /// where the outgoing value of the Last instruction is killed.
166 /// This information is important as if we know the outgoing value is
167 /// killed with no intervening uses, we can safely change its register.
168 ///
169 /// Without a kill instruction, we must assume the outgoing value escapes
170 /// beyond our model and either must not change its register or must
171 /// create a fixup FMOV to keep the old register value consistent.
172 ///
173 class Chain {
174 public:
175 /// The important (marker) instructions.
176 MachineInstr *StartInst, *LastInst, *KillInst;
177 /// The index, from the start of the basic block, that each marker
178 /// appears. These are stored so we can do quick interval tests.
179 unsigned StartInstIdx, LastInstIdx, KillInstIdx;
180 /// All instructions in the chain.
181 std::set<MachineInstr*> Insts;
182 /// True if KillInst cannot be modified. If this is true,
183 /// we cannot change LastInst's outgoing register.
184 /// This will be true for tied values and regmasks.
185 bool KillIsImmutable;
186 /// The "color" of LastInst. This will be the preferred chain color,
187 /// as changing intermediate nodes is easy but changing the last
188 /// instruction can be more tricky.
189 Color LastColor;
191 Chain(MachineInstr *MI, unsigned Idx, Color C)
192 : StartInst(MI), LastInst(MI), KillInst(nullptr),
193 StartInstIdx(Idx), LastInstIdx(Idx), KillInstIdx(0),
194 LastColor(C) {
195 Insts.insert(MI);
196 }
198 /// Add a new instruction into the chain. The instruction's dest operand
199 /// has the given color.
200 void add(MachineInstr *MI, unsigned Idx, Color C) {
201 LastInst = MI;
202 LastInstIdx = Idx;
203 LastColor = C;
204 assert((KillInstIdx == 0 || LastInstIdx < KillInstIdx) &&
205 "Chain: broken invariant. A Chain can only be killed after its last "
206 "def");
208 Insts.insert(MI);
209 }
211 /// Return true if MI is a member of the chain.
212 bool contains(MachineInstr *MI) { return Insts.count(MI) > 0; }
214 /// Return the number of instructions in the chain.
215 unsigned size() const {
216 return Insts.size();
217 }
219 /// Inform the chain that its last active register (the dest register of
220 /// LastInst) is killed by MI with no intervening uses or defs.
221 void setKill(MachineInstr *MI, unsigned Idx, bool Immutable) {
222 KillInst = MI;
223 KillInstIdx = Idx;
224 KillIsImmutable = Immutable;
225 assert((KillInstIdx == 0 || LastInstIdx < KillInstIdx) &&
226 "Chain: broken invariant. A Chain can only be killed after its last "
227 "def");
228 }
230 /// Return the first instruction in the chain.
231 MachineInstr *getStart() const { return StartInst; }
232 /// Return the last instruction in the chain.
233 MachineInstr *getLast() const { return LastInst; }
234 /// Return the "kill" instruction (as set with setKill()) or NULL.
235 MachineInstr *getKill() const { return KillInst; }
236 /// Return an instruction that can be used as an iterator for the end
237 /// of the chain. This is the maximum of KillInst (if set) and LastInst.
238 MachineBasicBlock::iterator getEnd() const {
239 return ++MachineBasicBlock::iterator(KillInst ? KillInst : LastInst);
240 }
242 /// Can the Kill instruction (assuming one exists) be modified?
243 bool isKillImmutable() const { return KillIsImmutable; }
245 /// Return the preferred color of this chain.
246 Color getPreferredColor() {
247 if (OverrideBalance != 0)
248 return OverrideBalance == 1 ? Color::Even : Color::Odd;
249 return LastColor;
250 }
252 /// Return true if this chain (StartInst..KillInst) overlaps with Other.
253 bool rangeOverlapsWith(const Chain &Other) const {
254 unsigned End = KillInst ? KillInstIdx : LastInstIdx;
255 unsigned OtherEnd = Other.KillInst ?
256 Other.KillInstIdx : Other.LastInstIdx;
258 return StartInstIdx <= OtherEnd && Other.StartInstIdx <= End;
259 }
261 /// Return true if this chain starts before Other.
262 bool startsBefore(Chain *Other) {
263 return StartInstIdx < Other->StartInstIdx;
264 }
266 /// Return true if the group will require a fixup MOV at the end.
267 bool requiresFixup() const {
268 return (getKill() && isKillImmutable()) || !getKill();
269 }
271 /// Return a simple string representation of the chain.
272 std::string str() const {
273 std::string S;
274 raw_string_ostream OS(S);
276 OS << "{";
277 StartInst->print(OS, NULL, true);
278 OS << " -> ";
279 LastInst->print(OS, NULL, true);
280 if (KillInst) {
281 OS << " (kill @ ";
282 KillInst->print(OS, NULL, true);
283 OS << ")";
284 }
285 OS << "}";
287 return OS.str();
288 }
290 };
292 } // end anonymous namespace
294 //===----------------------------------------------------------------------===//
296 bool AArch64A57FPLoadBalancing::runOnMachineFunction(MachineFunction &F) {
297 bool Changed = false;
298 DEBUG(dbgs() << "***** AArch64A57FPLoadBalancing *****\n");
300 const TargetMachine &TM = F.getTarget();
301 MRI = &F.getRegInfo();
302 TRI = F.getRegInfo().getTargetRegisterInfo();
303 TII = TM.getSubtarget<AArch64Subtarget>().getInstrInfo();
304 RCI.runOnMachineFunction(F);
306 for (auto &MBB : F) {
307 Changed |= runOnBasicBlock(MBB);
308 }
310 return Changed;
311 }
313 bool AArch64A57FPLoadBalancing::runOnBasicBlock(MachineBasicBlock &MBB) {
314 bool Changed = false;
315 DEBUG(dbgs() << "Running on MBB: " << MBB << " - scanning instructions...\n");
317 // First, scan the basic block producing a set of chains.
319 // The currently "active" chains - chains that can be added to and haven't
320 // been killed yet. This is keyed by register - all chains can only have one
321 // "link" register between each inst in the chain.
322 std::map<unsigned, Chain*> ActiveChains;
323 std::set<std::unique_ptr<Chain>> AllChains;
324 unsigned Idx = 0;
325 for (auto &MI : MBB)
326 scanInstruction(&MI, Idx++, ActiveChains, AllChains);
328 DEBUG(dbgs() << "Scan complete, "<< AllChains.size() << " chains created.\n");
330 // Group the chains into disjoint sets based on their liveness range. This is
331 // a poor-man's version of graph coloring. Ideally we'd create an interference
332 // graph and perform full-on graph coloring on that, but;
333 // (a) That's rather heavyweight for only two colors.
334 // (b) We expect multiple disjoint interference regions - in practice the live
335 // range of chains is quite small and they are clustered between loads
336 // and stores.
337 EquivalenceClasses<Chain*> EC;
338 for (auto &I : AllChains)
339 EC.insert(I.get());
341 for (auto &I : AllChains)
342 for (auto &J : AllChains)
343 if (I != J && I->rangeOverlapsWith(*J))
344 EC.unionSets(I.get(), J.get());
345 DEBUG(dbgs() << "Created " << EC.getNumClasses() << " disjoint sets.\n");
347 // Now we assume that every member of an equivalence class interferes
348 // with every other member of that class, and with no members of other classes.
350 // Convert the EquivalenceClasses to a simpler set of sets.
351 std::vector<std::vector<Chain*> > V;
352 for (auto I = EC.begin(), E = EC.end(); I != E; ++I) {
353 std::vector<Chain*> Cs(EC.member_begin(I), EC.member_end());
354 if (Cs.empty()) continue;
355 V.push_back(std::move(Cs));
356 }
358 // Now we have a set of sets, order them by start address so
359 // we can iterate over them sequentially.
360 std::sort(V.begin(), V.end(),
361 [](const std::vector<Chain*> &A,
362 const std::vector<Chain*> &B) {
363 return A.front()->startsBefore(B.front());
364 });
366 // As we only have two colors, we can track the global (BB-level) balance of
367 // odds versus evens. We aim to keep this near zero to keep both execution
368 // units fed.
369 // Positive means we're even-heavy, negative we're odd-heavy.
370 //
371 // FIXME: If chains have interdependencies, for example:
372 // mul r0, r1, r2
373 // mul r3, r0, r1
374 // We do not model this and may color each one differently, assuming we'll
375 // get ILP when we obviously can't. This hasn't been seen to be a problem
376 // in practice so far, so we simplify the algorithm by ignoring it.
377 int Parity = 0;
379 for (auto &I : V)
380 Changed |= colorChainSet(std::move(I), MBB, Parity);
382 return Changed;
383 }
385 Chain *AArch64A57FPLoadBalancing::getAndEraseNext(Color PreferredColor,
386 std::vector<Chain*> &L) {
387 if (L.empty())
388 return nullptr;
390 // We try and get the best candidate from L to color next, given that our
391 // preferred color is "PreferredColor". L is ordered from larger to smaller
392 // chains. It is beneficial to color the large chains before the small chains,
393 // but if we can't find a chain of the maximum length with the preferred color,
394 // we fuzz the size and look for slightly smaller chains before giving up and
395 // returning a chain that must be recolored.
397 // FIXME: Does this need to be configurable?
398 const unsigned SizeFuzz = 1;
399 unsigned MinSize = L.front()->size() - SizeFuzz;
400 for (auto I = L.begin(), E = L.end(); I != E; ++I) {
401 if ((*I)->size() <= MinSize) {
402 // We've gone past the size limit. Return the previous item.
403 Chain *Ch = *--I;
404 L.erase(I);
405 return Ch;
406 }
408 if ((*I)->getPreferredColor() == PreferredColor) {
409 Chain *Ch = *I;
410 L.erase(I);
411 return Ch;
412 }
413 }
415 // Bailout case - just return the first item.
416 Chain *Ch = L.front();
417 L.erase(L.begin());
418 return Ch;
419 }
421 bool AArch64A57FPLoadBalancing::colorChainSet(std::vector<Chain*> GV,
422 MachineBasicBlock &MBB,
423 int &Parity) {
424 bool Changed = false;
425 DEBUG(dbgs() << "colorChainSet(): #sets=" << GV.size() << "\n");
427 // Sort by descending size order so that we allocate the most important
428 // sets first.
429 // Tie-break equivalent sizes by sorting chains requiring fixups before
430 // those without fixups. The logic here is that we should look at the
431 // chains that we cannot change before we look at those we can,
432 // so the parity counter is updated and we know what color we should
433 // change them to!
434 std::sort(GV.begin(), GV.end(), [](const Chain *G1, const Chain *G2) {
435 if (G1->size() != G2->size())
436 return G1->size() > G2->size();
437 return G1->requiresFixup() > G2->requiresFixup();
438 });
440 Color PreferredColor = Parity < 0 ? Color::Even : Color::Odd;
441 while (Chain *G = getAndEraseNext(PreferredColor, GV)) {
442 // Start off by assuming we'll color to our own preferred color.
443 Color C = PreferredColor;
444 if (Parity == 0)
445 // But if we really don't care, use the chain's preferred color.
446 C = G->getPreferredColor();
448 DEBUG(dbgs() << " - Parity=" << Parity << ", Color="
449 << ColorNames[(int)C] << "\n");
451 // If we'll need a fixup FMOV, don't bother. Testing has shown that this
452 // happens infrequently and when it does it has at least a 50% chance of
453 // slowing code down instead of speeding it up.
454 if (G->requiresFixup() && C != G->getPreferredColor()) {
455 C = G->getPreferredColor();
456 DEBUG(dbgs() << " - " << G->str() << " - not worthwhile changing; "
457 "color remains " << ColorNames[(int)C] << "\n");
458 }
460 Changed |= colorChain(G, C, MBB);
462 Parity += (C == Color::Even) ? G->size() : -G->size();
463 PreferredColor = Parity < 0 ? Color::Even : Color::Odd;
464 }
466 return Changed;
467 }
469 int AArch64A57FPLoadBalancing::scavengeRegister(Chain *G, Color C,
470 MachineBasicBlock &MBB) {
471 RegScavenger RS;
472 RS.enterBasicBlock(&MBB);
473 RS.forward(MachineBasicBlock::iterator(G->getStart()));
475 // Can we find an appropriate register that is available throughout the life
476 // of the chain?
477 unsigned RegClassID = G->getStart()->getDesc().OpInfo[0].RegClass;
478 BitVector AvailableRegs = RS.getRegsAvailable(TRI->getRegClass(RegClassID));
479 for (MachineBasicBlock::iterator I = G->getStart(), E = G->getEnd();
480 I != E; ++I) {
481 RS.forward(I);
482 AvailableRegs &= RS.getRegsAvailable(TRI->getRegClass(RegClassID));
484 // Remove any registers clobbered by a regmask or any def register that is
485 // immediately dead.
486 for (auto J : I->operands()) {
487 if (J.isRegMask())
488 AvailableRegs.clearBitsNotInMask(J.getRegMask());
490 if (J.isReg() && J.isDef() && AvailableRegs[J.getReg()]) {
491 assert(J.isDead() && "Non-dead def should have been removed by now!");
492 AvailableRegs.reset(J.getReg());
493 }
494 }
495 }
497 // Make sure we allocate in-order, to get the cheapest registers first.
498 auto Ord = RCI.getOrder(TRI->getRegClass(RegClassID));
499 for (auto Reg : Ord) {
500 if (!AvailableRegs[Reg])
501 continue;
502 if ((C == Color::Even && (Reg % 2) == 0) ||
503 (C == Color::Odd && (Reg % 2) == 1))
504 return Reg;
505 }
507 return -1;
508 }
510 bool AArch64A57FPLoadBalancing::colorChain(Chain *G, Color C,
511 MachineBasicBlock &MBB) {
512 bool Changed = false;
513 DEBUG(dbgs() << " - colorChain(" << G->str() << ", "
514 << ColorNames[(int)C] << ")\n");
516 // Try and obtain a free register of the right class. Without a register
517 // to play with we cannot continue.
518 int Reg = scavengeRegister(G, C, MBB);
519 if (Reg == -1) {
520 DEBUG(dbgs() << "Scavenging (thus coloring) failed!\n");
521 return false;
522 }
523 DEBUG(dbgs() << " - Scavenged register: " << TRI->getName(Reg) << "\n");
525 std::map<unsigned, unsigned> Substs;
526 for (MachineBasicBlock::iterator I = G->getStart(), E = G->getEnd();
527 I != E; ++I) {
528 if (!G->contains(I) &&
529 (&*I != G->getKill() || G->isKillImmutable()))
530 continue;
532 // I is a member of G, or I is a mutable instruction that kills G.
534 std::vector<unsigned> ToErase;
535 for (auto &U : I->operands()) {
536 if (U.isReg() && U.isUse() && Substs.find(U.getReg()) != Substs.end()) {
537 unsigned OrigReg = U.getReg();
538 U.setReg(Substs[OrigReg]);
539 if (U.isKill())
540 // Don't erase straight away, because there may be other operands
541 // that also reference this substitution!
542 ToErase.push_back(OrigReg);
543 } else if (U.isRegMask()) {
544 for (auto J : Substs) {
545 if (U.clobbersPhysReg(J.first))
546 ToErase.push_back(J.first);
547 }
548 }
549 }
550 // Now it's safe to remove the substs identified earlier.
551 for (auto J : ToErase)
552 Substs.erase(J);
554 // Only change the def if this isn't the last instruction.
555 if (&*I != G->getKill()) {
556 MachineOperand &MO = I->getOperand(0);
558 bool Change = TransformAll || getColor(MO.getReg()) != C;
559 if (G->requiresFixup() && &*I == G->getLast())
560 Change = false;
562 if (Change) {
563 Substs[MO.getReg()] = Reg;
564 MO.setReg(Reg);
565 MRI->setPhysRegUsed(Reg);
567 Changed = true;
568 }
569 }
570 }
571 assert(Substs.size() == 0 && "No substitutions should be left active!");
573 if (G->getKill()) {
574 DEBUG(dbgs() << " - Kill instruction seen.\n");
575 } else {
576 // We didn't have a kill instruction, but we didn't seem to need to change
577 // the destination register anyway.
578 DEBUG(dbgs() << " - Destination register not changed.\n");
579 }
580 return Changed;
581 }
583 void AArch64A57FPLoadBalancing::
584 scanInstruction(MachineInstr *MI, unsigned Idx,
585 std::map<unsigned, Chain*> &ActiveChains,
586 std::set<std::unique_ptr<Chain>> &AllChains) {
587 // Inspect "MI", updating ActiveChains and AllChains.
589 if (isMul(MI)) {
591 for (auto &I : MI->uses())
592 maybeKillChain(I, Idx, ActiveChains);
593 for (auto &I : MI->defs())
594 maybeKillChain(I, Idx, ActiveChains);
596 // Create a new chain. Multiplies don't require forwarding so can go on any
597 // unit.
598 unsigned DestReg = MI->getOperand(0).getReg();
600 DEBUG(dbgs() << "New chain started for register "
601 << TRI->getName(DestReg) << " at " << *MI);
603 auto G = llvm::make_unique<Chain>(MI, Idx, getColor(DestReg));
604 ActiveChains[DestReg] = G.get();
605 AllChains.insert(std::move(G));
607 } else if (isMla(MI)) {
609 // It is beneficial to keep MLAs on the same functional unit as their
610 // accumulator operand.
611 unsigned DestReg = MI->getOperand(0).getReg();
612 unsigned AccumReg = MI->getOperand(3).getReg();
614 maybeKillChain(MI->getOperand(1), Idx, ActiveChains);
615 maybeKillChain(MI->getOperand(2), Idx, ActiveChains);
616 if (DestReg != AccumReg)
617 maybeKillChain(MI->getOperand(0), Idx, ActiveChains);
619 if (ActiveChains.find(AccumReg) != ActiveChains.end()) {
620 DEBUG(dbgs() << "Chain found for accumulator register "
621 << TRI->getName(AccumReg) << " in MI " << *MI);
623 // For simplicity we only chain together sequences of MULs/MLAs where the
624 // accumulator register is killed on each instruction. This means we don't
625 // need to track other uses of the registers we want to rewrite.
626 //
627 // FIXME: We could extend to handle the non-kill cases for more coverage.
628 if (MI->getOperand(3).isKill()) {
629 // Add to chain.
630 DEBUG(dbgs() << "Instruction was successfully added to chain.\n");
631 ActiveChains[AccumReg]->add(MI, Idx, getColor(DestReg));
632 // Handle cases where the destination is not the same as the accumulator.
633 if (DestReg != AccumReg) {
634 ActiveChains[DestReg] = ActiveChains[AccumReg];
635 ActiveChains.erase(AccumReg);
636 }
637 return;
638 }
640 DEBUG(dbgs() << "Cannot add to chain because accumulator operand wasn't "
641 << "marked <kill>!\n");
642 maybeKillChain(MI->getOperand(3), Idx, ActiveChains);
643 }
645 DEBUG(dbgs() << "Creating new chain for dest register "
646 << TRI->getName(DestReg) << "\n");
647 auto G = llvm::make_unique<Chain>(MI, Idx, getColor(DestReg));
648 ActiveChains[DestReg] = G.get();
649 AllChains.insert(std::move(G));
651 } else {
653 // Non-MUL or MLA instruction. Invalidate any chain in the uses or defs
654 // lists.
655 for (auto &I : MI->uses())
656 maybeKillChain(I, Idx, ActiveChains);
657 for (auto &I : MI->defs())
658 maybeKillChain(I, Idx, ActiveChains);
660 }
661 }
663 void AArch64A57FPLoadBalancing::
664 maybeKillChain(MachineOperand &MO, unsigned Idx,
665 std::map<unsigned, Chain*> &ActiveChains) {
666 // Given an operand and the set of active chains (keyed by register),
667 // determine if a chain should be ended and remove from ActiveChains.
668 MachineInstr *MI = MO.getParent();
670 if (MO.isReg()) {
672 // If this is a KILL of a current chain, record it.
673 if (MO.isKill() && ActiveChains.find(MO.getReg()) != ActiveChains.end()) {
674 DEBUG(dbgs() << "Kill seen for chain " << TRI->getName(MO.getReg())
675 << "\n");
676 ActiveChains[MO.getReg()]->setKill(MI, Idx, /*Immutable=*/MO.isTied());
677 }
678 ActiveChains.erase(MO.getReg());
680 } else if (MO.isRegMask()) {
682 for (auto I = ActiveChains.begin(), E = ActiveChains.end();
683 I != E;) {
684 if (MO.clobbersPhysReg(I->first)) {
685 DEBUG(dbgs() << "Kill (regmask) seen for chain "
686 << TRI->getName(I->first) << "\n");
687 I->second->setKill(MI, Idx, /*Immutable=*/true);
688 ActiveChains.erase(I++);
689 } else
690 ++I;
691 }
693 }
694 }
696 Color AArch64A57FPLoadBalancing::getColor(unsigned Reg) {
697 if ((TRI->getEncodingValue(Reg) % 2) == 0)
698 return Color::Even;
699 else
700 return Color::Odd;
701 }
703 // Factory function used by AArch64TargetMachine to add the pass to the passmanager.
704 FunctionPass *llvm::createAArch64A57FPLoadBalancing() {
705 return new AArch64A57FPLoadBalancing();
706 }