cdb25bebd94470e456ef1db7913bfa1684ddab74
1 //===- AArch64InstrInfo.h - AArch64 Instruction Information -----*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file contains the AArch64 implementation of the TargetInstrInfo class.
11 //
12 //===----------------------------------------------------------------------===//
14 #ifndef LLVM_LIB_TARGET_AARCH64_AARCH64INSTRINFO_H
15 #define LLVM_LIB_TARGET_AARCH64_AARCH64INSTRINFO_H
17 #include "AArch64.h"
18 #include "AArch64RegisterInfo.h"
19 #include "llvm/Target/TargetInstrInfo.h"
20 #include "llvm/CodeGen/MachineCombinerPattern.h"
22 #define GET_INSTRINFO_HEADER
23 #include "AArch64GenInstrInfo.inc"
25 namespace llvm {
27 class AArch64Subtarget;
28 class AArch64TargetMachine;
30 class AArch64InstrInfo : public AArch64GenInstrInfo {
31 // Reserve bits in the MachineMemOperand target hint flags, starting at 1.
32 // They will be shifted into MOTargetHintStart when accessed.
33 enum TargetMemOperandFlags {
34 MOSuppressPair = 1
35 };
37 const AArch64RegisterInfo RI;
38 const AArch64Subtarget &Subtarget;
40 public:
41 explicit AArch64InstrInfo(const AArch64Subtarget &STI);
43 /// getRegisterInfo - TargetInstrInfo is a superset of MRegister info. As
44 /// such, whenever a client has an instance of instruction info, it should
45 /// always be able to get register info as well (through this method).
46 const AArch64RegisterInfo &getRegisterInfo() const { return RI; }
48 unsigned GetInstSizeInBytes(const MachineInstr *MI) const;
50 bool isAsCheapAsAMove(const MachineInstr *MI) const override;
52 bool isCoalescableExtInstr(const MachineInstr &MI, unsigned &SrcReg,
53 unsigned &DstReg, unsigned &SubIdx) const override;
55 bool
56 areMemAccessesTriviallyDisjoint(MachineInstr *MIa, MachineInstr *MIb,
57 AliasAnalysis *AA = nullptr) const override;
59 unsigned isLoadFromStackSlot(const MachineInstr *MI,
60 int &FrameIndex) const override;
61 unsigned isStoreToStackSlot(const MachineInstr *MI,
62 int &FrameIndex) const override;
64 /// Returns true if there is a shiftable register and that the shift value
65 /// is non-zero.
66 bool hasShiftedReg(const MachineInstr *MI) const;
68 /// Returns true if there is an extendable register and that the extending
69 /// value is non-zero.
70 bool hasExtendedReg(const MachineInstr *MI) const;
72 /// \brief Does this instruction set its full destination register to zero?
73 bool isGPRZero(const MachineInstr *MI) const;
75 /// \brief Does this instruction rename a GPR without modifying bits?
76 bool isGPRCopy(const MachineInstr *MI) const;
78 /// \brief Does this instruction rename an FPR without modifying bits?
79 bool isFPRCopy(const MachineInstr *MI) const;
81 /// Return true if this is load/store scales or extends its register offset.
82 /// This refers to scaling a dynamic index as opposed to scaled immediates.
83 /// MI should be a memory op that allows scaled addressing.
84 bool isScaledAddr(const MachineInstr *MI) const;
86 /// Return true if pairing the given load or store is hinted to be
87 /// unprofitable.
88 bool isLdStPairSuppressed(const MachineInstr *MI) const;
90 /// Hint that pairing the given load or store is unprofitable.
91 void suppressLdStPair(MachineInstr *MI) const;
93 bool getLdStBaseRegImmOfs(MachineInstr *LdSt, unsigned &BaseReg,
94 unsigned &Offset,
95 const TargetRegisterInfo *TRI) const override;
97 bool getLdStBaseRegImmOfsWidth(MachineInstr *LdSt, unsigned &BaseReg,
98 int &Offset, int &Width,
99 const TargetRegisterInfo *TRI) const;
101 bool enableClusterLoads() const override { return true; }
103 bool shouldClusterLoads(MachineInstr *FirstLdSt, MachineInstr *SecondLdSt,
104 unsigned NumLoads) const override;
106 bool shouldScheduleAdjacent(MachineInstr *First,
107 MachineInstr *Second) const override;
109 MachineInstr *emitFrameIndexDebugValue(MachineFunction &MF, int FrameIx,
110 uint64_t Offset, const MDNode *MDPtr,
111 DebugLoc DL) const;
112 void copyPhysRegTuple(MachineBasicBlock &MBB, MachineBasicBlock::iterator I,
113 DebugLoc DL, unsigned DestReg, unsigned SrcReg,
114 bool KillSrc, unsigned Opcode,
115 llvm::ArrayRef<unsigned> Indices) const;
116 void copyPhysReg(MachineBasicBlock &MBB, MachineBasicBlock::iterator I,
117 DebugLoc DL, unsigned DestReg, unsigned SrcReg,
118 bool KillSrc) const override;
120 void storeRegToStackSlot(MachineBasicBlock &MBB,
121 MachineBasicBlock::iterator MBBI, unsigned SrcReg,
122 bool isKill, int FrameIndex,
123 const TargetRegisterClass *RC,
124 const TargetRegisterInfo *TRI) const override;
126 void loadRegFromStackSlot(MachineBasicBlock &MBB,
127 MachineBasicBlock::iterator MBBI, unsigned DestReg,
128 int FrameIndex, const TargetRegisterClass *RC,
129 const TargetRegisterInfo *TRI) const override;
131 using TargetInstrInfo::foldMemoryOperandImpl;
132 MachineInstr *
133 foldMemoryOperandImpl(MachineFunction &MF, MachineInstr *MI,
134 const SmallVectorImpl<unsigned> &Ops,
135 int FrameIndex) const override;
137 bool AnalyzeBranch(MachineBasicBlock &MBB, MachineBasicBlock *&TBB,
138 MachineBasicBlock *&FBB,
139 SmallVectorImpl<MachineOperand> &Cond,
140 bool AllowModify = false) const override;
141 unsigned RemoveBranch(MachineBasicBlock &MBB) const override;
142 unsigned InsertBranch(MachineBasicBlock &MBB, MachineBasicBlock *TBB,
143 MachineBasicBlock *FBB,
144 const SmallVectorImpl<MachineOperand> &Cond,
145 DebugLoc DL) const override;
146 bool
147 ReverseBranchCondition(SmallVectorImpl<MachineOperand> &Cond) const override;
148 bool canInsertSelect(const MachineBasicBlock &,
149 const SmallVectorImpl<MachineOperand> &Cond, unsigned,
150 unsigned, int &, int &, int &) const override;
151 void insertSelect(MachineBasicBlock &MBB, MachineBasicBlock::iterator MI,
152 DebugLoc DL, unsigned DstReg,
153 const SmallVectorImpl<MachineOperand> &Cond,
154 unsigned TrueReg, unsigned FalseReg) const override;
155 void getNoopForMachoTarget(MCInst &NopInst) const override;
157 /// analyzeCompare - For a comparison instruction, return the source registers
158 /// in SrcReg and SrcReg2, and the value it compares against in CmpValue.
159 /// Return true if the comparison instruction can be analyzed.
160 bool analyzeCompare(const MachineInstr *MI, unsigned &SrcReg,
161 unsigned &SrcReg2, int &CmpMask,
162 int &CmpValue) const override;
163 /// optimizeCompareInstr - Convert the instruction supplying the argument to
164 /// the comparison into one that sets the zero bit in the flags register.
165 bool optimizeCompareInstr(MachineInstr *CmpInstr, unsigned SrcReg,
166 unsigned SrcReg2, int CmpMask, int CmpValue,
167 const MachineRegisterInfo *MRI) const override;
168 /// hasPattern - return true when there is potentially a faster code sequence
169 /// for an instruction chain ending in <Root>. All potential patterns are
170 /// listed
171 /// in the <Pattern> array.
172 bool hasPattern(MachineInstr &Root,
173 SmallVectorImpl<MachineCombinerPattern::MC_PATTERN> &Pattern)
174 const override;
176 /// genAlternativeCodeSequence - when hasPattern() finds a pattern
177 /// this function generates the instructions that could replace the
178 /// original code sequence
179 void genAlternativeCodeSequence(
180 MachineInstr &Root, MachineCombinerPattern::MC_PATTERN P,
181 SmallVectorImpl<MachineInstr *> &InsInstrs,
182 SmallVectorImpl<MachineInstr *> &DelInstrs,
183 DenseMap<unsigned, unsigned> &InstrIdxForVirtReg) const override;
184 /// useMachineCombiner - AArch64 supports MachineCombiner
185 bool useMachineCombiner() const override;
187 bool expandPostRAPseudo(MachineBasicBlock::iterator MI) const override;
188 private:
189 void instantiateCondBranch(MachineBasicBlock &MBB, DebugLoc DL,
190 MachineBasicBlock *TBB,
191 const SmallVectorImpl<MachineOperand> &Cond) const;
192 };
194 /// emitFrameOffset - Emit instructions as needed to set DestReg to SrcReg
195 /// plus Offset. This is intended to be used from within the prolog/epilog
196 /// insertion (PEI) pass, where a virtual scratch register may be allocated
197 /// if necessary, to be replaced by the scavenger at the end of PEI.
198 void emitFrameOffset(MachineBasicBlock &MBB, MachineBasicBlock::iterator MBBI,
199 DebugLoc DL, unsigned DestReg, unsigned SrcReg, int Offset,
200 const TargetInstrInfo *TII,
201 MachineInstr::MIFlag = MachineInstr::NoFlags,
202 bool SetNZCV = false);
204 /// rewriteAArch64FrameIndex - Rewrite MI to access 'Offset' bytes from the
205 /// FP. Return false if the offset could not be handled directly in MI, and
206 /// return the left-over portion by reference.
207 bool rewriteAArch64FrameIndex(MachineInstr &MI, unsigned FrameRegIdx,
208 unsigned FrameReg, int &Offset,
209 const AArch64InstrInfo *TII);
211 /// \brief Use to report the frame offset status in isAArch64FrameOffsetLegal.
212 enum AArch64FrameOffsetStatus {
213 AArch64FrameOffsetCannotUpdate = 0x0, ///< Offset cannot apply.
214 AArch64FrameOffsetIsLegal = 0x1, ///< Offset is legal.
215 AArch64FrameOffsetCanUpdate = 0x2 ///< Offset can apply, at least partly.
216 };
218 /// \brief Check if the @p Offset is a valid frame offset for @p MI.
219 /// The returned value reports the validity of the frame offset for @p MI.
220 /// It uses the values defined by AArch64FrameOffsetStatus for that.
221 /// If result == AArch64FrameOffsetCannotUpdate, @p MI cannot be updated to
222 /// use an offset.eq
223 /// If result & AArch64FrameOffsetIsLegal, @p Offset can completely be
224 /// rewriten in @p MI.
225 /// If result & AArch64FrameOffsetCanUpdate, @p Offset contains the
226 /// amount that is off the limit of the legal offset.
227 /// If set, @p OutUseUnscaledOp will contain the whether @p MI should be
228 /// turned into an unscaled operator, which opcode is in @p OutUnscaledOp.
229 /// If set, @p EmittableOffset contains the amount that can be set in @p MI
230 /// (possibly with @p OutUnscaledOp if OutUseUnscaledOp is true) and that
231 /// is a legal offset.
232 int isAArch64FrameOffsetLegal(const MachineInstr &MI, int &Offset,
233 bool *OutUseUnscaledOp = nullptr,
234 unsigned *OutUnscaledOp = nullptr,
235 int *EmittableOffset = nullptr);
237 static inline bool isUncondBranchOpcode(int Opc) { return Opc == AArch64::B; }
239 static inline bool isCondBranchOpcode(int Opc) {
240 switch (Opc) {
241 case AArch64::Bcc:
242 case AArch64::CBZW:
243 case AArch64::CBZX:
244 case AArch64::CBNZW:
245 case AArch64::CBNZX:
246 case AArch64::TBZW:
247 case AArch64::TBZX:
248 case AArch64::TBNZW:
249 case AArch64::TBNZX:
250 return true;
251 default:
252 return false;
253 }
254 }
256 static inline bool isIndirectBranchOpcode(int Opc) { return Opc == AArch64::BR; }
258 } // end namespace llvm
260 #endif