1 //===-- Thumb2ITBlockPass.cpp - Insert Thumb-2 IT blocks ------------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
10 #define DEBUG_TYPE "thumb2-it"
11 #include "ARM.h"
12 #include "ARMMachineFunctionInfo.h"
13 #include "Thumb2InstrInfo.h"
14 #include "llvm/ADT/SmallSet.h"
15 #include "llvm/ADT/Statistic.h"
16 #include "llvm/CodeGen/MachineFunctionPass.h"
17 #include "llvm/CodeGen/MachineInstr.h"
18 #include "llvm/CodeGen/MachineInstrBuilder.h"
19 #include "llvm/CodeGen/MachineInstrBundle.h"
20 using namespace llvm;
22 STATISTIC(NumITs, "Number of IT blocks inserted");
23 STATISTIC(NumMovedInsts, "Number of predicated instructions moved");
25 namespace {
26 class Thumb2ITBlockPass : public MachineFunctionPass {
27 public:
28 static char ID;
29 Thumb2ITBlockPass() : MachineFunctionPass(ID) {}
31 bool restrictIT;
32 const Thumb2InstrInfo *TII;
33 const TargetRegisterInfo *TRI;
34 ARMFunctionInfo *AFI;
36 virtual bool runOnMachineFunction(MachineFunction &Fn);
38 virtual const char *getPassName() const {
39 return "Thumb IT blocks insertion pass";
40 }
42 private:
43 bool MoveCopyOutOfITBlock(MachineInstr *MI,
44 ARMCC::CondCodes CC, ARMCC::CondCodes OCC,
45 SmallSet<unsigned, 4> &Defs,
46 SmallSet<unsigned, 4> &Uses);
47 bool InsertITInstructions(MachineBasicBlock &MBB);
48 };
49 char Thumb2ITBlockPass::ID = 0;
50 }
52 /// TrackDefUses - Tracking what registers are being defined and used by
53 /// instructions in the IT block. This also tracks "dependencies", i.e. uses
54 /// in the IT block that are defined before the IT instruction.
55 static void TrackDefUses(MachineInstr *MI,
56 SmallSet<unsigned, 4> &Defs,
57 SmallSet<unsigned, 4> &Uses,
58 const TargetRegisterInfo *TRI) {
59 SmallVector<unsigned, 4> LocalDefs;
60 SmallVector<unsigned, 4> LocalUses;
62 for (unsigned i = 0, e = MI->getNumOperands(); i != e; ++i) {
63 MachineOperand &MO = MI->getOperand(i);
64 if (!MO.isReg())
65 continue;
66 unsigned Reg = MO.getReg();
67 if (!Reg || Reg == ARM::ITSTATE || Reg == ARM::SP)
68 continue;
69 if (MO.isUse())
70 LocalUses.push_back(Reg);
71 else
72 LocalDefs.push_back(Reg);
73 }
75 for (unsigned i = 0, e = LocalUses.size(); i != e; ++i) {
76 unsigned Reg = LocalUses[i];
77 for (MCSubRegIterator Subreg(Reg, TRI, /*IncludeSelf=*/true);
78 Subreg.isValid(); ++Subreg)
79 Uses.insert(*Subreg);
80 }
82 for (unsigned i = 0, e = LocalDefs.size(); i != e; ++i) {
83 unsigned Reg = LocalDefs[i];
84 for (MCSubRegIterator Subreg(Reg, TRI, /*IncludeSelf=*/true);
85 Subreg.isValid(); ++Subreg)
86 Defs.insert(*Subreg);
87 if (Reg == ARM::CPSR)
88 continue;
89 }
90 }
92 static bool isCopy(MachineInstr *MI) {
93 switch (MI->getOpcode()) {
94 default:
95 return false;
96 case ARM::MOVr:
97 case ARM::MOVr_TC:
98 case ARM::tMOVr:
99 case ARM::t2MOVr:
100 return true;
101 }
102 }
104 bool
105 Thumb2ITBlockPass::MoveCopyOutOfITBlock(MachineInstr *MI,
106 ARMCC::CondCodes CC, ARMCC::CondCodes OCC,
107 SmallSet<unsigned, 4> &Defs,
108 SmallSet<unsigned, 4> &Uses) {
109 if (!isCopy(MI))
110 return false;
111 // llvm models select's as two-address instructions. That means a copy
112 // is inserted before a t2MOVccr, etc. If the copy is scheduled in
113 // between selects we would end up creating multiple IT blocks.
114 assert(MI->getOperand(0).getSubReg() == 0 &&
115 MI->getOperand(1).getSubReg() == 0 &&
116 "Sub-register indices still around?");
118 unsigned DstReg = MI->getOperand(0).getReg();
119 unsigned SrcReg = MI->getOperand(1).getReg();
121 // First check if it's safe to move it.
122 if (Uses.count(DstReg) || Defs.count(SrcReg))
123 return false;
125 // If the CPSR is defined by this copy, then we don't want to move it. E.g.,
126 // if we have:
127 //
128 // movs r1, r1
129 // rsb r1, 0
130 // movs r2, r2
131 // rsb r2, 0
132 //
133 // we don't want this to be converted to:
134 //
135 // movs r1, r1
136 // movs r2, r2
137 // itt mi
138 // rsb r1, 0
139 // rsb r2, 0
140 //
141 const MCInstrDesc &MCID = MI->getDesc();
142 if (MI->hasOptionalDef() &&
143 MI->getOperand(MCID.getNumOperands() - 1).getReg() == ARM::CPSR)
144 return false;
146 // Then peek at the next instruction to see if it's predicated on CC or OCC.
147 // If not, then there is nothing to be gained by moving the copy.
148 MachineBasicBlock::iterator I = MI; ++I;
149 MachineBasicBlock::iterator E = MI->getParent()->end();
150 while (I != E && I->isDebugValue())
151 ++I;
152 if (I != E) {
153 unsigned NPredReg = 0;
154 ARMCC::CondCodes NCC = getITInstrPredicate(I, NPredReg);
155 if (NCC == CC || NCC == OCC)
156 return true;
157 }
158 return false;
159 }
161 bool Thumb2ITBlockPass::InsertITInstructions(MachineBasicBlock &MBB) {
162 bool Modified = false;
164 SmallSet<unsigned, 4> Defs;
165 SmallSet<unsigned, 4> Uses;
166 MachineBasicBlock::iterator MBBI = MBB.begin(), E = MBB.end();
167 while (MBBI != E) {
168 MachineInstr *MI = &*MBBI;
169 DebugLoc dl = MI->getDebugLoc();
170 unsigned PredReg = 0;
171 ARMCC::CondCodes CC = getITInstrPredicate(MI, PredReg);
172 if (CC == ARMCC::AL) {
173 ++MBBI;
174 continue;
175 }
177 Defs.clear();
178 Uses.clear();
179 TrackDefUses(MI, Defs, Uses, TRI);
181 // Insert an IT instruction.
182 MachineInstrBuilder MIB = BuildMI(MBB, MBBI, dl, TII->get(ARM::t2IT))
183 .addImm(CC);
185 // Add implicit use of ITSTATE to IT block instructions.
186 MI->addOperand(MachineOperand::CreateReg(ARM::ITSTATE, false/*ifDef*/,
187 true/*isImp*/, false/*isKill*/));
189 MachineInstr *LastITMI = MI;
190 MachineBasicBlock::iterator InsertPos = MIB;
191 ++MBBI;
193 // Form IT block.
194 ARMCC::CondCodes OCC = ARMCC::getOppositeCondition(CC);
195 unsigned Mask = 0, Pos = 3;
197 // v8 IT blocks are limited to one conditional op unless -arm-no-restrict-it
198 // is set: skip the loop
199 if (!restrictIT) {
200 // Branches, including tricky ones like LDM_RET, need to end an IT
201 // block so check the instruction we just put in the block.
202 for (; MBBI != E && Pos &&
203 (!MI->isBranch() && !MI->isReturn()) ; ++MBBI) {
204 if (MBBI->isDebugValue())
205 continue;
207 MachineInstr *NMI = &*MBBI;
208 MI = NMI;
210 unsigned NPredReg = 0;
211 ARMCC::CondCodes NCC = getITInstrPredicate(NMI, NPredReg);
212 if (NCC == CC || NCC == OCC) {
213 Mask |= (NCC & 1) << Pos;
214 // Add implicit use of ITSTATE.
215 NMI->addOperand(MachineOperand::CreateReg(ARM::ITSTATE, false/*ifDef*/,
216 true/*isImp*/, false/*isKill*/));
217 LastITMI = NMI;
218 } else {
219 if (NCC == ARMCC::AL &&
220 MoveCopyOutOfITBlock(NMI, CC, OCC, Defs, Uses)) {
221 --MBBI;
222 MBB.remove(NMI);
223 MBB.insert(InsertPos, NMI);
224 ++NumMovedInsts;
225 continue;
226 }
227 break;
228 }
229 TrackDefUses(NMI, Defs, Uses, TRI);
230 --Pos;
231 }
232 }
234 // Finalize IT mask.
235 Mask |= (1 << Pos);
236 // Tag along (firstcond[0] << 4) with the mask.
237 Mask |= (CC & 1) << 4;
238 MIB.addImm(Mask);
240 // Last instruction in IT block kills ITSTATE.
241 LastITMI->findRegisterUseOperand(ARM::ITSTATE)->setIsKill();
243 // Finalize the bundle.
244 MachineBasicBlock::instr_iterator LI = LastITMI;
245 finalizeBundle(MBB, InsertPos.getInstrIterator(), llvm::next(LI));
247 Modified = true;
248 ++NumITs;
249 }
251 return Modified;
252 }
254 bool Thumb2ITBlockPass::runOnMachineFunction(MachineFunction &Fn) {
255 const TargetMachine &TM = Fn.getTarget();
256 AFI = Fn.getInfo<ARMFunctionInfo>();
257 TII = static_cast<const Thumb2InstrInfo*>(TM.getInstrInfo());
258 TRI = TM.getRegisterInfo();
259 restrictIT = TM.getSubtarget<ARMSubtarget>().restrictIT();
261 if (!AFI->isThumbFunction())
262 return false;
264 bool Modified = false;
265 for (MachineFunction::iterator MFI = Fn.begin(), E = Fn.end(); MFI != E; ) {
266 MachineBasicBlock &MBB = *MFI;
267 ++MFI;
268 Modified |= InsertITInstructions(MBB);
269 }
271 if (Modified)
272 AFI->setHasITBlocks(true);
274 return Modified;
275 }
277 /// createThumb2ITBlockPass - Returns an instance of the Thumb2 IT blocks
278 /// insertion pass.
279 FunctionPass *llvm::createThumb2ITBlockPass() {
280 return new Thumb2ITBlockPass();
281 }