]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Target/PowerPC/PPCISelLowering.h
Don't cache the instruction and register info from the TargetMachine, because
[opencl/llvm.git] / lib / Target / PowerPC / PPCISelLowering.h
1 //===-- PPCISelLowering.h - PPC32 DAG Lowering Interface --------*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the interfaces that PPC uses to lower LLVM code into a
11 // selection DAG.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
16 #define LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
18 #include "PPC.h"
19 #include "PPCInstrInfo.h"
20 #include "PPCRegisterInfo.h"
21 #include "PPCSubtarget.h"
22 #include "llvm/CodeGen/SelectionDAG.h"
23 #include "llvm/Target/TargetLowering.h"
25 namespace llvm {
26   namespace PPCISD {
27     enum NodeType {
28       // Start the numbering where the builtin ops and target ops leave off.
29       FIRST_NUMBER = ISD::BUILTIN_OP_END,
31       /// FSEL - Traditional three-operand fsel node.
32       ///
33       FSEL,
35       /// FCFID - The FCFID instruction, taking an f64 operand and producing
36       /// and f64 value containing the FP representation of the integer that
37       /// was temporarily in the f64 operand.
38       FCFID,
40       /// Newer FCFID[US] integer-to-floating-point conversion instructions for
41       /// unsigned integers and single-precision outputs.
42       FCFIDU, FCFIDS, FCFIDUS,
44       /// FCTI[D,W]Z - The FCTIDZ and FCTIWZ instructions, taking an f32 or f64
45       /// operand, producing an f64 value containing the integer representation
46       /// of that FP value.
47       FCTIDZ, FCTIWZ,
49       /// Newer FCTI[D,W]UZ floating-point-to-integer conversion instructions for
50       /// unsigned integers.
51       FCTIDUZ, FCTIWUZ,
53       /// Reciprocal estimate instructions (unary FP ops).
54       FRE, FRSQRTE,
56       // VMADDFP, VNMSUBFP - The VMADDFP and VNMSUBFP instructions, taking
57       // three v4f32 operands and producing a v4f32 result.
58       VMADDFP, VNMSUBFP,
60       /// VPERM - The PPC VPERM Instruction.
61       ///
62       VPERM,
64       /// Hi/Lo - These represent the high and low 16-bit parts of a global
65       /// address respectively.  These nodes have two operands, the first of
66       /// which must be a TargetGlobalAddress, and the second of which must be a
67       /// Constant.  Selected naively, these turn into 'lis G+C' and 'li G+C',
68       /// though these are usually folded into other nodes.
69       Hi, Lo,
71       TOC_ENTRY,
73       /// The following three target-specific nodes are used for calls through
74       /// function pointers in the 64-bit SVR4 ABI.
76       /// Restore the TOC from the TOC save area of the current stack frame.
77       /// This is basically a hard coded load instruction which additionally
78       /// takes/produces a flag.
79       TOC_RESTORE,
81       /// Like a regular LOAD but additionally taking/producing a flag.
82       LOAD,
84       /// LOAD into r2 (also taking/producing a flag). Like TOC_RESTORE, this is
85       /// a hard coded load instruction.
86       LOAD_TOC,
88       /// OPRC, CHAIN = DYNALLOC(CHAIN, NEGSIZE, FRAME_INDEX)
89       /// This instruction is lowered in PPCRegisterInfo::eliminateFrameIndex to
90       /// compute an allocation on the stack.
91       DYNALLOC,
93       /// GlobalBaseReg - On Darwin, this node represents the result of the mflr
94       /// at function entry, used for PIC code.
95       GlobalBaseReg,
97       /// These nodes represent the 32-bit PPC shifts that operate on 6-bit
98       /// shift amounts.  These nodes are generated by the multi-precision shift
99       /// code.
100       SRL, SRA, SHL,
102       /// CALL - A direct function call.
103       /// CALL_NOP is a call with the special NOP which follows 64-bit
104       /// SVR4 calls.
105       CALL, CALL_NOP,
107       /// CHAIN,FLAG = MTCTR(VAL, CHAIN[, INFLAG]) - Directly corresponds to a
108       /// MTCTR instruction.
109       MTCTR,
111       /// CHAIN,FLAG = BCTRL(CHAIN, INFLAG) - Directly corresponds to a
112       /// BCTRL instruction.
113       BCTRL,
115       /// Return with a flag operand, matched by 'blr'
116       RET_FLAG,
118       /// R32 = MFCR(CRREG, INFLAG) - Represents the MFCRpseud/MFOCRF
119       /// instructions.  This copies the bits corresponding to the specified
120       /// CRREG into the resultant GPR.  Bits corresponding to other CR regs
121       /// are undefined.
122       MFCR,
124       // EH_SJLJ_SETJMP - SjLj exception handling setjmp.
125       EH_SJLJ_SETJMP,
127       // EH_SJLJ_LONGJMP - SjLj exception handling longjmp.
128       EH_SJLJ_LONGJMP,
130       /// RESVEC = VCMP(LHS, RHS, OPC) - Represents one of the altivec VCMP*
131       /// instructions.  For lack of better number, we use the opcode number
132       /// encoding for the OPC field to identify the compare.  For example, 838
133       /// is VCMPGTSH.
134       VCMP,
136       /// RESVEC, OUTFLAG = VCMPo(LHS, RHS, OPC) - Represents one of the
137       /// altivec VCMP*o instructions.  For lack of better number, we use the
138       /// opcode number encoding for the OPC field to identify the compare.  For
139       /// example, 838 is VCMPGTSH.
140       VCMPo,
142       /// CHAIN = COND_BRANCH CHAIN, CRRC, OPC, DESTBB [, INFLAG] - This
143       /// corresponds to the COND_BRANCH pseudo instruction.  CRRC is the
144       /// condition register to branch on, OPC is the branch opcode to use (e.g.
145       /// PPC::BLE), DESTBB is the destination block to branch to, and INFLAG is
146       /// an optional input flag argument.
147       COND_BRANCH,
149       /// CHAIN = BDNZ CHAIN, DESTBB - These are used to create counter-based
150       /// loops.
151       BDNZ, BDZ,
153       /// F8RC = FADDRTZ F8RC, F8RC - This is an FADD done with rounding
154       /// towards zero.  Used only as part of the long double-to-int
155       /// conversion sequence.
156       FADDRTZ,
158       /// F8RC = MFFS - This moves the FPSCR (not modeled) into the register.
159       MFFS,
161       /// LARX = This corresponds to PPC l{w|d}arx instrcution: load and
162       /// reserve indexed. This is used to implement atomic operations.
163       LARX,
165       /// STCX = This corresponds to PPC stcx. instrcution: store conditional
166       /// indexed. This is used to implement atomic operations.
167       STCX,
169       /// TC_RETURN - A tail call return.
170       ///   operand #0 chain
171       ///   operand #1 callee (register or absolute)
172       ///   operand #2 stack adjustment
173       ///   operand #3 optional in flag
174       TC_RETURN,
176       /// ch, gl = CR6[UN]SET ch, inglue - Toggle CR bit 6 for SVR4 vararg calls
177       CR6SET,
178       CR6UNSET,
180       /// G8RC = ADDIS_GOT_TPREL_HA %X2, Symbol - Used by the initial-exec
181       /// TLS model, produces an ADDIS8 instruction that adds the GOT
182       /// base to sym\@got\@tprel\@ha.
183       ADDIS_GOT_TPREL_HA,
185       /// G8RC = LD_GOT_TPREL_L Symbol, G8RReg - Used by the initial-exec
186       /// TLS model, produces a LD instruction with base register G8RReg
187       /// and offset sym\@got\@tprel\@l.  This completes the addition that
188       /// finds the offset of "sym" relative to the thread pointer.
189       LD_GOT_TPREL_L,
191       /// G8RC = ADD_TLS G8RReg, Symbol - Used by the initial-exec TLS
192       /// model, produces an ADD instruction that adds the contents of
193       /// G8RReg to the thread pointer.  Symbol contains a relocation
194       /// sym\@tls which is to be replaced by the thread pointer and
195       /// identifies to the linker that the instruction is part of a
196       /// TLS sequence.
197       ADD_TLS,
199       /// G8RC = ADDIS_TLSGD_HA %X2, Symbol - For the general-dynamic TLS
200       /// model, produces an ADDIS8 instruction that adds the GOT base
201       /// register to sym\@got\@tlsgd\@ha.
202       ADDIS_TLSGD_HA,
204       /// G8RC = ADDI_TLSGD_L G8RReg, Symbol - For the general-dynamic TLS
205       /// model, produces an ADDI8 instruction that adds G8RReg to
206       /// sym\@got\@tlsgd\@l.
207       ADDI_TLSGD_L,
209       /// G8RC = GET_TLS_ADDR %X3, Symbol - For the general-dynamic TLS
210       /// model, produces a call to __tls_get_addr(sym\@tlsgd).
211       GET_TLS_ADDR,
213       /// G8RC = ADDIS_TLSLD_HA %X2, Symbol - For the local-dynamic TLS
214       /// model, produces an ADDIS8 instruction that adds the GOT base
215       /// register to sym\@got\@tlsld\@ha.
216       ADDIS_TLSLD_HA,
218       /// G8RC = ADDI_TLSLD_L G8RReg, Symbol - For the local-dynamic TLS
219       /// model, produces an ADDI8 instruction that adds G8RReg to
220       /// sym\@got\@tlsld\@l.
221       ADDI_TLSLD_L,
223       /// G8RC = GET_TLSLD_ADDR %X3, Symbol - For the local-dynamic TLS
224       /// model, produces a call to __tls_get_addr(sym\@tlsld).
225       GET_TLSLD_ADDR,
227       /// G8RC = ADDIS_DTPREL_HA %X3, Symbol, Chain - For the
228       /// local-dynamic TLS model, produces an ADDIS8 instruction
229       /// that adds X3 to sym\@dtprel\@ha. The Chain operand is needed
230       /// to tie this in place following a copy to %X3 from the result
231       /// of a GET_TLSLD_ADDR.
232       ADDIS_DTPREL_HA,
234       /// G8RC = ADDI_DTPREL_L G8RReg, Symbol - For the local-dynamic TLS
235       /// model, produces an ADDI8 instruction that adds G8RReg to
236       /// sym\@got\@dtprel\@l.
237       ADDI_DTPREL_L,
239       /// VRRC = VADD_SPLAT Elt, EltSize - Temporary node to be expanded
240       /// during instruction selection to optimize a BUILD_VECTOR into
241       /// operations on splats.  This is necessary to avoid losing these
242       /// optimizations due to constant folding.
243       VADD_SPLAT,
245       /// CHAIN = SC CHAIN, Imm128 - System call.  The 7-bit unsigned
246       /// operand identifies the operating system entry point.
247       SC,
249       /// CHAIN = STBRX CHAIN, GPRC, Ptr, Type - This is a
250       /// byte-swapping store instruction.  It byte-swaps the low "Type" bits of
251       /// the GPRC input, then stores it through Ptr.  Type can be either i16 or
252       /// i32.
253       STBRX = ISD::FIRST_TARGET_MEMORY_OPCODE,
255       /// GPRC, CHAIN = LBRX CHAIN, Ptr, Type - This is a
256       /// byte-swapping load instruction.  It loads "Type" bits, byte swaps it,
257       /// then puts it in the bottom bits of the GPRC.  TYPE can be either i16
258       /// or i32.
259       LBRX,
261       /// STFIWX - The STFIWX instruction.  The first operand is an input token
262       /// chain, then an f64 value to store, then an address to store it to.
263       STFIWX,
265       /// GPRC, CHAIN = LFIWAX CHAIN, Ptr - This is a floating-point
266       /// load which sign-extends from a 32-bit integer value into the
267       /// destination 64-bit register.
268       LFIWAX,
270       /// GPRC, CHAIN = LFIWZX CHAIN, Ptr - This is a floating-point
271       /// load which zero-extends from a 32-bit integer value into the
272       /// destination 64-bit register.
273       LFIWZX,
275       /// G8RC = ADDIS_TOC_HA %X2, Symbol - For medium and large code model,
276       /// produces an ADDIS8 instruction that adds the TOC base register to
277       /// sym\@toc\@ha.
278       ADDIS_TOC_HA,
280       /// G8RC = LD_TOC_L Symbol, G8RReg - For medium and large code model,
281       /// produces a LD instruction with base register G8RReg and offset
282       /// sym\@toc\@l. Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
283       LD_TOC_L,
285       /// G8RC = ADDI_TOC_L G8RReg, Symbol - For medium code model, produces
286       /// an ADDI8 instruction that adds G8RReg to sym\@toc\@l.
287       /// Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
288       ADDI_TOC_L
289     };
290   }
292   /// Define some predicates that are used for node matching.
293   namespace PPC {
294     /// isVPKUHUMShuffleMask - Return true if this is the shuffle mask for a
295     /// VPKUHUM instruction.
296     bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
298     /// isVPKUWUMShuffleMask - Return true if this is the shuffle mask for a
299     /// VPKUWUM instruction.
300     bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
302     /// isVMRGLShuffleMask - Return true if this is a shuffle mask suitable for
303     /// a VRGL* instruction with the specified unit size (1,2 or 4 bytes).
304     bool isVMRGLShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
305                             bool isUnary);
307     /// isVMRGHShuffleMask - Return true if this is a shuffle mask suitable for
308     /// a VRGH* instruction with the specified unit size (1,2 or 4 bytes).
309     bool isVMRGHShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
310                             bool isUnary);
312     /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the shift
313     /// amount, otherwise return -1.
314     int isVSLDOIShuffleMask(SDNode *N, bool isUnary);
316     /// isSplatShuffleMask - Return true if the specified VECTOR_SHUFFLE operand
317     /// specifies a splat of a single element that is suitable for input to
318     /// VSPLTB/VSPLTH/VSPLTW.
319     bool isSplatShuffleMask(ShuffleVectorSDNode *N, unsigned EltSize);
321     /// isAllNegativeZeroVector - Returns true if all elements of build_vector
322     /// are -0.0.
323     bool isAllNegativeZeroVector(SDNode *N);
325     /// getVSPLTImmediate - Return the appropriate VSPLT* immediate to splat the
326     /// specified isSplatShuffleMask VECTOR_SHUFFLE mask.
327     unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize);
329     /// get_VSPLTI_elt - If this is a build_vector of constants which can be
330     /// formed by using a vspltis[bhw] instruction of the specified element
331     /// size, return the constant being splatted.  The ByteSize field indicates
332     /// the number of bytes of each element [124] -> [bhw].
333     SDValue get_VSPLTI_elt(SDNode *N, unsigned ByteSize, SelectionDAG &DAG);
334   }
336   class PPCTargetLowering : public TargetLowering {
337     const PPCSubtarget &PPCSubTarget;
339   public:
340     explicit PPCTargetLowering(PPCTargetMachine &TM);
342     /// getTargetNodeName() - This method returns the name of a target specific
343     /// DAG node.
344     virtual const char *getTargetNodeName(unsigned Opcode) const;
346     virtual MVT getScalarShiftAmountTy(EVT LHSTy) const { return MVT::i32; }
348     /// getSetCCResultType - Return the ISD::SETCC ValueType
349     virtual EVT getSetCCResultType(LLVMContext &Context, EVT VT) const;
351     /// getPreIndexedAddressParts - returns true by value, base pointer and
352     /// offset pointer and addressing mode by reference if the node's address
353     /// can be legally represented as pre-indexed load / store address.
354     virtual bool getPreIndexedAddressParts(SDNode *N, SDValue &Base,
355                                            SDValue &Offset,
356                                            ISD::MemIndexedMode &AM,
357                                            SelectionDAG &DAG) const;
359     /// SelectAddressRegReg - Given the specified addressed, check to see if it
360     /// can be represented as an indexed [r+r] operation.  Returns false if it
361     /// can be more efficiently represented with [r+imm].
362     bool SelectAddressRegReg(SDValue N, SDValue &Base, SDValue &Index,
363                              SelectionDAG &DAG) const;
365     /// SelectAddressRegImm - Returns true if the address N can be represented
366     /// by a base register plus a signed 16-bit displacement [r+imm], and if it
367     /// is not better represented as reg+reg.  If Aligned is true, only accept
368     /// displacements suitable for STD and friends, i.e. multiples of 4.
369     bool SelectAddressRegImm(SDValue N, SDValue &Disp, SDValue &Base,
370                              SelectionDAG &DAG, bool Aligned) const;
372     /// SelectAddressRegRegOnly - Given the specified addressed, force it to be
373     /// represented as an indexed [r+r] operation.
374     bool SelectAddressRegRegOnly(SDValue N, SDValue &Base, SDValue &Index,
375                                  SelectionDAG &DAG) const;
377     Sched::Preference getSchedulingPreference(SDNode *N) const;
379     /// LowerOperation - Provide custom lowering hooks for some operations.
380     ///
381     virtual SDValue LowerOperation(SDValue Op, SelectionDAG &DAG) const;
383     /// ReplaceNodeResults - Replace the results of node with an illegal result
384     /// type with new values built out of custom code.
385     ///
386     virtual void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
387                                     SelectionDAG &DAG) const;
389     virtual SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const;
391     virtual void computeMaskedBitsForTargetNode(const SDValue Op,
392                                                 APInt &KnownZero,
393                                                 APInt &KnownOne,
394                                                 const SelectionDAG &DAG,
395                                                 unsigned Depth = 0) const;
397     virtual MachineBasicBlock *
398       EmitInstrWithCustomInserter(MachineInstr *MI,
399                                   MachineBasicBlock *MBB) const;
400     MachineBasicBlock *EmitAtomicBinary(MachineInstr *MI,
401                                         MachineBasicBlock *MBB, bool is64Bit,
402                                         unsigned BinOpcode) const;
403     MachineBasicBlock *EmitPartwordAtomicBinary(MachineInstr *MI,
404                                                 MachineBasicBlock *MBB,
405                                             bool is8bit, unsigned Opcode) const;
407     MachineBasicBlock *emitEHSjLjSetJmp(MachineInstr *MI,
408                                         MachineBasicBlock *MBB) const;
410     MachineBasicBlock *emitEHSjLjLongJmp(MachineInstr *MI,
411                                          MachineBasicBlock *MBB) const;
413     ConstraintType getConstraintType(const std::string &Constraint) const;
415     /// Examine constraint string and operand type and determine a weight value.
416     /// The operand object must already have been set up with the operand type.
417     ConstraintWeight getSingleConstraintMatchWeight(
418       AsmOperandInfo &info, const char *constraint) const;
420     std::pair<unsigned, const TargetRegisterClass*>
421       getRegForInlineAsmConstraint(const std::string &Constraint,
422                                    EVT VT) const;
424     /// getByValTypeAlignment - Return the desired alignment for ByVal aggregate
425     /// function arguments in the caller parameter area.  This is the actual
426     /// alignment, not its logarithm.
427     unsigned getByValTypeAlignment(Type *Ty) const;
429     /// LowerAsmOperandForConstraint - Lower the specified operand into the Ops
430     /// vector.  If it is invalid, don't add anything to Ops.
431     virtual void LowerAsmOperandForConstraint(SDValue Op,
432                                               std::string &Constraint,
433                                               std::vector<SDValue> &Ops,
434                                               SelectionDAG &DAG) const;
436     /// isLegalAddressingMode - Return true if the addressing mode represented
437     /// by AM is legal for this target, for a load/store of the specified type.
438     virtual bool isLegalAddressingMode(const AddrMode &AM, Type *Ty)const;
440     virtual bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const;
442     /// getOptimalMemOpType - Returns the target specific optimal type for load
443     /// and store operations as a result of memset, memcpy, and memmove
444     /// lowering. If DstAlign is zero that means it's safe to destination
445     /// alignment can satisfy any constraint. Similarly if SrcAlign is zero it
446     /// means there isn't a need to check it against alignment requirement,
447     /// probably because the source does not need to be loaded. If 'IsMemset' is
448     /// true, that means it's expanding a memset. If 'ZeroMemset' is true, that
449     /// means it's a memset of zero. 'MemcpyStrSrc' indicates whether the memcpy
450     /// source is constant so it does not need to be loaded.
451     /// It returns EVT::Other if the type should be determined using generic
452     /// target-independent logic.
453     virtual EVT
454     getOptimalMemOpType(uint64_t Size, unsigned DstAlign, unsigned SrcAlign,
455                         bool IsMemset, bool ZeroMemset, bool MemcpyStrSrc,
456                         MachineFunction &MF) const;
458     /// Is unaligned memory access allowed for the given type, and is it fast
459     /// relative to software emulation.
460     virtual bool allowsUnalignedMemoryAccesses(EVT VT, bool *Fast = 0) const;
462     /// isFMAFasterThanMulAndAdd - Return true if an FMA operation is faster than
463     /// a pair of mul and add instructions. fmuladd intrinsics will be expanded to
464     /// FMAs when this method returns true (and FMAs are legal), otherwise fmuladd
465     /// is expanded to mul + add.
466     virtual bool isFMAFasterThanMulAndAdd(EVT VT) const;
468   private:
469     SDValue getFramePointerFrameIndex(SelectionDAG & DAG) const;
470     SDValue getReturnAddrFrameIndex(SelectionDAG & DAG) const;
472     bool
473     IsEligibleForTailCallOptimization(SDValue Callee,
474                                       CallingConv::ID CalleeCC,
475                                       bool isVarArg,
476                                       const SmallVectorImpl<ISD::InputArg> &Ins,
477                                       SelectionDAG& DAG) const;
479     SDValue EmitTailCallLoadFPAndRetAddr(SelectionDAG & DAG,
480                                          int SPDiff,
481                                          SDValue Chain,
482                                          SDValue &LROpOut,
483                                          SDValue &FPOpOut,
484                                          bool isDarwinABI,
485                                          SDLoc dl) const;
487     SDValue LowerRETURNADDR(SDValue Op, SelectionDAG &DAG) const;
488     SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
489     SDValue LowerConstantPool(SDValue Op, SelectionDAG &DAG) const;
490     SDValue LowerBlockAddress(SDValue Op, SelectionDAG &DAG) const;
491     SDValue LowerGlobalTLSAddress(SDValue Op, SelectionDAG &DAG) const;
492     SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
493     SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
494     SDValue LowerSETCC(SDValue Op, SelectionDAG &DAG) const;
495     SDValue LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
496     SDValue LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
497     SDValue LowerVASTART(SDValue Op, SelectionDAG &DAG,
498                          const PPCSubtarget &Subtarget) const;
499     SDValue LowerVAARG(SDValue Op, SelectionDAG &DAG,
500                        const PPCSubtarget &Subtarget) const;
501     SDValue LowerSTACKRESTORE(SDValue Op, SelectionDAG &DAG,
502                                 const PPCSubtarget &Subtarget) const;
503     SDValue LowerDYNAMIC_STACKALLOC(SDValue Op, SelectionDAG &DAG,
504                                       const PPCSubtarget &Subtarget) const;
505     SDValue LowerSELECT_CC(SDValue Op, SelectionDAG &DAG) const;
506     SDValue LowerFP_TO_INT(SDValue Op, SelectionDAG &DAG, SDLoc dl) const;
507     SDValue LowerINT_TO_FP(SDValue Op, SelectionDAG &DAG) const;
508     SDValue LowerFLT_ROUNDS_(SDValue Op, SelectionDAG &DAG) const;
509     SDValue LowerSHL_PARTS(SDValue Op, SelectionDAG &DAG) const;
510     SDValue LowerSRL_PARTS(SDValue Op, SelectionDAG &DAG) const;
511     SDValue LowerSRA_PARTS(SDValue Op, SelectionDAG &DAG) const;
512     SDValue LowerBUILD_VECTOR(SDValue Op, SelectionDAG &DAG) const;
513     SDValue LowerVECTOR_SHUFFLE(SDValue Op, SelectionDAG &DAG) const;
514     SDValue LowerINTRINSIC_WO_CHAIN(SDValue Op, SelectionDAG &DAG) const;
515     SDValue LowerSCALAR_TO_VECTOR(SDValue Op, SelectionDAG &DAG) const;
516     SDValue LowerMUL(SDValue Op, SelectionDAG &DAG) const;
518     SDValue LowerCallResult(SDValue Chain, SDValue InFlag,
519                             CallingConv::ID CallConv, bool isVarArg,
520                             const SmallVectorImpl<ISD::InputArg> &Ins,
521                             SDLoc dl, SelectionDAG &DAG,
522                             SmallVectorImpl<SDValue> &InVals) const;
523     SDValue FinishCall(CallingConv::ID CallConv, SDLoc dl, bool isTailCall,
524                        bool isVarArg,
525                        SelectionDAG &DAG,
526                        SmallVector<std::pair<unsigned, SDValue>, 8>
527                          &RegsToPass,
528                        SDValue InFlag, SDValue Chain,
529                        SDValue &Callee,
530                        int SPDiff, unsigned NumBytes,
531                        const SmallVectorImpl<ISD::InputArg> &Ins,
532                        SmallVectorImpl<SDValue> &InVals) const;
534     virtual SDValue
535       LowerFormalArguments(SDValue Chain,
536                            CallingConv::ID CallConv, bool isVarArg,
537                            const SmallVectorImpl<ISD::InputArg> &Ins,
538                            SDLoc dl, SelectionDAG &DAG,
539                            SmallVectorImpl<SDValue> &InVals) const;
541     virtual SDValue
542       LowerCall(TargetLowering::CallLoweringInfo &CLI,
543                 SmallVectorImpl<SDValue> &InVals) const;
545     virtual bool
546       CanLowerReturn(CallingConv::ID CallConv, MachineFunction &MF,
547                    bool isVarArg,
548                    const SmallVectorImpl<ISD::OutputArg> &Outs,
549                    LLVMContext &Context) const;
551     virtual SDValue
552       LowerReturn(SDValue Chain,
553                   CallingConv::ID CallConv, bool isVarArg,
554                   const SmallVectorImpl<ISD::OutputArg> &Outs,
555                   const SmallVectorImpl<SDValue> &OutVals,
556                   SDLoc dl, SelectionDAG &DAG) const;
558     SDValue
559       extendArgForPPC64(ISD::ArgFlagsTy Flags, EVT ObjectVT, SelectionDAG &DAG,
560                         SDValue ArgVal, SDLoc dl) const;
562     void
563       setMinReservedArea(MachineFunction &MF, SelectionDAG &DAG,
564                          unsigned nAltivecParamsAtEnd,
565                          unsigned MinReservedArea, bool isPPC64) const;
567     SDValue
568       LowerFormalArguments_Darwin(SDValue Chain,
569                                   CallingConv::ID CallConv, bool isVarArg,
570                                   const SmallVectorImpl<ISD::InputArg> &Ins,
571                                   SDLoc dl, SelectionDAG &DAG,
572                                   SmallVectorImpl<SDValue> &InVals) const;
573     SDValue
574       LowerFormalArguments_64SVR4(SDValue Chain,
575                                   CallingConv::ID CallConv, bool isVarArg,
576                                   const SmallVectorImpl<ISD::InputArg> &Ins,
577                                   SDLoc dl, SelectionDAG &DAG,
578                                   SmallVectorImpl<SDValue> &InVals) const;
579     SDValue
580       LowerFormalArguments_32SVR4(SDValue Chain,
581                                   CallingConv::ID CallConv, bool isVarArg,
582                                   const SmallVectorImpl<ISD::InputArg> &Ins,
583                                   SDLoc dl, SelectionDAG &DAG,
584                                   SmallVectorImpl<SDValue> &InVals) const;
586     SDValue
587       createMemcpyOutsideCallSeq(SDValue Arg, SDValue PtrOff,
588                                  SDValue CallSeqStart, ISD::ArgFlagsTy Flags,
589                                  SelectionDAG &DAG, SDLoc dl) const;
591     SDValue
592       LowerCall_Darwin(SDValue Chain, SDValue Callee,
593                        CallingConv::ID CallConv,
594                        bool isVarArg, bool isTailCall,
595                        const SmallVectorImpl<ISD::OutputArg> &Outs,
596                        const SmallVectorImpl<SDValue> &OutVals,
597                        const SmallVectorImpl<ISD::InputArg> &Ins,
598                        SDLoc dl, SelectionDAG &DAG,
599                        SmallVectorImpl<SDValue> &InVals) const;
600     SDValue
601       LowerCall_64SVR4(SDValue Chain, SDValue Callee,
602                        CallingConv::ID CallConv,
603                        bool isVarArg, bool isTailCall,
604                        const SmallVectorImpl<ISD::OutputArg> &Outs,
605                        const SmallVectorImpl<SDValue> &OutVals,
606                        const SmallVectorImpl<ISD::InputArg> &Ins,
607                        SDLoc dl, SelectionDAG &DAG,
608                        SmallVectorImpl<SDValue> &InVals) const;
609     SDValue
610     LowerCall_32SVR4(SDValue Chain, SDValue Callee, CallingConv::ID CallConv,
611                      bool isVarArg, bool isTailCall,
612                      const SmallVectorImpl<ISD::OutputArg> &Outs,
613                      const SmallVectorImpl<SDValue> &OutVals,
614                      const SmallVectorImpl<ISD::InputArg> &Ins,
615                      SDLoc dl, SelectionDAG &DAG,
616                      SmallVectorImpl<SDValue> &InVals) const;
618     SDValue lowerEH_SJLJ_SETJMP(SDValue Op, SelectionDAG &DAG) const;
619     SDValue lowerEH_SJLJ_LONGJMP(SDValue Op, SelectionDAG &DAG) const;
621     SDValue DAGCombineFastRecip(SDValue Op, DAGCombinerInfo &DCI) const;
622     SDValue DAGCombineFastRecipFSQRT(SDValue Op, DAGCombinerInfo &DCI) const;
623   };
626 #endif   // LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H