1 //===-- PPCISelLowering.h - PPC32 DAG Lowering Interface --------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the interfaces that PPC uses to lower LLVM code into a
11 // selection DAG.
12 //
13 //===----------------------------------------------------------------------===//
15 #ifndef LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
16 #define LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
18 #include "PPC.h"
19 #include "PPCInstrInfo.h"
20 #include "PPCRegisterInfo.h"
21 #include "PPCSubtarget.h"
22 #include "llvm/CodeGen/SelectionDAG.h"
23 #include "llvm/Target/TargetLowering.h"
25 namespace llvm {
26 namespace PPCISD {
27 enum NodeType {
28 // Start the numbering where the builtin ops and target ops leave off.
29 FIRST_NUMBER = ISD::BUILTIN_OP_END,
31 /// FSEL - Traditional three-operand fsel node.
32 ///
33 FSEL,
35 /// FCFID - The FCFID instruction, taking an f64 operand and producing
36 /// and f64 value containing the FP representation of the integer that
37 /// was temporarily in the f64 operand.
38 FCFID,
40 /// Newer FCFID[US] integer-to-floating-point conversion instructions for
41 /// unsigned integers and single-precision outputs.
42 FCFIDU, FCFIDS, FCFIDUS,
44 /// FCTI[D,W]Z - The FCTIDZ and FCTIWZ instructions, taking an f32 or f64
45 /// operand, producing an f64 value containing the integer representation
46 /// of that FP value.
47 FCTIDZ, FCTIWZ,
49 /// Newer FCTI[D,W]UZ floating-point-to-integer conversion instructions for
50 /// unsigned integers.
51 FCTIDUZ, FCTIWUZ,
53 /// Reciprocal estimate instructions (unary FP ops).
54 FRE, FRSQRTE,
56 // VMADDFP, VNMSUBFP - The VMADDFP and VNMSUBFP instructions, taking
57 // three v4f32 operands and producing a v4f32 result.
58 VMADDFP, VNMSUBFP,
60 /// VPERM - The PPC VPERM Instruction.
61 ///
62 VPERM,
64 /// Hi/Lo - These represent the high and low 16-bit parts of a global
65 /// address respectively. These nodes have two operands, the first of
66 /// which must be a TargetGlobalAddress, and the second of which must be a
67 /// Constant. Selected naively, these turn into 'lis G+C' and 'li G+C',
68 /// though these are usually folded into other nodes.
69 Hi, Lo,
71 TOC_ENTRY,
73 /// The following three target-specific nodes are used for calls through
74 /// function pointers in the 64-bit SVR4 ABI.
76 /// Restore the TOC from the TOC save area of the current stack frame.
77 /// This is basically a hard coded load instruction which additionally
78 /// takes/produces a flag.
79 TOC_RESTORE,
81 /// Like a regular LOAD but additionally taking/producing a flag.
82 LOAD,
84 /// LOAD into r2 (also taking/producing a flag). Like TOC_RESTORE, this is
85 /// a hard coded load instruction.
86 LOAD_TOC,
88 /// OPRC, CHAIN = DYNALLOC(CHAIN, NEGSIZE, FRAME_INDEX)
89 /// This instruction is lowered in PPCRegisterInfo::eliminateFrameIndex to
90 /// compute an allocation on the stack.
91 DYNALLOC,
93 /// GlobalBaseReg - On Darwin, this node represents the result of the mflr
94 /// at function entry, used for PIC code.
95 GlobalBaseReg,
97 /// These nodes represent the 32-bit PPC shifts that operate on 6-bit
98 /// shift amounts. These nodes are generated by the multi-precision shift
99 /// code.
100 SRL, SRA, SHL,
102 /// CALL - A direct function call.
103 /// CALL_NOP is a call with the special NOP which follows 64-bit
104 /// SVR4 calls.
105 CALL, CALL_NOP,
107 /// CHAIN,FLAG = MTCTR(VAL, CHAIN[, INFLAG]) - Directly corresponds to a
108 /// MTCTR instruction.
109 MTCTR,
111 /// CHAIN,FLAG = BCTRL(CHAIN, INFLAG) - Directly corresponds to a
112 /// BCTRL instruction.
113 BCTRL,
115 /// Return with a flag operand, matched by 'blr'
116 RET_FLAG,
118 /// R32 = MFCR(CRREG, INFLAG) - Represents the MFCRpseud/MFOCRF
119 /// instructions. This copies the bits corresponding to the specified
120 /// CRREG into the resultant GPR. Bits corresponding to other CR regs
121 /// are undefined.
122 MFCR,
124 // EH_SJLJ_SETJMP - SjLj exception handling setjmp.
125 EH_SJLJ_SETJMP,
127 // EH_SJLJ_LONGJMP - SjLj exception handling longjmp.
128 EH_SJLJ_LONGJMP,
130 /// RESVEC = VCMP(LHS, RHS, OPC) - Represents one of the altivec VCMP*
131 /// instructions. For lack of better number, we use the opcode number
132 /// encoding for the OPC field to identify the compare. For example, 838
133 /// is VCMPGTSH.
134 VCMP,
136 /// RESVEC, OUTFLAG = VCMPo(LHS, RHS, OPC) - Represents one of the
137 /// altivec VCMP*o instructions. For lack of better number, we use the
138 /// opcode number encoding for the OPC field to identify the compare. For
139 /// example, 838 is VCMPGTSH.
140 VCMPo,
142 /// CHAIN = COND_BRANCH CHAIN, CRRC, OPC, DESTBB [, INFLAG] - This
143 /// corresponds to the COND_BRANCH pseudo instruction. CRRC is the
144 /// condition register to branch on, OPC is the branch opcode to use (e.g.
145 /// PPC::BLE), DESTBB is the destination block to branch to, and INFLAG is
146 /// an optional input flag argument.
147 COND_BRANCH,
149 /// CHAIN = BDNZ CHAIN, DESTBB - These are used to create counter-based
150 /// loops.
151 BDNZ, BDZ,
153 /// F8RC = FADDRTZ F8RC, F8RC - This is an FADD done with rounding
154 /// towards zero. Used only as part of the long double-to-int
155 /// conversion sequence.
156 FADDRTZ,
158 /// F8RC = MFFS - This moves the FPSCR (not modeled) into the register.
159 MFFS,
161 /// LARX = This corresponds to PPC l{w|d}arx instrcution: load and
162 /// reserve indexed. This is used to implement atomic operations.
163 LARX,
165 /// STCX = This corresponds to PPC stcx. instrcution: store conditional
166 /// indexed. This is used to implement atomic operations.
167 STCX,
169 /// TC_RETURN - A tail call return.
170 /// operand #0 chain
171 /// operand #1 callee (register or absolute)
172 /// operand #2 stack adjustment
173 /// operand #3 optional in flag
174 TC_RETURN,
176 /// ch, gl = CR6[UN]SET ch, inglue - Toggle CR bit 6 for SVR4 vararg calls
177 CR6SET,
178 CR6UNSET,
180 /// G8RC = ADDIS_GOT_TPREL_HA %X2, Symbol - Used by the initial-exec
181 /// TLS model, produces an ADDIS8 instruction that adds the GOT
182 /// base to sym\@got\@tprel\@ha.
183 ADDIS_GOT_TPREL_HA,
185 /// G8RC = LD_GOT_TPREL_L Symbol, G8RReg - Used by the initial-exec
186 /// TLS model, produces a LD instruction with base register G8RReg
187 /// and offset sym\@got\@tprel\@l. This completes the addition that
188 /// finds the offset of "sym" relative to the thread pointer.
189 LD_GOT_TPREL_L,
191 /// G8RC = ADD_TLS G8RReg, Symbol - Used by the initial-exec TLS
192 /// model, produces an ADD instruction that adds the contents of
193 /// G8RReg to the thread pointer. Symbol contains a relocation
194 /// sym\@tls which is to be replaced by the thread pointer and
195 /// identifies to the linker that the instruction is part of a
196 /// TLS sequence.
197 ADD_TLS,
199 /// G8RC = ADDIS_TLSGD_HA %X2, Symbol - For the general-dynamic TLS
200 /// model, produces an ADDIS8 instruction that adds the GOT base
201 /// register to sym\@got\@tlsgd\@ha.
202 ADDIS_TLSGD_HA,
204 /// G8RC = ADDI_TLSGD_L G8RReg, Symbol - For the general-dynamic TLS
205 /// model, produces an ADDI8 instruction that adds G8RReg to
206 /// sym\@got\@tlsgd\@l.
207 ADDI_TLSGD_L,
209 /// G8RC = GET_TLS_ADDR %X3, Symbol - For the general-dynamic TLS
210 /// model, produces a call to __tls_get_addr(sym\@tlsgd).
211 GET_TLS_ADDR,
213 /// G8RC = ADDIS_TLSLD_HA %X2, Symbol - For the local-dynamic TLS
214 /// model, produces an ADDIS8 instruction that adds the GOT base
215 /// register to sym\@got\@tlsld\@ha.
216 ADDIS_TLSLD_HA,
218 /// G8RC = ADDI_TLSLD_L G8RReg, Symbol - For the local-dynamic TLS
219 /// model, produces an ADDI8 instruction that adds G8RReg to
220 /// sym\@got\@tlsld\@l.
221 ADDI_TLSLD_L,
223 /// G8RC = GET_TLSLD_ADDR %X3, Symbol - For the local-dynamic TLS
224 /// model, produces a call to __tls_get_addr(sym\@tlsld).
225 GET_TLSLD_ADDR,
227 /// G8RC = ADDIS_DTPREL_HA %X3, Symbol, Chain - For the
228 /// local-dynamic TLS model, produces an ADDIS8 instruction
229 /// that adds X3 to sym\@dtprel\@ha. The Chain operand is needed
230 /// to tie this in place following a copy to %X3 from the result
231 /// of a GET_TLSLD_ADDR.
232 ADDIS_DTPREL_HA,
234 /// G8RC = ADDI_DTPREL_L G8RReg, Symbol - For the local-dynamic TLS
235 /// model, produces an ADDI8 instruction that adds G8RReg to
236 /// sym\@got\@dtprel\@l.
237 ADDI_DTPREL_L,
239 /// VRRC = VADD_SPLAT Elt, EltSize - Temporary node to be expanded
240 /// during instruction selection to optimize a BUILD_VECTOR into
241 /// operations on splats. This is necessary to avoid losing these
242 /// optimizations due to constant folding.
243 VADD_SPLAT,
245 /// CHAIN = SC CHAIN, Imm128 - System call. The 7-bit unsigned
246 /// operand identifies the operating system entry point.
247 SC,
249 /// CHAIN = STBRX CHAIN, GPRC, Ptr, Type - This is a
250 /// byte-swapping store instruction. It byte-swaps the low "Type" bits of
251 /// the GPRC input, then stores it through Ptr. Type can be either i16 or
252 /// i32.
253 STBRX = ISD::FIRST_TARGET_MEMORY_OPCODE,
255 /// GPRC, CHAIN = LBRX CHAIN, Ptr, Type - This is a
256 /// byte-swapping load instruction. It loads "Type" bits, byte swaps it,
257 /// then puts it in the bottom bits of the GPRC. TYPE can be either i16
258 /// or i32.
259 LBRX,
261 /// STFIWX - The STFIWX instruction. The first operand is an input token
262 /// chain, then an f64 value to store, then an address to store it to.
263 STFIWX,
265 /// GPRC, CHAIN = LFIWAX CHAIN, Ptr - This is a floating-point
266 /// load which sign-extends from a 32-bit integer value into the
267 /// destination 64-bit register.
268 LFIWAX,
270 /// GPRC, CHAIN = LFIWZX CHAIN, Ptr - This is a floating-point
271 /// load which zero-extends from a 32-bit integer value into the
272 /// destination 64-bit register.
273 LFIWZX,
275 /// G8RC = ADDIS_TOC_HA %X2, Symbol - For medium and large code model,
276 /// produces an ADDIS8 instruction that adds the TOC base register to
277 /// sym\@toc\@ha.
278 ADDIS_TOC_HA,
280 /// G8RC = LD_TOC_L Symbol, G8RReg - For medium and large code model,
281 /// produces a LD instruction with base register G8RReg and offset
282 /// sym\@toc\@l. Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
283 LD_TOC_L,
285 /// G8RC = ADDI_TOC_L G8RReg, Symbol - For medium code model, produces
286 /// an ADDI8 instruction that adds G8RReg to sym\@toc\@l.
287 /// Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
288 ADDI_TOC_L
289 };
290 }
292 /// Define some predicates that are used for node matching.
293 namespace PPC {
294 /// isVPKUHUMShuffleMask - Return true if this is the shuffle mask for a
295 /// VPKUHUM instruction.
296 bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
298 /// isVPKUWUMShuffleMask - Return true if this is the shuffle mask for a
299 /// VPKUWUM instruction.
300 bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
302 /// isVMRGLShuffleMask - Return true if this is a shuffle mask suitable for
303 /// a VRGL* instruction with the specified unit size (1,2 or 4 bytes).
304 bool isVMRGLShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
305 bool isUnary);
307 /// isVMRGHShuffleMask - Return true if this is a shuffle mask suitable for
308 /// a VRGH* instruction with the specified unit size (1,2 or 4 bytes).
309 bool isVMRGHShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
310 bool isUnary);
312 /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the shift
313 /// amount, otherwise return -1.
314 int isVSLDOIShuffleMask(SDNode *N, bool isUnary);
316 /// isSplatShuffleMask - Return true if the specified VECTOR_SHUFFLE operand
317 /// specifies a splat of a single element that is suitable for input to
318 /// VSPLTB/VSPLTH/VSPLTW.
319 bool isSplatShuffleMask(ShuffleVectorSDNode *N, unsigned EltSize);
321 /// isAllNegativeZeroVector - Returns true if all elements of build_vector
322 /// are -0.0.
323 bool isAllNegativeZeroVector(SDNode *N);
325 /// getVSPLTImmediate - Return the appropriate VSPLT* immediate to splat the
326 /// specified isSplatShuffleMask VECTOR_SHUFFLE mask.
327 unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize);
329 /// get_VSPLTI_elt - If this is a build_vector of constants which can be
330 /// formed by using a vspltis[bhw] instruction of the specified element
331 /// size, return the constant being splatted. The ByteSize field indicates
332 /// the number of bytes of each element [124] -> [bhw].
333 SDValue get_VSPLTI_elt(SDNode *N, unsigned ByteSize, SelectionDAG &DAG);
334 }
336 class PPCTargetLowering : public TargetLowering {
337 const PPCSubtarget &PPCSubTarget;
338 const PPCRegisterInfo *PPCRegInfo;
339 const PPCInstrInfo *PPCII;
341 public:
342 explicit PPCTargetLowering(PPCTargetMachine &TM);
344 /// getTargetNodeName() - This method returns the name of a target specific
345 /// DAG node.
346 virtual const char *getTargetNodeName(unsigned Opcode) const;
348 virtual MVT getScalarShiftAmountTy(EVT LHSTy) const { return MVT::i32; }
350 /// getSetCCResultType - Return the ISD::SETCC ValueType
351 virtual EVT getSetCCResultType(EVT VT) const;
353 /// getPreIndexedAddressParts - returns true by value, base pointer and
354 /// offset pointer and addressing mode by reference if the node's address
355 /// can be legally represented as pre-indexed load / store address.
356 virtual bool getPreIndexedAddressParts(SDNode *N, SDValue &Base,
357 SDValue &Offset,
358 ISD::MemIndexedMode &AM,
359 SelectionDAG &DAG) const;
361 /// SelectAddressRegReg - Given the specified addressed, check to see if it
362 /// can be represented as an indexed [r+r] operation. Returns false if it
363 /// can be more efficiently represented with [r+imm].
364 bool SelectAddressRegReg(SDValue N, SDValue &Base, SDValue &Index,
365 SelectionDAG &DAG) const;
367 /// SelectAddressRegImm - Returns true if the address N can be represented
368 /// by a base register plus a signed 16-bit displacement [r+imm], and if it
369 /// is not better represented as reg+reg.
370 bool SelectAddressRegImm(SDValue N, SDValue &Disp, SDValue &Base,
371 SelectionDAG &DAG) const;
373 /// SelectAddressRegRegOnly - Given the specified addressed, force it to be
374 /// represented as an indexed [r+r] operation.
375 bool SelectAddressRegRegOnly(SDValue N, SDValue &Base, SDValue &Index,
376 SelectionDAG &DAG) const;
378 /// SelectAddressRegImmShift - Returns true if the address N can be
379 /// represented by a base register plus a signed 14-bit displacement
380 /// [r+imm*4]. Suitable for use by STD and friends.
381 bool SelectAddressRegImmShift(SDValue N, SDValue &Disp, SDValue &Base,
382 SelectionDAG &DAG) const;
384 Sched::Preference getSchedulingPreference(SDNode *N) const;
386 /// LowerOperation - Provide custom lowering hooks for some operations.
387 ///
388 virtual SDValue LowerOperation(SDValue Op, SelectionDAG &DAG) const;
390 /// ReplaceNodeResults - Replace the results of node with an illegal result
391 /// type with new values built out of custom code.
392 ///
393 virtual void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
394 SelectionDAG &DAG) const;
396 virtual SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const;
398 virtual void computeMaskedBitsForTargetNode(const SDValue Op,
399 APInt &KnownZero,
400 APInt &KnownOne,
401 const SelectionDAG &DAG,
402 unsigned Depth = 0) const;
404 virtual MachineBasicBlock *
405 EmitInstrWithCustomInserter(MachineInstr *MI,
406 MachineBasicBlock *MBB) const;
407 MachineBasicBlock *EmitAtomicBinary(MachineInstr *MI,
408 MachineBasicBlock *MBB, bool is64Bit,
409 unsigned BinOpcode) const;
410 MachineBasicBlock *EmitPartwordAtomicBinary(MachineInstr *MI,
411 MachineBasicBlock *MBB,
412 bool is8bit, unsigned Opcode) const;
414 MachineBasicBlock *emitEHSjLjSetJmp(MachineInstr *MI,
415 MachineBasicBlock *MBB) const;
417 MachineBasicBlock *emitEHSjLjLongJmp(MachineInstr *MI,
418 MachineBasicBlock *MBB) const;
420 ConstraintType getConstraintType(const std::string &Constraint) const;
422 /// Examine constraint string and operand type and determine a weight value.
423 /// The operand object must already have been set up with the operand type.
424 ConstraintWeight getSingleConstraintMatchWeight(
425 AsmOperandInfo &info, const char *constraint) const;
427 std::pair<unsigned, const TargetRegisterClass*>
428 getRegForInlineAsmConstraint(const std::string &Constraint,
429 EVT VT) const;
431 /// getByValTypeAlignment - Return the desired alignment for ByVal aggregate
432 /// function arguments in the caller parameter area. This is the actual
433 /// alignment, not its logarithm.
434 unsigned getByValTypeAlignment(Type *Ty) const;
436 /// LowerAsmOperandForConstraint - Lower the specified operand into the Ops
437 /// vector. If it is invalid, don't add anything to Ops.
438 virtual void LowerAsmOperandForConstraint(SDValue Op,
439 std::string &Constraint,
440 std::vector<SDValue> &Ops,
441 SelectionDAG &DAG) const;
443 /// isLegalAddressingMode - Return true if the addressing mode represented
444 /// by AM is legal for this target, for a load/store of the specified type.
445 virtual bool isLegalAddressingMode(const AddrMode &AM, Type *Ty)const;
447 virtual bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const;
449 /// getOptimalMemOpType - Returns the target specific optimal type for load
450 /// and store operations as a result of memset, memcpy, and memmove
451 /// lowering. If DstAlign is zero that means it's safe to destination
452 /// alignment can satisfy any constraint. Similarly if SrcAlign is zero it
453 /// means there isn't a need to check it against alignment requirement,
454 /// probably because the source does not need to be loaded. If 'IsMemset' is
455 /// true, that means it's expanding a memset. If 'ZeroMemset' is true, that
456 /// means it's a memset of zero. 'MemcpyStrSrc' indicates whether the memcpy
457 /// source is constant so it does not need to be loaded.
458 /// It returns EVT::Other if the type should be determined using generic
459 /// target-independent logic.
460 virtual EVT
461 getOptimalMemOpType(uint64_t Size, unsigned DstAlign, unsigned SrcAlign,
462 bool IsMemset, bool ZeroMemset, bool MemcpyStrSrc,
463 MachineFunction &MF) const;
465 /// Is unaligned memory access allowed for the given type, and is it fast
466 /// relative to software emulation.
467 virtual bool allowsUnalignedMemoryAccesses(EVT VT, bool *Fast = 0) const;
469 /// isFMAFasterThanMulAndAdd - Return true if an FMA operation is faster than
470 /// a pair of mul and add instructions. fmuladd intrinsics will be expanded to
471 /// FMAs when this method returns true (and FMAs are legal), otherwise fmuladd
472 /// is expanded to mul + add.
473 virtual bool isFMAFasterThanMulAndAdd(EVT VT) const;
475 private:
476 SDValue getFramePointerFrameIndex(SelectionDAG & DAG) const;
477 SDValue getReturnAddrFrameIndex(SelectionDAG & DAG) const;
479 bool
480 IsEligibleForTailCallOptimization(SDValue Callee,
481 CallingConv::ID CalleeCC,
482 bool isVarArg,
483 const SmallVectorImpl<ISD::InputArg> &Ins,
484 SelectionDAG& DAG) const;
486 SDValue EmitTailCallLoadFPAndRetAddr(SelectionDAG & DAG,
487 int SPDiff,
488 SDValue Chain,
489 SDValue &LROpOut,
490 SDValue &FPOpOut,
491 bool isDarwinABI,
492 DebugLoc dl) const;
494 SDValue LowerRETURNADDR(SDValue Op, SelectionDAG &DAG) const;
495 SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
496 SDValue LowerConstantPool(SDValue Op, SelectionDAG &DAG) const;
497 SDValue LowerBlockAddress(SDValue Op, SelectionDAG &DAG) const;
498 SDValue LowerGlobalTLSAddress(SDValue Op, SelectionDAG &DAG) const;
499 SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
500 SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
501 SDValue LowerSETCC(SDValue Op, SelectionDAG &DAG) const;
502 SDValue LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
503 SDValue LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
504 SDValue LowerVASTART(SDValue Op, SelectionDAG &DAG,
505 const PPCSubtarget &Subtarget) const;
506 SDValue LowerVAARG(SDValue Op, SelectionDAG &DAG,
507 const PPCSubtarget &Subtarget) const;
508 SDValue LowerSTACKRESTORE(SDValue Op, SelectionDAG &DAG,
509 const PPCSubtarget &Subtarget) const;
510 SDValue LowerDYNAMIC_STACKALLOC(SDValue Op, SelectionDAG &DAG,
511 const PPCSubtarget &Subtarget) const;
512 SDValue LowerSELECT_CC(SDValue Op, SelectionDAG &DAG) const;
513 SDValue LowerFP_TO_INT(SDValue Op, SelectionDAG &DAG, DebugLoc dl) const;
514 SDValue LowerINT_TO_FP(SDValue Op, SelectionDAG &DAG) const;
515 SDValue LowerFLT_ROUNDS_(SDValue Op, SelectionDAG &DAG) const;
516 SDValue LowerSHL_PARTS(SDValue Op, SelectionDAG &DAG) const;
517 SDValue LowerSRL_PARTS(SDValue Op, SelectionDAG &DAG) const;
518 SDValue LowerSRA_PARTS(SDValue Op, SelectionDAG &DAG) const;
519 SDValue LowerBUILD_VECTOR(SDValue Op, SelectionDAG &DAG) const;
520 SDValue LowerVECTOR_SHUFFLE(SDValue Op, SelectionDAG &DAG) const;
521 SDValue LowerINTRINSIC_WO_CHAIN(SDValue Op, SelectionDAG &DAG) const;
522 SDValue LowerSCALAR_TO_VECTOR(SDValue Op, SelectionDAG &DAG) const;
523 SDValue LowerMUL(SDValue Op, SelectionDAG &DAG) const;
525 SDValue LowerCallResult(SDValue Chain, SDValue InFlag,
526 CallingConv::ID CallConv, bool isVarArg,
527 const SmallVectorImpl<ISD::InputArg> &Ins,
528 DebugLoc dl, SelectionDAG &DAG,
529 SmallVectorImpl<SDValue> &InVals) const;
530 SDValue FinishCall(CallingConv::ID CallConv, DebugLoc dl, bool isTailCall,
531 bool isVarArg,
532 SelectionDAG &DAG,
533 SmallVector<std::pair<unsigned, SDValue>, 8>
534 &RegsToPass,
535 SDValue InFlag, SDValue Chain,
536 SDValue &Callee,
537 int SPDiff, unsigned NumBytes,
538 const SmallVectorImpl<ISD::InputArg> &Ins,
539 SmallVectorImpl<SDValue> &InVals) const;
541 virtual SDValue
542 LowerFormalArguments(SDValue Chain,
543 CallingConv::ID CallConv, bool isVarArg,
544 const SmallVectorImpl<ISD::InputArg> &Ins,
545 DebugLoc dl, SelectionDAG &DAG,
546 SmallVectorImpl<SDValue> &InVals) const;
548 virtual SDValue
549 LowerCall(TargetLowering::CallLoweringInfo &CLI,
550 SmallVectorImpl<SDValue> &InVals) const;
552 virtual bool
553 CanLowerReturn(CallingConv::ID CallConv, MachineFunction &MF,
554 bool isVarArg,
555 const SmallVectorImpl<ISD::OutputArg> &Outs,
556 LLVMContext &Context) const;
558 virtual SDValue
559 LowerReturn(SDValue Chain,
560 CallingConv::ID CallConv, bool isVarArg,
561 const SmallVectorImpl<ISD::OutputArg> &Outs,
562 const SmallVectorImpl<SDValue> &OutVals,
563 DebugLoc dl, SelectionDAG &DAG) const;
565 SDValue
566 extendArgForPPC64(ISD::ArgFlagsTy Flags, EVT ObjectVT, SelectionDAG &DAG,
567 SDValue ArgVal, DebugLoc dl) const;
569 void
570 setMinReservedArea(MachineFunction &MF, SelectionDAG &DAG,
571 unsigned nAltivecParamsAtEnd,
572 unsigned MinReservedArea, bool isPPC64) const;
574 SDValue
575 LowerFormalArguments_Darwin(SDValue Chain,
576 CallingConv::ID CallConv, bool isVarArg,
577 const SmallVectorImpl<ISD::InputArg> &Ins,
578 DebugLoc dl, SelectionDAG &DAG,
579 SmallVectorImpl<SDValue> &InVals) const;
580 SDValue
581 LowerFormalArguments_64SVR4(SDValue Chain,
582 CallingConv::ID CallConv, bool isVarArg,
583 const SmallVectorImpl<ISD::InputArg> &Ins,
584 DebugLoc dl, SelectionDAG &DAG,
585 SmallVectorImpl<SDValue> &InVals) const;
586 SDValue
587 LowerFormalArguments_32SVR4(SDValue Chain,
588 CallingConv::ID CallConv, bool isVarArg,
589 const SmallVectorImpl<ISD::InputArg> &Ins,
590 DebugLoc dl, SelectionDAG &DAG,
591 SmallVectorImpl<SDValue> &InVals) const;
593 SDValue
594 createMemcpyOutsideCallSeq(SDValue Arg, SDValue PtrOff,
595 SDValue CallSeqStart, ISD::ArgFlagsTy Flags,
596 SelectionDAG &DAG, DebugLoc dl) const;
598 SDValue
599 LowerCall_Darwin(SDValue Chain, SDValue Callee,
600 CallingConv::ID CallConv,
601 bool isVarArg, bool isTailCall,
602 const SmallVectorImpl<ISD::OutputArg> &Outs,
603 const SmallVectorImpl<SDValue> &OutVals,
604 const SmallVectorImpl<ISD::InputArg> &Ins,
605 DebugLoc dl, SelectionDAG &DAG,
606 SmallVectorImpl<SDValue> &InVals) const;
607 SDValue
608 LowerCall_64SVR4(SDValue Chain, SDValue Callee,
609 CallingConv::ID CallConv,
610 bool isVarArg, bool isTailCall,
611 const SmallVectorImpl<ISD::OutputArg> &Outs,
612 const SmallVectorImpl<SDValue> &OutVals,
613 const SmallVectorImpl<ISD::InputArg> &Ins,
614 DebugLoc dl, SelectionDAG &DAG,
615 SmallVectorImpl<SDValue> &InVals) const;
616 SDValue
617 LowerCall_32SVR4(SDValue Chain, SDValue Callee, CallingConv::ID CallConv,
618 bool isVarArg, bool isTailCall,
619 const SmallVectorImpl<ISD::OutputArg> &Outs,
620 const SmallVectorImpl<SDValue> &OutVals,
621 const SmallVectorImpl<ISD::InputArg> &Ins,
622 DebugLoc dl, SelectionDAG &DAG,
623 SmallVectorImpl<SDValue> &InVals) const;
625 SDValue lowerEH_SJLJ_SETJMP(SDValue Op, SelectionDAG &DAG) const;
626 SDValue lowerEH_SJLJ_LONGJMP(SDValue Op, SelectionDAG &DAG) const;
628 SDValue DAGCombineFastRecip(SDValue Op, DAGCombinerInfo &DCI) const;
629 SDValue DAGCombineFastRecipFSQRT(SDValue Op, DAGCombinerInfo &DCI) const;
630 };
631 }
633 #endif // LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H