1 /*===- X86DisassemblerDecoderCommon.h - Disassembler decoder -------*- C -*-==*
2 *
3 * The LLVM Compiler Infrastructure
4 *
5 * This file is distributed under the University of Illinois Open Source
6 * License. See LICENSE.TXT for details.
7 *
8 *===----------------------------------------------------------------------===*
9 *
10 * This file is part of the X86 Disassembler.
11 * It contains common definitions used by both the disassembler and the table
12 * generator.
13 * Documentation for the disassembler can be found in X86Disassembler.h.
14 *
15 *===----------------------------------------------------------------------===*/
17 /*
18 * This header file provides those definitions that need to be shared between
19 * the decoder and the table generator in a C-friendly manner.
20 */
22 #ifndef X86DISASSEMBLERDECODERCOMMON_H
23 #define X86DISASSEMBLERDECODERCOMMON_H
25 #include "llvm/Support/DataTypes.h"
27 #define INSTRUCTIONS_SYM x86DisassemblerInstrSpecifiers
28 #define CONTEXTS_SYM x86DisassemblerContexts
29 #define ONEBYTE_SYM x86DisassemblerOneByteOpcodes
30 #define TWOBYTE_SYM x86DisassemblerTwoByteOpcodes
31 #define THREEBYTE38_SYM x86DisassemblerThreeByte38Opcodes
32 #define THREEBYTE3A_SYM x86DisassemblerThreeByte3AOpcodes
33 #define THREEBYTEA6_SYM x86DisassemblerThreeByteA6Opcodes
34 #define THREEBYTEA7_SYM x86DisassemblerThreeByteA7Opcodes
36 #define INSTRUCTIONS_STR "x86DisassemblerInstrSpecifiers"
37 #define CONTEXTS_STR "x86DisassemblerContexts"
38 #define ONEBYTE_STR "x86DisassemblerOneByteOpcodes"
39 #define TWOBYTE_STR "x86DisassemblerTwoByteOpcodes"
40 #define THREEBYTE38_STR "x86DisassemblerThreeByte38Opcodes"
41 #define THREEBYTE3A_STR "x86DisassemblerThreeByte3AOpcodes"
42 #define THREEBYTEA6_STR "x86DisassemblerThreeByteA6Opcodes"
43 #define THREEBYTEA7_STR "x86DisassemblerThreeByteA7Opcodes"
45 /*
46 * Attributes of an instruction that must be known before the opcode can be
47 * processed correctly. Most of these indicate the presence of particular
48 * prefixes, but ATTR_64BIT is simply an attribute of the decoding context.
49 */
50 #define ATTRIBUTE_BITS \
51 ENUM_ENTRY(ATTR_NONE, 0x00) \
52 ENUM_ENTRY(ATTR_64BIT, 0x01) \
53 ENUM_ENTRY(ATTR_XS, 0x02) \
54 ENUM_ENTRY(ATTR_XD, 0x04) \
55 ENUM_ENTRY(ATTR_REXW, 0x08) \
56 ENUM_ENTRY(ATTR_OPSIZE, 0x10) \
57 ENUM_ENTRY(ATTR_VEX, 0x20) \
58 ENUM_ENTRY(ATTR_VEXL, 0x40)
60 #define ENUM_ENTRY(n, v) n = v,
61 enum attributeBits {
62 ATTRIBUTE_BITS
63 ATTR_max
64 };
65 #undef ENUM_ENTRY
67 /*
68 * Combinations of the above attributes that are relevant to instruction
69 * decode. Although other combinations are possible, they can be reduced to
70 * these without affecting the ultimately decoded instruction.
71 */
73 /* Class name Rank Rationale for rank assignment */
74 #define INSTRUCTION_CONTEXTS \
75 ENUM_ENTRY(IC, 0, "says nothing about the instruction") \
76 ENUM_ENTRY(IC_64BIT, 1, "says the instruction applies in " \
77 "64-bit mode but no more") \
78 ENUM_ENTRY(IC_OPSIZE, 3, "requires an OPSIZE prefix, so " \
79 "operands change width") \
80 ENUM_ENTRY(IC_XD, 2, "may say something about the opcode " \
81 "but not the operands") \
82 ENUM_ENTRY(IC_XS, 2, "may say something about the opcode " \
83 "but not the operands") \
84 ENUM_ENTRY(IC_XD_OPSIZE, 3, "requires an OPSIZE prefix, so " \
85 "operands change width") \
86 ENUM_ENTRY(IC_64BIT_REXW, 4, "requires a REX.W prefix, so operands "\
87 "change width; overrides IC_OPSIZE") \
88 ENUM_ENTRY(IC_64BIT_OPSIZE, 3, "Just as meaningful as IC_OPSIZE") \
89 ENUM_ENTRY(IC_64BIT_XD, 5, "XD instructions are SSE; REX.W is " \
90 "secondary") \
91 ENUM_ENTRY(IC_64BIT_XS, 5, "Just as meaningful as IC_64BIT_XD") \
92 ENUM_ENTRY(IC_64BIT_XD_OPSIZE, 3, "Just as meaningful as IC_XD_OPSIZE") \
93 ENUM_ENTRY(IC_64BIT_REXW_XS, 6, "OPSIZE could mean a different " \
94 "opcode") \
95 ENUM_ENTRY(IC_64BIT_REXW_XD, 6, "Just as meaningful as " \
96 "IC_64BIT_REXW_XS") \
97 ENUM_ENTRY(IC_64BIT_REXW_OPSIZE, 7, "The Dynamic Duo! Prefer over all " \
98 "else because this changes most " \
99 "operands' meaning") \
100 ENUM_ENTRY(IC_VEX, 1, "requires a VEX prefix") \
101 ENUM_ENTRY(IC_VEX_XS, 2, "requires VEX and the XS prefix") \
102 ENUM_ENTRY(IC_VEX_XD, 2, "requires VEX and the XD prefix") \
103 ENUM_ENTRY(IC_VEX_OPSIZE, 2, "requires VEX and the OpSize prefix") \
104 ENUM_ENTRY(IC_VEX_W, 3, "requires VEX and the W prefix") \
105 ENUM_ENTRY(IC_VEX_W_XS, 4, "requires VEX, W, and XS prefix") \
106 ENUM_ENTRY(IC_VEX_W_XD, 4, "requires VEX, W, and XD prefix") \
107 ENUM_ENTRY(IC_VEX_W_OPSIZE, 4, "requires VEX, W, and OpSize") \
108 ENUM_ENTRY(IC_VEX_L, 3, "requires VEX and the L prefix") \
109 ENUM_ENTRY(IC_VEX_L_XS, 4, "requires VEX and the L and XS prefix")\
110 ENUM_ENTRY(IC_VEX_L_XD, 4, "requires VEX and the L and XD prefix")\
111 ENUM_ENTRY(IC_VEX_L_OPSIZE, 4, "requires VEX, L, and OpSize")
114 #define ENUM_ENTRY(n, r, d) n,
115 typedef enum {
116 INSTRUCTION_CONTEXTS
117 IC_max
118 } InstructionContext;
119 #undef ENUM_ENTRY
121 /*
122 * Opcode types, which determine which decode table to use, both in the Intel
123 * manual and also for the decoder.
124 */
125 typedef enum {
126 ONEBYTE = 0,
127 TWOBYTE = 1,
128 THREEBYTE_38 = 2,
129 THREEBYTE_3A = 3,
130 THREEBYTE_A6 = 4,
131 THREEBYTE_A7 = 5
132 } OpcodeType;
134 /*
135 * The following structs are used for the hierarchical decode table. After
136 * determining the instruction's class (i.e., which IC_* constant applies to
137 * it), the decoder reads the opcode. Some instructions require specific
138 * values of the ModR/M byte, so the ModR/M byte indexes into the final table.
139 *
140 * If a ModR/M byte is not required, "required" is left unset, and the values
141 * for each instructionID are identical.
142 */
144 typedef uint16_t InstrUID;
146 /*
147 * ModRMDecisionType - describes the type of ModR/M decision, allowing the
148 * consumer to determine the number of entries in it.
149 *
150 * MODRM_ONEENTRY - No matter what the value of the ModR/M byte is, the decoded
151 * instruction is the same.
152 * MODRM_SPLITRM - If the ModR/M byte is between 0x00 and 0xbf, the opcode
153 * corresponds to one instruction; otherwise, it corresponds to
154 * a different instruction.
155 * MODRM_FULL - Potentially, each value of the ModR/M byte could correspond
156 * to a different instruction.
157 */
159 #define MODRMTYPES \
160 ENUM_ENTRY(MODRM_ONEENTRY) \
161 ENUM_ENTRY(MODRM_SPLITRM) \
162 ENUM_ENTRY(MODRM_FULL)
164 #define ENUM_ENTRY(n) n,
165 typedef enum {
166 MODRMTYPES
167 MODRM_max
168 } ModRMDecisionType;
169 #undef ENUM_ENTRY
171 /*
172 * ModRMDecision - Specifies whether a ModR/M byte is needed and (if so) which
173 * instruction each possible value of the ModR/M byte corresponds to. Once
174 * this information is known, we have narrowed down to a single instruction.
175 */
176 struct ModRMDecision {
177 uint8_t modrm_type;
179 /* The macro below must be defined wherever this file is included. */
180 INSTRUCTION_IDS
181 };
183 /*
184 * OpcodeDecision - Specifies which set of ModR/M->instruction tables to look at
185 * given a particular opcode.
186 */
187 struct OpcodeDecision {
188 struct ModRMDecision modRMDecisions[256];
189 };
191 /*
192 * ContextDecision - Specifies which opcode->instruction tables to look at given
193 * a particular context (set of attributes). Since there are many possible
194 * contexts, the decoder first uses CONTEXTS_SYM to determine which context
195 * applies given a specific set of attributes. Hence there are only IC_max
196 * entries in this table, rather than 2^(ATTR_max).
197 */
198 struct ContextDecision {
199 struct OpcodeDecision opcodeDecisions[IC_max];
200 };
202 /*
203 * Physical encodings of instruction operands.
204 */
206 #define ENCODINGS \
207 ENUM_ENTRY(ENCODING_NONE, "") \
208 ENUM_ENTRY(ENCODING_REG, "Register operand in ModR/M byte.") \
209 ENUM_ENTRY(ENCODING_RM, "R/M operand in ModR/M byte.") \
210 ENUM_ENTRY(ENCODING_VVVV, "Register operand in VEX.vvvv byte.") \
211 ENUM_ENTRY(ENCODING_CB, "1-byte code offset (possible new CS value)") \
212 ENUM_ENTRY(ENCODING_CW, "2-byte") \
213 ENUM_ENTRY(ENCODING_CD, "4-byte") \
214 ENUM_ENTRY(ENCODING_CP, "6-byte") \
215 ENUM_ENTRY(ENCODING_CO, "8-byte") \
216 ENUM_ENTRY(ENCODING_CT, "10-byte") \
217 ENUM_ENTRY(ENCODING_IB, "1-byte immediate") \
218 ENUM_ENTRY(ENCODING_IW, "2-byte") \
219 ENUM_ENTRY(ENCODING_ID, "4-byte") \
220 ENUM_ENTRY(ENCODING_IO, "8-byte") \
221 ENUM_ENTRY(ENCODING_RB, "(AL..DIL, R8L..R15L) Register code added to " \
222 "the opcode byte") \
223 ENUM_ENTRY(ENCODING_RW, "(AX..DI, R8W..R15W)") \
224 ENUM_ENTRY(ENCODING_RD, "(EAX..EDI, R8D..R15D)") \
225 ENUM_ENTRY(ENCODING_RO, "(RAX..RDI, R8..R15)") \
226 ENUM_ENTRY(ENCODING_I, "Position on floating-point stack added to the " \
227 "opcode byte") \
228 \
229 ENUM_ENTRY(ENCODING_Iv, "Immediate of operand size") \
230 ENUM_ENTRY(ENCODING_Ia, "Immediate of address size") \
231 ENUM_ENTRY(ENCODING_Rv, "Register code of operand size added to the " \
232 "opcode byte") \
233 ENUM_ENTRY(ENCODING_DUP, "Duplicate of another operand; ID is encoded " \
234 "in type")
236 #define ENUM_ENTRY(n, d) n,
237 typedef enum {
238 ENCODINGS
239 ENCODING_max
240 } OperandEncoding;
241 #undef ENUM_ENTRY
243 /*
244 * Semantic interpretations of instruction operands.
245 */
247 #define TYPES \
248 ENUM_ENTRY(TYPE_NONE, "") \
249 ENUM_ENTRY(TYPE_REL8, "1-byte immediate address") \
250 ENUM_ENTRY(TYPE_REL16, "2-byte") \
251 ENUM_ENTRY(TYPE_REL32, "4-byte") \
252 ENUM_ENTRY(TYPE_REL64, "8-byte") \
253 ENUM_ENTRY(TYPE_PTR1616, "2+2-byte segment+offset address") \
254 ENUM_ENTRY(TYPE_PTR1632, "2+4-byte") \
255 ENUM_ENTRY(TYPE_PTR1664, "2+8-byte") \
256 ENUM_ENTRY(TYPE_R8, "1-byte register operand") \
257 ENUM_ENTRY(TYPE_R16, "2-byte") \
258 ENUM_ENTRY(TYPE_R32, "4-byte") \
259 ENUM_ENTRY(TYPE_R64, "8-byte") \
260 ENUM_ENTRY(TYPE_IMM8, "1-byte immediate operand") \
261 ENUM_ENTRY(TYPE_IMM16, "2-byte") \
262 ENUM_ENTRY(TYPE_IMM32, "4-byte") \
263 ENUM_ENTRY(TYPE_IMM64, "8-byte") \
264 ENUM_ENTRY(TYPE_IMM3, "1-byte immediate operand between 0 and 7") \
265 ENUM_ENTRY(TYPE_RM8, "1-byte register or memory operand") \
266 ENUM_ENTRY(TYPE_RM16, "2-byte") \
267 ENUM_ENTRY(TYPE_RM32, "4-byte") \
268 ENUM_ENTRY(TYPE_RM64, "8-byte") \
269 ENUM_ENTRY(TYPE_M, "Memory operand") \
270 ENUM_ENTRY(TYPE_M8, "1-byte") \
271 ENUM_ENTRY(TYPE_M16, "2-byte") \
272 ENUM_ENTRY(TYPE_M32, "4-byte") \
273 ENUM_ENTRY(TYPE_M64, "8-byte") \
274 ENUM_ENTRY(TYPE_LEA, "Effective address") \
275 ENUM_ENTRY(TYPE_M128, "16-byte (SSE/SSE2)") \
276 ENUM_ENTRY(TYPE_M256, "256-byte (AVX)") \
277 ENUM_ENTRY(TYPE_M1616, "2+2-byte segment+offset address") \
278 ENUM_ENTRY(TYPE_M1632, "2+4-byte") \
279 ENUM_ENTRY(TYPE_M1664, "2+8-byte") \
280 ENUM_ENTRY(TYPE_M16_32, "2+4-byte two-part memory operand (LIDT, LGDT)") \
281 ENUM_ENTRY(TYPE_M16_16, "2+2-byte (BOUND)") \
282 ENUM_ENTRY(TYPE_M32_32, "4+4-byte (BOUND)") \
283 ENUM_ENTRY(TYPE_M16_64, "2+8-byte (LIDT, LGDT)") \
284 ENUM_ENTRY(TYPE_MOFFS8, "1-byte memory offset (relative to segment " \
285 "base)") \
286 ENUM_ENTRY(TYPE_MOFFS16, "2-byte") \
287 ENUM_ENTRY(TYPE_MOFFS32, "4-byte") \
288 ENUM_ENTRY(TYPE_MOFFS64, "8-byte") \
289 ENUM_ENTRY(TYPE_SREG, "Byte with single bit set: 0 = ES, 1 = CS, " \
290 "2 = SS, 3 = DS, 4 = FS, 5 = GS") \
291 ENUM_ENTRY(TYPE_M32FP, "32-bit IEE754 memory floating-point operand") \
292 ENUM_ENTRY(TYPE_M64FP, "64-bit") \
293 ENUM_ENTRY(TYPE_M80FP, "80-bit extended") \
294 ENUM_ENTRY(TYPE_M16INT, "2-byte memory integer operand for use in " \
295 "floating-point instructions") \
296 ENUM_ENTRY(TYPE_M32INT, "4-byte") \
297 ENUM_ENTRY(TYPE_M64INT, "8-byte") \
298 ENUM_ENTRY(TYPE_ST, "Position on the floating-point stack") \
299 ENUM_ENTRY(TYPE_MM, "MMX register operand") \
300 ENUM_ENTRY(TYPE_MM32, "4-byte MMX register or memory operand") \
301 ENUM_ENTRY(TYPE_MM64, "8-byte") \
302 ENUM_ENTRY(TYPE_XMM, "XMM register operand") \
303 ENUM_ENTRY(TYPE_XMM32, "4-byte XMM register or memory operand") \
304 ENUM_ENTRY(TYPE_XMM64, "8-byte") \
305 ENUM_ENTRY(TYPE_XMM128, "16-byte") \
306 ENUM_ENTRY(TYPE_XMM256, "32-byte") \
307 ENUM_ENTRY(TYPE_XMM0, "Implicit use of XMM0") \
308 ENUM_ENTRY(TYPE_SEGMENTREG, "Segment register operand") \
309 ENUM_ENTRY(TYPE_DEBUGREG, "Debug register operand") \
310 ENUM_ENTRY(TYPE_CONTROLREG, "Control register operand") \
311 \
312 ENUM_ENTRY(TYPE_Mv, "Memory operand of operand size") \
313 ENUM_ENTRY(TYPE_Rv, "Register operand of operand size") \
314 ENUM_ENTRY(TYPE_IMMv, "Immediate operand of operand size") \
315 ENUM_ENTRY(TYPE_RELv, "Immediate address of operand size") \
316 ENUM_ENTRY(TYPE_DUP0, "Duplicate of operand 0") \
317 ENUM_ENTRY(TYPE_DUP1, "operand 1") \
318 ENUM_ENTRY(TYPE_DUP2, "operand 2") \
319 ENUM_ENTRY(TYPE_DUP3, "operand 3") \
320 ENUM_ENTRY(TYPE_DUP4, "operand 4") \
321 ENUM_ENTRY(TYPE_M512, "512-bit FPU/MMX/XMM/MXCSR state")
323 #define ENUM_ENTRY(n, d) n,
324 typedef enum {
325 TYPES
326 TYPE_max
327 } OperandType;
328 #undef ENUM_ENTRY
330 /*
331 * OperandSpecifier - The specification for how to extract and interpret one
332 * operand.
333 */
334 struct OperandSpecifier {
335 OperandEncoding encoding;
336 OperandType type;
337 };
339 /*
340 * Indicates where the opcode modifier (if any) is to be found. Extended
341 * opcodes with AddRegFrm have the opcode modifier in the ModR/M byte.
342 */
344 #define MODIFIER_TYPES \
345 ENUM_ENTRY(MODIFIER_NONE) \
346 ENUM_ENTRY(MODIFIER_OPCODE) \
347 ENUM_ENTRY(MODIFIER_MODRM)
349 #define ENUM_ENTRY(n) n,
350 typedef enum {
351 MODIFIER_TYPES
352 MODIFIER_max
353 } ModifierType;
354 #undef ENUM_ENTRY
356 #define X86_MAX_OPERANDS 5
358 /*
359 * The specification for how to extract and interpret a full instruction and
360 * its operands.
361 */
362 struct InstructionSpecifier {
363 ModifierType modifierType;
364 uint8_t modifierBase;
365 struct OperandSpecifier operands[X86_MAX_OPERANDS];
367 /* The macro below must be defined wherever this file is included. */
368 INSTRUCTION_SPECIFIER_FIELDS
369 };
371 /*
372 * Decoding mode for the Intel disassembler. 16-bit, 32-bit, and 64-bit mode
373 * are supported, and represent real mode, IA-32e, and IA-32e in 64-bit mode,
374 * respectively.
375 */
376 typedef enum {
377 MODE_16BIT,
378 MODE_32BIT,
379 MODE_64BIT
380 } DisassemblerMode;
382 #endif