]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Target/X86/Disassembler/X86DisassemblerDecoderCommon.h
Remove A6/A7 opcode maps. They can all be handled with a TB map, opcode of 0xa6/0xa7...
[opencl/llvm.git] / lib / Target / X86 / Disassembler / X86DisassemblerDecoderCommon.h
1 /*===-- X86DisassemblerDecoderCommon.h - Disassembler decoder -----*- C -*-===*
2  *
3  *                     The LLVM Compiler Infrastructure
4  *
5  * This file is distributed under the University of Illinois Open Source
6  * License. See LICENSE.TXT for details.
7  *
8  *===----------------------------------------------------------------------===*
9  *
10  * This file is part of the X86 Disassembler.
11  * It contains common definitions used by both the disassembler and the table
12  *  generator.
13  * Documentation for the disassembler can be found in X86Disassembler.h.
14  *
15  *===----------------------------------------------------------------------===*/
17 /*
18  * This header file provides those definitions that need to be shared between
19  * the decoder and the table generator in a C-friendly manner.
20  */
22 #ifndef X86DISASSEMBLERDECODERCOMMON_H
23 #define X86DISASSEMBLERDECODERCOMMON_H
25 #include "llvm/Support/DataTypes.h"
27 #define INSTRUCTIONS_SYM  x86DisassemblerInstrSpecifiers
28 #define CONTEXTS_SYM      x86DisassemblerContexts
29 #define ONEBYTE_SYM       x86DisassemblerOneByteOpcodes
30 #define TWOBYTE_SYM       x86DisassemblerTwoByteOpcodes
31 #define THREEBYTE38_SYM   x86DisassemblerThreeByte38Opcodes
32 #define THREEBYTE3A_SYM   x86DisassemblerThreeByte3AOpcodes
33 #define XOP8_MAP_SYM      x86DisassemblerXOP8Opcodes
34 #define XOP9_MAP_SYM      x86DisassemblerXOP9Opcodes
35 #define XOPA_MAP_SYM      x86DisassemblerXOPAOpcodes
37 #define INSTRUCTIONS_STR  "x86DisassemblerInstrSpecifiers"
38 #define CONTEXTS_STR      "x86DisassemblerContexts"
39 #define ONEBYTE_STR       "x86DisassemblerOneByteOpcodes"
40 #define TWOBYTE_STR       "x86DisassemblerTwoByteOpcodes"
41 #define THREEBYTE38_STR   "x86DisassemblerThreeByte38Opcodes"
42 #define THREEBYTE3A_STR   "x86DisassemblerThreeByte3AOpcodes"
43 #define XOP8_MAP_STR      "x86DisassemblerXOP8Opcodes"
44 #define XOP9_MAP_STR      "x86DisassemblerXOP9Opcodes"
45 #define XOPA_MAP_STR      "x86DisassemblerXOPAOpcodes"
47 /*
48  * Attributes of an instruction that must be known before the opcode can be
49  * processed correctly.  Most of these indicate the presence of particular
50  * prefixes, but ATTR_64BIT is simply an attribute of the decoding context.
51  */
52 #define ATTRIBUTE_BITS                  \
53   ENUM_ENTRY(ATTR_NONE,   0x00)         \
54   ENUM_ENTRY(ATTR_64BIT,  (0x1 << 0))   \
55   ENUM_ENTRY(ATTR_XS,     (0x1 << 1))   \
56   ENUM_ENTRY(ATTR_XD,     (0x1 << 2))   \
57   ENUM_ENTRY(ATTR_REXW,   (0x1 << 3))   \
58   ENUM_ENTRY(ATTR_OPSIZE, (0x1 << 4))   \
59   ENUM_ENTRY(ATTR_ADSIZE, (0x1 << 5))   \
60   ENUM_ENTRY(ATTR_VEX,    (0x1 << 6))   \
61   ENUM_ENTRY(ATTR_VEXL,   (0x1 << 7))   \
62   ENUM_ENTRY(ATTR_EVEX,   (0x1 << 8))   \
63   ENUM_ENTRY(ATTR_EVEXL,  (0x1 << 9))   \
64   ENUM_ENTRY(ATTR_EVEXL2, (0x1 << 10))  \
65   ENUM_ENTRY(ATTR_EVEXK,  (0x1 << 11))  \
66   ENUM_ENTRY(ATTR_EVEXKZ, (0x1 << 12))  \
67   ENUM_ENTRY(ATTR_EVEXB,  (0x1 << 13))
69 #define ENUM_ENTRY(n, v) n = v,
70 enum attributeBits {
71   ATTRIBUTE_BITS
72   ATTR_max
73 };
74 #undef ENUM_ENTRY
76 /*
77  * Combinations of the above attributes that are relevant to instruction
78  * decode. Although other combinations are possible, they can be reduced to
79  * these without affecting the ultimately decoded instruction.
80  */
82 /*           Class name           Rank  Rationale for rank assignment         */
83 #define INSTRUCTION_CONTEXTS                                                   \
84   ENUM_ENTRY(IC,                    0,  "says nothing about the instruction")  \
85   ENUM_ENTRY(IC_64BIT,              1,  "says the instruction applies in "     \
86                                         "64-bit mode but no more")             \
87   ENUM_ENTRY(IC_OPSIZE,             3,  "requires an OPSIZE prefix, so "       \
88                                         "operands change width")               \
89   ENUM_ENTRY(IC_ADSIZE,             3,  "requires an ADSIZE prefix, so "       \
90                                         "operands change width")               \
91   ENUM_ENTRY(IC_XD,                 2,  "may say something about the opcode "  \
92                                         "but not the operands")                \
93   ENUM_ENTRY(IC_XS,                 2,  "may say something about the opcode "  \
94                                         "but not the operands")                \
95   ENUM_ENTRY(IC_XD_OPSIZE,          3,  "requires an OPSIZE prefix, so "       \
96                                         "operands change width")               \
97   ENUM_ENTRY(IC_XS_OPSIZE,          3,  "requires an OPSIZE prefix, so "       \
98                                         "operands change width")               \
99   ENUM_ENTRY(IC_64BIT_REXW,         4,  "requires a REX.W prefix, so operands "\
100                                         "change width; overrides IC_OPSIZE")   \
101   ENUM_ENTRY(IC_64BIT_OPSIZE,       3,  "Just as meaningful as IC_OPSIZE")     \
102   ENUM_ENTRY(IC_64BIT_ADSIZE,       3,  "Just as meaningful as IC_ADSIZE")     \
103   ENUM_ENTRY(IC_64BIT_XD,           5,  "XD instructions are SSE; REX.W is "   \
104                                         "secondary")                           \
105   ENUM_ENTRY(IC_64BIT_XS,           5,  "Just as meaningful as IC_64BIT_XD")   \
106   ENUM_ENTRY(IC_64BIT_XD_OPSIZE,    3,  "Just as meaningful as IC_XD_OPSIZE")  \
107   ENUM_ENTRY(IC_64BIT_XS_OPSIZE,    3,  "Just as meaningful as IC_XS_OPSIZE")  \
108   ENUM_ENTRY(IC_64BIT_REXW_XS,      6,  "OPSIZE could mean a different "       \
109                                         "opcode")                              \
110   ENUM_ENTRY(IC_64BIT_REXW_XD,      6,  "Just as meaningful as "               \
111                                         "IC_64BIT_REXW_XS")                    \
112   ENUM_ENTRY(IC_64BIT_REXW_OPSIZE,  7,  "The Dynamic Duo!  Prefer over all "   \
113                                         "else because this changes most "      \
114                                         "operands' meaning")                   \
115   ENUM_ENTRY(IC_VEX,                1,  "requires a VEX prefix")               \
116   ENUM_ENTRY(IC_VEX_XS,             2,  "requires VEX and the XS prefix")      \
117   ENUM_ENTRY(IC_VEX_XD,             2,  "requires VEX and the XD prefix")      \
118   ENUM_ENTRY(IC_VEX_OPSIZE,         2,  "requires VEX and the OpSize prefix")  \
119   ENUM_ENTRY(IC_VEX_W,              3,  "requires VEX and the W prefix")       \
120   ENUM_ENTRY(IC_VEX_W_XS,           4,  "requires VEX, W, and XS prefix")      \
121   ENUM_ENTRY(IC_VEX_W_XD,           4,  "requires VEX, W, and XD prefix")      \
122   ENUM_ENTRY(IC_VEX_W_OPSIZE,       4,  "requires VEX, W, and OpSize")         \
123   ENUM_ENTRY(IC_VEX_L,              3,  "requires VEX and the L prefix")       \
124   ENUM_ENTRY(IC_VEX_L_XS,           4,  "requires VEX and the L and XS prefix")\
125   ENUM_ENTRY(IC_VEX_L_XD,           4,  "requires VEX and the L and XD prefix")\
126   ENUM_ENTRY(IC_VEX_L_OPSIZE,       4,  "requires VEX, L, and OpSize")         \
127   ENUM_ENTRY(IC_VEX_L_W,            4,  "requires VEX, L and W")               \
128   ENUM_ENTRY(IC_VEX_L_W_XS,         5,  "requires VEX, L, W and XS prefix")    \
129   ENUM_ENTRY(IC_VEX_L_W_XD,         5,  "requires VEX, L, W and XD prefix")    \
130   ENUM_ENTRY(IC_VEX_L_W_OPSIZE,     5,  "requires VEX, L, W and OpSize")       \
131   ENUM_ENTRY(IC_EVEX,               1,  "requires an EVEX prefix")             \
132   ENUM_ENTRY(IC_EVEX_XS,            2,  "requires EVEX and the XS prefix")     \
133   ENUM_ENTRY(IC_EVEX_XD,            2,  "requires EVEX and the XD prefix")     \
134   ENUM_ENTRY(IC_EVEX_OPSIZE,        2,  "requires EVEX and the OpSize prefix") \
135   ENUM_ENTRY(IC_EVEX_W,             3,  "requires EVEX and the W prefix")      \
136   ENUM_ENTRY(IC_EVEX_W_XS,          4,  "requires EVEX, W, and XS prefix")     \
137   ENUM_ENTRY(IC_EVEX_W_XD,          4,  "requires EVEX, W, and XD prefix")     \
138   ENUM_ENTRY(IC_EVEX_W_OPSIZE,      4,  "requires EVEX, W, and OpSize")        \
139   ENUM_ENTRY(IC_EVEX_L,             3,  "requires EVEX and the L prefix")       \
140   ENUM_ENTRY(IC_EVEX_L_XS,          4,  "requires EVEX and the L and XS prefix")\
141   ENUM_ENTRY(IC_EVEX_L_XD,          4,  "requires EVEX and the L and XD prefix")\
142   ENUM_ENTRY(IC_EVEX_L_OPSIZE,      4,  "requires EVEX, L, and OpSize")         \
143   ENUM_ENTRY(IC_EVEX_L_W,           3,  "requires EVEX, L and W")               \
144   ENUM_ENTRY(IC_EVEX_L_W_XS,        4,  "requires EVEX, L, W and XS prefix")    \
145   ENUM_ENTRY(IC_EVEX_L_W_XD,        4,  "requires EVEX, L, W and XD prefix")    \
146   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE,    4,  "requires EVEX, L, W and OpSize")       \
147   ENUM_ENTRY(IC_EVEX_L2,            3,  "requires EVEX and the L2 prefix")       \
148   ENUM_ENTRY(IC_EVEX_L2_XS,         4,  "requires EVEX and the L2 and XS prefix")\
149   ENUM_ENTRY(IC_EVEX_L2_XD,         4,  "requires EVEX and the L2 and XD prefix")\
150   ENUM_ENTRY(IC_EVEX_L2_OPSIZE,     4,  "requires EVEX, L2, and OpSize")         \
151   ENUM_ENTRY(IC_EVEX_L2_W,          3,  "requires EVEX, L2 and W")               \
152   ENUM_ENTRY(IC_EVEX_L2_W_XS,       4,  "requires EVEX, L2, W and XS prefix")    \
153   ENUM_ENTRY(IC_EVEX_L2_W_XD,       4,  "requires EVEX, L2, W and XD prefix")    \
154   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE,   4,  "requires EVEX, L2, W and OpSize")       \
155   ENUM_ENTRY(IC_EVEX_K,             1,  "requires an EVEX_K prefix")             \
156   ENUM_ENTRY(IC_EVEX_XS_K,          2,  "requires EVEX_K and the XS prefix")     \
157   ENUM_ENTRY(IC_EVEX_XD_K,          2,  "requires EVEX_K and the XD prefix")     \
158   ENUM_ENTRY(IC_EVEX_OPSIZE_K,      2,  "requires EVEX_K and the OpSize prefix") \
159   ENUM_ENTRY(IC_EVEX_W_K,           3,  "requires EVEX_K and the W prefix")      \
160   ENUM_ENTRY(IC_EVEX_W_XS_K,        4,  "requires EVEX_K, W, and XS prefix")     \
161   ENUM_ENTRY(IC_EVEX_W_XD_K,        4,  "requires EVEX_K, W, and XD prefix")     \
162   ENUM_ENTRY(IC_EVEX_W_OPSIZE_K,    4,  "requires EVEX_K, W, and OpSize")        \
163   ENUM_ENTRY(IC_EVEX_L_K,           3,  "requires EVEX_K and the L prefix")       \
164   ENUM_ENTRY(IC_EVEX_L_XS_K,        4,  "requires EVEX_K and the L and XS prefix")\
165   ENUM_ENTRY(IC_EVEX_L_XD_K,        4,  "requires EVEX_K and the L and XD prefix")\
166   ENUM_ENTRY(IC_EVEX_L_OPSIZE_K,    4,  "requires EVEX_K, L, and OpSize")         \
167   ENUM_ENTRY(IC_EVEX_L_W_K,         3,  "requires EVEX_K, L and W")               \
168   ENUM_ENTRY(IC_EVEX_L_W_XS_K,      4,  "requires EVEX_K, L, W and XS prefix")    \
169   ENUM_ENTRY(IC_EVEX_L_W_XD_K,      4,  "requires EVEX_K, L, W and XD prefix")    \
170   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_K,  4,  "requires EVEX_K, L, W and OpSize")       \
171   ENUM_ENTRY(IC_EVEX_L2_K,          3,  "requires EVEX_K and the L2 prefix")       \
172   ENUM_ENTRY(IC_EVEX_L2_XS_K,       4,  "requires EVEX_K and the L2 and XS prefix")\
173   ENUM_ENTRY(IC_EVEX_L2_XD_K,       4,  "requires EVEX_K and the L2 and XD prefix")\
174   ENUM_ENTRY(IC_EVEX_L2_OPSIZE_K,   4,  "requires EVEX_K, L2, and OpSize")         \
175   ENUM_ENTRY(IC_EVEX_L2_W_K,        3,  "requires EVEX_K, L2 and W")               \
176   ENUM_ENTRY(IC_EVEX_L2_W_XS_K,     4,  "requires EVEX_K, L2, W and XS prefix")    \
177   ENUM_ENTRY(IC_EVEX_L2_W_XD_K,     4,  "requires EVEX_K, L2, W and XD prefix")    \
178   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_K, 4,  "requires EVEX_K, L2, W and OpSize")     \
179   ENUM_ENTRY(IC_EVEX_B,             1,  "requires an EVEX_B prefix")             \
180   ENUM_ENTRY(IC_EVEX_XS_B,          2,  "requires EVEX_B and the XS prefix")     \
181   ENUM_ENTRY(IC_EVEX_XD_B,          2,  "requires EVEX_B and the XD prefix")     \
182   ENUM_ENTRY(IC_EVEX_OPSIZE_B,      2,  "requires EVEX_B and the OpSize prefix") \
183   ENUM_ENTRY(IC_EVEX_W_B,           3,  "requires EVEX_B and the W prefix")      \
184   ENUM_ENTRY(IC_EVEX_W_XS_B,        4,  "requires EVEX_B, W, and XS prefix")     \
185   ENUM_ENTRY(IC_EVEX_W_XD_B,        4,  "requires EVEX_B, W, and XD prefix")     \
186   ENUM_ENTRY(IC_EVEX_W_OPSIZE_B,    4,  "requires EVEX_B, W, and OpSize")        \
187   ENUM_ENTRY(IC_EVEX_L_B,           3,  "requires EVEX_B and the L prefix")       \
188   ENUM_ENTRY(IC_EVEX_L_XS_B,        4,  "requires EVEX_B and the L and XS prefix")\
189   ENUM_ENTRY(IC_EVEX_L_XD_B,        4,  "requires EVEX_B and the L and XD prefix")\
190   ENUM_ENTRY(IC_EVEX_L_OPSIZE_B,    4,  "requires EVEX_B, L, and OpSize")         \
191   ENUM_ENTRY(IC_EVEX_L_W_B,         3,  "requires EVEX_B, L and W")               \
192   ENUM_ENTRY(IC_EVEX_L_W_XS_B,      4,  "requires EVEX_B, L, W and XS prefix")    \
193   ENUM_ENTRY(IC_EVEX_L_W_XD_B,      4,  "requires EVEX_B, L, W and XD prefix")    \
194   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_B,  4,  "requires EVEX_B, L, W and OpSize")       \
195   ENUM_ENTRY(IC_EVEX_L2_B,          3,  "requires EVEX_B and the L2 prefix")       \
196   ENUM_ENTRY(IC_EVEX_L2_XS_B,       4,  "requires EVEX_B and the L2 and XS prefix")\
197   ENUM_ENTRY(IC_EVEX_L2_XD_B,       4,  "requires EVEX_B and the L2 and XD prefix")\
198   ENUM_ENTRY(IC_EVEX_L2_OPSIZE_B,   4,  "requires EVEX_B, L2, and OpSize")         \
199   ENUM_ENTRY(IC_EVEX_L2_W_B,        3,  "requires EVEX_B, L2 and W")               \
200   ENUM_ENTRY(IC_EVEX_L2_W_XS_B,     4,  "requires EVEX_B, L2, W and XS prefix")    \
201   ENUM_ENTRY(IC_EVEX_L2_W_XD_B,     4,  "requires EVEX_B, L2, W and XD prefix")    \
202   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_B, 4,  "requires EVEX_B, L2, W and OpSize")       \
203   ENUM_ENTRY(IC_EVEX_K_B,           1,  "requires EVEX_B and EVEX_K prefix")             \
204   ENUM_ENTRY(IC_EVEX_XS_K_B,        2,  "requires EVEX_B, EVEX_K and the XS prefix")     \
205   ENUM_ENTRY(IC_EVEX_XD_K_B,        2,  "requires EVEX_B, EVEX_K and the XD prefix")     \
206   ENUM_ENTRY(IC_EVEX_OPSIZE_K_B,    2,  "requires EVEX_B, EVEX_K and the OpSize prefix") \
207   ENUM_ENTRY(IC_EVEX_W_K_B,         3,  "requires EVEX_B, EVEX_K and the W prefix")      \
208   ENUM_ENTRY(IC_EVEX_W_XS_K_B,      4,  "requires EVEX_B, EVEX_K, W, and XS prefix")     \
209   ENUM_ENTRY(IC_EVEX_W_XD_K_B,      4,  "requires EVEX_B, EVEX_K, W, and XD prefix")     \
210   ENUM_ENTRY(IC_EVEX_W_OPSIZE_K_B,  4,  "requires EVEX_B, EVEX_K, W, and OpSize")        \
211   ENUM_ENTRY(IC_EVEX_L_K_B,         3,  "requires EVEX_B, EVEX_K and the L prefix")       \
212   ENUM_ENTRY(IC_EVEX_L_XS_K_B,      4,  "requires EVEX_B, EVEX_K and the L and XS prefix")\
213   ENUM_ENTRY(IC_EVEX_L_XD_K_B,      4,  "requires EVEX_B, EVEX_K and the L and XD prefix")\
214   ENUM_ENTRY(IC_EVEX_L_OPSIZE_K_B,  4,  "requires EVEX_B, EVEX_K, L, and OpSize")         \
215   ENUM_ENTRY(IC_EVEX_L_W_K_B,       3,  "requires EVEX_B, EVEX_K, L and W")               \
216   ENUM_ENTRY(IC_EVEX_L_W_XS_K_B,    4,  "requires EVEX_B, EVEX_K, L, W and XS prefix")    \
217   ENUM_ENTRY(IC_EVEX_L_W_XD_K_B,    4,  "requires EVEX_B, EVEX_K, L, W and XD prefix")    \
218   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_K_B,4,  "requires EVEX_B, EVEX_K, L, W and OpSize")       \
219   ENUM_ENTRY(IC_EVEX_L2_K_B,        3,  "requires EVEX_B, EVEX_K and the L2 prefix")       \
220   ENUM_ENTRY(IC_EVEX_L2_XS_K_B,     4,  "requires EVEX_B, EVEX_K and the L2 and XS prefix")\
221   ENUM_ENTRY(IC_EVEX_L2_XD_K_B,     4,  "requires EVEX_B, EVEX_K and the L2 and XD prefix")\
222   ENUM_ENTRY(IC_EVEX_L2_OPSIZE_K_B, 4,  "requires EVEX_B, EVEX_K, L2, and OpSize")         \
223   ENUM_ENTRY(IC_EVEX_L2_W_K_B,      3,  "requires EVEX_B, EVEX_K, L2 and W")               \
224   ENUM_ENTRY(IC_EVEX_L2_W_XS_K_B,   4,  "requires EVEX_B, EVEX_K, L2, W and XS prefix")    \
225   ENUM_ENTRY(IC_EVEX_L2_W_XD_K_B,   4,  "requires EVEX_B, EVEX_K, L2, W and XD prefix")    \
226   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_K_B,4,  "requires EVEX_B, EVEX_K, L2, W and OpSize")       \
227   ENUM_ENTRY(IC_EVEX_KZ_B,           1,  "requires EVEX_B and EVEX_KZ prefix")             \
228   ENUM_ENTRY(IC_EVEX_XS_KZ_B,        2,  "requires EVEX_B, EVEX_KZ and the XS prefix")     \
229   ENUM_ENTRY(IC_EVEX_XD_KZ_B,        2,  "requires EVEX_B, EVEX_KZ and the XD prefix")     \
230   ENUM_ENTRY(IC_EVEX_OPSIZE_KZ_B,    2,  "requires EVEX_B, EVEX_KZ and the OpSize prefix") \
231   ENUM_ENTRY(IC_EVEX_W_KZ_B,         3,  "requires EVEX_B, EVEX_KZ and the W prefix")      \
232   ENUM_ENTRY(IC_EVEX_W_XS_KZ_B,      4,  "requires EVEX_B, EVEX_KZ, W, and XS prefix")     \
233   ENUM_ENTRY(IC_EVEX_W_XD_KZ_B,      4,  "requires EVEX_B, EVEX_KZ, W, and XD prefix")     \
234   ENUM_ENTRY(IC_EVEX_W_OPSIZE_KZ_B,  4,  "requires EVEX_B, EVEX_KZ, W, and OpSize")        \
235   ENUM_ENTRY(IC_EVEX_L_KZ_B,           3,  "requires EVEX_B, EVEX_KZ and the L prefix")       \
236   ENUM_ENTRY(IC_EVEX_L_XS_KZ_B,        4,  "requires EVEX_B, EVEX_KZ and the L and XS prefix")\
237   ENUM_ENTRY(IC_EVEX_L_XD_KZ_B,        4,  "requires EVEX_B, EVEX_KZ and the L and XD prefix")\
238   ENUM_ENTRY(IC_EVEX_L_OPSIZE_KZ_B,    4,  "requires EVEX_B, EVEX_KZ, L, and OpSize")         \
239   ENUM_ENTRY(IC_EVEX_L_W_KZ_B,         3,  "requires EVEX_B, EVEX_KZ, L and W")               \
240   ENUM_ENTRY(IC_EVEX_L_W_XS_KZ_B,      4,  "requires EVEX_B, EVEX_KZ, L, W and XS prefix")    \
241   ENUM_ENTRY(IC_EVEX_L_W_XD_KZ_B,      4,  "requires EVEX_B, EVEX_KZ, L, W and XD prefix")    \
242   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_KZ_B,  4,  "requires EVEX_B, EVEX_KZ, L, W and OpSize")       \
243   ENUM_ENTRY(IC_EVEX_L2_KZ_B,          3,  "requires EVEX_B, EVEX_KZ and the L2 prefix")       \
244   ENUM_ENTRY(IC_EVEX_L2_XS_KZ_B,       4,  "requires EVEX_B, EVEX_KZ and the L2 and XS prefix")\
245   ENUM_ENTRY(IC_EVEX_L2_XD_KZ_B,       4,  "requires EVEX_B, EVEX_KZ and the L2 and XD prefix")\
246   ENUM_ENTRY(IC_EVEX_L2_OPSIZE_KZ_B,   4,  "requires EVEX_B, EVEX_KZ, L2, and OpSize")         \
247   ENUM_ENTRY(IC_EVEX_L2_W_KZ_B,        3,  "requires EVEX_B, EVEX_KZ, L2 and W")               \
248   ENUM_ENTRY(IC_EVEX_L2_W_XS_KZ_B,     4,  "requires EVEX_B, EVEX_KZ, L2, W and XS prefix")    \
249   ENUM_ENTRY(IC_EVEX_L2_W_XD_KZ_B,     4,  "requires EVEX_B, EVEX_KZ, L2, W and XD prefix")    \
250   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_KZ_B, 4,  "requires EVEX_B, EVEX_KZ, L2, W and OpSize")       \
251   ENUM_ENTRY(IC_EVEX_KZ,             1,  "requires an EVEX_KZ prefix")             \
252   ENUM_ENTRY(IC_EVEX_XS_KZ,          2,  "requires EVEX_KZ and the XS prefix")     \
253   ENUM_ENTRY(IC_EVEX_XD_KZ,          2,  "requires EVEX_KZ and the XD prefix")     \
254   ENUM_ENTRY(IC_EVEX_OPSIZE_KZ,      2,  "requires EVEX_KZ and the OpSize prefix") \
255   ENUM_ENTRY(IC_EVEX_W_KZ,           3,  "requires EVEX_KZ and the W prefix")      \
256   ENUM_ENTRY(IC_EVEX_W_XS_KZ,        4,  "requires EVEX_KZ, W, and XS prefix")     \
257   ENUM_ENTRY(IC_EVEX_W_XD_KZ,        4,  "requires EVEX_KZ, W, and XD prefix")     \
258   ENUM_ENTRY(IC_EVEX_W_OPSIZE_KZ,    4,  "requires EVEX_KZ, W, and OpSize")        \
259   ENUM_ENTRY(IC_EVEX_L_KZ,           3,  "requires EVEX_KZ and the L prefix")       \
260   ENUM_ENTRY(IC_EVEX_L_XS_KZ,        4,  "requires EVEX_KZ and the L and XS prefix")\
261   ENUM_ENTRY(IC_EVEX_L_XD_KZ,        4,  "requires EVEX_KZ and the L and XD prefix")\
262   ENUM_ENTRY(IC_EVEX_L_OPSIZE_KZ,    4,  "requires EVEX_KZ, L, and OpSize")         \
263   ENUM_ENTRY(IC_EVEX_L_W_KZ,         3,  "requires EVEX_KZ, L and W")               \
264   ENUM_ENTRY(IC_EVEX_L_W_XS_KZ,      4,  "requires EVEX_KZ, L, W and XS prefix")    \
265   ENUM_ENTRY(IC_EVEX_L_W_XD_KZ,      4,  "requires EVEX_KZ, L, W and XD prefix")    \
266   ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_KZ,  4,  "requires EVEX_KZ, L, W and OpSize")       \
267   ENUM_ENTRY(IC_EVEX_L2_KZ,          3,  "requires EVEX_KZ and the L2 prefix")       \
268   ENUM_ENTRY(IC_EVEX_L2_XS_KZ,       4,  "requires EVEX_KZ and the L2 and XS prefix")\
269   ENUM_ENTRY(IC_EVEX_L2_XD_KZ,       4,  "requires EVEX_KZ and the L2 and XD prefix")\
270   ENUM_ENTRY(IC_EVEX_L2_OPSIZE_KZ,   4,  "requires EVEX_KZ, L2, and OpSize")         \
271   ENUM_ENTRY(IC_EVEX_L2_W_KZ,        3,  "requires EVEX_KZ, L2 and W")               \
272   ENUM_ENTRY(IC_EVEX_L2_W_XS_KZ,     4,  "requires EVEX_KZ, L2, W and XS prefix")    \
273   ENUM_ENTRY(IC_EVEX_L2_W_XD_KZ,     4,  "requires EVEX_KZ, L2, W and XD prefix")    \
274   ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_KZ, 4,  "requires EVEX_KZ, L2, W and OpSize")     
276 #define ENUM_ENTRY(n, r, d) n,
277 typedef enum {
278   INSTRUCTION_CONTEXTS
279   IC_max
280 } InstructionContext;
281 #undef ENUM_ENTRY
283 /*
284  * Opcode types, which determine which decode table to use, both in the Intel
285  * manual and also for the decoder.
286  */
287 typedef enum {
288   ONEBYTE       = 0,
289   TWOBYTE       = 1,
290   THREEBYTE_38  = 2,
291   THREEBYTE_3A  = 3,
292   XOP8_MAP      = 4,
293   XOP9_MAP      = 5,
294   XOPA_MAP      = 6
295 } OpcodeType;
297 /*
298  * The following structs are used for the hierarchical decode table.  After
299  * determining the instruction's class (i.e., which IC_* constant applies to
300  * it), the decoder reads the opcode.  Some instructions require specific
301  * values of the ModR/M byte, so the ModR/M byte indexes into the final table.
302  *
303  * If a ModR/M byte is not required, "required" is left unset, and the values
304  * for each instructionID are identical.
305  */
307 typedef uint16_t InstrUID;
309 /*
310  * ModRMDecisionType - describes the type of ModR/M decision, allowing the
311  * consumer to determine the number of entries in it.
312  *
313  * MODRM_ONEENTRY - No matter what the value of the ModR/M byte is, the decoded
314  *                  instruction is the same.
315  * MODRM_SPLITRM  - If the ModR/M byte is between 0x00 and 0xbf, the opcode
316  *                  corresponds to one instruction; otherwise, it corresponds to
317  *                  a different instruction.
318  * MODRM_SPLITMISC- If the ModR/M byte is between 0x00 and 0xbf, ModR/M byte
319  *                  divided by 8 is used to select instruction; otherwise, each
320  *                  value of the ModR/M byte could correspond to a different
321  *                  instruction.
322  * MODRM_SPLITREG - ModR/M byte divided by 8 is used to select instruction. This
323                     corresponds to instructions that use reg field as opcode
324  * MODRM_FULL     - Potentially, each value of the ModR/M byte could correspond
325  *                  to a different instruction.
326  */
328 #define MODRMTYPES            \
329   ENUM_ENTRY(MODRM_ONEENTRY)  \
330   ENUM_ENTRY(MODRM_SPLITRM)   \
331   ENUM_ENTRY(MODRM_SPLITMISC)  \
332   ENUM_ENTRY(MODRM_SPLITREG)  \
333   ENUM_ENTRY(MODRM_FULL)
335 #define ENUM_ENTRY(n) n,
336 typedef enum {
337   MODRMTYPES
338   MODRM_max
339 } ModRMDecisionType;
340 #undef ENUM_ENTRY
342 /*
343  * ModRMDecision - Specifies whether a ModR/M byte is needed and (if so) which
344  *  instruction each possible value of the ModR/M byte corresponds to.  Once
345  *  this information is known, we have narrowed down to a single instruction.
346  */
347 struct ModRMDecision {
348   uint8_t     modrm_type;
350   /* The macro below must be defined wherever this file is included. */
351   INSTRUCTION_IDS
352 };
354 /*
355  * OpcodeDecision - Specifies which set of ModR/M->instruction tables to look at
356  *   given a particular opcode.
357  */
358 struct OpcodeDecision {
359   struct ModRMDecision modRMDecisions[256];
360 };
362 /*
363  * ContextDecision - Specifies which opcode->instruction tables to look at given
364  *   a particular context (set of attributes).  Since there are many possible
365  *   contexts, the decoder first uses CONTEXTS_SYM to determine which context
366  *   applies given a specific set of attributes.  Hence there are only IC_max
367  *   entries in this table, rather than 2^(ATTR_max).
368  */
369 struct ContextDecision {
370   struct OpcodeDecision opcodeDecisions[IC_max];
371 };
373 /*
374  * Physical encodings of instruction operands.
375  */
377 #define ENCODINGS                                                              \
378   ENUM_ENTRY(ENCODING_NONE,   "")                                              \
379   ENUM_ENTRY(ENCODING_REG,    "Register operand in ModR/M byte.")              \
380   ENUM_ENTRY(ENCODING_RM,     "R/M operand in ModR/M byte.")                   \
381   ENUM_ENTRY(ENCODING_VVVV,   "Register operand in VEX.vvvv byte.")            \
382   ENUM_ENTRY(ENCODING_WRITEMASK, "Register operand in EVEX.aaa byte.")         \
383   ENUM_ENTRY(ENCODING_CB,     "1-byte code offset (possible new CS value)")    \
384   ENUM_ENTRY(ENCODING_CW,     "2-byte")                                        \
385   ENUM_ENTRY(ENCODING_CD,     "4-byte")                                        \
386   ENUM_ENTRY(ENCODING_CP,     "6-byte")                                        \
387   ENUM_ENTRY(ENCODING_CO,     "8-byte")                                        \
388   ENUM_ENTRY(ENCODING_CT,     "10-byte")                                       \
389   ENUM_ENTRY(ENCODING_IB,     "1-byte immediate")                              \
390   ENUM_ENTRY(ENCODING_IW,     "2-byte")                                        \
391   ENUM_ENTRY(ENCODING_ID,     "4-byte")                                        \
392   ENUM_ENTRY(ENCODING_IO,     "8-byte")                                        \
393   ENUM_ENTRY(ENCODING_RB,     "(AL..DIL, R8L..R15L) Register code added to "   \
394                               "the opcode byte")                               \
395   ENUM_ENTRY(ENCODING_RW,     "(AX..DI, R8W..R15W)")                           \
396   ENUM_ENTRY(ENCODING_RD,     "(EAX..EDI, R8D..R15D)")                         \
397   ENUM_ENTRY(ENCODING_RO,     "(RAX..RDI, R8..R15)")                           \
398   ENUM_ENTRY(ENCODING_FP,     "Position on floating-point stack in ModR/M "    \
399                               "byte.")                                         \
400                                                                                \
401   ENUM_ENTRY(ENCODING_Iv,     "Immediate of operand size")                     \
402   ENUM_ENTRY(ENCODING_Ia,     "Immediate of address size")                     \
403   ENUM_ENTRY(ENCODING_Rv,     "Register code of operand size added to the "    \
404                               "opcode byte")                                   \
405   ENUM_ENTRY(ENCODING_DUP,    "Duplicate of another operand; ID is encoded "   \
406                               "in type")                                       \
407   ENUM_ENTRY(ENCODING_SI,     "Source index; encoded in OpSize/Adsize prefix") \
408   ENUM_ENTRY(ENCODING_DI,     "Destination index; encoded in prefixes")
410 #define ENUM_ENTRY(n, d) n,
411   typedef enum {
412     ENCODINGS
413     ENCODING_max
414   } OperandEncoding;
415 #undef ENUM_ENTRY
417 /*
418  * Semantic interpretations of instruction operands.
419  */
421 #define TYPES                                                                  \
422   ENUM_ENTRY(TYPE_NONE,       "")                                              \
423   ENUM_ENTRY(TYPE_REL8,       "1-byte immediate address")                      \
424   ENUM_ENTRY(TYPE_REL16,      "2-byte")                                        \
425   ENUM_ENTRY(TYPE_REL32,      "4-byte")                                        \
426   ENUM_ENTRY(TYPE_REL64,      "8-byte")                                        \
427   ENUM_ENTRY(TYPE_PTR1616,    "2+2-byte segment+offset address")               \
428   ENUM_ENTRY(TYPE_PTR1632,    "2+4-byte")                                      \
429   ENUM_ENTRY(TYPE_PTR1664,    "2+8-byte")                                      \
430   ENUM_ENTRY(TYPE_R8,         "1-byte register operand")                       \
431   ENUM_ENTRY(TYPE_R16,        "2-byte")                                        \
432   ENUM_ENTRY(TYPE_R32,        "4-byte")                                        \
433   ENUM_ENTRY(TYPE_R64,        "8-byte")                                        \
434   ENUM_ENTRY(TYPE_IMM8,       "1-byte immediate operand")                      \
435   ENUM_ENTRY(TYPE_IMM16,      "2-byte")                                        \
436   ENUM_ENTRY(TYPE_IMM32,      "4-byte")                                        \
437   ENUM_ENTRY(TYPE_IMM64,      "8-byte")                                        \
438   ENUM_ENTRY(TYPE_IMM3,       "1-byte immediate operand between 0 and 7")      \
439   ENUM_ENTRY(TYPE_IMM5,       "1-byte immediate operand between 0 and 31")     \
440   ENUM_ENTRY(TYPE_RM8,        "1-byte register or memory operand")             \
441   ENUM_ENTRY(TYPE_RM16,       "2-byte")                                        \
442   ENUM_ENTRY(TYPE_RM32,       "4-byte")                                        \
443   ENUM_ENTRY(TYPE_RM64,       "8-byte")                                        \
444   ENUM_ENTRY(TYPE_M,          "Memory operand")                                \
445   ENUM_ENTRY(TYPE_M8,         "1-byte")                                        \
446   ENUM_ENTRY(TYPE_M16,        "2-byte")                                        \
447   ENUM_ENTRY(TYPE_M32,        "4-byte")                                        \
448   ENUM_ENTRY(TYPE_M64,        "8-byte")                                        \
449   ENUM_ENTRY(TYPE_LEA,        "Effective address")                             \
450   ENUM_ENTRY(TYPE_M128,       "16-byte (SSE/SSE2)")                            \
451   ENUM_ENTRY(TYPE_M256,       "256-byte (AVX)")                                \
452   ENUM_ENTRY(TYPE_M1616,      "2+2-byte segment+offset address")               \
453   ENUM_ENTRY(TYPE_M1632,      "2+4-byte")                                      \
454   ENUM_ENTRY(TYPE_M1664,      "2+8-byte")                                      \
455   ENUM_ENTRY(TYPE_M16_32,     "2+4-byte two-part memory operand (LIDT, LGDT)") \
456   ENUM_ENTRY(TYPE_M16_16,     "2+2-byte (BOUND)")                              \
457   ENUM_ENTRY(TYPE_M32_32,     "4+4-byte (BOUND)")                              \
458   ENUM_ENTRY(TYPE_M16_64,     "2+8-byte (LIDT, LGDT)")                         \
459   ENUM_ENTRY(TYPE_SRCIDX8,    "1-byte memory at source index")                 \
460   ENUM_ENTRY(TYPE_SRCIDX16,   "2-byte memory at source index")                 \
461   ENUM_ENTRY(TYPE_SRCIDX32,   "4-byte memory at source index")                 \
462   ENUM_ENTRY(TYPE_SRCIDX64,   "8-byte memory at source index")                 \
463   ENUM_ENTRY(TYPE_DSTIDX8,    "1-byte memory at destination index")            \
464   ENUM_ENTRY(TYPE_DSTIDX16,   "2-byte memory at destination index")            \
465   ENUM_ENTRY(TYPE_DSTIDX32,   "4-byte memory at destination index")            \
466   ENUM_ENTRY(TYPE_DSTIDX64,   "8-byte memory at destination index")            \
467   ENUM_ENTRY(TYPE_MOFFS8,     "1-byte memory offset (relative to segment "     \
468                               "base)")                                         \
469   ENUM_ENTRY(TYPE_MOFFS16,    "2-byte")                                        \
470   ENUM_ENTRY(TYPE_MOFFS32,    "4-byte")                                        \
471   ENUM_ENTRY(TYPE_MOFFS64,    "8-byte")                                        \
472   ENUM_ENTRY(TYPE_SREG,       "Byte with single bit set: 0 = ES, 1 = CS, "     \
473                               "2 = SS, 3 = DS, 4 = FS, 5 = GS")                \
474   ENUM_ENTRY(TYPE_M32FP,      "32-bit IEE754 memory floating-point operand")   \
475   ENUM_ENTRY(TYPE_M64FP,      "64-bit")                                        \
476   ENUM_ENTRY(TYPE_M80FP,      "80-bit extended")                               \
477   ENUM_ENTRY(TYPE_M16INT,     "2-byte memory integer operand for use in "      \
478                               "floating-point instructions")                   \
479   ENUM_ENTRY(TYPE_M32INT,     "4-byte")                                        \
480   ENUM_ENTRY(TYPE_M64INT,     "8-byte")                                        \
481   ENUM_ENTRY(TYPE_ST,         "Position on the floating-point stack")          \
482   ENUM_ENTRY(TYPE_MM,         "MMX register operand")                          \
483   ENUM_ENTRY(TYPE_MM32,       "4-byte MMX register or memory operand")         \
484   ENUM_ENTRY(TYPE_MM64,       "8-byte")                                        \
485   ENUM_ENTRY(TYPE_XMM,        "XMM register operand")                          \
486   ENUM_ENTRY(TYPE_XMM32,      "4-byte XMM register or memory operand")         \
487   ENUM_ENTRY(TYPE_XMM64,      "8-byte")                                        \
488   ENUM_ENTRY(TYPE_XMM128,     "16-byte")                                       \
489   ENUM_ENTRY(TYPE_XMM256,     "32-byte")                                       \
490   ENUM_ENTRY(TYPE_XMM512,     "64-byte")                                       \
491   ENUM_ENTRY(TYPE_VK1,        "1-bit")                                         \
492   ENUM_ENTRY(TYPE_VK8,        "8-bit")                                         \
493   ENUM_ENTRY(TYPE_VK16,       "16-bit")                                        \
494   ENUM_ENTRY(TYPE_XMM0,       "Implicit use of XMM0")                          \
495   ENUM_ENTRY(TYPE_SEGMENTREG, "Segment register operand")                      \
496   ENUM_ENTRY(TYPE_DEBUGREG,   "Debug register operand")                        \
497   ENUM_ENTRY(TYPE_CONTROLREG, "Control register operand")                      \
498                                                                                \
499   ENUM_ENTRY(TYPE_Mv,         "Memory operand of operand size")                \
500   ENUM_ENTRY(TYPE_Rv,         "Register operand of operand size")              \
501   ENUM_ENTRY(TYPE_IMMv,       "Immediate operand of operand size")             \
502   ENUM_ENTRY(TYPE_RELv,       "Immediate address of operand size")             \
503   ENUM_ENTRY(TYPE_DUP0,       "Duplicate of operand 0")                        \
504   ENUM_ENTRY(TYPE_DUP1,       "operand 1")                                     \
505   ENUM_ENTRY(TYPE_DUP2,       "operand 2")                                     \
506   ENUM_ENTRY(TYPE_DUP3,       "operand 3")                                     \
507   ENUM_ENTRY(TYPE_DUP4,       "operand 4")                                     \
508   ENUM_ENTRY(TYPE_M512,       "512-bit FPU/MMX/XMM/MXCSR state")
510 #define ENUM_ENTRY(n, d) n,
511 typedef enum {
512   TYPES
513   TYPE_max
514 } OperandType;
515 #undef ENUM_ENTRY
517 /*
518  * OperandSpecifier - The specification for how to extract and interpret one
519  *   operand.
520  */
521 struct OperandSpecifier {
522   uint8_t encoding;
523   uint8_t type;
524 };
526 /*
527  * Indicates where the opcode modifier (if any) is to be found.  Extended
528  * opcodes with AddRegFrm have the opcode modifier in the ModR/M byte.
529  */
531 #define MODIFIER_TYPES        \
532   ENUM_ENTRY(MODIFIER_NONE)
534 #define ENUM_ENTRY(n) n,
535 typedef enum {
536   MODIFIER_TYPES
537   MODIFIER_max
538 } ModifierType;
539 #undef ENUM_ENTRY
541 #define X86_MAX_OPERANDS 5
543 /*
544  * The specification for how to extract and interpret a full instruction and
545  * its operands.
546  */
547 struct InstructionSpecifier {
548   /* The macro below must be defined wherever this file is included. */
549   INSTRUCTION_SPECIFIER_FIELDS
550 };
552 /*
553  * Decoding mode for the Intel disassembler.  16-bit, 32-bit, and 64-bit mode
554  * are supported, and represent real mode, IA-32e, and IA-32e in 64-bit mode,
555  * respectively.
556  */
557 typedef enum {
558   MODE_16BIT,
559   MODE_32BIT,
560   MODE_64BIT
561 } DisassemblerMode;
563 #endif